Example MPC5744P XBIC_1 fault injection on DMA transfer GHS614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5744P XBIC_1 fault injection on DMA transfer GHS614

Example MPC5744P XBIC_1 fault injection on DMA transfer GHS614

********************************************************************************

* Detailed Description:

*

*

* This example demonstrate functionality of XBIC_1 error injection

*  capability. The fault is generated on DMA transfer to SRAM.

*  After fault generation it is propagated to FCCU unit as NCF[59].

*

* ------------------------------------------------------------------------------

* Test HW:  MPC57xx

* Maskset:  1N65H

* Target :  internal_FLASH

* Fsys:     200 MHz PLL with 40 MHz crystal reference

*

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎07-16-2015 04:07 AM
Updated by: