******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL1 to maximum allowed freq. PLL1 is system frequency, * PLL0 in initialized to 50MHz * initializes peripherals clock (MOTC_CLK is set to 5MHz) * initializes ETimer to count mode providing delay * initializes interrupts, blinking one LED by ETimer interrupt, * * * * Test HW: X-MPC5744PE257DC, MPC57xx motherboard * MCU: PPC5744PFMMM8 1N65H * Fsys: 200 MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: User LED 1 connected to A0 (P8.0), * * * ------------------------------------------------------------------------------
View full article