* Detailed Description: * This example shows, how to use interrupt hardware vector mode. In the example * PIT3 and PIT2 interrupts are implemented. PIT interrupt toggle LED every second. * * * This example also shows, how to implement IVOR exceptions for core 0. * IVOR1 handler with while(1) loop is ready to use. * * * For correct HW vector mode setup, following files was added to the project: * * - exceptions.s * - handlers_vle.s * - HW_vector.c * * * Following files has been modified (all changes are marked by comment): * * - 56xx_flash.ld * - Vector.c * - MPC57xx__Interrupt_Init.c * * Following file was removed from project (files are still place in project, but * not compiled and linked) * * - intc_sw_handlers.S * - intc_SW_mode_isr_vectors_MPC5744P.c * * * * Test HW: MPC567XADAT516, MPC567XEVBFXMB * MCU: PPC5676RDMVY1 3N23A * Fsys: 180 MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: User LED 1 connected to J241, * User LED 1 connected to J242. *
記事全体を表示