MCUXpresso IDE知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso IDE Knowledge Base

标签

讨论

排序依据:
We are pleased to announce that MCUXpresso IDE v11.3.0 (build 5222) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.2.1.   Installer Downloads To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation    Notification of future releases To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.3.0 - January 2021 Upgraded: Eclipse version to 2020.06 (Eclipse Platform 4.16.0 /  CDT9.11.1). Upgraded: IDE now integrates with OpenJDK8. Upgraded: GNU ARM Embedded Toolchain to GCC9-2020-q2-update. Integrated: GNU test coverage (gcov) and performance analysis (gprof) tools and Eclipse plugins. Upgraded: Version v9 of MCUXpresso Config Tools. Upgraded: Newer SEGGER J-Link software (v6.88c). Upgraded: Newer PEmicro plugin (v4.8.5). Added: i.MX RT1170 B0 support. Added: i.MX RT1024 support. Added: RT500 B2 support. Added: K32W061 support. Added: K32W041AM support. Added: LPC55S06 support. Added: MCU-Link probe debug support. Feature: Added Energy Measurement view, aiming to replace the Power Measurement view. Main capabilities: The new view comes with the same feature-set as the old Power Measurement view; From a GUI perspective, it offers consistent look & feel with other views that display and controls graphs (e.g. Global Variables, SWO-related views); Compatible with existing LPCXpresso boards having on-board power measurement circuits; Power and energy estimation capability: in order to enable power/energy measurement/estimation the user should add a reference voltage in the Config tab section from Energy Measurement view. For convenience and more precise measurement, the user can press "Read from target" which will automatically generate a reference voltage computed as an average value (of the voltage) measured for the last 500msec. Energy and power will be displayed in the status line of the plot area, showing the min/max/average power values and the energy value for the measurements visible in the graph, or over a particular time range selection. Multiprobe and multiview support: the feature is capable to open multiple views, each view can be connected to a different probe (that is capable to measure analog). The probe can be selected from Probe Discovery feature available in the Energy Measurement view toolbar. Data collecting during an out-of-debug session and also during an active debug session; Data collecting with an active debug session while the core is in debug mode. Behavior is controlled via toolbar buttons; Configuration of the server-side (rltool) and of the IDE using the Config tab within the view; Import/Export data functionality for offline analysis: (buttons on the Energy view toolbar). The user is able to save (Export data, in a zip format) the data collected within the view, having the possibility to load the saved data (Import data) later, in the same view or another one. Loading saved data in the Energy Measurement is not requiring physical connection to the target; Extended LPC-Link2 support for all targets having onboard measurement circuit: LPCXpresso546x8/540xx/54S0xx, LPCXpresso54102, LPCXpresso51U68/54114, QN90x0/JN518x/K32W0x1. As a side note, if there is any other LPC-Link2 board having power measurement capability, the user can use an existing configuration (and change the resistor value if necessary); See MCUXpresso_IDE_Energy_Measurement.pdf (or Help -> Help Contents) for details. Feature: Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose (for LinkServer debug connection only). That means, in the case of multicore projects on which primary project refers one or several secondary projects, debug sessions will be automatically started for secondary projects after initiating debug with the primary project. Option is set by default on: Window -> references -> MCUXpresso IDE -> Debug Options -> LinkServer Options -> Miscellaneous -> Enable Auto-debug slave project(s) for multicore projects. If you don't want to have this feature enabled (so if you want to start debug sessions for each core independently), uncheck this option. Similar, Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose for PEmicro too. Option is set by default on: Window -> Preferences -> MCUXpresso IDE -> Debug Options -> PEMicro Options -> Enable Auto-debug slave project(s) for multicore projects. Improvement: Enhance SWO views: SWO Config: added new Tab for data traffic statistics, configuration for ITM Stimulus ports; SWO Profile: added samples and details tabs; SWO Data: added plot (similar to Global Variables); SWO Stats: moved inside SWO Config; ITM Console: added one tab for each stimulus port. Improvement: [RT600] Clean up on RT600 flash drivers: Add drivers for MXIC_OPI connected via FlexSPI_A port; Add drivers for QSPI drivers (SFDP) connected via FlexSPI_B port; Add drivers for QSPI drivers (SFDP) connected via FlexSPI_A port; Remove MIMXRT600_SFDP_* drivers generated by the old project (SDK now references the new drivers). Improvement: Drop-down boxes from several tables require two user operations for reaching the actual items from the list. Reduced now to a single operation (single click). Improvement: Extend CLI functionality - Add new command to list SDK info:   -filter=<string> : filters the available information based on regex expression string. e.g. -filter=K64 will display all data containing K64 string. See SDK command line documentation within the layout (MCUXpresso_SDK_Command_Line_User_Guide.pdf). Improvement: Merge c_include path section into cpp_include path section for cpp project in project settings. Improvement: New project wizard is now capable to handle HW with dual primary/secondary roles (i.e. RT1170). From SDK Wizard page, any core can be selected according with the secondary/primary SDK description, plus it can be selected as standalone (application). Improvement: Community forum accessible now from the main toolbar too (together with the older link from Help->MCUXpresso IDE support forum). The default selection will open the community web inside the IDE. If you want to set the default browser as external browser, use Window->Preferences->General->Web browser->"Use external web browser". Fixed: [RT500] QSPI flash drivers: driver was incorrectly using QSPI DDR instead of SDR. Fixed: [RT500][RT600] J-Link launch config default resets: Re-enable resets in J-Link launches for RT500/RT600 The most recent J-Link versions properly handle resets for RT500 & RT600 devices. Fixed: [RT500] Unable to Restart flash-based session on EVK RevC1 board. Fixed: [RT685] "Unsupported or unrecognized format error" dialog when using the installed SDK. Fixed: [LPC55S69] Implemented DWT (Data Watchpoint and Trace) component for ArmV8. This fixes the SWO Data trace not working issue. Fixed: [LPC55S06] SWO support. Fixed: [LPC55xx] LinkServer debug cannot recover LPC55xx from deep sleep. Fixed: [LPC845] Debug fails when SRAM is split into sub-blocks. Fixed: [LPC4337] Flash programming over JTAG not working on the M4 core. Fixed: [LPC54114] SWO Trace is not working with PEmicro. Fixed: [FRDM-K64] Removed unexpected warning reported in map file in a project. Fixed: [JN5189/QN9090/KW32W041AM] Improve OOB experience with (factory) erased devices. Fixed: IDE 'Utility' menu does not work for linked Folders. Fixed: Defined symbols are added prematurely (even when no component is selected in NPW). Fixed: Selection of a driver in NPW makes the Library Type and Floating Type to become empty. Fixed: "ERROR: fatal error: board.h: No such file or directory" error reported if build a new created project with no board support. Fixed: Library type is not changing correctly when using SDK Wizard. Fixed: SDKs for older LPCs failing to set CRP up correctly. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Issues when uninstalling a SDK plugin. Now "Installed SDKs" and "Install MCUXpresso SDK" views are in sync and report the right installation status of a SDK. Fixed: On explicit include paths in the project setting, the include paths are mixed between asm and c type. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Null pointer exception on generating example xml. Fixed: Build error when use MCUXpresso IDE command line with non-existing include. Fixed: SDK command line: pre and/or post build steps options not available in example.xml file. Fixed: J-Link scripts needed by SDK examples are not copied correctly when installing the SDK from a folder. Fixed: MCUXpresso linked projects compile errors on multicore platforms. Fixed: Compile errors reported on a project imported from a generate example.xml. Also fixed the CLI build failing on the same example.xml scenario. Fixed: Unexpected memory usage reported (over 100% occupied memory) by Image Info. Fixed: Programming empty pages for ERASE_WO devices when flash hashing is enabled. Fixed: 'debug interface type' identification shown in the "Debug messages" console. Fixed: "Terminate" operation does not kill the redlinkserv.exe process. Fixed: "Terminate" button appears disabled after the first "Suspend" for PEMicro and J-Link debug connection. Fixed: J-Link auto selection results in not working connection. Fixed: Flash programming using J-Link via JTAG. Fixed: The running environment (PC/SP) for RAM applications is now properly initialized by the debugger when using J-Link/PEmicro. Fixed: Debugger Console output stops working when debugging secure project. Fixed: Error reported when SWO clock speed dialogue cancelled. Fixed: FreeRTOS tasks list not populated correctly in some situations. Fixed: SVD viewer shows-up with empty peripherals list. Fixed: Live Variables: Unable to create expression with casts. Fixed: Global Variables: T0 will remain -0 while moving the Graph to the right. Fixed: [Dark Theme] highlighting makes text unreadable. Fixed: [Dark Theme] Text is not visible for Blocked jobs in FreeRTOS. Fixed: [Dark Theme] Peripherals view - some registers have yellow background making it hard to read. Fixed: [Dark Theme] Line highlighting in editor makes variables text unreadable. Fixed: [Dark Theme] Display issue for the "Probes discovered" window on Mac. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: [Dark Theme] Manage SDK Components window is not updated. Fixed: [Dark Theme] Various improvements on Disassembly, Memory, Peripherals, headers in views, editor, git plugin. Fixed: [Dark Theme] Install plugin SDKs window shows white rectangles around icons. Fixed: [Dark Theme] Line number background is too bright. Fixed: [Dark Theme] Install MCUXpresso SDK view shows white background while selecting table headers.
查看全文
We are pleased to announce that MCUXpresso IDE v24.9 (build 25) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.10.0 release  and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History  Summary of Changes - version 24.09  Release versioning schema changed to YY.MM.build_number Upgraded: Newer LinkServer software (v24.9.75). Upgraded: Newer SEGGER J-Link software (v8.10). Upgraded: Newer PEmicro plugins (v5.9.2). Updated: Version v16.1 of MCUXpresso Config Tools. Feature: [SDK Integration] Synchronization with SDK v2.16.100. Feature: [LinkServer] Upgraded MCU-Link version to 3.148. Feature: [LinkServer] Added initial support for MIMXRT700. Feature: [LinkServer] Added LinkServer flash programming utility for executing flash operations using the graphical user interface. Refer to docs/LinkFlash.md from LinkServer installation for additional details regarding the GUI flash support. Feature: [LinkServer] Added LinkServer application runner for use in CD/CI testing environments. Feature: [LinkServer] LinkServer flash load and flash verify commands now accept multiple files as arguments. Improvement: [IDE] Generated linker scripts now reference the BSD-3-Clause license. Improvement: [IDE] The IDE is now capable to update the MCU-Link probes firmware by retrieving the latest compatible firmware from nxp.com. Improvement: [LinkServer] Binaries are now compiled as 64-bit applications on Windows. Improvement: [LinkServer] Install x86 and x64 versions of Microsoft Visual C++ Redistributable on Windows. Improvement: [LinkServer] Added MCXN9xx FlexSPI flash driver to examples. Improvement: [LinkServer] Added disable GDET sequence to MCXN9xx and MCXN5xx preconnect scripts. Improvement: [LinkServer] Added standalone entries (no board) for MCXN9xx, MCXN5xx, MCXN2xx, MCXA1xx devices. Fixed: [FreeRTOS] Runtime percentage is always 0 inside Tasks view for FreeRTOS v10 (non-SMP). Fixed: [LinkServer] MCXN9xx FlexSPI flash driver problem (reproducible on some FRDM-MCXN947 boards). Fixed: [LinkServer] RT1020, RT1160/RT1170/RT1180 flash drivers in SDP mode. Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
This tip will show you how to re-trigger a full probe discovery.  The feature is very useful for the customer who may use multiple debug probes. The first time you debug a project, MCUXpresso IDE will perform a probe discovery operation and display the discovered Debug Probes for selection. This will show all Supported Probes that are attached to your computer. (Here you can see the default P&E Micro OpenSDA of FRDM-KL25Z board was found.) For any future debug sessions, the stored probe selection will be automatically used to match the project being debugged with the previously used debug probe. This greatly simplifies the case where multiple debug probes are being used. However, if a debug operation is performed and the previously remembered debug probe cannot be found, then a debug probe discovery operation will be performed from within the same family e.g. MCUXpresso IDE LinkServer, P&E Micro or SEGGER J-Link. (Here you can see there are two Probe search options: Search for PEMicroDBB97E74 again and Search for other attached PE Micro probes.) But if you want to use a different debug probe(for example: debug FRDM-KL25Z board with SEGGER JLink), click this blue debug icon will meet problem. Supported Probes dialog only show P&E Micro probes, it will not search other family of debug probes e.g. MCUXpresso IDE LinkServer or SEGGER J-Link.   Once a launch configuration file has been created, it will be used for the projects future debug operations. If you wish to use the project with a different debug probe, then simply delete the existing launch configuration and allow a new one to be automatically used on the next debug operation. Now click blue debug icon re-trigger a full probe discovery, and it show all Supported Probes that are attached to your computer again.
查看全文
We are pleased to announce that MCUXpresso IDE v11.9.1 (build 2170) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.9.0 release and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.9.1 - April 2024 Upgraded: Newer LinkServer software (v1.5.30) Upgraded: Newer SEGGER J-Link software (v7.96c). Upgraded: Newer PEmicro plugins (v5.7.8). Updated: Version v15.1 of MCUXpresso Config Tools. Improvement: [IDE] Updated licensing text from the About window. Improvement: [IDE] Support Eclipse variables for J-Link script file inside launch configuration. Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs returns an error if the IDE isn't installed in the default location. Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs fails to import some SDKs. Fixed: [IDE][Config Tools Integration] Fix some performance issues. Fixed: [IDE][Welcome page] Release notes text shown in What's New section might be incorrectly rendered. Fixed: [KW45/K32W1][J-Link] Debug after flash erase does not work.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
MCUXpresso IDE combines the best features of the LPCXpresso IDE and Kinetis Design Studio. For users more familiar with KDS, here’s a high level overview of some of the things that are different in basic interactions with this new tool.   Quickstart Panel. One of the biggest and most useful changes is the Quickstart panel in the lower left hand corner of the IDE. This is where users import MCUXpresso SDK projects, build projects, debug projects, and modify some project settings.   Importing SDK Example Projects This is now done via the Quickstart Panel, and by default will create a unique copy of the project inside the workspace directory with all the necessary source files for the board, drivers, and source so it can be easily shared.   Debugging SDK Projects This is also now done via the Quickstart Panel, and is straightforward. One important thing to note though is that if you want to change the debugger protocol (ie move from CMSIS-DAP to Segger JLink) you need to delete both the .launch files in the project so that the debugger settings will reset.   Semihosting If default options are kept when importing in SDK projects, semihosting is used for printf commands. See this Community post for details on how to use the UART for printf instead (which is connected to the OpenSDA circuit on development boards), as well as how to switch between the two options.   Importing SDKs New device support is added to MCUXpresso IDE by importing SDK packages. There’s an XML file inside the SDK packages that tell it all the information the IDE needs to know. Reference this Community post for some of the options you have in how to import an SDK into the IDE, and also refer to Section 4 of the MCUXpresso User Guide or this in-depth training video.   MCUXpresso SDK This is just a re-branding of Kinetis SDK 2.x now that it supports more than just Kinetis devices, so there are no significant differences with this new name change.   Porting a KDS project to MCUXpresso There is no automatic tool to take a KDS project and convert it to a MCUXpresso project, so there is some manual work involved in porting a KDS project to MCUXpresso IDE. The recommended path would be to import/create the closest MCUXpresso SDK project, and then copy in the custom source code and other modifications. Minimal code re-write should be required since the drivers are the same. They are also both Eclipse/GCC based IDEs so predefines should be straight forward to port over. 
查看全文
We are pleased to announce that MCUXpresso IDE v11.6.1 (build 8255) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.6.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.6.1 - October 2022 Upgraded: Newer SEGGER J-Link software (v7.70d). Upgraded: Version v12.1 of MCUXpresso Config Tools. Improvement: [Flash drivers] Included K32W041AM flash driver in layout examples. Fixed: [SWO][RT1170] SWO trace timing is not accurate when the trace clock is different from the core clock (e.g. for Cortex-M7 based devices). This misbehavior is visible in SWO Interrupts view. Fixed: [SWO][Counters] Cycle counter does not update while running and the Total value is wrong. Fixed: [NPW] Failed to create correct project for K22FX512 and SDK 2.3.1. Fixed: [NPW] Can’t use New Project wizard with two SDKs for the same board. Fixed: [NPW] SDK_DEBUGCONSOLE_UART option (which redirects the standard printf to UART) ignored when importing SDK examples. Fixed: [SDK Integration] Error thrown at build on FRDM-KL0Z from Import SDK example. Fixed: [Flash drivers] In provided /ide/Examples/Flashdrivers/NXP/iMXRT/iMXRT117x_FlexSPI_SFDP.zip, the octal flash RST control pin needs to be 0xOD (1.8V) instead 0x0A (3.3V). Fixed: [Project Manager] Missing Floating Point options for Cortex-M33 architecture. Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
查看全文
We are pleased to announce that MCUXpresso IDE v11.8.1 (build 1197) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.8.0 release and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.8.1 - October 2023 Upgraded: Newer SEGGER J-Link software (v7.92l). Upgraded: Newer PEmicro plugin (v5.7.3). Added: Support for i.MX RT1180 device and MIMXRT1180-EVK board. Added: Support for KE1xZ512 devices and X-FRDM-KE17Z512 board. Added: Support for MCXA153 device and FRDM-MCXA153 board. Improvement: [Toolchain Integration] Added C++20 and C++23 entries in the list of supported compiler dialects. Fixed: [Debugger][RW61x] Connect script does not halt after SYSRESET when secure project is in flash. Fixed: [Flash Programmer] Some problems related to flash blank command. Fixed: [SDK Integration] Device-specific preprocessor defines are not taken in consideration when changing device package.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.  
查看全文
We are pleased to announce that MCUXpresso IDE v11.3.1 (build 5262) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.3.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.3.1 - April 2021 Upgraded: Newer SEGGER J-Link software (v6.98a). Upgraded: Newer PEmicro plugin (v4.9.1). Added: 88MW320 support. Added: K32W041A support. Added: i.MX RT1160 support. Feature: Added MCU-Link firmware version check in MCUXpresso IDE: When connecting to target, "Probes discovered" will indicate if there are debugger probes that would require update; Each discovered probe will clearly indicate (by a warning icon) if a firmware update is available; Tooltip on the mentioned probes will indicate the firmware's download location and its version. Fixed: [RT1170] Can't download image to RT1170-EVK when SRAM_ITC_cm7 is located as the first item in RAM blocks in Memory configuration editor. Fixed: [RT1170][CM4 boot] Error programming flash in SDP or empty flash situations. Fixed: [RT5xx/RT6xx] wrong image type (at offset 0x24) in generated executable file. Fixed: [KW38] Instruction Trace window does not pull the assembler instructions. Fixed: [K32W041AM] SWO Trace not working. Fixed: SDK cannot set default launch config options for Segger. Fixed: Exception if the IDE is launched right after installation process, having all checkboxes for additional documentation selected. Fixed: Welcome page not appearing at startup. Fixed: Program and Erase Flash shortcuts from Quickstart Panel are also launching an unexpected debug session on the end of their normal operation. Fixed: LinkServer: Modifying from debugger 8-bit or 16-bit data residing at addresses not aligned to 32 bits may alter data beyond the intended range up to the next 32-bit address.
查看全文
We are pleased to announce that MCUXpresso IDE v11.5.1 (build 7266) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.5.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.5.1 - April 2022 Upgraded: CDT from CDT 10.3.0 to CDT 10.3.3. This is intended to address: https://bugs.eclipse.org/bugs/show_bug.cgi?id=575903 issue. Upgraded: Newer SEGGER J-Link software (v7.62c). Upgraded: Newer PEmicro plugin (v5.2.0). Added: [NPI] RT1060X (RT1060 phantom) support. Feature: [Flash Programmer][RT1160/RT117x] Add flash driver for QSPI on FlexSPI2 Port A. Fixed: [Debugger] Notifications about new MCU-Link firmware releases may not be shown in the Probes Discovery dialog. Fixed: [Debugger] Debug operations are slow while Peripherals+ window is open on targets with lots of registers (like RT1160 or RT117x). Fixed: [Project Manager][RT1160/RT117x] Flood of the -D__MULTICORE_MASTER in the .cproject. Fixed: [Project Manager][RT1160/RT117x] M7 C++ project failed to load the M4 project (in the case of multicore configuration) on a particular application. Now exdata sections are placed before heap and stack sections in generated linker files (when using Managed Linker Script configuration) compared with previous version where exdata sections were placed before data sections. Fixed: [Peripherals+][LPC546xx] EMC register location/offset is incorrect in Peripherals+ window. Fixed: [Energy Measurement] Instability if Energy Measurement view is used together with SWO Profile Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
查看全文
We are pleased to announce that MCUXpresso IDE v11.4.1 (build 6260) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.4.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.4.1 - September 2021 Upgraded: Newer SEGGER J-Link software (v7.54b, 32-bit version on Windows, 64-bit version on Linux/macOS). Upgraded: Newer PEmicro plugin (v5.1.0). Added: MCU-Link Pro probe support. Improvement: [SWO/Energy Measurement] Improved data collection rate. This aims to decrease the rate of lost packets (SWO) and gaps (Energy Measurement) at higher speed rates. Improvement: [LPC55xx] Add support in LinkServer flash drivers for programming data to the last flash sector (up to and excluding the reserved region). Fixed: [SWO] NPE obtained in the case of some SWO error types. This prevents the error dialogs to appear (the exceptions go silently). Fixed: [Energy Measurement] Detect data stream corruption and gracefully terminate Energy Measurement or SWO data retrieval if this situation arises. Fixed: [Energy Measurement] Sometimes stale data remains after clearing the data. Fixed: [Energy Measurement] No energy consumption info is displayed when measuring high (> 1W) power. Fixed: [Energy Measurement] No data is displayed after a while when measuring high currents. Fixed: [FreeRTOS TAD] Heap5 data not shown in Heap Usage view. Fixed: [Azure RTOS TAD] Azure RTOS debug session closes unexpectedly when using non-CM7 devices.
查看全文
  We are pleased to announce that MCUXpresso IDE v11.2.1 (build 4149) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.2.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.2.1 - October 2020 Upgraded: newer SEGGER J-Link software (v6.86). Upgraded: newer PEmicro plugin (v4.7.6). Upgraded: Version v8.1 of MCUXpresso Config Tools. Added: i.MX RT1170 B0 support. Added: i.MX RT1024 support. Added: LPC55S06 support. Added: K32W061 support. Added: MCU-Link debug probe support. MCU-Link is a new debug probe solution being developed for NXP LPC, Kinetis and i.MX RT targets. Feature: Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose (for LinkServer debug connection only). That means, in the case of multicore projects on which master project refers one or several slave projects, debug sessions will be automatically started for slave projects after initiating debug with the master project. Option is set by default on: Window -> Preferences -> MCUXpresso IDE -> Debug Options -> LinkServer Options -> Miscellaneous -> Enable Auto-debug slave project(s) for multicore projects. If you don't want to have this feature enabled (so if you want to start debug sessions for each core independently), uncheck this option. Improvement: Community forum accessible now from the main toolbar too (together with the older link from Help->MCUXpresso IDE support forum). The default selection will open the community web inside the IDE. If you want to set the default browser as external browser, use Window->Preferences->General->Web browser->"Use external web browser". Improvement: [RT600] Clean up on RT600 flash drivers (SDK now references the new drivers): Add drivers for MXIC_OPI connected via FlexSPI_A port Add drivers for QSPI drivers (SFDP) connected via FlexSPI_B port Add drivers for QSPI drivers (SFDP) connected via FlexSPI_A port Remove MIMXRT600_SFDP_* drivers generated by the old project Fixed: [RT595] Cannot debug flash application with J-Link. Fixed: [RT500][RT600] JLink launch config default resets: Re-enable resets in JLink launches for RT500/RT600 The most recent JLink versions properly handle resets for RT500 & RT600 devices. Fixed: [RT500] QSPI flash drivers: driver was incorrectly using QSPI DDR instead of SDR. Fixed: [LPC55S69] Implemented DWT (Data Watchpoint and Trace) component for ArmV8. This fixes the SWO Data trace not working issue. Fixed: Sometimes the linkserver semihosting console stops working. Fixed: 'mismatched input' warning reported for linker file. Fixed: Flash programming using JLink via JTAG. Fixed: The running environment (PC/SP) for RAM applications is now properly initialized by the debugger when using JLink/PEmicro. Fixed: JLink scripts needed by SDK examples are not copied correctly when installing the SDK from a folder. Fixed: Selection of a driver in NPW makes the Library Type and Floating Type to become empty. Fixed: [Dark Theme] highlighting makes text unreadable. Fixed: [Dark Theme] not working on Ubuntu 18. Fixed: [Dark Theme] Text is not visible for Blocked jobs in FreeRTOS. Fixed: [Dark Theme] Peripherals view - some registers have yellow background making it hard to read. Fixed: [Dark Theme] Line highlighting in editor makes variables text unreadable. Fixed: [Dark Theme] Display issue for the "Probes discovered" window on Mac. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: [RT5xx] Unable to Restart flash-based session on EVK Rev C1 board. Fixed: [LPC55xx] LinkServer debug cannot recover LPC55xx from deep sleep. Fixed: [LPC4337] Flash programming over JTAG not working on the M4 core. Fixed: [LPC845] Debug fails when SRAM is split into sub-blocks. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Not all dependency components are linked to project when the dependency is added from Config Tools. Fixed: Initialize execution environment when debugging RAM target application using Segger J-Link. Fixed: NPE occurred while using board SDK creator and adding a flash driver.
查看全文
This video shows how to import any of the SDK example projects and use it as a starting point for you own project. Enjoy!
查看全文
This video shows how to import MCUXpresso SDKs into the MCUXpresso IDE.
查看全文
[中文翻译版] 见附件 原文链接: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2019/06/12/using-lpc55s69-sdk-trustzone-examples-with-mcuxpresso-ide-v1100
查看全文
This exercise demonstrates how to port a project using MCUXpresso IDE and SDK from one RT MCU to another.  The exercise starts with an SDK demo project for the MIMXRT1060-EVK board, and ports to the IMXRT1050-EVKB board.   The "MCUXpresso IDE User Guide" installed with the IDE gives this warning: changing a project’s associated MCU should not be undertaken unless you have a total grasp of the consequence of this change.  Therefore rather than changing a project’s associated MCU, it is strongly recommended that instead a new project is generated for the desired MCU and this new project is edited as required.  However, on occasion it may be expedient to reset a project’s MCU (and associated SDK)   I also recommend using a SDK project intended for the final MCU, and just port the application source files to it.  But here are the steps to port the project.  Also note, these two boards use different flash types by default.  In this example, the IMXRT1050-EVKB was reworked to use the QSPI flash on the board following Appnote AN12108.  Once the RT1050 EVK is modified to use the QSPI flash, it is the same flash used on the RT1060 EVK.   Resources used in this exercise: IMXRT1050-EVKB board RevA1 MIMXRT1060-EVK board RevA2 MCUXpresso IDE v11.2.0 MCUXpresso SDK from Welcome | MCUXpresso SDK Builder  EVKB-IMXRT1050_SDK_2.8.2 EVK-MIMXRT1060_SDK_2.8.2   Attached to this post are two projects: Starting_evkmimxrt1060_iled_blinky.zip was the original SDK example running on the RT1060 EVK evkbmimxrt1050_iled_blinky_ported.zip is the final ported project, running from QSPI and RT1050     Following the "MCUXpresso IDE User Guide" section "Changing the MCU (and associated SDK)", changed the MCU to MIMXRT1052xxxxB.  Also changed the flash driver to MIMXRT1050_SFDP_QSPI.cfx.  If using Segger JLink, see https://wiki.segger.com/i.MXRT1050 to change the flash algorithm to QSPI.   And then changed the package/part number to MIMXRT1052DVL6B.   Changed the project name to evkbmimxrt1050_iled_blinky_ported Changed the C Compiler Preprocessor definitions to the SDK device CPU_MIMXRT1052DVL6B   Replaced the files from the SDK package EVKB-IMXRT1050_SDK_2.8.2 (Note: MCUXpresso IDE supports "SDK Project Component Management", which could also be used for updating some of these files.  See section "SDK Project Component Management" of the IDE user guide.  But I replaced the files manually myself from the RT1050 SDK package): device folder with the SDK files from EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052.  startup file from \EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052\mcuxpresso\ drivers files from \EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052\drivers\ board files, can use an SDK example for the ported device, or generate the clock_config and pin_mux files from the MCUXpresso Config tools xip files would also need to be updated if flash configuration changes.  In this example, both boards are using the same QSPI flash, and these files are the same.   Delete the .launch debug configuration file in the project.  MCUXpresso IDE will regenerate it.   With these changes, the ported project runs on the RT1050 EVK.
查看全文
Checking disassemble code is often needed for programmers when developing a project. This article will introduce two methods of generating disassemble file with GNU utility objdump under MCUXpresso IDE 10.1.0. If user needs demo code, please send me community internal message.
查看全文
As part of my university engagement, I have posted an overview article about the new MCUXpresso IDE: (external link): MCUXPresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse  I hope you find it useful, Erich
查看全文
1. Introduction In embedded system development, debugging and log output are critical for ensuring code correctness and optimizing performance. By monitoring system status in real time, capturing abnormal behavior, and recording key data, developers can quickly locate issues and verify functionality. In resource-constrained embedded environments, choosing the right debugging tools and methods significantly impacts development efficiency. MCXN947, a high-performance microcontroller launched by NXP, offers multiple debugging and logging solutions, among which ITM (Instrumentation Trace Macrocell) and UART printing are the most commonly used. ITM leverages the Cortex-M core’s debugging capabilities to transmit data at high speed via the debug interface, making it suitable for scenarios with strict real-time requirements. UART printing, on the other hand, outputs logs through the UART peripheral, offering strong versatility and suitability for production environments. This article explains how to use these two output methods in MCUXpresso IDE to improve development efficiency and system reliability. 2. Principles and Features of ITM and UART Printing 2.1 ITM – Principles and Features Working Principle: ITM (Instrumentation Trace Macrocell) is a debugging feature provided by the Cortex-M core. It transmits data in real time through the debug interface (e.g., SWD/JTAG) using SWO. Developers can use the ITM_SendChar() function to send debugging information to the ITM port, which is then captured by the debugger and displayed in the IDE’s debug console. Advantages: High-speed transmission: ITM uses the bandwidth of the debug interface, achieving speeds far higher than UART (typically over 10 Mbps). Low CPU overhead: ITM is handled by hardware, consuming almost no CPU resources. No extra peripherals: Does not rely on UART or other peripherals, saving hardware resources. Disadvantages: Debugger dependency: Requires a connected debugger (e.g., MCU-Link, J-Link) and cannot be used directly in production environments. Complex configuration: Proper ITM port and debugger settings are needed, which may be challenging for beginners. 2.2 UART Printing – Principles and Features Working Principle: UART printing sends debugging information to a serial terminal via the UART peripheral. Developers typically redirect the printf function to UART, enabling standard library functions for log output. Data is transmitted through TX/RX pins and can be viewed on a PC using serial tools (e.g., PuTTY, Tera Term). MCUXpresso IDE also integrates a terminal for UART debugging. Advantages: Highly versatile: Almost all embedded boards support UART, making it widely applicable. Production-ready: Does not require a debugger and can be used directly in production environments. Easy to implement: Simple configuration, ideal for beginners and rapid prototyping. Disadvantages: Lower speed: Limited by UART baud rate, resulting in lower transmission efficiency. Peripheral resource usage: Occupies UART peripherals and pins, which may affect other functions. Poor real-time performance: Due to interrupt delays and baud rate limitations, unsuitable for high real-time scenarios. 2.3 Summary of Comparison The following table summarizes the main characteristics of ITM versus UART printing: Feature ITM UART Printing Transmission Speed High (10 Mbps or more) Low (typically 115200 bps) CPU Overhead Low Higher Peripheral Dependency None Requires UART peripheral & pins Debugger Dependency Required Not required Production Suitability Not suitable Suitable Configuration Complexity Complex Simple Real-time Performance High Low   Usage Scenarios: ITM: Ideal for development-phase debugging with high real-time requirements (e.g., motor control, signal processing). UART Printing: Suitable for production logging, beginner-friendly setups, and general debugging needs. 3. Implementation Steps in MCUXpresso IDE 3.1 Using ITM Printing Hardware Requirement: Ensure the chip’s SWO pin is connected to the debugger’s SWO interface. Software Configuration: 1) When creating a new project, select “Redirect printf/scanf to ITM” to redirect printf/scanf to ITM.                            2) Configure the Trace clock:   /*!< Switch TRACE to TRACE_DIV */ CLOCK_AttachClk(kTRACE_DIV_to_TRACE); /*!< Set up dividers */ /*!< Set TRACECLKDIV divider to value 3 */ CLOCK_SetClkDiv(kCLOCK_DivTraceClk, 3U);    3)In MCUXpresso IDE, open the SWO ITM Console and configure Core Clock and Trace Clock settings.     4)View the output results in the ITM console. 3.2 Using UART Printing 1)When creating a new project, select SDK Debug Console to UART to set DebugConsole to use UART.          2)Use MCUXpresso IDE’s peripheral tools to configure DebugConsole-UART.    3)Configure UART TX/RX pins using the Pins tool.  4)Connect the serial hardware and view the output results in a terminal.  4. Conclusion ITM and UART printing each have their advantages. Developers should choose the appropriate method based on project requirements. ITM is better suited for high real-time debugging during development, while UART printing is ideal for production environments and general debugging.
查看全文
Attached MCUXpresso IDE fact sheet gives an overview about the IDE and its capabilities. More information is available on MCUXpresso IDE|NXP .
查看全文