MCUXpresso IDE知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso IDE Knowledge Base

标签

讨论

排序依据:
As a heads-up: several uses reported a problems with downloading the MCUXpresso IDE setup/installer program. If pressing the 'Download' button, you might come back to the login screen (to log into your NXP user account): The likely reason for this is that your NXP account needs re-activation. You should see a link to open a SR (Service Request) which you could use. Otherwise post a comment here so your account can be re-activated. I hope this helps, Erich
查看全文
This document provides some sample codes and steps for relocating Code and Data into RAM/FLASH. Please look at them with projects in attachment. It is based on “MCUXpresso_IDE_User_Guide.pdf”, so about the understanding of some macros, you can check on that document. This document is based on FRDM-K64, MCUXpressoIDE_10.0.2_411. You can use it on other chips too.   1. Introduce the “Memory configuration editor” 2.1. Relocating Data into RAM 2.1 Relocating Code into RAM 2.3 Relocating Code into Flash 3.Reference  
查看全文
MCUXpresso IDE combines the best features of the LPCXpresso IDE and Kinetis Design Studio. For users more familiar with KDS, here’s a high level overview of some of the things that are different in basic interactions with this new tool.   Quickstart Panel. One of the biggest and most useful changes is the Quickstart panel in the lower left hand corner of the IDE. This is where users import MCUXpresso SDK projects, build projects, debug projects, and modify some project settings.   Importing SDK Example Projects This is now done via the Quickstart Panel, and by default will create a unique copy of the project inside the workspace directory with all the necessary source files for the board, drivers, and source so it can be easily shared.   Debugging SDK Projects This is also now done via the Quickstart Panel, and is straightforward. One important thing to note though is that if you want to change the debugger protocol (ie move from CMSIS-DAP to Segger JLink) you need to delete both the .launch files in the project so that the debugger settings will reset.   Semihosting If default options are kept when importing in SDK projects, semihosting is used for printf commands. See this Community post for details on how to use the UART for printf instead (which is connected to the OpenSDA circuit on development boards), as well as how to switch between the two options.   Importing SDKs New device support is added to MCUXpresso IDE by importing SDK packages. There’s an XML file inside the SDK packages that tell it all the information the IDE needs to know. Reference this Community post for some of the options you have in how to import an SDK into the IDE, and also refer to Section 4 of the MCUXpresso User Guide or this in-depth training video.   MCUXpresso SDK This is just a re-branding of Kinetis SDK 2.x now that it supports more than just Kinetis devices, so there are no significant differences with this new name change.   Porting a KDS project to MCUXpresso There is no automatic tool to take a KDS project and convert it to a MCUXpresso project, so there is some manual work involved in porting a KDS project to MCUXpresso IDE. The recommended path would be to import/create the closest MCUXpresso SDK project, and then copy in the custom source code and other modifications. Minimal code re-write should be required since the drivers are the same. They are also both Eclipse/GCC based IDEs so predefines should be straight forward to port over. 
查看全文
View Webinar Recording
查看全文
We are pleased to announce that MCUXpresso IDE v11.8.0 (build 1165) is now available. This is  a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.7.1.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.8.0 - August 2023 Upgraded: Eclipse version to 2022.12 (Eclipse Platform 4.26.0 / CDT 11.0.0). Upgraded: MCUXpresso IDE integrated with OpenJDK Runtime Environment Temurin-17.0.5+8. Upgraded: GNU ARM Embedded Toolchain to version 12.2.Rel1. Upgraded: Version v14 of MCUXpresso Config Tools. Upgraded: ARM CMSIS-Pack Eclipse Plug-ins 2.8.0. Upgraded: Newer SEGGER J-Link software (v7.88m). Upgraded: Newer PEmicro plugin (v5.6.7). Synchronization with SDK v2.14.x. Added support for MCXN9xx devices. Added support for RW61x devices. Feature: New IDE build for Mac with native Apple silicon support. See download section for the new product. Feature: LinkServer LPC-Link2 firmware now softloaded as v5.460 which offers support for powering certain RT1xxx EVK boards (which incorporate on-board debug probes based on LPC-Link2 hardware) through the USB debug connection. Feature: [Open-CMSIS-Pack] Extended integration with ARM CMSIS-Pack Eclipse Plug-ins.  Now adding a new Open-CMSIS-Pack component is managed by ARM CMSIS-Pack Eclipse Plug-in. This brings support for: components dependency. multiple component selection. automatically check dependencies in the new multiple component selection view. copy configuration and template files to project. Note. If a project was created with the previous version of Open-CMSIS-Pack support, you'll be asked to remove or to keep the added components. Choosing "keep" involves preserving sources only, not the links with Open-CMSIS-Pack Manager. If you need to have them managed by ARM CMSIS-Pack Eclipse Plug-in (for the above mentioned available features) please choose "remove" and add them back. Feature: Added support for selecting library type in SDK CLI. Now redlib, newlib, newlib_nano can be selected as options when generating a project. Check MCUXpresso_IDE_Command_Line_User_Guide.pdf for details. Improvement: [SDK Integration] Allow the possibility to switch a project from one MCU device to another. Improvement: [SDK Integration] Reduced time required to import examples from zipped SDKs. Improvement: [SDK Integration] Optimize initial SDK GitHub cloning time by deferring cloning of examples until actually needed. Improvement: [Debugger] Discover Probes dialog warns if using MCU-Link probes running firmware which is incompatible with the current IDE version. Improvement: [Debugger] Add possibility to disable auto-debug of secondary project based on target name in Debug Options preferences. Improvement: [RTOS] Add preferences to control enablement of RTOS TAD logging consoles. This prevents showing up unwanted or not used consoles. Go to Preferences -> MCUXpresso IDE -> RTOS TAD -> (Desired) RTOS -> Logging configuration and select or unselect "Create logging console and log messages from TAD plugin". Improvement: [SWO] Error caused by input in the ITM console now should also be displayed inside the console. Improvement: [IDE][Quickstart Panel] Added link to executable import wizard in Quickstart Panel. Improvement: [IDE] Add 'bash' shell executable in buildtools/bin folder on Windows. Improvement: [Installer] Support silent installation for Linux installers (deb.bin packages). This can be executed using: <install_package>.deb.bin -- --acceptLicense. Fixed: [SDK Integration] Unexpected disk space consumption at "Refresh" operation. Fixed: [SDK Integration] Error reported when creating a project from GitHub SDK with a board selection from a standalone SDK. Fixed: [SDK Integration] Include Paths list is duplicated after refreshing SDK components. Fixed: [SDK Integration] New Project Wizard incorrectly computes anyOf dependency for multi core component. Fixed: [SDK Integration] C startup file is incorrectly added in C++ project after refreshing SDK components. Fixed: [SDK Integration] App SW Packs fail to import on IDE starting with IDE v11.7.0 and SDK v2.12 and v2.13. Fixed: [SDK Integration] Exception error is displayed when user scrolls in component list from SDK Wizard window. Fixed: [SDK Integration] Cloning more than one GitHub SDK repository makes the second repository unusable. Fixed: [SDK Integration] Deselecting components with dependencies doesn't display warnings. Fixed: [SDK Integration] Unable to deactivate an already installed Git SDK repository from Installed SDKs view. Fixed: [SDK Integration] Build error is obtained when some specific components (serial_manager_*) are changed from SDK Management -> Manage SDK Components view. Fixed: [SDK Integration] Progress is incorrectly reported in NPW and SDK Import Wizard. Fixed: [SDK Integration] Importing projects may introduce wrong dependencies between SDK components which result in build failure. Fixed: [Toolchain integration] Building some projects may be shown as failed due to linker warnings misinterpreted as errors. Fixed: [Toolchain Integration] Project is always rebuilt after restarting the IDE. Fixed: [Executable Importer] Cannot use Binary Utilities with the imported ELF. Fixed: [Managed Linker Script] Sometimes .bss sections are unexpectedly part of the output bin/s19 images. These are now declared as NOLOAD in the linker scripts. Fixed: [Flash Programmer] KW45B41Z board should not have Resurrect locked Kinetis device option. Fixed: [Flash Programmer] Flash tool not writing .flash_config section from ELF. Fixed: [Debug][LPC55S36 A1] Restart does not work. Fixed: [Debug] Null pointer exception when creating new launch config for LinkServer. Fixed: [Debug] Broken SWO functionality on non LPC-Link2/MCULink probes (Arm ULINKplus). Fixed: [Debug][Multicore] "Step Return All Debug sessions" throws error while in source code. Fixed: [Debug][ARMv6-M] The default VECTRESET set for flash reset has no effect since it is not supported for ARMv6-M MCUs. Use SOFT reset instead. Fixed: [Debug][PEmicro & LinkServer] GUI Flash Tool fields are pre-filled with wrong information for PEmicro when a debug launch is previously created, or are not implemented when using LinkServer debug probes. Fixed: [Debug][PEmicro] TrustZone projects cannot be debugged because non-secure image is not programmed in flash. Fixed: [Debug][LinkServer] Semihosting operations fail while debugger is detached and may not recover when re-attaching. Fixed: [Debug][LinkServer] Various semihosting operations fail when using LinkServer debug probe. Fixed: [Debug][LinkServer][SWO] Support for SWO trace using CMSIS-DAP1.1 SWO probes is broken. Fixed: [Debug][LinkServer] Debug session launch is very slow on LinkServer compared to other probes on some Windows PCs. Fixed: [Debug][Linkserver] Cannot boot LPC-Link1 when a LPC-Link2 probe configured for DFU booting is also present. Fixed: [Energy Measurement] View should not allow attaching to debug session on targets with no measurement support. Fixed: [Enery Measurement] Error might be encountered when successively connecting various probes and using "Out of debug" mode. Fixed: [FreeRTOS] Exception occasionally encountered when resuming or pausing the debug session of a FreeRTOS project with non-stop GDB option disabled and Peripherals Window open. Fixed: [FreeRTOS] In 'freertos_hello' example application, 'hello' task is shown as "Running" even before having the scheduler running. Fixed: [SWO] When SWO Counters view is resumed, also the SWO Data view is resumed automatically. Fixed: [IDE] IDE Linker File Parser fails for question mark operator. Fixed: [IDE] Update icons to address some problems on dark theme and high DPI (macOS Retina) displays.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available
查看全文
This video shows how to import MCUXpresso SDKs into the MCUXpresso IDE.
查看全文
Semihosting printf with MCUXpresso IDE When importing MCUXpresso SDK projects into MCUXpresso IDE, they will be configured by default to use “semihosting” for the terminal output. This means the project will use the debugger connection to send terminal characters instead of the UART. More information on semihosting can be found on this Community document and in Section 11.4 of the MCUXpresso User Guide.   Note that the information in this post is only applicable when using the MCUXpresso IDE, as the projects for other IDEs will use the UART by default when opening up their respective MCUXpresso SDK projects. Also semihosting only works when there is an active debug connection to the device.    printf with semihosting:   printf with UART Terminal (with TeraTerm):   How to choose UART output during the project import In order to use the UART for MCUXpresso IDE projects, some configuration settings need to be modified when importing in the project. First, you will need to uncheck the “Enable semihosting” option to clear the box. This will tell the project to use the normal libraries and not the semihosting libraries.   Then on the next screen, you’ll want to uncheck the “Redirect SDK “PRINTF” to C library “printf”” box to clear it. This will tell the project to use the MCUXpresso SDK source files for printf instead of the generic C files. This allows you to debug, and modify if desired, the printf functionality found inside the MCUXpresso SDK. Section 5.1.2 of the MCUXpresso IDE User Guide describes the options on this screen in more detail.     Switching between semihosting and UART If you’re already imported the project and wish to switch between using semihosting or the UART, you can do this from the “Quick Settings” menu inside the Quickstart panel.    If moving from semi-hosting to UART, this will change the library used to “nohost-nf” and set SDK_DEBUGCONSOLE define to 1 inside the pre-processor settings. If moving from UART to semi-hosting, this will change the library to “semihost-nf” and set SDK_DEBUGCONSOLE define to 0.    If you're not seeing any printf output, double check you have the right settings.    Note that when importing the project initially and “Enable semihosting” is deselected and “Redirect SDK “PRINTF” to C library “printf”” is deselected in order to use the UART for terminal output, there is no SDK_DEBUGCONSOLE defined in the project settings. However inside the debug console SDK code itself, there is a #if statement so that if that value is not defined, then that define is set to 1, and hence why the SDK debug console is still used in that case.
查看全文
For the previous KDS or CodeWarrior users, they may not create and use static library under MCUXpresso IDE without a hitch, because the methods are not exactly same. MCUXpresso IDE supports adding static library in user project with “Smart Update” wizard. This feature is derived from LPCXpresso IDE.  However, “Smart Update” wizard is only available for natively supported LPC products in MCUXpresso 10.1.0 and lower versions.  It will support all LPC and Kinetis product in MCUXpresso IDE future release. For MCUXpresso natively supported LPC product, using “Smart Update” to add library is very convenient. User can learn its usage from this article: Creating and Linking to Library Projectshttps://community.nxp.com/message/630594 For Kinetis product, the only way to add library to project is by hand. This article will take an example with MK64F demo, illustrating how to create and use static library under MCUXpresso IDE step by step.  It will also be good for all LPC and Kinetis users to understand how user project works with external static libraries under MCUXpresso.  If user needs demo code of this article, please send me community internal message. Thanks for the suggestion from LPCX support        
查看全文
Dear Community, The purpose of this document is to show how to integrate projects from the file system to MCUXpresso IDE. It is actually not that complicated as you might have imagined.  Let's begin... The import project(s) from file system option is included in the Quickstart Panel, which is located in the lower left corner of the IDE. Type / Paste the location of the folder (either zipped or unpacked). Then, click Next button. Finally, select all the project folders / examples you want to be imported. Now, they will be accessible and available from the Project explorer. Happy development! Best regards, Ivan R.
查看全文
1. Introduction In embedded system development, debugging and log output are critical for ensuring code correctness and optimizing performance. By monitoring system status in real time, capturing abnormal behavior, and recording key data, developers can quickly locate issues and verify functionality. In resource-constrained embedded environments, choosing the right debugging tools and methods significantly impacts development efficiency. MCXN947, a high-performance microcontroller launched by NXP, offers multiple debugging and logging solutions, among which ITM (Instrumentation Trace Macrocell) and UART printing are the most commonly used. ITM leverages the Cortex-M core’s debugging capabilities to transmit data at high speed via the debug interface, making it suitable for scenarios with strict real-time requirements. UART printing, on the other hand, outputs logs through the UART peripheral, offering strong versatility and suitability for production environments. This article explains how to use these two output methods in MCUXpresso IDE to improve development efficiency and system reliability. 2. Principles and Features of ITM and UART Printing 2.1 ITM – Principles and Features Working Principle: ITM (Instrumentation Trace Macrocell) is a debugging feature provided by the Cortex-M core. It transmits data in real time through the debug interface (e.g., SWD/JTAG) using SWO. Developers can use the ITM_SendChar() function to send debugging information to the ITM port, which is then captured by the debugger and displayed in the IDE’s debug console. Advantages: High-speed transmission: ITM uses the bandwidth of the debug interface, achieving speeds far higher than UART (typically over 10 Mbps). Low CPU overhead: ITM is handled by hardware, consuming almost no CPU resources. No extra peripherals: Does not rely on UART or other peripherals, saving hardware resources. Disadvantages: Debugger dependency: Requires a connected debugger (e.g., MCU-Link, J-Link) and cannot be used directly in production environments. Complex configuration: Proper ITM port and debugger settings are needed, which may be challenging for beginners. 2.2 UART Printing – Principles and Features Working Principle: UART printing sends debugging information to a serial terminal via the UART peripheral. Developers typically redirect the printf function to UART, enabling standard library functions for log output. Data is transmitted through TX/RX pins and can be viewed on a PC using serial tools (e.g., PuTTY, Tera Term). MCUXpresso IDE also integrates a terminal for UART debugging. Advantages: Highly versatile: Almost all embedded boards support UART, making it widely applicable. Production-ready: Does not require a debugger and can be used directly in production environments. Easy to implement: Simple configuration, ideal for beginners and rapid prototyping. Disadvantages: Lower speed: Limited by UART baud rate, resulting in lower transmission efficiency. Peripheral resource usage: Occupies UART peripherals and pins, which may affect other functions. Poor real-time performance: Due to interrupt delays and baud rate limitations, unsuitable for high real-time scenarios. 2.3 Summary of Comparison The following table summarizes the main characteristics of ITM versus UART printing: Feature ITM UART Printing Transmission Speed High (10 Mbps or more) Low (typically 115200 bps) CPU Overhead Low Higher Peripheral Dependency None Requires UART peripheral & pins Debugger Dependency Required Not required Production Suitability Not suitable Suitable Configuration Complexity Complex Simple Real-time Performance High Low   Usage Scenarios: ITM: Ideal for development-phase debugging with high real-time requirements (e.g., motor control, signal processing). UART Printing: Suitable for production logging, beginner-friendly setups, and general debugging needs. 3. Implementation Steps in MCUXpresso IDE 3.1 Using ITM Printing Hardware Requirement: Ensure the chip’s SWO pin is connected to the debugger’s SWO interface. Software Configuration: 1) When creating a new project, select “Redirect printf/scanf to ITM” to redirect printf/scanf to ITM.                            2) Configure the Trace clock:   /*!< Switch TRACE to TRACE_DIV */ CLOCK_AttachClk(kTRACE_DIV_to_TRACE); /*!< Set up dividers */ /*!< Set TRACECLKDIV divider to value 3 */ CLOCK_SetClkDiv(kCLOCK_DivTraceClk, 3U);    3)In MCUXpresso IDE, open the SWO ITM Console and configure Core Clock and Trace Clock settings.     4)View the output results in the ITM console. 3.2 Using UART Printing 1)When creating a new project, select SDK Debug Console to UART to set DebugConsole to use UART.          2)Use MCUXpresso IDE’s peripheral tools to configure DebugConsole-UART.    3)Configure UART TX/RX pins using the Pins tool.  4)Connect the serial hardware and view the output results in a terminal.  4. Conclusion ITM and UART printing each have their advantages. Developers should choose the appropriate method based on project requirements. ITM is better suited for high real-time debugging during development, while UART printing is ideal for production environments and general debugging.
查看全文
We are pleased to announce that MCUXpresso IDE v25.06 (build 136) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v24.12 release and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 25.06 Upgraded: Arm GNU Toolchain to version 14.2.Rel1. Upgraded: Newer LinkServer software (v25.6.131). Upgraded: Newer SEGGER J-Link software (v8.44). Upgraded: Newer PEmicro plugins (v6.0.3). Upgraded: Version v25.06 of MCUXpresso Config Tools. Feature: [IDE] Remove MCUXpresso IDE-specific support for management of Open-CMSIS packs. Feature: [IDE][LinkServer] Automatic LinkServer update from within the IDE. Feature: [IDE][SDK integration] Synchronization with SDK v25.06. Note: Only MCUXpresso IDE packages downloaded from mcuxpresso.nxp.com are supported. GitHub SDK format is currently not supported. Feature: [LinkServer] Added support for MCXW235, MCXW236 devices. Feature: [LinkServer] Added initial support for MCXA345, MCXA346 devices and FRDM-MCXA346 board. Feature: [LinkServer] Added initial support for MCXA175, MCXA176, MCXA255, MCXA256, MCXA355, MCXA356 devices. Feature: [LinkServer] Added support to allow custom pre-attach initializations. Feature: [LinkServer] Added --exit-timeout option for runner to limit the time it waits for application termination. Feature: [LinkServer] Discontinued support for legacy RedProbe and RedProbe+ probes. Feature: [LinkServer] Added possibility to associate LinkServer with existing MCUXpresso IDE installations at install time. Fixed: [IDE installer] Desktop shortcut is not created for non-administrative user.   Known issues The IDE occasionally crashes on Ubuntu 24. Crash dumps refer to GTK-specific code and experiments show that forcing GTK4 usage inside the IDE could be a workaround for the problem. Note: additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.  
查看全文
We are pleased to announce that MCUXpresso IDE v24.12 (build 148) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v24.09 release  and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History  Summary of Changes - version 24.12  Upgraded: Newer LinkServer software (v24.12.21). Upgraded: Newer SEGGER J-Link software (v8.12a). Upgraded: Newer PEmicro plugins (v5.9.5). Upgraded: Version v24.12 of MCUXpresso Config Tools. Feature: [LinkServer] Upgraded MCU-Link version to 3.152. Feature: Support for KW47, MCXW72 devices, and KW47-EVK, KW47-LOC, MCX-W72-EVK, FRDM-MCXW72, MCX-W72-LOC boards. Feature: Support for MCXA165, MCXA166, MCXA175, MCXA176, MCXA275, and MCXA276 devices. Feature: Support for MIMXRT700. Feature: [SDK Integration] Synchronization with SDK v24.12.  Note: Only MCUXpresso IDE packages downloaded from mcuxpresso.nxp.com are supported. GitHub SDK format is currently not supported. Feature: [IDE] Automatic probe selection and device/board verification when using CMSIS-DAP-based probes with target information available. Improvement: [IDE] When importing multiple projects and no associated installed SDK is found, show only one dialog message dialog listing all projects and missing SDKs. Install MCUXpresso SDKs view can then be opened from the dialog. Fixed: [IDE] The SDK details associated with a project are not updated after associating other compatible SDK. Fixed: [IDE] Project Settings node from Project Explorer shows incorrect SDK version once associating other SDK with project. Fixed: [SDK Integration] Preprocessor defines might be incorrect when importing some example projects that are linked to other projects. Fixed: [Debug][J-Link] Restart for RAM debug does not work for some MCUs when using J-Link. Fixed: [Application Code Hub] Some projects might not be recognized as valid MCUXpresso IDE projects because they do not use the NXP GitHub.
查看全文
We are pleased to announce that MCUXpresso IDE v24.9 (build 25) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.10.0 release  and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History  Summary of Changes - version 24.09  Release versioning schema changed to YY.MM.build_number Upgraded: Newer LinkServer software (v24.9.75). Upgraded: Newer SEGGER J-Link software (v8.10). Upgraded: Newer PEmicro plugins (v5.9.2). Updated: Version v16.1 of MCUXpresso Config Tools. Feature: [SDK Integration] Synchronization with SDK v2.16.100. Feature: [LinkServer] Upgraded MCU-Link version to 3.148. Feature: [LinkServer] Added initial support for MIMXRT700. Feature: [LinkServer] Added LinkServer flash programming utility for executing flash operations using the graphical user interface. Refer to docs/LinkFlash.md from LinkServer installation for additional details regarding the GUI flash support. Feature: [LinkServer] Added LinkServer application runner for use in CD/CI testing environments. Feature: [LinkServer] LinkServer flash load and flash verify commands now accept multiple files as arguments. Improvement: [IDE] Generated linker scripts now reference the BSD-3-Clause license. Improvement: [IDE] The IDE is now capable to update the MCU-Link probes firmware by retrieving the latest compatible firmware from nxp.com. Improvement: [LinkServer] Binaries are now compiled as 64-bit applications on Windows. Improvement: [LinkServer] Install x86 and x64 versions of Microsoft Visual C++ Redistributable on Windows. Improvement: [LinkServer] Added MCXN9xx FlexSPI flash driver to examples. Improvement: [LinkServer] Added disable GDET sequence to MCXN9xx and MCXN5xx preconnect scripts. Improvement: [LinkServer] Added standalone entries (no board) for MCXN9xx, MCXN5xx, MCXN2xx, MCXA1xx devices. Fixed: [FreeRTOS] Runtime percentage is always 0 inside Tasks view for FreeRTOS v10 (non-SMP). Fixed: [LinkServer] MCXN9xx FlexSPI flash driver problem (reproducible on some FRDM-MCXN947 boards). Fixed: [LinkServer] RT1020, RT1160/RT1170/RT1180 flash drivers in SDP mode. Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
We are pleased to announce that MCUXpresso IDE v11.10.0 (build 3148) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.9.1 release and we recommend that all existing users download and install this new version.   Installer Downloads      To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History  Important note: J-Link package Version V7.96o is unusable on macOS (Intel and Apple silicon packages). Therefore, if you are running MCUXpresso IDE v11.10.0 on a macOS, you will be unable to debug with J-Link probes. Starting with J-Link Version V7.96s, the issue was fixed by Segger.   You are required to manually download the new J-Link package and install it. Once installed, you will need to instruct the IDE to use the new J-Link installation by following the steps: 1. Open the IDE. 2. Go to MCUXpresso IDE > Settings… 3. Expand MCUXpresso IDE -> Debug Options -> J-Link Options category. 4. Enable Custom Path inside the J-Link path configuration section. 5. Browse to the new J-Link installation folder.   Note: the path must be configured for each workspace used with MCUXpresso IDE v11.10.0. If you prefer to change the path to J-Link for all workspaces, you can execute the following command:   /Applications/MCUXpressoIDE_11.10.0_3148/ide/MCUXpressoIDE.app/Contents/MacOS/mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.segger:jlink.default.install.path=/Applications/SEGGER/<JLinkPath>   Summary of Changes - version 11.10.0 - July 2024 Upgraded: Eclipse version to 2023.12 (Eclipse Platform 4.30.0 / CDT 11.4.0). Upgraded: GNU ARM Embedded Toolchain to version 13.2.Rel1. Note1: Debugging info is enforced to DWARF version 4 ("-gdwarf-4"). Note2: The IDE no longer uses the "-ffreestanding" compiler flag when creating projects with NPW. GNU GCC 13 does not allow anymore the inclusion of non-freestanding library headers in freestanding environments. Upgraded: ARM CMSIS-Pack Eclipse Plug-ins 2.9.0. Upgraded: Newer xPack Windows Build Tools (v4.4.1-2). Upgraded: Newer LinkServer software (v1.6.133). Upgraded: Newer SEGGER J-Link software (v7.96o). Upgraded: Newer PEmicro plugins (v5.8.2). Upgraded: Version v16 of MCUXpresso Config Tools. Added debug support for MCXA156 device and FRDM-MCXA156 board. Added debug support for MCXW71x device and FRDM-MCXW7X board. Added debug support for MCXC041, MCXC242 and MCXC444 devices and the respective FRDM-MCXC041, FRDM-MCXC242 and FRDM-MCXC444 boards. Updated debug support for RW612 rev A2 silicon. Feature: [Documentation] Update to new format according to latest NXP guidelines. Feature: [IDE] Rework Other Symbols tab on a launch configuration to add possibility to download extra images. Feature: [IDE] MCU-Link probes firmware can now be updated automatically from within Probes Discovered dialog. Feature: [IDE] Use a J-Link path configuration section similar to LinkServer (see J-Link Preferences page). Feature: [IDE] Add support for displaying .md (markdown format) files. Feature: [FreeRTOS v11] Add preliminary support in TAD views in LinkServer GDB thread awareness. Feature: [Zephyr RTOS] Add TAD views for timers, mutexes, events and semaphores. Feature: [SDK Handling] Add preference to control refresh of available remote plugin SDKs at IDE startup. Feature: [Toolchain integration] Inform about "freestanding" usage and about the changes brought by GCC 13. Markers are created in Problems view. Feature: [Linux Installer] Add an explicit user consent regarding installation of udev rules. Improvement: [IDE] Show warning about invalid or incompatible LinkServer at IDE startup. Improvement: [IDE][NPW] Projects created using the New Project Wizard no longer contain the devicespecific include in the main source file. Improvement: [IDE][SDK Handling] SDKs installed through the "Install MCUXpresso SDKs" are no longer installed using the P2 Eclipse mechanism. They are installed as file system SDKs instead. Improvement: [IDE][SDK Handling] Complete cleanup after uninstalling a GitHub SDK. Improvement: [IDE][Toolchain integration] Allow managing C++ include paths from Quickstart Panel => Quick Settings. Improvement: [IDE][Toolchain integration] Revise enforcement of DWARF 4 in imported projects. Improvement: [IDE][Application Code Hub] Offer to install missing SDK used by projects imported after cloning a remote repository. Improvement: [IDE] Better layout for multicore-related filtering controls in PEmicro preferences page. Improvement: [IDE] Support Eclipse variables for J-Link script file inside launch configuration. Improvement: [Linux Installer] LinkServer deb installers now install a versioned product, allowing multiple product instances. Improvement: [Linux Installer] Allow installation even without libncurses5/libncursesw5 (build tools dependencies). Improvement: [Windows Installer] Better handling of systems with case sensitive enabled paths. Fixed: [IDE] When using absolute paths for artifact names, intermediate .args response files for linker/archiver are not generated. Fixed: [IDE] Custom LinkServer path not taken into account when launching redlinkserv. Fixed: [IDE][Command line] Eclipse returns non-zero exit code when building project without having the associated SDK installed. Fixed: [IDE][GUI Flash Tool] Preserve connect script field when switching tabs. Fixed: [IDE][Trace] Instruction trace configuration fails to correctly link/chain watchpoints comparators. Fixed: [RTOS] "Unknown" task names in the FreeRTOS tasks list view after stepping from "main". Fixed: [MQX][LinkServer] GDB thread awareness fails to show and debug 23+ threads. Fixed: [Debug][LinkServer] Problems related to evaluation of complex expressions in LinkServer scripts (.scp). Fixed: [Debug][LinkServer] Increased the maximum number of supported probes in Redlink Server from 8 to 16. Fixed: [Debug][LinkServer] Fix a problem related to restart after flash load. Fixed: [Debug][LinkServer] Problems related to soft reset for MIMXRT1170 and MIMXRT1160 when debugging Cortex-M4 applications in RAM. Fixed: [Debug][PEmicro][MCXN2xx] TrustZone projects cannot be reliably debugged with PEmicro probes. Fixed: [Debug][PEmicro][MCXN5xx] Flash driver for external QSPI flash is not available, thus programming/debugging fails. Fixed: [Debug][PEmicro] Step over does not work after restart and after reading the list of FreeRTOS tasks. Fixed: [Debug][J-Link][RT1170] Unable to program a CM4 flash image. Fixed: [SDK Integration] Compilation might fail after adding/refreshing certain SDK components from IDE (depending on SDK definition). Fixed: [SDK Integration] Mutually exclusive dependencies are not handled correctly. Fixed: [SDK Integration] Incorrect handling of project template components for imported SDK examples. Fixed: [SDK Integration] Config files contributed by components are incorrectly handled when example projects already contain the same configuration files. Fixed: [SDK Integration] NPW now properly considers device_core dependencies, preventing incorrect component addition for the wrong core. Fixed: [Windows Installer] Cannot open the documentation page from the shortcut available in the Start menu. Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
We are pleased to announce that MCUXpresso IDE v11.9.1 (build 2170) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.9.0 release and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.9.1 - April 2024 Upgraded: Newer LinkServer software (v1.5.30) Upgraded: Newer SEGGER J-Link software (v7.96c). Upgraded: Newer PEmicro plugins (v5.7.8). Updated: Version v15.1 of MCUXpresso Config Tools. Improvement: [IDE] Updated licensing text from the About window. Improvement: [IDE] Support Eclipse variables for J-Link script file inside launch configuration. Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs returns an error if the IDE isn't installed in the default location. Fixed: [IDE][SDK Handling] Automatic import of plugin SDKs fails to import some SDKs. Fixed: [IDE][Config Tools Integration] Fix some performance issues. Fixed: [IDE][Welcome page] Release notes text shown in What's New section might be incorrectly rendered. Fixed: [KW45/K32W1][J-Link] Debug after flash erase does not work.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
We are pleased to announce that MCUXpresso IDE v11.9.0 (build 2144) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.8.1.  Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.9.0 - January 2024 Upgraded: Eclipse version to 2023.06 (Eclipse Platform 4.28.0 / CDT 11.2.0). Upgraded: MCUXpresso IDE integrated with OpenJDK Runtime Environment Temurin-17.0.7+7. Upgraded: GNU ARM Embedded Toolchain to version 12.3.Rel1. Note. Debugging info is enforced to DWARF version 4 ("-gdwarf-4"). Upgraded: ARM CMSIS-Pack Eclipse Plug-ins 2.9.0. Upgraded: Newer SEGGER J-Link software (v7.94b). Upgraded: Newer PEmicro plugin (v5.7.6). Upgraded: Version v15 of MCUXpresso Config Tools. Added: Initial support for MCXN2xx devices and FRDM-MCXN236 board. Feature: [MCXN9xx] Update debug support for A1 silicon. Feature: [App Code Hub] The IDE now offers views and wizards that allow users to import projects by directly interacting with Application Code Hub website. Feature is accessible through the File -> Import -> Application Code Hub wizard, the dedicated Quickstart link, by opening the view using Window -> Show View -> Other -> Application Code Hub, or by using Help -> Additional Resources -> Application Code Hub menu entry. Feature: [SDK Integration] Synchronization with SDK v2.15.abc and manifest schema version 3.14. Feature: [SDK Integration] Support complex dependencies for board, core, device, toolchain, compiler. Feature: [SDK Integration] Support new "template" type of SDK component containing predefined code snippets, visible to users in the UI of new project wizard and component manager to allow users to add the files with the snippets into projects. Also, added CLI support for this type by "use.all.templates" property for the "example.build" and "project.build" commands. By default, the option is set to false, so no template source is added to the project. Feature: [SDK Integration] Existing Import Remote SDK Git repository flow improved - a wizard is now used to clone and import the SDK. Feature: [SDK Integration] Automatic import of plugin SDKs from previous IDEs versions when upgrading to newer version. Feature: [SDK Integration] Add "change.sdk.roots" command in CLI mode that allows updating the built-in SDK search locations. Feature: [RT1160/RT1170/RT1020] Update flashloaders to work with non-default dummy cycle values. Feature: LinkServer debug solution is now installed by the MCUXpresso IDE installer as a separate tool and support files from the IDE that were LinkServer-specific are now part of the actual LinkServer package. The IDE implicitly uses the automatically installed LinkServer but a custom LinkServer can be configured using the Preferences page. A symbolic link to the installed LinkServer is also created inside the IDE layout (see <MCUXpressoIDE>/ide/LinkServer). Improvement: [IDE] Make Welcome page theme-aware and create content for dark theme.  Improvement: [IDE] Speed-up automatic generation of Makefiles. Improvement: [Windows installer] Disabled maximum path length limitation. Improvement: [Windows installer] Install J-Link USB drivers on Windows (starting with J-Link V7.92l installer, drivers are no longer installed by default) Improvement: [SDK Integration] Reduced GitHub SDK loading time when starting IDE. Improvement: [NPW/Manage SDK Components] Optimized component selection, minimizing time and eliminating freezes when selecting several components. Improvement: [NPW] Performance improvements when changing core selection. Fixed: [IDE] Too many identical confirmation windows appear if a required (by project) SDK is not installed. Fixed: [IDE] J-Link RAM debug sessions fail to set PC and SP correctly. Fixed: [IDE / Toolchain integration] The IDE automatically switches to using response files inside the generated linker command, for command lines exceeding 32K in length. Behavior is specific to Windows hosts, where there's a 32K length limit for a command line. Fixed: [IDE / Toolchain integration] Archiver ends with error when lots of object files are passed to the tool. IDE now passes object files through response files when command line exceeds 32K in length. Fixed: [SDK Integration] Recreating or uninstalling a GitHub SDK deletes the manifest file from the repository and breaks the SDK. Fixed: [NPW] Link section memory range used by secondary Multicore project specified during project creation is not reflected in final project settings. Fixed: [RT1180 B0] Semihosting PRINTF does not work properly with LinkServer when heap is located in cacheable memory. Fixed: [RT1180 B0] Connect script leaves DMA4 controller with error status indication.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
We are pleased to announce that MCUXpresso IDE v11.8.1 (build 1197) is now available.  This is a maintenance release that builds upon the previous MCUXpresso IDE v11.8.0 release and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built-in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.8.1 - October 2023 Upgraded: Newer SEGGER J-Link software (v7.92l). Upgraded: Newer PEmicro plugin (v5.7.3). Added: Support for i.MX RT1180 device and MIMXRT1180-EVK board. Added: Support for KE1xZ512 devices and X-FRDM-KE17Z512 board. Added: Support for MCXA153 device and FRDM-MCXA153 board. Improvement: [Toolchain Integration] Added C++20 and C++23 entries in the list of supported compiler dialects. Fixed: [Debugger][RW61x] Connect script does not halt after SYSRESET when secure project is in flash. Fixed: [Flash Programmer] Some problems related to flash blank command. Fixed: [SDK Integration] Device-specific preprocessor defines are not taken in consideration when changing device package.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.  
查看全文
We are pleased to announce that MCUXpresso IDE v11.7.1 (build 9221) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.7.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.7.1 - March 2023 Upgraded: Newer SEGGER J-Link software (v7.86e). Upgraded: Newer PEmicro plugin (v5.5.5). Upgraded: Version v13.1 of MCUXpresso Config Tools. Added support for LPC553x/S3x revision A1 device. Added support for LPC860 revision A1 device. Added support for KW45/K32W1 revision A2 device. Improvement: [SWO] Added preference for SWO ITM rxBuffer reading timeout in Preferences -> MCUXpresso IDE -> SWO Trace -> ITM_RxBuffer send timeout. This is intended to allow timeout increase in case user determines the application is not able to consume full amount of (so it will appear to lose) data sent by host debugger with the current timeout settings. Fixed: [Debug] Can't create a new launch configuration after using GUI Flash Tool on PEmicro. Fixed: [X-KW45B41Z-EVK][MCU-Link] Debug error reported when using MCU-Link firmware 3.x. Fixed: [Debug][PN7642] Update reset script to fix Restart behavior in the IDE (not fully performing reset on certain clocks / peripherals). Fixed: [Energy Measurement][Power Profile] Trigger configuration is visible for LPC-Link2 probes. Fixed: [SWO] Starting debug session with SWO counters or interrupts views opened results in error. Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
查看全文
We are pleased to announce that MCUXpresso IDE v11.7.0 (build 9198) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.6.1.   Installer Downloads To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation    Notification of future releases To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.7.0 - January 2023 Upgraded: Eclipse version to 2022.06 (Eclipse Platform 4.24.0 / CDT 10.7.0). Upgraded: MCUXpresso IDE integrated with JRE Eclipse Temurin (HotSpot engine, build 11.0.17+8). Upgraded: Windows 10/11 version 22H2 and macOS 13 (Ventura) support. Upgraded: Version v13 of MCUXpresso Config Tools. Upgraded: Synchronization with SDK v2.13.x. Upgraded: Newer SEGGER J-Link software (v7.84a). Upgraded: Newer PEmicro plugin (v5.4.1). Added MIMXRT1170-EVKB board support. Added K32W1, KW45, PN7642 devices support. Note. [KW45] Because ECC RAM is enabled by default, debug application in RAM might not work if the application image contains unaligned sections. In order to avoid this situation be sure at least one of the following rules is considered: - enable the ECC RAM initialization in the connect script (< layout >/ide/binaries/Scripts/KW45B41_connect.scp - see the comment from line 6). - use at least 4-byte aligned data structures/variables. Feature: [LinkServer] Support MCU-Link probes running V3.x firmware versions (based on CMSIS-DAP 2.1, using bulk/WinUSB endpoints). Feature: [Boot Configuration] Added Target Boot Control option (in LinkServer launch configuration) to configure device boot mode on the reset requests (issued during a debug session). This feature is only available on MCU-Link debug probe having ISPx boot control features implemented. See "Changing target boot configuration" section from User Guide. Feature: [Open-CMSIS-Pack] Added possibility to explore Open-CMSIS packs and import (middleware) components into an Eclipse project. Note that in the current version of the feature, component dependencies shall be manually added by users. A future version will automatically resolve dependencies and add them into the project: Set a path to work with Open-CMSIS Packs: Preferences ->  CMSIS-Packs -> CMSIS-pack root folder (you can let the existing  one as default) Load/Download/Import Packs: Perspective -> Open Perspective -> Other -> CMSIS-Pack Manager. From Packs view (toolbar) you can: Reload, Check for updates on Web, Import Packs from disc, etc. Once desired packs are available, you can add them into the Eclipse project by right-click on project entry in Project Explorer -> SDK Management -> Add components from Open-CMSIS-Pack and select the desired one from the "Add Open-CMSIS component to project" wizard. The component will be then available on Project Explorer view (the sources being linked to the original pack location), and also on Project Settings with details about its hierarchical path. Components can be deleted from project by selecting the component from Project Explorer -> < select project > -> Project Settings -> Open-CMSIS components, right-click on it, and choose "Delete Open-CMSIS component". Feature: [SDK Integration][SDK GitHub] Added support for paths relative to the manifest file inside the example projects. Feature: [Elf Importer] Import ELF binary/executable. This is available from File -> Import -> C/C++ -> MCUXpresso Executable Importer. Feature: [MQX RTOS] Support for MQX RTOS GDB thread awareness to allow multithread debugging. Note that Task Aware Debug (TAD) views in Eclipse will be added in a future IDE version. Feature: [SDK Integration][Complex dependencies] Support for < not > operator in the dependency conditions. Feature: [SDK Integration] Migrated to https://github.com/NXP-mcuxpresso/mcux-sdk new site. Feature: [SDK Integration] Provide CLI utility to merge sub-manifest files: added the manifest.merge command: Running the headless mode with -help manifest.merge generates a template property file, which contains the following: manifest.xml (location of the manifest containing references to sub-manifests). repo.location (repository where the manifest specified in the manifest.xml property is located). merged.manifest.xml (location of the result manifest file). All properties from the template file must be specified for the command to run. The manifest specified in the manifest.xml file must be inside the repository specified. Improvement: [NPW][NHS3xxx] Added NHS3xxx support on Preinstalled MCUs section. Improvement: [Flash Drivers] Various size optimization for flash drivers binaries. Improvement: [SDK Integration] Right Click on Installed SDKs pane provides new option to link with "Download and Install SDKs" feature. Improvement: [Energy Measurement / Power Profile] Display the currently configured measurement range for MCU-Link probes. Improvement: [SWO] Both trace clock and core clock are now exposed for user, for devices that have a TRACECLK different than the core clock (i.e. Cortex-M7). Improvement: [IDE][Quickstart Panel] Added preferences to control activation and auto-selection inside Project Explorer. Check these options on Preferences -> MCUXpresso IDE -> Quickstart Panel ->  Project Explorer activation and auto-selection of a project. Improvement: [IDE] Add watchpoint capability from the Peripheral (memory rendering) view. Improvement: [Power Profile] Add new configuration tab for data gathering controlled by trigger in Power profile. Power Profile and Energy Measurement views now both have the UI that allows collecting data based on a trigger; the two views do not share the configuration but they each hold their own user input. This configuration UI will be disabled if either Power profile or Energy Measurement is in play mode. Improvement: [Multicore] A post build step in an multicore environment is now calling a new utility tool (called mcux-fixelf) for multicore image processing purpose. The invoked command can be identified in Preferences -> MCUXpresso IDE -> Default tool settings -> Multicore slave template. This is intended for now to replace previous dd utility call plus some additional patches (like fixes for linker's forced relaxation on exidx/extab sections, shifting on secondary core's sections performed when linking full multicore image). Fixed: [RTOS] Add preferences to control persistence of RTOS TAD logs. Fixed: [Zephyr RTOS] When using J-Link and a Zephyr application built with CONFIG_INIT_STACKS=y, after opening the Zephyr TAD View, the view defaults to not showing the stack high water marks. Fixed: [FreeRTOS] "Tasks" and "Heap Usage" views throw errors after resume. Fixed: [FreeRTOS] Timer List view displays a Java exception instead of a user friendly error message. Fixed: [SWO] Silent error (in log) reported after using the SWO Data view and pressing the "Terminate" button. Fixed: [SWO] Continuous refreshing in SWO Config view when opening a debug session. Fixed: [SWO] After terminating a debug session, if one of the SWO views is left running, an error message will continuously appear in the error log. Fixed: [SWO] The timeline in SWO Interrupts View may be inaccurate for Cortex-M7 based devices. Fixed: [SWO][Power Profile] Missing some of the available rates for PC sampling. Fixed: [SWO] SWO not properly closed/disposed when the view is closed. This spoils the data collected when the view is reopened and a next SWO data collection session is started. Fixed: [SWO] "Unlock access" operation for CoreSight components configuration is missing from the "SWO and Trace console" log. Fixed: [SWO] NPE thrown in error log when debug session starts with SWO Data view opened. Fixed: [Power Profile][SWO Profile] Wrong initial values displayed for profile sample rates (0.0Hz). Fixed: [Energy Measurement] Previously used probe/debug context not displayed/kept after terminating session. Fixed: [Energy Measurement] Voltage "Read from target" fails if analog source is selected first. Fixed: [Energy Measurement] IDE crashes when Auto Scale button is pressed before doing any configuration. Fixed: [Energy Measurement] Unable to interact with the view (zoom in/out, export data) after terminating a running debug session while collecting analog data. Fixed: [Energy Measurement] Attaching to a debug session while data collection is in progress discards data already collected. Fixed: [Energy Measurement] Canceling an import archive will corrupt the already loaded plot. Fixed: [Energy Measurement] Wrong status message after changing to an out-of-debug probe while linked to debug context. Fixed: [Energy Measurement] t_last (the last time for the x-axis of the graph) label displays incorrect values when zooming in. Fixed: [Energy Measurement] Cannot re-export Energy Measurement data after import. Fixed: [Energy Measurement] "Horizontal Measurement" does not work properly. Fixed: [Install MCUXpresso SDKs] IDE filters now compatible SDKs versions. Note. The fix is working for IDE versions no older than MCUXpresso IDE 11.5.0. Fixed: [SDK Integration] Unexpected "Memory type EEPROM for project 'null' is not supported" error message displayed after a project is created. Fixed: [SDK Integration] On the "MCUXpresso IDE SDK uninstall" view, the buttons are no longer visible. Fixed: [SDK Integration] The component dependencies are not correctly solved in the case of switching cores when creating a new (multicore) project. Fixed: [SDK Integration] The generated linker script file name shall follow the project name. Fixed: [SDK Integration] Cannot find J-Link debugger script referenced in SDK (e.g. for RT1170 multicore projects). Fixed: [SDK Integration] Multiple SDKs are unexpectedly enabled / disabled if they share the same identifier (so pointing to the same device target). Note. The behavior after this fix is that for older workspaces, all the SDKs will be enabled. User will have to manually disable (or uninstall) undesired SDKs. Fixed: [SDK Integration] Missing source paths when adding components within SDK Component Manager view. Fixed: [SDK Integration][Ubuntu] Project names and descriptions are not displayed in the correct format on certain boards. Fixed: [SDK Component Management] Changed the handling of the "Cancel" button during "Refreshing SDK Components". If the user pressed "Cancel" to abort comparison, the file was silently not replaced and the update mechanism continued with the next file. Fixed: [NPW][SDK components selector] Board template cannot be deselected. Fixed: [NPW] Errors after creating a new project with the same name. Fixed: [Debugger][LPC541xx][PEmicro] Starting a multicore debug session, the secondary cores are not able to execute application (wrong suspended state is shown instead). Fixed: [Global Variables] The panning option in the graph is not enabled by default. Fixed: [Global Variables] View not loading globals from ELFs specified in Other Executables section of a debug config. Fixed: [Linker scripts] Some projects could produce axf files which fail to program in GUI Flash Tool. Fixed: [Multicore] Unexpected secondary core's data sections shifting in the final multicore application image. Fixed: [Multicore] Command line build in headless mode fails for multicore projects. Fixed: [Project Manager] Missing header files in Project Explorer when using linked sources. Fixed: [IDE][Probes discovered] The "OK" and "Cancel" buttons change location after a while or after clicking in different places. Fixed: [IDE] Creating "baremetal" project fails and gives internal error. Fixed: [IDE] NPE for Heap & Stack view with using make file project. Fixed: [IDE] Different syntax coloring when project sources are copied vs linked. Fixed: [IDE][PEmicro] IDE freezes while doing flash erase after a plain load image error encountered. Fixed: [Dark Theme] Project highlight in Project Explorer is white.   Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
查看全文
We are pleased to announce that MCUXpresso IDE v11.6.1 (build 8255) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.6.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.6.1 - October 2022 Upgraded: Newer SEGGER J-Link software (v7.70d). Upgraded: Version v12.1 of MCUXpresso Config Tools. Improvement: [Flash drivers] Included K32W041AM flash driver in layout examples. Fixed: [SWO][RT1170] SWO trace timing is not accurate when the trace clock is different from the core clock (e.g. for Cortex-M7 based devices). This misbehavior is visible in SWO Interrupts view. Fixed: [SWO][Counters] Cycle counter does not update while running and the Total value is wrong. Fixed: [NPW] Failed to create correct project for K22FX512 and SDK 2.3.1. Fixed: [NPW] Can’t use New Project wizard with two SDKs for the same board. Fixed: [NPW] SDK_DEBUGCONSOLE_UART option (which redirects the standard printf to UART) ignored when importing SDK examples. Fixed: [SDK Integration] Error thrown at build on FRDM-KL0Z from Import SDK example. Fixed: [Flash drivers] In provided /ide/Examples/Flashdrivers/NXP/iMXRT/iMXRT117x_FlexSPI_SFDP.zip, the octal flash RST control pin needs to be 0xOD (1.8V) instead 0x0A (3.3V). Fixed: [Project Manager] Missing Floating Point options for Cortex-M33 architecture. Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
查看全文