MCUXpresso IDE ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE Knowledge Base

ラベル

ディスカッション

ソート順:
We are pleased to announce that MCUXpresso IDE v11.5.1 (build 7266) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.5.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.5.1 - April 2022 Upgraded: CDT from CDT 10.3.0 to CDT 10.3.3. This is intended to address: https://bugs.eclipse.org/bugs/show_bug.cgi?id=575903 issue. Upgraded: Newer SEGGER J-Link software (v7.62c). Upgraded: Newer PEmicro plugin (v5.2.0). Added: [NPI] RT1060X (RT1060 phantom) support. Feature: [Flash Programmer][RT1160/RT117x] Add flash driver for QSPI on FlexSPI2 Port A. Fixed: [Debugger] Notifications about new MCU-Link firmware releases may not be shown in the Probes Discovery dialog. Fixed: [Debugger] Debug operations are slow while Peripherals+ window is open on targets with lots of registers (like RT1160 or RT117x). Fixed: [Project Manager][RT1160/RT117x] Flood of the -D__MULTICORE_MASTER in the .cproject. Fixed: [Project Manager][RT1160/RT117x] M7 C++ project failed to load the M4 project (in the case of multicore configuration) on a particular application. Now exdata sections are placed before heap and stack sections in generated linker files (when using Managed Linker Script configuration) compared with previous version where exdata sections were placed before data sections. Fixed: [Peripherals+][LPC546xx] EMC register location/offset is incorrect in Peripherals+ window. Fixed: [Energy Measurement] Instability if Energy Measurement view is used together with SWO Profile Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
記事全体を表示
We are pleased to announce that MCUXpresso IDE v11.5.0 (build 7232) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.4.1.   Installer Downloads To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation    Notification of future releases To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.5.0 - January 2022 Upgraded: Eclipse version to 2021.06 (Eclipse Platform 4.20.0 / CDT 10.3.0). Upgraded: MCUXpresso IDE integrated with OpenJDK11 (HotSpot engine build 11.0.11+9). Upgraded: GNU ARM Embedded Toolchain to version 10.3-2021.07. Upgraded: Version v11 of MCUXpresso Config Tools. Upgraded: Windows 11 and macOS 12.0.1 (Monterey) support. Upgraded: Newer SEGGER J-Link software (v7.60b, 64-bit version). Upgraded: Newer PEmicro plugin (v5.1.6). Synchronization with SDK v2.11.x and manifest schema version 3.9. Synchronization with FreeRTOS 10.4.3. Added: LPC55S36 support. Added: PN7640 support. Added: IMXRT685-AUD-EVK support. Feature: [FreeRTOS] Added Task Notifications view. Separate FreeRTOS view was added to display task notification list for each task, including status and value properties.      Feature: [SDK Integration] Integration with GitHub SDK repository: Support for installing a remote SDK GitHub repository. Support for installing an already cloned repository. Ability to contribute a project back to SDK GitHub repository.      Feature: [SVD] User can specify a custom SVD file location inside of a project. This can be achieved from Project Properties -> Run/Debug Settings -> MCU Settings -> SVD Selection. The file will be used by Peripherals+ view when debugging that project.      Feature: [Energy Measurement] Extensions and improvements: Data gathering enabled / disabled by trigger signal MCU-Link Pro and on-board probes with energy measurement circuitry can use a GPIO signal as a trigger/enable (input) for the energy measurement. Note. This feature requires firmware version MCU-LINK CMSIS-DAP v2.249 (or greater).                    Increase the maximum analog data collection time limit from 5 minutes previously to unlimited time, depending on the available space on disk. Note. Exported energy measurement session from an older MCUXpresso version is not compatible within MCUXpresso v11.5.0 version. Improve the performance of retrieving measurement data from the probe. This minimizes the chance of experiencing lost data packets which, in earlier versions, sometimes manifested as gaps (of few ms in length) in the data plot when sampling at high data rates. Even in the unlikely circumstances of still missing some measurement data packets, the IDE can now supplement the missing data by reconstructing it from a lower resolution version of the same data (averaged at probe level) to correct the energy/power calculation. When this situation arises the corresponding range on the plot is drawn as a compact area (due to lacking variation between samples normally present in the high resolution measurement data).      Feature: [SWO] Target configuration is now optional within SWO functionality. Depending on debug probe type, the user may choose not to automatically configure the target inside the "SWO Trace Config" view, so the user can then make his own registers configuration within the application. Feature: [SWO] A new console named "SWO and Trace Console" displays all configuration and register settings performed while configuring SWO. Feature: [Debugger][J-Link] Auto-debug secondary project(s) for multicore is now added for J-Link debug session too (now all debug connection types are offering this support). Option is set by default on: Window -> Preferences -> MCUXpresso IDE -> Debug Options -> J-Link Options -> Enable Auto-debug secondary project(s) for multicore projects. Feature: [Flash Programmer][RT1170] Add flash driver for the (non-default) Octal flash device on the EVK board. Feature: [IDE] The IDE does not internally use WMI command line utility anymore (deprecated as of Windows 10, version 21H1). PowerShell will be used instead. Fixed: [Project Manager] "Remove path from __FILE__" option not working for projects with linked sources (not copied into workspace). Fixed: [Project Manager] Project-relative connect and reset scripts do not work. Fixed: [Project Manager][LPC55S69] Changing RAM size from project properties results in build errors. Fixed: [Project Manager] "Restart" or "Terminate and Relaunch" are not enabled for custom made PEmicro launches. Fixed: [Energy Measurement] Unable to export data after terminating current analysis and cleaning up debug processes. Fixed: [Energy Measurement] Cancelling an import data operation is not working. Fixed: [Energy Measurement] Can't start a new measurement session if there is a measurement connection left active in another IDE instance. Fixed: [Debugger] Terminate button throws exception after the debug session using LinkServer. Fixed: [Debugger][CM33] `cmbreakset` doesn't work from redlinkserv console. Fixed: [Debugger][RT1160/RT1170] CPU doesn't halt on faults. Fixed: [Debugger][RT1160/RT1170] CM4 example does not reach main. Fixed: [Debugger][J-Link] Restart not working when debugging an application executing from SRAM (debugger not initializing program counter and stack pointer). Fixed: [Debugger][LinkServer] Debug connection uses excessive host CPU power. Fixed: [Debugger][LinkServer] SWD/JTAG pins are now disabled after terminating a LinkServer debug session. Fixed: [Debugger][LinkServer] Launch configurations referring absolute paths of ELF files are considered invalid. Fixed: [SDK Integration] Unable to select UART with single click when using "Import SDK example(s)" wizard. Fixed: [SDK Integration] [RT1170] Project building fails after adding SSARC driver. Fixed: [SDK Integration] Synchronize Semihost/UART option check with library type (semihost/nohost) selection. Note. This behavior applies to both GUI and CLI. Even if the example description specifies a default IO library type, this will be overwritten by the IDE if the chosen IO model is incompatible with it. Fixed: [SDK Integration] Build fails after removing SDK components that have additional libraries. Fixed: [Azure RTOS ThreadX] Threads view shows odd values for stack usage on all threads. Fixed: [SWO] Profiling counters view displays some wrong values. Fixed: [SWO] Profiling counters are created and accessed even when SWO not configured or available, causing memory access errors. Fixed: [SWO] Statistics (from SWO Trace Config view) indicates wrong information. Fixed: [SWO] IDE freezes for a period when detecting/setting SWO clock. Fixed: [SWO] ITM console does not work. Fixed: [Quick start panel] Copy-paste and multiple selection does not work for project properties. Fixed: [Peripherals+] Most of PWM registers are not shown. Fixed: [Dark Theme] Some of the view names inside SWO Views are not readable. Fixed: [IDE] Sometimes, ConcurrentModificationException exception message is seen when starting MCUXpressoIDE 11.4.1. Improvement: [IDE] Auto-resize columns from Probes Discovered dialog to accommodate length of displayed strings. Improvement: [IDE] Memory configuration editor dialog is now resizable. Fixed: [ImageInfo] Various features indicate files/information from the wrong project in the case of multiple projects having similar names within the workspace. Fixed: [ImageInfo] CallGraph indicates wrong (negative) stack usage value for the "Exception Handlers" virtual node. This field should be empty for virtual (non-existent) nodes. Fixed: [Global Variables] Sometimes the decimal number format displays empty values in the view. Fixed: [Installer][macOS] Re-installing the same MCUXIDE build version results in errors when launching the product. Fixed: [Installer] Uninstall sometimes fails when processes associated with current installation are open.   Known issues Please follow the KnownIssues.txt file from installation layout for a detailed list. Note. Additional issues that will be found post-release will be added in an online version also aiming to describe workarounds when available.
記事全体を表示
We are pleased to announce that MCUXpresso IDE v11.4.1 (build 6260) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.4.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.4.1 - September 2021 Upgraded: Newer SEGGER J-Link software (v7.54b, 32-bit version on Windows, 64-bit version on Linux/macOS). Upgraded: Newer PEmicro plugin (v5.1.0). Added: MCU-Link Pro probe support. Improvement: [SWO/Energy Measurement] Improved data collection rate. This aims to decrease the rate of lost packets (SWO) and gaps (Energy Measurement) at higher speed rates. Improvement: [LPC55xx] Add support in LinkServer flash drivers for programming data to the last flash sector (up to and excluding the reserved region). Fixed: [SWO] NPE obtained in the case of some SWO error types. This prevents the error dialogs to appear (the exceptions go silently). Fixed: [Energy Measurement] Detect data stream corruption and gracefully terminate Energy Measurement or SWO data retrieval if this situation arises. Fixed: [Energy Measurement] Sometimes stale data remains after clearing the data. Fixed: [Energy Measurement] No energy consumption info is displayed when measuring high (> 1W) power. Fixed: [Energy Measurement] No data is displayed after a while when measuring high currents. Fixed: [FreeRTOS TAD] Heap5 data not shown in Heap Usage view. Fixed: [Azure RTOS TAD] Azure RTOS debug session closes unexpectedly when using non-CM7 devices.
記事全体を表示
Important Note. Previously announced MCUXpresso IDE v11.4.0 build 6224 has been replaced by build 6237 to address a potential problem related to the Eclipse updater mechanism which under some circumstances could inadvertently update the Java Runtime Environment to a newer version (jre-15) which is incompatible with the IDE. When this problem arises the MCUXpresso IDE will no longer start. In the case you have previously installed MCUXpresso IDE build 6224, it is highly recommended to uninstall it and install build 6237 instead.   We are pleased to announce that MCUXpresso IDE v11.4.0 (build 6237) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.3.1.   Installer Downloads To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation    Notification of future releases To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.4.0 - July 2021 Upgraded: Eclipse version to 2020.12 (Eclipse Platform 4.18.0 /  CDT 10.1.0). Upgraded: IDE now integrates with OpenJDK11 (HotSpot engine,  v11.0.10). Upgraded: GNU ARM Embedded Toolchain to 10-2020-q4-major. Note that on top of GNU ARM Embedded Toolchain 10-2020-q4-major,  gcclib was recompiled using the bug fix from https://gcc.gnu.org/bugzilla/show_bug.cgi?id=99157. This patch prevents the run-time application corruption when using -mcmse support (applied for armv8m only). Upgraded: Version v10 of MCUXpresso Config Tools. Upgraded: Newer SEGGER J-Link software (v7.50, 32-bit version on Windows, 64-bit version on Linux/macOS). Note that v7.50 comes with a 64-bit version of Windows. This 64-bit version is compatible and can be used if desired, but please note that the MCUXpresso IDE 11.4.0 installation does not include this and only partial testing has been possible due to timing of the release. If you prefer to use the 64-bit version on Windows: Install 64-bit Windows SEGGER J-Link software Go to IDE -> Preferences -> MCUXpresso IDE -> Debug Options ->  J-Link Options -> J-Link Server executable and change it from the existing path to the 64-bit version installation path, i.e. for the default installation path:  C:\Program Files\SEGGER\JLink\JLinkGDBServerCL.exe Upgraded: Newer PEmicro plugin (v5.0.4). Upgraded: FreeRTOS TAD synchronization with FreeRTOS v10.4.3. Added: MKE1xZ support. Feature: [Azure RTOS ThreadX] Added GDB thread awareness. The user is able to see threads in Debug view (only when using all-stop debug mode, similar to FreeRTOS usage) and also the register context associated with the current selected thread. Feature: [Azure RTOS ThreadX] Added views, similar to the FreeRTOS, for: Thread list, Message queues, Semaphores, Mutexes, Event flags, Timers, Memory block pools, Memory byte pools. These views are available under a new menu group called "RTOS", where older FreeRTOS views can be also found. Feature: [Azure RTOS ThreadX] Added the ability to export trace data generated by the application at run-time. Decoding of exported data is done using Microsoft's Azure RTOS TraceX host-based analysis tool. Detailed procedure is described in the Azure RTOS User Guide. Feature: [Energy Measurement] Added measurement/plot capability for MCU-Link Pro and on-board probes. Power measurement can be done using: The new MCU-Link double channel measurement capability (simultaneously measured current and voltage); Existing capability (used over LPC-Link2 probes) of caching voltage measurement to use on power computation over current measurement. Feature: [Offline Peripherals] Added offline peripheral view. With this view, the peripheral registers can be inspected outside of a debug session. A device selector or the current project selection can be used to load register information for a particular device. Additionally, an SVD file can be imported. Feature: [Debugger][MCU-Link] Differentiation of MCU-Link product names used when MCU-Link probes enumerate on USB: Example: base model: MCU-LINK (r0FF) CMSIS-DAP V2.219 Pro model : MCU-LINK Pro (r0C7) CMSIS-DAP V2.219 on-board  : MCU-LINK on-board (r0CF) CMSIS-DAP V2.219 Feature: [Debugger][J-Link] Added possibility to connect to a remote gdb server. In launch configuration -> J-Link Debugger tab -> GDB Server Settings, use Server execution option to set a remote server. Improvement: [Debugger][J-Link] Add nickname for J-Link probes in Probes Discovered Dialog and in J-Link Debugger tab. Improvement: [Debugger][PEmicro] Added nickname for PEmicro probes in Probes Discovered Dialog. Feature: [SDK Integration] UART console is the default debug console when importing a project. Feature: [Flash Programmer] External flash drivers for i.MX RT500 and i.MX RT600 available as examples in <install_dir>/ide/Examples/Flashdrivers/NXP/iMXRT. Improvement: [Peripherals+] Peripherals+ view design was changed to support register group expansion directly into the Peripherals+ view, with no extra Memory View usage. Consequently, all elements shown before in Memory View are now available directly in the Peripherals+ view: values, bitfields, details. Reset value can be inspected as well together with the rest of the register elements. Improvement: [IDE] Added a link to MCU-Link firmware page in 'Additional resources' menu entry under Help's main menu. Improvement: [IDE] Toolbar naming and grouping: some icons re-grouped to reflect better categories and functionalities. Improvement: [SWO] Adapt SWO trace config error to better reflect possible causes. Improvement: [Flash Programmer] Use probe serial number instead of probe index when generating command line. Fixed: [Flash Programmer][Command Prompt] Wrong usage of double quotes in GUI Flash Tool Command Line generates errors in command prompt execution. Fixed: [Flash Programmer][J-Link][Command Prompt - Windows] GUI Flash Tool preview command - lower pane script not working when project name contains spaces. Fixed: [Flash Programmer] Cannot program flash from Quickstart Panel if "preview command" is checked in launch config. Fixed: [Flash Programmer] Wrong usage of double quotes in GUI Flash Tool Command Line. Fixed: [Debugger] Cannot relaunch (using "Terminate and Relaunch") a running session. Fixed: [Debugger] Suspend "bubble" project crashes debugger connection on LinkServer when using Non-Stop mode. Fixed: [Debugger] Debugger sets two breakpoints at the same address when debugging with J-Link. This generates a warning when trying to restart the debug session. Fixed: [Debugger] Always meet "Not Responding" issue when clicking the debug button without build first (for larger projects). Fixed: [Debugger] J-Link debug button does nothing when load image is set. Fixed: [Debugger] hello_world doesn't read the input from the console. Fixed: [Debugger] "Interrupt failed" pop-up error window during debug with FRDM-K64F and LPC-Link2 for some projects. Fixed: [Debugger] First attempt to manually modify the PC register is ignored. Fixed: [Debugger] Exceptions occurring while closing a project with an active debug session. Fixed: [Debugger] Restart not working in attach mode. Fixed: [Debugger][88MW320] Attach to a running target with PEmicro on FreeRTOS projects starts with faults. Fixed: [Debugger][88MW320] Cannot debug twice with J-Link and PEmicro. Fixed: [Debugger][FreeRTOS] Heap and Stack Usage View shall work with FreeRTOS enabled projects. Fixed: [Debugger] Multiple J-Link instances (named as "3rd party CMSIS-DAP") appear in Probes Discovered view: now these are filtered out. If a user still wants to see them, check the option from Preferences -> Debug Options -> J-Link Options -> Enable discovering of "3rd party CMSIS-DAP" probes. Fixed: [Debugger][J-Link] Master core in multicore context will be attached (instead a regular debug session) to target after debugging. Fixed: [Debugger][iMX RT595] Unable to flash application using crt_emu_cm_redlink raw command: Added preconnectscript argument to stub; Added --preconnectscript in the IDE's flash tool preview command window bottom; Note: Preconnect scripts have been changed to use variable a% instead of p% to receive the probe index. The user might need to update custom preconnect scripts. Fixed: [Energy Measurement] Format Y axis using a scale suitable for all displayed values (when having large Oy scale to represent data). Fixed: [Energy measurement] Unable to exit probe discovery for boards with unsupported firmware for SWO. Fixed: [Energy Measurement] The Energy measurement cannot collect if associated with a debug session and SWO is not initialized. Fixed: [Energy Measurement] Making a selection on the plot may lose part of the status line. Fixed: [Energy Measurement] Negative zero (-0.00) values shown. Fixed: [Energy Measurement] Lot of remaining allocated heap after clearing a plot. Fixed: [Energy Measurement] Incorrect representation of individual samples when the probe has been booted for some time: there are multiple values represented at the same point in time. Fixed: [Energy Measurement] Table containing analog sources not empty after terminating analysis session. Fixed: [Energy Measurement] When a view is already connected to a board and the underlying board is changed (without using the Terminate button), a subsequent operation will cause an error dialog with two entries and no useful information. View becomes unusable after this point. Fixed: [Energy Measurement] Export contains much more data than intended. Fixed: [Energy Measurement] Power/energy info in status line does not follow the currently visible part of the measurement. Fixed: [Energy Measurement] IDE now reports an error in the case the connection was interrupted while collecting power measurement data. Fixed: [Energy Measurement] Wrong resistor values displayed for QN9090 measurement circuit. Fixed: [Energy Measurement] Fixed 'None' in Tooltip for Cursor options in the Energy measurement toolbar. Fixed: [Energy Measurement] Export contains much more data than intended (from previous measurements). Fixed: [Energy Measurement] Old recorded values displayed on the graph. This makes a starting graph to look having unexpected data. Fixed: [Energy Measurement] Reading from target never finishes in some situations. Fixed: [Energy Measurement] Not all plotted values are using the same scale. This results into some values being displayed with wrong values. Fixed: [SWO][RT1010/RT1170/RT1160] Fixed SWO support for LinkServer. Fixed: [SWO] detecting clock feature is not overwriting the value. This is inducing some errors on enabling SWO features. Fixed: [SWO] Misleading error message when trying to enable SWO on sub-cores in a multicore environment. Fixed: [FreeRTOS] Sometimes cannot suspend FreeRTOS application using LinkServer. Fixed: [FreeRTOS] Modifying a register causes it to be set to 0. Fixed: [FreeRTOS] Attach to a FreeRTOS application returns faults. Fixed: [FreeRTOS] Empty tooltip for "Runtime" column from Tasks list view. Fixed: [FreeRTOS] Queue items incorrectly decoded in the Queues list view. Fixed: [FreeRTOS] No FreeRTOS queue data details shown. Fixed: [FreeRTOS] LinkServer FreeRTOS awareness does not activate in case of secure projects. Fixed: [FreeRTOS] GDB shuts-down when restarting RTOS debug session while stopped at BP. Fixed: [SDK Integration] The 'Open SDK handling preference page' button opens an unexpected option from Preferences. Fixed: [SDK Integration] SDK component replacement options is ignored. Fixed: [SDK Integration] It is not possible to disable "--sort-section=alignment" linker option from SDK generators. Fixed: [SDK Integration][SDK Details Page] Various NPE when using the details in Outline view. Fixed: [SDK Importer] Sometimes, board memory ranges are missing when importing an example project. Fixed: [SDK Importer] MCUXIDE mixes files from different versions of packages while importing examples. Fixed: [SDK Importer] All SDKs are present after clicking on the outside of SDKs image areas. Fixed: [SDK Importer] The linked example from Board SDK Wizard is not visible in Import SDK example Wizard. Fixed: [SDK Importer] Selected SDK, in the case of multiple SDKs using the same device, is not honored when importing or creating an example project. Fixed: [SDK Importer] SDK Import Wizard gives the wrong selection after it's opened and choose expand arrow. Fixed: [SDK Importer] CMSIS component with "type: CMSIS" is ignored when importing sdk project. Fixed: [SDK Importer] Boards vs device filter doesn't work when clicking in "Available boards" section but outside the board picture areas. Fixed: [SDK Importer] Non-multicore projects of boards with multicore support have master decorator when created. Fixed: [SDK Importer] Doc folder is declared as source folder in versions 2.9.x of the RT SDK. Fixed: [SDK Importer] SDK cannot set default launch config options for J-Link. Fixed: [SDK Importer] Fail to use an SDK with "/" included in the family name. Fixed: [SDK Importer] Project-specific linker file is ignored for MCUXIDE. Fixed: [SDK Importer] Default components are now displayed for a device project. Fixed: [SDK Importer] "Select SDKs for selected MCU" widget is not correctly populated when 2 SDK are installed for the same device. Fixed: [SDK CLI] project.build command exits with null pointer exception when use.all.components is set on true. Fixed: [SDK CLI] example.build command not working on multicore projects. Fixed: [SDK CLI] Command line will generate project name with not allowed character ("(", ")"). Fixed: [SDK CLI] Null pointer exception when using sdk.validate command. Fixed: [SDK CLI] Null pointer exception obtained when using -help argument. Fixed: [NPW] Creating a project using "Makefile Project using Existing Code" template, fails at debugging with LinkServer. Fixed: [NPW] Device project template is not correctly referred when using NPW to create a project with "selected device without board". Fixed: [NPW] Unable to create a project for the second board when 2 SDK for the same device are installed. Fixed: [Image Info] missing functions from CallGraph building in release build configuration. Fixed: [Image Info] CallGraph doesn't display stack info for c symbols located within cpp sources. Fixed: [IDE] Key binding conflict reported with new workspace. Fixed: [IDE] Tooltips missing for PEmicro Debugger Launch Configuration Startup Tab. Fixed: [Dark Theme] Usage in Heap and Stack Usage view. Fixed: [Dark Theme] pop-up hover not readable for longer preference text. Fixed: [Dark Theme] Selection is not visible in the Installed SDKs list. Fixed: [Dark Theme] MCUXpresso Icon in Smart Import Wizard shows white corners. Fixed: [Installer] Uninstaller error in the case of uninstall with a started eclipse session.   Known issues LPC55S16 TrustZone examples might not work with J-Link. Workaround: Use LPC-Link2 FW on on-board probes for TrustZone projects. SWO issues on iMX RT500 / iMX RT600 / LPC55xx when debugging with J-Link. Workaround: Choose other debugger probes for SWO usage on that particular list of devices. ITM console does not work as input console. Workaround: none, this will be fixed in a further release version. While installing the product, users may encounter a security alert from the operating system stating that some of the software comes from an unknown publisher. Workaround: If this happens it is safe to allow access. This will be corrected in a future release. In the case of an SDK component removal, the build process will fail if the component was also containing linked libraries. Workaround: Manually remove the libraries referenced by that component at project settings -> MCU Linker -> Libraries, then rebuild. 88MW320 with PEmicro and SDK version 2.9.5 or older: Debugging a project linked to flash with a PEmicro probe stops with faults at the start of the debug session. The target does reach main() if the execution is continued after the faults. Workaround: To remove the faults, enable "Launch Configuration -> Startup tab -> Set PC (absolute hex address or symbol)" and set it to "ResetISR". This workaround should not be used when attaching. "Open MCUXpresso SDK Builder" web link (from "Installed SDKs" view) is not correctly rendered within Eclipse's Internal Browser feature due to discontinued support for Internet Explorer for NXP web pages. Workaround: Go to Preferences -> General -> Web Browser and select "Use external web browser".
記事全体を表示
We are pleased to announce that MCUXpresso IDE v11.3.1 (build 5262) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.3.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.3.1 - April 2021 Upgraded: Newer SEGGER J-Link software (v6.98a). Upgraded: Newer PEmicro plugin (v4.9.1). Added: 88MW320 support. Added: K32W041A support. Added: i.MX RT1160 support. Feature: Added MCU-Link firmware version check in MCUXpresso IDE: When connecting to target, "Probes discovered" will indicate if there are debugger probes that would require update; Each discovered probe will clearly indicate (by a warning icon) if a firmware update is available; Tooltip on the mentioned probes will indicate the firmware's download location and its version. Fixed: [RT1170] Can't download image to RT1170-EVK when SRAM_ITC_cm7 is located as the first item in RAM blocks in Memory configuration editor. Fixed: [RT1170][CM4 boot] Error programming flash in SDP or empty flash situations. Fixed: [RT5xx/RT6xx] wrong image type (at offset 0x24) in generated executable file. Fixed: [KW38] Instruction Trace window does not pull the assembler instructions. Fixed: [K32W041AM] SWO Trace not working. Fixed: SDK cannot set default launch config options for Segger. Fixed: Exception if the IDE is launched right after installation process, having all checkboxes for additional documentation selected. Fixed: Welcome page not appearing at startup. Fixed: Program and Erase Flash shortcuts from Quickstart Panel are also launching an unexpected debug session on the end of their normal operation. Fixed: LinkServer: Modifying from debugger 8-bit or 16-bit data residing at addresses not aligned to 32 bits may alter data beyond the intended range up to the next 32-bit address.
記事全体を表示
We are pleased to announce that MCUXpresso IDE v11.3.0 (build 5222) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.2.1.   Installer Downloads To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation    Notification of future releases To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.3.0 - January 2021 Upgraded: Eclipse version to 2020.06 (Eclipse Platform 4.16.0 /  CDT9.11.1). Upgraded: IDE now integrates with OpenJDK8. Upgraded: GNU ARM Embedded Toolchain to GCC9-2020-q2-update. Integrated: GNU test coverage (gcov) and performance analysis (gprof) tools and Eclipse plugins. Upgraded: Version v9 of MCUXpresso Config Tools. Upgraded: Newer SEGGER J-Link software (v6.88c). Upgraded: Newer PEmicro plugin (v4.8.5). Added: i.MX RT1170 B0 support. Added: i.MX RT1024 support. Added: RT500 B2 support. Added: K32W061 support. Added: K32W041AM support. Added: LPC55S06 support. Added: MCU-Link probe debug support. Feature: Added Energy Measurement view, aiming to replace the Power Measurement view. Main capabilities: The new view comes with the same feature-set as the old Power Measurement view; From a GUI perspective, it offers consistent look & feel with other views that display and controls graphs (e.g. Global Variables, SWO-related views); Compatible with existing LPCXpresso boards having on-board power measurement circuits; Power and energy estimation capability: in order to enable power/energy measurement/estimation the user should add a reference voltage in the Config tab section from Energy Measurement view. For convenience and more precise measurement, the user can press "Read from target" which will automatically generate a reference voltage computed as an average value (of the voltage) measured for the last 500msec. Energy and power will be displayed in the status line of the plot area, showing the min/max/average power values and the energy value for the measurements visible in the graph, or over a particular time range selection. Multiprobe and multiview support: the feature is capable to open multiple views, each view can be connected to a different probe (that is capable to measure analog). The probe can be selected from Probe Discovery feature available in the Energy Measurement view toolbar. Data collecting during an out-of-debug session and also during an active debug session; Data collecting with an active debug session while the core is in debug mode. Behavior is controlled via toolbar buttons; Configuration of the server-side (rltool) and of the IDE using the Config tab within the view; Import/Export data functionality for offline analysis: (buttons on the Energy view toolbar). The user is able to save (Export data, in a zip format) the data collected within the view, having the possibility to load the saved data (Import data) later, in the same view or another one. Loading saved data in the Energy Measurement is not requiring physical connection to the target; Extended LPC-Link2 support for all targets having onboard measurement circuit: LPCXpresso546x8/540xx/54S0xx, LPCXpresso54102, LPCXpresso51U68/54114, QN90x0/JN518x/K32W0x1. As a side note, if there is any other LPC-Link2 board having power measurement capability, the user can use an existing configuration (and change the resistor value if necessary); See MCUXpresso_IDE_Energy_Measurement.pdf (or Help -> Help Contents) for details. Feature: Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose (for LinkServer debug connection only). That means, in the case of multicore projects on which primary project refers one or several secondary projects, debug sessions will be automatically started for secondary projects after initiating debug with the primary project. Option is set by default on: Window -> references -> MCUXpresso IDE -> Debug Options -> LinkServer Options -> Miscellaneous -> Enable Auto-debug slave project(s) for multicore projects. If you don't want to have this feature enabled (so if you want to start debug sessions for each core independently), uncheck this option. Similar, Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose for PEmicro too. Option is set by default on: Window -> Preferences -> MCUXpresso IDE -> Debug Options -> PEMicro Options -> Enable Auto-debug slave project(s) for multicore projects. Improvement: Enhance SWO views: SWO Config: added new Tab for data traffic statistics, configuration for ITM Stimulus ports; SWO Profile: added samples and details tabs; SWO Data: added plot (similar to Global Variables); SWO Stats: moved inside SWO Config; ITM Console: added one tab for each stimulus port. Improvement: [RT600] Clean up on RT600 flash drivers: Add drivers for MXIC_OPI connected via FlexSPI_A port; Add drivers for QSPI drivers (SFDP) connected via FlexSPI_B port; Add drivers for QSPI drivers (SFDP) connected via FlexSPI_A port; Remove MIMXRT600_SFDP_* drivers generated by the old project (SDK now references the new drivers). Improvement: Drop-down boxes from several tables require two user operations for reaching the actual items from the list. Reduced now to a single operation (single click). Improvement: Extend CLI functionality - Add new command to list SDK info:   -filter=<string> : filters the available information based on regex expression string. e.g. -filter=K64 will display all data containing K64 string. See SDK command line documentation within the layout (MCUXpresso_SDK_Command_Line_User_Guide.pdf). Improvement: Merge c_include path section into cpp_include path section for cpp project in project settings. Improvement: New project wizard is now capable to handle HW with dual primary/secondary roles (i.e. RT1170). From SDK Wizard page, any core can be selected according with the secondary/primary SDK description, plus it can be selected as standalone (application). Improvement: Community forum accessible now from the main toolbar too (together with the older link from Help->MCUXpresso IDE support forum). The default selection will open the community web inside the IDE. If you want to set the default browser as external browser, use Window->Preferences->General->Web browser->"Use external web browser". Fixed: [RT500] QSPI flash drivers: driver was incorrectly using QSPI DDR instead of SDR. Fixed: [RT500][RT600] J-Link launch config default resets: Re-enable resets in J-Link launches for RT500/RT600 The most recent J-Link versions properly handle resets for RT500 & RT600 devices. Fixed: [RT500] Unable to Restart flash-based session on EVK RevC1 board. Fixed: [RT685] "Unsupported or unrecognized format error" dialog when using the installed SDK. Fixed: [LPC55S69] Implemented DWT (Data Watchpoint and Trace) component for ArmV8. This fixes the SWO Data trace not working issue. Fixed: [LPC55S06] SWO support. Fixed: [LPC55xx] LinkServer debug cannot recover LPC55xx from deep sleep. Fixed: [LPC845] Debug fails when SRAM is split into sub-blocks. Fixed: [LPC4337] Flash programming over JTAG not working on the M4 core. Fixed: [LPC54114] SWO Trace is not working with PEmicro. Fixed: [FRDM-K64] Removed unexpected warning reported in map file in a project. Fixed: [JN5189/QN9090/KW32W041AM] Improve OOB experience with (factory) erased devices. Fixed: IDE 'Utility' menu does not work for linked Folders. Fixed: Defined symbols are added prematurely (even when no component is selected in NPW). Fixed: Selection of a driver in NPW makes the Library Type and Floating Type to become empty. Fixed: "ERROR: fatal error: board.h: No such file or directory" error reported if build a new created project with no board support. Fixed: Library type is not changing correctly when using SDK Wizard. Fixed: SDKs for older LPCs failing to set CRP up correctly. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Issues when uninstalling a SDK plugin. Now "Installed SDKs" and "Install MCUXpresso SDK" views are in sync and report the right installation status of a SDK. Fixed: On explicit include paths in the project setting, the include paths are mixed between asm and c type. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Null pointer exception on generating example xml. Fixed: Build error when use MCUXpresso IDE command line with non-existing include. Fixed: SDK command line: pre and/or post build steps options not available in example.xml file. Fixed: J-Link scripts needed by SDK examples are not copied correctly when installing the SDK from a folder. Fixed: MCUXpresso linked projects compile errors on multicore platforms. Fixed: Compile errors reported on a project imported from a generate example.xml. Also fixed the CLI build failing on the same example.xml scenario. Fixed: Unexpected memory usage reported (over 100% occupied memory) by Image Info. Fixed: Programming empty pages for ERASE_WO devices when flash hashing is enabled. Fixed: 'debug interface type' identification shown in the "Debug messages" console. Fixed: "Terminate" operation does not kill the redlinkserv.exe process. Fixed: "Terminate" button appears disabled after the first "Suspend" for PEMicro and J-Link debug connection. Fixed: J-Link auto selection results in not working connection. Fixed: Flash programming using J-Link via JTAG. Fixed: The running environment (PC/SP) for RAM applications is now properly initialized by the debugger when using J-Link/PEmicro. Fixed: Debugger Console output stops working when debugging secure project. Fixed: Error reported when SWO clock speed dialogue cancelled. Fixed: FreeRTOS tasks list not populated correctly in some situations. Fixed: SVD viewer shows-up with empty peripherals list. Fixed: Live Variables: Unable to create expression with casts. Fixed: Global Variables: T0 will remain -0 while moving the Graph to the right. Fixed: [Dark Theme] highlighting makes text unreadable. Fixed: [Dark Theme] Text is not visible for Blocked jobs in FreeRTOS. Fixed: [Dark Theme] Peripherals view - some registers have yellow background making it hard to read. Fixed: [Dark Theme] Line highlighting in editor makes variables text unreadable. Fixed: [Dark Theme] Display issue for the "Probes discovered" window on Mac. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: [Dark Theme] Manage SDK Components window is not updated. Fixed: [Dark Theme] Various improvements on Disassembly, Memory, Peripherals, headers in views, editor, git plugin. Fixed: [Dark Theme] Install plugin SDKs window shows white rectangles around icons. Fixed: [Dark Theme] Line number background is too bright. Fixed: [Dark Theme] Install MCUXpresso SDK view shows white background while selecting table headers.
記事全体を表示
  We are pleased to announce that MCUXpresso IDE v11.2.1 (build 4149) is now available. This is a maintenance release that builds upon the previous MCUXpresso IDE v11.2.0 release, and we recommend that all existing users download and install this new version.   Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory or downloaded from: https://www.nxp.com/mcuxpresso/ide/documentation   Notification of future releases  To receive notifications about future releases, please follow : MCUXpresso IDE - Release History    Summary of Changes - version 11.2.1 - October 2020 Upgraded: newer SEGGER J-Link software (v6.86). Upgraded: newer PEmicro plugin (v4.7.6). Upgraded: Version v8.1 of MCUXpresso Config Tools. Added: i.MX RT1170 B0 support. Added: i.MX RT1024 support. Added: LPC55S06 support. Added: K32W061 support. Added: MCU-Link debug probe support. MCU-Link is a new debug probe solution being developed for NXP LPC, Kinetis and i.MX RT targets. Feature: Auto-debug slave project(s) for multicore projects option becomes default option for multicore debug purpose (for LinkServer debug connection only). That means, in the case of multicore projects on which master project refers one or several slave projects, debug sessions will be automatically started for slave projects after initiating debug with the master project. Option is set by default on: Window -> Preferences -> MCUXpresso IDE -> Debug Options -> LinkServer Options -> Miscellaneous -> Enable Auto-debug slave project(s) for multicore projects. If you don't want to have this feature enabled (so if you want to start debug sessions for each core independently), uncheck this option. Improvement: Community forum accessible now from the main toolbar too (together with the older link from Help->MCUXpresso IDE support forum). The default selection will open the community web inside the IDE. If you want to set the default browser as external browser, use Window->Preferences->General->Web browser->"Use external web browser". Improvement: [RT600] Clean up on RT600 flash drivers (SDK now references the new drivers): Add drivers for MXIC_OPI connected via FlexSPI_A port Add drivers for QSPI drivers (SFDP) connected via FlexSPI_B port Add drivers for QSPI drivers (SFDP) connected via FlexSPI_A port Remove MIMXRT600_SFDP_* drivers generated by the old project Fixed: [RT595] Cannot debug flash application with J-Link. Fixed: [RT500][RT600] JLink launch config default resets: Re-enable resets in JLink launches for RT500/RT600 The most recent JLink versions properly handle resets for RT500 & RT600 devices. Fixed: [RT500] QSPI flash drivers: driver was incorrectly using QSPI DDR instead of SDR. Fixed: [LPC55S69] Implemented DWT (Data Watchpoint and Trace) component for ArmV8. This fixes the SWO Data trace not working issue. Fixed: Sometimes the linkserver semihosting console stops working. Fixed: 'mismatched input' warning reported for linker file. Fixed: Flash programming using JLink via JTAG. Fixed: The running environment (PC/SP) for RAM applications is now properly initialized by the debugger when using JLink/PEmicro. Fixed: JLink scripts needed by SDK examples are not copied correctly when installing the SDK from a folder. Fixed: Selection of a driver in NPW makes the Library Type and Floating Type to become empty. Fixed: [Dark Theme] highlighting makes text unreadable. Fixed: [Dark Theme] not working on Ubuntu 18. Fixed: [Dark Theme] Text is not visible for Blocked jobs in FreeRTOS. Fixed: [Dark Theme] Peripherals view - some registers have yellow background making it hard to read. Fixed: [Dark Theme] Line highlighting in editor makes variables text unreadable. Fixed: [Dark Theme] Display issue for the "Probes discovered" window on Mac. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: [RT5xx] Unable to Restart flash-based session on EVK Rev C1 board. Fixed: [LPC55xx] LinkServer debug cannot recover LPC55xx from deep sleep. Fixed: [LPC4337] Flash programming over JTAG not working on the M4 core. Fixed: [LPC845] Debug fails when SRAM is split into sub-blocks. Fixed: [Dark Theme] Low contrast on text vs. background when a word is high-lighted by having cursor selection on it. Fixed: Outline view displays empty table header when selecting an SDK. Fixed: Not all dependency components are linked to project when the dependency is added from Config Tools. Fixed: Initialize execution environment when debugging RAM target application using Segger J-Link. Fixed: NPE occurred while using board SDK creator and adding a flash driver.
記事全体を表示
This video shows how to create, build and debug a new SDK project with MCUXpresso IDE. Enjoy!
記事全体を表示
This video shows how to import any of the SDK example projects and use it as a starting point for you own project. Enjoy!
記事全体を表示
The MCUXpresso IDE has a versatile way to create different binary files (S-Record/S19, Intel Hex or raw Binary) which then can be used by other tools like flash programmer or bootloaders. Check out the IDE documentation (menu Help > MCUXpresso IDE User Guide): where you can search for any topics like this: See as well the following article (external link) on that subject: MCUXpresso IDE: S-Record, Intel Hex and Binary Files | MCU on Eclipse  Enjoy!
記事全体を表示
Attached MCUXpresso IDE fact sheet gives an overview about the IDE and its capabilities. More information is available on MCUXpresso IDE|NXP .
記事全体を表示
This document contains a history of the releases of MCUXpresso IDE, with links to the announcement blog for each release.   Receive email notification for new releases If you would like to receive notifications when a new version of MCUXpresso IDE is released, please make sure to follow this document.   Release History   June 2025 MCUXpresso IDE v25.06 December 2024 MCUXpresso IDE v24.12 September 2024 MCUXpresso IDE v24.9 July 2024 MCUXpresso IDE v11.10.0 April 2024 MCUXpresso IDE v11.9.1 January 2024 MCUXpresso IDE v11.9.0 October 2023 MCUXpresso IDE v11.8.1 August 2023 MCUXpresso IDE v11.8.0  March 2023 MCUXpresso IDE v11.7.1  January 2023 MCUXpresso IDE v11.7.0  October 2022 MCUXpresso IDE v11.6.1  July 2022 MCUXpresso IDE v11.6.0  April 2022 MCUXpresso IDE v11.5.1  January 2022 MCUXpresso IDE v11.5.0  September 2021 MCUXpresso IDE v11.4.1  August 2021 MCUXpresso IDE v11.4.0 b6224 replaced by b6237 to fix an eclipse updater issue. July 2021 MCUXpresso IDE v11.4.0  April 2021 MCUXpresso IDE v11.3.1  January 2021 MCUXpresso IDE v11.3.0  October 2020 MCUXpresso IDE v11.2.1  July 2020 MCUXpresso IDE v11.2.0   March 2020 MCUXpresso IDE v11.1.1  December 2019 MCUXpresso IDE v11.1.0  MCUXpresso IDE v11.1.0 SDK Handling Hotfix (January 2020) September 2019 MCUXpresso IDE v11.0.1 MCUXpresso IDE v11.0.1 Segger-LPC Debug Hotfix (September 2019) MCUXpresso IDE v11.0.1 LPC55xx Debug Hotfix (October 2019) June 2019 MCUXpresso IDE v11.0.0 February 2019 MCUXpresso IDE v10.3.1 December 2018 MCUXpresso IDE v10.3.0 July 2018 MCUXpresso IDE v10.2.1 May 2018 MCUXpresso IDE v10.2.0 January 2018 MCUXpresso IDE v10.1.1 November 2017 MCUXpresso IDE v10.1.0 July 2017 MCUXpresso IDE v10.0.2 March 2017 MCUXpresso IDE v10.0.0
記事全体を表示
Checking disassemble code is often needed for programmers when developing a project. This article will introduce two methods of generating disassemble file with GNU utility objdump under MCUXpresso IDE 10.1.0. If user needs demo code, please send me community internal message.
記事全体を表示
[中文翻译版] 见附件 原文链接: https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2019/06/12/using-lpc55s69-sdk-trustzone-examples-with-mcuxpresso-ide-v1100
記事全体を表示
As part of my university engagement, I have posted an overview article about the new MCUXpresso IDE: (external link): MCUXPresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse  I hope you find it useful, Erich
記事全体を表示
This exercise demonstrates how to port a project using MCUXpresso IDE and SDK from one RT MCU to another.  The exercise starts with an SDK demo project for the MIMXRT1060-EVK board, and ports to the IMXRT1050-EVKB board.   The "MCUXpresso IDE User Guide" installed with the IDE gives this warning: changing a project’s associated MCU should not be undertaken unless you have a total grasp of the consequence of this change.  Therefore rather than changing a project’s associated MCU, it is strongly recommended that instead a new project is generated for the desired MCU and this new project is edited as required.  However, on occasion it may be expedient to reset a project’s MCU (and associated SDK)   I also recommend using a SDK project intended for the final MCU, and just port the application source files to it.  But here are the steps to port the project.  Also note, these two boards use different flash types by default.  In this example, the IMXRT1050-EVKB was reworked to use the QSPI flash on the board following Appnote AN12108.  Once the RT1050 EVK is modified to use the QSPI flash, it is the same flash used on the RT1060 EVK.   Resources used in this exercise: IMXRT1050-EVKB board RevA1 MIMXRT1060-EVK board RevA2 MCUXpresso IDE v11.2.0 MCUXpresso SDK from Welcome | MCUXpresso SDK Builder  EVKB-IMXRT1050_SDK_2.8.2 EVK-MIMXRT1060_SDK_2.8.2   Attached to this post are two projects: Starting_evkmimxrt1060_iled_blinky.zip was the original SDK example running on the RT1060 EVK evkbmimxrt1050_iled_blinky_ported.zip is the final ported project, running from QSPI and RT1050     Following the "MCUXpresso IDE User Guide" section "Changing the MCU (and associated SDK)", changed the MCU to MIMXRT1052xxxxB.  Also changed the flash driver to MIMXRT1050_SFDP_QSPI.cfx.  If using Segger JLink, see https://wiki.segger.com/i.MXRT1050 to change the flash algorithm to QSPI.   And then changed the package/part number to MIMXRT1052DVL6B.   Changed the project name to evkbmimxrt1050_iled_blinky_ported Changed the C Compiler Preprocessor definitions to the SDK device CPU_MIMXRT1052DVL6B   Replaced the files from the SDK package EVKB-IMXRT1050_SDK_2.8.2 (Note: MCUXpresso IDE supports "SDK Project Component Management", which could also be used for updating some of these files.  See section "SDK Project Component Management" of the IDE user guide.  But I replaced the files manually myself from the RT1050 SDK package): device folder with the SDK files from EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052.  startup file from \EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052\mcuxpresso\ drivers files from \EVKB-IMXRT1050_SDK_2.8.2.zip\devices\MIMXRT1052\drivers\ board files, can use an SDK example for the ported device, or generate the clock_config and pin_mux files from the MCUXpresso Config tools xip files would also need to be updated if flash configuration changes.  In this example, both boards are using the same QSPI flash, and these files are the same.   Delete the .launch debug configuration file in the project.  MCUXpresso IDE will regenerate it.   With these changes, the ported project runs on the RT1050 EVK.
記事全体を表示
This tip will show you how to re-trigger a full probe discovery.  The feature is very useful for the customer who may use multiple debug probes. The first time you debug a project, MCUXpresso IDE will perform a probe discovery operation and display the discovered Debug Probes for selection. This will show all Supported Probes that are attached to your computer. (Here you can see the default P&E Micro OpenSDA of FRDM-KL25Z board was found.) For any future debug sessions, the stored probe selection will be automatically used to match the project being debugged with the previously used debug probe. This greatly simplifies the case where multiple debug probes are being used. However, if a debug operation is performed and the previously remembered debug probe cannot be found, then a debug probe discovery operation will be performed from within the same family e.g. MCUXpresso IDE LinkServer, P&E Micro or SEGGER J-Link. (Here you can see there are two Probe search options: Search for PEMicroDBB97E74 again and Search for other attached PE Micro probes.) But if you want to use a different debug probe(for example: debug FRDM-KL25Z board with SEGGER JLink), click this blue debug icon will meet problem. Supported Probes dialog only show P&E Micro probes, it will not search other family of debug probes e.g. MCUXpresso IDE LinkServer or SEGGER J-Link.   Once a launch configuration file has been created, it will be used for the projects future debug operations. If you wish to use the project with a different debug probe, then simply delete the existing launch configuration and allow a new one to be automatically used on the next debug operation. Now click blue debug icon re-trigger a full probe discovery, and it show all Supported Probes that are attached to your computer again.
記事全体を表示
MCUXpresso SDK packages are downloaded as .zip files. If you are using a 3 rd party IDE such as IAR or Keil, then the package must be unzipped in order to access the project files. Also an unzipped SDK folder must be available for the MCUXpresso Config Tools. This is why the default recommendation is to go ahead and unzip a downloaded SDK package.   However if using MCUXpresso IDE, then either the zipped or unzipped SDK can be imported into the MCUXpresso IDE. A zipped SDK will save disk space and can be imported into the IDE more quickly than an unzipped SDK folder. MCUXpresso’s IDE part support is extended by importing MCUXpresso SDKs into the IDE, so this can save some time if you need to add a new device. Also note that your SDK package must support MCUXpresso, and thus must have been recently created in the SDK Builder (after March 24th) with explicit support for MCUXpresso in the package, else you will get an error when trying to import it.  When an MCUXpresso SDK zip package or folder is drag-and-dropped into the IDE, a copy of that zip/folder is made and put into the C:\Users\<user_name>\mcuxpresso\SDKPackages directory. Thus you can delete the original copy that was downloaded to save disk space.     If the imported SDK was zipped, then when creating or importing example projects, the SDK source files are always copied into the workspace. If the imported SDK was unzipped, then you are given the option to either copy the SDK source files into the workspace (which is the default), or the SDK files can be referenced directly as linked references.   If an SDK is imported as a zipped file, it can be later unzipped from inside the MCUXpresso IDE. This unzipping has been optimized so it’s much faster than unzipping it via a program like WinZip. When unzipping inside the MCUXpresso IDE, the zip file that was in the MCUXpresso SDKPackages folder will automatically be deleted from the hard drive once its finished unzipping. You can then use this unzipped folder for that SDK location when using the MCUXpresso Config tools.       You can also add MCUXpresso SDKs by placing an SDK package (zipped or unzipped) into that default SDKPackages directory (C:\Users\<user_name>\mcuxpresso\SDKPackage) and restarting the MCUXpresso IDE.    Finally you can also specify additional directories that MCUXpresso IDE should search for SDK files (both zipped or unzipped) by going to Window -> Preferences -> MCUXpresso IDE -> SDK Options. This can be useful for keeping a repository of SDKs in a special location on your hard drive. For SDKs stored outside the default location though, the "Delete SDK" function is disabled inside the IDE, and the extra search paths are only saved per workspace, so if you choose another workspace, it won't know about the new SDK folders until you re-add the path. If multiple SDKs are found for the same device in different locations, the IDE select the package to use by priority on the list (top has priority).    More detailed information on pre-installed part support and importing SDKs can be found in Section 4 of the MCUXpresso IDE User's Guide, as well as in this informative training video. 
記事全体を表示