Layerscape ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape Knowledge Base

ディスカッション

ソート順:
In the U-Boot log, the names of the Ethernet interfaces are printed in the format <name>@<interface type>, for example, DPMAC2@xgmii. DPMAC is a DPAA2 object that identifies the physical interface.  For Linux, in TinyDistro as well as in Ubuntu distribution, by default, only one MAC is enabled as a standard Kernel Ethernet Interface. This interface is named eth0 by default (or eth1 if PCI Express network interface card is discovered first). For details regarding creation of a DPAA2 network interface (DPNI) in Linux, refer to LS1088ARDB/LS1088ARDB-PB - How to create a DPAA2 network interface (DPNI) in Linux The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LS1088ARDB.  Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro and Ubuntu userland) Description ETH0 DPMAC2@xgmii not enabled by default XFI optical interface ETH1 DPMAC1@xgmii not enabled by default XFI copper interface ETH2 DPMAC7@qsgmii  not enabled by default QSGMII copper interface ETH3 DPMAC8@qsgmii  not enabled by default QSGMII copper interface ETH4 DPMAC9@qsgmii  not enabled by default QSGMII copper interface ETH5 DPMAC10@qsgmii  not enabled by default QSGMII copper interface ETH6 DPMAC3@qsgmii  not enabled by default QSGMII copper interface ETH7 DPMAC4@qsgmii  not enabled by default QSGMII copper interface ETH8 DPMAC5@qsgmii  eth0 by default (or eth1 if PCI Express network interface card is discovered first) QSGMII copper interface ETH9 DPMAC6@qsgmii  not enabled by default QSGMII copper interface The table below shows the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux for LS1088ARDB-PB. Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro and Ubuntu userland) Description DPMAC1 DPMAC1@xgmii not enabled by default XFI optical interface DPMAC2 DPMAC2@xgmii not enabled by default XFI copper interface DPMAC3 DPMAC3@qsgmii not enabled by default QSGMII copper interface DPMAC4 DPMAC4@qsgmii not enabled by default QSGMII copper interface DPMAC5 DPMAC5@qsgmii eth0 by default (or eth1 if PCI Express network interface card is discovered first) QSGMII copper interface DPMAC6 DPMAC6@qsgmii not enabled by default QSGMII copper interface DPMAC7 DPMAC7@qsgmii not enabled by default QSGMII copper interface DPMAC8 DPMAC8@qsgmii not enabled by default QSGMII copper interface DPMAC9 DPMAC9@qsgmii not enabled by default QSGMII copper interface DPMAC10 DPMAC10@qsgmii not enabled by default QSGMII copper interface
記事全体を表示
Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-19.06-V4.14 LSDK-19.06-V4.14 where LSDK-19.06-V4.14 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to the device tree, open and edit arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-ls1043a-rdb.dtb is in arch/arm64/boot/dts/freescale/. Copying the compiled kernel images and device tree to the SD card Plug the SD card into the Linux host machine. Mount the SD card partition that contains Linux kernel images and device tree. sudo mkdir <mount_location> sudo mount /dev/sdX <mount_location> Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0. Replace Image, Image.gz, and fsl-ls1043a-rdb.dtb on the SD card with the new files compiled in the steps above. sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-ls1043a-rdb.dtb <mount_location> sudo umount /dev/sdX Plug the SD card into LS1043ARDB and boot the board to Ubuntu using the SD card.  If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card. You can confirm that Linux kernel and device tree is updated on the SD card by running this command and checking the timestamp. root@localhost:~# uname -a Linux localhost 4.14.104 #2 SMP PREEMPT Wed Aug 21 17:14:01 IST 2019 aarch64 aarch64 aarch64 GNU/Linux
記事全体を表示
Please note that the LSDK memory layout for TF-A boot flow explained in this topic is only applicable for LSDK 18.12 and newer releases.  The following table shows the memory layout of various firmware stored in NOR/NAND/QSPI flash device or SD card on all QorIQ Reference Design Boards. When the board boots from NOR flash, the NOR bank from which the board boots is considered as the "current bank" and the other bank is considered as the "alternate bank". For example, if LS1043ARDB boots from NOR bank 4, to update an image on NOR bank 0, you need to use the "alternate bank" address range,0x64000000 - 0x64F00000. Firmware Definition MaxSize Flash Offset (QSPI/NAND flash) Absolute address (NOR bank 0 on LS1043ARDB, LS1021ATWR) Absolute address  (NOR bank 4 LS1043ARDB, LS1021ATWR) Absolute address (NOR bank 0 on LS2088ARDB) Absolute address (NOR bank 4 on LS2088ARDB) SD Start Block No. RCW + PBI + BL2 (bl2.pbl) 1 MiB 0x00000000 0x60000000 0x64000000 0x580000000 0x584000000 0x00008 ATF FIP Image (fip.bin) BL31 + BL32 + BL33 4 MiB 0x00100000 0x60100000 0x64100000 0x580100000 0x584100000 0x00800 Boot firmware environment 1 MiB 0x00500000 0x60500000 0x64500000 0x580500000 0x584500000 0x02800 Secure boot headers 2 MiB 0x00600000 0x60600000 0x64600000 0x580600000 0x584600000 0x03000 Secure header or DDR PHY FW 512 KiB 0x00800000 0x60800000 0x64800000 0x580800000 0x584800000 0x04000 Fuse provisioning header 512 KiB 0x00880000 0x60880000 0x64880000 0x580880000 0x584880000 0x04400 DPAA1 FMAN ucode 256 KiB 0x00900000 0x60900000 0x64900000 0x580900000 0x584900000 0x04800 QE/uQE firmware 256 KiB 0x00940000 0x60940000 0x64940000 0x580940000 0x584940000 0x04A00 Ethernet PHY firmware 256 KiB 0x00980000 0x60980000 0x64980000 0x580980000 0x584980000 0x04C00 Script for flashing image 256 KiB 0x009C0000 0x609C0000 0x649C0000 0x5809C0000 0x5849C0000 0x04E00 DPAA2-MC or PFE firmware 3 MiB 0x00A00000 0x60A00000 0x64A00000 0x580A00000 0x584A00000 0x05000 DPAA2 DPL 1 MiB 0x00D00000 0x60D00000 0x64D00000 0x580D00000 0x584D00000 0x06800 DPAA2 DPC 1 MiB 0x00E00000 0x60E00000 0x64E00000 0x580E00000 0x584E00000 0x07000 Device tree(needed by uefi) 1 MiB 0x00F00000 0x60F00000 0x64F00000 0x580F00000 0x584F00000 0x07800 Kernel lsdk_linux.itb 16 MiB 0x01000000 NA NA NA NA 0x08000 Ramdisk rfs 32 MiB 0x02000000 NA NA NA NA 0x10000 The following figures highlight the changes in the flash layout for previous boot flow (with PPA) and flash layout for TF-A boot flow. Flash layout for previous boot flow (with PPA)   Changed flash layout for TF-A boot flow
記事全体を表示
The attached patch is to support DDR3L in LS1043A. The SDK version is Linux-LS1043A-SDK-V0.5-SOURCE-20151223-yocto.iso. Not SDK2.0. The DDR3L part number is two Winbond W632GU6KB(16M x 8 banks x 16 bits DDR3L SDRAM).
記事全体を表示
This document introduces a method to separate control plane and data plane between GPP(ARM) and AIOP based on different L4 protocols implemented in the AIOP software. So far, in the current MC version, this scenario could not be implemented from WRIOP using DPDMUX, so it is a good choice for users to separate the traffic in AIOP.   1. Basic Concept of DPAA2 Objects   2. AIOP Application to Implement Control in ARM and Data Plane in AIOP   3. Build AIOP Application Project with CodeWarrior   4. Running AIOP Application Program on LS2085ARDB
記事全体を表示
Currently rate limiting is supported on TX side only via IOCTL call FM_PORT_IOC_SET_RATE_LIMIT. A user-space application has to be implement which opens the character driver interface of the TX port and issue the IOCTL. The rate_limit structure (mentioned below) has to be filled to implement the restriction.   For example:   fd = open ("/dev/fm0_port_tx5", O_RDWR);   err = ioctl(fd, FM_PORT_IOC_SET_RATE_LIMIT, &fm_port);   Structure to pass to the IOCTL: /**************************************************************************//** @Description@@   A structure for defining Tx rate limiting (Must match struct t_FmPortRateLimit defined in fm_port_ext.h) *//***************************************************************************/ typedef struct ioc_fm_port_rate_limit_t { uint16_t max_burst_size;         /**< in KBytes for Tx ports, in frames for offline parsing ports. (note that for early chips burst size is rounded up to a multiply of 1000 frames).*/     uint32_t rate_limit; /**< in Kb/sec for Tx ports, in frame/sec for offline parsing ports. Rate limit refers to data rate (rather than line rate). */ ioc_fm_port_dual_rate_limiter_scale_down rate_limit_divider; /**< For offline parsing ports only. Not-valid for some earlier chip revisions */ } ioc_fm_port_rate_limit_t; Further information in the below link. http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2283674.html
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.  Also the TF-A boot flow is applicable only for LS1088ARDB-PB. LS1088ARDB is not supported LSDK 18.12 release onwards. To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For QSPI NOR flash boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_qspi.pbl BL2 binary: Platform initialization binary RCW binary for QSPI NOR flash fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image Follow these steps to compile and deploy TF-A  binaries (bl2_qspi.pbl and fip.bin) in QSPI NOR flash. Compile PBL binary from RCW source file Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_qspi.pbl and fip.bin) for QSPI NOR flash Program TF-A binaries to QSPI NOR flash Step 1: Compile PBL binary from RCW source file  You need to compile the rcw_1600_qspi.bin binary to build the bl2_qspi.pbl binary. Clone the  rcw repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ cd ls1088ardb If required, make changes to the rcw files. $ make   The compiled PBL binary for QSPI NOR flash on LS1088ARDB-PB, rcw_1600_qspi.bin, is available at rcw/ls1088ardb/FCQQQQQQQQ_PPP_H_0x1d_0x0d/.   See the rcw/ls1088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12  $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls1088ardb_tfa_defconfig $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.12 U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OP-TEE binary You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-ls1088ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for QSPI NOR flash Clone the atf repository and compile the TF-A binaries, bl2_qspi.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.12 LSDK-18.12 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=ls1088ardb bl2 SPD=opteed BOOT_MODE=qspi pbl RCW=<path_to_rcw_binary>/rcw_1600_qspi.bin The compiled BL2 binaries, bl2.bin and bl2_qspi.pbl are available at atf/build/ls1088ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_qspi.pbl binary needs to be recompiled. To compile the BL2 binary without OPTEE: make PLAT=ls1088ardb bl2 BOOT_MODE=qspi pbl RCW=<path_to_rcw_binary>/rcw_1600_qspi.bin Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=ls1088ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/ls1088ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: make PLAT=ls1088ardb fip BOOT_MODE=sd BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to QSPI NOR flash Boot LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI , SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Please ensure that you are using LS1088ARDB-PB to flash the TF-A binaries, as LS1088ARDB is not supported LSDK 18.12 release onwards. Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive   Load TF-A binaries from the TFTP server For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Program QSPI NOR flash1: => sf probe 0:1 Flash bl2_qspi.pbl: => tftp 0xa0000000 bl2_qspi.pbl => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Flash fip.bin: => tftp 0xa0000000 fip.bin => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from QSPI NOR flash1: => qixis_reset altbank LS1088ARDB-PB will boot with TF-A. In the boot log, you will see: => NOTICE: UDIMM 18ASF1G72AZ-2G6B1 NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1 NOTICE: BL2: v1.5(release):LSDK-18.12 NOTICE: BL2: Built : 16:23:18, Feb 8 2019 NOTICE: BL31: v1.5(release):LSDK-18.12 NOTICE: BL31: Built : 16:25:08, Feb 8 2019 NOTICE: Welcome to LS1088 BL31 Phase For steps to deploy TF-A binaries on SD card, see LS1088ARDB-PB - How to deploy TF-A binaries on SD card
記事全体を表示
Follow these steps to update DPAA2 MC firmware and DPC images in QSPI flash, if you are booting LS1088ARDB from the QSPI flash memory.  qixis_reset boots the board from QSPI flash0 (aka bank0) and qixis_reset altbank boots the board from QSPI flash1 (aka bank4). “sf probe 0:1” means that the alternate bank will be written to. So if you boot from flash0, then enter sf probe 0:1, the commands that follow will program flash1. Prerequisites Linux machine. It is recommended to install Ubuntu 18.04 on the Linux machine. Obtaining MC firmware Download the prebuilt MC firmware image from the git repository: https://github.com/NXP/qoriq-mc-binary/tree/integration/ls1088a Obtaining DPC image Clone mc-utils repository and compile the DPC image. git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils cd mc-utils/ git checkout LSDK-18.09 make -C config/ The compiled dpc.0x1D-0x0D.dtb is available at /mc-utils/config/ls1088a/RDB/. Flash MC firmware image on LS1088ARDB QSPI flash In U-Boot, boot from flash0, program flash1:  
記事全体を表示
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.                                                       To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For NOR boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_nor.pbl BL2 binary: Platform initialization binary RCW binary for NOR boot  fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image   Follow these steps to compile and deploy TF-A  binaries (bl2_nor.pbl and fip.bin) on the NOR flash. Compile RCW binary Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_nor.pbl and fip.bin) for NOR boot Program TF-A binaries to the NOR flash Step 1: Compile RCW binary  You need to compile the rcw_1800.bin binary to build the bl2_nor.pbl binary. Clone the  rcw repository and compile the PBL binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09  $ cd ls2088ardb If required, make changes to the rcw files. $ make The compiled PBL binary for NOR boot on LS2088ARDB, rcw_1800.bin, is available at rcw/ls2088ardb/FFFFFFFF_PP_HH_0x2a_0x41 See the rcw/ls2088ardb/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make ls2088ardb_tfa_defconfig $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building the LSDK 18.12 and onwards U-Boot binary.                                                              The compiled U-Boot binary, u-boot.bin, is available at u-boot/.   Step 3: [Optional] Compile OPTEE binary  You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE.   Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-ls2088ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for NOR boot Clone the atf repository and compile the TF-A binaries, bl2_nor.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-19.09 LSDK-19.09 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=ls2088ardb bl2 SPD=opteed BOOT_MODE=nor BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_1800.bin The compiled BL2 images, bl2.bin and bl2_nor.pbl are available at atf/build/ls2088ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_nor.pbl binary needs to be recompiled. To compile the BL2 binary without OPTEE: $ make PLAT=ls2088ardb bl2 BOOT_MODE=nor pbl RCW=<path_to_rcw_binary>/rcw_1800.bin                     Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=ls2088ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/ls2088ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: $ make PLAT=ls2088ardb fip BOOT_MODE=nor BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT                                                                     Step 5: Program TF-A binaries to NOR flash Boot LS2088ARDB from NOR flash. Ensure that the switches and jumpers are set to boot the board from NOR bank 0.  SW5[1:8] = 1111 1111 SW3[1:8] = 0001 0010 SW4[1:8] = 1111 1111 SW6[1:8] = 1111 1111 SW7[1:8] = 0100 0010 SW9[1:8] = 0100 0000 SW8[1:8] = 0111 1111 In addition to the above switch settings, make sure the following jumper settings are correct (for RDB Rev E and later) J14 = 1-2, for NOR boot Boot from NOR bank 0: => qixis_reset For LS2088ARDB, in boot log, you'll see: Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 0 TF-A binaries can be loaded to LS2088ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA).   Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xgmii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS2088ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                                                              => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC1@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC1@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC1@xgmii device host 192.168.1.1 is alive Load TF-A binaries from the TFTP server For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow.                   Flash bl2_nor.pbl to NOR bank 4 (after booting from NOR bank 0). => tftp 82000000 bl2_nor.pbl => erase 0x584000000 +$filesize;cp.b 82000000 0x584000000 $filesize Flash fip.bin to NOR bank 4 (after booting from NOR bank 0). => tftp 82000000 fip.bin => erase 0x584100000 +$filesize;cp.b 82000000 0x584100000 $filesize Boot from NOR bank 4: => qixis_reset altbank LS2088ARDB will boot with TF-A. In the boot log, you will see: NOTICE: UDIMM 18ASF1G72AZ-2G3B1 NOTICE: 16 GB DDR4, 64-bit, CL=13, ECC on, 256B, CS0+CS1 NOTICE: UDIMM 18ASF1G72AZ-2G3B1 NOTICE: 4 GB DDR4, 32-bit, CL=11, ECC on, CS0+CS1 NOTICE: BL2: v1.5(release):LSDK-19.09 NOTICE: BL2: Built : 16:04:08, Nov 4 2019 NOTICE: BL31: v1.5(release):LSDK-19.09 NOTICE: BL31: Built : 16:40:39, Nov 4 2019 NOTICE: Welcome to LS2088 BL31 Phase U-Boot 2019.04 (Nov 04 2019 - 15:57:49 +0530) SoC: LS2088AE Rev1.1 (0x87090011) Clock Configuration: CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz CPU6(A72):1800 MHz CPU7(A72):1800 MHz Bus: 700 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s Reset Configuration Word (RCW): 00000000: 483038b8 48480048 00000000 00000000 00000010: 00000000 00000000 00a00000 00000000 00000020: 01e01180 00002581 00000000 00000000 00000030: 00400c0b 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 412a0000 00040000 Model: Freescale Layerscape 2080a RDB Board Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 4 ....... Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in NOR bank 0 supports the command by typing ls at the U-Boot prompt: => ls ls - Lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in NOR bank 0. For steps to update composite firmware image in NOR bank, see Layerscape Software Development Kit User Guide .            Use the following command if the SD card is formatted/created using LSDK flex-installer command: => load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => load mmc 0:2 $load_addr bl2_nor.pbl Use the following command if the SD card is formatted/created on a Windows PC: => fatload <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: => fatload mmc 0:2 $load_addr bl2_nor.pbl Use the following command if the SD card is formatted/created on a Linux PC: => ext2load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]] For example: =>ext2load mmc 0:2 $load_addr bl2_nor.pbl Also note that LSDK flex-installer command puts the images on the IInd partition, so 0:2 is used in the load command. If the SD card is formatted on Windows PC or Linux PC for single partition only, then 0 should be used instead of 0:2 in the fatload/ext2load command.    Load bl2_nor.pbl image from the storage device => load mmc 0:2 0xa0000000 <image name> => print filesize For example: => load mmc 0:2 0xa0000000 bl2_nor.pbl => print filesize filesize=14379 Or => load usb 0:2 0xa0000000 <image name> => print filesize Or => load scsi 0:2 0xa0000000 <image name> => print filesize Program bl2_nor.pbl to NOR bank 4 (after booting from NOR bank 0): => erase 0x584000000 +$filesize;cp.b 0xa0000000 0x584000000 $filesize Load fip.bin image from the storage device => load mmc 0:2 0xa0000000 <image name> => print filesize For example: => load mmc 0:2 0xa0000000 fip.bin => print filesize filesize=131510 Or => load usb 0:2 0xa0000000 <image name> => print filesize Or => load scsi 0:2 0xa0000000 <image name> => print filesize Program fip.bin to NOR bank 4 (after booting from NOR bank 0): => erase 0x584100000 +$filesize;cp.b 0xa0000000 0x584100000 $filesize Boot from NOR bank 4: => qixis_reset altbank LS2088ARDB will boot with TF-A.
記事全体を表示
Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On the Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-18.09-V4.14 LSDK-18.09-V4.14 where LSDK-18.09-V4.14 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to device tree, open and edit arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-ls1046a-rdb.dtb is in arch/arm64/boot/dts/freescale/. Copying the compiled kernel images and device tree to SD card Plug the SD card into the Linux host machine. List the disks that are accessible to the computer: $ cat /proc/partitions Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen.  The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced.  If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0. Mount the SD card partition that contains Linux kernel images and device tree: $ sudo mount /dev/sdX  <mount_location> Replace Image, Image.gz, and fsl-ls1046a-rdb.dtb on the SD card with the new files compiled in the steps above. sudo cp linux/arch/arm64/boot/Image linux/arch/arm64/boot/Image.gz linux/arch/arm64/boot/dts/freescale/fsl-ls1046a-rdb.dtb <mount_location> sudo umount /dev/sdX Plug the SD card into LS1046ARDB and boot the board to Ubuntu using the SD card: => cpld reset sd In boot log, you’ll see: Board: LS1046ARDB, boot from SD If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
Follow these steps to update the DPAA1 FMan ucode image on the SD card.  Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-19.06 The prebuilt FMan ucode images, fsl_fman_ucode_ls1043_r1.1_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1043_r1.1 refers to the LS1043A silicon revision 1.1. See qoriq-fm-ucode/readme for a description of the ucode version numbers. SD card start block number for DPAA1 FMan ucode image Image  SD card start block number DPAA1 FMan ucode image 0x04800 = 18432 Refer Flash layout for new boot flow with TF-A for complete listing of the SD card start block numbers for all LSDK firmware images. Programming DPAA1 FMan ucode image to SD card Option 1: Load image on SD card plugged into Linux host via dd command Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin of=/dev/sdX bs=512 seek=18432 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.                                                   Remove the SD card from the Linux host machine. Plug the SD card into LS1043ARDB and boot the board to Ubuntu using the SD card. You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card. Option 2: Load image on SD card plugged into board from the TFTP server Boot LS1043ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows: SW3[1:8] = 10110011 SW4[1:8] = 00010010 SW5[1:8] = 10100010 Boot from NOR bank 0: => cpld reset For LS1043ARDB, in boot log, you'll see: Board: LS1043ARDB, boot from vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5 Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1043ARDB Ethernet and FMC port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                        => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load FMan ucode image from the TFTP server Flash the FMan ucode image: => tftp 0xa0000000 fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin Program the FMan ucode image to SD card: => mmc write 0xa0000000 0x04800 <blk_cnt> Address  0x04800 is the SD card block number for the FMan ucode image.  ReferFlash layout for new boot flow with TF-A for the complete flash memory layout. Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load FMan ucode from the TFTP server, if the bytes transferred is 37560 (92b8 hex), then blk_cnt is calculated as "37560/512 = 73 (49 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 5 (5 hex) sectors, for this example, mmc write command will be: => mmc write 0xa0000000 0x04800 4E You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card.
記事全体を表示
View Webinar Recording
記事全体を表示
#lx2160a‌ #lx2160a reference design board‌ #edge_devices‌ #edge-node‌
記事全体を表示
Follow these steps to update the DPAA1 FMan ucode image on the SD card.  Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.12 The prebuilt FMan ucode images, fsl_fman_ucode_ls1046_r1.0_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1046_r1.0 refers to the LS1046A silicon revision 1.0. See qoriq-fm-ucode/readme for a description of the ucode version numbers. SD card start block number for DPAA1 FMan ucode image Image  SD card start block number DPAA1 FMan ucode image 0x04800 = 18432 Refer Flash layout for new boot flow with TF-A for complete listing of the SD card start block numbers for all LSDK firmware images. Programming DPAA1 FMan ucode image to SD card Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=fsl_fman_ucode_ls1046_r1.0_<ucode version>.bin of=/dev/sdX bs=512 seek=18432 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.                             Remove the SD card from the Linux host machine. Plug the SD card into LS1046ARDB and boot the board to Ubuntu using the SD card. You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 01001110 and SW5 [1:8] = 00100000, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1046ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
記事全体を表示
View Webinar Recording
記事全体を表示
DPDK(Data Plane Development Kit) provides a simple, complete framework for fast packet processing in data plane applications. This IPsec security gateway application demonstrates the implementation of a security gateway using DPDK cryptodev framework with crypto protocol offloading support. This document introduces DPDK IPsec gateway application architecture, DPAA2 SEC driver and ipsec-secgw application implementation for crypto protocol offloading, running ipsec-secgw application on LS2088ARDB.
記事全体を表示
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images in QSPI NOR flash. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1. Obtaining MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls1088a/ $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09 The prebuilt MC firmware image, mc_10.10.0_ls1088a_20180814.itb, is available at /qoriq-mc-binary/ls1088a/. Note that the name of the MC firmware image may vary depending on the release version used.  Obtaining DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x1D-0x0D.dtb and dpl-eth.0x1D_0x0D.dtb images are available at /mc-utils/config/ls1088a/RDB/. Note that the name of the DPC and DPL images may vary depending on the release version used.  Flashing MC firmware, DPC, and DPL images to QSPI NOR flash Boot LS1088ARDB/LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI, SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For example: For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 The images can be loaded to the LS1088ARDB/LS1088ARDB-PB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive Load images from a TFTP server Program QSPI NOR flash1: sf probe 0:1 Flash MC firmware: => tftp 0x80000000 mc_10.10.0_ls1088a_20180814.itb => print filesize => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize Address 0xa00000 is the location of MC firmware in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: => tftp 0x80000000 dpc.0x1D-0x0D.dtb => print filesize  => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: => tftp 0x80000000 dpl-eth.0x1D_0x0D.dtb => print filesize  => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize Address 0xd00000 is the location of DPL image in QSPI NOR flash. Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load images from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on the storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Flash MC firmware: Load MC firmware image from the storage device => load mmc 0:2 80000000 <mc firmware> For example: => load mmc 0:2 80000000 mc_10.10.0_ls1088a_20180814.itb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program MC firmware image to QSPI NOR flash: => sf erase 0xa00000 +$filesize && sf write 0x80000000 0xa00000 $filesize  Address 0xa00000 is the location of MC firmware in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPL image: Load DPL image from the storage device => load mmc 0:2 80000000 <dpl image> For example: => load mmc 0:2 80000000 dpl-eth.0x1D_0x0D.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPL image to QSPI NOR flash: => sf erase 0xd00000 +$filesize && sf write 0x80000000 0xd00000 $filesize  Address 0xd00000 is the location of DPL image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Flash DPC image: Load DPC image from the storage device => load mmc 0:2 80000000 <dpc image> For example: => load mmc 0:2 80000000 dpc.0x1D-0x0D.dtb => print filesize Or => load usb 0:2 80000000 <image name> => print filesize Or => load scsi 0:2 80000000 <image name> => print filesize Program DPC image to QSPI NOR flash: => sf erase 0xe00000 +$filesize && sf write 0x80000000 0xe00000 $filesize Address 0xe00000 is the location of DPC image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
記事全体を表示
This Documentation shows how to make a mass production NAND Flash image for QorIQ IFC NAND flash interface by external NAND Flash programmer.
記事全体を表示
The u-boot in SDK2.0 has a bug on SGMII2.5 support. Need to add the patch.
記事全体を表示