LPC微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Microcontrollers Knowledge Base

讨论

排序依据:
This content was originally contributed to lpcware.com by Massimo Manca Example application for the "LPC4300 Getting started Kit" to learn and to use the multi processor communication and the newest peripherals of LPC43xx MCU family. System resources used and assignment to the cores: The Cortex-M4 core handles the application logic, manages the 4 touch keys and 4 leds (via the PCA9502 I2C 8 bit I7O expander), the lcd display and the real time clock. The Cortex-M0 core is dedicated to the printer management using the RS232 on board interface (in near future SCT and SGPIO will be used to interface a thermal printing head). The cores communicates using inter processor communication mechanisms minimizing the data passed from M4 to M0 and providing a simple security mechanism.
查看全文
LPC4300 10-bit ADC module Introduction        LPC4300 Series microcontrollers combine the high performance and flexibility of an asymmetric dual-core architecture (ARM Cortex-M4F and Cortex-M0 coprocessor) with multiple high-speed connectivity options, advanced timers, analog, and optional security features to secure code and data communications. DSP capabilities enable all LPC43xx families to support complex algorithms in data-intensive application. Flash and Flashless options support large, flexible internal and external memory configurations.         LPC4370/LPC43S70 products provide 12-bit high-speed ADC module with up to 80MSamples/s. This document does not test 12-bit high-speed ADC performance. LPC43xx/LPC43Sxx series products provide two 10-bit SAR ADC module with below features: *   Measurement range 0 to 3.3 V *   10-bit conversion time = 2.45 us (up to 400K Samples/s) *   Burst conversion mode for single or multiple inputs *   Support hardware/software trigger *   Support Interrupt/DMA mode Test hardware platform introduction         This test hardware platform uses Keil MCB4357 evaluation board (OM13040), which enables customer to create and test working programs based on the LPC4300 family of Dual Core ARM Cortex™-M4/M0 devices. Keil MCB4357 with below features:  204 MHz LPC4357 device with ARM Cortex-M4 processor and Cortex-M0 coprocessor 136 KB On-Chip SRAM 1 MB dual bank On-Chip Flash On-Board Memory: 16 MB NOR Flash, 4 MB Quad-SPI Flash, 16 MB SDRAM & 16 KB EEPROM (I²C) Color QVGA TFT LCD with touchscreen High-speed USB 2.0 Host/Device/OTG interface (USB host + Micro USB Device/OTG connectors) Full-speed USB 2.0 Host/Device interface (USB host + micro USB Device connectors) MicroSD Card Interface Analog Voltage Control for ACD Input Audio CODEC with Line-In/Out and Microphone/headphone connector + Speaker Debug Interface Connectors 20-pin JTAG (0.1 inch) 10-pin Cortex debug (0.05 inch) 20-pin Cortex debug + ETM Trace (0.05 inch connector Test software introduction       This test software uses LPCOpen software ADC demo, the software version is V2.20.       ADC demo default path is:       ..\lpcopen_2_19_keil_iar_keil_mcb_4357\applications\lpc18xx_43xx\iar\keil_mcb_4357\periph_example.eww      LPCOpen software [periph_example.eww] project provides LPC4357 most modules driver application demos. The ADC demo need precompile MCB4357 board support package (lib_lpc_board_keil_mcb_4357) and LPC43xx chip driver (lib_lpc_chip_43xx). MCB4357 board support package provides MCB4357 board related pins configuration, clock configuration, on-board external memory configuration, Ethernet PHY driver configuration and board hardware resource configuration; LPC43xx chip driver provides LPC43xx modules driver API function.       ADC demo provides three modes to get ADC conversion value: polling mode, interrupt mode and DMA mode. The demo config 10-bit ADC module with 400K Samples/s and ARM Cortex-M4 core clock frequency with 204MHz. The test uses Timer0 module as time-base and counter reference clock is same with ARM Cortex-M4 core clock frequency (204MHz).       Timer0 initialization code comments: ADC module initialization code comments: ADC polling mode code comments: ADC interrupt mode code comments: ADC DMA mode code comments: Test result     The test will use TIMER0 counter to calculate each test item time interval.      The test includes below test items:      Single/no burst: ADC convert one time with burst mode disabled      100K/no burst: ADC convert 100K times with burst mode disabled      Single/burst: ADC convert one time with burst mode enabled      100K/burst: ADC convert 100K times with burst mode enabled
查看全文
LPC4088 Closed Payment Loop Demo - Connecting the boards together In order to use the demo, the three boards (Embedded Artists Base Board, LPC4088 OEM module, CLRC663 Blueboard) must be connected together. Please follow below steps to accomplish this. 1) Place the LPC4088 OEM module in the baseboard. 2) Secure the 7" LCD board ontop of the baseboard using the supplied plastic spacers. Connect the two boards electrically together by using the supplied flatcable. 3) Connect the Blueboard to the base board. This is done by 8 wires and a USB-A to USB Mini-B cable. The USB connecting is only used for +5V and GND, not for data. For the 8 wire conenctions, please refer to the table below. EA Baseboard Blueboard Function USB UBS 5V supply / GND +3V3, [J4] 2 3V3 3.3V supply GPIO37, [J5] 23 P2.4 CLRC663 Interface Select0 GPIO40, [J3] 28 P2.5 CLRC663 Interface Select1 GPIO38, [J3] 27 P0.3 CLRC663 Reset I2C-SDA, [J5] 25 SDA SDA I2C-SCL, [J5] 26 SCL SCL - P2.0 CLRC663 I 2 C address, connect to GND - P2.1 CLRC663 I 2 C address, connect to GND Proceed to "Compiling the software & flashing the board".
查看全文
#ISP‌ #bootrom‌ memremap‌
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341477
查看全文
1 Abstract       MCB1700 is the evaluation board from KEIL, the onboard chip is LPC1758, LPC1768 or LPC1769 which is based on ARM cortex-M3.       EmWin is the embedded graphics library developed by SEGGER, it is now offered by NXP in library form for free commercial use with NXP microcontrollers. The software bundle offered by NXP includes the emWin Color basic package, the Window Manager/Widgets module including the GUIBuilder, the Memory Devices module for flicker-free animation, the Antialiasing module for smooth display of curves, lines and fonts, the Font Converter and the VNC Server.        NXP have provided the MCB1700 emWin board support packages: emWin 5.14 BSP version 1.0 for MCB1700  This package includes three IDE project: IAR, MDK and LPCXpresso, but now, when customer use it, normally will find these questions: LPCXpresso project have the build error MDK project have the build error Some MCB1700 boards can’t work after downloading this code, LCD always display white, no other pictures.     This document is mainly talking about these three problems and give the according solutions to make the MCB1700 emWin_mcb1700_bsp work. 2 Code issue analysis and solutions      Customer need to download the emWin_mcb1700_bsp at first from the above link, and install it, after the package is installed in default, the source code can be found in this path: C:\nxp\emWin\NXP_emWin514_MCB1700_BSP 2.1 keil project build error       This chapter mainly describe the emWin_mcb1700_bsp keil project build error and it’s solutions. 2.1.1 Problem reproduction       Open the emWin_mcb1700_bsp keil project with keil IDE, you may find there has 6 errors like the following picture: All these errors are related to the GUI function which is included in the emwin lib, after click the GUI folder, you will find the lib is emWin_514 which is the old emWin lib. So people can try to use the newest lib from the nxp website. 2.1.2 Problem solution     Download the newest emWin lib from this link:    emwin 5.30 Pre-Compiled Libraries for NXP ARM MCUs    After install it, copy emWin_M3.lib from folder: NXP_emWin530\emWin_library\Keil\ to NXP_emWin514_MCB1700_BSP\GUI folder. Then add this new lib to the KEIL project’s GUI folder like this:    After the emWin_M3.lib is added, remove the build of old lib emWin_514_Keil4_M3_LE.lib, just deselect item include in Target build in the right click options like this: Save and rebuild it again, you will find the error is disappeared. 2.2 LPCXpresso project build error     This chapter mainly describe the emWin_mcb1700_bsp LPCXpresso project build error and it’s solutions. 2.2.1 LPCXpresso project problem reproduction Open LPCXpresso project, and build it, you may find these problems:     All the errors are C/C++ Problem. 2.2.2 LPCXpresso project problem solution     Choose project->properties, change the language standard to GNU C90 stand like this:   Click button “ Apply”,  then rebuild it again, you will find the error is disappeared: Of course, you also can change the lib to the newest one, just like the method in the KEIL project, use the newest LPCXpresso emWin lib from this folder:  NXP_emWin530\emWin_library\LPCXpresso\libemWin_M3.a   2.3 Code function problem in some MCB1700 board      This part is mainly taking about the function problem in some MCB1700 boards, give the analysis and the according solutions. 2.3.1 Code function problem reproduction       After the build problem is solved, customer can download the code to the MCB1700 board by debugger or programmer, no matter with LPC1758, LPC1768 or LPC1769. After testing some MCB1700 boards, we found some board always display white, the emwin function doesn’t work, but some board can display the correct picture. All these boards seems the same.       I have compared these boards carefully, I found the series number in the LCD have difference, now I list it as follows:   MCB LCD Series number RESULT MCB1758 A774A-43-P101210-4072 OK MCB1758 A774A-61-P120814-4074 Abnormal, LCD display white MCB1769 A774A-22-P120814-4074 Abnormal, LCD display white MCB1769 A774A-57-P120814-4074 Abnormal, LCD display white      From the above form, we can find all the MCB boards which can’t work have one feature: the LCD series number contains P120814, so it should be related to the LCD controller, but what the controller on these MCB1700 boards? After download the LCD_Blinky code from the KEIL IDE install path: C:\Keil_v5\ARM\Boards\Keil\MCB1700\LCD_Blinky I found this project can display the picture correctly, so I do the debugging and the source code checking, after that I get the LCD with P120814 is using the HX8347-D LCD controller which from Himax company. But the LCD diver code in emWin MCB1700 BSP is for SPFD5408 LCD controller.   2.3.2 Code function problem solutions     Here take MDK project as an example, describe how to modify the emWin_MCB1700_BSP code and make it work in those not working MCB1700 boards. After the analysis in the above chapter, you will get that the main problem is caused by the LCD driver, so the code modification is mainly about the LCDConf.c file, this code in this file is for the LCD driver configuration. 2.3.2.1 Modify the display orientation     Comment the old DISPLAY_ORIENTATION definition, and define it like this: //#define DISPLAY_ORIENTATION (GUI_SWAP_XY) #define DISPLAY_ORIENTATION (GUI_MIRROR_X | GUI_SWAP_XY)   2.3.2.2 Modify the LCD controller initialization code From chapter 2.3.1, we can get the LCD on the not working MCB1700 board is HX8347-D, the HX8347 LCD controller initialization code should be modified like this: static void _InitController(void) { #ifndef WIN32     GUI_X_Delay(10);   LCD_X_SPI_Init();   GUI_X_Delay(10);     /* Driving ability settings ------------------------------------*/     wr_reg(0xEA, 0x00);       /* Power control internal used (1)    */     wr_reg(0xEB, 0x20);       /* Power control internal used (2)    */     wr_reg(0xEC, 0x0C);       /* Source control internal used (1)   */     wr_reg(0xED, 0xC7);       /* Source control internal used (2)   */     wr_reg(0xE8, 0x38);       /* Source output period Normal mode   */     wr_reg(0xE9, 0x10);       /* Source output period Idle mode     */     wr_reg(0xF1, 0x01);       /* RGB 18-bit interface ;0x0110       */     wr_reg(0xF2, 0x10);             /* Adjust the Gamma Curve --------------------------------------*/     wr_reg(0x40, 0x01);     wr_reg(0x41, 0x00);     wr_reg(0x42, 0x00);     wr_reg(0x43, 0x10);     wr_reg(0x44, 0x0E);     wr_reg(0x45, 0x24);     wr_reg(0x46, 0x04);     wr_reg(0x47, 0x50);     wr_reg(0x48, 0x02);     wr_reg(0x49, 0x13);     wr_reg(0x4A, 0x19);     wr_reg(0x4B, 0x19);     wr_reg(0x4C, 0x16);       wr_reg(0x50, 0x1B);     wr_reg(0x51, 0x31);     wr_reg(0x52, 0x2F);     wr_reg(0x53, 0x3F);     wr_reg(0x54, 0x3F);     wr_reg(0x55, 0x3E);     wr_reg(0x56, 0x2F);     wr_reg(0x57, 0x7B);     wr_reg(0x58, 0x09);     wr_reg(0x59, 0x06);     wr_reg(0x5A, 0x06);     wr_reg(0x5B, 0x0C);     wr_reg(0x5C, 0x1D);     wr_reg(0x5D, 0xCC);       /* Power voltage setting ---------------------------------------*/     wr_reg(0x1B, 0x1B);     wr_reg(0x1A, 0x01);     wr_reg(0x24, 0x2F);     wr_reg(0x25, 0x57);     wr_reg(0x23, 0x88);       /* Power on setting --------------------------------------------*/     wr_reg(0x18, 0x36);       /* Internal oscillator frequency adj  */     wr_reg(0x19, 0x01);       /* Enable internal oscillator         */     wr_reg(0x01, 0x00);       /* Normal mode, no scrool             */     wr_reg(0x1F, 0x88);       /* Power control 6 - DDVDH Off        */     GUI_X_Delay(200);     wr_reg(0x1F, 0x82);       /* Power control 6 - Step-up: 3 x VCI */     GUI_X_Delay(50);                     wr_reg(0x1F, 0x92);       /* Power control 6 - Step-up: On      */     GUI_X_Delay(50);     wr_reg(0x1F, 0xD2);       /* Power control 6 - VCOML active     */     GUI_X_Delay(50);       /* Color selection ---------------------------------------------*/     wr_reg(0x17, 0x55);       /* RGB, System interface: 16 Bit/Pixel*/     wr_reg(0x00, 0x00);       /* Scrolling off, no standby          */       /* Interface config --------------------------------------------*/     wr_reg(0x2F, 0x11);       /* LCD Drive: 1-line inversion        */     wr_reg(0x31, 0x00);     wr_reg(0x32, 0x00);       /* DPL=0, HSPL=0, VSPL=0, EPL=0       */       /* Display on setting ------------------------------------------*/     wr_reg(0x28, 0x38);       /* PT(0,0) active, VGL/VGL            */     GUI_X_Delay(200);     wr_reg(0x28, 0x3C);       /* Display active, VGL/VGL            */   //  wr_reg(0x16, 0x00);       /* Mem Access Control (MX/Y/V/L,BGR)  */       /* Display scrolling settings ----------------------------------*/     wr_reg(0x0E, 0x00);       /* TFA MSB                            */     wr_reg(0x0F, 0x00);       /* TFA LSB                            */     wr_reg(0x10, 320 >> 8);   /* VSA MSB                            */     wr_reg(0x11, 320 & 0xFF); /* VSA LSB                            */     wr_reg(0x12, 0x00);       /* BFA MSB                            */     wr_reg(0x13, 0x00);       /* BFA LSB                            */ #endif }   2.3.2.3 Modify the LCD_X_Config configuration    From the emWin display drivers website in the Segger: https://www.segger.com/emwin-display-drivers.html You can find the HX8347 display driver is GUIDRV_FlexColor, the parameter pfFunc in function GUIDRV_FlexColor_SetFunc is GUIDRV_FLEXCOLOR_F66712.   So, modify GUIDRV_FlexColor_SetFunc in the LCD_X_Config function like this: GUIDRV_FlexColor_SetFunc(pDevice, &PortAPI, GUIDRV_FLEXCOLOR_F66712, GUIDRV_FLEXCOLOR_M16C0B16);     After the modification, then save and rebuild it. At last, download the code to the MCB1700 board which was not working before, download the code to the board, press the RESET button on the board, you will find the LCD displays the GRAPH_DATA_XY demo picture like this:   2.3.3 Other applications testing    After the above code modification for the not working MCB1700 board, if you have interest, you also can try the other application to display other pictures. In folder  NXP_emWin514_MCB1700_BSP\Application, there still has a lot of other applications, you just need to add it to the application folder in the project, then the LCD can display the according picture,  now list some application’s testing result. 2.3.3.1 GUI_WIDGET_GraphYtDemo.c   2.3.3.2 GUI_HelloWorld.c     2.3.3.3 GUI_ALPHA_TransparentDialogDemo.c   2.3.3.4 WM_RadialMenu.c   3 Conclusion    From the above detail descriptions, you will know emWin_MCB1700_bsp KEIL project build error can be fixed by changing the lib to the newest emwin lib, LPCXpresso project build error can be fixed by changing the language standard to GNU C90, the function problem in some MCB1700 is mainly caused by the mismatch LCD driver, just modify the code to the according LCD driver can fix the LCD display white problem.    Wish this document can help those customers who are using the emWin_MCB1700_bsp on the MCB1700 board, the modified project also in the attachment for your reference.
查看全文
Now that you've downloaded & unzipped your LPCXpresso54608 SDK, let's open IAR Embedded Workbench IDE. Note: You must have at least IAR Embedded Workbench version 7.80.3.12146 to use this board Once open, select File>Open>Workspace Navigate to the location where you unzipped your SDK files. Within this folder there are plenty of SDK based demos for you to explore our microcontroller.  We will use one of them to guide you through this tutorial, but definitely take time to try all of them! Select boards>lpcxpresso54608>demo_apps>touch_cursor>iar>touch_cursor Once the workspace is loaded, you will see the project files on the left.  Along the toolbar the first highlighted item is 'Build' select it. Once your console shows no errors you can select the 'Download and Debug' a few icons to the right of 'Build' Your debug session will start and will look like the following window.  Once it opens 'touch_cursor.c' and has a green arrow next to the main function you can select 'Go' After you have successfully flashed the board with this demo you will see the following on your board. This demo utilizes the touch interface on the screen to read where you are touching and updates the cursor position to the last known location.   Remember that other demos and sample code are provided in the root folder of the SDK download.   Be sure to explore these demos and reach out on the community if you need help!
查看全文
Hello Community! This document is provided as a hands-on lab guide.  The intent of the lab is to demonstrate how to program the LPCXpresso804 board with the MCUXpresso IDE making use of the SDK examples and the PLU module drivers. The PLU configuration tool will be used to create a new schematic design that will be programmed to the PLU. Setup The following items need to be installed on your computer to complete the lab: Software: •    SDK_2.4.1_LPCXpresso804: -    Copy link into browser: https://mcuxpresso.nxp.com/en/select?device=LPCXpresso804 -    Select ‘MCUXpresso IDE’ or ‘All Toolchains’ in the Toolchain IDE drop-down -    Select ‘Download SDK’ •    MCUXpresso IDE version 10.2.1: -    Can be installed at following link: https://www.nxp.com/mcuxpresso/ide •    PLU configuration tool -    Can be installed at this link: https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-applications-processors/i.mx-rt-series/i.mx-rt1060-crossover-processor-with-arm-cortex-m7-core:i.MX-RT1060?tab=Design_Tools_Tab   Hardware: •    LPCXpresso804 Development Board (OM40001): https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/lpcxpresso-boards/lpcxpresso804-for-the-lpc804-family-of-mcus:OM40001?tab=Design_Tools_Tab •    PLU Shield Board •    1 Micro USB cable Hope this guide is helpful! Any comments are welcome. Best Regards, Carlos Mendoza Technical Support Engineer
查看全文
I already have several customers met SB file loading error Inject command 'receive-sb-file' while working on LPC55S6xx 1B version. There is significant change of Secure Boot in LPC55S6xx 1B version and 0A version. To solve this problem, we need to understand it first.     1  SB2.1  vs. SB2.0 SB2 container is described in elftosb User’s Guide. SB file config file contains configuration commands that will be processed after SB2 file is loaded in the device. The image location is stated in the "sources" .bd file section. SB key in text file is used for encryption with elftosb command line tool.   The 0A version of the LPC55S6xx silicon supports version 2.0 of the SB image format. The 1B version of the LPC55S6xx silicon supports version 2.1 of the SB image format. The main difference between version 2.0 and version 2.1 is in the usage of the digital signature. SB 2.0 is encrypted and SB2.1 is encrypted + signed.     2. SB file Preparation and Usage   Example of use (Encrypted SB2):   elftosb -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" "input.bin"   where -f = family lpc55xx -k = path to KEK file (SBKEK) -c = path to command file to be processed:   options { flags = 0x4; // 0x8 encrypted + signed, 0x4 encrypted buildNumber = 0x1; productVersion = "1.00.00"; componentVersion = "1.00.00"; } sources { inputFile = extern(0); } section (0) {       erase 0x0..0x40000; load inputFile > 0x0; }   -o = path to output file   files... = path to files (usually image files), which will be replacing placeholders defined in command file, paths can be hardcoded in command file and then not inserted as input   Example of use (Encrypted + Signed SB):   1 root key   elftosb.exe -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" -s "selfsign_privatekey_rsa2048.pem" -S "selfsign_v3.der.crt" -R "selfsign_v3.der.crt" -h "RKTH.bin" "input.bin"   4 root keys   elftosb.exe  -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" -s private_key_1_2048.pem -S certificate_1_2048.der.crt -R certificate_1_2048.der.crt -R certificate_2_2048.der.crt -R certificate_3_2048.der.crt -R certificate_4_2048.der.crt -h "RHKT.bin" "input.bin"   where -f = family lpc55xx -k = path to KEK file (SBKEK) c = path to command file to be processed   options { flags = 0x8; // 0x8 encrypted + signed, 0x4 encrypted buildNumber = 0x1; productVersion = "1.00.00"; componentVersion = "1.00.00"; } sources { inputFile = extern(0); } section (0) {       erase 0x0..0x40000; load inputFile > 0x0; }   -o = path to output file -s = path to private key of certificate used for signing -S = path(s) to certificates in certificate chain, each certificate in chain must be specified with new -S switch in order of how was chain created (root certificate first) -R = path(s) to root certificate(s), 1-4 root certificates can be specified, each root certificate must be specified with new -R switch, one of the root certificates must be first certificate specified by -S switch -h = path and name of output binary file generated by elftosb, which contain hash of hashes of all root certificates (RKTH), which must be uploaded to the device register files... = path to files (usually image files), which will be replacing placeholders defined in command file, paths can be hardcoded in command file and then not inserted as input The SB2.0 file created with the updated binary image can be loaded into the device through ISP command handler with command “receive-sb-file“   blhost -p COMxx receive-sb-file <path to the secured binary(.sb2)>   The SB2.1 file created with the updated binary image can be loaded into the device through ISP command handler with command “receive-sb-file“ but keep in mind that before sending SB2.1 file into device has to be there already RKTH in CMPA (see AN12283 chapter 5.5 CMPA preparation) and enabled RoT keys in ROTKH_REVOKE field at CFPA page address 0x9DE18 (see chapter AN12283 5.4 CFPA preparation).   blhost -p COMxx receive-sb-file <path to the secured binary(.sb2)>   After successfully loading the SB2 file it is executed as configured in SB configuration file (.bd file). The above figure shows an example of SB configuration file. When the file is executed, the internal flash address from 0x0 to 0x40000 is erased. After flash erase operation, the image mentioned in the sources parameter is loaded to address 0x0. Reset the device after these operations. The updated image loaded into internal flash starts to execute.    English and Chinese versions of this article are both attached.
查看全文
The LPC800 series is a 32-bit, Arm® Cortex®-M0+-based MCU portfolio offering a range of low-power, space efficient, low-pin-count options for basic microcontroller applications. Unique among low-end devices, the LPC800 series MCUs include differentiated product features, such as an NFC communication interface, programmable logical unit (PLU), mutual capacitive touch, switch matrix for flexible configuration, patent-approved SCTimer/PWM, and more – including a comprehensive enablement offering to help you get to market faster. LPC80x 15 MHz|Arm Cortex-M0+|32-bit Microcontrollers (MCUs)|NXP  Webinar series are now available for on-demand viewing, you can get access to the webinars by clicking on the following links:   (5/31) Part I: Thinking about migrating from 8-bit? Wait no longer - LPC80x MCUs are your 32-bit answer! Learn more about the LPC80x MCU family, discover the features, target applications, tools, software and how to get started right away with your 32-bit design.   (6/07) Part II: Creative ways to leverage the LPC804 MCU’s integrated programmable logic feature Continuing its history of innovation in MCUs, NXP introduces a programmable logic unit (PLU) to the LPC family for the first time with the LPC804 MCU. We'll show you how easy it is set up the PLU as we will explore several real-world examples of the challenges many face, but can be overcome with this unique feature.   (6/14) Part III: Get started fast with this comprehensive enablement offering for LPC800 MCUs In May 2018, NXP expanded the MCUXpresso suite of software and tools to include full support for the LPC800 MCU family. Learn about the MCUXpresso IDE, configuration tools and SDK support that is now available for the most cost-effective and compelling family of Arm-based 8-bit replacement microcontrollers available.   (6/21) Part IV: Got NFC? LPC8N04 does - Learn how to leverage this unique feature in your next design? Learn more about the LPC8N04 MCU, its features, and how to get started with NFC quickly by leveraging the available development   Presentations for the webinars are also available now!
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2019/05/05/trustzone-with-armv8-m-and-the-nxp-lpc55s69-evk
查看全文
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-342406
查看全文
MCUXpresso Config Tools is now available! You can access it on the following link: Welcome to MCUXpresso | MCUXpresso Config Tools  Overview. MCUXpresso Config Tools provides a set of system configuration tools that help users of all levels with a Kinetis or LPC-based MCU solution. Let it be your guide from first evaluation to production development. High Quality, Comprehensive Enablement - Production-grade, rigorously tested software and tools. - Easy-to-use SDK, IDE and configuration tools. Compatibility Across MCUs - Supports Kinetis, LPC Cortex-M. - Easy migration and scalability between MCUs. Note: i.MX Cortex-M device support coming in 2017 Interoperability Across Tools - Common experience and broader support through fewer, more cohesive software and tools. - Seamless development using SDK, IDE and Config tools together. - SDK and configuration tools also support the large ecosystem of NXP’s partner IDEs. Features. Architecture - CMSIS-CORE compatible - Single driver for each peripheral - Transactional APIs w/ optional DMA support for communication peripherals Integrated RTOS - FreeRTOS, µC/OS-II & -III - RTOS-native driver wrappers Integrated Stacks and Middleware - USB Host, Device and OTG - lwIP, FatFS - Crypto acceleration plus wolfSSL & mbedTLS - SD and eMMC card support Reference Software - Peripheral driver usage examples - Application demos - FreeRTOS usage demos License - BSD 3-clause for startup, drivers, USB stack Toolchains - IAR®, ARM® Keil®, GCC w/ Cmake - + MCUXpresso IDE Quality - Production-grade software - MISRA 2004 compliance - Checked with Coverity® static analysis tools Configuration and development tools.   SDK Builder packages custom SDKs based on user selections of MCU, evaluation board, and optional software components. Pins, Clocks, and Peripheral(1) tools generate initialization C code for custom board support. Project Generator(1) creates new SDK projects  or clones existing ones. Power Estimation tool provides energy and battery-life estimates based on a user’s application model Power Analyzer(1) measures and displays energy consumption data. (1)Coming 2017 Related links: Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE  https://community.nxp.com/docs/DOC-333369   
查看全文
This article introduces how to create a custom board MCUXpresso SDK and how to use it, mainly includes three parts: Part1: Generating a Board Support Configuration (.mex) Part2: Create a Custom Board SDK Using the Board SDK Wizard Part3. Using the Custom SDK to Create a New Project   Requirements: MCUXpresso IDE v11.1.1, MCUXpresso SDK for LPC845, LPC845-BRK board. This method works for all NXP mcu which support by MCUXpresso SDK. About detail steps, please refer to attachment. Thanks!
查看全文
This content was originally contributed to lpcware.com by Cam Thompson This project is a simple data logging example that takes readings from various sensors, and log the information to a web page. The Cortex-M4 is used to collect and process sample data, and the Cortex-M0 is used to run a web server for supplying data to web clients. This allows data to be viewed on any web browser, including portable devices such as smart phones and tablets. The web data logging example was implemented using the Hitex LPC4300 evaluation board, which has all the necessary components. The LPC43xx has a built-in ethernet controller accessible by either core, and the Hitex evaluation board provides the physical layer. An on-board 128x32 pixel Chip-on-Glass (COG) LCD display, four touch sensors, and several LEDs are used for implementing a simple user interface. The LPC43xx contains a Real-Time Clock (RTC) which is used to record the date and time of data samples.
查看全文
This is a quick introduction that shows how to interface a popular GPS module to the LPC845 Breakout Board using the UART drivers from the MCUXpresso SDK. This example reads and parses GPS data from the module when the user button is pressed and outputs the information to a host computer console via the board's VCOM interface.    UART Protocol The UART function uses two TPU channels to provide a 2-wire (TxD and RxD) asynchronous serial interface. One TPU channel is configured to function as the serial transmitter (TxD), and another TPU channel is configured to function as a serial receiver (RxD).    Adafruit Flora Wearable GPS The module used for this example is built around the MTK3339 chipset, a no-nonsense, high-quality GPS module that can track up to 22 satellites on 66 channels, has an excellent high-sensitivity receiver. It can do up to 10 location updates a second for high speed, high sensitivity logging or tracking. Power usage is very low, only 20 mA during navigation. Adafruit took this module and mounted it on one of their super-compact Flora boards, which are very easy to connect up to the LPC845 Breakout:     Figure 1. Flora Wearable GPS.   GPS Module Example NXP provides example packages that include projects to use the principal's peripherals that the board include: ADC, I2C, PWM, USART, Captouch, and SPI.   What we need: LPC845 Breakout Board MCUXpresso IDE V10.3.0 SDK_2.5.0_LPC845 NXP example packages Adafruit Flora Wearable GPS Micro USB cable   Once downloaded, we import the library project into the workspace using the ''Import project(s) from file system... from the Quickstart panel in MCUXpresso IDE:     Figure 2. Import projects   Then browse the examples packages archive file:     Figure 3. Select Example package.   Press next, and see that are a selection of projects to import, in this case, only keep select the LPC845_BoB_GPS how it looks in the picture below:     Figure 4. Select GPS project   Connections Now, with the project already in the workspace is time to set up the connection between the LPC845 Breakout board and the GPS module, as shown in the table below:     Table 1. LPC845 to GPS module.   The Flora module has the signals clearly printed on their silkscreen which really helps .     Figure 5. LPC845 Breakout Board to GPS module connections.   Once the connections are made, its time to build and run the example code, use the build and debug button inside the IDE. Now open a terminal program and connect to the COM port the board enumerated as. Configure the terminal with these settings:  115200 baud rate.   No parity.  8 data bits  1 stop bit   Place the GPS module outside. Once the GPS has located the satellite data, the red LED on the GPS will stop blinking. If you see the LED blinking once a second, it does not yet have a fix! It can take many minutes to get a fix if the module sees any satellites immediately. Once it has a fix, press the user button (K1) to display the GPS data in the serial monitor, which includes the current date and time in UTC. It will also give you your latitude, longitude and approximate altitude with the Serial monitor. Figure 6. GPS Print Out.
查看全文
Hello I have worked on Eclipse for developing applications. I am using NXP's  LPC1769 chip. I have made a documentation on setting up an Eclipse environment.Initially I worked on two basic projects i.e. GPIO toggling and Seven segment display. For running any application ,environment setup is is very important. In this documentation, I have mentioned some links and videos which worked for me. For setting up eclipse environment you need to set up tool chains and paths properly otherwise it will show path errors while compiling any project. Hope it would be helpful!
查看全文