LPC微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Microcontrollers Knowledge Base

讨论

排序依据:
#lpc5410x‌ #fifo‌ #timeout‌
查看全文
#lpc5410x‌ #fifo‌ #timeout‌
查看全文
This documents describes how to use this tool in order to generate the routing and muxing for pins. This tool is available as an online WEB application https://mcuxpresso.nxp.com Pins Tool Overview The Pins Tool is an easy-to-use way to configure the pins of the device. The Pins Tool software enables you to create, inspect, change, and modify any aspect of the pin configuration and muxing of the device. This document introduces you to the Pins Tool. It describes the basic components of the tool and lists the steps to configure and use the tool to configure the pins. This tool is provided as an online WEB application. You need to generate a downloadable MCUXpresso SDK v.2 package. The below link shows the steps for do that. Generating a downloadable MCUXpresso SDK v.2 package  User interface The Pins Tool consists of several views. Using the Pins Tool The Pins Tool is designed to configure routing of signals from peripherals either to pins or to internal signals. To define routing path, first select a peripheral, then select the signal, and finally select the pin. 1. Select a peripheral for example GPIO. The following image illustrates the filtering controls in the Pins view. 2.  Route the selected Signal to the desired pin. It is possible to easily identify routed pins/peripherals in the package using highlighting. By default, the current selection (pin/peripheral) is highlighted in the package view. • Red indicates that the pin has an error. • Green indicates that the pin is muxed or used. • Light grey indicates that the pin is available for mux, but is not muxed or used. • Yellow border around the pin such that the other color is still visible indicates that the pin is selected. For example, by peripheral or by pin. 3. Select one of non-conflicting/available pins. Once you have selected Peripheral, Signal, and Route to, the pin configuration is done. Later, it is also possible to configure the pin electrical features. Use the table drop down menu to configure the pin. To configure pins, start from left to right – select the peripheral first, then select required signal, and finally select the routed pin. The italic value indicates that the value is not configured and it shows the after-reset value and no code is generated, so the configuration relies on the after reset value or the values configured from the different functions. Code generation The tool generates source code that can be incorporated into an application to initialize pins routing. The source code is generated automatically on change or can be generated manually by selecting the main menu Pins > Generate Now. The generated code is shown in the Sources tab on the right window. It shows all generated files and each file has its own tab. It is also possible to copy and paste the generated code into the source files. The view generates code for each function. In addition, it is possible to Export generated source using the Export option. 1. Select Pins > Export 2. Click Next. 3. Select the name of the zip file and click Finish. Your download should automatically begin.  Enjoy!!   Related links: Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  MCUXpresso Config Tools is now available!   How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE 
查看全文
Today's Data Acquisition Applications require separate ICs for input, processing, and output. With the new LPC4370, designers have a complete data acquisition solution on a single chip. With the release of NXP’s new LPC4370 Cortex-M4F microcontroller, we wanted to provide engineers with the tools necessary to evaluate its high-performance signal processing capabilities (up to 204 MHz) and its host of advanced features and peripherals including the 12-bit ADC at 80 Msps with up to six channels.   The result is a new product from Embedded Artists, named LabTool.  LabTool is as an add-on board to NXP’s LPC-Link 2 debugger and demoboard platform.  The LabTool includes a hardware daughter board and software running on the PC that enables the Link2 to be used as a logic analyzer, oscilloscope, and signal generator. It is designed around NXP’s new LPC4370 microcontroller, and the hardware can serve as a development platform for this MCU.   LPC4370 and LabTool Key Components Follow the URLs in the table to find more information on the product and its key components. LPC4370 The LPC4370, ARM Cortex-M4F based microcontrollers, are complete data acquisition solutions on a single chip. The LPC4370 provide the fast digital and analog inputs, the high performance processing capabilities, and the hi-speed output needed for data acquisition applications. Running up to 204MHz, the ARM Cortex-M4F of the LPC4370 is the industry’s fastest Cortex-M microcontroller. The Cortex-M4F is a next generation 32-bit core that offers system enhancements such as low power consumption, enhanced debug features, and a high level of support block integration. Download the LPC4370 documentation: LPC4370 BGA256 Product Information Page LPC4370 BGA100 Product Information Page LPC4370 User Manual and Data Sheet LPC4300 Series Leaflet LPC-Link2 LPC-Link 2 is an extensible, stand-alone debug probe that can be configured to support various development tools and IDEs using a variety of different downloadable firmware images. It can also be used as an evaluation board in its own right for the NXP LPC4370 triple core MCU. And through the use of an add-on board from Embedded Artists, it can be used as an oscilloscope or logic analyzer! For more information on the Link 2, view our NXP.com page. LabTool LabTool can be purchased as a kit that includes the Link2 main board plus the add-on board, or the two can be purchased separately.  A connector with 26 probe wires is included, and is the only accessory required for using the tool.  The probes feature a 2.54mm pigtail end, for easily connecting to headers and jumpers on a target platform.  A set of compatible microgrippers may also be useful, but must be purchased separately. Purchase LabTool, download documentation and the GUI at Embedded Artists product page.   LabTool also available for purchase at: Watch the video here.   LabTool Features   The LabTool consists of both a hardware platform and a software GUI, which combine together in providing the following set of features that are commonly used by electronic designers during bench debugging.  A standard 5.0V supply from your high-speed USB2.0 connector provides the power needed to operate the board, as well as the high-speed communication channel for the data stream.   Digital Channels 10 channel logic analyzer supporting 100MHz (2ch), 80Mhz (4ch), 50MHz (8ch), 20MHz (10ch) Selectable edge-sensitive and level-sensitive triggers give you flexibility in how the signal is displayed. 11 channel digital signal generator up to 80Mhz, at 3.3 volts logic level. Included with the digital interface are three protocol analyzers.  You can monitor SPI, I2C and UART with a built-in interpreter that shows the timing of clock and data transfers in the GUI. Demonstration signals are provided already on the board, by means of an LPC812 microcontroller.  This devices generates heartbeat PWM, four digital counters (at 750KHz, 1.5MHz, 3.0Mhz and 6.0MHz), plus SPI, I2C and UART data streams.  These signals can be used for quickly verifying the tools is up and running, and provides reference signals for comparing to your own design when measured by the LabTool.   Analog Channels   2 channel oscilloscope sampling at 80Msps (1ch), 40MHz (2ch), with 6MHz bandwidth rating.  The voltage range that can be sampled is a very wide range at +/- 25 volts.  Input impedance is 1Mohm. 2 channel analog output generation at 40KHz bandwidth, at +/- 5 volts.  Three built-in waveform generators support sine, square and triangle waveforms.   GUI   LabTool comes with a feature rich software interfaced developed by Embedded Artists.  The GUI gives users the capability to manage the digital and analog channels through: Dialogs for selecting digital and analog inputs channels One-shot and continuous sampling Sorting and moving of signals Applying application-specific signal names Saving settings in a project file Exporting collected data to .csv formatted files Appling SPI, I2C or UART protocol analyzers to selected channels Using four cursors to measure and interpret waveforms     Open Source Environment   The GUI is developed using Qt framework, and can be provided as open source. Source code for the firmware operating on the LPC4370 is also planned to be released for use among the community of NXP users.  Developers are encouraged to use this firmware as a starting point for creating exciting new applications based on LPC4370! Getting Started   A comprehensive user guide for the LabTool is available from Embedded Artists at the link given above. Tips for getting started:   Refer to the user guide and notes on Embedded Artists web site for the most recent instructions.  Here are some tips that have helped our testers and expert industry users to get started smoothly.   Install the GUI software first.  USB drivers (needed at step #2 below) are copied to the installation folder during this step. Attach the LabTool add-on board to the Link2 (see image below for proper orientation). Driver installation may take several minutes, and is accomplished in two steps.   When the hardware is first connected to a USB port, the driver for the Link2 must be installed.  This driver is included with the LPC-Link2 Configuration Tool.  The device manager shows the hardware is enumerated as “LPC Device”. Once the Link2 driver is loaded, the next step allows the LabTool GUI to be started.  The first time the GUI runs, it will detect the LabTool hardware, and will load an additional driver.  This driver is located in a sub-folder from the location where the LabTool software package was installed.  The device manager shows the hardware is now enumerated as “NXP LabTool”   Once the GUI is running, check that “LabTool Device” is displayed in the section marked “Selected device” in the diagram above. The probe bundle has each wire function labeled on the silk screen of the PCB.  Check these carefully to find cable D0, and connect it to the demonstration signal  labeled “PWM_LED” on the header at the bottom right corner of the board.  In the GUI, choose “Add Signal” and select D0 as an input channel; press OK.  Set a falling edge trigger and a sample rate of 2MHz.  Choose continuous sampling, and view the results in the waveform view.  It’s that simple!   Correct Orientation   Correct orientation is required.  Be sure the expansion headers on the Link2 are aligned properly to the connectors on the LabTool add-on board.  The USB port is located at the end opposite from the BNC connectors.     Industry Experts and NXP Testers   We asked leading experts in the embedded community to test the LPC4370 and LabTool, create some test code, and let us know what they thought of the whole process.  Below are their evaluations:   Industry Experts   Kevin Townsend has been working with LPC microcontrollers since the ARM7 LPC2000 products were released. He specializes in ARM Cortex-M0/M3/M4 design and development with interest in low power and wireless sensors. He is active in the open source HW world as Lead Engineer at Adafruit Industries. Kevin tested the LPC4370 and wrote a review on his blog site, www.microbuilder.eu. To read his insightful commentary follow this link.   Bob Boys is a Product Manager for Keil MDK and ARM DS-5 tools at ARM with multiple years of experience in the industry. He holds a Masters in Information Sciences and has worked with a variety of hardware and software platforms around the ARM Cortex family of products. Bob decided to test out the oscilliscope feature of the LabTool. See his review below.   Dirceu Rodriguez, Jr. is a computer engineer with a master's degree in electrical engineering. As an independent consultant, he tests new products with particular interest in the areas of wireless sensor networks, ARM processors, DSP, motor control, and medical applications. (Review coming soon)   Massimo Manca has 20+ years of experience in the industry. He has worked on a variety of applications with more than 30 different microcontroller families. Massimo gave the LabTool and Link2 a thorough testing on all parts.  Initial comments are provided below, with an additional review coming soon.   NXP Testers NXP Application Engineers have tested the LPC4370 and LabTool for themselves.  Their feedback and use cases are shown below.     Using the SPI Protocol Analyzer     Using LabTool to evaluate Rotary Encoder and QEI peripheral     Investigating I2C/SMBus issue using LabTool     Comparing the LabTool to a commercially available signal analyzer   Evaluations and Reports Kevin Townsend hosts a blog on his microbuilder.eu site. Read his insightful commentary here.   Bob Boys from ARM, Ltd. wrote:   I tested the scope part as this is what I am most interested in.  LabTool in this respect worked quite well compared to other USB scopes I have used that cost mush more.  I tested it on a two node CAN network and the SWO Serial Wire Output: both on a Keil MCB1700 (LPC1768) board.   I liked these things: 1)    Easy to change from neg/pos slope or no trigger. 2)    Changing the trigger point was very easy although I liked using the no trigger setting better to initially get a waveform going. 3)    Determining the timing was easy and surprisingly accurate.  At first I was getting very bad frequencies but after I calibrated the LabTool per the instruction it was fine. 4)    Setting the cursors was easy – but see point 5 below. 5)    The waveform faithfulness compared to my HP 100 mHZ scope was quite good. 6)    Installing the software was easy although I had some initial trouble with the USB drivers – it could detect it and under device the labtool Device was grayed out.  I had to uninstall the previous LPC-Link 2 USB drivers (which had worked OK for me) – it showed it was not installed correctly or something like that -  it had a small yellow icon in Device manager.  Now it works fine. 7)    Single shot and continuous collection works easier than on my HP.   I thought these could be improved: 1)    The scope selection is called Analog.  I was confused – why not just label it scope ? 2)    I had some difficulty getting a waveform displayed sometimes – I had to fiddle with it. 3)    I was not able to erase a waveform so sometimes I didn’t know if I had  a new one or nothing or ????  Making this part easier to use might be worth it. 4)    I could not make the waveform bigger or shift it up or down (position). 5)    When I clicked on a cursor icon to bring it up into the screen – the waveform shifted and it looked like (to me anyway) to have disappeared.  It was there – It took me a while to figure this out. 6)    CAN is a differential signal but it seemed to work.  A differential input would be nice.  So would a CAN Analyzer. 7)    I had a hard time getting the “DC” to work – “AC” was always better and easier. 😎    The ability to change the waveform colour might be a good idea.   Following are the results of two tests.   CAN on one channel: 1)    500 kHz is correct ! 2)    The waveform (at 80 MHz) is good – the overshoots are not visible on the HP but I didn’t adjust the tiny capacitor screws on the LabTool.  There are more of the resolution errors shown on the rise and fall edge than my HP – but HP still has some.  Not a big deal. Here is the CAN frame using two channels:  Even though I had to reduce the sampling freq to 40 mHz – it still looks good.   The ability to move the waveforms vertically (and maybe a polarity switch) would be nice.     SWO: Very often customers must measure the frequency on the SWO pin if they can’t get the Serial Wire Viewer (SWV) working and they do not know what their CPU clock is. A scope makes this easy and – LabTool did very good – I think sometimes the SWO pin can go up to 1 mHz and more – but this example at 1.25 worked fine. 1.25MHz as shown here is correct ! I compared all these waveforms to my HP and LabTool did quite well. Massimo Manca wrote:   After some hours of test my feeling is that the digital part works quite well, the I2C, SPI and UART interpreters are useful and well designed. Should be very interesting to have also a CAN interpreter and a 1-Wire interpreter.   Another thing should be useful is to define the priority of the triggers on the digital signals. I mean that should be useful for instance to define the trigger on the UART - D0 line with the highest priority so the other signals will be captured only it is already captured on its trigger front.   I should need to go back to my lab to test better the analog inputs. My feeling is that the signal is not perfect due to some interference by my laptop. Should be interesting to connect a USB isolator between the boards and the PC to see what changes.   The next step will be to test the board freely always using the demo signals without following the example list. I will provide update with the results.   Using the SPI Protocol Analyzer   Lately I’ve been working with one of NXP’s solution kits.  This kit includes an LPC812 Xpresso board and a daughterboard with the SEN300 sensor.  The sensor measures temperature, humidity and light.  It interfaces the microcontroller through a 4-wire SPI bus (SCK, MISO, MOSI, CS) running at 300kHz.   Considering that an end user of this solution kit may want to add another node on the SPI bus, it should be necessary to increase the communication rate from 300kHz to a higher speed, and allow for transfers to/from the additional device using the same SPI peripheral.  Types of SPI devices that could be considered are a simple LCD for displaying the sensor readings, or an EEPROM for data logging.   After I selected new dividers for the SPI master clock to increase the clock rate to 3MHz, the communication interface broke down.  I setup the LabTool digital interfaces D0 to D3 and configured the SPI protocol analyzer to use these for the corresponding SPI signals.  Following are some screen shots and the conclusion of the problem.   Normally the communication seemed to be occuring just fine.  I noticed that the chip select signal (Digital 3) was active low outside the boundaries of the waveform view in the LabTool GUI. From time to time, actually more often than not, the SPI analyzer could not interpret the transfer data, and showed “Frame Error” was occurring.   By changing the trigger to the rising edge of the chip select, I could see this occurring more frequently.  At that time, the chip select signal was momentarily toggling high/idle and then low/active in the middle of a data transfer.   I began stepping through the code to find the routines that set and cleared the state of the chip select (a simple digital output port).   I found that the routine that handles the SPI transmit/receive buffers could get out of sync with the function controlling the chip select output, and cause message transfers to overlap.  By adding some simple logic to ensure the chip select was not idled before the SPI buffers were serviced, the problem went away.  Here is a screen shot of a good SPI transfer at the higher SCK rate.   Using LabTool and the SPI protocol analyzer feature, I was able to identify the problem in the communication interface, and then use a debugger to finish checking the root cause.   Using LabTool to evaluate Rotary Encoder and QEI peripheral   Motor control applications often use the feedback from a rotary encoder in a closed loop control system.  The LPC4370 microcontroller includes a QEI peripheral (Quadrature Encoder Interface) that decodes these signals directly.  By monitoring both the number of pulses and the relative phase of the two signals, you can track the position, direction of rotation, and velocity.  In this example, we’ve measured the QEI signal sequence with LabTool.  The type of Rotary Encoder used in this project is SXA-4EG05E1024BM with 1024 pulses per round.   The encoder ouputs A,B and Zero terms. So we connect the encoder with LabTool through DIO0~DIO2. LabTool should also be connected with the Encoder’s gound pin to ensure they share a common gound.  Use one of the available grounding probes on the 26-pos connector (e.g. probe #4), to make this connection.   DIO0 -> A Term   DIO1-> B Term   DIO2-> Zero   Open the LabTool application program on your PC, and connect the LabTool using the USB connection. The GUI will show that LabTool is connected when the text "LabTool Device" changes from red to black text.  Now, you can click the “Add Signal” button and choose D0, D1 & D2 digital signals as below picture shows. We’ll rotate the Encoder by hand, so we set the “Sample Rate” as 100kHz.   Set the D2 Digital capture on rising edge.   Click the “Capture->Continuous” or button to start sampling the digital input channels.  When we rotate the Encoder, the signal capture below is displayed with LabTool. We can move the triggers C1&C2, C3&C4 to measure the signal’s frequency and duty cycle.   If we want to measure a whole cycle from the Encoder, we can set the “Sample Rate” as 50Mhz, then rotate the Encoder and capture the entire waveform shown next. LabTool's logic analyzer feature is very powerful and useful for motor control applications measurng the feedback from a rotary encoder.   Investigating I2C/SMBus issue using LabTool   One of our customers is designing-in the NXP Microcontroller in a SAS (Serially Attached SCSI) Server system. This controller is used to manage the overall backplane activities and interfaces to the host SAS Controller on SMBUS/I2C Bus. The customer was facing major issue of I2C Bus hanging.  As such, it was difficult to diagnose the issue as there were multiple slave devices on the bus. Coincidently, we had this LabTool lying around and I thought of using it in debugging the issue. Initially, I isolated this controller from the I2C bus and hooked it up to another I2C Master. While monitoring the bus activity on the LabTool’s I2C Analyzer, apparently the overall communication was just fine as shown below.   On a closer look, I noticed that the clock (SCL) was getting stretched a bit at times, but nothing unusual. I then connected this controller back in the system and monitored the I2C bus activity on I2C Analyzer again. And no surprise, the bus hanging problem was getting reproduced as seen in the capture below. After the clock stretching interval, the clock (D2=SCL) line was holding it’s status as low and data (D1=SDA) was high. It was clear that the problem appears only when there are multiple slaves connected to a SMBUS/I2C Bus Master. It gave me some direction to think and investigate more on similar lines. Gone through the details of SMBUS/I2C peripheral on SAS Controller and as usual googled for I2C issues with multiple slaves.  Finally got a clue while going through the minute details of SMBus specifications. Though it’s normal to use I2C slaves/devices with SMBus master and vice a versa, there are subtle differences in the specifications. The most vital difference is the Timeout and (as a consequence of timeout) minimum clock speed. There’s no time out in I2C specifications, any device can stretch the Clock as long as it wants. While the SMBus clearly specifies the time out of 35msec, where slave devices resets their interfaces whenever Clock goes low for longer than the timeout. Use of such timeout also dictates a minimum speed for the clock, because it can never go static. Thus, the SMBus has a minimum-clock-speed specification of 10kHz.   To comply with the SMBus specifications Slave devices should have this time out implemented. I then added a small piece of code to generate this timeout using one of the available timers and that resolved the issue. Thanks to the LabTool!   Comparing the LabTool to a commercially available signal analyzer   There are three key features of LabTool that are useful to any developer:   80MHz sample rate using digital inputs D0 to D3 and up to 60MHz for one Analog Input. You can analyze any UART, SPI or I2C communication. You have 4 cursors to measure your signals.   Here is a comparison versus another USB-hosted signal analyzer.  We will call it "AnalyzerB" in this article.   Features and Price: Regarding AnalyzerB, the cheaper option is the product SX at $169.0 USD, it has only 8 digital input/output with a maximum sample rate of 24MHz. The most comparable product will be the AX product with a pricing of $795 USD with also 8 digital input/output with 2 analog oscilloscope inputs but you can capture maximum at 24Msps and only one analog input at any time. The AX product also can analyze CAN, PS/2, SM bus and 1-Wire communication. These options could be added easily to the PC software.   So, the pricing of $129.00 USD for the NXP LabTool is a very good pricing and with the source code available you won't have any limit to customize or improve the LabTool.   Using the Tools: I did a zoom in the PWM signals in order to get a more detail measurement and I will compare these signals measurements with the AnalyzerB tool.     D7 is 2MHz D8 is between 3.33MHz and 5MHz D9 is between 3.33MHz and 2.5MHz D10 is between 1.42MHz and 1.66MHz I had these measurements because the sample rate is at 10MHz and LabTool is using the upper channels. Now I did a measurement using AnalyzerB tool.  It couldn’t read the 12MHz signal (channel 0); the sample rate is at 12MSPS. I had to increase to 24MSPS (MAX) in order to be able to measure the 12MHz signal. The frequency measurement in each signal was exactly 1.5MHz channel 3, 3MHz channel 2, 6MHz channel 1 and 12MHz channel 0 without any variation.   Now, using the LabTool I change the 4 PWM signals to channels 0 to 3 and increase the sample rate up to 100MHz. I had the following:   The frequency in the signals is: D0 is 12.5MHz and 10MHz D1 is 6.25MHz and 5.55MHz D2 is 2.94MHz and 3.12MHz D3 is 1.51MHz and 1.47MHz   The AnalyzerB tool didn’t show any variation in the frequency measurements. It might be because the LabTool has more precision. I went up to 100MHz sample rate and I had the same frequency measurements in each signal. Maybe the AnalyzerB is using some other method to implement an average or it might be over sampling to improve the measurement. I might need to have a third logic analyzer to see what tool is getting a right measurement.   I had some trouble using the LabTool GUI.  For example, I didn't know that LabTool is connected at first since the "LabTool Device" indication was not highlighted.  Also it was difficult to know how to choose the protocol analyzer, so that Combo Box could be improved.  It is clear that the LabTool has more resolution when using the lowest channels. The AnalyzerB tool has only a maximum of 25MSMP for all combinations. So the LabTool has an advantage because it could be 100MHz sample rate in 2 digital channels.   I like the LabTool but it might be a good idea to include test clips for each of the signals because not all the time the target circuit will have pins to plug the actual test points. These test clips will give more functionally to the LabTool.  Also, I would like to have more information about the actual LabTool system if it will be like a reference design for customer, like the source code for the LabTool software and also the firmware for the MCU.   The LabTool could be used for debugging without any issue; I think that the Start Guide should be updated with more detail information to improve the usability.
查看全文
Description The brushless DC (BLDC) motor control design example describes how to connect and control up to four brushless DC motors using a single NXP microcontroller from the ARM968-based LPC2900 series, making this a low cost solution. Four dedicated motor control PWM blocks keep the CPU load low while running four motors. This allows the microcontroller to still perform other tasks in Hardware used Hitex LPC2939 or LPC2929 evaluation board Hitex BLDC motor control extension board (4x) Interface board Maxon EC32 80W brushless servo motor with Quadrature Encoder Interface (QEI) Three of the Hitex BLDC motor boards are driven as-is (spinning their on-board motors). The fourth board is driving the Maxon EC32 motor using the quadrature encoder interface. The interface board is used to create the correct pin-out that makes it possible to connect the four motor control extension boards to the LPC29xx evaluation board. Block Diagram Documentation BLDC Motor Control Products Below are recommended microcontrollers for use in BLDC motor control applications. Comparison Table Product Pins On-Chip Flash On-Chip RAM Comments LPC2939 208 768KB 56KB Base microcontroller used in the design example. LPC2930 208 0KB 56KB A lower-cost microcontroller with the same amount of pins but without on-chip flash memory. LPC2929 144 768KB 56KB Same on-chip memory as on the LPC2939 but in a smaller package and without USB Host functionality. LPC2927 144 512KB 56KB Same as LPC2929 but with less on-chip flash memory. More Information Image BLDC Motor Control Demo at ESC SV 2009 Schematics LPC2939 Evaluation Board BLDC Motor Control Extension Board Interface Board Example Code BLDC Motor Control Bill of Materials BLDC Motor Controlhttp://www.lpcware.com/sites/default/files/bom.xls Disclaimer This design example shows possible hardware and software techniques used to implement the design. It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application. This design example may include information from 3rd parties and/or information which may require further licensing or otherwise. Additional hardware or software design may be required. NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example. lpc2939.eval_.board_.schematics.pdf 143.6 KB documentation.pdf 243.48 KB bldc.board_.schematics.pdf 188.85 KB interface.board_.zip 2 MB example.code_.zip 72.55 KB bom.xls 3.87 KB
查看全文
#isp‌ #bootrom‌ #memremap‌
查看全文
This content was originally contributed to lpcware.com by Steve Sabram This example project implements acoustic range, finite infinite response (FIR) filters using the LPC4350 demo board and the ARM CMSIS DSP library. A sound resource of a science fiction “zap gun” plays out the headphone jack of the demo board. This sound sample is great for demonstration since it has many low-, mid-, and high-frequency components along the acoustical band. You play the sound resource by touching the capacitive touch buttons on the demo board as explained by the menu shown on the demo board’s LCD. It is best to listen to the sound with a headphone or ear buds. Each of the four buttons plays the same sound resource differently: 1)  Raw – The unprocessed sound plays according to its format (sample rate of 44.1 kHz, 16-bit sample and mono sound). 2)  Low Pass – filtered through a low pass, Butterworth filter with a cutoff of 5 kHz, similar to the bandwidth of a common analog telephone. When played, notice that high pitch components are removed similar       to the sound heard over a telephone. 3)  High Pass – filtered through a high pass, Butterworth filter with a low frequency cutoff of 8 kHz. Notice that the sound is lower in volume since only the upper harmonic components are played. 4)  Backward Mask – The sound resource sample plays in reverse order. The “Zap!” is now a “Zoup!” The digital filters were designed with a favorite public domain tool, WinFilter (http://www.winfilter.20m.com/)       accompanying this example. With exposure of this free DSP design tool via NXP, I hope its author expands its features.
查看全文
Description The Telephone Answering Machine Design Example is a sophisticated telephone answering machine that provides everything commercial devices offer and more. Noteworthy features include improved voice quality and increased storage capacity over commercial machines. Additionally, Internet connectivity enables convenient messaging in the form of SMS messages or e-mails from anywhere in the world. Virtual answering machines can be set up for four different users. A user-friendly interface makes learning how to use this device and taking advantage of its many special features easy for anyone, regardless of their electronics savvy. The highly efficient system is designed around an LPC2138 microcontroller, which features an ARM7 RISC processor. Built with a small handful of components, the Telephone Answering Machine Design Example is cost-effective. The thoughtful inclusion of an external flash memory card and well-chosen algorithms for nearly unlimited storage capacity of crystal-clear messages contribute to the success of the design. Block Diagram Documentation Telephone Answering Machine Products Below are recommended microcontrollers for use in implementing a telephone answering machine. Comparison Table Product Pins On-Chip Flash On-Chip RAM Comments LPC2138 64 512KB 32KB Base microcontroller used in the design example. LPC2136 64 256KB 32KB A lower-cost microcontroller with the same amount of on-chip RAM but with only half the on-chip flash memory. LPC2146 64 256KB 32KB + 8KB An upgraded microcontroller with a USB interface. USB could be used instead of Ethernet to connect to a PC if Internet functionality is not desired. More Information Images Working Prototype Circuit Blocks Answer Flow Telephone Answering Machine Schematics Example Code Bill of Materials Disclaimer This design example shows possible hardware and software techniques used to implement the design. It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application. This design example may include information from 3rd parties and/or information which may require further licensing or otherwise. Additional hardware or software design may be required. NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example. documentation.pdf 927.44 KB schematics.pdf 92.13 KB example.code_.zip 646.98 KB bom.txt 1.39 KB
查看全文
Description The Audio Player Design Example, based on an NXP LPC2138 ARM7-based microcontroller, delivers high-quality, uncompressed, 16-bit digital audio playback. This design allows engineers to add MP3 music or sound effects to a variety of consumer applications at a very low cost. Entertaining sounds could be added to children's items or music clips could be easily added to products targeted at teens. There is no limit to the number of existing applications that could be enhanced by inexpensively adding high-quality sound or music. Block Diagram Documentation Audio Player Products Below are recommended microcontrollers for use in implementing this design to a system. Comparison Table Product Pins On-Chip Flash On-Chip RAM Comments LPC2138 64 512KB 32KB Base microcontroller used in the design example. LPC2136 64 256KB 32KB A lower-cost microcontroller with the same amount of on-chip RAM but with only half the on-chip flash memory. LPC2146 64 256KB 32KB + 8KB An upgraded microntroller with more on-chip RAM allowing for a real-time MP3 software decoder. The added USB interface allows file transfer with a personal computer. LPC2148 64 512KB 32KB + 8KB An upgrade to the LPC2138 microntroller, the LPC2148 substitutes Full-speed USB 2.0 device functionality for a slightly higher cost. More Information Images Working Prototype DAC Circuit                                                       SD Card InterfaceSchematics Audio Player Example Code Audio Player Disclaimer This design example shows possible hardware and software techniques used to implement the design. It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application. This design example may include information from 3rd parties and/or information which may require further licensing or otherwise. Additional hardware or software design may be required. NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example. documentation.pdf 418.54 KB schematics.zip 123.65 KB example.code_.zip 719.42 KB
查看全文
Welcome to the LPC4350 Hitex Board Getting Started Guide! This page will walk new owners of the LPC4350 development platform from Hitex through bringing the board up with the example projects. Connecting the Hardware Here is a photo of a typical hardware setup. The board is connected to a PC through a JTAG debugging interface and a USB-serial cable. +5V center-positive power is also applied to X14. If a 5V regulated power supply is not available, the board may be powered by USB connected to one of the USB connectors using the included cable. To date we have tested this board with a Keil ULink 2, ULink Pro, and the Segger JLink but any JTAG-capable tool should be able to debug with the LPC4350. The example projects should run without modification on Keil MDK. To see the debugging output from the example code on the serial-to-usb cable, first the driver must be installed. Many cables use chips from FDTI and the drivers can be downloaded from here: FDTI VCP Drivers. To view the serial output, any standard terminal program such as Tera Term can be used. LPC4300 Hitex Board with Connections LPC4350 PDL Examples and Flash Drivers The example code for this board can be downloaded from here: LPC4350 PDL There are 53 code examples. Once the code has been downloaded, it should be unzipped. The unzipped peripheral driver library includes an Examples directory containing examples that work with each peripheral on the LPC4350 dual-core microcontroller. Also included are flash drivers located in the Tools\Flash\Keil_Binaries directory. If using ARM/Keil MDK V4.22 and earlier, these should be copied to the C:\Keil\ARM\Flash directory. Later tool versions should include these drivers. LPC4350 PDL Examples and Flash Drivers If you are using the Hitex LPC4350 board using the ARM/Keil MDK, the driver library projects have several configurations built-in. They can build for Internal SRAM, build for SPIFI (external 1 MB QSPI flash on the Hitex board), or build for Hitex Flash (external parallel flash on the Hitex board).The best performance will be achieved with building for Internal SRAM, but if you would like the board to boot on its own without a debugger, then the code will have to be built either for SPIFI or for Hitex Flash. LPC4350 PDL Keil Project Configurations LPC4350 PDL Boot Jumpers Once you have successfully programmed the flash on the Hitex board, there is one step left before the LPC4350 can boot from external flash. That final step is to configure the boot mode using the boot mode jumpers. LPC4350 PDL Boot Jumpers Here is a diagram that shows how to configure the boot jumpers on the LPC4350 Hitex board. The boards are shipped with the center two positions shorted with jumpers. This configures the LPC4350 to boot from the "EMC" (External Memory Controller) which is connected to the parallel flash on the Hitex board. When using the sample projects with the Keil tool, after building a project, the LOAD button can be used to program it into Flash memory for stand-alone booting. To debug a project that has been programed in to Flash, you may need to click the LOAD button to configure the memory controller on the LPC4350 (if it has been reset) before entering debug mode. LPC4350 PDL Boot Jumper Diagram We can ship boards with two example projects flashed in them- one loads when the board is configured to boot from Parallel Flash, and a second loads when the board is configured to boot from QSPI flash. Recent boards are shipped with a Mass Storage Class ROM USB demo in parallel Flash and an LED/button demo in QSPI Flash. Using the SD/MMC Card Slot The SD/MMC Card Slot, on the right edge of the board in the photo above, can accept an SD card to read and write data. Before this slot will work properly, several jumpers must be configured on the Hitex board. The jumpers needed are: Jumper Block Jumper Settings SV3 positions 7-8 and 13-4 must be open SV6 positions 1-2, 3-4, 7-8, 15-16, 17-18 must be open SV12 all positions must be shorted JP9 position 1-2 must be shorted Next- load the Usb_MassStorage example from the USBDEV_ROM directory. This Mass Storage Class example has been extended with sdio drivers. Insert an SD card (we have tested 2GB) into the SD connector on the right side of the board. Connect X2 (USB1, high-speed) to a PC. You should see a disk drive on the PC and be able to read and write the SD card. Operation at 204 MHz The LPC4350 is qualified to operate at up to 204 MHz, but normally starts up at a slower speed to make design easier. In particular, even if memories and power subsystems are not designed to support 204 MHz, booting is still possible. To run the LPC4350 at 204 MHz, take a look at the BOOTFAST example project. This project supports the same configurations (SRAM, Parallel Flash, and QSPI Flash) as the other examples, but after startup, it relocates some code to internal SRAM, and then it reconfigures the parallel flash and SPIFI peripheral to a high speed mode and increases the clock speed to 204 MHz. This is a good way to see how a standard system would boot. Typically, the most critical code would also be located within internal SRAM which runs at 204 MHz with zero wait states while other less performance-intensive code could be located in external Flash, SRAM, or QSPI flash which are set up to run at 102 MHz in this example. Multi-Core Operation The LPC4350 contains two cores, a Cortex-M4 and a Cortex-M0 which both operate at 204 MHz. An example that demonstrates how you can use the cores together is located in Examples\DUALCORE\Mbx_Demo. This example sets up a mailbox mechanism to facilitate communication between the two cores. The M0 core is assigned the task of outputting serial communications via UART 1. This example includes a multi-project workspace. Once the workspace is opened, the M0 project must be built first before the M4 project can be built. For more details, see the abstract in the M4 project. State Configurable Timer (SCT) The LPC4350 contains a special timer called the State Configurable Timer (SCT). The SCT is a timer with a state machine integrated into it. It is great for doing complex signal generation such as PWM waveforms. An SCT example is provided in the LPC4350 code repository which emulates the behavior of a simple traffic light. The example is called SCT_TrafficLight and is in the SCT subdirectory of the Examples directory in the code bundle. To use this example, you must assemble a PCB with four LEDs and two pushbuttons. Here is a photo of an example board: SCT Traffic Light SCT Traffic Light Schematic The traffic light should be connected as follows: Signal Port Connector Signal Wire Color CTOUT_0 P4_2 X11, pin 7 Red LED red CTOUT_1 P4_1 JP20, pin 2 Yellow LED yellow CTOUT_2 P4_4 JP22, pin 2 Green LED green CTOUT_3 P4_3 X11, pin 6 White LED red CTIN_2 P4_10 X11, pin 13 WALK Button blue CTIN_3 P7_3 SV18, pin 16 RESET button yellow GND ADC ADC, GND Common black Traffic Light Connections If you would like to edit the state machine used in the traffic light example, you will need to use the LPCXpresso or Red Suite tool, which has "Red State," a state-machine editor, built-in. Here is an image of the state machine used in the traffic light example: Traffic Light Diagram Once you have edited the state machine, click "Generate Code." You can test the state machine within LPCXpresso if you have a Red Probe or an LPC-Link probe, or you can copy the following source code files from the LPCXpresso project over to the Keil SCT project: sct_fsm.c, sct_fsm.h, and sct_user.h and make use of a JLink or uLink. Serial GPIO (SGPIO) The LPC4350 contains a peripheral called Serial GPIO which is similar to a bank of shift registers with some extra logic for bonding and counters for timing. The SGPIO is great for implementing standard or custom digital data interfaces. To demo this peripheral, we have configured it to implement four I2S ports to add 7.1 8-speaker audio capability to the LPC4300 family. The example for this will soon be provided in the LPC4350 code repository. The example will be called SGPIO_71 and will be in the SGPIO subdirectory of the Examples directory in the code bundle. To use this example, you need a demonstration PCB with four stereo audio codecs on board. Here is a photo of an example board: LPC4350 Codec Board The codec board should be connected as follows: Signal Connector Wire Color MCLK SV16, pin 6 blue LRCLK SV3, pin 11 green SCLK SV5, pin 6 yellow GND GND post near U23 black V33 JP5, pin 2 red - - - SDIN0 SV13, pin 4 blue SDIN1 SV5, pin 4 green SDIN2 SV16, pin 4 yellow SDIN3 SV3, pin 3 blue LPC4300 Hitex Codec Connections Once you have connected the codec board, you should be able to connect the Hitex board to your PC using a USB cable to connector X2. After running the example project, a stereo USB speaker device should appear on your PC which can accept audio and mirror it onto two of the stereo audio channels.
查看全文
View Webinar Recording
查看全文
        In recent years of MCU technology evolving, booting from the external flash seems to become more and more popular, actually, LPC already has employed this technology for many years.         NXP's recently released the LPC540xx family which continues the trend of high-performance flash-less MCU.         The developers may be a bit confused with the external FLASH which is used for storing the program, as they are used to directly using the internal FLASH for programming and debugging the chip. But, don't worry, let me introduce it in the following sections. LPC54018's three ways of loading program        In general, RAM stores data, however, RAM can also store programs. In previous projects, we occasionally move some key functions in RAM in order to improve the execution speed of these programs. The current implementation is to put all the programs in RAM more thoroughly. Based on this idea, you can directly use the debugger to load the executable image into the on-chip RAM and this method is called RAM TARGET.       After downloading the executable program image file to the external flash, when the bootloader loads the complete image to on-chip RAM to run, the method is called the Plain Load Image method.             Actually, both of these above ideas are routine, chip designers have also created a "super-capability" that allows the chip to directly execute external FLASH programs (Execute In Place, XIP). With this 'superpower', no matter whether the program boot from the external FLASH or the internal FLASH, there is no difference in operating performance.       The RAM TARGET method mentioned above is only suitable for debugging the application. Once the chip is powered off or reset, the downloaded program in the RAM will disappear. Meanwhile, the size of the RAM also give some restrictions for debugging.        In the Plain Load and XIP modes, the executable image file is stored in the external flash. After MCU is powered, the bootloader which is resided in ROM copies the first 512 bytes from the image (vector components and image header) into internal SRAMX at location 0x0000 0000 to validate the vector table and image header to confirm the booting mode. And the program will not be lost after power-off or reset. Fig1 illustrates the boot process of LPC54018. Fig1 LPC54018 boot process flow Experiment show         Board: LPCXpresso54018 board (OM40003) Fig1 LPCXpresso54018 board       Demo code: Hello world (From the SDK), modifying the hello world code in below way, which points out the load program way and date time. PRINTF("hello world. XXXXXXXX \r\n");    PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍ Experiment 1: RAM Target         Demo code: Hello world (From the SDK), modifying the hello world code in below way. PRINTF("hello world. RAM Target \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍      Note: Setting the Reset: Core when debugging the demo Fig2 Setting the Reset: Core Running testing: As the Fig3 illustrates, it would print the below message when debugging the demo, however, after reset, it would run the plain load image which is programmed before, as the RAM lost the hello world demo. Fig3 RAM Target runing testing Experiment 2: Plain Load Image        Demo code: Hello world (From the SDK), modifying the hello world code in below way. PRINTF("hello world. PLAIN LOAD IMAGE \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍‍      Download image to external flash:        1. Build the demo to generate a bin file.           This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.        2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):             a. Open SEGGER J-FLASH Lite, select device LPC54018.             b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)                 Note: if can not success( press SW4 and reset the board, and try to erase again) Fig4 Erase the external flash              c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device' Fig5 Program the external flash Running testing: Fig6 illustrates the result of  running the plain load image. Fig6 Plain load image runing testing Experiment 3: XIP Image        Demo code: Hello world qspi_xip (From the SDK), modifying the code in below way. PRINTF("hello world. PLAIN LOAD IMAGE \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍‍‍      Download image to external flash:        1. Build the demo to generate a bin file.        2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):            a. Open SEGGER J-FLASH Lite, select device LPC54018.            b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)            Note: if can not success( press SW4 and reset the board, and try to erase again) Fig7 Erase the external flash           c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device' Fig8 Program the external flash      Running testing:      Fig9 illustrates the result of  running the plain load image. Fig9 XIP image runing testing  
查看全文
The following document contains a list of documents, questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in LPC or MCUXpresso you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table  FAQ: MCUXpresso Software and Tools  How to create a new LPC project using LPCOpen and MCUXpresso IDE  Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  Using the MCUXpresso Pins Tool   MCUXpresso Config Tools is now available!   LPC55xx Multicore Applications with MCUXpresso IDE  LPC information LPC5460x MCU Family Overview  USB with NXP Microcontrollers LWIP memory requirements  LPC800 Four-Part Webinar Series!  The LPC804 Programmable Logic Unit (PLU)   LPC84x Technical Training - Now Available Guides and Examples Flashing and Installing the new firmware and drivers for LPC11U35 debug probes  Enabling debug output  USB FLASH download, programming, and security tool (DFUSec)  DMA Ping-Pong application  Getting start with LPCXpresso54608 & emWin Graphics;  Capacitive Touch example using the LPC845 Breakout Board  OLED Display Application Example using LPC845 Breakout Board and SPI  Mixed-Signal Logic Analyzer & Oscilloscope (Lab Tool) Solution  LPC FAQ How to calculate the value of crystal load capacitors? Can I send a message with X/Y/Z bits in the ID?  What is the difference between error active and error passive? What is the sample point for?  How can I verify the configured CAN bitrate, using an oscilloscope? 
查看全文
This article is about how to use MCUXpresso Config Tool to create a USB project from start. The method is the same to all MCUXpresso Config Tool supported MCUs Demo: Creating USB composite HID mouse + keyboard project. Prequisities: LPCXpresso55S69-EVK MCUXPresso IDE 11.1.1 SDK package for LPCXpresso55S69 ,SDK_2.7.1_LPCXpresso55S69. The SDK has to be imported into MCUXPresso IDE (in Installed SDKs). Step by step guide is attached. Enjoy it :-).
查看全文
In this document, I will explain how to create a project to use the SPIFI library version 1.03 with the LPC4370. For this we will need the following tools: MCUXpresso IDE 10.2. Link LPC-LINK2 to use it as an evaluation board for the LPC4370. Link External debugger. In my case, I used another LPC-LINK2 board. LPCOpen v2_12 for the LPC4370, this version comes with the installation of MCUXpresso IDE. SPIFI library v1.3. Link Code Example lpcopen_2_12_lpcxpresso_ngx_xplorer_1830_SPIFI_v1.0. Link First, download and install all the tools needed. In your workspace of MCUXpresso we will import (1) three projects of the LPCOpen v2_12 for the LPC4370: periph_blinky, lpc_board_nxp_lpclink2_4370 and lpc_chip_43xx.  The LPCOpen zip file is in the next path of your PC: C:\nxp\MCUXpressoIDE_10.2.1_795\ide\Examples\LPCOpen (2) Extract the files of the zip named lpclibspifi_lpcxpresso_1.03_68 that we downloaded before. The folder that we need is spifilib_m4f. Drag and drop this folder into the Project Explorer on your workspace of the LPC4370, after choosing copy and you should see the spifilib_m4f in your Project Explorer. Once you imported correctly the SPIFI library, select the library (1) on the project explorer window and build it (2). Once you do this you should see that a new folder called Debug appear (3). Now we need to edit the properties of the periph_blinky example to add the library spifilib_m4f to the project. To do this, right click on the project and click properties. Once in the properties window click on C/C++ Build (1) > Settings (2) > Includes (under the section MCU C Compiler) (3). In the includes window click Add… (1) > Workspace (2) > spifilib_m4f (3) > inc (4) > click OK (5) on the window Folder Selection > click OK (6) on the window Add directory path. You should see the following on the include paths. Now, go to the libraries (1) option under the section MCU Linker, on the section Libraries (-I) click Add… (2) finally write the name of the library (spifilib_m4f) (3) and click OK (4). Under the section Library search path (-L) click Add… (1) > Workspace (2) > spifilib_m4f (3) > Debug (4) > OK (5). If you see the same as shown in the below image you are good to go so click Apply and close. To check if you did the below steps correct let’s do the following. On the project periph_blinky in the file systick.c include the file spifilib_api.h and compile the project. If the project compiles without problems it means that you imported correctly the spifi library. If you found problems please stop and repeat all the steps mentioned before. Now that we added successfully the library we can start to migrate the example for the LPC1830 that we download before. First, unzip the file lpcopen_2_12_lpcxpresso_ngx_xplorer_1830_SPIFI_v1.0. Once you unzipped the file go to the following path: spifilib_blinky > example > src. Open the file named Blinky.c and copy all the content of the file. Now go to the file systick.c on your workspace of MCUXpresso within the project periph_blinky, delete all the content of this file and paste what you copied before. Do not compile at this point or you will receive multiple errors! Go back to the path spifilib_blinky > example > src on your PC. Drag and drop the file called spifi_setup.c into the folder src of your project periph_blinky on your Workspace. Open the file that we just copy into our workspace and go to line 46 of the code. Here we are creating a buffer of 64KB that we will use later to write in the SPIFI. The __BSS(RAM3) is to save this buffer in the RAM block three of memory. The problem here is that the block of RAM3 in the LPC4370 is not big enough to store the buffer of 64KB (see below image), so let’s change this for either RAM or RAM2 that are big enough to store the buffer. Now that we added the spifi_setup file let’s go back to the systick.c file and add the external declaration for the function spifiSetUp. At this point, if we compile the project we shouldn’t see any problems, only some warnings because of the functions and variables that we are not using. We are almost done, we are missing the most important thing. With this demo you will be writing, deleting and reading the SPIFI memory, this means that you cannot be executing form the SPIFI flash memory. You need to move to the RAM memory all the functions that are going to make this. This is the reason why in the file systick.c we don’t have any function that interacts directly with the SPIFI, this will make much easier the work of moving all the functions that interact with the SPIFI memory to RAM. The function spifiSetUp is the one that will make all the tests on the SPIFI and it is in the spifi_setup file, so we will need to move this entire file to RAM along with the SPIFI library. We will use three different scripts to move the library and the file spifi_setup to RAM. You can learn more about this in the following community post: https://community.nxp.com/thread/389110. First, right click on the folder of the project > new > folder, the name of the folder must be linkscripts. According to the sections Relocating particular objects into RAM and Relocating particular libraries into RAM of the community post mentioned before we need to create three files in this new folder: main_text.ldt, main_rodata.ldt and main_data.ldt. To do this, right click on the folder linkscripts > new > file. Here is the content that you should have on the three files that we just created. Do not include on the files the text that is in bold, that's just for reference! File main_data.ldt *libspifilib_m4f.a:(.text*) *libspifilib_m4f.a:(.rodata .rodata.* .constdata .constdata.*) *spifi_setup.o(.text*) *spifi_setup.o(.rodata .rodata.* .constdata .constdata.*) . = ALIGN(${text_align}); *(.data*) File main_rodata.ldt *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .rodata) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .rodata.*) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .constdata) *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .constdata.*) . = ALIGN(${text_align}); File main_text.ldt *(EXCLUDE_FILE(*libspifilib_m4f.a: *spifi_setup.o) .text*) After finishing with the three files you are done with the demo! It’s important to mention that if you want to go inside the function spifiSetUp while debugging you need to set a breakpoint inside the function. While debugging we can see that before calling the function spifiSetUp we are running from the SPIFI flash memory and once we enter to the function we are running from RAM memory. Once we run the demo successfully we should see the following in a terminal and the LED1 will be blinking. Hope this guide is helpful! Best Regards, Victor.
查看全文
Dear Community User, We recently migrated content from the LPCWare.com forums into this community site. Migrated content can be found in the following two locations: LPCXpresso IDE for content from the LPCXpresso folder on the LPCWare.com forum, and LPC for all other content. All imported content will appear as posted by "LPCWARE" and will have the following message displayed at the top of each thread with the original username and date posted in LPCWare: If you wish to find the content you created in LPCWare you must: 1.-  Open the search box at the top right side of your community near your avatar. 2.- Type in the username you had set up in LPCWare and the results should automatically appear. All responses to postings in the original LPCWare.com forums are also preserved, so if you are looking for a response you or another particular user posted then you should also be able to locate those responses using the same search mechanism. All FAQs have been migrated to the NXP Community site. Several forum postings include references to FAQs and re-directs are in place to take you to their new location from those postings.
查看全文