LPC Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Microcontrollers Knowledge Base

Discussions

Sort by:
Overview          Ping-pong is a special case of a linked transfer which typically used more frequently than more complicated versions of linked transfers. A ping-pong transfer usually uses at least two buffers. At any one time, one buffer is being loaded or unloaded by DMA operations. The other buffers have the opposite operation being handled by software, readying the buffer for use when the buffer currently being used by the DMA controller is full or empty. The Fig 1 illustrates an example of descriptors for ping-pong from a peripheral to two buffers in memory. Fig 1 Implementation detail         To continuous transfer the converted result of the ADC to RAM, I’m going to use four 4 DMA descriptors to work in Ping-Pong mode to achieve this goal as the Fig 2 shows. Fig 2 Data flow via Ping-Pong mode Hardware introduction         LPCXpressor54114 Board(OM13089) Fig 3 LPCXpressor54114 Board        Demo code: LPCOpen Library Example code        The code is based on the periph_adc demo, using the SCTimer output as the hardware trigger of ADC, meanwhile, the ADC converted value is transferred to the appointed area of RAM automatically. #include "board.h" #define SCT_PWM            LPC_SCT #define NUM_BUFFERS 4 #define DMA_TRANSFER_SIZE 8 #define ADC_INPUT_CHANNEL 1 #define SCT_PWM_RATE   10000          /* PWM frequency 10 KHz */ #define SCT_PWM_PIN_OUT    7          /* COUT7 Generate square wave */ #define SCT_PWM_OUT        1          /* Index of OUT PWM */ uint16_t adcOut; ALIGN(512) DMA_CHDESC_T ADC_TransferDescriptors[NUM_BUFFERS]; uint16_t CapturedData[32]; uint16_t DMA_Sum=0; /** * * ADC IRQ not Used right now... Only for testing */ void ADC_SEQA_IRQHandler(void) {             /* If SeqA flags is set i.e. data in global register is valid then read it */         Chip_GPIO_SetPinState(LPC_GPIO, 0, 6, true);         //DEBUGOUT("ADC Output = %d\r\n", adcOut);         Chip_GPIO_SetPinState(LPC_GPIO, 0, 6, false);         Chip_ADC_ClearFlags(LPC_ADC,0xFFFFFFFF); } void DMA_IRQHandler(void) {         static uint16_t DMA_Sum=0;                 DMA_Sum++;                  if(DMA_Sum ==8)          {            DMA_Sum=4;          }             Chip_GPIO_SetPinState(LPC_GPIO, 0, 7,true);      /* Rrror interrupt on channel 0? */      if ((Chip_DMA_GetIntStatus(LPC_DMA) & DMA_INTSTAT_ACTIVEERRINT) != 0)      {           /* This shouldn't happen for this simple DMA example, so set the LED              to indicate an error occurred. This is the correct method to clear              an abort. */           Chip_DMA_DisableChannel(LPC_DMA, DMA_CH0);           while ((Chip_DMA_GetBusyChannels(LPC_DMA) & (1 << DMA_CH0)) != 0) {}           Chip_DMA_AbortChannel(LPC_DMA, DMA_CH0);           Chip_DMA_ClearErrorIntChannel(LPC_DMA, DMA_CH0);           Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);           Board_LED_Set(0, true);      }      Chip_GPIO_SetPinState(LPC_GPIO, 0,7,false);      /* Clear DMA interrupt for the channel */      LPC_DMA->DMACOMMON[0].INTA = 1; }      /***       *      ____  __  __    _       *     |  _ \|  \/  |  / \       *     | | | | |\/| | / _ \       *     | |_| | |  | |/ ___ \       *     |____/|_|  |_/_/   \_\       *     / ___|  ___| |_ _   _ _ __       *     \___ \ / _ \ __| | | | '_ \       *      ___) |  __/ |_| |_| | |_) |       *     |____/ \___|\__|\__,_| .__/       *                          |_|       */ void DMA_Steup(void) {         DMA_CHDESC_T Initial_DMA_Descriptor;                 ADC_TransferDescriptors[0].source = (uint32_t)&LPC_ADC->SEQ_GDAT[0];      ADC_TransferDescriptors[1].source = (uint32_t)&LPC_ADC->SEQ_GDAT[0];      ADC_TransferDescriptors[2].source = (uint32_t)&LPC_ADC->SEQ_GDAT[0];      ADC_TransferDescriptors[3].source = (uint32_t)&LPC_ADC->SEQ_GDAT[0];      ADC_TransferDescriptors[0].dest = (uint32_t)&CapturedData[(0+1)*DMA_TRANSFER_SIZE-1];      ADC_TransferDescriptors[1].dest = (uint32_t)&CapturedData[(1+1)*DMA_TRANSFER_SIZE-1];      ADC_TransferDescriptors[2].dest = (uint32_t)&CapturedData[(2+1)*DMA_TRANSFER_SIZE-1];      ADC_TransferDescriptors[3].dest = (uint32_t)&CapturedData[(3+1)*DMA_TRANSFER_SIZE-1];      //The initial DMA desciptor is the same as the 1st transfer descriptor.   It      //Will link into the 2nd of the main descriptors.      ADC_TransferDescriptors[0].next = (uint32_t)&ADC_TransferDescriptors[1];      ADC_TransferDescriptors[1].next = (uint32_t)&ADC_TransferDescriptors[2];      ADC_TransferDescriptors[2].next = (uint32_t)&ADC_TransferDescriptors[3];      //Link back to the 1st descriptor      ADC_TransferDescriptors[3].next = (uint32_t)&ADC_TransferDescriptors[0];      //For a test,  stop the transfers here.   The sine wave will look fine.      //ADC_TransferDescriptors[3].next = 0;      ADC_TransferDescriptors[0].xfercfg = (DMA_XFERCFG_CFGVALID |                                DMA_XFERCFG_RELOAD  |                                DMA_XFERCFG_SETINTA |                                DMA_XFERCFG_WIDTH_16 |                                DMA_XFERCFG_SRCINC_0 |                                DMA_XFERCFG_DSTINC_1 |                                DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));      ADC_TransferDescriptors[1].xfercfg = ADC_TransferDescriptors[0].xfercfg;      ADC_TransferDescriptors[2].xfercfg = ADC_TransferDescriptors[0].xfercfg;      ADC_TransferDescriptors[3].xfercfg = (DMA_XFERCFG_CFGVALID |                                DMA_XFERCFG_RELOAD  |                                DMA_XFERCFG_SETINTA |                               DMA_XFERCFG_WIDTH_16 |                               DMA_XFERCFG_SRCINC_0 |                               DMA_XFERCFG_DSTINC_1 |                               DMA_XFERCFG_XFERCOUNT(DMA_TRANSFER_SIZE));      Initial_DMA_Descriptor.source = ADC_TransferDescriptors[0].source;      Initial_DMA_Descriptor.dest =   ADC_TransferDescriptors[0].dest;      Initial_DMA_Descriptor.next =  (uint32_t)&ADC_TransferDescriptors[1];      Initial_DMA_Descriptor.xfercfg = ADC_TransferDescriptors[0].xfercfg;      /* DMA initialization - enable DMA clocking and reset DMA if needed */      Chip_DMA_Init(LPC_DMA);      /* Enable DMA controller and use driver provided DMA table for current descriptors */      Chip_DMA_Enable(LPC_DMA);      Chip_DMA_SetSRAMBase(LPC_DMA, DMA_ADDR(Chip_DMA_Table));      /* Setup channel 0 for the following configuration:         - High channel priority         - Interrupt A fires on descriptor completion */      Chip_DMA_EnableChannel(LPC_DMA, DMA_CH0);      Chip_DMA_EnableIntChannel(LPC_DMA, DMA_CH0);      Chip_DMA_SetupChannelConfig(LPC_DMA, DMA_CH0,     //(DMA_CFG_PERIPHREQEN     |                                    (DMA_CFG_HWTRIGEN        |                                     DMA_CFG_TRIGBURST_BURST |                                                          DMA_CFG_TRIGTYPE_EDGE   |                                        DMA_CFG_TRIGPOL_LOW    |    //DMA_CFG_TRIGPOL_HIGH                                        DMA_CFG_BURSTPOWER_1    |                                     DMA_CFG_CHPRIORITY(0)                                          )                                        );      //make sure ADC Sequence A interrupts is selected for for a DMA trigger      LPC_INMUX->DMA_ITRIG_INMUX[0] = 0;      /* Enable DMA interrupt */      NVIC_EnableIRQ(DMA_IRQn);      // The 1st descriptor is set up through the registers.      /* Setup transfer descriptor and validate it */      Chip_DMA_SetupTranChannel(LPC_DMA, DMA_CH0, &Initial_DMA_Descriptor);      //Use the transfer configuration for our 4 main descriptors      Chip_DMA_SetupChannelTransfer(LPC_DMA, DMA_CH0,     ADC_TransferDescriptors[0].xfercfg);      Chip_DMA_SetValidChannel(LPC_DMA, DMA_CH0);      } void SCT_PWM_Generate(void) {          /* Initialize the SCT as PWM and set frequency */      Chip_SCTPWM_Init(SCT_PWM);      Chip_SCTPWM_SetRate(SCT_PWM, SCT_PWM_RATE);      /* Setup Board specific output pin */      Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 14, IOCON_FUNC3 | IOCON_MODE_INACT | IOCON_DIGITAL_EN | IOCON_INPFILT_OFF);      /* Use SCT0_OUT7 pin */      Chip_SCTPWM_SetOutPin(SCT_PWM, SCT_PWM_OUT, SCT_PWM_PIN_OUT);              /* Start with 50% duty cycle */      Chip_SCTPWM_SetDutyCycle(SCT_PWM, SCT_PWM_OUT, Chip_SCTPWM_PercentageToTicks(SCT_PWM, 10));      Chip_SCTPWM_Start(SCT_PWM);    }      /***            *         _    ____   ____            *        / \  |  _ \ / ___|            *       / _ \ | | | | |            *      / ___ \| |_| | |___            *     /_/__ \_\____/ \____|            *     / ___|  ___| |_ _   _ _ __            *     \___ \ / _ \ __| | | | '_ \            *      ___) |  __/ |_| |_| | |_) |            *     |____/ \___|\__|\__,_| .__/            *                          |_|            */ void ADC_Steup(void) {     /*Set Asynch Clock to the Main clock*/     LPC_SYSCON->ADCCLKSEL = 0;     //Set the divider to 1 and enable.  note,  the HALT bit (30) and RESET (29) are not in the manual     LPC_SYSCON->ADCCLKDIV = 0;      /* Initialization ADC to 12 bit and set clock divide to 1 to operate synchronously at System clock */     Chip_ADC_Init(LPC_ADC, ADC_CR_RESOL(3) | ADC_CR_CLKDIV(0)| ADC_CR_ASYNC_MODE);       //select ADC Channel 1 as input     Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 30, IOCON_FUNC0 | IOCON_ANALOG_EN| IOCON_INPFILT_OFF);       LPC_ADC->INSEL = 0x01;     Chip_ADC_SetupSequencer(LPC_ADC,ADC_SEQA_IDX,                                                                          ADC_SEQ_CTRL_SEQ_ENA |                               ADC_SEQ_CTRL_CHANNEL_EN(ADC_INPUT_CHANNEL) |                                                 ADC_SEQ_CTRL_TRIGGER(2) |                               ADC_SEQ_CTRL_HWTRIG_POLPOS |                                                 ADC_SEQ_CTRL_HWTRIG_SYNCBYPASS |                               ADC_SEQ_CTRL_MODE_EOS |                                                 ADC_SEQ_CTRL_SEQ_ENA);     /* Enable Sequence A interrupt */     Chip_ADC_EnableInt(LPC_ADC, ADC_INTEN_SEQA_ENABLE);         /* Calibrate ADC */     if(Chip_ADC_Calibration(LPC_ADC) == LPC_OK) {         /* Enable ADC SeqA Interrupt */         NVIC_EnableIRQ(ADC_SEQA_IRQn);     }     else {         DEBUGSTR("ADC Calibration Failed \r\n");         return ;     } } int main(void) {       SystemCoreClockUpdate();     Board_Init();         DMA_Steup();     ADC_Steup();     SCT_PWM_Generate();         while(1)     {}     } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍  Verification      Building the project, then click the   to debug;        Generate the sine wave: 1 KHz, 幅度:0~2 V,feed the wave the ADC via the J9_1(P0_30-ADC1);         Setting the breakpoint (Fig 4) to observe the ADC converted value CapturedData[32]; Fig 4                        4. To verifying the result, I collect several group of data and use the Excel to make these data graphical for checking. Fig 6 is an example. Fig 5 Fig 6 Fig 7 Fig 8
View full article
Recently I found some customers have a bit of problem when porting project from one MCU to another, so this article using simple steps demonstrates how to change MCU with MCUXpresso. There is also a video demonstrated the detail steps in attachment. Pay attention, as MCUXpresso User Guide says: All projects are associated with a particular MCU at creation time. The target MCU determines the project memory layout, startup code, LinkServer flash driver, libraries, supporting sources,launch configuration options etc. etc. so changing a project’s associated MCU should not be undertaken unless you have a total grasp of the consequence of this change. Therefore rather than changing a project’s associated MCU, it is strongly recommended that instead a new project is generated for the desired MCU and this new project is edited as required. However, on occasion it may be expedient to reset a project’s MCU (and associated SDK) and this can be achieved as follows. For example, changing lpc55s69 to lpc55s06, we need install SDKs for lpc55s69 and lpc55s06 before all the below steps. 1 - Change MCU & Package 1.1 – Change MCU Right click “MCU” under Project tree, choose “Edit MCU” Uncheck ”Preserve memory configuration”(it is checked by default)->choose LPC55S06->there is a warning, choose Yes. We can see the Memory details changed to lpc55s06, then click ”Apply and close”. 1.2 – Change Package 2 - Change Compiler Definitions In Properties view->Settings->MCU Compiler ->Preprocessor, change the definition for CPU from LPC55S69JBD100 to LPC55S06JBD64 as below: 3 – Change/add SDK driver for LPC55s06 Selected project, then click ”Manage SDK components”, choose the drivers our application used, for example, clock, power, usart. Click “OK”, then click “Yes” to update. Delete LPC55S69 device related files: Add “system_LPC55S06.c” and “system_LPC55S06.h” files: 4 - Change startup file. Delete LPC55s69 startup files, add “startup_lpc55s06.c”, we can find the startup file in any SDK demo. 5 - Change board related files. Refer to our own new board, change files under “board” folder, for example pins, uart number, here directly copy from SDK demo for LPCxpresso55s06 board. 6 - Test the project  function with new board Build project until no compile error, download and run it, result as below.        
View full article
This article introduces how to create a custom board MCUXpresso SDK and how to use it, mainly includes three parts: Part1: Generating a Board Support Configuration (.mex) Part2: Create a Custom Board SDK Using the Board SDK Wizard Part3. Using the Custom SDK to Create a New Project   Requirements: MCUXpresso IDE v11.1.1, MCUXpresso SDK for LPC845, LPC845-BRK board. This method works for all NXP mcu which support by MCUXpresso SDK. About detail steps, please refer to attachment. Thanks!
View full article
Introduction Amazon Web Services (AWS) is the world’s most comprehensive and broadly adopted cloud platform, offering over 165 fully-featured services from data centers globally. Millions of customers —including the fastest-growing startups, largest enterprises, and leading government agencies—trust AWS to power their infrastructure, become more agile, and lower costs.This document will take you step-by-step in a simple approach to adding peripherals to your AWS IOT and Alexa skills project. This is in continuation of the demo established in the following link, it is important to have this completed before continuing with this guide: Connecting the LPC55S69 to Amazon Web Services  Prerequisites - LPC55S69-EVK - Mikroe WiFi 10 Click - AWS Account - Alexa Developer Account - MCUXpresso IDE 11.2 - LPC55S69 SDK 2.8.0 Modifying "AWS_REMOTE_CONTROL_WIFI" In this example I will be adding a single-ended ADC peripheral. 1. First, create a separate .c and .h files in my source folder to keep it organized.  2. Initialize your peripheral. This includes your global variables, pins, clocks, interrupt handlers and other necessary peripheral configurations yours may have.  In my new_peripherals.c file, I add the following 2.1 Definitions: 2.2 Global variables: 2.3 Interrupt handler: 2.4 Initialization function: 2.5 Read ADC Function: 3.  Create header file with the two functions that will be used to enable the ADC, make sure to include the "fsl_lpadc"drivers. 4.  Add the ADC pin with pin configuration tool.  4.1 In this example I use PIO0_23 for the ADC0 Channel 0, 5. Add ADC_Init function to the main. 6. Now let's go ahead and modify "remote_control.c". Here we need to build the JSON text that we want updating our Thing's shadow with the ADC value, add the read function, add the variable in the initial shadow document and the keyword for our DeltaJSON. 6.1 First create global variables for the actual state of the ADC interaction and the parsed state. 6.2 Add external function which will read the ADC value. 6.3 Shadows use JSON shadow documents to store and retrieve data. A shadow’s document contains a state property that describes these aspects of the device’s state: desired: Apps specify the desired states of device properties by updating the desired object. reported: Devices report their current state in the reported object. delta: AWS IoT reports differences between the desired and the reported state in the delta object. 6.4 I've added the initial ADC state with a hard-coded 0, so that I can verify my Thing's shadow is initialized with the new information. 6.5 In the "void processShadowDeltaJSON(char *json, uint32_t jsonLength)" function, we need to add the condition for the change in state of the ADC. This will helps us identify when the action to read the ADC is requested. 6.6 Finally in the "prvShadowMainTask" function, we will create the action based on the above request. We can add some PRINTFs so that we know that the action is requested and processed properly through the serial console. As you may see I only want to update the ADC value when it is requested. Meaning the value of the ADC's state or parsed state is important. We will clear it to zero after we read the ADC and only update the value when it is 1. As opposed to the LEDState and parsedLEDState, where the value is important since it points to which color LED will be on/off. That's it you can build and run the project! Now we can add the Alexa Skill and the functionality in the AWS Lambda. MODIFYING AWS LAMBDA Since the lambda will be the connection between our LPCXpresso board and the Alexa Skill, we need to add the handler for  our new ADC requests. 1.  In this example we add the third request type which is the ADC event and the name of the callback function we will use.  2. The callback function "manage_ADC_request" will contain the attributes for reading and updating the shadow, this will consequently cause the change in delta shadow so our LPC55S69 will read the ADC pin. In addition, the utterances sent to the Alexa skill as well as how we want Alexa to respond will also be defined here.  As you may observe our function builds the JSON payload to update the shadow with a "1" when it is called and ignores the led and accelerometer values. We delay for 2.5 seconds to allow the LPC to read and write the ADC value in the necessary field and send the updated shadow. Then the Lambda will read the shadow and create the return message.  With this we construct the answer for Alexa. MODIFYING ALEXA SKILLS 1.  First create a custom 'intent'. Here is the general definition of what the utterances will be to request an action from the AWS Thing.    1.1 The name needs to match the name used for the event in the Lambda. In this example it is ADC_INTENT 2. Before we create the utterances, let's create the slot types. This is the list of all the words possible that may come to mind that a user might say to request a reading from the ADC.  2.1 The name of the slot type is not crucial, however please note it as we will need it later.  2.2 Add slot values. You can add as many as you think are necessary. For recommendations on custom slot values please check, best practices for sample utterances. 2.3 Go back to the general view of the ADC_INTENT, scroll down and we will add how the slot will be included in the utterances. In this example I use adc_name, however the name here is also not crucial. Select the slot type list we created earlier. 2.4 Now scroll back up and lets begin adding the sample utterances. This can be any command that you believe a user can say to invoke this action. You do not need to include the wake word here. In brackets add the name of your intent slot, in this case it is {adc_name}. That's it! You can save and rebuild the model. You are now ready to test it. You can do so through the 'Test' tab on the developer's console. In addition if you have an Alexa device or the SLN-ALEXA-IOT, you can test it by speaking with Alexa directly. In your LPCXpresso55S69 you can connect the 3.3V or the 0V to the ADC pin so you can see how the value is returned every request. 
View full article
The series of LPC540XX chips are flashless, only LPC54018JXM and LPC54S018JXM integrate internal QSPI Flash. The typical part numbers are LPC54018J2(4)M and LPC54S018J2(4)M. Some customers have questions about the concept of SPIFI interface and clock configuration when using this series of chips. This article mainly explains this. Introduction to SPIFI SPIFI (SPI Flash Interface) is an SPI Flash interface that can help microcontrollers replace large-size, high-cost parallel Flash with small-size, low-cost serial Flash. Using SPIFI technology, the external serial FLash can be mapped to microcontroller memory to achieve on-chip memory read effect, that is, cost can be optimized and Flash size can be increased while ensuring the operating speed. The electrical interface of SPIFI is as follows:   In the LPC540XX series of chips, if the part number includes M, QSPI Flash is integrated inside chip; if the part number does not include M, the QSPI Flash is externally connected to chip. The following picture shows the comparison of LPC54S018JXM and LPC54S018 in SPIFI structure:   SPIFI clock frequency description Taking LPC54S018J4M as an example, the SPIFI clock frequency is described below in the UserManual. SPIFI supports 1/2/4bit transmission mode. In 4bit transmission mode, the maximum transmission rate is SPIFI_CLK/2 bytes per second. The data transmission rate is up to 52Mbytes /s, that is, it takes two clock to transmit one byte. If you want to configure the SPIFI transmission rate to 52Mbytes /s, it needs to be in 4bit mode, so SPIFI_CLK is configured to 104M.     The SPIFI clock source is as follows in LPC54S018J4M Datasheet. By default, the SPIFI clock source is FRO96. For example, when the SPIFI clock is configured to 96M, in 4bit transmission mode, the transmission rate is 96/2=48Mbyte/s.   The LPC54S018J4M uses W25Q32JV-DTR as the internal SPIFI Flash. The figure below shows the maximum clock frequency it supports. In 4bit transmission mode, the maximum transmission rate is 133/2=66.5Mbyte/s, which is greater than SPIFI's maximum transmission rate of 52Mbyte/s. It shows that the maximum data transmission rate of W25Q32JV can meet the requirements of LPC54S018J4M QSPI Flash interface for communication rate.   3.Change SPIFI clock frequency The description of the SPIFI clock frequency in UserManual is as follows. In setup_lpc54s018m.c, the SPIFI clock frequency is defined on the address with an offset of 0X1C (the macro is defined as IMG_BAUDRATE), and the initial value is 0. According to the following table, when IMG_BAUDRATE=0, the SPIFI clock frequency is 24M. Since the default SPIFI clock source is the internal clock FRO96M, the SPIFI clock can be configured up to 96MHz in the following table by modifying the value of IMG_BAUDRATE.          There are two ways to modify the SPIFI clock.   3.1 Modify the SPIFI clock through IMG_BAUDRATE Before the main function runs, IMG_BAUDRATE is obtained by BOOT ROM to set the SPIFI clock frequency. If the requirement for the SPIFI clock rate is less than or equal to 96M, it is recommended to directly change the macro definition of IMG_BAUDRATE in setup_lpc54s018m.c to change the SPIFI clock frequency, as follows:   3.2 Modify the SPIFI clock through system config Another method is to modify the SPIFI clock frequency by changing the SPIFI frequency division coefficient in user code, as follows:   The result is as follows. The SPIFI clock frequency is set to 96M.   If you want to configure a higher SPIFI working clock, such as 104M, you must use a higher frequency external clock source to adjust the PLL coefficient and SPIFI frequency division coefficient in order to achieve the required clock frequency.
View full article
The documentation discusses how to generate phase-shift PWM signals based on SCTimer/PWM module, the code is developed based on MCUXpresso IDE version 10.3 and LPCXpresso5411x board. The LPC family has SCTimer/PWM module and CTimer modules, both of them can generate PWM signals, but only the SCTimer/PWM module  can generate phase-shift PWM signals. In the code, only the match registers are used to generate events, I/O signals are not used.  The match0 register is set up as (SystemCoreClock/100), which determines the PWM signal frequency. The the match1 register is set up as 0x00, which generate event1. The the match2 register is set up as (SystemCoreClock/100)/2;, which generate event2. The duty cycle is (SystemCoreClock/100)/2-0x00= (SystemCoreClock/100)/2, which is 50% duty cycle, the cycle time is (SystemCoreClock/100). The event1 sets the SCT0_OUT1, event2 clears the SCT0_OUT1, so SCT0_OUT1 has 50% duty cycle. The the match3 register is set up as (SystemCoreClock/100)/4;, which generate even3. The the match4 register is set up as 3*(SystemCoreClock/100)/4, which generate event4. The duty cycle is 3*(SystemCoreClock/100)/4  -  (SystemCoreClock/100)/4= (SystemCoreClock/100)/2, which is 50% duty cycle. The event3 sets the SCT0_OUT2, event4 clears the SCT0_OUT2, so SCT0_OUT2 has 50% duty cycle. The phase shift is (SystemCoreClock/100)/4 - 0x00= (SystemCoreClock/100)/4, which corresponds 90 degree phase shift. PWM initilization code: //The SCT0_OUT1 can output PWM signal with 50 duty cycle from PIO0_8 pin //The SCT_OUT2 can output PWM signal with 50 duty cycle fron PIO0_9 pin //The SCT0_OUT1 and SCT0_OUT2 PWM signal has 90 degree phase shift. void SCT0_PWM(void) {     SYSCON->AHBCLKCTRL[1]|=(1<<2); //SET SCT0 bit     SCT0->CONFIG = (1 << 0) | (1 << 17); // unified 32-bit timer, auto limit     SCT0->SCTMATCHREL[0] = SystemCoreClock/100; // match 0 @ 100 Hz = 10 msec     SCT0->EVENT[0].STATE = 0xFFFFFFFF; // event 0 happens in all states     //set event1     SCT0->SCTMATCHREL[1]=0x00;     SCT0->EVENT[1].STATE = 0xFFFFFFFF; // event 1 happens in all states     SCT0->EVENT[1].CTRL = (1 << 12)|(1<<0); // match 1 condition only     //set event2     SCT0->SCTMATCHREL[2]=(SystemCoreClock/100)/2;     SCT0->EVENT[2].STATE = 0xFFFFFFFF; // event 2 happens in all states     SCT0->EVENT[2].CTRL = (1 << 12)|(2<<0); // match 2 condition only     //set event3     SCT0->SCTMATCHREL[3]=(SystemCoreClock/100)/4;     SCT0->EVENT[3].STATE = 0xFFFFFFFF; // event 3 happens in all states     SCT0->EVENT[3].CTRL = (1 << 12)|(3<<0); // match 3 condition only     //set event4     SCT0->SCTMATCHREL[4]=3*(SystemCoreClock/100)/4;     SCT0->EVENT[4].STATE = 0xFFFFFFFF; // event 4 happens in all states     SCT0->EVENT[4].CTRL = (1 << 12)|(4<<0); // match 4 condition only     //PWM output1 signal     SCT0->OUT[1].SET = (1 << 1); // event 1 will set SCT1_OUT0     SCT0->OUT[1].CLR = (1 << 2); // event 2 will clear SCT1_OUT0     SCT0->RES |= (3 << 2); // output 0 toggles on conflict     //PWM output2 signal     SCT0->OUT[2].SET = (1 << 3); // event 3 will set SCT1_OUT0     SCT0->OUT[2].CLR = (1 << 4); // event 4 will clear SCT1_OUT0     SCT0->RES = (3 << 4); // output 0 toggles on conflict     //PWM start     SCT0->CTRL &= ~(1 << 2); // unhalt by clearing bit 2 of the CTRL } Pin initialization code: //PIO0_8 PIO0_8 FC2_RXD_SDA_MOSI SCT0_OUT1 CTIMER0_MAT3 //PIO0_9 PIO0_9 FC2_TXD_SCL_MISO SCT0_OUT2 CTIMER3_CAP0 - FC3_CTS_SDA_SSEL0 void SCTimerPinInit(void) {     //Enable the     SCTimer clock     SYSCON->AHBCLKCTRL[0]|=(1<<13); //set IOCON bit     //SCTimer pin assignment     IOCON->PIO[0][8]=0x182;     IOCON->PIO[0][9]=0x182;     IOCON->PIO[0][10]=0x182; } Main Code: #include <stdio.h> #include "board.h" #include "peripherals.h" #include "pin_mux.h" #include "clock_config.h" #include "LPC54114_cm4.h" void SCT0_Init(void); void SCTimerPinInit(void); void P1_9_GPIO(void); void SCT0_PWM(void); int main(void) {       /* Init board hardware. */     BOARD_InitBootPins();     BOARD_InitBootClocks();     BOARD_InitBootPeripherals();     printf("Hello World\n");    // SCT0_Init();    // P1_9_GPIO();     SCTimerPinInit();     SCT0_PWM();     /* Force the counter to be placed into memory. */     volatile static int i = 0 ;     /* Enter an infinite loop, just incrementing a counter. */     while(1) {         i++ ;     }     return 0 ; } The Yellow channel is PIO0_8 pin output signal, which is SCT0_OUT1 PWM output signal. The Bule channel is PIO0_9 pin output signal, which is SCT0_OUT2 PWM output signal.
View full article
Contents 1. Principle of energy measurement 2. Energy measurement test   2.1 Use in non-Debug state   2.2 Use in Debug state   During the operation of MCU, real-time measurement of board current and voltage is of great significance to the stability of system power consumption. Especially in scenarios that are sensitive to voltage and current fluctuations, it is particularly important to collect and analyze high-frequency samples. MCUXpresso IDE integrates the power measurement function, which can measure the current and voltage of the development board in real time and calculate the real-time power consumption. Based on MCUXpresso IDE v11.5.0, this article mainly explains power measurement function usage. 1.   Principle of energy measurement Currently the MCUXpresso IDE energy measurement function supports the following development boards: -LPCXpresso546x8/540xx/54S0xx -LPCXpresso54102 -LPCXpresso51U68/54114 -QN9090-DK006/ JN5189-DK006/IOTZKB-DK006 -QN9080DK The power measurement actually uses the LPC-Link2/MCU-Link debugger on the development board to collect the conversion value of the A/D conversion chip, and perform software calculation to obtain the power measurement result. Taking LPCXpresso54628 development board as an example, the following is the circuit diagram of the power measurement part: Fig.1 The MAX9634TEUK+T is a precision current amplifier. And ADC122S021 is a 12-bit A/D converter with dual-channel sampling, its rate can reach 200ksps. ADC122S021 collects LPC54xx_CURR and SHLD_CURR voltages, IDE sets Target resistor (Total Rvsense in the figure) and Shield resistor (resistance value corresponding to SHLD_CURR) in advance. The LPC-Link2 debugger can calculate the voltage, current and power consumption information by collecting AD conversion values. 2.   Energy measurement test Taking LPCXpresso54628 development board as an example. Open the menu bar : Analysis->Energy Measurement. The Energy Measurement interface will appear in the lower right corner of the screen, which is divided into Plot drawing and Config configuration interface. It can be used in Debug state or in non-Debug state during measurement. Test the case of LED small light flickering and observe the changes of voltage, current and energy consumption. Note that the LPC-Link2 debugger version should be CMSIS-DAP probe version 5.147 and above. 2.1 Use in non-Debug state Click the button  in energy measurement interface and select the measured in the config interface. You can select the target voltage, target current and shielding current. The sampling rate can be selected as 50ksps, 62.5ksps or 100ksps. First select the model of the development board to be tested, and then continue to select the target resistance and shielding resistance. The target resistance value is selected according to the jumper cap description in Figure 1. The resistance value of the shielding resistance is the fixed resistance value of development board. As shown in the figure below: Fig.2 Select the target voltage to be measured, and click the button to run the Energy Measurement interface. You can see the slight fluctuation of voltage in the plot interface and view the average voltage through the delimited area of horizontal measurement, as follows: Fig.3 Select the target current to be measured. Before measuring the target current, click Read from target on the config interface to calculate the average value of the target voltage within 0.5s for subsequent power consumption calculation. Click the run button to see that the target current fluctuates slightly with the flashing of the small light in the plot interface. At the same time, check the average current, power consumption and energy consumption through the delimited area of horizontal measurement, as follows: Fig.4 2.2 Use in Debug state When used in the debug state, you can use MCUXpresso IDE or KEIL to enter the debugging state. Click the button on the energy measurement interface to read the power consumption in the debug state. The measurement process is the same as the non-Debug state, as follows: Fig.5 This is a general enablement document of how to use energy measurement feature in debug and non-debug mode. For more, please refer  MCUXpresso_IDE_Energy_Measurement. pdf under MCUXpresso IDE install folder.    
View full article
Recently, customers reported that the number of PWM generated by SCTimer module was inconsistent between LPC55s06 user manual and data sheet. There are many kinds of PWM generation formats, so the maximum number of PWM generated by SCTimer is also different. I think the user manual and data sheet are not very clear, so this paper makes a specific analysis. It mainly depends on SCTimer resources, such as the number of events and output channels. For all LPC series, the mechanism of SCTimer generating PWM is the same. Therefore, this paper takes LPC55s6 as an example. LPC55s06 user manual: The SCTimer/PWM supports: – Eight inputs. – Ten outputs. – Sixteen match/capture registers. – Sixteen events. – Thirty two states. According to the different control modes of generating PWM wave, this paper is divided into single-edge PWM control, dual-edge PWM control and center-aligned PWM control. 1. Single-edge PWM control The figure below shows two single-edge control PWM waves with different duty cycles and the same PWM cycle length.   It can be seen from the above figure that the two PWM waves require three events: when the counter reaches 41, 65 and 100 respectively. Because of the same PWM cycle length, all PWM outputs need only one period event. Summary: The cycle length of all PWM waves are the same, so only one period event is required. The duty cycles of each PWM are different, and each PWM requires an event. The SCTimer of LPC55s06 has 16 events, one is used as PWM period event, and there are 15 left. Theoretically, 15 channels of PWM can be generated. However, LPC55s06 has only 10 outputs, so it can generate up to 10 single-edge control PWM waves. 2. Dual-edge PWM control The figure below shows three Dual-edge control PWM waves with different duty cycles and the same PWM cycle length.   It can be seen from the above figure that the three PWM waves require seven events: when the counter reaches 1, 27, 41, 53, 65, 78, 100.  Summary: PWM cycle length control needs one event, and each PWM duty cycle needs two events to trigger. The SCTimer of LPC55s06 has 16 events, one as PWM frequency event, and the remaining 15, so it can generate up to 7 dual-edge control PWM waves. 3. Center-aligned PWM control Center-aligned PWM control is a special case of dual-edge PWM control. The figure below shows two center-aligned PWM waves with different duty cycles and the same PWM duty length.   It can be seen from the above figure that the two center-aligned PWM waves need three events in total, which are the PWM cycle length and the duty cycle trigger of the two PWM waves. Because the left and right are symmetrical, only one event is needed to control the duty cycle of one PWM. Summary: All PWM have the same cycle length, so an event is required. The duty cycle of each PWM circuit is different, but the left and right are symmetrical, and an event trigger is required for each circuit. The SCTimer of LPC55s06 has 16 events, one is used as PWM cycle length, and there are 15 left. Theoretically, 15 channels of PWM can be generated, but LPC55s06 has only 10 outputs, so it can generate up to 10 channels of unilateral control PWM wave. Summary:   Maximum number of PWM generated by LPC55s6 SCTimer: Single-edge PWM control: 10 Dual-edge PWM control: 7 Center-aligned control: 10   The number of SCTimer events and output channels is different with different chips, but the analysis method is the same. Customers can analyze whether the SCTimer in a certain chip meets the requirements.
View full article
1. General Jointly developed by NXP and Embedded Artists, the MCU-Link Pro is a fully featured debug probe that can be used with MCUXpresso IDE and 3rd party IDEs that support CMSIS-DAP and/or J-Link protocols. MCU-Link Pro is based on NXP’s MCU-Link architecture, found in the MCU-Link low cost debug probe and on board evaluation boards, and runs the same firmware as all these implementations. In addition to SWD debug, SWO profiling and a USB to UART bridge features (VCOM) found in the base MCU-Link, the Pro model adds a J-Link LITE firmware option, energy measurement, analog signal monitor, USB to SPI and I2C bridging capability and an on-board LPC804 for peripheral emulation. MCU-Link Pro is based on the dual Arm® Cortex-M33® core LPC55S69 microcontroller, and features a high speed USB interface, providing high performance debug at low cost. The USB bridging feature is supported by the free LIBUSBSIO host library from NXP. MCU-Link Pro is compatible with Windows 10, MacOS and Linux. The product comes with the necessary firmware installed, with free utilities provided to enable future firmware updates from NXP to be installed. MCU-Link Pro kit provides all parts that need to be used. Kit Contains MCU-Link Pro debug probe 10 pin to 10 pin Cortex debug cable 10 pin to 20 pin Cortex debug cable Digital port / analog input adapter cable Spare jumpers 2. MCU-Link Pro Overview MCU-Link Pro has complete functions. This article mainly introduces the usage and precautions of several basic functions, including SWD debugging, UART (VCOM) and energy measurement. The following figure is the reference diagram of MCU Link Pro, covering all functions, and the highlighted part is the function used in this article.   2.1 SWD debug As a debugger, the most basic function of MCU Link Pro is debugging, and now commonly used is SWD debug. When you get the development board, you can see that there are three SWD interfaces on it. Only J7 is the SWD interface to debug target board. It is on the opposite side of the USB interface to facilitate the connection and debugging of the target board. The other two interfaces J3 and J11 are SWD interfaces of LPC55s69 and LPC804 respectively. Another important function of this debugger is that it can supply power to the target board. The use method is to connect J6 with jumper, and 1.8V and 3.3V power supply can be selected through J5. The specific connection is shown in the figure below: - Connect the SWD interface of J7 and target board with debug line. - J6 connecting jumper cap (supplying power to target board).  The USB cable connects J1 and the computer, so you can debug with MCUXpresso IDE or other IDEs. CMSIS-DAP and J-Link debugging protocols are supported. For how to update the debugger firmware, please refer to:https://www.nxp.com/document/guide/getting-started-with-the-mcu-link-pro:GS-MCU-LINK-PRO   2.2 UART (VCOM) Usage In the development and debug stage, users often need to print information through the serial port. Using MCU Link Pro, without additional hardware, directly connect the TX and Rx of target UART with the Rx / TX of UART of MCU Link Pro. Through the VCOM function, you can print information from the USB port to the serial port assistant at the PC end. The specific connection is shown in the figure below: - J19-8 (purple line) connects UART TX of target board - J19-9 (gray line) connects the UART RX of the target board - J19-1 (GND) connect GND of target board - J14 disconnected - J6 plug in the jumper cap (supply power to the target board)   2.3 Energy measurement The MCU Link Pro board contains a circuit that can measure the current or voltage of the target board, and it can be calibrated automatically every time it is powered on without manual intervention. There are two maximum measurement ranges for energy measurement. If the data is higher than the maximum range, the measurement result is inaccurate. The two maximum measurement ranges are as follows, which need to be configured with J16, J17 and J18.   Energy measurement needs to be used with MCUXpresso IDE, and the results are displayed in the IDE interface. Use J9 port on the board. The specific connection is shown in the figure below: - J9-1 connects the power supply end of the target board. - J9-3 connects the chip ends of the target board. - J9-2 connects the GND of the target board For details on how to use the MCU Xpress IDE interface, please refer to:<MCUXpresso_IDE_Energy_Measurement.pdf> 3. Test result The test results are as follows:          
View full article
Contents 1. Introduction 1 2. USB Demo based on MCUXpresso SDK 1     2.1 Update USB device demo: USB0->USB1 2     2.2 Update USB host demo: USB0->USB1 2     2.3 Update USB ROM demo: USB0-> USB1 3 3. USB Demo based on LPCOpen 3 4. Notes and Recap 4  1.     Introduction Most of LPC devices integrate USB module. NXP LPC currently integrates full-speed USB (FS, Full Speed, 12Mbps) and high-speed (HS, High Speed, 480Mbps) USB. Specifically, for the LPC series: - Some LPCs such as LPC55xx and LPC54xxx integrate both HS USB and FS USB. Usually USB0 is FS USB and USB1 is HS USB. - Some LPCs such as LPC43xx and LPC18xx integrate two HS USBs, so USB0 and USB1 are both HS USBs. The two most well-known NXP software packages for LPC series are MCUXpresso SDK and LPCOpen. MCUXpresso SDK is mainly for LPC products launched in recent years, while LPCOpen is used for earlier LPC derivatives. The USB demos included in these two packages run on USB0 by default. Most of NXP USB demos are for USB0 by default. This article is to introduce how to switch a USB0 demo to USB1 demo based on different software packages. 2.     USB Demo based on MCUXpresso SDK (e.g. LPC54XXX, LPC55XX) The MCUXpresso SDK USB demo codes are categorized as: - USB as Device: e.g. usb_device_cdc_vcom, usb_device_hid_generic, etc. - USB as Host: e.g. usb_host_hid_mouse, usb_host_msd_fatfs, etc. - USB demo based on USB ROM API: e.g. usb_rom_device_audio,usb_rom_device_cdc, etc. 2.1  Update USB device demo: USB0->USB1 Taking usb_device_cdc_vcom demo as an example. To switch to USB1, simply change the corresponding code in usb_device_config.h file as follows. /*! @brief LPC USB IP3511 FS instance count*/ #define USB_DEVICE_CONFIG_LPCIP3511FS (0U) /*! @brief LPC USB IP3511 HS instance count*/ #define USB_DEVICE_CONFIG_LPCIP3511HS (1U) After the change, recompile the program to run. The program was updated to USB1 device demo. 2.2   Update USB host demo: USB0->USB1 Taking usb_host_hid_mouse demo code as an example, to switch to USB1, modify the macro definition in usb_host_config.h as follows: #defineUSB_HOST_CONFIG_KHCI (0U) #defineUSB_HOST_CONFIG_EHCI (0U) #define USB_HOST_CONFIG_OHCI (0U) #define USB_HOST_CONFIG_IP3516HS (1U)   The program is recompiled and run. The program was updated to USB1 host demo. 2.3  Update USB ROM demo: USB0-> USB1 ( e.g. LPC54XXX Series) USB ROM demo calls the USB ROM API, there is no way to switch the default USB0 to USB1 by modifying macro definitions. In order to update code to USB1 demo, the recommended steps are as below: -USB HS DEVICE and USB PHY clock configuration -Change to use USB HS ISR -Locate the related buffer into USB RAM. -Set the USB ROM handle to be HS If user has difficulties in revising the code by self, user can apply demo code from NXP LPC online support team by creating a private case. 3.     USB Demo based on LPCOpen (e.g. LPC43XX, LPC18XX) Some legacy LPCs run on LPCOpen, such as LPC43xx series, LPC18xx series. Their USB0 and USB1 are both high-speed. The default USB demo is for USB0 as well. To switch to USB1, we can uncomment #define USE_USB1 and comment #define USE_USB0 in app_usbd_cfg.h. // #define USE_USB0  #define USE_USB1 Taking usbd_rom_cdc_uart demo as an example:   Recompile and run, the program is updated to USB1 demo. 4.     Notes and Recap The focus of this article is on software modification of converting USB0 to USB1 on NXP SW package. Regarding the hardware, customer needs to check the specific demo board user guide. For example, when we use HS USB, it may be necessary to provide an external power supply, and the jumper also needs to be adjusted to build a well hardware environment for HS USB operation. I will not dwell on them here. This article summarizes methods of switching USB0 to USB1 for several commonly used LPC series on MCUXpresso SDK and LPCOpen package. customers who need USB1 demo code can find the corresponding modification methods in this article for their own software and chips. Official routines are only used for demo board demos and chip learning. If for commercial usage, user needs to learn USB in depth and be responsible for own application.  
View full article
After LPC54XXX enter ISP mode, there are two methods to upgrade the application through UART/I2C/SPI/USB. One method is to change the ISP pin state when power on, and the other method is to reinvoke ISP Boot ROM in source code during code running. The first method does not require user to write any code, and the operation is simple, but the disadvantage is that it is not flexible and is not suitable for on-site operation; The second method is more flexible and is widely used in Secondary Bootloader applications developed by yourself, but it requires users to write their own code. In actual development, because the USB port of personal computer is easy to use, the method of using the USB port for application upgrade is becoming more and more popular. Unfortunately, we currently do not have instructions for upgrading the application by the USB port in ISP mode. So we write this article to share the method here.   There are two methods to enter ISP mode: Method 1: Enter ISP mode to upgrade the application during power on On the hardware side, configure the ISP0~2 pins before power-on or reset, and the MCU enters ISP mode to upgrade the application. The pin configuration method is as follows: Figure 1.   Method 2: Activate Reinvoke ISP in source code to upgrade the application In ISP mode, the application is upgraded through UART/I2C/SPI/USB. This article focuses on the USB method. Here for USB, Both USB0 (Full Speed) and USB1 (High Speed) of LPC54XXX can be used for application upgrade. There are two USB upgrade modes: DFU (Device Firmware Updata) and MSC (Mass Storage Device Class), as follows: Figure 2.   Select the application upgrade mode by modifying byte 0 and byte 1 of the ISP parameter array. The key code is as follows Figure 3.   There are 3 key point we need to pay attention in Figure 3: -When isp_mode[0] is configured as 0xAA, it is DFU mode, otherwise it is MSC mode (for example, isp_mode[0] is configured as 0xFF). -When isp_mode[1] is configured as 8, USB FS is used, and when it is configured as 9, USB HS is used. -Enter the ISP mode through the Chip_IAP_ReinvokeISP function. 2.1 Use DFU for application upgrade Tool preperation: To work with DFU, dfu-util tool is needed to use DFU to upgrade the application, you can download the DFU tool on the DFU official website. The link is as follows: http://dfu-util.sourceforge.net/ NXP also includes the dfu-util tool in LPCScrypt. If you have downloaded LPCScrypt, you can use it directly in the bin directory.   DFU update application Steps: Take LPC54628 as an example, ISP is configured as DUF mode, and USB1 is used to upgrade the application. Modify the relevant code in Figure 3, as follows: isp_mode[0] = 0xAA; isp_mode[1] = SL_USBHS; Build and download the application to the MCU, power on again, and connect USB1 to the computer. Here Enter the dfu-util tool directory and copy the .bin file to the current directory. Use the command: ./dfu-util -l   Find the DFU devices. Use the command: ./dfu-util -D .\lpcxpresso54628_gpio_led_output.bin -a 0 Download the lpcxpresso54628_gpio_led_output.bin file to the device with alt number 0. Alt0 is "FLASH", alt1 is "RAM", and the specific operations are as follows:   Figure 4.   After downloading the application successfully, reset the MCU and observe the blinking phenomenon of the LED on the development board.   2.2 Use MSC for application upgrade Take LPC54628 as an example, ISP is configured as MSC mode, and USB1 is used to upgrade the application. Modify the relevant code in Figure 3, as follows: isp_mode[0] = 0xFF; isp_mode[1] = SL_USBHS; Build and download the application to the MCU, power on again, and connect USB1 to the computer. You will found another disk in my computer, as follows: Figure 5.   Then do the following to update firmware: -Remove the original firmware.bin in the CRP DISABLD disk. -Rename the application (for example, lpcxpresso54628_gpio_led_output.bin) to firmware.bin. -Copy the application firmware.bin to the CRP DISABLD disk. -Reset the MCU, if the LED is observed blinking, it proves that the application has been successfully upgraded. Note: The application must be renamed, and the rename cannot be performed in the CRP DISABLD disk.   Demo project:lpcxpresso54628_flashiap.zip Application upgrade file:lpcxpresso54628_gpio_led_output.bin (generated by SDK demo code)
View full article
Some customers want to generate CRC checksum during compile project, while the GUN tool chain in MCUXpresso IDE doesn’t include CRC checksum calculation function, so we need  the help of CRC checksum tools. In this article, use SRecord. About detail theoretical knowledge of SRecord, please refer to https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/ In this thread, mainly describe the steps about how to generate CRC checksum with MCUXpresso IDE post-build, through a hands on.   Environment: LPC54S018 chip MCUXpresso IDE SRecord tool (http://srecord.sourceforge.net/)   Purpose: Generate and place CRC checksum to 0x10000170 of LPC54s018 after compile project. In image header for LPC540xx devices, the offset 0x10 is crc_value, in LPC54s018 , the address is 0x10000170. so we need save CRC checksum value in  this  place.   Steps: Import SDK demo “led_blinky” into MCUXpresso IDE (Just use this demo to demonstrate).   Enable Compute CRC, because there is one bit in Image header for LPC540xx,Just add “ADD_CRC” or “ADD_CRC =1”, build project.     Can check from S19 file: When choose no CRC computation (no defined “ ADD_CRC “ symbol), the data in address 0x0164 bit0 is 1,   When choose compute CRC, the data in address 0x0164 bit0 is 0,        Download SRecord from http://srecord.sourceforge.net/ After download, srec_cat.exe is the main program we used. Place srec_cat.exe utility in a common directory (to reuse it even if you change the project or even the MCUXpresso IDE version). Be sure you add that “common directory” in the PATH environment variable, then be sure the eclipse was restarted to “see” the PATH content.   Create command file crc_add.txt, and place it under" Debug" folder of project. (About detail commands, please refer to SRecord Reference Manual.) # srec_cat command file to add the CRC and produce application file to be flashed # Usage: srec_cat @filename #first: create CRC checksum lpcxpresso54s018m_led_blinky.srec # input file -fill 0xFF 0x10000180 0x10010000 # fill code area with 0xff -crop 0x10000180 0x10010000 # just keep code area for CRC calculation below (CRC will be at 0x1FFFE..0x1FFFF) -CRC16_Big_Endian 0x10000170 -CCITT # calculate big endian CCITT CRC16 at given address. -crop 0x10000170 0x10000172 # keep the CRC itself #second: add application file lpcxpresso54s018m_led_blinky.srec # input file -fill 0xFF 0x10000180 0x10010000 # fill code area with 0xff -crop 0x10000000 0x10000170 0x10000172 0x10010000 #keep all except CRC #finally, produce the output file -Output # produce output lpcxpresso54s018m_led_blinky_crc.srec   Add post-build command to create srecord file with CRC checksum. arm-none-eabi-objcopy -v -O srec "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.srec" & srec_cat.exe @CRC_add.txt   7) Build project, the .srec with CRC checksum file will under Debug folder:         Pay attention: For the format of image header of LPC540xx devices, we need enable compute CRC and put the CRC value in the specific address. while for other chips, maybe do not need enable, and also can place it in your own address.   Reference: https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/        
View full article
How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE This document gives an overview of SDK v.2.0 for LPC5411x and also describes the steps required to build, run, and debug an example application provided in the SDK using LPCXpresso IDE. The steps described in the document are for the LPCXpresso54114 board (OM13089).   SDK for LPC5411x Derivatives Overview   The Software Development Kit (SDK) provides comprehensive software support for Microcontrollers. The SDK includes a flexible set of peripheral drivers designed to speed up and simplify development of embedded applications. Along with the peripheral drivers, the SDK provides an extensive and rich set of example applications covering everything from basic peripheral use case examples to full demo applications. The SDK also contains RTOS kernels and various other middleware to support rapid development on devices. SDK board support provides example applications for development and evaluation boards. Board support packages are found inside of the top level boards folder, and each supported board has its own folder (a SDK package can support multiple boards). Within each <board_name> folder there are various sub-folders to classify the type of examples they contain. These include (but are not limited to): demo_apps: Full-featured applications intended to highlight key functionality and use cases of the target MCU. These applications typically use multiple MCU peripherals and may leverage stacks and middleware. driver_examples: Simple applications intended to concisely illustrate how to use the SDK’s peripheral drivers for a single use case. These applications typically only use a single peripheral, but there are cases where multiple are used (for example, ADC conversion using DMA). rtos_examples: Basic FreeRTOS examples showcasing the use of various RTOS objects (semaphores, queues, and so on) and interfacing with the SDK’s RTOS drivers multicore_examples: Applications for both cores showing the usage of multicore software components and the interaction between cores.   Build, run and debug a SDK example   This section describes the steps required to configure LPCXpresso IDE to build, run, and debug an example application. The hello_world demo application targeted for the LPCXpresso54114 is used as an example, though these steps can be applied to any example application in the SDK.   1. Download and install the latest LPCXpresso version from the next link: http://www.nxp.com/products/software-and-tools/software-development-tools/software-tools/lpc-microcontroller-utilities/lpcxpresso-ide-v8.2.2:LPCXPRESSO 2. Follow the steps describe here to download the Software Development Kit (SDK) v2.0 for LPCXpresso54114: Generating a downloadable MCUXpresso SDK v.2 package  3. Select "File -> Import" from the LPCXpresso IDE menu. In the window that appears, expand the "General" folder and select "Existing Projects into Workspace". Then, click the "Next" button.       4. Click the "Browse" button next to the "Import from file:" option, and point to the example application project, which can be found using this path: <install_dir>/boards/<board_name>/<example_type>/<application_name>/lpcx/cm4 For this example, the specific location is: <install_dir_SDK_2.0_LPCXpresso54114>\boards\lpcxpresso54114\demo_apps\hello_world\lpcx\cm4 Then Click the "Finish" button. 5. There are two project configurations (build targets) supported for each SDK project: Debug – Compiler optimization is set to low, and debug information is generated for the executable. This target should be selected for development and debug. Release – Compiler optimization is set to high, and debug information is not generated. This target should be selected for final application deployment. So it is necessary to choose the appropriate build target. For this example, select the "Debug" target.   6. Build the project using the hammer icon. 7. Connect the development platform to your PC via USB cable between the Link2 USB connector (named Link for some boards) and the PC USB connector. If connecting for the first time, allow some seconds for the devices to enumerate.   8. In the Windows operating system environment, open the terminal application on the PC and connect to the debug serial port number. For this example it is used Tera Term.   Configure the terminal with these settings: 115200 No parity 8 data bits 1 stop bit    9. In LPCXpresso IDE, click on “Debug Configurations”. In the Debug Configurations dialog box, select the debug configuration that corresponds to the hardware platform you’re using. In this example, select is the CMSIS-DAP option under C/C++ (NXP Semiconductors) MCU Application. 10. After selecting the debugger interface, click the "Debug" button to launch the debugger. 11. Additional dialog windows may appear to select LPC-INK2 CMSIS-DAP emulator and core in case of multicore derivatives. Select it and click the "OK" button. Then select the Cortex-M4. The application is downloaded to the target and automatically run to main():    12. Start the application by clicking the "Resume" button. The hello_world application is now running and a banner is displayed on the terminal. Enjoy!!   Related links: Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  MCUXpresso Config Tools is now available!  
View full article
The following document contains a list of documents, questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in LPC or MCUXpresso you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table  FAQ: MCUXpresso Software and Tools  How to create a new LPC project using LPCOpen and MCUXpresso IDE  Introducing MCUXpresso SDK v.2 for LPC54xxx Series  Generating a downloadable MCUXpresso SDK v.2 package  Using the MCUXpresso Pins Tool   MCUXpresso Config Tools is now available!   LPC55xx Multicore Applications with MCUXpresso IDE  LPC information LPC5460x MCU Family Overview  USB with NXP Microcontrollers LWIP memory requirements  LPC800 Four-Part Webinar Series!  The LPC804 Programmable Logic Unit (PLU)   LPC84x Technical Training - Now Available Guides and Examples Flashing and Installing the new firmware and drivers for LPC11U35 debug probes  Enabling debug output  USB FLASH download, programming, and security tool (DFUSec)  DMA Ping-Pong application  Getting start with LPCXpresso54608 &amp; emWin Graphics;  Capacitive Touch example using the LPC845 Breakout Board  OLED Display Application Example using LPC845 Breakout Board and SPI  Mixed-Signal Logic Analyzer &amp; Oscilloscope (Lab Tool) Solution  LPC FAQ How to calculate the value of crystal load capacitors? Can I send a message with X/Y/Z bits in the ID?  What is the difference between error active and error passive? What is the sample point for?  How can I verify the configured CAN bitrate, using an oscilloscope? 
View full article