Kinetis Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Microcontrollers Knowledge Base

Discussions

Sort by:
Hello Freedom community users Bheema has posted on the Element14 community a very clear tutorial (accessible following the link below) to create from scratch a basic project example featuring the SLCD of the FRDM-KL46Z with Processor Expert. Freescale Freedom development platform: [FRDM-K... | element14 Those steps should be very useful to create your own project featuring SLCD display and better understand the constraints of this peripheral. Happy SLCD Displaying Greg
View full article
Hello Freedom users I have created another full board review this time for the FRDM-KL05Z always including clear instructions to program and debug your first project. I'm still working on the video version (looking for a better accent :smileyconfused:), but the commands illustrated by screen captures should be easy to follow. Freescale Freedom development platform: [FRDM-K... | element14 Enjoy Greg
View full article
  Hello Freedom community users Few weeks before, I produced for the Element14 community a full video review of the FRDM-KL46Z including all the steps to program and debug your first project example. Video has a length of less than 13 min so your evaluation of the Kinetis KL46 should be really quick and easy http://www.element14.com/community/community/designcenter/kinetis_kl2_freedom_board/blog/2014/06/17/frdm-kl46z-full-review-and-getting-started-in-video Enjoy Greg
View full article
近期有客户提出需求,要求通过外部Flash编程工具烧写Flash Program Flash IFR区域。 目前P&E Cyclone MAX和Segger J-Flash均无法实现对IFR区域编程。 客户可以使用软件的方式来编程IFR提供的单次烧写区域,存储客户产品信息,例如MAC地址等。 Program Flash单次烧写区域提供了64个字节,只允许烧写一次,通过Program Once和Read Once命令来读写这个区域。 下图为单次烧写区域在Prgoram Flash IFR的具体位置, IFR独立于FTFL Flash空间,可以理解成另外一个Flash模块。 Program Once和Read Once命令每次调用可以读取Program Flash单次烧写区域的4个字节,通过命令参数的数据索引号可以通过多次操作遍历整个64个字节。 附件中的例程使用Program Once命令编写MAC地址到单次烧写区域,之后通过Read Once命令读取MAC地址信息。 例程环境: IAR Workbench + TWR-K60D100M
View full article
Introduction What is a gated timer and why would I need one? A gated timer is a timer whose clock is enabled (or "gated") by some external signal.  This allows for a low code overhead method of synchronizing a timer with an event and/or measuring an event. This functionality is not commonly included on Freescale microcontroller devices (this functionality is only included on devices that are equipped with the upgraded TPM v2 peripheral; currently K66, K65, KL13, KL23, KL33, KL43, KL03) but can be useful in some situations.  Some applications which may find a gated timer useful include asynchronous digital sampling, pulse width duty cycle measurement, and battery charging. How do I implement a gated timer with my Kinetis FTM or TPM peripheral? To implement a true gated timer with a Kinetis device (that does not have the TPM v2 peripheral), additional hardware will be required to implement the enable/disable functionality of a gated timer.  This note will focus on two different ways (low-true and high-true) to implement a gated timer.  The method used will depend on the requirements of your application. Implementing a gated timer for Kinetis devices without the TPM v2 peripheral requires the use of a comparator and a resistive network to implement a gated functionality (NOTE:  Level shifters could be used to replace the resistive network described; however, a resistive network is likely more cost effective, and thus, is presented in this discussion).  Figure 1 below is the block diagram of how to implement a gated timer functionality.  The theory behind this configuration will be explained in later sections. Theory of Operation Comparator and resistive network implementation The comparator is the key piece to implementing this functionality. For those with little experience with comparators (or need a refresher), a comparator is represented by the following figure.  Notice that there are three terminals that will be of relevance in this application: a non-inverting input (labeled with a '+' sign), an inverting input (labeled with a '-' sign), and an output. A comparator does just what the name suggests: it compares two signals and adjusts the output based on the result of the comparison.  This is represented mathematically in the figure below. Considering the above figure, output of the comparator will be a  logic high when the non-inverting input is at a higher electric potential than the inverting input.  The output will be a logic low if the non-inverting input is at a lower electric potential than the inverting input.  The output will be unpredictable if the inputs are exactly the same (oscillations may even occur since comparators are designed to drive the output to a solid high or solid low).  This mechanism allows the clock enable functionality that is required to implement a gated timer function provided that either the non-inverting or inverting input is a clock waveform and the opposite input is a stable logic high or low (depending on the desired configuration) and neither input is ever exactly equal.  Comparator Configurations There are two basic signal configurations that an application can use to enable the clock output out of the comparator: low-true signals and high-true signals.  These two signals and some details on their implementation are explained in the following two sections.  Low-true enable A low-true enable is an enable signal that will have zero electric potential (relative to the microcontroller) or a "grounded" signal in the "active" state.  This configuration is a common implementation when using a push button or momentary switch to provide the enable signal.  When using this type of signal, you will want to connect the enable signal to the non-inverting input of the comparator, and connect the clock signal to the inverting input. The high level of the enable signal should be guaranteed to always be the highest voltage of the input clock plus the maximum input offset of the comparator. To find the maximum input offset of the comparator, consult the device specific datasheet.  See the figure below to see a graphical representation of areas where the signal will be on and off. The external hardware used should ensure that the low level of the enable signal never dips below the lowest voltage of the input clock plus the maximum input offset of the comparator. The following figure displays one possible hardware configuration that is relatively inexpensive and can satisfy these requirements. High-true enable A high-true enable is an enable signal that will have an electric potential equal to VDD of the microcontroller in the "active" state.  This configuration is commonly implemented when the enable signal is provided by an active source or another microcontroller.  When interfacing with this type of signal, you will want to connect the enable signal to the inverting input of the comparator, and connect the clock signal to the non-inverting input.  When the comparator is in the inactive state, it should be at or below the lowest voltage of the clock signal minus the maximum input offset of the comparator.  Refer to the following figure for a diagram of the "on" and "off" regions of the high true configurations. The external hardware will need to guarantee that the when the enable signal is in the active state, it does not rise above the highest voltage of the clock signal minus the maximum input offset of the comparator. The following figure displays one possible hardware configuration that is relatively inexpensive and can satisfy these requirements. Clocking Options Clocking waveform requirements will vary from application to application.  Specifying all of the possibilities is nearly impossible.  The point of this section is to inform what options are available from the Kinetis family and provide some insight as to when it might be relevant to investigate each option. The Kinetis family provides a clock output pin for most devices to allow an internal clock to be routed to a pin.  The uses for this option can vary.  In this particular scenario, it will be used to provide the source clock for the comparator clock input. Here are the most common clock output pin options across the Kinetis K series devices.  (NOTE:  If the application requires a clock frequency that the CLKOUT signal cannot provide, a separate FTM or TPM instance or another timer module can be used to generate the required clock.) In the Kinetis L series devices, the following options will be available. The clock option selected should be the slowest allowable clock for the application being designed.  This will minimize the power consumption of the application.  For applications that require high resolution, the Bus, Flash, or Flexbus clock should be selected (note that the Flexbus clock can provide an independently adjustable clock, if it is not being used in the application, as it is always running).  However, if the target application needs to be more power efficient, the LPO or MCGIRCLK should be used.  The LPO for the Kinetis devices is a fixed 1 kHz frequency and will, therefore, only be useful in applications that require millisecond resolutions.
View full article
El programador USBDM es una interfaz de programación y depuración para los microcontroladores Freescale, existen varias versiones de esta herramienta, el programador MantaRay USBDM está basada en la versión para los microcontroladores HCS08(BDM) y Kinetis (SWDIO). Toda la información acerca de este proyecto puedes encontrarlo en http://usbdm.sourceforge.net/index.html BDM (Background debug mode) El puerto de programación BDM es una interfaz de programación desarrollada por Freescale para los microcontroladores HCS08 (8 bits) y Coldfire V1 (32 bits). Las características más sobresalientes sobre este puerto de programación es que solo utiliza un pin de programación (BKGD). Además de permitir la programación de la memoria flash, también permite el "debug in circuit" esto quiere decir que podemos depurar nuestro codigo en tiempo real a través del software Codewarrior. SWDIO Es la versión minima del JTAG para los microcontroladores Kinetis (Cortex ARM 32 bits) en la cual solo utiliza una linea de comunicación (SWDIO) y una señal de reloj (SWCLK). Este puerto esta en los Cortex M0 como son KL01, KL02, KL03, KL1x,KL2x,KE02,KE04 y KE06. El programador MantaRay USBDM permite la programación y la depuración de los microcontroladores de Freescale de la gama de 8 bits y 32 bits. Shrimp El complemento perfecto para el programador MantaRay USBDM es Shrimp, una pequeña tarjeta que tiene el tamaño exacta de un integrado con montaje DIP28 600mil, la cual, la hace una herramienta flexible, al hacer prototipos en una protoboard, y después en un prototipo final. La tarjeta Shrimp es compatible con los microcontroladores de 8 bits MC9S08PA16 y de 32 bits MKE02Z16, los dos totalmente compatibles en pines y periféricos. MC9S08PA16 8-Bit S08 central processor unit (CPU) – Up to 20 MHz bus at 2.7 V to 5.5 V across temperature range of -40 °C to 105 °C – Supporting up to 40 interrupt/reset sources – Supporting up to four-level nested interrupt – On-chip memory – Up to 16 KB flash read/program/erase over full operating voltage and temperature – Up to 256 byte EEPROM; 2-byte erase sector; program and erase while executing flash – Up to 2048 byte random-access memory (RAM) – Flash and RAM access protection MKE02Z16 • Operating characteristics – Voltage range: 2.7 to 5.5 V – Flash write voltage range: 2.7 to 5.5 V – Temperature range (ambient): -40 to 105°C • Performance – Up to 40 MHz ARM® Cortex-M0+ core and up to 20 MHz bus clock – Single cycle 32-bit x 32-bit multiplier – Single cycle I/O access port • Memories and memory interfaces – Up to 16 KB flash – Up to 256 B EEPROM – Up to 2 KB RAM Más información técnica la puedes encontrar en el siguiente link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KE02&nodeId=01624698C90DE4 http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08P&nodeId=01624684491437EDDD Muy pronto mas adelantos de este proyecto
View full article
In this document we are going to see how to use the attached code which implements the configuration of the FRDM-KL25 board as a USB HOST interfacing with a Numeric Keyboard and a 16x2 LCD. The project is compiled in the CodeWarrior IDE using Processor Expert and the Components to support the USB module of the USB Stack 4.1.1. How to add the Processor Expert USB components. The instructions to install the USB components to use them with Processor Expert are in the documentation of the USB Stack 4.1.1; here you can see the steps as well: Download the USB Stack 4.1.1 from the Freescale’s Website (USB Stack 4.1.1) Run the .exe file and install it in the default location. Open CodeWarrior and select Import Components in the Processor Expert button in menu bar. An Open windows will pop up, there you need to go to the path: <install folder>\Freescale USB Stack v4.1.1\ProcessorExpert\Components. To have the complete components and support for the USB module add each PEupd file repeating this step. Close CodeWarrior and open it again to ensure correct installation of the components. Check that the new components are available in the Components Library. About this Project. This project is based in the example code for Processor Expert in the USB Stack 4.1.1 USB_HID_MOUSE_HOST_MKL25Z128_PEx which implements the use of the FRDM-BOARD KL25 and a HID Mouse Device to interface with. In this project the HID Device is a Numeric Keyboard and the HOST Device (FRDM-KL25) is handling the data and printing them in a 16x2 LCD used in 8 bits mode (The LCDHTA component used here was created by Erich Styger; find the component an all the information about it here: http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/ and say Thank you Erich: “Thank you Erich”). Here you can find a video of the implementation of this application: HID HOST WITH FRDM-KL25 The hardware components are: FRMD-KL25 Rev.E Adafruit Prototype Shield v.5 LCD JHD-162A Numeric USB Keyboard (Product Name: Numpad i110, Model No. GK-100010) USB _host Inside the project you can see there is a folder called USB_Host an it contains two important folders with source files: App_keyboard: Contains the specific function for the Keyboard configuration: in use, attached detached, callbacks and more; contain how to handle the data coming from the device. The function process_kdb_buffer is where the data is transmitted to the LCD and use it for the application. Classes: contain the necessary function to handle a hid as the device. Handle all the functions necessary for the USB protocol. Note: The usb_classes.c and usb_classes.h files are generated by processor expert. I attach these two files as well to have a reference how these files must look like. This is because sometimes during the code generation process Processor Expert erases part of the code. I hope this project is useful for you. Best Regards, Adrian.
View full article
This application demonstrates the use of the FRDM-KL25 as a HID HOST. In this project the HID Device is a Numeric Keyboard and the HOST Device (FRDM-KL25) is handling the data and printing them in a 16x2 LCD used in 8 bits mode .
View full article
This is a port of the TWR_K60N512 "Audio" Demo into Kinetis Design Studio and into eGUI 3.0 (from 2.1). The original demo is from Petr Gargulak and was under "Freescale_embedded_GUI_SW.zip\_Official_Demos\EGUI_D4D_Demo\TWR_K60N512\BareMetal\CW_10_1" avaiable on the freescale website. Some of the major porting differnces (this may help others porting similar projects): KDS: KDS by default does not define 'asm()', switch these to '__asm()' or change compiler settings (see: Sorting out asm(); in KDS: How to change your compiler language to GNU ISO90) eGUI 2.1 -> 3.0: Autosize feature has gone, all object sizes now need to be declared Objects seem to add padding of some sort: even with objects where size was previously declared, these had to be increased by ~3px in each direction, else text/images would not render. 'D4D_OBJECT_SYS_FUNCTION' structure no longer contains 'type'. It suggests using strName instead to identifier object. D4D_TEXTBOX no longer has title or icon functionality. When building this project there will be ~7 warnings from the compiler, including 2 of my own. The code should function fine. note: TWR_LCD settings for this project, switches are set up with in following sequence: "01111110". regards, Rael S-R
View full article
           This is a demo of NFC device to read and write the contactless card. Kinets K60 tower board and NXP PN512 board are used for this test enviroment. These connected pins from K60 tower board to PN512 RF board are listed as below:   SPI1:     SPI1_SIN : PTE1/SDHC0_D0     SPI1_SCK : PTE2/SDHC0_DCLK     SPI1_SOUT : PTE3/SDHC0_CMD     SPI1_PCS0 : PTE4/SDHC0_D3     Reset:     PTB9   External interrupt:     PTA26         Because the SPI1 port is used as the host interface of pn512, it is necessary to enable the SPI1 driver in the user configuration file of MQX.           To open the project file in the /build folder with CW10.5.    And the PSP and BSP libraries had to be built before test image is built, as they are needed in this test project.   The following diagram shows the serial numbers and block data of reading from the test card of Mifare one.
View full article
Since the mbed Ethernet library and interface for FRDM-K64 have not yet been fully tested, instead of using mbed we will use one of the latest demo codes from MQX specifically developed for the FRDM-K64 platform. Before starting please make sure you have the following files and software installed in your computer: CodeWarrior 10.6 (professional or evaluation edition) MQX 4.1 for FRDM-K64 (it is not necessary to install full MQX 4.1) JLink_OpenSDA_V2.bin (this is the debugger application) * If you don't have a valid license, you can find a temporary license below, it will only be valid until 7/30/2014 and it will only be available online until 7/05/2014. Building the project The first step to use an MQX project is to compile the target/IDE libraries for the specific platform: 1. Open CodeWarrior and drag the file from the following path C:\Freescale\Freescale_MQX_4_1_FRDMK64F\build\frdmk64f\cw10gcc onto your project area: This will load all the necessary libraries to build the project, once they are loaded build them it is necessary to modify a couple of paths on the BSP: 2. Right click on the BSP project and then click on properties 3. Once the properties are displayed, expand the C/C++ Build option, click on settings, on the right pane expand the ARM Ltd Windows GCC Assembler and select the directories folder, this will display all the libraries paths the compiler is using 4. Double click on the "C\Freescale\CW MCU v10.6\MCU\ProcessorExpert\lib\Kinetis\pdd_100331\inc" path to modify it, once the editor window is open, change the path from "pdd_100331" to "pdd" 5. Repeat steps 2 and 3 for the ARM Ltd Windows GCC Compiler 6. Now you can build the libraries, build them one at a time by right clicking on the library and selecting build project, build them in the following order, it is imperative you do it in that order. BSP PSP MFS RTCS SHELL USBD USBH 7. Once all the libraries are built, import the web hvac demo, do it by dragging the .project file to your project area; the project is located in the following directory:                     C:\Freescale\Freescale_MQX_4_1_FRDMK64F\demo\web_hvac\build\cw10gcc\web_hvac_frdmk64f 8. Once the project is loaded, build it by right clicking on the project folder and select Build project Debugging the project To debug the project it is necessary to update the FRDM-K64 debugging application: Press the reset button on the board and connect the USB cable Once the board enumerates as "BOOTLOADER" copy the JLink_OpenSDA_vs.bin file to the unit Disconnect and reconnect the board On CodeWarrior (having previously compiled the libraries and project) click on debug configurations 5. Select the connection and click on debug 6. Open HVAC.h and change the IP Address to 192.168.1.202 Now the demo code has been downloaded to the platform you will need the following to access all the demo features: Router Ethernet Cable Serial Terminal The code enables a shell access through the serial terminal, it also provides web server access with a series of options to simulate an Heating Air Conditioning Ventilation System, the system was implemented using MQX and a series of tasks, for more details on how the task are created, the information regarding how to modify the code please check the attached document: Freescale MQX RTOS Example guide.
View full article
Here you will find both the code and project files for the USB Mouse project. In this project the USB module is configured as a device, the X and Y coordinates to move the cursor are obtained from the accelerometer measurements. Once the code is loaded it is necessary to disconnect the USB cable from the J26 USB connector and plug it to the K64 USB connector. Once the device enumerates you can use it as an air mouse. The left and right click buttons have not been enabled. To compile the project you must import the following libraries: USBMouse.h FXOS8700Q.h Code: #include "mbed.h" #include "USBMouse.h" #include "FXOS8700Q.h" //I2C lines for FXOS8700Q accelerometer/magnetometer FXOS8700Q_acc acc( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); USBMouse mouse; int main() {     acc.enable();     float faX, faY, faZ;     int16_t x = 0;     int16_t y = 0;       while (1)     {         //acc.getAxis(acc_data);         acc.getX(&faX);         acc.getY(&faY);         x = 10*faX;         y = 10*faY;               mouse.move(x, y);         wait(0.001);     } }
View full article
Here you will find the code and project files corresponding to the I2C-Accelerometer project. The accelerometer/magnetometer is connected to the I2C port, although bot the accelerometer and magnetometer are contained within a single package, they must be initialized individually. In this example the measurements from both devices (X,Y and Z axis) is performed and displayed at the serial terminal. In order to compile the project, the following library must be imported: FXOS8700Q.h Code: #include "mbed.h" #include "FXOS8700Q.h" //I2C lines for FXOS8700Q accelerometer/magnetometer FXOS8700Q_acc acc( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); FXOS8700Q_mag mag( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); //Temrinal enable Serial pc(USBTX, USBRX); MotionSensorDataUnits mag_data; MotionSensorDataUnits acc_data; int main() {     float faX, faY, faZ;     float fmX, fmY, fmZ;     acc.enable();     printf("\r\n\nFXOS8700Q Who Am I= %X\r\n", acc.whoAmI());     while (true)     {         acc.getAxis(acc_data);         mag.getAxis(mag_data);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", acc_data.x, acc_data.y, acc_data.z);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", mag_data.x, mag_data.y, mag_data.z);         acc.getX(&faX);         acc.getY(&faY);         acc.getZ(&faZ);         mag.getX(&fmX);         mag.getY(&fmY);         mag.getZ(&fmZ);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", faX, faY, faZ);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", fmX, fmY, fmZ);                 wait(1.0);     } }
View full article
Here you will find both the code and project files for the ADC project. This project configures the ADC to perform single conversions, by default this is performed using a 16 bit configuration. The code uses ADC0, channel 12, once the conversion is finished it is displayed at the serial terminal. Code: #include "mbed.h" AnalogIn AnIn(A0); DigitalOut led(LED1); Serial pc(USBTX,USBRX); float x; int main() {     pc.printf(" ADC demo code\r\n");     while (1)     {     x=AnIn.read();     pc.printf("ADC0_Ch12=(%d)\r\n", x);     wait(.2);     } }
View full article
Here you can find both the code and project files for the PWM project, in this example a single PWM channel belonging to the Flextimer 0 (PTC10/FTM_CH12) is enabled to provide a PWM signal with a 500ms period, the signal's duty cycle increases its period every 100ms, to visually observe the signal connect a led from the A5 pin in the J4 connector to GND (J3, pin 14). Code: #include "mbed.h" //PWM output channel PwmOut PWM1(A5); int main() {     PWM1.period_ms(500);     int x;     x=1;         while(1)     {         PWM1.pulsewidth_ms(x);         x=x+1;         wait(.1);         if(x==500)         {             x=1;         }     } }
View full article
Here you can find both the code and project files for the Serial communication project, in this example the serial port (UART) is configured to establish communication between the computer using a serial terminal and the evaluation board. The default baud rate for the serial port is 9600 bauds. The code also implements an echo function, any key pressed in the computer's keyboard will be captured and displayed in the serial terminal. If your computer does not have a serial terminal you can download Tera Term from the following link: Tera Term Open Source Project The communication is established through the USB cable attached to the OpenSDA USB port. Code: #include "mbed.h" //Digital output declaration DigitalOut Blue(LED3); //Serial port (UART) configuration Serial pc(USBTX,USBRX); int main() {     Blue=1;     pc.printf("Serial code example\r\n");        while(1)     {         Blue=0;         pc.putc(pc.getc());     }    }
View full article
Here you can find the code and project files for the Interrupt example, in this example 2 KBI interrupts are enabled, one assigned to SW2 and another to SW3, during the main routine the blue led is turned on, when the interrupt routines are triggered the blue led is turned off and the red or green led blink once, the interrupt was configured to detect falling edges only. Code: #include "mbed.h" DigitalOut Red(LED1); DigitalOut Blue(LED3); InterruptIn Interrupt(SW2); void blink() {     wait(.4);     Red=1;     Blue=0;     wait(.4);     Blue=1;     wait(.4); } int main() {     Interrupt.fall(&blink);     Blue=1;     while (1)     {         Red=!Red;         wait(.4);     } }
View full article
Here you can find the code and project files for the GPIO example, in this example the 3 colors of the RGB led are turned on sequentially when the SW2 push button is pressed, the led pin definition is shared throughout all the freedom platforms. The wait function can be defined in seconds, miliseconds or microseconds. Code: #include "mbed.h" //Delay declared in seconds /*GPIO declaration*/ DigitalOut Red(LED1);         DigitalOut Green(LED2); DigitalOut Blue(LED3); DigitalIn sw2(SW2); int main() {     /*Leds OFF*/     Red=1;     Green=1;     Blue=1;         while(1)     {         if(sw2==0)         {             Red = 0;             wait(.2);             Red = 1;             wait(1);                                Green=0;             wait(.2);             Green=1;             wait(1);                         Blue=0;             wait(.2);             Blue=1;             wait(1);         }     } }
View full article
Welcome to the FRDM-K64 mbed workshop, in this page you will find all the code examples we will review on this session. The program covers the following modules: GPIO Serial communication Interrupts PWM ADC I2C (Accelerometer) USB Ethernet Depending on how fast we advance during the session some of the modules might be skipped; however here you can find both the source code and binary files ready to be flashed into the FRDM-K64 development board. FRDM-K64Z120M The FRDM-K64 is fully compatible with the Arduino rapid prototyping system, the following image depicts the board's pinout, the green labels can be used directly into your mbed proyects, they have already been defined in the headers and libraries in order to make development easier. Sign up at mbed.org In order to create the projects covered on this session it is necessary to create an mbed user account, open the website and create a user account, if you have already signed up please log in. Mbed debugging application To enable the FRDM-K64 development board using the binary files generated by mbed it is necessary to update the board's firmware, follow the steps mentioned below in order to enable the board to be programmed: Press the board's reset button While pressing the reset button connect the board to your computer using the USB cable, it must be connected to the J26 USB connector. Once the unit has enumerated as "Bootloader", copy the 20140530_k20dx128_k64f_if_mbed.bin file into the unit Disconnect and reconnect the USB cable, the board must enumerate as "MBED" Serial communication driver To implement serial communication you need to install the serial driver in your computer, download the driver, once your board has enumerated as MBED execute the driver and wait for it to be finished, this might take a couple of minutes. Serial terminal In order to communicate with the board via serial port it is necessary to use a serial terminal, by default WIndows 7 and 8 do not have this application, XP does. If your OS does not feature a serial terminal, you can download the one at the bottom (Teraterm). ! Your board is now ready to be programmed using mbed!
View full article
      The MKW01Z device is highly-integrated, cost-effective, smart radio, sub-1 GHz wireless node solution composed of a transceiver supporting FSK, GFSK, MSK, or OOK modulations with a low-power ARM® Cortex M0+ CPU. The highly integrated RF transceiver operates over a wide frequency range including 315 MHz, 433 MHz, 470 MHz, 868 MHz, 915MHz, 928 MHz, and 955 MHz in the license-free Industrial, Scientific and Medical (ISM) frequency bands. This configuration allows users to minimize the use of external components.      The MPXY8600 is a sensor for use in applications that monitor tire pressure and temperature. It contains the pressure and temperature sensors, an X-axis and a Z-axis accelerometer, a microcontroller, an LF receiver and an RF transmitter all within a single package.        This setup offer customers to utilize Freescale MPXY8600/8700 as transmitter and MKW01 as receiver to form 315MHz, 433.92MHz TPMS transmitter and receiver  total solution.
View full article