Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
Recently I was told that there really lack of enough document && demo regarding the lwIP stack with SDK. So I would like to share more detail regarding this topic, and hope it will been helpful and useful. Introduction Small independent implementations of the TCP/IP protocol suite One of the most widely used TCP/IP stack Under a BSD-style license Support run in both bare metal and RTOS environment Suitable for use in embedded system with tens of free RAM and room for around 40 kilobytes of code ROM lwIP stack on KSDK     - <ksdk_install_dir>/middleware/tcpip/lwip lwIP stack on KSDK - Code Structure lwIP code structure is shown as below: src     This subfolder includes the latest stable lwIP 1.4.1 source code which can be downloaded from this link: download.savannah.gnu.org/releases/lwip/ port     This subfolder includes the adapter code which adapts lwIP stack to SDK. lwIP stack on KSDK - Source Code Structure of source code under is shown below: lwIP stack on KSDK – Adapter code <ksdk_install_dir>/middleware/tcpip/lwip/port <ksdk_install_dir>/middleware/tcpip/lwip/port/arch These Adapter code could be divided into four types:         Ethernet driver adapter code         OSA adapter code         Additional code         lwIP stack configuration code Ethernet Driver Adapter Code Provide Ethernet relevant interface including    − Ethernet hardware initialization    − Network interface initialization    − Send packet to Ethernet hardware    − Receive packet from Ethernet hardware    − Pass packet to lwIP stack Both polling and interrupt mode are provided for packet receiving     - In <ksdk_install_dir>/platform/drivers/inc/fsl_enet_driver.h,          #define ENET_RECEIVE_ALL_INTERRUPT 0 to enable polling mode.          Or set          #define ENET_RECEIVE_ALL_INTERRUPT 1 to enable interrupt mode. Ethernet driver adapter code provides ENET_receive API for polling mode Under RTOS environment, a separate task executing ENET_receive for packet receiving is created in Ethernet hardware initialization code for polling mode Under Bare Metal environment the ENET_receive API need to be called endlessly to do packet receiving OSA Adapter Code Provide OS dependent types and interface for RTOS environment (configured NO_SYS = 0)    −Semaphore    −Mutex    −Mailbox    −Thread Provide time tick for bare metal environment(NO_SYS = 1) sys_now to get the current time sys_assert to print an assertion messages and abort execution. Additional Code Provide definition and interface for:    −Typedefs    −Compiler hints for packing and platform specific    −Diagnostic output lwIP Stack Configuration Code Provides a way to override much of the behavior of lwIP based on opt.h.     − Module support (Code size)           Default inclusions:     ARP (LWIP_ARP)     UDP (LWIP_UDP) and UDP-Lite (LWIP_UDPLITE)     TCP (LWIP_TCP) -- this is a big one!     Statistics (LWIP_STATS)          ……          Default exclusions:    DHCP (LWIP_DHCP)    AUTOIP (LWIP_AUTOIP)    SNMP (LWIP_SNMP)    IGMP (LWIP_IGMP)    PPP (PPP_SUPPORT)    − Memory management (RAM usage)              lwIP’s custom heap-based mem_malloc              C standard library malloc and free              Memory pools lwIP Stack Porting Guide    Possible Situation for Porting New Soc with Limited RAM In current KSDK, the main RAM consumption for lwIP is show below: If resource on the new platform is not enough, could reduce ram consumption for ram_heap and pbuf_pool.         In lwip/port/lwipopts.h: #define MEM_SIZE                (12*1024)    /**the size of ram_heap/ #define PBUF_POOL_SIZE          10      /*the number of buffers in the pbuf pool. */ #define PBUF_POOL_BUFSIZE       1518 /* the size of each pbuf in the pbuf pool. */ pbuf_pool also support dynamically allocate from ram_heap.        In lwip/include/opt.h:          #define MEMP_MEM_MALLOC     1 /*Use mem_malloc/mem_free to do allocate*/ Use libc malloc/free to manage the memory allocation instead of mem_malloc/mem_free, memory definition for ram_heap is not needed.         #define MEM_LIBC_MALLOC       1 /*Use malloc/free/realloc provided by C-library*/   New Soc NOT Support PIT timer OSA adapter code should provide Bare metal lwIP stack with a 1ms period timer. Current the code use pit timer to do this and the definition in sys_arch.c is as below: #define HWTIMER_LL_DEVIF    kPitDevif      // Use hardware timer PIT #define HWTIMER_LL_SRCCLK   kBusClock     // Source Clock for PIT #define HWTIMER_LL_ID       3 #define HWTIMER_PERIOD          1000      // 1 ms interval If the new platform does not provide PIT, we could use other hardware timers to implement the 1ms period timer. Lightweight TCP/IP (lwIP) Stack Porting v Lightweight TCP/IP (lwIP) Stack Porting Guide Lightweight TCP/IP (lwIP) Stack Porting Guide
記事全体を表示
Nested Vectored Interrupt Controller Module by Vicente Gómez Freescale TIC. NVIC Explanation Hands-on IRQ using a pin. Interruption timers. Presentación de la NVIC (Nested Vectored Interrupt Controller) por Vicente Gómez, Freescale TIC. Explicación de la NVIC. Hands-On IRQ usando un pin. Timers con interrupción
記事全体を表示
USB secondary ISP bootloader for LPC11U68  Overview        A Secondary Bootloader (SBL) is a piece of code that allows a user application code to be downloaded using alternative channels other than the standard UART0 used by the internal bootloader (on chip). Possible secondary bootloaders can be written for USB, Ethernet, SPI, SSP, CAN, and even I/Os. The secondary bootloader utilizes IAP as a method to update the user’s application code.        The internal bootloader is the firmware that resides in the microcontroller’s boot ROM block and is executed on power-up and resets. After the boot ROM’s execution, the secondary bootloader would be executed, which will then execute the user application.      The purpose of this document is to use USB as an example for developing the secondary bootloader and the code was tested using the LPCXpresso 11U68 evaluation board.       The MSCD presents easy integration with a PC‘s operating systems. This class allows the embedded system’s flash memory space be represented as a folder in Windows/Linux. The user can update the flash with the binary image using drag and drop, so the following sections will present a guideline for development and implementation of the USB secondary bootloader design, configuration, and test.      USB secondary bootloader code is base on the USB Mass Storage Class demo. However in this application note, we do not attempt to explain how the Mass Storage Class is implemented. Fig 1 LPCXpresso Board for LPC11U68 Setup file (sbl_config.h)       This file configures the secondary bootloader. The user should change this according to their application.       Some definitions and explanation: MAX_USER_SECTOR – This parameter is device dependent. In a 256 KB device, it will be 29 sectors, however the size of the last 5 sectors become the 32 KB instead of the 4 KB, so in the application, MAX_USER_SECTOR chooses 23 (Fig 2). CRP – Code Read Protection. This parameter allows select the desired CRP level. Choosing CRP3, the primary bootloader’s entry mechanism check will be bypassed. Fig 3 for CRP details. Fig 2 Flash sectors in LPC11U68 Fig 3 Code Read Protection (CRP) Secondary bootloader entry        The boot sequence shown below is used when entering the secondary USB bootloader. Fig 4 Using an entry pin      The secondary USB bootloader will check the status of a GPIO pin to determine if it should enter into programming mode. This is the easiest way since no post processing is needed. And this secondary bootloader uses P0.16. Automatic secondary bootloader entry       If the secondary USB bootloader detects that no user application is present upon reset, it will automatically enter programming mode. ISP entry disabled     If the secondary USB bootloader detects that a user application has already been installed and that CRP is set to level 3, then it will not enter ISP mode. Bootloader size        Since the bootloader resides within user programmable flash, it should be designed as small as possible. The larger the secondary USB bootloader is the less flash space is available to the user application. By default, the USB bootloader has been designed to fit within the first two flash sectors (Sector 0-1) so that the user application can start from sector 2. Code placement in flash       The secondary bootloader is placed at the starting address 0x0 so that it will be executed by the LPC11U68 after reset. Flash programming is based on a sector-by-sector basis. This means that the code for the user application should not be stored in any of the same flash sectors as the secondary bootloader and for efficient use of the flash space, the user application should be flashed into the next available empty sector after the bootloader.        In the application, the start sector is 3 (0x0000_3000) which is used to store the user application code. User application execution        If the SW2 button is not depressed, the secondary bootloader will start the execution of the user application. Execution of the user application is performed by updating the stack pointer (SP) and program counter (PC) registers. The SP points to the new location where the user application has allocated the top of its stack .The PC on the other hand contains the location of the first executable instruction in the user application. From here on the CPU will continue normal execution and initializations specified on the user application. By default, the bootloader uses 2 flash sectors. Therefore, to utilize the remaining flash, the secondary bootloader will look for the user application at 0x00003000 Handing interrupts      The LPC11U68 contains a NVIC (Nested Vectored Interrupt Controller) that handles all interrupts. When an interrupt occurs the processor uses the vector table to locate the address of the handler.      On the LPC11U68 the vector table is located in the same area of flash memory as the secondary bootloader. The secondary bootloader is designed to be permanently resident in flash memory and therefore it is not possible to update the contents of the vector table every time a new application is downloaded.       The Cortex-M3 core allows the vector table to be remapped; however this is not the case with the Cortex-M0. Because of this, the secondary bootloader has been designed to redirect the processor to the handler listed in a vector table located in the application area of flash memory, see Fig 5. Fig 5 User application       To execute the user application the secondary USB bootloader will load the new SP and PC values into their respective registers, allowing the CPU to execute the new code correctly. Therefore, the user application must be built so that it can run from that starting address. In the application, this address is 0x00003E00. So relocate the user application storage area by following corresponding IDE’s User Guide.  Testing  Creating the binary file             In this application, I build the demos_switch_blinky which is from the LPCOpen library to create the binary which is compatible with the secondary USB bootloader. The binary see Table 1. 08 04 00 10 B5 09 00 00 07 07 00 00 9B 09 00 00 00 00 00 00 00 00 00 00 00 00 00 00 A1 E1 FF EF 00 00 00 00 00 00 00 00 00 00 00 00 A7 09 00 00 00 00 00 00 00 00 00 00 E5 09 00 00 27 03 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 01 03 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E1 09 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 38 B5 63 4C 25 68 28 07 07 D5 96 20 E0 60 61 48 00 78 00 28 01 D1 00 F0 F7 F8 20 68 0C 21 29 40 01 43 21 60 31 BD 38 B5 5A 4C A0 78 40 1C A0 70 C0 B2 65 28 34 DB 00 25 A5 70 20 78 00 28 2F D0 60 78 00 28 03 D0 02 28 16 D0 0A D3 20 E0 01 21 00 F0 CA F8 00 21 01 20 00 F0 C6 F8 00 21 02 20 13 E0 01 21 01 20 00 F0 BF F8 00 21 00 20 00 F0 BB F8 00 21 02 20 08 E0 01 21 00 F0 B5 F8 00 21 01 20 00 F0 B1 F8 00 21 01 20 00 F0 AD F8 00 E0 65 70 60 78 40 1C 60 70 C0 B2 03 28 00 DB 65 70 31 BD F8 B5 00 F0 36 F9 00 F0 C2 F8 3A 48 01 68 02 22 91 43 01 60 01 68 38 4A 0A 40 02 60 35 4F 01 20 38 70 36 48 00 68 0A 21 00 F0 2B F9 1E 21 00 F0 28 F9 40 1E 00 26 80 21 49 04 88 42 0C D2 30 49 48 60 30 48 02 68 12 02 12 0A C0 23 1B 06 13 43 03 60 8E 60 07 20 08 60 01 20 2B 49 08 60 23 4C 20 00 00 F0 18 F9 29 48 01 68 80 22 12 03 0A 43 02 60 20 68 01 21 01 43 21 60 20 68 01 21 88 43 20 60 20 68 80 21 88 43 20 60 A6 60 FA 20 80 00 60 60 20 68 40 21 01 43 21 60 20 68 80 21 01 43 21 60 20 68 80 20 80 04 1A 49 08 60 20 68 30 21 01 43 21 60 18 4D 28 78 00 28 12 D1 38 78 00 28 0E D0 00 21 00 20 00 F0 3E F8 00 21 01 20 00 F0 3A F8 00 21 02 20 00 F0 36 F8 FA 20 80 00 E0 60 3E 70 E8 7B 00 28 E6 D1 01 20 38 70 E3 E7 00 40 02 40 04 00 00 10 00 20 00 A0 FF FF FE FF 00 00 00 10 10 E0 00 E0 20 ED 00 E0 1C 80 04 40 14 82 04 40 00 E1 00 E0 01 00 00 A0 49 01 40 18 83 54 70 47 10 B5 32 4C 20 00 00 F0 BF F8 E1 21 49 02 20 00 00 F0 C7 F8 03 20 E0 60 81 20 A0 60 80 20 20 63 10 BD 00 00 03 28 00 DB 70 47 80 B5 01 23 4B 40 2D A1 0A 5C 2B A1 09 5C A0 20 00 06 FF F7 DC FF 01 BD 00 00 03 28 00 DB 70 47 10 B5 A0 21 09 06 24 A2 12 5C 92 00 89 18 8C 22 92 01 01 23 00 BF 21 A4 20 5C 83 40 8B 50 10 BD 00 00 F8 B5 FF F7 C7 FF A0 25 2D 06 28 00 00 F0 B6 F8 00 24 00 BF 18 A6 31 5D 88 00 28 18 80 22 92 01 80 18 00 BF 15 A2 12 5D 03 68 01 27 97 40 1F 43 07 60 01 23 28 00 FF F7 A9 FF 64 1C 03 2C EA DB F1 BD 00 00 80 B5 07 48 01 68 80 22 52 02 0A 43 02 60 19 22 0A A1 04 48 00 F0 98 F8 01 BD 00 00 00 80 00 40 80 80 04 40 00 40 04 40 80 B5 FF F7 E9 FF 00 F0 B1 F8 01 BD 02 02 02 00 11 10 12 00 00 03 81 00 00 04 81 00 00 05 81 00 00 08 81 00 00 09 81 00 00 0B 02 00 00 0C 02 00 00 0D 02 00 00 0E 02 00 00 12 81 00 00 13 81 00 00 17 01 00 01 09 01 00 01 0B 81 00 01 0E 81 00 01 14 82 00 01 15 82 00 01 16 81 00 01 17 82 00 01 1A 81 00 01 1B 81 00 01 1D 81 00 02 00 01 00 02 01 01 00 02 03 82 00 80 B5 00 F0 EF F8 01 49 08 60 01 BD 00 00 00 10 80 B5 03 4A 12 68 12 69 52 68 90 47 02 BD 00 00 F8 1F FF 1F 03 48 01 68 80 22 D2 05 0A 43 02 60 70 47 00 00 80 80 04 40 15 49 01 22 8A 61 0A 68 80 23 5B 01 13 43 0B 60 07 21 81 60 10 21 81 62 70 47 70 B5 04 00 0D 00 01 20 0E 49 08 60 00 F0 8F F8 06 00 29 01 FF F7 D3 FF 01 00 E0 68 80 22 02 43 E2 60 C8 B2 20 60 08 04 00 0E 60 60 E0 68 80 22 90 43 E0 60 30 00 FF F7 C2 FF 70 BD 00 00 80 80 04 40 98 80 04 40 02 48 01 68 40 22 0A 43 02 60 70 47 80 80 04 40 00 2A 00 D1 70 47 30 B4 0C 68 23 0C 25 0A E4 B2 00 2C 12 D0 02 2C 01 D0 0A D3 11 E0 ED B2 AC 00 04 19 02 2D 01 DB F4 25 00 E0 F0 25 63 51 07 E0 2D 06 AC 0D 04 19 23 66 02 E0 2D 06 AC 0D 03 51 09 1D 52 1E E0 D1 30 BC 70 47 FE E7 38 B5 20 20 00 F0 E8 F8 00 20 00 90 11 48 02 E0 00 99 49 1C 00 91 00 99 81 42 F9 DB 01 20 00 F0 1F F8 0D 48 01 68 01 24 03 22 91 43 21 43 01 60 80 20 00 F0 C7 F8 09 4D 23 20 28 60 80 20 00 F0 CB F8 68 68 C0 07 FC D5 2C 67 03 20 00 F0 10 F8 31 BD 00 00 C4 09 00 00 10 C0 03 40 08 80 04 40 42 49 FF E7 08 60 00 20 48 60 01 20 48 60 70 47 3F 49 F7 E7 43 A0 CA 05 12 0F 92 00 80 58 C9 06 C9 0E 49 1C 49 00 FF F7 49 FF 00 BD 00 B5 00 20 3B 49 03 22 8B 6E 13 40 11 D0 02 2B 11 D0 02 D3 03 2B 10 D0 00 BD 89 6B 0A 40 08 D0 01 2A 03 D0 03 2A 1A D1 31 48 00 E0 2F 48 00 68 00 BD 2D 48 00 BD C9 69 D6 E7 8B 6B 1A 40 08 D0 01 2A 03 D0 03 2A 05 D1 29 48 00 E0 27 48 00 68 00 E0 25 48 09 68 C9 06 C9 0E 49 1C 48 43 00 BD 00 00 00 00 10 B5 00 20 22 4C 03 21 A2 6E 0A 40 30 D0 02 2A 15 D0 21 D3 03 2A 2C D1 A2 6B 11 40 08 D0 01 29 03 D0 03 29 05 D1 19 48 00 E0 17 48 00 68 00 E0 14 48 21 68 C9 06 C9 0E 49 1C 48 43 19 E0 E1 69 14 A0 CA 05 12 0F 92 00 80 58 C9 06 C9 0E 49 1C 49 00 FF F7 EB FE 0C E0 A2 6B 11 40 08 D0 01 29 03 D0 03 29 05 D1 09 48 00 E0 07 48 00 68 00 E0 04 48 21 6F FF F7 DA FE 10 BD 00 00 40 80 04 40 70 80 04 40 00 1B B7 00 D0 09 00 00 D4 09 00 00 08 80 04 40 00 00 00 00 C0 27 09 00 90 05 10 00 C0 5C 15 00 F0 B3 1A 00 20 0B 20 00 00 9F 24 00 E0 32 29 00 C0 C6 2D 00 50 97 31 00 E0 67 35 00 70 38 39 00 00 09 3D 00 40 16 40 00 80 23 43 00 C0 30 46 00 0B 49 0A 68 10 43 09 4A 02 40 C8 20 00 02 10 43 08 60 70 47 06 49 0A 68 82 43 04 48 10 40 C8 22 12 02 02 43 0A 60 70 47 00 00 00 00 FF 25 00 00 38 82 04 40 70 B4 01 21 00 22 13 E0 04 68 00 1D 0C 42 02 D0 4D 46 6D 1E 64 19 22 60 24 1D 1B 1F 04 2B FA D2 25 00 9E 07 01 D5 22 80 AD 1C 0B 40 00 D0 2A 70 03 68 00 1D 00 2B E7 D1 70 BC 70 47 10 B5 07 49 79 44 18 31 06 4C 7C 44 16 34 04 E0 08 1D 0A 68 89 18 88 47 01 00 A1 42 F8 D1 10 BD 08 00 00 00 14 00 00 00 9D FF FF FF 08 00 00 00 00 00 00 10 00 00 00 00 00 F0 0B F8 00 28 01 D0 FF F7 DE FF 00 20 00 BF 00 BF FF F7 0C FD 00 F0 02 F8 01 20 70 47 80 B5 00 F0 02 F8 01 BD FE E7 07 46 38 46 00 F0 02 F8 FB E7 FE E7 20 21 09 03 26 31 18 20 AB BE F9 E7 01 48 80 47 01 48 00 47 D9 09 00 00 C5 09 00 00 00 BF 00 BF 00 BF 00 BF FF F7 D2 FF 00 1B B7 00 00 80 00 00 80 B5 FF F7 DF FD 01 BD FE E7 FE E7 FE E7                                                    Table 1 Drag and drop the binary file Running the secondary bootloader, and connect a USB cable between the PC and the J3, see Fig 6; Fig 6 Drag and drop the binary file to the driver, see Fig 7;    Fig 7 Review the values of the user application in the relative area , see Fig 8; Fig 8
記事全体を表示
The Multipurpose Clock Generator module explained by Ali Piña, Freescale TIC. MCG Module Explanation Connection Diagram Operation Modes Hands On Toggle a LED in FEI (FLL engaged Internal) switch to PEE (PLL Engaged External). Watch changes. Switch from different operation modes. El Módulo de MCG (Multipurpose Clock Generator) presentado por Ali Piña, Freescale TIC. Explicación del Modulo MCG. Diagrama de conexiones Modos de operación. Hands-On Togglear un LED en modo FEI (FLL engaged Internal) y cambiar a PEE(PLL Engaged External). Observar cambios. Moverse entre varios modos de operación
記事全体を表示
飞思卡尔拥有成套的电机控制处理器产品、强大的工具和专家支持,为大量应用提供高性价比且节能的电机控制解决方案,您可以在飞思卡尔官网电机控制主页上找到相应的电机控制参考方案。链接如下: http://www.freescale.com/zh-Hans/webapp/sps/site/homepage.jsp?code=MOTORCONTROLHOME 下文也列出BLDC和PMSM常用的控制参考方案,方便查询。 BLDC(无刷直流电机)参考设计 M0+方案 AN4776 - BLDC motor control with Hall sensor based on FRDM-KE02Z 附代码包AN4776SW AN4869 - 基于FRDM-KE04Z和Tower Board的BLDC电机正弦波控制 附代码包AN4869SW AN4796 - 基于FRDM-KE02Z和Tower Board的无传感器BLDC电机控制 附代码包AN4796SW AN4862 - 利用MKV10x实现三相BLDC无传感器控制   附代码包AN4862SW DRM144 - Three-phase BLDC sensorless motor control application AN4870 - Tuning 3-Phase BLDC motor sensorless control using MKV10  附代码包AN4870SW DRM151 - 采用Kinetis KEA128 MCU的3相无传感器BLDC电机控制参考设计 M4方案 AN4376 - 基于 kinetis 和 MQX 的带霍尔传感器的无刷直流电机控制 AN4254 - 在Freescale MQX实时操作系统下进行电机控制 DRM135 - 3-phase BLDC sensorless control with Kinetis MCU (MQX) 附代码包DRM135SW AN4597 - BLDC Sensorless Algorithm Tuning Three-Phase BLDC Sensorless Motor Control Using the MKV4x In Quadcopter Application 附代码包AN5169SW DSC方案 AN4413 - BLDC Motor Control with Hall Sensors Driven by DSC  附软件包AN4413SW AN1916 - 基于 56800/E 数字信号处理器和霍尔传感器的三相 BLDC电机控制 DRM025 - 3-Phase BLDC Motor Control with Hall Sensors Using 56F805 Designer DRM022 - 3-Phase BLDC Drive Control with Hall Sensors Reference Design AN1913 - 3-phase BLDC Motor Control with Sensorless Back-EMF ADC Zero Crossing Detection using DSP 56F80x AN1914 - 3-Phase BLDC Motor Control with Sensorless Back EMF Zero Crossing Detection Using DSP56F80x DRM108 - 采用 MC56F8006 的 BLDC 无传感器参考设计 DRM077 - PMSM and BLDC Sensorless Motor Control using the 56F8013 Device Designer DRM078 - 3-Phase BLDC Drive Using Variable DC Link Six-Step Inverter Designer DRM027 - 3-Phase Sensorless BLDC Motor Control with Back-EMF Zero Crossing Detection Using 56F805 Designer DRM098 - Direct PFC Using the MC56F8013 DRM070 - Three-Phase BLDC Motor Sensorless Control Using MC56F8013/23 Design DRM026 - 3-Phase BLDC Motor Control with Sensorless BACK-EMF ADC Zero Crossing Detection Using 56F805 AN1961 - 3-Phase BLDC Motor Control with Quadrature Encoder Using the 56F800/E PMSM(永磁同步电机)参考设计 M0+方案 AN5049 - Three-Phase PMSM Sensorless FOC Using the MKV10Z32 with Automated Motor Parameters Identification 附代码包AN5049SW AN4935 - 利用Kinetis KV10实现适用于风扇的PMSM无传感器磁场定向控制 (FOC)   附代码包AN4935SW DRM148 - 无位置PMSM矢量控制参考设计 M4方案 DRM128 - PMSM Vector Control with Quadrature Encoder on Kinetis AN4911 - 利用MKV31F实现三相PMSM无传感器FOC  附代码包AN4911SW AN5004 - Sensorless PMSM Control on MKV46F256 Using Kinetis SDK 附代码包AN5004SW AN4912 - Tuning 3-Phase PMSM Sensorless control application using MCAT Tool DRM140 - PMSM Sensorless Vector Control on Kinetis AN4489 - Using CMSIS-DSP Algorithms with MQX and Kinetis MCUs AN4381 - Configuring the FlexTimer for position and speed measurement AN3729 - Using FlexTimer in ACIM/PMSM Motor Control Applications MCLIBCORETXM4UG - Set of General Math and Motor Control Functions for Cortex M4 core PMSMCONUG - PMSM Vector Control with Encoder on Kinetis AN4680 - PMSM electrical parameters measurement DSC方案 AN4656 - PMSM FOC of Industrial Drives using the 56F84789 PMSMUG - PMSM Field-Oriented Control Using MC56F84789 DSC With Encoders DRM098 - Direct PFC Using the MC56F8013 DRM029 - 3-Phase PM Synchronous Motor Control with Quadrature Encoder Using 56F805 Designer DRM102 - PMSM Vector Control with Single-Shunt Current-Sensing Using MC56F8013/23 Design DRM018 - 3-Phase PM Synchronous Motor Torque Vector Control Using 56F805 Designer DRM036 - Sine Voltage Powered 3-Phase Permanent Magnet Synchronous Motor with Hall Sensors Designer AN5014 - Three-Phase PMSM Sensorless FOC using MC56F82748 and MC56F84789 with Automated Motor Parameter Identification  附代码包AN5014SW DRM110 - Sensorless PMSM Control for an H-axis Washing Machine Drive Designer DRM099 - Sensorless PMSM Vector Control with a Sliding Mode Observer for Compressors Using MC56F8013 DRM139 - Dual Sensorless PMSM Field-Oriented Control With Power Factor Correction on MC56F84789 DSC AN4608 - 在MC56F84789上使用PWM和ADC,驱动双PMS电机FOC AN4583 - MC56F84789 Peripherals Synchronization for Interleaved PFC Control                 若文档链接有变动或失效,请在飞思卡尔官方网站上通过文档名称(如AN4912、DRM139等)搜索相应文档。
記事全体を表示
KL17 reference manual V4.1 and V5.1 with updated Figure 13-2. Kinetis Bootloader Start-up Flowchart at page 179 There with modification to add "is direct boot valid" check. Please check below picture for the detailed info: The "is direct boot valid" check function is not supported for KL17 product, the correct flow chart should be below: The "is direct boot valid" check function is reserved for further parts(such as KL82), which has one bit in BCA filed to control running code in QSPI Flash or internal Flash: Thank you for the attention.
記事全体を表示
@@This article describes how to do in-system reprogramming of Kinetis for Cortex-M4 core devices using standard communication media such as SCI. Most of the codes are written in C so that make it easy to migrate to other MCUs. The solution has been adopted by customers. This bootloader is based on FRDM-K22 demo board and KDS3.0. The bootloader and user application source codes are provided. GUI is also provided. Customer can make their own bootloader applications based on them. The application can be used to upgrade single target board and multi boards connected through networks such as RS485. The bootloader application checks the availability of the nodes between the input address range, and upgrades firmware nodes one by one automatically. Key features of the bootloader: Able to update (or just verify) multiple devices in a network. Application code and bootloader code are in separated projects, convenient for mass production and firmware upgrading. Bootloader code size is small, only around 3k, which reduces on chip memory resources. Source code available, easy for reading and migrating. For Cortex-M0+ products, please refer to here :Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+ , it based on FRDM-KL26. The main difference between Cortex-M4 and Cortex-M0+ is the FLASH program routine. - In Cotex-M4 core kinetis, we need copy the Flash operating routines to RAM. In the bootloader code, the copy to ram code is realized in the function of “FLASH_Initialization()”: Byte buffer[200]={0}; - In Cotex M0+ core kinetis, we do not need to copy the Flash operating routines to RAM. Platform Control Register (MCM_PLACR) is added. The MCM_PLACR register selects the arbitration policy for the crossbar masters and configures the flash memory controller. Enabling ESFC bit can stall flash controller when flash is busy.  Setting ESFC bit can well-balance time sequence of Flash reading and writing – when writing Flash, reading Flash instruction can wait, and vice versa. Using ESFC bit can make our flash programming easier. Thus one Flash can write itself, which is not possible for other one Flash MCU without ESFC bit control. ESFC bit is easy to be set in C code: For more information, please see attached document and code. User can also download the document and source code from Github: https://github.com/jenniezhjun/Kinetis-Bootloader.git
記事全体を表示
1. 飞思卡尔常用调试工具 2. 使用OpenSDA平台作为J-Link调试Kinetis 3. 使用OpenSDA平台作为USBDM调试Kinetis 4. 使用MTB模块快速跟踪定位Cortex-M0+指令执行状态(Use MTB in Cortex-M0+ to trace instructions) 5. KL25被加密,芯片锁死问题? 6. 对比几款流行的Kinetis调试器速度 7. 修复Jlink固件损坏的方法 8. Jlink调试Kinetis L系列的使用方法 9. CMSIS-DAP调试器在IAR v7.1中问题(Probe not Found)修复 10. FRDM_KL26 虚拟串口安装失败的解决方法 11. 使用J-Link TCP-IP Server通过以太网远程下载程序到Kinetis 12.Kinetis LOCK的原因及解决方案​
記事全体を表示
This years annual hacker security conference known as DEFCON used a couple of NXP devices for this years electronic badge. This document is to explain how to program the device and add extra components. The badge was developed by Grand Idea Studio, with engineering help from NXP, and this presentation has details about the development of the badge. I'm the NXP systems engineer that was helping people get started with reprogramming their badge at Defcon, and wanted to create something that gives all the details on how to do that yourself.  Full schematics and firmware source code can be found at: http://www.grandideastudio.com/defcon-27-badge/   The badge has these two NXP devices:  KL27  - MKL27Z64VDA4 - 48Mhz ARM Cortex M0+ microcontroller w/ 64KB flash (Datasheet and Reference Manual) NXH2261UK- Near Field Magnetic Induction (NFMI) chip for the wireless communication. Has a range on the badge of about 6 inches (15cm), but the technology can work a bit further. It's often found in high end headphones because BLE waves are disrupted by your head but these waves aren't. Also less power consumption. Using the serial port: There's a serial interface which prints out helpful information and there's some "secrets" available if you have a completely leveled up badge. It'll also be really helpful if you're writing new code to hack your badge for printf debugging. Note that you cannot program the board by default over the serial port. This particular chip doesn't support that, though some of our other chips do. It of course would be possible to write a serial bootloader for it, but that's definitely not beginner level. You'll need two pieces of hardware: 1) Header Pins 3) Serial-to-USB converter Header Pin: You can solder on a header to the PCB footprint. Because of the quartz, the leads would need to be flat on the PCB. A Harwin M20-8770442 will fit the footprint and is what was provided at the soldering village and what you see in the photos below. You could also try creating your own header.  Serial to USB Converter: Since almost no computer today comes with a serial port, a serial to USB converter dongle is needed. It'll have four pins: GND, Power, TX, and RX. The DEFCON badge runs at 1.8V, but the chip itself is rated up to 3.6V, so a 3.3V dongle can be used *as long as you do not connect the power pin on the serial header*. You only need to connect GND, RX, and TX. In a production design you would not want an IO voltage above VCC, but for hacking purposes it'll work, and I've used it all week without an issue on multiple boards.  There's a lot of options. Here's a 1.8V one if you want to be extra cautious or a 3.3V one that already comes with connectors for $8. Anything that transmits at 1.8V or 3.3V will work so you may already have one, but again, just don't connect the power pin.    Software: You'll need to install a serial terminal program like TeraTerm or Putty.  1) Plug the 3.3V or 1.8V USB converter dongle into your computer and it should enumerate as a COM port.  2) Connect the GND line on the dongle to GND on the header 3) Connect the TX pin on the dongle to the RX pin on the header 4) Connect the RX pin on the dongle to the TX pin on the header (it is not RX to RX, I spent 2 whole days tearing my hair out over that during my robotics project in college) 5) DO NOT CONNECT THE POWER PIN  5) Should look like the following when finished 6) In your serial terminal program, connect to the COM port your dongle enumerated as 7) Find the serial port settings menu (in TeraTerm it's in Setup->Serial Port from the menu bar) , and set the baud rate to 115200. The other settings should not need to be changed (8 data bits, no parity, 1 stop bit).  😎 In the terminal, press enter. You should get a > prompt 9) In the terminal, press the '?' key on your keyboard, and hit enter, you'll see the menu.         10) Note that the key you press won't show up in the terminal, but just press Enter and then the command will be run 11) Hit Ctrl+x to exit interactive mode and turn back on the radio.  12) While not in interactive mode, the terminal will display the transmit packet of any badge you bring close to it.  Reprogramming Your Badge: Hardware:  There's two pieces of hardware needed: 1) Programmer/debugger 2) Programming cable Program Debugger: Most any ARM Cortex M debug programmer can be used, as the KL27 chip has a ARM M0+ core. I'd recommend the LPC-Link2 as it's only $20 and can be bought directly from NXP or from most distributors (like Mouser or DIgikey). Search for "OM13054". But you could also use a J-Link, PEMicro, or others if you already have an ARM programmer. Cable: The DEFCON badge has the footprint for a Tag Connect TC2050-IDC-NL-050-ALL. Because this cable is meant for manufacture programming and not day-to-day debugging, if you plan on stepping through code, you'll also want to pop off the the quartz front and get some retainer clips to keep the programmer connected to the board. If you just simply want to reprogram the board, you can just snip off the 3 long guide clips, and press the cable against the PCB while holding your hand steady for the ~5 seconds it takes to flash it each time.  Alternatively if you already have a JTAG/SWD cable and have soldering skills, you can use some fine gauge wire and hack up your own converter to your board like /u/videlen did with some true hacker soldering. However as /u/int23h pointed out, because it's using Single Wire Debug (SWD) you only need to really solder 2 of the pins, SWDIO and SWDCLK. However nRESET is also recommended as it'll let you take control of the device if it's in sleep mode (which it is most of the time). Power (which is needed so the programmer knows what voltage to send the signals at) and GND you can get from the serial header. Software There's three pieces of software you'll need:  1) Compiler 2) MCUXpresso SDK for the KL27  3) Badge source code Compiler: Recommended Option: Latest version of MCUXpresso IDE - available for Windows, Mac, and Linux Second Option: Download older version of MCUXpresso IDE for Windows from the DEFCON media server  Third Option: If you use the latest SDK, you can easily use ARM-GCC, IAR, or Keil tool chains as well.  MCUXpresso SDK: Recommend Option: Download latest SDK version for KL27 - includes setup for MCUXpresso IDE, ARM-GCC, IAR, and Keil compilers Other option: Download the older 2.4.2 SDK version on the DEFCON server which only has MCUXpresso IDE compiler support.  Badge Source: Recommended Option: Download zip off Joe Grand Website: http://www.grandideastudio.com/wp-content/uploads/dc27_bdg_source.zip  Other option: Download from DEFCON media server. However the .project and .cproject files do not show up by default, so you must make sure to explicitly download them as well and put them in the main firmware folder (at the same level as the .mex file). These are the exact same files as in the zip.  wget -r -np -R "index.html*" https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/ wget  https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/.cproject wget  https://media.defcon.org/DEF%20CON%2027/DEF%20CON%2027%20badge/Firmware/.project  Getting Started with MCUXpresso IDE:      1) Open up MCUXpresso IDE. When it asks for a workspace directory to use, select (or make) a new empty directory that is in a different location than where you          downloaded the firmware source.       2) Drag and drop the SDK .zip file from your file system into the MCUXpresso IDE "Installed SDKs" window. This is how the compiler learns about the KL27 device and the flash algorithms.  3) Drag and drop the badge firmware folder from a file explorer window into the MCUXpresso IDE "Project Explorer" window 4) In the Quickstart panel hit Build 5) In the Console tab, you should see the message that it compiled successfully 7) In the Quickstart panel hit Debug.  If you're not using a LPC Link2 for programming, you'll need to hold Shift when clicking this the first time so it'll rescan for your debugger.  If using the latest MCUXpresso IDE, you'll see a dialog box that the launch configuration needs to be updated. Click on "Yes".    7) A dialog box will come up confirming your debug probe. 😎 Connect the programming cable to the board and press to make a good connection. Make sure the alignment pins match up with the alignment holes on the PCB, and that pin 1 (the red stripe) matches the photo below. You may hear the badge beep, as it's being reset. 9) Then hit OK in the dialog box to start programming. Make sure to keep the probe held there until the programming is finished - about 5 seconds. 10) You should see it program successfully and hear the board beep as it reboots.  Programming Troubleshooting/Tips: If you're not using a LPC Link2, hold down the Shift key when you hit the Debug button, and it'll re-search for new probes. Also make sure your debug settings and probe is using SWD mode and not JTAG mode.  If you have the programming cable not lined up with the pads, you'll see this error. Re-align your probe and try again. Also you must have power from the battery as the MCU needs to be turned on while programming. You can hit the GUI flash programmer at the top for a quicker download experience since it won't load the debug view. Useful if just flashing the device without wanting to step through code.  Finally, some of the game state variables are stored in the non-volitale internal flash, and may not automatically get erased when reprogramming the firmware as the programmer doesn't realize that area of flash memory is being used and thus to save time, doesn't bother to erase it. You can force a complete erase of the flash to wipe all the game variables by setting the mass erase option. Double click on the dc27_badge LinkServer Debug.launch file which contains the debug settings, and go to GUI Flash Tool->Program and set Program (mass erase first).  Getting Started with ARM-GCC: To make this easier, you'll need to download the latest SDK from the NXP website first.  Follow the instructions in Section 6 of the MCUXpresso SDK User Guide for how to setup the environment and test it out on Hello World. You can then use that project for copying the badge source code into. I'm sure someone can put together a Makefile for the badge specifically. See this series of blog posts on how to use the SDK (compiling/debugging) with arm-gcc in Linux. My badge isn't working: First thing to try is power cycling the badge by gently prying the battery out (with a butter knife or something) and putting it back in. A couple of things might happen: If nothing at all happens, you battery might be dead. Try replacing the battery.  If nothing at all happens still, the battery holder might be loose. Use a multimeter ot measure the voltage between GND and VCC on the serial header, it should read 1.8V. If it does not, check the battery holder. If you hear beeps, all 6 LEDs light up, and then 4 LEDs (2 on each side) flash in sync a few times, it means there was an issue communicating with the NFMI device. This could be due to a loose solder joint on one of the chips or the I2C pull up resistors (SCL and SDA on the pinout image). You could also do a reflow if you have the equipment, but it may not be fixable. Also could see if see any I2C communication on those SCL/SDA pins. If you hear a normal startup beep, the lights flash, and then it goes back to the startup beep, and so on, forever, something is causing the MCU to keep resetting. Could be a short or ESD damage. Check soldering. Connecting your board to a serial terminal and see how far it gets in the boot process to help narrow down the cause.  Sometimes the flags don't get saved properly. A power cycle usually works, and could also try reflashing the badge.  If your badge isn't responding to other badges with the NFMI, it could be one of two things: Your copper antenna is loose/broken/missing. This happened a lot. Solder it back on. If missing, it's a Sunlord MTNF6040FS3R7JTFY01 but it's not available online anywhere at the moment. Datasheet is here. See this post for more details on possible alternatives. If you were previously in interactive mode, you have to explicitly exit it with Ctrl+X to receive packets again.  Further hacking: For basic hacking of the code, try changing your game flags to trick it to giving you a fully unlocked badge. From there, you could try to make your own chameleon badge like others have done (https://github.com/japd06/defcon27_badge and https://github.com/nkaminski/DC27-badge-CFW and https://github.com/NickEngmann/Jackp0t among others if you want ideas). Or make your own songs with the piezo. Or some ASCII art on the terminal. For more advanced hacking on the badge, PTE22 and PTE23, the TX and RX pins on the serial header, could be programmed to be ADC input pins instead. Or timer inputs or outputs for PWM or input capture.  And with some good soldering, you could even add an additional I2C device by soldering to the resistor points. t.   Finally if you want a more flexible platform for exploring embedded development, you can pick up a FRDM-KL27Z dev kit for $20 which has the same chip as the badge. You can buy it direct or all major distributors online. The programmer and serial interface are built into the board so you only need to use a USB cable to do all the programming. The KL27 SDK also includes dozens of example programs that show how to use all the features of the chip and there's some getting started videos (mostly what I covered already in this post though). While it does not have a NFMI chip on it, it does have USB support, as well as an Arduino hardware footprint on it so it can be easily expanded with extra boards. You can find the example programs by going to "Import SDK examples" from the Quickstart panel window.  If you have any more questions about the badge, post a response! 
記事全体を表示
    感谢Baolei之前在weekly meeting上分享的关于在Codewarrior环境下实现printf的重定向技巧,从而在CW调试环境下的Console上实现调试信息的打印功能,我将其移植到IAR环境下并进行了测试,可以实现调试信息的交互,完全可以替代串口的功能,在这里写出来分享给大家,再次感谢baolei的分享~     通过串口打印调试信息或者实现上下位机交互是我们最常使用的调试手段之一,毕竟实现起来无论是硬件成本(接出两根线Txd和Rxd,外加一个电平转换芯片)还是软件成本(下位机写好UART驱动,上位机直接超级终端或者一些第三方串口调试助手)都是相对较低的,所以这种方式还是灰常受广大“攻城师”们欢迎的。不过如果由于I/O资源紧缺串口被用做其他用处或者板子直接没有引出串口的话(是不是产生共鸣了,呵呵),那该怎么办呢?     当然,所谓时代不同了(liao)(顺口想说“男女都一样呢”,呵呵,哎,都是生在旧社会长在红旗下的孩子啊),随着嵌入式开发生态系统越来越完善,目前也是有越来越多的Poweful开发工具支持丰富的调试功能(支持打印调试信息和交互等),但是涉及到一些版权的问题价格上还是有点小贵的(对一些小企业来说还是难以接受的),所以这个时候就需要我们动动脑筋去摸索摸索其他的方法(所谓路是探索出来的),事实证明破釜沉舟下人的潜力是无限的,呵呵,这里就分享一个折衷的办法去解决大家一直苦恼的问题,即使用IAR虚拟的串口终端来实现信息的交互和打印,下面进入正题: 测试平台:IAR6.6 + FRDM KE02开发板(我目前手里有这个,其他平台都可以) 测试代码:KE驱动库(KEXX_DRIVERS_V1.0.1_DEVD\kexx_drv_lib_release_r1.0.1\build\iar\ke02\platinum) 这里稍微提一句,我测试的是KE驱动库的代码,但是实际上只要你看懂了我下面的解决方法(授之以渔而不是鱼),其他代码都是类似的。 1)打开KE02 platinum的IAR工程,进入到platinum.c文件,找到main函数如下图1,可以看到其调用了printf打印函数,而该工程是默认调用底层串口的,我们跳转到该函数的定义如图2,再继续跳转到out_char的函数定义如图3,这下就屡清楚了,我们可以很直观的看到工程默认是调用UART底层的,呵呵,下面我们就要动手改造它对printf进行重定向; 2)首先我们需要注释掉printf的实现函数,将其屏蔽掉,然后需要给printf一个重新指向的地址,下面就该我们常见的<stdio.h>这位老兄出场了(貌似当初自打我开始接触Turbo C的时候就已经用到它了,老生常谈的“Hello world”就是调用它内部的printf来实现的)。我们找到Common.h文件,将<stdio.h>添加到其中,如下图,这样凡是需要printf的文件只需要添加common.h头文件即可: 3)这里先说说stdio.h文件的作用,我们打开stdio.h文件可以看到其内部定义了标准输入输出函数,包括我们常见的scanf和printf等函数,而这些函数所调用的底层即为IAR提供的链接到其Terminal的驱动,所以……懂的,呵呵。除此之外,我们肯定不满足只输出打印(给人略显低端的感觉有木有),所以为了体现我们不是“土豪”,我觉着有必要让它交互起来,实现真正的串口功能(因为一些类似bootloader或shell之类的还是需要输入参数的进行交互的),我在main函数添加了scanf语句用来测试输入功能,如下: 4)准备工作就绪,编译链接整个工程,然后下载到KE02的板子中并进入到Debug调试环境中,点击View->Terminal I/O调出虚拟终端,然后全步运行,就可以看到Terminal下开始打印调试信息,如下图1。当然显示输出有点小case了,我们再试试输入功能,在input框中输入‘a’,然后回车,如下图2,perfect: 5)还没完,我们要玩就玩高端大气上点档次的,我们再探索探索呢,结果又发现个小惊喜,我们点击上图右下角的“Input Mode”,弹出设置框如下,很高端啊有木有: 呵呵,看完之后是不是有种跃跃欲试的兴奋呢,呵呵,just have a try and enjoy it~ 附件为我修改之后的工程代码,仅供参考~
記事全体を表示
Background: NXP SC18IS602B I2C bus to SPI bridge chip is using TSSOP16 package, which is 16 leads; 0.65 mm pitch; 5 mm x 4.4 mm x 1.1 mm body. Customer requires to use a smaller package to emulate the SC18IS602B function. Kinetis L series MKL03Z16VFK4R product uses QFN24 package with 4 mm x 4 mm x 0.58 mm body. Demo Overview The I2C to SPI Bridge demo provides a replacement solution demo of SC18IS602B chip. The demo is based on FRDM-KL03Z board using I2C0 module as I2C slave and SPI0 module as SPI master. Provided data buffer size is 400bytes. The demo software is based on KSDK V2.0 for FRDM-KL03Z software. I2C slave interface: Pin number                 Function              FRDM-KL03Z jumper PTB3                          I2C0_SCL           J2-10 PTB4                          I2C0_SDA           J2-9   SPI master interface: Pin number                 Function              FRDM-KL03Z jumper PTA5                           SPI0_SS             J2_3 PTA6                           SPI0_MISO         J2_5 PTA7                           SPI0_MOSI         J2_4 PTB0                           SPI0_SCK           J2_6   INT pin (indicates if I2C to SPI Bridge allows i2c master start a new i2c transfer, low is active) Pin number                 Function              FRDM-KL03Z jumper PTB11                        GPIO output         J2_2   Connect I2C master with FRDM-KL03Z I2C slave interface and connect SPI slave with FRDM-KL03Z SPI master interface; Connect FRDM-KL03Z GND to I2C master and SPI slave before add power to those boards.  Below is the hardware platform connection way: I2C to SPI Bridge Demo Function For the KL03 chip with one SPI0_PCS0 chip select pin, I2C to SPI Bridge demo only supports function ID 0x01 as SPI write command. For example: if i2c master want to write 8bytes (0x21,0x22...0x28) to SPI slave, the i2c master needs to send below data to FRDM-KL03Z board:   [START] + [I2C Slave address+/W] + [0x01](Function ID) + [0x21](data 1) + [0x22](data 2) + ... +[0x28](data 😎 + [STOP]     I2C to SPI bridge demo supports Function ID 0xF0 to configure SPI interface: There provides four SPI baud rate: 6Mbps/3Mbps/1.5Mbps/1Mbps. More detailed info, please check below picture (picture abstracted from SC18IS602B datasheet): For example: customer could configure SPI baud rate to 3Mbps with send below data to FRDM-KL03Z board:        [START] + [I2C Slave address+/W] + [0Xf0](Function ID) + [0x01](data 1) + [STOP] Hardware Platform The demo is based on FRDM-KL03Z board, using internal IRC48M clock as system and bus clock source. There doesn’t need external clock source. Toolchain supported - IAR embedded Workbench 7.60.1  (Tested) - Keil MDK 5.18a - GCC ARM Embedded 2015-4.9-q3 - Kinetis Development Studio IDE 3.2.0 Running the Demo Connect a USB cable between the host PC and the USB port on the target board. Open a serial terminal with the following settings:     - 9600 baud rate     - 8 data bits     - No parity     - One stop bit     - No flow control Download the program to the target board. I2C master start to configure SPI interface      I2C to SPI bridge board I2C address is 0x7E. I2C master write data to SPI slave    I2C master write 10bytes to SPI slave, it will send 11bytes (includes one function ID 0x01). The first data is 0xAA and the last data is 0x22.    After I2C to SPI Bridge receive the data, it will send 10bytes to SPI slave.        I2C to SPI Bridge receive 10 bytes     I2C to SPI Bridge send 10bytes to SPI slave I2C master read data from SPI slave    I2C master read 10bytes(0x10 to 0x19) from SPI slave need to write data to SPI slave at first, then read data from I2C to SPI bridge data buffer directly.    Here just shows read 10bytes from I2C to SPI bridge data buffer. Attached I2C to SPI Bridge demo software default location is: ..\SDK_2.0_FRDM-KL03Z\boards\frdmkl03z\user_apps\i2c_to_spi
記事全体を表示
Gracias a la excelente respuesta por parte de los concursantes, les informamos que daremos a conocer los proyectos finalistas el próximo martes 26 de Noviembre de 2013, a través de la comunidad Freescale y redes sociales; recibimos proyectos con gran potencial que aún están siendo evaluados por nuestros jueces. A continuación te compartimos los criterios a evaluar: • Alineación con las tendencias del futuro (Salud y Seguridad, Efecto Net,Going Green) • Creatividad • Innovación • Utilidad de la aplicación • Beneficio ambiental potencial para el uso del producto. Los finalistas seleccionados tendrán la oportunidad de presentar su prototipo en el evento Freescale Cup 2013 el día 7 de Diciembre de 2013 en el Tecnológico de Monterrey, Campus Guadalajara; donde el proyecto ganador será elegido por los asistentes al evento, a través de la comunidad Freescale y redes sociales. Recuerda que el ganador viajará con todos los gastos pagados al Freescale Technology Forum (FTF) en Dallas, Texas. Mantente atento el próximo martes 26 de Noviembre de 2013 y descubre los proyectos finalistas, tú puedes ser uno de ellos.
記事全体を表示
This demo is about driving TFT LCD by FlexBus module on MAPS-K22 board.       MAPS-K22 brief description: High performance Freescale ARM Cortex™ M4 SoC MK22FN512VLL12​ with 120MHz core clock, 512KB Flash and 128K RAM. Support Graphic LCD by Flexbus interface. Power supply from Micro USB 5V. Support ISO7816 smart card by UART interface. Support connector for Peripheral, Application and Socket MAPS board. SDK 1.0 Software release FlexBus Overview       The FlexBus module is a hardware module that: Provides memory expansion and provides connection to external peripherals with a parallel bus Can be directly connected to the following asynchronous or synchronous slave-only devices with little or no additional circuitry: External ROMs Flash memories Programmable logic devices Other simple target (slave) devices Block diagram Pin functions Pins allocation Demo illustration       After run the demo, the TFT LCD will display the Freescale logo as below, and I’ve also attached the demo. Welcome to download it.
記事全体を表示
Since the mbed Ethernet library and interface for FRDM-K64 have not yet been fully tested, instead of using mbed we will use one of the latest demo codes from MQX specifically developed for the FRDM-K64 platform. Before starting please make sure you have the following files and software installed in your computer: CodeWarrior 10.6 (professional or evaluation edition) MQX 4.1 for FRDM-K64 (it is not necessary to install full MQX 4.1) JLink_OpenSDA_V2.bin (this is the debugger application) * If you don't have a valid license, you can find a temporary license below, it will only be valid until 7/30/2014 and it will only be available online until 7/05/2014. Building the project The first step to use an MQX project is to compile the target/IDE libraries for the specific platform: 1. Open CodeWarrior and drag the file from the following path C:\Freescale\Freescale_MQX_4_1_FRDMK64F\build\frdmk64f\cw10gcc onto your project area: This will load all the necessary libraries to build the project, once they are loaded build them it is necessary to modify a couple of paths on the BSP: 2. Right click on the BSP project and then click on properties 3. Once the properties are displayed, expand the C/C++ Build option, click on settings, on the right pane expand the ARM Ltd Windows GCC Assembler and select the directories folder, this will display all the libraries paths the compiler is using 4. Double click on the "C\Freescale\CW MCU v10.6\MCU\ProcessorExpert\lib\Kinetis\pdd_100331\inc" path to modify it, once the editor window is open, change the path from "pdd_100331" to "pdd" 5. Repeat steps 2 and 3 for the ARM Ltd Windows GCC Compiler 6. Now you can build the libraries, build them one at a time by right clicking on the library and selecting build project, build them in the following order, it is imperative you do it in that order. BSP PSP MFS RTCS SHELL USBD USBH 7. Once all the libraries are built, import the web hvac demo, do it by dragging the .project file to your project area; the project is located in the following directory:                     C:\Freescale\Freescale_MQX_4_1_FRDMK64F\demo\web_hvac\build\cw10gcc\web_hvac_frdmk64f 8. Once the project is loaded, build it by right clicking on the project folder and select Build project Debugging the project To debug the project it is necessary to update the FRDM-K64 debugging application: Press the reset button on the board and connect the USB cable Once the board enumerates as "BOOTLOADER" copy the JLink_OpenSDA_vs.bin file to the unit Disconnect and reconnect the board On CodeWarrior (having previously compiled the libraries and project) click on debug configurations 5. Select the connection and click on debug 6. Open HVAC.h and change the IP Address to 192.168.1.202 Now the demo code has been downloaded to the platform you will need the following to access all the demo features: Router Ethernet Cable Serial Terminal The code enables a shell access through the serial terminal, it also provides web server access with a series of options to simulate an Heating Air Conditioning Ventilation System, the system was implemented using MQX and a series of tasks, for more details on how the task are created, the information regarding how to modify the code please check the attached document: Freescale MQX RTOS Example guide.
記事全体を表示
        IAR使用过程中有一点不太方便的是:当我们打开一个工程之后,如果再直接双击其他eww文件试图打开另外的工程,那么原来的工程就会被覆盖。解决这个问题的方法是:        1. 双击FileTypesMan.exe(该软件见附件,32位系统请解压filetypesman_x86.zip文件,64位系统请解压filetypesman_x64.zip文件)。打开该软件之后,找到.eww 格式并单击一下,显示界面如下图所示:             2. 双击open 所在行,对此条目进行更改,将Command-Line 中的内容:C:\PROGRA~2\IARSYS~1\EMBEDD~1.0\common\bin\IarIdePm.exe "%1" 先复制出来,Default Action 不选,Disable勾选,如下图所示:       3.在FileTypesMan界面的下方区域点击右键,选择New Action,如下图所示:            4.新建action 如下图所示,Action Name和Menu Caption 可随便命名,Command-Line 将上一步复制的内容粘贴过来即可。Default Action 勾选,Disable不选。          5. 最后配置如下图所示:       经过以上简单设置之后,就可以通过直接双击eww文件打开多个工程了。                  Original Attachment has been moved to: filetypesman_x64.zip Original Attachment has been moved to: filetypesman_x86.zip
記事全体を表示
Hi, all The default AN2295 UART bootloader doesn't work well on K21/other Kinetis because of using FEI and complicated autocalibration mechanism. I made a simple version to make it works on MK21DX128VMC5, FYI. Readm.txt: UART bootloader for K21. (Default is MK21DX128VMC5) 128KB_Pflash_64KB_Dflash.icf is application link script example for MK21DX128 used together with UART bootloader, UART bootloader use 0x0 - 0xFFF. Q: Why need this patch? A: The original AN2295 use internal RC and FLL output as system clock. The calibration mechanism is not stable. The main change of this patch is to use external cystal plus PLL as system clock to communicate with PC software. Changes to AN2295 1) Add MK21D5.h for K21 support 2) Add AN2295_TWR_K21_cfg.h for K21 support(Copy from AN2295_TWR_K60_cfg.h) 3) AN2295_TWR_K21_cfg.h    1> #define KINETIS_MODEL K21_50MHz    2> #define KINETIS_FLASH FLASH_128K    3> #define BOOT_UART_BASE UART2_BASE_PTR       #define BOOT_UART_GPIO_PORT PORTE_BASE_PTR       #define BOOT_UART_GPIO_PIN_RX   17       #define BOOT_UART_GPIO_PIN_TX   16    4> #define BOOT_PIN_ENABLE_NUM        7 4) Add mcg folder and mcg.c/mcg.h 5) kinetis_params.h:    1> Modify SRS_REG/SRS_POR_MASK/INIT_CLOCKS_TO_MODULES to meet MK21D5.h    2> Add PORT_PCR_PS_MASK for BOOTLOADER_PIN_ENABLE_INIT to enable Pull-up. 6) bootloader.h: #define BOOT_WAITING_TIMEOUT 500. PC software can't communicate to bootloader if only 1s delay. 7) bootloader.c:    1> #include "mcg.h"    2> Use 25MHz PEE:       SIM_CLKDIV1 = ( 0    | SIM_CLKDIV1_OUTDIV1(1)                            | SIM_CLKDIV1_OUTDIV2(1)                            | SIM_CLKDIV1_OUTDIV4(1));             (void)pll_init(8000000,       /* CLKIN0 frequency */                      LOW_POWER,     /* Set the oscillator for low power mode */                      CRYSTAL,       /* Crystal or canned oscillator clock input */                      4,             /* PLL predivider value */                      25,            /* PLL multiplier */                      MCGOUT);       /* Use the output from this PLL as the MCGOUT */    3> Restore to FEI mode before jump to Application:       pee_pbe(8000000);       pbe_fbe(8000000);       fbe_fei(32768); Knowing issues: 1) Don't use virtualCOM from OSJTAG, it's very hard to communicate with PC software. Use RS232 in TWR-SER2. 2) BOOTLOADER_CRC_ENABLE must be 0, otherwise PC software will report unknown protocol version
記事全体を表示
Test Environment: FRDM-KL43Z Rev. A MCUXpresso IDE v10.2.0 MCUXpresso SDK for FRDM-KL43Z V2.4.1(2018-06-18) Create new project in MCUXpresso IDE select [New project...], there will pop the SDK Wizard panel, then select [frdmkl43z]: Then, click [Next] will enter into [Configure the project] panel, we can set the [Project name] and select [flexio_i2s] in [driver]: Click [Finish], the new project was created. In general, the project is based on [hello_world] project with board default console available. In [Project Explorer], we could find the <fsl_flexio_i2s.c> & <fsl_flexio_i2s.h> & <fsl_flexio.c> & <fsl_flexio.h> files in drivers folder: Edit the code The application note AN5397 detailed introduce how FlexIO emulate I2S bus communication. The MCUXpresso SDK <flexio_i2s> driver using the AN5397 showed second solution to use two timers and two shifters. Please check here to get more detailed info. The I2S signal was below, we need to use four FlexIO pins to provide: BCLK, Fss, TxData & RxData. In <pin_mux.c> file, it need to config pin function, we use PTD7 pin provide I2S BCLK clock; PTD6 pin as I2S Frame_sync pin; PTD5 pin as Tx data pin; PTD6 pin as Rx data pin; In <frdmkl43z_flexio_i2s_interrupt_tx.c>,  config flexio_i2s and config the audio frame format: Please check attached source code for the detailed project info. Test result From the actual measured I2S signal, it shows the 8 bytes was sent out:
記事全体を表示
Download Kinetis M bare-metal drivers and software examples installation file. Changes in 4.1.6 : Modified FreeRTOS kernel to disable all interrupts prior entry to critical section and enable all interrupts upon exiting from critical section. This kernel behavior is compatible with standard FreeRTOS port to the ARM Cortex-M0 core. All freertos_cfg header files updated to reflect kernel change. Updated PLL_Disable macro and Quad Timer driver. Added UART_SetBaudRate macro. Removed RCM_ClrResetFlags macro. Fixed issue of generating callback events after conversion for these ADC channels with interrupt disabled.
記事全体を表示