Kinetis微控制器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Microcontrollers Knowledge Base

讨论

排序依据:
The NXP VID/PID program (Vendor ID and Product ID program) covers all MCUs and MPUs sold by NXP. The USB VID/PID Program enables NXP customers without USB-IF membership to obtain free USB Product IDs (PIDs) under the NXP Vendor ID (VID).   What is USB VID/PID Program? The NXP USB VID program will allow users to apply for the NXP VID and get up to 3 FREE PIDs. For more details, please create a support ticket and associated FAQ below.   Steps to apply for the NXP USB VID/PID Program Step 1: Create a support ticket with relevant details for instance company name, PIDs, purpose. Step 2: NXP will review the request and if approved, will issue you the PIDs. Note: The moment we receive a customer's request to the time they obtain a free VID/PID, there may be a delay of a month. FAQ for the USB VID/PID Program Can I use this VID for any microcontroller in the NXP portfolio? >> No. This program is intended only for the Cortex M based series of LPC Microcontrollers and Kinetis Microcontrollers, and Cortex A based series of i.MX Application Processors.   What are the benefits of using the NXP VID/PID Program? >> USB-IF membership not required >> Useful for low volume production runs that do not exceed 10,000 units >> Quick time to market   Can I use the NXP VID and issued PID/s for USB certification? >> You may submit a product using the NXP VID and issued PID/s for compliance testing to qualify to use the Certified USB logo in conjunction with the product, but you must provide written authorization to use the VID from NXP at the time of registration of your product for USB certification. Additionally, subject to prior approval by USB-IF, you can use the NXP VID and assigned PID/s for the purpose of verifying or enabling interoperability.   What are the drawbacks of using the NXP VID/PID program? >> Production run cannot exceed 10,000 units. See NXP VID application for more details. >> Up to 3 PIDs can be issued from NXP per customer. If more than 3 PIDs are needed, you have to get your own VID from usb.org: http://www.usb.org/developers/vendor/ >> The USB integrators list is only visible to people who are members of USB-IF. NXP has full control on selecting which products will be visible on the USB integrators list.   How do I get the VID if I don't use NXP’s VID? >> You can get your own VID from usb.org. Please visit http://www.usb.org/developers/vendor/   Do I also get the license to use the USB-IF’s trademarked and licensed logo if I use the NXP VID? >> No. No other privileges are provided other than those listed in the NXP legal agreement. If you wish to use USB-IF’s trademarked and licensed USB logo, please follow the below steps:                 1. The company must be a USB vendor (i.e. obtain a USB vendor ID).                 2. The company must execute the USB-IF Trademark License Agreement.                 3. The product bearing the logo must successfully pass USB-IF Compliance Testing and appear on the Integrators List under that company’s name.   Can I submit my product for compliance testing using the NXP VID and assigned PIDs? >> Yes, you would be able to submit your products for USB-IF certification by using the NXP VID and assigned PID. However, if the product passes the compliance test and gets certified, it will be listed under “NXP Semiconductors” in the Integrators list. Also, you will not have access to use any of the USB-IF trademarked and licensed USB logos. How long does it take to obtain the PID from NXP? >> It can take up to 4 weeks to get the PIDs from NXP once the application is submitted.   Are there any restrictions on the types of devices that can be developed using the NXP issued PIDs? >> This service requireds the USB microcontroller to be NXP products.   Can I choose/request for a specific PID for my application? >> No. NXP will not be able to accommodate such requests.
查看全文
Introduction With the growth of the Internet of Things (IoT), more and more applications are incorporating the use of sensors while also requiring power efficiency and increased performance.  A popular interface for these sensors is the I2C protocol. The I2C bus is a great protocol that is a true multi-master protocol and allows for each bus to contain many devices.  As the performance demand of the application grows, so will the speed of the I2C bus as it will be necessary to get more data from the sensors and/or at a faster rate.  Many applications may already have a need to operate an I2C bus at 400 kHz or more.  Higher data rates means the MCU core will need to spend more time servicing the I2C transactions.  The DMA module is one good way to free up the core in order to let it tend to other aspects of the application.  This can add much needed or much desired performance to applications.  Especially applications that may be using small, power efficient, single core MCUs. It may seem like an easy, straight-forward task to add I2C reads from a sensor to an application.  However I2C is a time sensitive protocol and consequently, so is the I2C peripherals on MCUs.  It is important to understand the time requirements and how to overcome them. The recommended approach is to use DMA to transfer the received I2C data to the desired buffer in your application software.  This document is going to outline how to setup your DMA and provide an example of how to do this for a KW40 device using the Kinetis SDK version 1.3.  The KW40 is being targeted because this is a small, power efficient MCU that incorporates a radio for your wireless applications and as such, it is likely that your application could need this DMA approach.  The KSDK version 1.3 is being targeted because this version of the SDK does not currently support DMA transactions for the I2C peripheral. Understanding the Kinetis I2C peripheral module Before getting into the specifics of creating a DMA enabled I2C driver, it is important to understand some basics of the Kinetis I2C peripheral module.  This module handles a lot of the low-level timing.  However the I2C registers must be serviced in a timely manner to operate correctly.  Take the case of a master reading data from a typical I2C sensor as shown in the diagram below. In the diagram above, the red lines indicate points in the transaction where software or DMA needs to interact with the I2C peripheral to ensure the transaction happens correctly.  To begin a transaction the core must change the MST bit which puts a start bit on the bus (marked by symbol ST).  Immediately following this, the core should then also write the target slave's address (Device Address) including the read/write bit (R/W).  Once this transaction is complete, the I2C will issue an interrupt and then the core should write the register address to be read from. Upon completion of that being put on the bus, the I2C will issue another interrupt and the master should then put a repeated start (SR) on the bus as well as the slave's address again.  Now the slave will send data to the master (once the master begins the transaction by issuing a dummy read of the I2C data register).  In the standard configuration, the I2C peripheral will automatically send the NAK or AK depending on the configuration of the TXAK bit in the I2C peripheral.  Because of this automation, it is important that this bit be handled properly and is configured one frame in advance. Furthermore, to ensure that the NAK bit is sent at the appropriate time, the TXAK bit must be set when the second to last byte is received.  The timing of this configuration change is very important to ensuring that the transaction happens properly. This document will describe how to use DMA to receive the data.  The DMA will be configured before the transaction begins and will be used to receive the data from the slave.  The document will also discuss options to handle proper NAK'ing of the data to end the transaction. Writing a DMA I2C master receive function The first step in adding DMA capability to your SDK driver is to create a new receive function with an appropriate name.  For this example, the newly created receive function is named I2C_DRV_MasterReceiveDataDMA.  To create this function, the I2C_DRV_MasterReceive function (which is called for both blocking and non-blocking) was copied and then modified by removing the blocking capability of the function. Then in this function, after the dummy read of the IIC data register that triggers the reception of data, the DMA enable bit of the I2C control register is written. /*FUNCTION********************************************************************** * * Function Name : I2C_DRV_MasterReceiveDataDMA * Description   : Performs a non-blocking receive transaction on the I2C bus *                 utilizing DMA to receive the data. * *END**************************************************************************/ i2c_status_t I2C_DRV_MasterReceiveDataDMA(uint32_t instance,                                                const i2c_device_t * device,                                                const uint8_t * cmdBuff,                                                uint32_t cmdSize,                                                uint8_t * rxBuff,                                                uint32_t rxSize,                                                uint32_t timeout_ms) {     assert(instance < I2C_INSTANCE_COUNT);     assert(rxBuff);       I2C_Type * base = g_i2cBase[instance];     i2c_master_state_t * master = (i2c_master_state_t *)g_i2cStatePtr[instance];             /* Return if current instance is used */     OSA_EnterCritical(kCriticalDisableInt);         if (!master->i2cIdle)     {         OSA_ExitCritical(kCriticalDisableInt);         return kStatus_I2C_Busy;     }         master->rxBuff = rxBuff;     master->rxSize = rxSize;     master->txBuff = NULL;     master->txSize = 0;     master->status = kStatus_I2C_Success;     master->i2cIdle = false;     master->isBlocking = true;     OSA_ExitCritical(kCriticalDisableInt);             while(I2C_HAL_GetStatusFlag(base, kI2CBusBusy));     I2C_DRV_MasterSetBaudRate(instance, device);         /* Set direction to send for sending of address. */     I2C_HAL_SetDirMode(base, kI2CSend);       /* Enable i2c interrupt.*/     I2C_HAL_ClearInt(base);     I2C_HAL_SetIntCmd(base, true);       /* Generate start signal. */     I2C_HAL_SendStart(base);       /* Send out slave address. */     I2C_DRV_SendAddress(instance, device, cmdBuff, cmdSize, kI2CReceive, timeout_ms);       /* Start to receive data. */     if (master->status == kStatus_I2C_Success)     {         /* Change direction to receive. */         I2C_HAL_SetDirMode(base, kI2CReceive);                 /* Send NAK if only one byte to read. */         if (rxSize == 0x1U)         {         I2C_HAL_SendNak(base);         }         else         {         I2C_HAL_SendAck(base);         }                 /* Dummy read to trigger receive of next byte in interrupt. */         I2C_HAL_ReadByte(base);                 /* Now set the DMA bit to let the DMA take over the reception. */         I2C_C1_REG(I2C1) |= I2C_C1_DMAEN_MASK;                 /* Don't wait for the transfer to finish. Exit immediately*/     }     else if (master->status == kStatus_I2C_Timeout)     {         /* Disable interrupt. */         I2C_HAL_SetIntCmd(base, false);                 if (I2C_HAL_GetStatusFlag(base, kI2CBusBusy))         {         /* Generate stop signal. */         I2C_HAL_SendStop(base);         }                 /* Indicate I2C bus is idle. */         master->i2cIdle = true;     }         return master->status; } After writing the DMA driver, a DMA specific transfer complete function must be implemented. This is needed in order for the application software to signal to the driver structures that the transfer has been completed and the bus is now idle. In addition, the DMA enable bit needs to be cleared in order for other driver functions to be able to properly use the IIC peripheral. void I2C_DRV_CompleteTransferDMA(uint32_t instance) {     assert(instance < I2C_INSTANCE_COUNT);     I2C_Type * base = g_i2cBase[instance];     i2c_master_state_t * master = (i2c_master_state_t *)g_i2cStatePtr[instance];         I2C_C1_REG(base) &= ~(I2C_C1_DMAEN_MASK | I2C_C1_TX_MASK);     I2C_C1_REG(base) &= ~I2C_C1_MST_MASK;;        /* Indicate I2C bus is idle. */     master->i2cIdle = true; } DMA Configuration Next, the application layer needs a function to configure the DMA properly, and a DMA callback is needed to properly service the DMA interrupt that will be used as well as post a semaphore. But before diving into the specifics of that, it is important to discuss the overall strategy of using the DMA in this particular application. After every transaction, the data register must be serviced to ensure that all of the necessary data is received.  One DMA channel can easily be assigned to service this activity.  After the reception of the second to last data byte, the TXAK bit must be written with a '1' to ensure that the NAK is put on the bus at the appropriate time. This is a little trickier to do.  There are three options: A second dedicated DMA channel can be linked to write the I2C_C1 register every time the I2C_D register is serviced.  This option will require a second array to hold the appropriate values to be written to the I2C_C1 register.  The following figure illustrates this process. The second DMA channel can be linked to write the I2C_C1 register after the second to last data byte has been received.  This option would require that the primary DMA channel be set to receive two data bytes less than the total number of desired data bytes.  The primary DMA channel would also need to be re-configured to receive the last two bytes (or the application software would need to handle this).  However this could be a desirable programming path for applications that are memory constrained as it reduces the amount of memory necessary for your application. The primary DMA channel can be set to receive two data bytes less than the total number of desired data bytes and the core (application software) can handle the reception of the last two bytes.  This would be a desirable option for those looking for a simpler solution but has the drawback that in a system where the core is already handling many other tasks, there may still be issues with writing the TXAK bit on time. This example will focus on option number 1, as this is the simplest, fully automatic solution.  It could also easily be modified to fit the second option as the programmer would simply need to change the number of bytes to receive by the primary DMA and add some reconfiguration information in the interrupt to service the primary DMA channel. DMA Channel #1 The first DMA channel is configured to perform 8-bit  transfers from the I2C data register (I2C_D) to the buffer to hold the desired data.  This channel should transfer the number of desired bytes minus one.  The final byte will be received by the core.  Other DMA configuration bits that are important to set are the cycle steal bit, disable request bit, peripheral request bit (ERQ), interrupt on completion of transfer (EINT), and destination increment (DINC).  It also important to configure the link channel control to perform a link to channel LCH1 after each cycle-steal transfer and LCH1 should be configured for the channel that will transfer from memory to the I2C control register (I2C_C1).  The first DMA channel is configured as shown below. // Set Source Address (this is the UART0_D register       DMA_SAR0 = (uint32_t)&I2C_D_REG(base);             // Set BCR to know how many bytes to transfer       // Need to set to desired size minus 1 because the last will be manually       // read.        DMA_DSR_BCR0 = DMA_DSR_BCR_BCR(destArraySize - 1);             // Clear Source size and Destination size fields.        DMA_DCR0 &= ~(DMA_DCR_SSIZE_MASK                     | DMA_DCR_DSIZE_MASK                     );       // Set DMA as follows:       //     Source size is byte size       //     Destination size is byte size       //     D_REQ cleared automatically by hardware       //     Destination address will be incremented after each transfer       //     Cycle Steal mode       //     External Requests are enabled       //     Interrupts are enabled       //     Asynchronous DMA requests are enabled.       //     Linking to channel LCH1 after each cycle steal transfer       //     Set LCH1 to DMA CH 1.        DMA_DCR0 |= (DMA_DCR_SSIZE(1)             // 1 = 8-bit transfers                    | DMA_DCR_DSIZE(1)           // 1 = 8-bit transfers                    | DMA_DCR_D_REQ_MASK                    | DMA_DCR_DINC_MASK                    | DMA_DCR_CS_MASK                    | DMA_DCR_ERQ_MASK                    | DMA_DCR_EINT_MASK                    | DMA_DCR_EADREQ_MASK                    | DMA_DCR_LINKCC(2)          // Link to LCH1 after each cycle-steal transfer                    | DMA_DCR_LCH1(1)            // Link to DMA CH1                    );       // Set destination address       DMA_DAR0 = (uint32_t)destArray; DMA Channel #2 The second DMA channel, which is the linked channel, should be configured to perform 8-bit transfers that transfer data from an array in memory (titled ack_nak_array in this example) to the I2C control register (I2C_C1).  This channel should also disables requests upon completion of the entire transfer, and enable the cycle-steal mode.  In this channel, the source should be incremented (as opposed to the destination as in the first channel). This channel is configured as shown below: // Set Source Address (this is the UART0_D register       DMA_SAR1 = (uint32_t)ack_nak_array;             // Set BCR to know how many bytes to transfer       // Need to set to desired size minus 1 because the last will be manually       // read.       DMA_DSR_BCR1 = DMA_DSR_BCR_BCR(destArraySize - 1);             // Clear Source size and Destination size fields.        DMA_DCR1 &= ~(DMA_DCR_SSIZE_MASK                     | DMA_DCR_DSIZE_MASK                     );             // Set DMA as follows:       //     Source size is byte size       //     Destination size is byte size       //     D_REQ cleared automatically by hardware       //     Destination address will be incremented after each transfer       //     Cycle Steal mode       //     External Requests are disabled       //     Asynchronous DMA requests are enabled.       DMA_DCR1 |= (DMA_DCR_SSIZE(1)             // 1 = 8-bit transfers                    | DMA_DCR_DSIZE(1)           // 1 = 8-bit transfers                    | DMA_DCR_D_REQ_MASK                    | DMA_DCR_SINC_MASK                    | DMA_DCR_CS_MASK                    | DMA_DCR_EADREQ_MASK                    );             // Set destination address       DMA_DAR1 = (uint32_t)&I2C_C1_REG(base); Once the DMA channels are initialized, the only action left is to configure the interrupts, enable the channel in the DMA MUX, and create the semaphore if it has not already been created.  This is done as shown below. //Need to enable the DMA IRQ       NVIC_EnableIRQ(DMA0_IRQn);       //////////////////////////////////////////////////////////////////////////       // MUX configuration       // Enables the DMA channel and select the DMA Channel Source        DMAMUX0_CHCFG0 = DMAMUX_CHCFG_SOURCE(BOARD_I2C_DMAMUX_CHN); //DMAMUX_CHCFG_ENBL_MASK|DMAMUX_CHCFG_SOURCE(0x31); //0xb1;       DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK;             /* Create semaphore */       if(semDmaReady == NULL){         semDmaReady = OSA_EXT_SemaphoreCreate(0);       } Finally, the DMA initialization function also initializes the ack_nak_array.  This is only necessary when implementing the first DMA strategy.  The second DMA strategy would only need to write a single value at the correct time.  The array initialization for strategy #1 is shown below.  Note that the values written to the array are 0xA1 plus the appropriate value of the TXAK bit.  By writing 0xA1, it is ensured that the I2C module will be enabled in master mode with the DMA enable bit set. // Initialize Ack/Nak array       // Need to initialize the Ack/Nak buffer first       for( j=0; j < destArraySize; j++)       {           if(j >= (destArraySize - 2))           {               ack_nak_array[j] = 0xA1 | I2C_C1_TXAK_MASK;           }           else           {               ack_nak_array[j] = 0xA1 & (~I2C_C1_TXAK_MASK);           }       } DMA Interrupt Handler Now a DMA interrupt handler is required.  A minimum of overhead will be required for this example as the interrupt handler simply needs to service the DONE bit and post the semaphore created in the initialization.  The DMA interrupt handler is as follows: void DMA0_IRQHandler(void) {     // Clear pending errors or the done bit     if (((DMA_DSR_BCR0 & DMA_DSR_BCR_DONE_MASK) == DMA_DSR_BCR_DONE_MASK)         | ((DMA_DSR_BCR0 & DMA_DSR_BCR_BES_MASK) == DMA_DSR_BCR_BES_MASK)         | ((DMA_DSR_BCR0 & DMA_DSR_BCR_BED_MASK) == DMA_DSR_BCR_BED_MASK)         | ((DMA_DSR_BCR0 & DMA_DSR_BCR_CE_MASK) == DMA_DSR_BCR_CE_MASK))     {         // Clear the Done MASK and set semaphore, dmaDone         DMA_DSR_BCR0 |= DMA_DSR_BCR_DONE_MASK;         //dmaDone = 1;         OSA_SemaphorePost(semDmaReady);     } } Using your newly written driver function Once all of these items have been taken care of, it is now time for the application to use the functions. It is expected that the DMA will be initialized before calling the DMA receive function.  After the first call, the DMA can be re-initialized every time or could simply be reset with the start address of the arrays and byte counter (this is the minimum of actions that must be performed).  Then the application should ensure that the transaction happened successfully.   Upon a successful call to the I2C_DRV_MasterReceiveDataDMA function, the application should wait for the semaphore to be posted.  Once the semaphore posts, the application software should wait for the Transfer Complete flag to become set.  This ensures that the application does not try to put a STOP signal on the bus before the NAK has been physically put on the bus.  If the STOP signal is attempted out of sequence, the I2C module could be put in an erroneous state and the STOP signal may not be sent.  Next, the I2C_DRV_CompleteTransferDMA function should be called to send the STOP signal and to signal to the driver structures that the bus is idle.  At this point, the I2C transaction is now fully complete and there is still one data byte that hasn't been transferred to the receive buffer.  It is the application's responsibility to perform one last read of the Data register to receive the last data byte of the transaction. /* Now initialize the DMA */    dma_init(BOARD_I2C_INSTANCE, Buffer, ack_nak_buffer, FXOS8700CQ_READ_LEN); //Init DMAMUX       returnValue = I2C_DRV_MasterReceiveDataDMA(BOARD_I2C_INSTANCE, &slave,                                                   cmdBuff, 1, Buffer, FXOS8700CQ_READ_LEN, 1000); if (returnValue != kStatus_I2C_Success)    {        return (kStatus_I2C_Fail);    } /* Wait for the DMA transaction to complete */    OSA_SemaphoreWait(semDmaReady, OSA_WAIT_FOREVER);       /* Need to wait for the transfer to complete */ for(temp=0; temp<250; temp++)     {         if(I2C_HAL_GetStatusFlag(base, kI2CTransferComplete))         {             break;         }     }       /* Now complete the transfer; this includes sending the I2C STOP signal and       clearing the DMA enable bit */    I2C_DRV_CompleteTransferDMA(BOARD_I2C_INSTANCE);       // Once the Transfer is complete, there is still one byte sitting in the Data    // register.      Buffer[11] = I2C_D_REG(g_i2cBase[BOARD_I2C_INSTANCE]); Conclusion To summarize, as consumers demand more and more power efficient technology with more and more functionality, MCU product developers need to cram more functionality in small power efficient MCUs.  Relying on DMA for basic data transfers is one good way to improve performance of smaller power efficient MCUs with a single core. This can be particularly useful in applications where an MCU needs to pull information from and I2C sensor.  To do this, there are three methods of implementing an I2C master receive function in your SDK 1.3 based application. Use two DMA channels.  The first to transfer from the I2C Data register to the destination array.  A second dedicated DMA channel can be linked to write the I2C_C1 register every time the I2C_D register is serviced. Use two DMA channels.  The first to transfer from the I2C Data register to the destination array. The second DMA channel can be linked to write the I2C_C1 register only after the second to last data byte has been received. Use a single DMA channel can be set to receive two data bytes less than the total number of desired data bytes and the core (application software) can handle the reception of the last two bytes. The recommendation of this document is to implement the first or second option as these are fully automatic options requiring the least intervention by the core.
查看全文
在KE系列MCU中提供了多种寄存器用于实现GPIO的控制:    -PDOR寄存器,用于写入或读取IO的输出状态    -PSOR寄存器,用于置位IO口    -PCOR寄存器,用于清零IO口    -PTOR寄存器,用于翻转IO口    -PDIR寄存器,用于读取IO口的输入状态 当我们想要将PTA0置1时,有多种方法可以选择:    1. 直接操作寄存器,PDOR或PSOR都可以实现:          GPIOA->PDOR |= 0x0001;          GPIOA->PSOR |= 0x0001;          直接操作寄存器的效率更高,但可读性较差。    2. 使用官方的库函数操作       GPIO_PinSet(GPIOA, GPIO_PTA0);       库函数的可读性很好,但显得有些啰嗦,字符较多。 通过KE的BME来实现GPIO的操作能够很好的解决上面的问题,只用将附件中的头文件gpio_bitdef.h包含到工程里,再调用里边的宏定义就可以了。 对PTA0置位和清零可以使用下面的语句: POUTA0 = -1; POUTA0 = 0; 读取PTA0的输入状态则可以使用: tmp = PINA0; 上面的语句是不是看上去简洁了很多呢。 实际上上面GPIO的读写指令,是通过BME的BFI(位域插入)和BFX(位域提取)指令来实现的。 -其中ADDR是存储空间内的地址,我们最终操作的还是GPIO的寄存器,因此在两个指令中分别取GPIOA的PDOR寄存器地址和PDIR寄存器地址。 -bit则表示需要插入或提取位域的起始位置,由于这里是PTA0,PTA0位于寄存器的最低位,因此这里填入了0。 -width则表示需要插入或提取位域的宽度,我们只对单个管脚进行操作,也就是单个位进行操作,宽度自然就是1了。 需要注意的是,BFI(位域插入)指令在插入时,是将对应位插入到目的地址。因此,如果直接为POUTxx赋值为1的话,有可能出现错误。 POUTA0 = 0x01;//正确 POUTA1 = 0x02;//正确 POUTA2 = 0x04;//正确 POUTA1 = 0x01;//错误 为了避免这种情况,我们可以在IO口需要置位时,直接将POUTxx赋值为-1,即0xFFFF FFFF,这样保证了每一位的值都为1。 #define BME_BFI(ADDR,bit,width)        (*(volatile uint32_t *)((((uint32_t)ADDR&0xFFFF))   \                                   | (5 <<28)  \                                   | ((bit)<<23) | ((width-1))<<19)) #define BME_BFX(ADDR,bit,width)        (*(volatile uint32_t *)(((uint32_t)ADDR&0xFFFF)    \                                   | (5 <<28)  \                                   | ((bit)<<23) | ((width-1))<<19))  #define POUTA0 BME_BFI(&GPIOA->PDOR,0,1) #define PINA0 BME_BFX(&GPIOA->PDIR,0,1) ‍‍‍‍‍‍‍‍‍‍
查看全文
Hi: Kinetis's ADC have no multi channels sequence sampling function, compared with LPC's ADC. But we could use DMA for such case, attached are two demos: 1.multi_channels_edma_ADC_DMA_SW_TRIG Description: use SW trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; 2.multi_channels_edma_ADC_DMA_LPIT_HW_TRIG Description: use LPIT timely trigger DMA transfer for 6 ADC channels, DMA ch0 is for ADC channels transfer, DMA ch1 is for ADC sample result transfer in DMA ch1 ISR, report ADC sample are done; but LPIT could trigger continuously without SW engage.
查看全文
The following document contains a list of documents , questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in Kinetis processors or MCUXpresso, you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table FAQ: MCUXpresso Software and Tools  Getting Started with MCUXpresso and FRDM-K64F  Generating a downloadable MCUXpresso SDK v.2 package  Quick Start Guide – Using MCUXpresso SDK with PINs&amp;CLOCKs Config Tools  Moving to MCUXpresso IDE from Kinetis Design Studio Kinetis Microcontrollers Guides and examples Using RTC module on FRDM-KL25Z  Baremetal code examples using FRDM-K64F Using IAR EWARM to program flash configuration field Understanding FlexIO  Kinetis K80 FAQ How To: Secure e-mail client (SMTP + SSL) with KSDK1.3 + WolfSSL for FRDM-K64F  Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+  PIT- ADC- DMA Example for FRDM-KL25z, FRDM-K64F, TWR-K60D100 and TWR-K70  USB tethering host (RNDIS protocol) implementation for Kinetis - How to use your cellphone to provide internet connectivity for your Freedom Board using KSDK Write / read the internal flash Tracking down Hard Faults  How to create chain of pbuf's to be sent? Send data using UDP.  Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading  USB VID/PID numbers for small manufacturers and such like  Open SDA and FreeMaster OpenSDAv2  Freedom OpenSDA Firmware Issues Reported on Windows 10 Let´s start with FreeMASTER!  The Kinetis Design Studio IDE (KDS IDE) is no longer being actively developed and is not recommended for new designs. The MCUXpresso IDE has now replaced the Kinetis Design Studio IDE as the recommended software development toolchain for NXP’s Kinetis, LPC and i.MX RT Cortex-M based devices. However, this documents continue to receive considerable amount of views in 2019 which means it could be useful to some people. Kinetis Design Studio New Kinetis Design Studio v3.2.0 available Using Kinetis Design Studio v3.x with Kinetis SDK v2.0  GDB Debugging with Kinetis Design Studio  KDS Debug Configurations (OpenOCD, P&amp;E, Segger) How to use printf() to print string to Console and UART in KDS2.0  Kinetis Design Studio - enabling C++ in KSDK projects  Using MK20DX256xxx7 with KDS and KSDK  Kinetis SDK Kinetis SDK FAQ  Introducing Kinetis SDK v2  How to: install KSDK 2.0  Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt 
查看全文
The 5V Kinetis E series MCUs are designed to maintain high robustness for complex electrical noise environments and high-reliability applications. Kinetis EA series MCUs using the same architecture with automotive level operation temperature range, are various used for auto body electrical application. There was a reality customer requirement to let KEA core running the application (light a LED) within 20ms from power up. It need to know the whole startup processing for KE/KEA product. Please check below picture to get more info about boot sequence: During the power up phase, after VDD rising to VPOR voltage threshold, there with about 15us delay before internal IRC start oscillating. T2 interval is FLL acquisition time to make FLL generating clock. The Reset_b pin is released and then the system is released from reset. After that, the NVM starts internal initialization. Flash Controller is released from reset and begins initialization operations while the core is still halted before the flash initialization completes. When the flash Initialization completes (16 μs) , the core sets up the stack, program counter (PC), and link register (LR). The processor reads the start SP (SP_main) from vector-table offset 0. The core reads the start PC from vector-table offset 4. LR is set to 0xFFFF_FFFF. The CPU begin to execute the first instruction. Overview the whole power up processing, FLL acquisition time is the longest time interval almost 1ms, then following power up time about 0.1ms (using 17KV/sec VDD ramp-up slew rate). There seems a lot of time left to run the chip initialization code and application code. Customer requirement (power up to light a led within 20ms) should be matched without any problem. While, during customer test, there seems it need to take more than 30ms to find the LED be lighten after power up. In order to check the issue, we get the customer test code and find there with below clock initialization code: void Clk_Init() {                 ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/                 ICS_C3= 0x90;                                    /* Reference clock frequency = 31.25 KHz*/                       while(!(ICS_S & ICS_S_LOCK_MASK));  /* Wait for FLL lock, now running at 40 MHz (1280 * 31.25Khz) */                                               ICS_C2|=ICS_C2_BDIV(1)  ;                    /*BDIV=2, Bus clock = 20 MHz*/                 ICS_S |= ICS_S_LOCK_MASK ;              /* Clear Loss of lock sticky bit */      } We do a test to check the Clk_init() function execution time and find it will take almost 25ms. We toggle a GPIO pin and almost 25ms for checking ICS status register [LOCK] be asserted. KE/KEA product using ICS module as clock source, which default mode is FEI. In general, during the chip initialization, using ICS status register [LOCK] bit to check if the FLL cock is stable or not. From KE/KEA product datasheet, the Max. FLL acquisition time is 2ms. Why the ICS_S[LOCK] bit be asserted need take more than 25ms? After double check with ICS IP owner, we get below info: The FLL_S[LOCK] bit act as “LOCK detection”, the LOCK bit will be set if FLL clock frequency stays within the tolerance 6% for 20ms~30ms. After acquisition time (max. 2ms) FLL achieved clock accuracy as same as LOCK bit be asserted. After ICS configuration modified, customer can call a 2ms delay routine to make sure FLL acquisition clock successfully before executing the application code. 
查看全文
Latest version of the AN2295 universal bootloader includes support for IAR 7.6 IDE. - added support for Kinetis E MCUs - Kinetis K,L,M,E,W,V support
查看全文
This is an example for the Kinetis KE02Z devices, showing how to program the EEPROM with initial values when the flash is programmed.  The example works on the FRDM-KE02Z40M board, and was written with Kinetis Design Studio (KDS) v3.0.0.  The example also uses Processor Expert (PEx) to configure the UART and erase/program the EEPROM.  The EEPROM programming works with the P&E Micro Multilink Universal debugger, as well as the P&E Micro OpenSDA debugger app for the FRDM-KE02Z40M board. To program the EEPROM with initial values, the application declares constants for the EEPROM locations, and initializes these in the source code in eeprom.c. Compiler pragmas/attributes are used to force the linker to place these constants in EEPROM, using the m_eeprom memory section defined in the linker command file \Project_Settings\Linker_Files\ProcessorExpert.ld.  The P&E Micro flash programming algorithms initialize the EEPROM in 4Byte words. Therefore, any initialized EEPROM locations should be in aligned 4Byte words. This example initializes the first 4Bytes in the EEPROM as 0, 64, 128, 192. The example uses a terminal program to display EEPROM information.  It connects to the OpenSDA COM port on the FRDM-KE02Z40M board using UART1 from the KE02Z. The terminal settings are:   Baud Rate: 38,400   Data: 8bit   Parity: None   Stop: 1bit   Flow Control: None The example prints 5 bytes of EEPROM to the terminal after reset: the 4 initialized bytes, plus the following EEPROM byte which was not initialized. Then the example increments the first byte, and decrements the second byte, and writes the new values back to EEPROM.  The other 3 bytes are not changed. Then the application prints the new EEPROM values of all 5 bytes.  Everytime the MCU is reset, it will print the existing EEPROM data and then the changed data.  Below is the example output from the terminal after initially programming the KE02Z, and then doing a single reset: Terminal output:   KE02Z EEPROM example   EEPROM values after reset = 0 64 128 192 255   EEPROM values after updating = 1 63 128 192 255   KE02Z EEPROM example   EEPROM values after reset = 1 63 128 192 255   EEPROM values after updating = 2 62 128 192 255
查看全文
This is an update to the KE0x Driver Library package with the example projects ported to Kinetis Design Studio (KDS).  These examples support the following boards: FRDM-KE02 FRDM-KE04 FRDM-KE06 The examples were tested with KDS v3.0.0
查看全文
1.jicheng0622-AET-电子技术应用 2.wuyage-AET-电子技术应用 3.fanxi123-AET-电子技术应用
查看全文
      In the practical KE KEA usage, a lot of customers meet the watchdog can’t reset problems. Some customers find when they want to enable the watchdog, but can’t really enable the watchdog by set the EN bit in register WDOG_CS1; Some customers find when in debug mode, the EN bit WDOG_S1 register always be clear, but from the reference manual, this bit should be set after reset, even they check their code, and make sure they didn’t disable the watchdog;  There also have some customers find when they use the KEXX_DRIVERS_V1.2.1_DEVD code, and set the timeout value register by themselves, but the watchdog can’t reset in the timeout value. Now according to these problems, this document will analyze it and give the recommendation to avoid these problems.      From the above problem description, we can get that there actually mainly 2 reasons caused these problems: 1, software configuration; 2, debugger usage 1.  Software configuration   1) Start code disable the watchdog In the KE KEA sample code, after reset, the chip will enter in the start code at first, the start code always disable the watchdog at first, if the watchdog is disabled, the watchdog can’t be enable just by set the EN bit in register WDOG_CS1, because bit EN in register WDOG_CS1 is the write-once bit after reset. It only can be modified when the UPDATE bit is set and with 128 bus clocks after performing the unlock write sequence. Now how to find the disable code in the start code? Take KEXX_DRIVERS_V1.2.1_DEVD sample code as an example IAR: from crt0.s, will find the watchdog disable code WDOG_DisableWDOGEnableUpdate();  in the start function. The above IAR start picture is for KE, but in the KEA start file, you can’t see the start function in the KEA sample code which download from the freescale web, just find the __iar_program_start in cstartup_M_KEA128.s after the reset happens, but where is the __iar_program_start function, it can’t be searched in the whole project. Actually __iar_program_start is the default program entry function, it include the following function: You can find it will enter __low_level_init function, the watchdog disable code is just in  __low_level_init function. MDK:  From startup_MK0XZ4.s will find the watchdog disable code in the SystemInit function. Codewarrior: From __arm_start.c file, will find the watchdog disable code in __init_hardware function. 2) Codewarrior script init_kinetis.tcl disable the watchdog      To the Codewarrior, just comment the disable watchdog code in the __arm_start.c file is not enough to check the watchdog enable after reset, because in the codewarrior connect script init_kinetis.tcl, there also have the watchdog disable code.      If you want to find the state of EN bit in register WDOG_S1 after reset, you must disable all these watchdog disable code.   3) Timeout register configuration incorrect From the header file MKE02Z2.h, we can find the time out register define like this:   union {                                          /* offset: 0x4 */     __IO uint16_t TOVAL;                             /**< WDOG_TOVAL register., offset: 0x4 */     struct {                                         /* offset: 0x4 */       __IO uint8_t TOVALH;                             /**< Watchdog Timeout Value Register: High, offset: 0x4 */       __IO uint8_t TOVALL;                             /**< Watchdog Timeout Value Register: Low, offset: 0x5 */     } TOVAL8B; This structure means that customer can define the watchdog timeout value by separated unit8 TOVALH, TOVALL or just defined it with unint16 TOVAL. But actually in the IAR project usage, take an example, use 1khz as the clock source for watchdog, then want to set the timeout value as 1s, it means the timeout value should be 1000=0x03e8, so one of the customers configure it like this:    You can find, we need the TOVALL= 0XE8, TOVALH=0X03, but from the test result, the register is TOVALL= 0X03, TOVALH=0Xe8, this will cause the timeout value is much larger than 1000, that is why customer can’t reset the mcu after 1s, because the register configuration is not correct. It is caused by the IAR int16 store endian mode, the default IAR endian mode is little endian mode. So in the practical usage, it is recommended to use the separated time out value definition. 2. debugger usage When in debug mode with IDE, some customers find even they comment all the watchdog disable code, they still can’t reset the MCU by the watchdog. After check the register WDOG_S1, bit EN is 0, it means the watchdog is disabled. But from the reference manual, we get that after reset, the EN bit should be 1. What caused this? After test, we find this actually caused by the debugger, the debugger hardware which you are using. Eg, in the same project which already comment all the watchdog disable code, SEGGER JLINK will still disable the watchdog, but the PE opensda or PE multilink won’t do this, the EN bit is enabled by default, the following is the test picture, take codewarrior as an example: 1) JLINK 2) PE Opensda or PE multilink    So, if you want to test the watchdog in debug mode, and want the EN is set after reset, you can choose PE debugger tool instead of JLINK, but this JLINK feature is just influence the debug mode, after you download the code to the chip flash, and after reset, the EN bit in WDOG_S1 will still be set. Wish this document will help you get out the problem of watchdog can’t be reset.
查看全文
1 Abstract Stepper motor can be controlled by the electrical pulse signal with the open loop system, it use the electrical pulse signal realize the angular movement or linear movement.  The speed and position of the stepper motor is determined by the pulse frequent and the pulse number. Stepper motor can be used in the low speed area application, with higher work efficiency and low noise. KE02 is the 5V kinetis E series MCU, it is based on ARM Cortex M0+ core, KE series are designed to maintain high robustness for complex electrical noise environment and high reliability application. For these advantages, KE02 is fit the Stepper motor control application. This document is mainly about how use the KE02 realize the Stepper motor speed, step and direction control. It can use the UART in the PC to control the Stepper motor speed. The following picture is the control diagram.                                                                              Fig.1 2. Motor control parameter calculation      Just as Fig.1 shows, KE02 should control the EN, DIR, PWM signal to the motor driver, then realize the stepper motor control. EN is the motor driver enable signal, 0 is enable, 1 is disable; DIR is the stepper motor direction control, 0, clockwise, 1 anticlockwise; PWM is the pulse signal to control the step and speed for the stepper motor.       Stepper motor is 1.8’, it means a round have 360’/1.8’= 200 steps. But because the Motor driver have the divider, it is 32, so one stepper motor round should have 200*32 = 6400 steps.       KE02 system, it use the external 10Mhz crystal, and configure both core and bus frequent to 20Mhz,  it use FTM0 module as the motor pulse generate module, bus clock with 32 prescale used as the FTM0 clock source, choose up counter. If need to change the motor speed and control step, just control the FTM PWM frequent and PWM counter. For Stepper motor, one FTM period means one motor step. From the reference manual of KE02, we get that, the FTM period in up counting mode is: (MOD-CNTIN+1)*period of the FTM counter clock, if want to change the frequent of motor, just calculate the MOD of FTM is ok, then count the number of the FTM cycle, now assume CNTIN =0, then: Tftm= (32/20Mhz)*(MOD+1) From the Stepper Motor and it’s driver, we get that one step time is : Tmstep= 60/(V*6400) V is the speed of Motor, the unit is round/minute. Because Tftm=Tmstep, then we know: MOD= (60/(V*6400))*(20Mhz/32)-1                     (F1) In this document, we calculate the speed of 150 round/minute, 110 round/minute, 80 round/minute, 50 round/minute and 0.1 round/minute, according to (F1), we can get the MOD for each speed as the following: 150 round/minute   MOD=38 110 round/minute   MOD=52 80 round/minute     MOD=72 50 round/minute     MOD=116 0.1 round/minute    MOD=58592 If each speed need to do 10 Stepper motor round, then just control the speed counter number to: 10*6400=64000. 3. MCU pin assignment PTF0 : DIR PTF1 : EN PTA0 : PWM PTC6 : UART1_RX PTC7 : UART1_TX 4. code writing (1)FTM initial code void STEEPMOTOR_PWM_Init(uint16 MODdata) {                    SIM_SCGC |= SIM_SCGC_FTM0_MASK;                 FTM0_SC = 0;                 FTM0_C0SC = 0 ;                 FTM0_C0SC = FTM_CnSC_MSB_MASK |FTM_CnSC_ELSA_MASK ;                 FTM0_C0V = 0;                 FTM0_C0V = MODdata>>1;                 FTM0_MOD=MODdata;                 FTM0_SC |=FTM_SC_CLKS(1) | FTM_SC_PS(5) | FTM_SC_TOIE_MASK                 enable_irq(17); //enable interrupt } MODdata can choose the different Stepper motor speed, eg, 150 round/minute, MODdata is 38. (2) interrupt service function void FTM0_IRQHandler(void) {                                 FTM0_SC  &= ~FTM_SC_TOF_MASK;//clear the TOF flag. roundcount++;                 if(roundcount >= 64000) {FTM0_C0SC = 0x00; FTM0_SC &= ~(FTM_SC_TOIE_MASK);} } It can used for the step counter, and when reach the 10round, then stop the motor( stop the FTM output). (3)Speed choose with UART input void Motor_Speed_GPIO_CTRL_30round(void) {                 char motormode=0;                 uint32 COMPDATA=0;                                 printf("\n 1 for 150 round/minute\n\r");                 printf("\n 2 for 110 round/minute\n\r");                 printf("\n 3 for 80 round/minute\n\r");                    printf("\n 4 for 50 round/minute\n\r");                    printf("\n 5 for 0.1 round/minute\n\r");                 motormode = UART_getchar(PC_TERM_PORT);                                     switch(motormode)                                 {                                    case '1':                                                       STEEPMOTOR_PWM_Init(38);//150 round/minute                                                         break;                                   case '2':                                                       STEEPMOTOR_PWM_Init(52);//110 round/minute                                                         break;                                   case '3':                                                                       STEEPMOTOR_PWM_Init(72);//80 round/minute                                                          break;                                   case '4':                                                                       STEEPMOTOR_PWM_Init(116);//50 round/minute                                                         break;                                   case '5':                                                                       STEEPMOTOR_PWM_Init(58592);//0.1 round/minute                                                         break;                                                                                default: break;                                 }                                 while( roundcount < 64000 ) {} //10 round                                 Disable_PWM;                                 printf("\n %c 10round PWM is finished ", motormode);                                 roundcount=0; } 5 DEMO About the test code, please find it from the attachment.
查看全文
Revise History: Version 23: NXP kinetis bootloader GUI upgrade from v1.0 to v1.1: added 04 extended linear address record  and 02 sector address record processing for hex format. This article describes how to do in-system reprogramming of Kinetis devices using standard communication media such as SCI. Most of the codes are written in C so that make it easy to migrate to other MCUs. The solution has been already adopted by customers. The pdf document is based on FRDM-KL26 demo board and Codewarrior 10.6.  The bootloader and user application source codes are provided. GUI and video show are also provided. Now the bootloader source code is ported to KDS3.0, Keil5.15 and IAR7.40 which are also enclosed in the SW package. Customer can make their own bootloader applications based on them. The application can be used to upgrade single target board and multi boards connected through networks such as RS485. The bootloader application checks the availability of the nodes between the input address range, and upgrades firmware nodes one by one automatically. ​ Key features of the bootloader: Able to update (or just verify) either single or multiple devices in a network. Application code and bootloader code are in separated projects, convenient for mass production and firmware upgrading. Bootloader code size is small, only around 2K, which reduces the requirement of on chip memory resources. Source code available, easy for reading and migrating. GUI supports S19,HEX and BIN format burning images. For more information, please see attached document and code. The attached demo code is for KL26 which is Cortex - M0+ core. For Cortex-M4 core demo, refer this url: https://community.freescale.com/docs/DOC-328365 User can also download the document and source code from Github: https://github.com/jenniezhjun/Kinetis-Bootloader.git Thanks for the great support from Chaohui Guo and his team. NOTE: The bootloader and GUI code are all open source, users can revise them based on your own requirement. Enjoy Bootloader programming 🙂
查看全文
When using ADCs it is not enough to just configure the module, add a clock signal, apply the Nyquist criteria and hope for the best, because normally that is just not enough. Even if we use the best software configuration, sampling rate, conversion time, etc; we might end up with noisy conversions, and worst of all a low ENOB figure which sums up in a lousy, low resolution ADC application. To complement the software end you need to follow some basic hardware design rules, some of them might seem logical, other might even weird or excessive however they are the key to a successful conversion, I took the time to compile a short list of effective design best practices trying to cover the basics of ADC design. If you think I missed something feel free to comment and ask for more information. Ground Isolation Because ground is the power return for all digital circuits and analog circuits, one of the most basic design philosophies is to isolate digital and analog grounds. If the grounds are not isolated, the return from the analog circuitry will flow through the analog ground impedance and the digital ground current will flow through the analog ground, usually the digital ground current is typically much greater than the analog ground current.  As the frequency of digital circuits increases, the noise generated on the ground increases dramatically. CMOS logic families are of the saturating type; this means the logic transitions cause large transient currents on the power supply and ground. CMOS outputs connect the power to ground through a low impedance channel during the logic transitions. Digital logic waveforms are rectangular waves which imply many higher frequency harmonic components are induced by high speed transmission lines and clock signals.                              Figure 1: Typical mixed signal circuit grounding                              Figure 2: Isolated mixed signal circuit grounding Inductive decoupling Another potential problem is the coupling of signal from one circuit to another via mutual inductance and it does not matter if you think the signals are too weak to have a real effect, the amount of coupling will depend on the strength of the interference, the mutual inductance, the area enclosed by the signal loop (which is basically an antenna), and the frequency. It will also depend primarily on the physical proximity of the loops, as well as the permeability of the material. This inductive coupling is also known as crosstalk in data lines.                               Figure 3: Coupling induced noise It may seem logical to use a single trace as the return path for the two sources (dotted lines). However, this would cause the return currents for both signals to flow through the same impedance, in addition; it will maximize the area of the interference loops and increase the mutual inductance by moving the loops close together. This will increase the mutual noise inductance and the coupling between the circuits. Routing the traces in the manner shown below minimizes the area enclosed by the loops and separates the return paths, thus separating the circuits and, in turn, minimizing the mutual noise inductance.                               Figure 4: Inductance decoupling layout Power supply decoupling The idea after power decoupling is to create a low noise environment for the analog circuitry to operate. In any given circuit the power supply pin is really in series with the output, therefore, any high frequency energy on the power line will couple to the output directly, which makes it necessary to keep this high frequency energy from entering the analog circuitry. This is done by using a small capacitor to short the high frequency signals away from the chip to the circuit’s ground line. A disadvantage of high frequency decoupling is it makes a circuit more prone to low frequency noise however it is easily solved by adding a larger capacitor. Optimal power supply decoupling A large electrolytic capacitor (10 μF – 100 μF) no more than 2 in. away from the chip. A small capacitor (0.01 μF – 0.1 μF) as close to the power pins of the chip as possible. A small ferrite bead in series with the supply pin (Optional).                               Figure 5: Power supply decoupling layout Treat signal lines as transmission lines Although signal coupling can be minimized it cannot be avoided, the best approach to effectively counteract its effects on signal lines is to channel it into a conductor of our choice, in this case the circuit’s ground is the best choice to channel the effects of inductive coupling; we can accomplish this by routing ground lines along signal lines as close as manufacturing capabilities allow. An very effective way to accomplish this is routing signals in triplets, these works for both digital and analog signals.The advantages of doing so are an improved immunity not only to inductive coupling but also immunity to external noise. Optimal routing: Routing in “triplets” (S-G-S) provide good signal coupling with relatively low impact on routing density Ground trace needs to be connected to the ground pins on the source and destination devices for the signal traces Spacing should be as close as manufacturing will allow                               Figure 6: Transmission line routing Signal acquisition circuit To improve noise immunity an external RC acquisition circuit can be added to the ADC input, it consists of a resistor in series with the ADC input and a capacitor going from the input to the circuit’s ground as the figure below shows:                                                             Figure 7: ADC with an external acquisition circuit The external RC circuit values depend on the internal characteristics and configuration of the ADC you use, such as the availability of an internal gain amplifier or the ADC’s architecture; the equation and circuit shown here represents a simplified form of ADC used in Freescale devices. The equivalent sampling resistance RSH is represented by total serial resistance connected between sampling capacitance and analog input pin (sampling switch, multiplexor switches etc.). The sampling capacitance CSH is represented by total parallel capacitance. For example in a case of Freescale SAR ADC equivalent sampling capacitance contains bank of capacitances. The equation shown how to calculate the value of the input resistor based on the values of both the input and sample and hold circuit. It must be noted the mentioned figures could have an alternate designation in any given datasheet; the ones mentioned here are specific to Kinetis devices: TAQ=      Acquisition time (.5/ADC clock) CIN=       Input capacitance (33pF min) CSH=      Sample & Hold circuit capacitance ( CDAIN in datasheet) VIN=       Input voltage level VCSH0= Initial voltage across S&H circuit (0V) VSFR=    Full scale voltage (VDDA) N=           bit resolution Note:  Special care must be taken when performing the calculation since a deviation from the correct values will result in a significant conversion error due to signal distortion.
查看全文
Although most of us have a basic understanding of how an ADC works and how to understand some of the basic figures that define an ADC performance, that is far from really understanding how to fully interpret and use the figures depicted in a datasheet ADC section. With all those numbers it is easy to get lost on which ones to look at when we want to know how it will react to conditions such as frequency, signal amplitude, temperature, etc; having such knowledge would allow us to better fit a specific ADC to your application and take full advantage of its features. Having this in mind I took the time to compile some information related to what the most common figures that describe an ADC performance depicted in a datasheet mean, most of the material can be found in any Analog to Digital Conversion theory book; as I mentioned before this is just a general compilation of knowledge I hope will help you better understand those specifications. It assumes those of us who use datasheets are somehow familiar with the basic working of ADCs, so I will spare the basic concepts. Now down to business, this is a extract of a typical ADC section from a microcontroller's datasheet: I am almost certain not a lot of people who use microcontrollers, and more specifically ADCs; have a clear idea of what Total Unadjusted Error, Integral Non-Linearity or Differential Non-Linearity describe in the behavior of an ADC. Even though I will try to describe in detail the most common parameters I might miss some others and there is the possibility some of the information might not be as accurate as I would like it to be, if any of you reading this brief document have specific questions regarding any parameter I describe or miss by all means comment. Common ADC electrical characteristics depicted in datasheets EQ          Quantization error      Since the analog input to an ADC can take any value, but the digital output is quantized, there may be a difference of up to ½ Less Significant Bit between the actual analog input and the exact value of the digital output. This is known as the quantization error or quantization uncertainty as shown below. In ac (sampling) applications this quantization error gives rise to quantization noise. SINAD, SNR and ENOB (Signal to Noise plus Distortion, SIgnal to Noise Ratio and Effective Number of Bits)      Signal-to-Noise-and Distortion (SINAD, or S/(N + D) is the ratio of the rms signal amplitude to the mean value of the root-sum square (rss) of all other spectral components, including harmonics, but excluding dc. SINAD is a good indication of the overall dynamic performance of an ADC      as a function of input frequency because it includes all components which make up noise (including thermal noise) and distortion. It is often plotted for various input amplitudes. SINAD is equal to THD + N if the bandwidth for the noise measurement is the same. SINAD is often converted      to effective-number-of-bits (ENOB) using the relationship for the theoretical SNR of an ideal N-bit ADC: SNR = 6.02N + 1.76 dB, the equation is solved for N, and the value of SINAD is substituted for SNR.      Effective number of bits (ENOB) is a measure of the dynamic performance of an analog to digital converter and its associated circuitry. The resolution of an ADC is specified by the number of bits used to represent the analog value, in principle giving 2 N signal levels for an N-bit signal. However, all real ADC circuits introduce noise and distortion. ENOB specifies the resolution of an ideal ADC circuit that would have the same resolution as the circuit under consideration. Often ENOB is calculated using the relationship for the theoretical SNR of an ideal N-bit ADC: SNR =      6.02N + 1.76 dB, the equation is solved for N, and the value of SINAD is substituted for SNR. SFDR      Spurious Free Dynamic Range     One of the most significant specification for an ADC used in a communications application is its spurious free dynamic range (SFDR). SFDR of an ADC is defined as the ratio of the rms signal amplitude to the rms value of the peak spurious spectral content measured over the bandwidth      of interest. SFDR is generally plotted as a function of signal amplitude and may be expressed relative to the signal amplitude (dBc) or the ADC full-scale (dBFS) as shown in Figure n. For a signal near full-scale, the peak spectral spur is generally determined by one of the first few harmonics of the fundamental. However, as the signal falls several dB below full-scale, other spurs generally occur which are not direct harmonics of the input signal. This is because of the differential nonlinearity of the ADC transfer function as discussed earlier. Therefore, SFDR      considers all sources of distortion, regardless of their origin. INL      Integral Non-Linearity     Integral nonlinearity (acronym INL) is the maximum deviation between the ideal output of an ADC and the actual output level (after offset and gain errors have been removed). The transfer function of an ADC should ideally be a line and the INL measurement depends on the ideal line selected. Two often used lines are the best fit line, which is the line that minimizes the INL result and the endpoint line which is a line that passes through the points on the transfer function corresponding to the lowest and highest input code. In all cases, the INL is the maximum distance between the ideal line selected and the actual transfer function. DNL        Differential Non-Linearity      Differnetial NonLinearity relates to the linearity of the code transitions of the converter. In the ideal case, a change of 1 LSB in digital code corresponds to a change of exactly 1 LSB of analog signal. In an ADC there should be exactly 1 LSB change of analog input to move from one           digital transition to the next. Differential linearity error is defined as the maximum amount of deviation of any quantum (or LSB change) in the entire transfer function from its ideal size of 1 LSB. Where the change in analog signal corresponding to 1 LSB digital change is more or less than 1 LSB, there is said to be a DNL error. The DNL error of a converter is normally defined as the maximum value of DNL to be found at any transition across the range of the converter. The following figure shows the non-ideal transfer functions for an ADC and shows the effects of the DNL error.      A common result of excess DNL in ADCs is missing codes resulting from DNL < –1 LSB. THD      Total Harmonic Distortion Total harmonic distortion (THD) is the ratio of the rms value of the fundamental signal to the mean value of the root-sum-square of its harmonics (generally, only the first 5 are significant). THD of an ADC is also generally specified with the input signal close to full-scale, the harmonics of the input signal can be distinguished from other distortion by their location in the frequency spectrum. The second and third harmonics are generally the only ones specified on a data sheet because they tend to be the largest. EFS     Full Scale Error Full-scale error can be defined as the difference between the actual value triggering the transition to full-scale and the ideal analog full-scale transition value. Full-scale error is equal to the offset error + gain error Offset error The transfer characteristics of both DACs and ADCs may be expressed as a straight line given by D = K + GA, where D is the digital code, A is the analog signal, and K and G are constants. In a unipolar converter, the ideal value of K is zero. The offset error is the amount by which the actual value of K differs from its ideal value. Gain error The gain error is the amount by which G differs from its ideal value, and is generally expressed as the percentage difference between the two, although it may be defined as the gain error contribution (in mV or LSB) to the total error at full-scale. TUE      Total Unadjusted Error This is the result of performing conversions without having calibrated the ADC, it is dominated by the uncalibrated gain and uncalibrated offset terms in the data sheet. Although most devices will be well within the data sheet limits, it should be noted that they are not centered around zero and full range of the incoming analog signal is not guaranteed. Therefore, an uncalibrated ADC will always show unknown levels of gain and offset error, thus reflecting the worst case of conversion error the module can provide.
查看全文
For Remote Control means, that is needed two computers - Server Computer and User Computer, which will be in connection. There are two types of connection, which can be used - HTTP or DCOM. There are two different ways how to set up the remote control in Windows. I made the tutorial, which describes both types of Remote Control. Ok - so, let´s start! HTTP Settings On the Server Computer side: 1. Plug the board to the Server Computer 2. Go to Remote Communication Server 3. Set HTTP connection and choose the right COM Port according the plugged board If the plugged board is on e.g. COM23, it is possible to edit number of Port in Device Manager On the User PC side: 1. Open FreeMASTER,  go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (HTTP) and type the IP address of the server, do not forget join to IP address :8080 3. And start communication by STOP button to successful connection DCOM Settings On the Server Computer side: 1. Plug board to the Server Computer 2. Launch DCOM in FreeMASTER Remote Server Choose COM according plugged board or edit COM according to step 2 - Server Computer in HTTP Connection (up). 3. Setting permissions for the user, User PC. Right click on Computer -> Manage. In Computer Management click to Distributed COM Users. In Distributed COM Users Properties add the user, User Computer. After that, set the permissions in Component Services. In cmd type dcomcnfg.exe In Component Services go to Computers -> My Computer -> DCOM Config -> MCB FreeMASTER Remote Server Application Right click on MCB FreeMASTER Remote Server Application and go to Properties. In Security Tab is possible to add the permissions. There are 3 types of permissions. First permission - Launch and Activation Permissions. There are 4 permission options. Local Launch and Remote Launch means, that user, User Computer can launch e.g. FM Remote Server Application. But for success communication is needed allowing Local Activation and Remote Activation. Second permission - Access Permissions. Click to Edit and Allow Local Access and Remote Access for the user. Do not forget that if there is a change of permissions, specifically allowing, it is necessary for User to log out and log in. On the User Computer side: 1. Open Freemaster, go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (DCOM) and for filling Connect string is possible to use Configure. Definitely, type the IP address of the server and ;Port Name. 3. And start communication by STOP button in FreeMASTER to successful connection And now.. you can do anything 🙂
查看全文
1. How Calibration works There are three main sub-blocks important in understanding how the Kinetis SAR module works.  There is a capacitive DAC, a comparator, and the SAR engine that controls the module. Of those blocks, the DAC is most susceptible to variations that can cause linearity problems in the SAR. The DAC is architected with three sets of binary weighted capacitors arrayed in banks, as in Figure 1. The capacitors that represent the most significant bits of the SAR (B15:B11) are connected directly to the inputs of the comparator. The next bank of five capacitors (B10:B6) is connected to the top plate of the MSB array through an intentionally oversized scaling capacitor. The final six capacitors that makeup the least significant bits of the SAR (B5:B0) are correspondingly connected to the top plate of the middle bank of capacitors through another scaling capacitor. Figure 1. Arrangement of DAC capacitors Only the MSB capacitor bank is calibrated. Because the first scaling capacitor is intentionally oversized, each of the non-calibrated MSB capacitors will have an effective capacitance too small to yield accurate results. However, because they are always too small, we can measure the amount oferror that each of those capacitors would cause individually, and add that back in to the result. Calibration starts with the smallest of the LSB capacitors, B11. The SAR samples Vrefl on all of the capacitors that are lower-than or equal-to the capacitor under test (CUT), while connecting all of the smaller capacitors to Vrefh. The top plate of all of the MSB capacitors is held at VDDA while this happens. After the sampling phase is complete, the top plates of the MSB capacitors are allowed to float, and the bottom plates of the MSBs not under test are connected to Vrefl. This allows charge to redistribute from the CUT to the smaller capacitors. Finally, an 11 bit SAR algorithm (corresponding with the 11 capacitors that are smaller than the MSB array) is performed which produces a result that indicates the amount of error that the CUT has compared to an ideally sized capacitor. This process is repeated for each of the five MSBs on both the plus side and minus side DACs and the five error values that are reported correspond to the five MSBs accordingly. All of these error values are about the same magnitude, with a unit of 16-bit LSBs. See Figure 2 for an example. Figure 2. Example of calibration on bit 11 The DAC MSB error is cumulative. That is, if bit 11 of the DAC is set, then the error is simply the error of that bit. However if bit 12 of the DAC is set, the total error is equivalent tothe error reported on bit 12, plus the error reported on bit 11. For each MSB the error is calculated as below, where Ex is the error found during the calibration for its corresponding MSB bit: When bit 11 of the DAC is set: CLx0 = E0. When bit 12 of the DAC is set: CLx1 = E0+E1. When bit 13 of the DAC is set: CLx2 = E2 + E1 + 2E0. When bit 14 of the DAC is set: CLx3 = E3 + E2 + 2E1 + 4E0. When bit 15 of the DAC is set: CLx4 = E4 + 2E3 + 4E2 + 8E1 + 16E0 Figure 3. Effect of calibration error on ADC response These are the values that are then placed in each of the CLxx calibration results registers. Figure 3 shows how the errors would accumulate if all of the CLxx registers were set to zero. The offset and gain registers are calculated based on these values as well. Because of this, the gain and offset registers calibrate only for errors internal to the SAR itself. Self calibration does not compensate for board or system level gain or offset issues. 2. Recommended Calibration Procedure From the above description it is evident that the calibration procedure is in effect several consecutive analog to digital conversions. These are susceptible to all of the same sources of error of any ADC conversion. Because what is primarily being measured is the error in the size of the MSB capacitors; the recommendation is to configure the SAR in such a way as to make for the most accurate conversions possible in the environment that the SAR is being calibrated in. Noise is the primary cause of run-to-run variation in this process,so steps should be taken to reduce the impact of noise during the calibration process. Such as: All digital IO should be silent and unnecessary modules should be disabled. The Vrefh should be as stable and high a voltage as possible, since higher Vrefh means larger ADC code widths. An isolated Vrefh pin would be ideal. Lacking that, using an isolated VDDA as the reference would be preferable to using VREFO. The clock used should be as noise free as possible, and less than or equal to 6 MHz. For this purpose the order of desirable clock sources for calibration would be OSC > PLL > FLL > ASYNC The hardware averaging should be set to the maximum 32 samples. The Low Power Conversion bit should be set to 0. The calibration should be done at room temperature. The High Speed Conversion and Sample Time Adder will not have much effect in most situations, and the Diff and Mode bits are completely ignored by the calibration routine. The calibration values should be taken for each instance of the SAR on a chip in the above conditions. They should be stored in nonvolatile memory and then written into their appropriate registers whenever the ADC register values are cleared. In some instances, the system noise present will still cause the calibration routine to exhibit greater than desired run-to-run variation. One rule of thumb would be to repeat calibration several times and look at the CLx0 registers. If the value reported in that register varies by more than three, the following procedure can be implemented. Run the calibration routine several times. Twenty to forty times. Place the value of each of the calibration registers into a corresponding array. Perform a bubble sort on each array and find the median value for each of the calibration registers. Use  these median values as described for typical calibration results.
查看全文