FRDM Training Hub

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM Training Hub

FRDM Training Hub


Restricted Beta Program

  • Comprehensive software and tools for seamless prototyping and rapid development
  • Scale your project with modular, quick-start FRDM and expansion boards
  • Leverage our application code hub or GoPoint to access 180+ code snippets and demos

  • Leverage FRDM Training Hub to learn from the experts
  • Not sure where to start ?

讨论

排序依据:
This document assumes FRDM-iMX91 board is flashed with a Linux image. For flashing instructions, refer to FRDM-iMX91_Board_Flashing guide. Then, follow this document to download software applications to test Wi-Fi, Bluetooth, and 802.15.4 performance. Hardware Prerequisites Windows or Linux PC with 64-bit OS 2 spare USB ports on PC FRDM-iMX91 Development Board Bluetooth LE device: Mobile phone which can configured as central or peripheral Wi-Fi Access Point: Standalone or mobile hotspot Wi-Fi Station: Mobile phone used as a station OPENTHREAD: 1 Another OT enabled board   Required PC Software   Serial Terminal program Setting for terminal: Baud rate:115200, Parity: none, Data bits: 8, Stop bits: 1 Windows:   PUTTY or teraterm  and USB Device driver  Linux:           Minicom (Command to download the tool : sudo apt-get install minicom)   Iperf Windows:    Download Iperf version 3.0.11 from here. Linux:            Download Debian package of IPerf 3.0.11 for Ubuntu 16.04 from here. $ wget https://iperf.fr/download/ubuntu/iperf3_3.0.11-1_amd64.deb   Install the package using the command below. $ sudo dpkg -i /path/to/package/iperf3_3.0.11-1_amd64.deb   Required Mobile Software   Iperf Application (iperf 3) Android:  HE.NET Network Tools on Google Play iOS:   HE.NET Network Tools on AppStore   nRF Connect Application Android:   nRF Connect on Google Play iOS:    nRF Connect on App Store   Required EVK Software Linux BSP Image  Version: L6.6.52_2.2.0 Link: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L6.6.52_2.2.0_MX91&appType=file1&DOWNLOAD_ID=null   To download the pre-built image, please refer to https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX   hands-on Labs   Lab1 - WIFI Hands-on Lab2 - Bluetooth LE GATT Profile  Lab3 - OpenThread  Lab4-WIFI_Bluetooth-LE_OpenThread   Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here   
查看全文
FRDM-IMX91 Hardware Introduction The FRDM i.MX 91 development board is a low-cost and compact development board with NXP i.MX91 applications processor. On-board NXP IW610 Tri-Radio module supports Wi-Fi 6 + Bluetooth Low Energy 5.4 + 802.15.4. NXP releases Debian every six months and releases Yocto every year for this board. The FRDM i.MX 91 development board is ideal for developing modern Industrial and IoT applications. Get to know FRDM-IMX 91 Development Board   Specifications: 1x Arm® Cortex®-A55​ MAYA-W476-00B, Wi-Fi + BLE 5.4 + 802.15.4​​ Module on-board, IW610 2x GbE Ethernet (1xETER, 1xTSN) M.2 Key-E for Wi-Fi/BLE/802.15.4​ LPDDR4 16-bit 1GB eMMC 5.1, 8GB MicroSD 3.0 card slot 3x USB 2.0 Type-C connector (1-Debug, 1-PD, 1-USB2.0) + One USB 2.0 Type-A​ 40 pin (2x20) Expansion I/O One 2x5 Pin NXP interface (1- CAN, Two channels for ADC, I2C/I3C expansion)   Features FRDM-IMX91 eMMC 8GB DRAM NANYA 1GB PMIC PCA9451 WiFi Module u-blox MAYA-W476-00B on-board USB TYPE Type-C+Type-A ENET 2xGbE M.2 (Key E) SDIO Wi-Fi / BLE Y (rework needed) HDMI N Display (Parallel RGB LCD) 2x20 EXPI Camera (Parallel Camera) 2x20 EXPI 2x20 Expansion Interface Y CAN BUS Y MicroSD Y UART Y Audio  MQS Remote Debug N Power Connector Type-C PCB layers 10 Base Board DIM 6.5x10.5cm     NXP Devices On-board   PMIC PCA9451AHNY Real time clock/calendar PCF2131 WIFI/BLE/802.15.4 Tri-Radio IW610 in u-blox module CAN Transceiver TJA1051T/3 USB Type-C CC and SBU Protection IC NX20P0407  High-Voltage USB PD Power Switch NX20P5090UK USB PD and Type-C High-Voltage Sink/Source Combo Switch with Protection NX20P3483UK IIC Extends GPIO PCAL6524/ PCAL6408A Expansion Boards TM050RDH03-41: LCD display module 5” TFT 800X480, RGB, 120.7 mm x75.8 mm7inch MX93AUD-HAT: Audio expansion board with multiple features ​8MIC-RPI-MX8: 8-microphone array proto board for voice enablement Trainings   FRDM-IMX91 SW Release Package  FRDM-IMX91 Connectivity training   Documentation  −FRDM-IMX91 Quick Start Guide −FRDM-IMX91 Board User Manual -FRDM-IMX91 Software User Guide   Useful Links −i.MX Yocto Project User’s Guide​ −i.MX Linux User’s Guide ​−i.MX Linux Reference Manual​ −i.MX Porting Guide -i.MX Debian Linux SDK User Guide
查看全文
Load drivers of wireless module into board Bring-up Bluetooth Scan/pair/connect Bluetooth with smartphone Hands-on Bluetooth A2DP sink/source profile demo play audio on remote Bluetooth headset or speaker using Bluetooth A2DP source profile play audio on FRDM i.MX 93 board from smart phone using Bluetooth A2DP sink profile Bluetooth A2DP Source and Sink Profile Demo    Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
查看全文
This article will give a brief introduction of FRDM-IMX8MPLUS software release, including Yocto BSP release and Debian release. FRDM-IMX Yocto BSP Release i.MX FRDM Development software release contains prebuilt images, documentation, and i.MX FRDM Yocto layer for FRDM-IMX boards. It also includes support for Matter.  Based on i.MX SW 2024 Q3 BSP release Linux kernel: 6.6.36_2.1.0 u-boot: 2024.04 i.MX FRDM Yocto layer source: https://github.com/nxp-imx-support/meta-imx-frdm For more details, please check i.MX FRDM Software User Guide. FRDM-IMX8MPLUS accessories and corresponding dtb: 7-inch Waveshare LCD: imx8mp-frdm-waveshare.dtb DY1212W-4856 LVDS: imx8mp-frdm-boe-wxga-lvds0-panel.dtb imx8mp-frdm-boe-wxga-lvds1-panel.dtb RPI-CAM-MIPI MIPI CSI: imx8mp-frdm-ap1302.dtb imx8mp-frdm-dual-ap1302.dtb IMX-OS08A20 MIPI CSI: imx8mp-frdm-os08a20.dtb imx8mp-frdm-dual-os08a20.dtb 8MIC-RPI-MX8: imx8mp-frdm-8mic.dtb 2EL M.2 Module: imx8mp-frdm-iw612-otbr.dtb Build FRDM-IMX8MPLUS Yocto image: Download i.MX SW 2024 Q3 release: $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $ repo sync Integrate meta-imx-frdm layer into Yocto code base: $ cd ${MY_YOCTO}/sources $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git Yocto project setup: $ cd ${MY_YOCTO} $ MACHINE=imx8mpfrdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx8mp Build images: $ bitbake imx-image-full Flash SD card image using dd: $ zstdcat imx-image-full-imx8mpfrdm.rootfs.wic.zst | sudo dd of=/dev/sdx bs=1M && sync Or use uuu to burn image to SD card: $ uuu -b sd_all imx-image-full-imx8mpfrdm.rootfs.wic.zst FRDM-IMX8MPLUS Matter Support Based on i.MX Matter 2024 Q3 To include Matter support, please follow below steps to include Matter layer into Yocto build. Download i.MX SW 2024 Q3 BSP Release: $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $ repo sync Download i.MX Matter Yocto layer: $ cd ${MY_YOCTO}/sources/meta-nxp-connectivity $ git remote update $ git checkout imx_matter_2024_q3 Integrate meta-imx-frdm layer into Yocto code base: $ cd ${MY_YOCTO}/sources $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git Yocto Project Setup: $ cd ${MY_YOCTO} $ MACHINE=imx8mpfrdm-matter DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-matter-setup.sh bld-xwayland-imx8mpfrdm Build images: $ bitbake imx-image-multimedia FRDM-IMX8MPLUS Debian Release FRDM-IMX8MPLUS has support on Debian 12 OS. i.MX Debian Linux SDK distribution is a combination of NXP-provided kernel and boot loaders with a Debian distro user-space image, which includes: Debian-based rootfs Debian Base (basic packages) Debian Server (more packages without GUI Desktop) Debian Desktop (with GNOME GUI Desktop) Linux kernel BSP components various applications (graphics, multimedia, networking, connectivity, security, and AI/ML) For more details of NXP Debian Linux SDK Distribution, please check NXP Debian Linux SDK User Guide. Quick Start with Debian: To create an SD card with Debian for FRDM-IMX8MPLUS, please follow below steps. Download flex-installer on the Linux host $ wget http://www.nxp.com/lgfiles/sdk/lsdk2412/flex-installer $ chmod +x flex-installer $ sudo mv flex-installer /usr/bin Plug the SD card into the Linux host and install the images as below # format SD card $ flex-installer -i pf -d /dev/sdx # automatically download and install images into SD card $ flex-installer -i auto -d /dev/mmcblk1 -m imx8mpfrdm Plug the SD card into FRDM-IMX8MPLUS board and install the extra packages as below  1. Setup Ethernet network interface by DHCP or setting it manually $ dhclient -i end0 2. Set correct system time, for example $ date -s "22 Nov 2024 09:00:00" 3. Install extra packages for GNOME GUI Desktop version $ debian-post-install-pkg desktop 4. Or install extra packages for Server version without GUI Desktop $ debian-post-install-pkg server 5. After finishing the installation, run the reboot command to boot up the Debian Desktop/Server system Building Debian Images with Flexbuild: To build Debian image with Flexbuild for FRDM-IMX8MPLUS, please follow below steps. Set up the build environment $ git clone https://github.com/nxp/flexbuild $ cd flexbuild && source setup.env #Continue to run commands below in case you need to build in Docker due to lack of Ubuntu 22.04 or Debian 12 host $ bld docker $ source setup.env Build image with Flexbuild $ bld -m imx8mpfrdm Flexbuild usage: To build individual part of the image, please check below command list for Flexbuild usage. $ bld uboot -m imx8mpfrdm (compile u-boot image for imx8mpfrdm) $ bld linux (compile linux kernel for all arm64 i.MX machines) $ bld bsp -m imx8mpfrdm (generate BSP firmware) $ bld boot (generate boot partition tarball including kernel, dtb, modules, distro bootscript for iMX machines) $ bld multimedia (build multimedia components for i.MX platforms) $ bld rfs -r debian:server (generate Debian server rootfs) $ bld apps -r debian:server (compile apps against runtime dependencies of Debian server RootFS) $ bld merge-apps -r debian:server (merge iMX-specific apps into target Debian server RootFS) $ bld packrfs -r debian:server (pack and compress target debian server rootfs) Related Documentation i.MX FRDM Software User Guide i.MX Debian Linux SDK User Guide More information about i.MX productions can be found at(http://www.nxp.com/imxlinux) i.MX Yocto Project User’s Guide​ i.MX Linux User’s Guide​ i.MX Linux Reference Manual​ i.MX Porting Guide Debian documents at http://www.nxp.com/nxpdebian
查看全文
i.MX FRDM Development (FRDM) software release contains prebuilt images, documentation, and i.MX FRDM Yocto layer for FRDM-IMX boards. It also includes support for Matter and Debian release. This article will give a brief introduction of FRDM-IMX91 software release. For more details, please check i.MX FRDM Software User Guide. FRDM-IMX91 Yocto BSP Release Based on i.MX SW 2024 Q3 BSP release Linux kernel: 6.6.36_2.1.0 u-boot: 2024.04 i.MX FRDM Yocto layer source: https://github.com/nxp-imx-support/meta-imx-frdm FRDM-IMX91 BSP changes: U-boot: Add basic support for FRDM-IMX91 Kernel: Add basic support for FRDM-IMX91 and add support for kinds of accessories FRDM-IMX91 Yocto layer: Add Yocto layer for FRDM-IMX91 and integrate u-boot/kernel patches FRDM-IMX91 accessories and corresponding dtb: 5 inch Tianma LCD: imx91-11x11-frdm-tianma-wvga-panel.dtb RPI-CAM-INTB: imx91-11x11-frdm-mt9m114.dtb MX91AUD-HAT or MX91AUD-HAT + 8MIC-RPI-MX8: imx91-11x11-frdm-aud-hat.dtb 8MIC-RPI-MX8: imx91-11x11-frdm-8mic.dtb 2LL M.2 Module: imx91-11x11-frdm.dtb Build FRDM-IMX91 Yocto Image: Download i.MX SW 2024 Q3 Release: $ repo init -uhttps://github.com/nxp-imx/imx-manifest-b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $ repo sync Integrate meta-imx-frdm layer into Yocto code base: $ cd ${MY_YOCTO}/sources $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git Yocto Project Setup: $ cd ${MY_YOCTO} $ MACHINE=imx91frdm DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-setup.sh -b frdm-imx91 Build images: $ bitbake imx-image-full Flashing SD card image using dd: $ zstdcat imx-image-full-imx91frdm.rootfs.wic.zst | sudo dd of=/dev/sdx bs=1M && sync Or using uuu to burn image to SD card: $ uuu -b sd_all imx-image-full-imx91frdm.rootfs.wic.zst FRDM-IMX91 Matter Support Based on i.MX Matter 2024 Q3 To include Matter support, please follow below steps to include Matter layer into Yocto build. Download i.MX SW 2024 Q3 BSP Release: $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml $ repo sync Download i.MX Matter Yocto layer: $ cd ${MY_YOCTO}/sources/meta-nxp-connectivity $ git remote update $ git checkout imx_matter_2024_q3 Integrate meta-imx-frdm layer into Yocto code base: $ cd ${MY_YOCTO}/sources $ git clone https://github.com/nxp-imx-support/meta-imx-frdm.git Yocto Project Setup: $ cd ${MY_YOCTO} $ MACHINE=imx91frdm-iwxxx-matter DISTRO=fsl-imx-xwayland source sources/meta-imx-frdm/tools/imx-frdm-matter-setup.sh bld-xwayland-imx91 Build images: $ bitbake imx-image-multimedia FRDM-IMX91 Debian Release FRDM-IMX91 has support for Debian 12 OS. i.MX Debian Linux SDK distribution is a combination of NXP-provided kernel and boot loaders with a Debian distro user-space image, which includes: Debian-based rootfs Debian Base (basic packages) Debian Server (more packages without GUI Desktop) Debian Desktop (with GNOME GUI Desktop) Linux kernel BSP components various applications (graphics, multimedia, networking, connectivity, security, and AI/ML) For more details of NXP Debian Linux SDK Distribution, please check NXP Debian Linux SDK Distribution for i.MX and Layerscape. Quick Start with Debian: To create an SD card with Debian for FRDM-IMX91, please follow below steps. Download flex-installer on the Linux host $ wget http://www.nxp.com/lgfiles/sdk/lsdk2412/flex-installer $ chmod +x flex-installer $ sudo mv flex-installer /usr/bin Plug the SD card into the Linux host and install the images as below # format SD card $ flex-installer -i pf -d /dev/sdb # automatically download and install images into SD card $ flex-installer -i auto -d /dev/mmcblk1 -m imx91frdm Plug the SD card into the FRDM-IMX91 board and install the extra packages as below         1. Setup Ethernet network interface by DHCP or setting it manually $ dhclient -i end0         2. Set correct system time, for example $ date -s "22 Nov 2024 09:00:00"         3. Install extra packages for GNOME GUI Desktop version $ debian-post-install-pkg desktop         4. Or install extra packages for Server version without GUI Desktop $ debian-post-install-pkg server         5. After finishing the installation, run the reboot command to boot up the Debian Desktop/Server system  Building Debian Images with Flexbuild: To build Debian image with Flexbuild for FRDM-IMX91, please follow below steps. Set up the build environment $ git clone https://github.com/nxp/flexbuild $ cd flexbuild && source setup.env #Continue to run commands below in case you need to build in Docker due to lack of Ubuntu 22.04 or Debian 12 host $ bld docker $ source setup.env Build image with Flexbuild $ bld -m imx91frdm Flexbuild usage: To build individual part of the image, please check below command list for Flexbuild usage $ bld uboot -m imx91frdm (compile u-boot image for imx91frdm) $ bld linux (compile linux kernel for all arm64 i.MX machines) $ bld bsp -m imx91frdm (generate BSP firmware) $ bld boot (generate boot partition tarball including kernel, dtb, modules, distro bootscript for iMX machines) $ bld multimedia (build multimedia components for i.MX platforms) $ bld rfs -r debian:server (generate Debian server rootfs) $ bld apps -r debian:server (compile apps against runtime dependencies of Debian server RootFS) $ bld merge-apps -r debian:server (merge iMX-specific apps into target Debian server RootFS) $ bld packrfs -r debian:server (pack and compress target debian server rootfs) Related Documentation FRDM-IMX91 Documents: FRDM-IMX91 Quick Start Guide FRDM-IMX91 Board User Manual i.MX FRDM Software User Guide More information about i.MX productions can be found at(http://www.nxp.com/imxlinux) i.MX Yocto Project User’s Guide​ i.MX Linux User’s Guide​ i.MX Linux Reference Manual​ i.MX Porting Guide Debian documents at http://www.nxp.com/nxpdebian i.MX Debian Linux SDK User Guide
查看全文
Discover how to build and deploy machine learning models for time series data using NXP’s eIQ Time Series Studio. This two-part training covers fan state classification and real-time anomaly detection on the FRDM-MCXN947 development board.
查看全文
The FRDM-i.MX 91 development board enables Advance HMI Solutions supporting Industrial and consumer HMI, Enriched user experience, Immersive Audio Processing, Voice Solutions, and Interconnected Devices (smarter edge devices) among other applications. This document explains how to set up FRDM-i.MX 91 development board. This includes the hardware connections, flashing the Linux image, and accessing the debug console.   FRDM-IMX91 Board Flashing Guide Video   Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
查看全文
This article mainly introduces the design of the FRDM-MCXE247 and how to import and run ACH examples. Through this article, readers can gain a detailed understanding of the main resources of the FRDM-MCXE247 board, design files, and how to import, download, and run an SDK example.   Hardware Requirements One FRDM-MCXE247 board A personal computer One USB Type-C cable   Software Requirements SDK25.06.00_FRDM-MCXE247 (Download from: https://mcuxpresso.nxp.com) MCUXpresso IDE v25.6 or later (Download from: MCUXpresso IDE | NXP) Serial Terminal Software for PC: Windows: PUTTY or Tera Term USB Device Driver   Board User Manual The FRDM-MCXE247 board is a design and evaluation platform based on the NXP MCX E247 microcontroller (MCU). The MCX E247 MCU is based on an Arm Cortex-M4F core, running at speeds of up to 112 MHz with a 2.70 V–5.5 V supply. The FRDM-MCXE247 board includes: One MCX E247 device 64 Mbit external serial flash (Winbond) FXLS8974CFR3 I2C accelerometer sensor NMH1000 I2C magnetic switch Three TJA1057BTK CAN PHYs Ethernet PHY RGB LED Push buttons MCU-Link debug probe circuit The board is compatible with Arduino shield modules, Pmod boards, and mikroBUS. For debugging, the board uses an onboard (OB) debug probe, MCU-Link OB, based on the NXP LPC55S16 MCU. In this document, the MCX E247 is referred to as the target MCU, and the LPC55S16 as the debug MCU. This document provides detailed information about the FRDM-MCXE247 board interfaces, accelerometer, power supplies, clocks, connectors, jumpers, push buttons, LEDs, and the MCU-Link OB debug probe. You can download the FRDM-MCXE247 Board User Manual [UM12286] from: https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXE247   Getting Started The Getting Started page provides not only an introduction to the board but also instructions on how to import SDK projects. https://www.nxp.com/document/guide/getting-started-with-the-frdm-mcxe247-board:GS-FRDM-MCXE247   Application Code Hub We provide several MCXE247 application code hub examples. You can find the project code from the following links and import them into MCUXpresso IDE to run: https://mcuxpresso.nxp.com/appcodehub?search=an-mc-pmsm-mcxe247 https://mcuxpresso.nxp.com/appcodehub?search=an-using-mcxe247-quadspi-module https://mcuxpresso.nxp.com/appcodehub?search=an-mcxe24x-flextimer-example https://mcuxpresso.nxp.com/appcodehub?search=an-mcxe24x-csec-getting-started   Hands-on The following video demonstrates how to import, download, and run an SDK project using MCUXpresso IDE, using the Hello World example as a case study. please see attached video.  
查看全文
GoPoint   GoPoint is a user-friendly application that allows the user to launch preselected demonstrations included in the NXP provided BSP and follows the quarterly release roadmap for BSP How to launch GoPoint     GoPoint Demo On FRDM-IMX93 Board Since FRDM-IMX93 board’s BSP is based on standard BSP release, GoPoint is included in FRDM-IMX93 Yocto build by default. List of 9 demos available on FRDM-IMX93 Board: Image Classification Object Detection Selfie Segmenter i.MX Smart Fitness DMS (Driver Monitor System) ML Benchmark Video Test i.MX Smart Kitchen i.MX E-Bike VIT   Image Classification Demo Image classification is a ML task that attempts to comprehend an entire image as a whole. The goal is to classify the image by assigning it to a specific label. Typically, it refers to images in which only one object appears and is analyzed. This example is using NNStreamer.            Object Detection Demo Object detection is the ML task that detects instances of objects of a certain class within an image. A bounding box and a class label are found for each detected object. This example is using NNStreamer.        Selfie Segmenter Demo Selfie Segmenter showcases the ML capabilities of i.MX 93 by using the NPU to accelerate an instance segmentation model. This model lets you segment the portrait of a person and can be used to replace or modify the background of an image. This example is using NNStreamer.         i.MX Smart Fitness Demo i.MX Smart Fitness showcases the i.MX' Machine Learning capabilities by using an NPU to accelerate two Deep Learning vision-based models. Together, these models detect a person present in the scene and predict 33 3D-keypoints to generate a complete body landmark, known as pose estimation. From the pose estimation, the application tracks the 'squats' fitness exercise.          DMS (Driver Monitor System) Demo This application showcases the capability of implementing DMS on i.MX 93 platform, and the performance boost brought by Neural Processing Unit (NPU). DMS uses four ML models in total to achieve face detection, capturing face landmark and iris landmark, smoking detection and calling detection.         ML Benchmark Demo This example is based on benchmark_model tool in Tensorflow Lite framework, which allows to easily compare the performance of TensorFlow Lite models running on CPU (Cortex-A) and NPU.   Video Test Demo This is a simple demo that allows users to play back video captured on a camera or a test source. It’s based on gstreamer pipeline.            i.MX Smart Kitchen Demo i.MX Smart Kitchen showcases the Multimedia capabilities of i.MX to emulate an interactive kitchen through a GUI controlled by voice commands. The GUI is based on LVGL (Little Versatile Graphic Library) and NXP's Voice Intelligent Technology (VIT) supports the voice commands. Usage: Keyword + command       i.MX E-Bike VIT Demo i.MX E-Bike VIT showcases the Multimedia capabilities of i.MX to emulate an interactive ebike through a GUI controlled by voice commands. The GUI is based on LVGL (Little Versatile Graphic Library) and NXP's Voice Intelligent Technology (VIT) supports the voice commands. Usage: Keyword + command         Useful Link GoPoint User Guide: https://www.nxp.com/webapp/Download?colCode=GPNTUG GoPoint repo: https://github.com/nxp-imx-support/nxp-demo-experience-demos-list/tree/lf-6.6.36_2.1.0 (Including source code of demo: Selfie Segmenter, DMS, ML benchmark, Video test) Image Classification/Object Detection: https://github.com/nxp-imx/eiq-example/tree/lf-6.6.36_2.1.0 i.MX Smart Fitness: https://github.com/nxp-imx-support/imx-smart-fitness i.MX Smart Kitchen: https://github.com/nxp-imx-support/smart-kitchen i.MX E-Bike VIT: https://github.com/nxp-imx-support/imx-ebike-vit
查看全文
Prerequisites  Hardware  FRDM-RW612 evaluation board  USB-C Cable Software Visual Studio Code VS Code Serial Terminal Software: Tera Term You can use any serial terminal you have, but we are using Tera Term for the training slides Step by Step instructions document is here Step by Step video:    
查看全文
Prerequisites  Hardware  FRDM-RW612 evaluation board  USB-C Cable Mobile phone (Android or IOS) Software Visual Studio Code VS Code Serial Terminal Software: Tera Term You can use any serial terminal you have, but we are using Tera Term for the training slides IoT Toolboox App Available for Android and iPhone app stores. Step by Step instructions document is here Step by Step video:
查看全文
Prerequisites  Hardware  FRDM-RW612 evaluation board  USB-C Cable Software Visual Studio Code VS Code Serial Terminal Software: Tera Term You can use any serial terminal you have, but we are using Tera Term for the training slides LCD-PAR-S035 display  Step by Step instructions document is here  Step by Step video:
查看全文
In this lab, you will learn how to: Load wireless module into board Bring-up Bluetooth + 802.15.4 firmware Initialize the 802.15.4 interface on the FRDM-i.MX93 board. Configure and bring up the 802.15.4 interface. Create a thread network. Add nodes to the thread network. Verify thread network connectivity. Exchange data between thread nodes.   OpenTread Hands-on Demo Guide  Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
查看全文
  The FRDM i.MX 8M Plus development board is a low-cost and compact development board with NXP i.MX 8M Plus applications processor. On-board NXP IW612 Tri-Radio module supports Wi-Fi 6 + Bluetooth Low Energy 5.4 + 802.15.4. NXP releases Debian every six months and releases Yocto every year for this board. The FRDM i.MX 8M Plus development board is ideal for developing modern Industrial and IoT applications.   Get to know FRDM-IMX8MPLUS Development Boaard     Specifications 4× Arm® Cortex®A53 + 1× Arm Cortex-M7 LPDDR4 32-bit 4GB eMMC 5.1, 32GB QSPI NOR flash, 32 MB Power Management IC (PMIC) MicroSD 3.0 card slot One USB 3.0 Type-C connector One USB 2.0 Type-C for debug One USB 3.0 Type-A connector One USB Type-C PD only Onboard Wi-Fi® 6 + Bluetooth® LE 5.4/802.15.4 module Optional M.2 Key-E for Wi-Fi/ BT/802.15.4 M.2 Key-M for SSD Multiple display interface:     MIPI-DSI connector 2x4 data lane LVDS w/ Backlight HDMI connector Two MIPI-CSI connectors One 2x5 Pin NXP custom interface with: One CAN port I2C expansion Two 1 Gbps Ethernet Port0 supports POE Port1 supports TSN External RTC with coin cell connector 40 pin (2 x 20) expansion I/O     Feature FRDM-IMX8MPLUS eMMC 32GB DRAM Micron 4GB PMIC PCA9450C WiFi Module u-blox MAYA-W276 on-board USB Type-C+Type-A ENET 2xGbE M.2 (Key E) SDIO WiFi / BT Y (rework needed) M.2 (Key M) PCIE Y HDMI Y MIPI DSI Panel 22 Pins FPC HDR LVDS Panel 40 Pins 2mm HDR MIPI CSI camera 22 Pins FPC HDR 2x20 Expansion Interface Y CAN BUS Y MicroSD Y UART Y Audio WM8962B Remote Debug N NXP Connector (CAN, I2C) Y Power Connector Type-C PCB layers 6 Board DIM 12x13cm       NXP Devices On-Board PMIC PCA9450C USB PD TCPC PHY IC PTN5110 High-Voltage USB PD Power Switch NX20P5090UK I2C  Extends  GPIO PCAL6416A USB3.0 Switch CBTL02043A I2C Repeater PCA9509PDP Bi-directional Level Shifter NTS0104 CAN Transceiver TJA1051T/3 USB Sink & Source combo power switch NX20P3483UK USB Type-C CC and SBU Protection IC NX20P0407 Real-time clock/calendar PCF2131 Wi-Fi, BT, 802.15.4 Tri-Radio IW612 (in u-blox Module)     Expansion Boards RPI-CAM-MIPI: IAS camera to 22 Pins FPC camera adapter Waveshare 7'' DSI LCD: 7inch Capacitive Touch, 1024×600 DY1212W-4856 TFT LCD panel with LVDS interface: 12.1" (WXGA) TFT LCD panel with LVDS interface ​8MIC-RPI-MX8: 8-microphone array proto board for voice enablement   Trainings   Generic FRDM-IMX8MPLUS Software Release Deploy Android14 on FRDM-iMX8MP Lf6.6.36   Useful Links −i.MX Yocto Project User’s Guide​ −i.MX Linux User’s Guide ​−i.MX Linux Reference Manual​ −i.MX Porting Guide -i.MX Debian Linux SDK User Guide
查看全文
In this lab, you will learn how to: Load wireless module into board Bring-up Bluetooth The bring-up of 802.15.4 Initialize the 802.15.4 interface on the FRDM-i.MX91 board. Configure and bring up the 802.15.4 interface. Create a thread network. Add nodes to the thread network. Verify thread network connectivity. Exchange data between thread nodes.   OpenTread Hands-on Demo Guide Video   Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
查看全文
Getting Started Video:   This guide provides step-by-step instructions on how to verify successful communication with the Ara240 module and the runtime software environment to interface  with the FRDM i.MX 95 development board.   Out of the Box   Get Familiar with the Ara240 Module   Ara240 Module [Top view] Ara240 Module [Back view]                Connecting the M.2 Module   This section explains how to connect Ara240, a discrete module, to the FRDM i.MX 95 development board. The instructions in the FRDM i.MX 95 Quick Start Guide will walk you through the boot-up process for the pre-loaded Embedded Linux image on the board and how to connect the USB debug cable. For additional details, see the official FRDM i.MX 95 Development Board documentation. References: FRDM i.MX 95 Quick Start Guide FRDM i.MX 95 Development Board product page FRDM i.MX 95 getting started page Getting Started with ARA2-M2-16G-GT Follow the steps below to connect the Ara240 module to the FRDM i.MX 95 development board: Important: Ensure the board is powered off before making any connections. Insert the Ara240 module into the M.2 Key-M socket on the FRDM i.MX 95 development board. Using the screw provided, secure the module. Connect the fan cable to the board’s fan header (refer to the FRDM i.MX 95 board documentation for the exact header location). Connect the Ara240 to the FRDM i.MX 95 development board.     Power on the Board   Follow the instructions to power on (boot) the board found in the Getting Started with FRDM-IMX95. After powering on, verify that the fan and green LED indicators Ara240 module are on are on.   Get the Software   This section will walk you through the Ara240 Runtime software development kit (SDK), a streamlined subset of the Ara240 SDK designed for rapid enablement and execution on NXP platforms. The Runtime SDK simplifies installation and configuration, enabling developers to quickly deploy and run AI/ML workloads on the Ara240 module with minimal effort. Overview   Refer to Ara240 software release notes for details on the Ara240 software development kit (SDK) The Getting Started page for Ara240 only outlines usage on specific i.MX development platforms For any other platforms please reach out to your NXP representative for guidance.   Module Enumeration and Software Configuration   This section provides instructions to verify proper installation of Ara240 module and configuration of the Ara240 Runtime SDK on the FRDM i.MX 95 development board. Verify Device Detection   Once the board has successfully booted, connect to the serial debug port to monitor system logs. To confirm that the Ara240 module is being detected by the board, run the following command: $ lspci | grep 1e58   Expected output: 0000:01:00.0 Processing accelerators: Device 1e58:0002 (rev 02)   Enable Ara240 device   For quick enablement, the Ara240 Runtime SDK starts at boot time. Refer to the Ara240 Runtime SDK documentation for detailed instructions and environment setup steps.   Developer Experience   This section provides an overview of Ara240 runtime software enablement using the FRDM i.MX 95 development board. Verify Setup Environment   Use the following guidance on how to connect required devices. For most of the demos, you would need a camera, keyboard, mouse, internet connection and a HDMI display monitor. Setup preparation for FRDM i.MX 95 board [Top view]   Setup preparation for FRDM i.MX 95 board [Back view]   NOTE: You might need to use a USB hub to connect keyboard, mouse and camera at the same time.   Runtime setup Description:   Runtime SDK delivers a complete runtime environment that enables AI/ML acceleration on the Ara240 module. To run demo applications, ensure that the Ara240 bring-up process has been successfully completed and the system is ready for demo evaluation. Refer to the Runtime SDK documentation for detailed guidance on: Verifying correct installation of the Runtime SDK. Checking and updating the Ara240 firmware version. Validating proxy service bring-up status. Executing benchmark tests on Ara240. Following these steps ensures that the module is properly initialized and ready for use. Ara240 supports the execution of CNNs, LLMs, VLMs, and agentic frameworks, enabling advanced AI workloads to run directly on Ara. For comprehensive examples and end-to-end workflow guidance, please refer to the Ara SDK documentation page.
查看全文
Customer may want to deploy Android 14 on FRDM-iMX8MP. This doc gives an introduction about how to deploy Android OS14 on FRDM-iMX8MP   Hardware: FRDM-iMX8MP, Power supply cable, usb cable x2,  Ubuntu PC Outline: Follow the below steps: Setup the Android 14 source environment based on LF6.6.36. Apply FRDM-iMX8MP patches in kernel, uboot, mkimage, and device directory. Build the image for FRDM-iMX8MP Flash the image   1. Setup the environment On the Linux PC, set up the Android Source environment according to Section 2- Section 3 from the Android User’s Guide Rev. android-14.0.0_2.1.0 and do not build the image yet. $ cd ~ (or any other directory you like) $ tar xzvf imx-android-14.0.0_2.1.0.tar.gz To generate the i.MX Android release source code build environment, execute the following commands: $ source ~/imx-android-14.0.0_2.1.0/imx_android_setup.sh Prepare the build environment for U-Boot and Linux kernel. This step is mandatory because there is no GCC cross-compile tool chain in the one in AOSP codebase. An approach is provided to use the self-installed GCC cross-compile tool chain for both AArch32 and AArch64. Change to the top-level build directory and set up the environment for building. This only configures the current terminal $ cd ${MY_ANDROID} $ source build/envsetup.sh 2. Apply FRDM-iMX8MP patches into AOSP   Apply the patch in device/nxp, copy all the patches into android_build/device/nxp, and then running the command: $ git apply --check 0001-device-nxp-add-FRDM-i.MX8MP-Android14-basic-support.patch $ git apply 0001-device-nxp-add-FRDM-i.MX8MP-Android14-basic-support.patch Apply the patches in uboot, copy all the patches into android_build/vendor/nxp-opensource/uboot-imx, and then running the command: $ git am *.patch Apply the patches in kernel, copy all the patches into android_build/vendor/nxp-opensource/kernel-imx, and then running the command: $ git am *.patch Apply the patch in mkimage, copy all the patches into android_build/vendor/nxp-opensource/ imx-mkimage, and then running the command: $ git am *.patch     3. Build the image for FRDM-iMX8MP Execute the Android lunch command: $ lunch frdm_8mp-trunk_staging-userdebug Execute the imx-make.sh script to generate the image. $ ./imx-make.sh -j4 2>&1 | tee build-log.txt NOTE: The following outputs are generated by default in ${MY_ANDROID}/out/target/product/frdm_8mp:   4. Flash the image The board image files can be flashed into the target board using Universal Update Utility (UUU). For the UUU binary file, download it from GitHub: uuu release page on GitHub.  To achieve more flexibility, two script files are provided to invoke UUU to automatically flash all Android images. uuu_imx_android_flash.sh for Linux OS uuu_imx_android_flash.bat for Windows OS For this release, these two scripts are validated on UUU 1.5.179 version. Download the corresponding version from GitHub: For Linux OS, download the file named uuu. For Windows OS, download the file named uuu.exe. Perform the following steps to download the board images: Download the UUU binary file from GitHub as described before. Install UUU into a directory contained by the system environment variable of "PATH". Make the board enter serial download mode. Change the board's SW5 (boot mode) to 0001 (from 1-4 bit) to enter serial download mode. Power on the board. Use the USB cable to connect the USB 3.0 dual-role port (with silkprint "PORT1") on the board to your host PC. On the Linux system, open the shell terminal. For example, you can execute a command as follows: $ sudo ./uuu_imx_android_flash.sh -f imx8mp -p frdm -a -e On the Windows system, open the command-line interface in administrator mode. The corresponding command is as follows: $ uuu_imx_android_flash.bat -f imx8mp -p frdm -a -e NOTE: If you want to change the dtb, you can add -d dtb_feature. Also, you can check all the info by using the command: uuu_imx_android_flash.bat Power off the board and Change the board's SW5 (boot mode) to 0010 (from 1-4 bit) to enter emmc boot mode
查看全文
Hands On This hands-on describes how to run the Low Power Reference Design demo on FRDM-MCXW23. Two low-power reference design applications are provided in the reference design folder for the MCXW23: Low power peripheral application demonstrating the low power feature on an advertiser peripheral Bluetooth LE device. Low power central application demonstrating the low power feature on a scanner central Bluetooth LE device. These applications aim at providing: A reference design application for low power/timing optimization on a Bluetooth Low Energy application. These can be used in first intent for porting a new application on low power. A way for measuring the power consumption, wake-up time, and active time in various power modes. The default low-power mode used in different modes are shown as follows: CM33 (core main power domain) and RADIO (core radio power domain) could be active in of the state as follows: – Sleep mode – Deep-sleep mode – Power-down mode – Deep-power down mode CM33 is woken up (core wake-up power domain) and performs system initialization and some pre-processing RADIO woke-up and transceiver are ready to operate. If the software allows, the CM33 can enter in Inactive mode: The transceiver is performing one or more RX/TX sequences CM33 is processing the received or transmitted packets The transceiver is put back in Sleep mode CM33 enters low-power (Deep-sleep mode)   Running the Health care IoT reference design application Once the MCXW23 device is programmed with the low-power reference design demo project, and after a power cycle, it starts to advertise every 1000 mS as soon as the hardware and software initializations are completed. When advertising stops the main domain and radio domain will go to Deep-sleep mode. The MCU stays in this mode until the wake-up from one of the wake up sources. By default, the wake up sources are the wake up button, timer IRQ watchdog IRQ. At wake-up, the device starts to advertise immediately, just like waking up from a Power-On-Reset. Running the low-power central reference design application   The application behavior is as follows: At POR, start scanning immediately, scanning stops on connection establishment. It establishes automatically a connection with a low-power reference design application (lp refdes app) or a temperature sensor by checking the temperature sensor service's UUID in the advertising message and retrieves the temperature value. Note that Low Power Reference Design needs to connect to the peripheral application having an RSSI value lower than the threshold, to accomplish this try to keep the boards close to each other at the beginning. On disconnect, the Application core and radio core go to Deep Sleep mode with full RAM retention. If gAppRestartScanAfterConnect is set to 1, the radio core restarts the scan activity. Application core still goes to Deep Sleep mode between messages from CM3. SW2 button has no effect. Shell over LPUART peripheral outputs scanning, connection information, and temperature value.   Hardware Requirements   FRDM-MCX23 Board x 2 Personal Computer Type C USB Cable x 2 Ammeter to measure current (Optional)   Software Requirements   IDE: Visual Studio Code 1.91.1 SDK: SDK v2.16.100 for FRDM-MCXW71 SPSDK Tool Windows OS (It was used Windows 10 for this hands-on) NXP IoT Toolbox (For Android or iOS device) Hardware changes to measure current In order to measure the current consumption in FRDM-MCX23 we have the following options: Measure current in JP4. This will give you the overall consumption of the board, but this will not require hardware modifications. Measure current in JP1. This is the current for peripheral circuits in the board. For this option JP1 must be populated and SH200 must be cut. Measure current in JP2. This is the MCU current consumption. For this option JP2 must be populated and SH201 must be cut.     For this hand on we will measure current in JP2 to get the MCU consumptions in low power.   Note: In order to make downloads in NXP website, it is necessary to have an account. Please, register and log-in for moving forward. MCUXpresso for Visual Studio Code MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. The extension enables NXP developers to use one of the most popular embedded editor tools and provides an easy and fast way to create, build and debug applications based on MCUXpresso SDK or Zephyr projects.               Install it following the next steps: Download Visual Studio Code from Microsoft Store or visual studio code web page Download Visual Studio Code - Mac, Linux, Windows Access to vscode for MCUX wiki and download MCUXpresso Installer  Dependency Installation · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub Run MCUXpresso Installer and for this Hands On install at least MCUXpresso SDK Developer Arm GNU Toolchain PEmicro   Installing the FRDM-MCXW23 SDK v 25.06.00. Each MCU has its own SDK that includes driver, examples, middleware, docs and other components. To get and build the demo, let’s install the SDK into VS Code:        Once MCUXpresso for Visual Studio Code is installed open VS Code. Go to MCUXpresso for VS Code extension that is on the tools column at the left. Look for INSTALLED REPOSITORIES option and press ‘+’. Detail steps are described in                                                    Use the steps for import a remote Git repository wiki page. Working with MCUXpresso SDK · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub Search for Revision v25.06.00 or newer and complete installation.   Installing SPSDK. The SPSDK is a unified, reliable, and easy to use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment. The library allows the user to connect and communicate with the device, configure the device, prepare, download, and upload data including security operations. Follow next steps for installation: Create python virtual environment. Open a Command Prompt window Write  python -m venv <name>​ Active the virtual environment: cd <name> cd Scripts activate Make sure that your prompt starts with the selected “<name>”                                                                         Install SPSDK from Github into your Python virtual environment. pip install -U spsdk Wait until the installation is completed. From now on you can use the virtual environment when it is needed, just open cmd open the Scripts or bin folder and write activate as in previous steps. Make a Full flash erase using Blhost SPSDK. Open SPSDK virtual environment Open a command prompt Change directory to open Scripts folder under SPSDK virtual environment Write activate Make sure your prompt starts with virtual environment name                                                              Move command prompt to Virtual environment folder                                                                                          Open Device Manager to check the MCU-Link COM                                                                                                        In your board set the jumpers JP13 and JP14 to connect pin 2 to 3.                                                                          Plug your board to your computers USB port, then press SW3, while keep pressing SW3 press Reset button (SW1) for a second, then make sure to release SW1 first, then release SW5.                                                                                                                                                   Use Blhost command to make sure board communication is set up correctly                             a. >blhost -p comxx get-property 1 ​   7. Use this Blhost command to erase your on-board flash                                                               b. >blhost -p comxx flash-erase-all ​   8. Restore JP13 and JP14 to connect to pin 1 to 2   Section 1. Run Low Power Reference Design Open VS code Go to MCUXpresso for VS Code extension that is on the tools column at the left. Go to PROJECTS section and select “Import Example Application from and Installed Repository”                                                                                                                                                                                               Select “frdmmcxw23_health_care_iot_peripheral_bm” project as in the next image and create the project                                                                                                                                          Repeat previous step for “frdmmcxw23_health_care_iot_central” Go back to Projects view and build the projects clicking “Build Selected” icon                                         Connect USB cable to MCU-LINK (J10) connector on both boards Open a Serial terminal on PC for the serial device with these settings on the two boards: - 115200 baud rate - No parity - One stop bit - No flow control To identify the appropriate COM, open the Device Manager and look for MCU-Link VCom Port                                                                                                                                                                                                        9. Select “frdmmcxw23_health_car_iot_central” and click on debug to flash the code into one board   Click on “Continue” button or press “F5” key on your keyboard to continue running the downloaded program on device. 11. Click on “Stop” button or press “Shift + F5” to terminate the debug session.        12. Open a Serial terminal on PC for the serial device with these settings on the two boards: - 460800 baud rate - No parity - One stop bit - No flow control To identify the appropriate COM, open the Device Manager and look for MCU-Link VCom Port 13. Repeat the steps from 9 to 11 with the "frdmmcxw23_health_care_iot_peripheral_bm" project into the second board Clean serial terminals Click SW1 button to reset the central board. Click SW5 button to start the Health care IoT peripheral demo. In the terminal you will see that the boards are communicating each other each second after the boards stablish connection. Central Device Peripheral Device       As expected the Peripheral device connects to the central device send the temp information. The peripheral device will keep advertising each second to report temperature and battery status, after this time it goes to Deep sleep mode. The next step is to measure the current, connect the ammeter on JP2 in the peripheral device. Figure 1 measuring an advertising interval Figure 2 Board after pressing sw5 Figure 3 Board init services and start advertising until central scan connection You can have more information about the Reference application Health Care IoT Central/Peripheral and how to modify the project to change adv interval or disable services on the application note: AN14659 MCX W23 Bluetooth Low Energy Power Consumption Analysis  
查看全文
Hands On  Goal of this lab is to show the SDK example implementing the wireless UART profile and we will move forward in making some meaningful modifications to the example itself with the goal to show where in the code the end user should enter the relevant application software for the application.    Hardware Requirements  Personal Computer  FRDM-MCXW23 Board   Type C USB Cable    Smartphone    Software Requirements  IDE: Visual Studio Code 1.91.1  SDK: SDK v2.16.100 for FRDM-MCXW23  SPSDK Tool  Windows OS (It was used Windows 10 for this hands-on)  NXP IoT Toolbox (For Android or iOS device)  Terminal program, like PuTTY or Tera Term  Note:  In order to make downloads in NXP website, it is necessary to have an account. Please, register and log-in for moving forward.  MCUXpresso for Visual Studio Code  MCUXpresso for Visual Studio Code (VS Code) provides an optimized embedded developer experience for code editing and development. The extension enables NXP developers to use one of the most popular embedded editor tools and provides an easy and fast way to create, build and debug applications based on MCUXpresso SDK or Zephyr projects.   Install it following the next steps:  Download Visual Studio Code from Microsoft Store or visual studio code web page Download Visual Studio Code - Mac, Linux, Windows  Access to vscode for MCUX wiki and download MCUXpresso Installer  Dependency Installation · nxp-mcuxpresso/vscode-for-mcux Wiki · GitHub  Run MCUXpresso Installer and for this Hands On install at least  MCUXpresso SDK Developer  Arm GNU Toolchain   PEmicro    Installing the FRDM-MCXW23 SDK v25.06.00.  Each MCU has its own SDK that includes driver, examples, middleware, docs and other components. To get and build the demo, let’s install the SDK into VS Code:   Once MCUXpresso for Visual Studio Code is installed open VS Code.  Go to MCUXpresso for VS Code extension that is on the tools column at the left.  Look for INSTALLED REPOSITORIES option and press ‘+’. Detail steps are described in                                     -Use the steps for import a remote Git repository                                   -wiki page.               4.Search for FRDM-MCXW23 v 25.06.00 SDK and complete installation.  Section 1. Wireless of simply less wires?  Open VS code   Go to MCUXpresso for VS Code extension that is on the tools column at the left.    Go to PROJECTS section and select “Import Example Application from and Installed Repository”            4.Select “frdmmcxw23_wireless_uart_bm” project as in the next image and create the project    5. Now you should have the “frdmmcxw23_wireless_uart_bm” in your workspace. Build the projects clicking “Build Selected” icon to make sure the build process succeeds with zero errors and warnings.      6. To make sure your board becomes “unique” we need to change the name of it as it appears in the BLE scanning process. To do this we need to modify a line of code in the app_config.c . In some SDK this file is only referenced from the SDK project. To avoid problems with the future projects we need to have selected the Freestanding option when importing the project.   In project explorer go to your project “frdmmcxw23_wireless_uart_bm” and open this explorer to find the “app_config.c” file.    Once opened, browse to line 76 and make the following modification  From  .aData = (uint8_t*)"NXP_WU" to  .aData = (uint8_t*) "Custom_string"   IMPORTANT: Custom_string can be any string that is supposed to be unique in the class (your initials, name of your dog, anything meaningful to you only) Please note the string needs to be 7 characters maximum to avoid any other modifications in the code. In this Lab guide we will modify the string using “NXP_DT”  We will then do the following modification  .aData = (uint8_t*)"NXP_DT" 7. Verify that the modification succeeded by Building the project again and making sure you don’t get any error or warning.   8. Let us, at this point, get familiar with the board and the switches that we need to use to have the application running in the correct way.  The application makes use of two switches, the ROLESW-SW5 (Role Switch) and the SCANSW-SW2 (scan Switch), the establishment of a BLE connection is shown by the CONNLED (connection LED), please refer to the picture below to see where the switches and the LEDs are located on the FRDM-MCXW71 board.    9. Open a Serial terminal on PC for the serial device with these settings on the two boards:   115200 baud rate   No parity   One stop bit  No flow control   To identify the appropriate COM, open the Device Manager and look for MCU-Link VCom Port    10. We are now ready to start evaluating the example, Select “frdmmcxw23_wireless_uart_bm” and click on debug to flash the code into one board    11.Click on “Continue” button or press “F5” key on your keyboard to continue running the downloaded program on device.     You will immediately start noticing two things, the RGB LED (showing white color) and the BLUE LED on the board will start blinking at the same rate and you will see the “Wireless UART Starting as GAP Central” on the terminal.    12. The microcontroller is acting at this stage with the role that your smartphone is supposed to take in the example, to change the role click now the ROLESW=SW4 on the board to change the role to peripheral, the “switched role to GAP Peripheral” message on the terminal should be shown       13. It is now time to make the board visible to a Bluetooth scan, to do this press once the SCANSW=SW2 switch, you should notice now the RBG LED on the board stops blinking and only the CONNLED will continue. The “Advertising…” message should be now prompted on the terminal     14. It is time now to access the IoT Toolbox app on your smartphone and select Wireless UART    15. Once you click on “Wireless_UART” you should see a list of Wireless UART compatible devices advertising in that moment in the region around you (only the one under use at this stage in the picture below identified by NXP_DT)    16. If everything went correctly the BLE communication is in place, and you will observe the following three conditions: A. The BLUE LED on the board becomes solid blue  B.The terminal will report the communication is in place by prompting “Connected to device 0 as peripheral”    C. The screen on your app will look like the following, please note the DICONNECT button at the top right of the screens that shows your smartphone is connected to the FRDM board     17. Type any character(s) into the text box on the IoT toolbox and press the Send button to wirelessly transmit character between the App and the MCXW71 device. Every character you will send from the app will be prompted on the console. At this point we have verified the basic way of working of the Wireless UART app that comes as part of the device’ s SDK.   Congratulations you have reached the end of the first part of the lab, you can now close the IoT Toolbox app on your smartphone and click on Terminate to stop debugging the application on the MCXW23 board.  18. It is now time to make some modifications on out of the box example to add additional interactions between the app and the board at hardware level, the goal is to become more familiar with the software stack in use and the available hardware resources.   As first step, we need to identify the right file where we will incorporate the modifications, the file we need to work on is called wireless_uart.c, same as with app_config.c this file is in the SDK folder so to avoid modifications on the SDK source we have to had imported the example as a freestanding application as show in the first parb of the lab. In window explorer go to your project “frdmmcxw23_wireless_uart_bm” and open the explorer to find the “wireless_uart.c” & “wireless_uart.h” files.      19. In the wireless_uart.c file we need to add the declarations, variables and includes to configure the LEDs commands. Let us start with the variables declarations, somewhere around line 267 (doesn’t really matter the exact number of the line you add the declaration on) add the following lines:  uint8_t command_uart; uint8_t command_lenght; 20. We now need a more complex function to be declared to handle the LED’s behavior as well as the initialization of the ports and pins used, we will command the RGB LED located on the FRDM-MCXW23 board. In the Public functions section of the file (around line 271) place the following commandLed() function (use the copy_and_paste.txt file provided for this lab to avoid any formatting issues)    static void command_led(void) {     if( (command_uart >= '0' && command_uart <= '4') && (command_lenght <= 2))     {         switch(command_uart)         {             case '0':                     GPIO_PortClear(GPIO, 0U, 1<<0); //Turn on Green LED                     GPIO_PortClear(GPIO, 0U, 1<<1); //Turn on Red LED                     GPIO_PortClear(GPIO, 0U, 1<<4); //Turn on Blue LED                 break;             case '1':                     GPIO_PortSet(GPIO, 0U, 1<<0); //Turn off Green LED                     GPIO_PortClear(GPIO, 0U, 1<<1); //Turn on Red LED                     GPIO_PortSet(GPIO, 0U, 1<<4); //Turn off Blue LED                 break;             case '2':                     GPIO_PortClear(GPIO, 0U, 1<<0); //Turn on Green LED                     GPIO_PortSet(GPIO, 0U, 1<<1); //Turn off Red LED                     GPIO_PortSet(GPIO, 0U, 1<<4); //Turn off Blue LED                 break;             case '3':                     GPIO_PortSet(GPIO, 0U, 1<<0); //Turn off Green LED                     GPIO_PortSet(GPIO, 0U, 1<<1); //Turn off Red LED                     GPIO_PortClear(GPIO, 0U, 1<<4); //Turn on Blue LED                 break;             case '4':                     GPIO_PortSet(GPIO, 0U, 1<<0); //Turn off Green LED                     GPIO_PortSet(GPIO, 0U, 1<<1); //Turn off Red LED                     GPIO_PortSet(GPIO, 0U, 1<<4); //Turn off Blue LED                 break;             default:             break;         }     } } 21. To make use of the instructions that manipulate the GPIOs in the wireless_uart.c file we need to make sure they are reachable from the file itself, we ensure this with the following include statement which needs to be added in the include file section of the wireless_uart.c file (around line 30)  #include "fsl_gpio.h" 22. It is now necessary to call the above defined commandLed function in the whole BLE software flow, and, in particular it needs to be called in the BleApp_ReceivedUartStream function defined in the wireless_uart.c files somewhere around line 1440. Include then the commandLed() function just after the following line(s) of code (highlighted in yellow the function to be added and the position)   #if (defined(SERIAL_MANAGER_NON_BLOCKING_MODE) && (SERIAL_MANAGER_NON_BLOCKING_MODE > 0U)) serial_manager_status_t status = SerialManager_InstallTxCallback((serial_write_handle_t)s_writeHandle, Uart_TxCallBack, pBuffer); (void)status; assert(kStatus_SerialManager_Success == status); (void)SerialManager_WriteNonBlocking((serial_write_handle_t)s_writeHandle, pBuffer, streamLength); #endif /*SERIAL_MANAGER_NON_BLOCKING_MODE > 0U*/ } command_led(); /* update the previous device ID */ previousDeviceId = peerDeviceId; } 23. As last modification we need to ensure the commands sent by the user through the IoT toolkit App are correctly captured in the application. Locate the BleApp_GattServerCallback function in the wireless_uart.c file and add the two lines highlighted in yellow below considering the exact position in the code      static void BleApp_GattServerCallback ( deviceId_t deviceId, gattServerEvent_t *pServerEvent ) { uint16_t tempMtu = 0; switch (pServerEvent->eventType) { case gEvtAttributeWrittenWithoutResponse_c: { if (pServerEvent->eventData.attributeWrittenEvent.handle == (uint16_t)value_uart_stream) { command_uart=*pServerEvent->eventData.attributeWrittenEvent.aValue; command_lenght = pServerEvent->eventData.attributeWrittenEvent.cValueLength; BleApp_ReceivedUartStream(deviceId, pServerEvent->eventData.attributeWrittenEvent.aValue, pServerEvent->eventData.attributeWrittenEvent.cValueLength); } break; } case gEvtMtuChanged_c: { /* update stream length with minimum of new MTU */ (void)Gatt_GetMtu(deviceId, &tempMtu); tempMtu = gAttMaxWriteDataSize_d(tempMtu); mAppUartBufferSize = mAppUartBufferSize <= tempMtu ? mAppUartBufferSize : tempMtu; } break; default: { ; /* No action required */ } break; } }   24. We are now done with the code modifications, let us repeat the steps we need to build, Debug and connect through the IoT Toolkit Wireless UART option to see if the modifications are working as expected. Once you are connected to the FRDM-MCXW23 board through the App you can enter, as done before, any character and it will be prompted back through the terminal, now, entering 1 will turn the RBG RED LED on, 2 will turn the RGB BLUE LED on, 3 will turn the RGB GREEN on, 0 will turn the RBG LED white and 4 will turn the RBG LED off.     NOTE: you can see from the code, in the commandLed() function that we are setting up and configuring the GPIOs every time the UART receives the characters, 1, 2, 3 or 0.     BONUS: Change the code and use/add other trigger commands. Change the LED colors you can showcase. Send messages though UART once a special character (or a combination of them) is received.   Congratulations, you have reached the end of the Wireless or simply less wires. 
查看全文
This document is intended to guide you in the installation of the necessary tools and repository for start running matter examples and development. Matter (previously known as Project CHIP) is a single, unified, application-layer connectivity standard designed to enable developers to connect and build reliable, secure IoT ecosystems and increase compatibility among Smart Home and Building devices. Backed by major brands and developed through collaboration within the Connectivity Standards Alliance (previously known as the Zigbee Alliance), Matter is an open-source royalty-free connectivity standard built with market-proven technologies using Internet Protocol (IP) and compatible with Thread and Wi-Fi network transports. Building solutions and leading standards efforts, NXP provides scalable, flexible and secure platforms for the variety of use cases Matter addresses – from end nodes to gateways – so device manufacturers can focus on their product innovation. NXP’s Matter solutions go beyond just the connectivity with comprehensive capabilities for the compute and security requirements for IoT devices.
查看全文