Connects - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

讨论

排序依据:
A hands-on session to show how to prepare and program device for CSEc security operations. Session also covers both bare metal and SDK approach to program CSEc module.
查看全文
People today face way too many options, especially when it comes to so called smart devices which can easily contain 50+ functional settings. With most people only using a few preferred settings, this session shows product managers, UI designers, and engineers how to leverage NXP’s out of the box Face Rec based Friction Free Interface production grade platform to rapidly add a truly seamless interface to devices such as appliances, home comfort systems, and alarm/safety/security panels, as well as many types of industrial equipment. By recognizing who you are and what you prefer based on past usage, today’s smart machines can tailor their interface to meet end consumer needs person by person (including controlling access) significantly improving customer satisfaction. Wi-Fi and/or connection to the cloud is NOT required to move your interface design to the next level!
查看全文
Emerging Connected and Automated Vehicles (CAVs) require far more compute horsepower, more memory bandwidth, and more high speed IO connectivity than the vehicles in show rooms today. NXP’s highest performance multicore Arm product family (Layerscape) was developed for networking and industrial infrastructure, however their integration and performance per watt has made them attractive in a variety of ‘transportation’ applications, including planes, trains, and now, automobiles. This session will provide an overview of the product family, and its transportation centric use cases.
查看全文
The number of ECUs in a car is increasing dramatically on a year by year basis. Modern cars are starting to introduce the concept of centralizing multiple domains (Infotainment, ADAS, etc.) in a single ECU and separate them using technologies like virtualization, multicore or multiple SOCs. Although separated, these entities need to communicate and implementing a software communication solution which is scalable, portable, open and easy to program is key to offering a complete software enablement to our customers. This session will present NXP software solution for communication within a domain and between domains controllers in an ECU.
查看全文
A key challenge to the deployment of Edge compute IoT is management and security of 1000s to millions of Edge compute nodes. EdgeScale simplifies this by providing a cloud-based management framework leveraging the hardware security features of Layerscape processors. Learn how you can use EdgeScale to manage a heterogenious set of Edge compute nodes, and use it with your choice of Edge compute framework - AWS Greengrass, Azure IoT Edge and others.
查看全文
The session is intended for engineers either getting started or are interested in seeing how to use AUTOSAR MCAL to generate and implement code. “Hello world” level examples are presented using the Tresos configuration tool to generate code which is then used in application code. Examples are based on NXP’s MCAL application provided with the released product.
查看全文
The continued growth of processing capabilities and new features introduced with the ARM®v8 based System-on-Chip has made virtualization a realistic option for embedded system developers. With virtualization, system architects can design solutions that reduce the size, weight, power, and cost of legacy systems by consolidating disparate software functions onto a single chip, even if those different software functions require different operating systems or otherwise incompatible software stacks. Virtualization allows architects to partition and isolate software components with different safety, security, or licensing requirements. The virtual machine manager, or hypervisor, is the key piece of software technology enabling virtualization. Open source hypervisor, Xen, supports the ARMv8 processor family.
查看全文
Explores the fast-growing Automotive Gateway market, identifying key use cases and requirements, and how gateways will evolve over the next decade.
查看全文
Review of NXP’s current CAN portfolio and CAN functions, our support for CAN FD and an overview of the breakthrough products keeping CAN highly relevant for the new generation of vehicles.
查看全文
Join this session to learn about the i.MX 8/8X application processors that offer a natural migration path from the successful i.MX 6 series for industrial and automotive markets. This class will highlight the feature enhancements in CPU performance, graphics, multimedia, audio and connectivity. And will cover the basics on security, machine learning, build and distribution of Linux and Android systems, management of storage devices, graphics and demo settings. You will leave the session with the knowledge on the features of the i.MX 8/8X and how to get up and running quickly on the development boards.
查看全文
Create awareness and understanding of the Service Oriented Architecture. Illustration of concepts and status based on AMP Linux BSP.
查看全文
The GD3100 is a  programmable high-voltage gate driver with advanced functional safety (FuSa), control, and protection features, developed for automotive and eMobility applications. This presentation will give a brief review of HV power devices such as Si IGBTs and WBG MOSFETs. Then the talk will focus on key features of the GD3100 that are important for implementation of high traction inverters, DC/DC converters, or on-board chargers (OBCs) using Si IGBTs or SiC MOSFETs.
查看全文
Designing automotive gateway applications using SDK drivers, software stacks and FreeRTOS.
查看全文
What is new, value proposition against competition, current and future plans for collateral, tools & reference designs; SPIDrive Hbridge, Q100 eSwitch.
查看全文
Design, Software & Services Hands-On Workshop: Design with Embedded Solutions for the Always-On Market Using the New LPC54114 Power-Efficient MCU  DES-N2084 & DES-N1956 Hands-On Workshop: FreeRTOS Solutions for Kinetis MCUs  DES-N1960 Hands-On Workshop Kinetis Enablement  Hands-On Workshop: Securing the IoT One Edge Node at a Time with Kinetis DES-N1931 i.MX 6QuadPlus and i.MX 6DualPlus Applications Processors-Performance-Tier Multicores for Visually Stunning Graphics-Centric Applications  DES-N1940 i.MX 8 Graphics Architecture   Kinetis® MCU Security Technology  Linear Technology: Proven & Scalable Power Solutions for the Latest QorIQ Series Processors  Logic Devices: Case Studies of Practical Examples of Power, Space and Cost Savings with NXP Innovative Logic Solutions Micron Technology: Memory Choices for NXP Microprocessors  Security 101: Introduction to Security Acceleration in QorIQ® Processors  TQ-Systems: How to Speed Up and Optimize Your Design with Modular Approach  USB Type-C Overview  Smart Home & Buildings Bluetooth® Smart Mesh: Simple and Easy-to-Use Low-Power Wireless Networking Protocol Hands-On Workshop: Advanced Thread® Stack Class on Routing, Border Router, Security, Low Power and Commissioning  Hands-On Workshop: Use NFC Pairing to Connect Multiple Bluetooth® and Wi-Fi® Devices with a Simple Tap  How to Choose the Right NFC Solution for Your Use Case Insight & Innovation LPC Microcontrollers Portfolio, Enablement Overview and Roadmap  INS-N1819 Sensor Deep-Dive Demos and Data Collection Techniques  Secure Mobile, Healthcare & Wearables MHW-N1990 Enabling Ultimate Miniaturization and Customization with the Latest Single Chip System Module Technology  MHW-N2009 Hands-On Workshop Develop your IoT and Wearable Applications Instantly with Hexiwear.pdf  MHW-N1917 Wireless Charging Lets You Cut that Cord!  Smart Machinery & Industrial Automation SMI-N1948 Hands-On Workshop - Kinetis Motor Suite.pdf  Smart Networks NET-N1865 Introduction to QorIQ LS1012A - the Worlds Smallest and Lowest Power 64-bit Processor.pdf 
查看全文
Lecture showing and analyzing SqueezeNet CNN classifier demo on S32V234. See how S32V234 can use CNNs to process and classify images in a power-efficient manner.
查看全文
With a number of vehicles being connected to the internet, the need to have a secure environment inside the vehicle is increasing. This session will present secure use cases for edge nodes microcontroller in the vehicle and how the S32K can achieve them. Topics including what is security, NXP 4 layer of automotive security, and S32K CSEc.
查看全文
During this session, we will discuss the new memories supported on the new i.MX8 processor family. For DRAM, this will include DDR4 and Low Power DDR4 (LPDDR4). For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. This year, we will provide additional information on LPDDR4X (X=lower power I/O) as well as eMMC 5.1 high performance features including command queueing, and several new Cache operations. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems.  
查看全文
In the last 10 years, Green Hills has observed carmaker and Tier 1 customers expand from the traditional segments of powertrain, airbags and braking ECUs into graphics-rich dashboards, open source operating sytems and the secure Connected Car. A leading requirement is ECU consolidation while keeping ASIL safety intact. This requires the run-time architecture to safety and securely run guest operating systems Linux or Android on the same single core (or across multiple cores as SMP) alongside safety or security-critical applications like instrument clusters, gateways, V2X and ADAS. Here, we'll take a closer look at the customer’s pain points and goals, and we’ll summarize various industry solutions, including the INTEGRITY Multivisor secure hypervisor.
查看全文