コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
S32 Design Studio 3.0 S32V234 focus on configuration tools pin wizard, clocks config, with SDK configuration, FreeRTOS configuration and use building and running a project showing debug with S32 debugger on the m4 with code on target. Configuration tools suite formed from pins, clocks, peripherals, DCD, IVT are offering a complete view of the platform with complete access to all the details directly from the tool and possibility to generate, build and debug the applications.
記事全体を表示
A deep dive into the pixel processing pipeline of the i.MX 8. Attendees will get a detailed insight into the available accelerators for 2D, 3D, Video, Vision, AI, Capture and Display and how they enable the multimedia and safety features of the eCockpit.
記事全体を表示
I2C master and slave devices are used in many system for various reasons. NXP offers the widest portfolio of I2C devices. This class will introduce the I2C-Bus interface, address some common pitfalls when designing with I2C-Bus, and present solutions to these challenges.
記事全体を表示
Introduction on RCI (Remote Control Interface) for our RF products (Lizard, MantraCS, MantraF). System integration and development made easy using the RCI firmware together with the Configuration Development Kit (CDK).
記事全体を表示
Join this session to get a glimpse of where you will see i.MX 8/8X in the near future and why graphics, ML, AI, video, image processing, vision, connectivity, audio and voice functions make the i.MX 8 series ideal for Automotive and Industrial applications. Learn about the i.MX 8/8X families that are comprised of common subsystems establishing an unmatched range of performance scaling with pin-compatible options and the highest level of software reuse. In addition, learn more about the upcoming i.MX 8DualMax product line to help customers meet additional cost performance scaling across the i.MX 8 family.
記事全体を表示
A hands-on session to show how to prepare and program device for CSEc security operations. Session also covers both bare metal and SDK approach to program CSEc module. The NVM part will cover the enablement/configuration of the different types of memory and tools that NXP provides for calculating the endurance.
記事全体を表示
Introduction to A100x secure authenticators including new A1007, as part of overall training authentication protocols, what to look for in security IC and potential use cases.
記事全体を表示
Introduction to the ISO26262/EC61508 standard - with emphasis on how to apply it, cross BL designing for advanced functional safety requirements- ASIL B/C/D.
記事全体を表示
Attendees will gain knowledge and experience with S32K Cookbook application note examples to enable to enable successful customer designs. All examples will have an overview, and several will be exercised. Attendees must bring their laptop and pre-install S32 Design Studio for Arm.
記事全体を表示
i.MX offers some of the most versatile platforms for multimedia and display applications. Join this session to get an in depth view of how i.MX 8/8X’s multimedia systems, including GPU, Display, Vision, Virtualization and Machine Learning come together to provide customers with a scalable set of powerful media capabilities for auto infotainment.
記事全体を表示
This presentation dedicated to IVI provides an overview of the software and hardware enablement available to accelerate customer time-to-market and reduce development risks. Namely i.MX 8, Ethernet Switch and PHY, audio tuner and amplifier, power management, supported by a Linux Genivi compliant BSP.
記事全体を表示
IoT is all about ‘’Sense, Think and Act’’. Automation systems and decision making algorithms running in the Cloud or on the Edge need to be fed with the right data, actuators must be integrity protected and receive valid commands. Moreover data protection, Privacy and protection of business models become paramount to any IoT deployment. NXP’s new generation of embedded Secure Element SE050 redefines security and trust anchoring in IoT devices. Part of NXP’s ’Plug & Trust‘ solutions delivering security right out of the box, the new SE050 is the convergence between integrity protection of a trusted IoT platform, flexible and secured connections of edge to multiple Cloud services, and secure sensing. In this session the new SE050 security enclave for IoT devices will be introduced, along with the new use cases it enables for edge sensors as well as gateways and edge computing platforms.
記事全体を表示
Overview of NXP’s General Purpose and Integrated Solutions (GPIS) Portfolio with focus on the S32K and S32M (MagniV) products.  
記事全体を表示
The autonomous vehicle of the future will set new requirements on safety, reliability and dependability. In this talk we will review resulting requirements on vehicle architectures of the future and how they will be enabled by Smart Actuators.
記事全体を表示
Learn about the key technical features of our general purpose microcontroller family integrating Arm® Cortex®-M4F or M0+ cores. This session will provide a general overview around scalability, low-power, security, safety, software and solution buildup to help accelerate our customer’s time to market on automotive and ultra-reliable applications.
記事全体を表示
The automotive industry is rapidly evolving and the car is being transformed from a simple mode of transport to a personalized mobile information hub. All these new electronic functions bring great benefits to the driver, increasing comfort, convenience, safety and efficiency. But these features come with new risks, too. Modern vehicles feature wireless interfaces connect the in-vehicle systems of these ‘Connected Cars’ to external networks, which form entry points for hackers. This session will describe a proposal for a layered automotive security architecture providing a defense-in-depth approach to securing a vehicle including secure external interfaces, secure domain isolation, secure internal communication and secure software execution. In addition, the session will describe how all these security layers can be supported through the full vehicle life cycle of design, build, use and scrap.
記事全体を表示
Ethernet adoption in new OEM platforms is accelerating, as a result of increased media, communication, and ADAS streams between different end points in vehicles. The required Quality of Service and synchronization is typically achieved through the implementation of Audio Video Bridging (AVB) specifications, or derivatives of AVB. NXP has a unique position in the market given our capability to offer a full solution for AVB in the car, from end points (MPUs as well as MCUs), PHYs, switches, plus the needed software stacks. In addition, the software stacks are full featured, including critical but often initially forgotten components such as Media Clock Recovery. Get an introduction to the basis of the AVB technology, and how NXP can help you deploy AVB in your products.
記事全体を表示
Learn how to move from physical to virtual network functions (VNFs) on ARM QorIQ platforms using KVM virtual machines and Docker containers with native DPAA2 and virtual virtio devices. Leverage packet processing, crypto acceleration and advanced offloads from DPDK/ODP and Linux native guest applications. Connect VNFs through virtual switching either using optimized user space implementations or offloading datapath into DPAA2 Advanced IO Processor. Make use of the switching functions provided by DPAA2 integrated Edge Virtual Bridge and L2 Switch. Leverage OPNFV integration and take advantage of distributed VNFs via Service Function Chaining.
記事全体を表示
Security is becoming a quintessential topic for any OEM, and possibly for the entire industry, as evolutions of Autonomous drive capabilities are inexorably tied to the ability to secure the car. A number of components in the security architecture of nodes in any vehicle are very close to the SoC, exploiting hardware capabilities to achieve intended functionality. Answering customer needs, NXP is providing a Trusted Execution Environment (TEE) stack, which provides a significant number of security features required by the Automotive needs. Get an introduction to the basis of NXP’s TEE stack, capabilities, and how does this integrates in the typical secure node architecture.
記事全体を表示
A hands-on session to show how to prepare and program device for CSEc security operations. Session also covers both bare metal and SDK approach to program CSEc module.
記事全体を表示