Connects - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

讨论

排序依据:
Learn about the key benefits and target applications of the new K27/K28 MCUs with extra-large embedded memory and power-efficient dual-USB MCUs based on ARM® Cortex-M4® core.
查看全文
Deep dive into the vision processing architecture of the i.MX 8 family. Learn how to access the advanced processing features, the vision SDK, and the vision-based applications enabled by the i.MX 8 processor. This class provides an introduction to understanding the unique way in which machine vision is handled by i.MX 8. It forms a basic introduction class that is a precursor to the more advanced "Call Your Shot!" pool table demo class.
查看全文
This session is for those of you who have never programmed in the Qt Framework. It will guide you through the basics – from setting up the environment to developing two basic applications, a calculator and a thermometer display. You will also have the opportunity to interact with these demos.
查看全文
In electronic systems, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in various customer systems.
查看全文
Get a deep dive into the brand new Vulkan API from Khronos. Learn how the programming paradigms have changed from OpenGL ES, how to use Vulkan API and its enormous performance advantages, and how to unlock the full potential of i.MX 8 series GPUs.
查看全文
Join this session to learn how NXP security technology should be leveraged to secure the onboarding credentials using the LPC54S0xx MCU with state of the art security technology.
查看全文
This session will focus on tire localization: Dual axis sensors enable rotation rate detection and determination of drivers / passenger side in seconds. NogaroE: Enhanced features added to a proven volume production TPMS sensor. Gen 4x4: Next-generation of ultra-low power TPMS sensors in smallest package features increased accuracy and processing power.
查看全文
In the past, auto HMI developers approached the instrument cluster, infotainment system and any other auxiliary driver displays as separate projects, each with their own unique challenges and requirements. With eCockpit HMI developers are tasked with approaching the cluster, IVI system, HUD, rear-seat entertainment and other screens in the vehicle as a single system of displays that have been fragmented within the vehicle and even run on a singular MPU. Examine the requirements for these new integrated cockpit systems. Discuss how design teams can deliver consistent language, look and feel across multiple displays with separate and varied purposes. Talk about the concerns related to safety and certification for system as it applies to a variety of auto standards and reveal how teams can successfully design these systems for a single processor family and reuse across low- high-end auto models.
查看全文
NXP’s end-to-end solution for USB Type-C offers ease-of-use integration into customer designs and includes AC/DC converter for power supplies, PD PHY and CC Logic Controller, direct charging, signal re-drivers, signal switches, load switches and authentication.
查看全文
Expect your platform to boot in less than one second...do your customer's demand it? Even if that is not fast enough for some cases...we will discuss what can be done to improve the booting performance. Learn from the experts on how to architect and optimize the boot process from boot ROM, boot loader through to OS and applications.
查看全文
Systems are complex, and increasing complexity does not translate to product differentiation. Extracting the maximum networking performance, battery life or graphics capability requires knowledge of the underlying silicon and software. Developer resources are tight, and shifting the focus to product development above platform development maximizes return on investment. Freescale has deep enablement technology, comprehensive support and a vibrant ecosystem available to assist getting your product to market quickly. For automotive, consumer, industrial and networking applications, learn how NXP extends the broad technology and support available today with custom access to experts. A brief overview of the products and services available across NXP will be augmented with case studies and expert Q&A.
查看全文
With focus on different applications, this session will highlight both the Kinetis and LPC families. We will present the new members of each family and provide you insight of what you could expect from these families going forward.
查看全文
This session covers NXP virtualization offering on Arm based platforms. The following will be covered: KVM; DPAA2 direct assignment; PCI direct assignment; VIRTIO I/O virtualization; DPDK/ODP enablement in Virtual Machine; VIRTIO IOMMU support for enhanced isolation in Virtual Machine; Linux Containers, Dockers; Libvirt; Performance analysis and optimization; Debugging support; Future plans; Universal CPE devices and SD-WAN forwarders and branch routers.
查看全文
Learn how to go from an IoT idea to a proof-of-concept as easy as 1-2-3 for a connected, secure, small-form factor IoT end node. The Rapid IoT kit integrates 30+ active components (11 NXP parts) with drivers, middleware, example applications and features an innovative web IDE with GUI-based programming, as well as mobile App and IoT cloud services.
查看全文
This class will provide an overview of NXP's broad and scalable MCU portfolio and give details on which product families are available for different markets and use cases. It will also give an overview of the unified tools, software and solutions that enable the portfolio.
查看全文
Learn how to develop a wireless connected product using BLE and/or Thread protocols.
查看全文
Concept of SD-CPE, virtualization of functions/applications on CPE, centralized management of CPE by orchestrator, advantages, and applications scenario in home, enterprise and industry.
查看全文
This session will provide an insight into all the sensor hardware and software tools, enabling customers to reduce their time to market. Find out about all the latest sensor tools and reference designs for IoT (Industrial/Medical) applications.
查看全文
You innovate to make the vehicle autonomous & the most complex node in the Internet of Things. Increasingly functionality from consumer components is needed in your solutions. NXP, the leader in Automotive and high-end compute in Networking, highlights 66 critical differences that may generically exist between automotive and consumer components. Identified by a ZVEI industry workgroup (German Association of Electronics Industry) they impact reliability, quality and lifetime of vehicles. Examples demonstrate how NXP’s capabilities across all product segments and performance ranges reduce your hidden risks providing an excellent starting point towards your autonomous vehicle.
查看全文
This is a highly integrated eLock platform for a rocket start in the Chinese (residential) access market. It features NFC, BLE, fingerprint, keypad entries and can be easily configured using WeChat “mini programs” platform for maximum compatibility with existing cell phones. Learn more about the products behind - NFC controller PN7362AU and BLE controller QN9021 – and how this highly integrated eLock solution can dramatically simplify the configuration for end users.
查看全文