Connects - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

Discussions

Sort by:
Presentation of NXP’s security solution for next-generation automotive SoCs, with a focus NXP solution offering (drivers, tools), functionalities and system design aspects the customers have to consider.
View full article
Learn how NXP provides support for ODP and DPDK without sacrificing performance. Learn how we're leveraging specific acceleration advantages of the NXP data plane architectures, such as packet IO, classification, scheduling, crypto, etc. This session will provide a comparative analysis and evolution of both of these open-source, platform independent and vendor-neutral standard APIs for optimized packet processing and traditional networking services in user space. It will help you choose the right API for your project, based on design requirements.   We will also cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
View full article
Learn about vision processing and technical capabilities of S32V’s dual-APEX acceleration engines, multi-core A53 processors, on-chip image signal processor (ISP) which differentiates S32V from other Arm based processors that can’t meet the same performance/power envelope. Attendees will get a demonstration of the graph tools available on our S32 Design Studio IDE that facilitate the creation of graphs for the APEX and ISP Engines.
View full article
You innovate to make the vehicle autonomous & the most complex node in the Internet of Things. Increasingly functionality from consumer components is needed in your solutions. NXP, the leader in Automotive and high-end compute in Networking, highlights 66 critical differences that may generically exist between automotive and consumer components. Identified by a ZVEI industry workgroup (German Association of Electronics Industry) they impact reliability, quality and lifetime of vehicles. Examples demonstrate how NXP’s capabilities across all product segments and performance ranges reduce your hidden risks providing an excellent starting point towards your autonomous vehicle.
View full article
Expect your platform to boot in less than one second...do your customer's demand it? Even if that is not fast enough for some cases...we will discuss what can be done to improve the booting performance. Learn from the experts on how to architect and optimize the boot process from boot ROM, boot loader through to OS and applications.
View full article
Join us to learn how to develop PCBs of all kinds and the complexity to perform well in harsh environments.
View full article
Many people involved in the electronics industry need a basic knowledge of semiconductor components in order to understand issues like manufacturing cycle time, semiconductor fab consolidation and failure analysis results. This session is geared towards a non-technical audience and gives a high-level overview of semiconductor devices and how they are made. The lecture begins with a brief overview of how semiconductor devices work. The bulk of the presentation describes the generic manufacturing flow for semiconductor devices with an emphasis on the complexity of the equipment/facilities used and the process time required.
View full article
Learn about the key benefits and target applications of the new K27/K28 MCUs with extra-large embedded memory and power-efficient dual-USB MCUs based on ARM® Cortex-M4® core.
View full article
Wireless (802.11) deployments are slated to overtake Ethernet switching revenue by the later part of the decade. Along with that volume, the new 802.11ax standard will deliver a 300% increase in useable performance along with higher density access for schools, airports, stadiums etc. Another driver is the demand for high bandwidth wireless within the home. Come learn about NXP's new Layerscape LA1575 and other innovative, integrated, programmable solutions available to address these increasing demands for wireless performance.
View full article
Adoption of Passive Keyless Entry / Go is growing rapidly, and adding such functionality in the car key introduces challenges for battery life and security. As such, a new class of motion sensor has been developed to address these challenges. In this class, the newest NXP motion sensor, FXLS8962AF, which boasts benchmark power consumption, EMC Class III compliance and full AEC-Q100 qualification is introduced. The sensor has been specifically designed for compatibility with NXP’s all-in-one IC for passive entry keys (i.e. TOKEN), and this class will explain how the two devices are being used together to improve battery life and enhance security in the passive entry system implementation.
View full article
Attendees will learn about modules on the S32K144 though brief tutorials and hands-on software examples. The lab will use NXP’s S32 Design Studio tools including Processor Expert and the S32K SDK. 
View full article
OpenIL is Linux® distro designed specifically for the industrial market. OpenIL is an ideal deployment for PLC, HMI, industrial control and automation systems. As an open source project based on buildroot to provide a compact filesystem for industrial usage, OpenIL supports LTS Linux kernel 4.1 and 4.9, Xenomai cobalt core, industrial IEEE®1588, time sensitive networking and many other features. A real-time baremetal framework supports relay control and robotic applications. Learn about OpenIL, the architecture, design objectives and roadmap. Understand how you can contribute to OpenIL and drive the direction of the community project.
View full article
Lecture to show NXP motor control model based solutions for S32K, MagniV and MPC57xx. Also includes training on BLDC/PMSM motor control using FreeMASTER, MCAT, and MATLAB.
View full article
Ensuring secure deployment of the billions of end nodes is a key enabler for the Internet of Tomorrow. The Kinetis K8x and Kinetis KL8x families are designed to deliver unsurpassed security for multi-application MCUs with hardware features such as Trust, Cryptographic acceleration, and Anti-Tamper to deliver a scalable, secure platform for embedded developers. This hands-on session will cover the needs of secure embedded applications, performing encrypted firmware updates, utilizing hardware cryptographic accelerators and extending trusted execution to external memories using an on-the-fly AES decryption module. Join this session to learn how your customers can get started creating their next secure node design.
View full article
The session will introduce an upcoming xEV traction motor power inverter platform system-play solution featuring a new MCU, new IGBT gate driver, and new safe SBC bound together with system enablement software and ASIL-D compliant safety support. A fully functional traction motor reference design being designed by partner Vepco will also be introduced based on a Power IGBT Module from Fuji Electric. The session will describe the platform’s components, software structure, value proposition, enablement support and go-to-market approach to help enhance understanding of the application and NXP solution as well as how to sell the system platform.
View full article
This class provides an introduction on the S32 Design Studio for Vision IDE with integrated Vision SDK in the development of vision processing applications for the S32V234 automotive vision processor. The lecture will overview the user interfaces of the S32DS IDE and the ISP and APEX2 Visual Graph Tools. The demonstration will cover the S32 Design Studio for Vision project development workflow including usage of the ISP and APEX2 Visual Graph Tools.
View full article
ADAS roadmaps, value proposition, current and future plans for tools and reference designs.
View full article
A key challenge to the deployment of Edge compute IoT is management and security of 1000s to millions of Edge compute nodes. EdgeScale simplifies this by providing a cloud-based management framework leveraging the hardware security features of Layerscape processors. Learn how you can use EdgeScale to manage a heterogenious set of Edge compute nodes, and use it with your choice of Edge compute framework - AWS Greengrass, Azure IoT Edge and others.
View full article
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the ARM® Cortex®-M core. Using either Kinetis or LPC development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
View full article