コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
Security is becoming a quintessential topic for any OEM, and possibly for the entire industry, as evolutions of Autonomous drive capabilities are inexorably tied to the ability to secure the car. A number of components in the security architecture of nodes in any vehicle are very close to the SoC, exploiting hardware capabilities to achieve intended functionality. Answering customer needs, NXP is providing a Trusted Execution Environment (TEE) stack, which provides a significant number of security features required by the Automotive needs. Get an introduction to the basis of NXP’s TEE stack, capabilities, and how does this integrates in the typical secure node architecture.
記事全体を表示
Get a deep dive into the brand new Vulkan API from Khronos. Learn how the programming paradigms have changed from OpenGL ES, how to use Vulkan API and its enormous performance advantages, and how to unlock the full potential of i.MX 8 series GPUs.
記事全体を表示
The region expects each OEM to make and sell 12% of its output as ZEVs by 2020, large cities ban classic ICE-vehicles, car makers announce new EVs with increasing cadence. This session shall give an overview of the main forces influencing the EV market, describe the main architectural approaches and system components as well as what growth potential this has for NXP.
記事全体を表示
NXP is a recognized automotive market leader in Motion Sensors, Pressure Sensors, and Magneto-Resistive Sensors with an ever growing base of products and solutions. Join this training session to learn about the latest evolutions of the sensor product roadmaps and targeted applications.
記事全体を表示
Customers are demanding more support from tools to develop their applications. This lecture provides an overview of the extensive capabilities of the S32DS IDEs for Arm and Power (e200). Some highlights: GNU toolchain with GCC Compiler; Integrated NXP tools: FreeMASTER, Math and motor control libraries and Processor Expert; Integrated NXP Software SDKs.
記事全体を表示
This session will cover Smart Home Applications and how sensors can be utilized to create such applications. Some key applications include Smart Door, Window Tamper Detect, Door Knock Detect, Smart HVAC filter, Smart Pill Box, Smart pool Pump, Smart Torch, Smart Stove and many more.
記事全体を表示
This presentation provides an overview of the new toolchain to support the S32 platform of MCUs and application processors, this includes an IDE with new project generation, extensive collateral for ease of use and getting started as well as the next-generation Debugger tools, a new Flash tool specifically design for the S32 platform, the S32 configuration tool plus numerous software products integarted into the toolchain for ease of customer use.
記事全体を表示
As LEDs continue to penetrate exterior automotive lighting applications by replacing traditional lighting solutions, there is an increasing demand for more safe, efficient, flexible and scalable electronics & driver ICs that can enable the full benefits of LEDs in these safety critical applications. This session will provide an overview of the requirements of Advanced Automotive Lighting Systems to provide safety in ADAS systems. Also the impact these system requirements have on the IC specifications, ranging from full system diagnostics, limp home modes, thermal and EMC considerations.
記事全体を表示
With focus on different applications, this session will highlight both the Kinetis and LPC families. We will present the new members of each family and provide you insight of what you could expect from these families going forward.
記事全体を表示
Technical presentation about hardware based secure CAN communication and the benefits for the ECU design, the system approach as well the support for IDPS.
記事全体を表示
The automotive market is moving towards electrification and autonomous driving. This trend needs ADAS electronic systems capable of making decisions. To manage the risk of operations, the development of these systems follows the highest ISO26262 Automotive Safety Integrity Level (ASIL D). All safety electronic systems require a safety microcontroller and a reliable, safe source of power management connected to the car battery: this is the System Basis Chip (SBC). Safety microcontrollers and safety system basis chips are the backbone of embedded system architectures. In this presentation, you’ll review the latest functional safety innovations at the power management level (SBC), from the development phase to system design, underscoring the link to reliability and how to enable hardware that is safety ready. A short introduction to the fault tolerant system will be also presented.
記事全体を表示
NXP is the leader in secure car access chipsets. This session will introduce car access trends and different use cases, products and system solutions for NFC and RF Auto.
記事全体を表示
As geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required, specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design. This session will review basic EM theory and introduce some new guidelines for designing compliant printed circuited boards.
記事全体を表示
Emerging Connected and Automated Vehicles (CAVs) require far more compute horsepower, more memory bandwidth, and more high speed IO connectivity than the vehicles in show rooms today. NXP’s highest performance multicore Arm product family (Layerscape) was developed for networking and industrial infrastructure, however their integration and performance per watt has made them attractive in a variety of ‘transportation’ applications, including planes, trains, and now, automobiles. This session will provide an overview of the product family, and its transportation centric use cases.
記事全体を表示
This session will provide an introduction to automotive cybersecurity. We will outline: NXP's automotive security product portfolio; industry standards and best practices; and NXP's global security organization, cybersecurity design and business practices.
記事全体を表示
In this session you will learn how to design and what to expect from our free software tools.
記事全体を表示
This course will provide an in-depth system analysis of High Voltage (HV) Electric We review how the MCU, GDIC and IGBTs function individually and as a system. We will discuss EV and HEV power systems and components for achieving a highly efficient and safe HV motor drive. Using system block diagrams and oscilloscope screen shots of NXP’s new HV IGBT GDIC, the GD3100, and Fuji GEN 7 IGBT modules as we will consider how to achieve smaller, more efficient and lower cost HV inverter designs. We will review SPI interface programmability that enables any IGBT to be tuned for maximum efficiency, thermal design considerations, layout considerations, power budget assessment, power up sequencing, managing short circuit faults, temperature monitoring and advanced features achieve system ASIL level D and ISO26262 certification.
記事全体を表示
Time-Sensitive Networking (TSN) makes deterministic Ethernet possible. TSN provides evolution for industrial real-time networks and is a set of IEEE® 802 Ethernet sub-standards defined by the IEEE TSN task group. In this session, learn about the key TSN standards and how they work together. Understand more about NXP solutions for both TSN endpoint and TSN switch with abundant software support based on Arm®v8 platforms.
記事全体を表示
This session will focus on tire localization: Dual axis sensors enable rotation rate detection and determination of drivers / passenger side in seconds. NogaroE: Enhanced features added to a proven volume production TPMS sensor. Gen 4x4: Next-generation of ultra-low power TPMS sensors in smallest package features increased accuracy and processing power.
記事全体を表示
During this session, we will discuss the new memories supported on the new i.MX8 processor family. For DRAM, this will include DDR4 and Low Power DDR4 (LPDDR4). For non-volatile memory this will include Octal SPI NOR (XccelaTM Flash) which offers up to 400MB/s as well as the latest eMMC 5.X devices that also support high speeds. These devices are offered with Commercial, Industrial or Automotive temperature and quality ratings. This year, we will provide additional information on LPDDR4X (X=lower power I/O) as well as eMMC 5.1 high performance features including command queueing, and several new Cache operations. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8 systems.  
記事全体を表示