コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
This class provides an introduction on the S32 Design Studio for Vision IDE with integrated Vision SDK in the development of vision processing applications for the S32V234 automotive vision processor. The lecture will overview the user interfaces of the S32DS IDE and the ISP and APEX2 Visual Graph Tools. The demonstration will cover the S32 Design Studio for Vision project development workflow including usage of the ISP and APEX2 Visual Graph Tools.
記事全体を表示
ADAS roadmaps, value proposition, current and future plans for tools and reference designs.
記事全体を表示
A key challenge to the deployment of Edge compute IoT is management and security of 1000s to millions of Edge compute nodes. EdgeScale simplifies this by providing a cloud-based management framework leveraging the hardware security features of Layerscape processors. Learn how you can use EdgeScale to manage a heterogenious set of Edge compute nodes, and use it with your choice of Edge compute framework - AWS Greengrass, Azure IoT Edge and others.
記事全体を表示
This hands-on session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs based on the ARM® Cortex®-M core. Using either Kinetis or LPC development hardware, attendees will build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application.
記事全体を表示
Modern logic provides much more than just the “glue” to connect complex devices in a system. This seminar will detail a case study of an actual customer application and demonstrate how the use of innovative NXP logic devices provides not only technical advantages in device cost, power and board space, but also in system cost related to power supply requirements, product packaging and supply chain costs (inventory, qualification, manufacturing). This seminar is intended for all design engineers, component engineers and purchasing agents with the goal of achieving the most overall cost efficient system design.
記事全体を表示
This presentation will explore key Time-Sensitive Networking (TSN) standards and how they relate to Automotive requirements. An overview of the relevant IEEE®  802.1 TSN standards will be given with examples of how these can be applied and used in the automotive environment. By the end of this session, the attendee will understand and be able to select the features they need based on their network use cases.
記事全体を表示
This session will give a deep dive of MagniV products and explain how to well position these products in different applications.
記事全体を表示
Hands-on getting started with MagniV. Participants will work with bare metal application code and Processor Expert, working with an S12ZVC development kit and CodeWarrior IDE. Short presentations followed by hands-on labs. Learn coding secrets for fast application startup!
記事全体を表示
The i.MX 8 architecture features two processor types: a powerful Arm® Cortex®-A for applications and a Cortex-M4 for real time processing. In this session you will learn how these cores can interact and what features are embedded on our SoC to ease development on this architecture.
記事全体を表示
This hands-on session sponsored and specially created by Turing Computer, will go over a step-by-step process of how you can add connectivity to your multimedia application using i.MX 6 and Linux. The laboratory will introduce you to the concepts of how to enable a 3G/4G modem under Linux, adding internet connectivity to your product, and will also guide you on how to enable an Wi-Fi radio. The final step will be to enable the bridge between the 3G/4G and Wi-Fi, creating a Hotspot for internet access. The hardware used during the lab is an i.MX 6 based System on Module (SoM) from Turing Computer and their evaluation kit, which includes a Wi-Fi and a 3G/4G module. Among the various applications that could benefit from such feature are: video streaming, IoT gateway, digital signage, automotive multimedia and many others.
記事全体を表示
Deep dive into the S32R Family and radar processing roadmap.
記事全体を表示
This session will go over all the available tools and documents provided by NXP to accelerate your design with i.MX applications processors, from hardware design check-lists, to DDR bring-up tools, from IOMUX aid tool to Yocto BSP customization. Get an insight of what NXP can provide to ease the development process.
記事全体を表示
This session explores the fast-growing vehicle gateway market and new applications for vehicle network processing. It will identify key use cases and requirements, and provide insights into how gateways will evolve over the next decade.
記事全体を表示
Overview of a platform solution that addresses the proliferation of Ethernet networks and enables new applications that will transform vehicles.
記事全体を表示
Lecture showing and analyzing SqueezeNet CNN classifier demo on S32V234. See how S32V234 can use CNNs to process and classify images in a power-efficient manner.
記事全体を表示
Signal integrity, EMI, RFI...They are all the result of how well you manage the Electromagnetic fields in your designs. EM fields live in spaces, not conductors. The material presented focuses on the basic physics of electromagnetic energy, presented in an entertaining and easy-to-understand format with plenty of diagrams. Attendees will discover how understanding the behavior of EM fields can help them to design PCBs that will be more robust and have better EMC performance. This is not rocket science, but an easy-to-understand application of PCB geometry.
記事全体を表示
Come see how new types of low- or battery-powered and space-constrained applications are made possible by the latest innovations in communications processors. Applications include portable storage, IoT gateways and embedded control.
記事全体を表示
This session will provide an update on the path the AUTOSAR standard is progressing and will discuss the various NXP software products that are readily integrable into the AUTOSAR framework. We will go in-depth into what the MCAL is and what extensions are available in the NXP AUTOSAR MCAL product.
記事全体を表示
Learn how to create a secure / non-secure application and debug on a secure Cortex-M33 NXP device.
記事全体を表示
In this class, you will learn to use NXP’s FreeMASTER debug tool to aid in system development and debug. Although it is has many uses in various applications, we will demonstrate the features and use of FreeMASTER to simplify the development process with a motor control example based on our MagniV MC9S12ZVMRM microcontroller. Participants will see how useful and easy it is to use and configure so that system variables can be adjusted on the fly or watch system parameters real time.
記事全体を表示