CodeWarrior Development Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Development Tools Knowledge Base

Labels

Discussions

Sort by:
Digital Signal Controllers (DSC) is populated in motor control, Power conversion, automotive and wireless charger, etc. Digital Signal Controllers|NXP    1. CodeWarrior Eclipse v11 Nearly all the DSC products can be supported by CodeWarrior eclipse. The latest CodeWarrior v11 can support DSC naturally on 64bit Windows 10 and windows 7 for all recommend run control interface. CodeWarrior eclipse v11 is our recommendation. CodeWarrior for Microcontrollers-Eclipse IDE 11.0|NXP  CodeWarrior 11.0.1 update just released in end of June, with this update, Unlimited License for all Code Size.         CodeWarrior Classic v8.3 Aside from CodeWarrior eclipse v11, we also have some customers prefer using classic CodeWarrior v8.3.  For some very old DSC product, for example DSP56F80x, it is supported by classic CodeWarrior for DSC v8.3 only. CodeWarrior® Development Tools for 56800/E DSC|NXP  CodeWarrior for DSC v8.3 doesn’t support 64bit Windows 10 and Windows7 naturally, because the ccs driver included in CodeWarrior v8.3 package only support old windows platform. We will explain how to configure the USB TAP run control interface on Windows 7 and Windows 10 64-bit for those using CodeWarrior development tools based on the Classic IDE rather than the Eclipse IDE. This workaround was tested and verified on Windows 7 64-bit and Windows 10 64-bit  for CodeWarrior DSC V8.3. Installation steps:        Install CodeWarrior v8.3 on a Windows 7 or Windows 10 64bit system. At the end of installation, three or four error messages appear regarding a problem installing the USB drivers. Ignore these errors.        Acquire latest ccs driver from CodeWarrior eclipse. Install CodeWarrior for Microcontrollers-Eclipse IDE 11.0|NXP  to a computer, Copy ccs folder from CodeWarrior v11 installation folder to CodeWarrior v8.3 install folder, replace original ccs folder.        Uninstall CodeWarrior eclipse v11. This step is optional.   Now you can use CodeWarrior v8.3 on new windows platform. Please NOTE: Officially CodeWarrior 8.3 was not designed for win7/10.  This doc is just a personal technical sharing. If user meets windows compatible issue of 8.3 on win7/10. Please move to CodeWarrior 11.
View full article
The StarCore C/C++ compiler, in conjunction with the assembler and the linker, generates binaries for the StarCore family of DSP. Freescale's DSP (Digital Signal Processors), built on StarCore technology, offer high-performance programmable devices for baseband, aerospace, defense, medical and test and measurement markets. The StarCore DSP portfolio provides customers with fully scalable and flexible solutions to get to market faster. Combine that with the low power and low cost of the StarCore DSPs and they are the ideal solution for your next design. Today we're bringing up The StarCore C/C++ Compiler User Guide, which explains how to operate this compiler. In addition, thedocument describes you how to optimize C/C++ source code to let the compiler take full advantage of the StarCore processor’s advanced hardware. Awesome, isn't it? Multitask documentation like this make it easier and better to start programming! Get a glance at this manual and start using CodeWarrior for StarCore DSP today! Don't be afraid and ask any questions to DebuggerGuys
View full article
The content is to tell user how to add nand flash(MT29F2G08ABBDA) support in CW 10.3.
View full article
You remember the previous post regarding the new awesome TAP for CodeWarrior applications?   Today I'd like you to meet this device shown up here. Is the CWH-STC-COP-YE, a removable probe tip for StarCore and DSC processors. This probe tip connects your StarCore or DSC processor target system’s ONCE port to the CodeWarrior TAP base unit’s 30-pin target connector.   And of course this tip is compatible with the CodeWarrior TAP previously mentioned (CWH-CTP-BASE-HE). As a matter fact, the base unit doesn't come with a probe tip, so it is necessary to acquire one of the tips available to debug your device. Check out the main features!   Features Removable probe tip Low-cost and economical to order several spares Allows base unit to work with several different target types System Requirements StarCore or DSC target system with ONCE header CodeWarrior TAP  
View full article
The CodeWarrior Development Studio provides a common interface for developing, debugging, and analyzing your applications. The project-oriented Workbench window provides numerous perspectives containing views, editors, and controls that appear in menus and tool bars. After creating a project, build your application, define a launch configuration, and then wait for data collection and data display.   The StarCore linker is a part of StarCore development tools and generates an executable file for the StarCore family of digital signal processors. In addition, the linker also lets you define a Linker Command File (LCF) that you use to instruct the linker to store different parts of the executable file in different areas of the processor address space. Currently, StarCore development tools support two linker versions: • SC100 • SC3000   The SC3000 linker specifically targets SC3850 family of processors. This user guide explains SC3000 linker. For information on SC100 linker, see StarCore SC100 Linker User Guide. What are you waiting for? Amazing features are right here, and  u p d a t e d!!
View full article
We talked of RTOS a little while ago. This time it's turn for The SmartDSP Operating System (OS), and more specifficly, SmartDSP API.   But, what is the SmartDSP OS? It is a Real Time Operating System (RTOS) that, in addition to providing drivers for the MSBA8100 processor, also runs on the following StarCore DSP-based processors: MSC815x MSC825x PSC9131   The StarCore CodeWarrior (CW) Development Studio includes SmartDSP OS royaltyfree source code. Further, SmartDSP OS has a high-level Application Programming Interface (API) that lets users develop integrated applications for StarCore processors. This Reference Manual documents SmartDSP OS API.   Having this API updated and available for processors MSC815x/MSC825x/PSC9131, possibilities of coding within CodeWarrior features become even broader. Start trying it up now!!!
View full article
The CodeWarrior Ethernet TAP probe is a tool that helps you develop and debug a number of processors and microcontrollers.   The Ethernet TAP probe uses advanced emulation technology to provide control of and visibility into your target system. Combined with a host debugger, it speeds the debugging process by letting you interactively control and examine the state of your target system.   The Ethernet TAP probe has these features: • Supports the following systems: PowerPC™ processors, StarCore processors, ColdFire® processors, 56800 Hybrid Controllers (processors and microcontrollers), ARM® processors, and RCF base-band controllers. (All products reference at Freescale web page!) • Supports all CPU core speeds. • Lets you control and debug software running in-target, with minimal intrusion into target system operation. • Lets you debug code in cache, ROM, RAM, and flash memory. • Provides high performance: – Split-second single-step execution. – Capable of download speeds greater than 12 MB per minute from host to target system.   ...and many more of them! Get it updated today!!!      
View full article
Inside {CW10 install folder}\eclipse there is ecd.exe which is used to run build projects from command line. this article focuses on ecd.exe usage with examples. Especially How to use ecd.exe command to build, generateMakefiles,make and reference a project.
View full article
If you recently acquired the CodeWarrior Development Suite, you'll find this document very useful; it provides access and technical support to a multitude of CodeWarrior products.   This quick start also explains how to register your CodeWarrior Development Suite (Section A). Section Bexplains how to activate and install one of your products. Section C describes other items that come with your CodeWarrior Development Suite, and Section D discusses the available purchase options. Section E contains the Technical Support Certificate. As you may not have access to fully license all the CodeWarrior products, keep the following Web link handy, as it lists all the products in the differently priced levels of the CodeWarrior Development Suites (Basic, Standard and Professional). www.freescale.com/CodeWarriorSuites Check it out now! CodeWarrior Development Suite Quick Start
View full article
The rumors say that CodeWarrior (CW) can be turn into a faster and lighter tool to get optimal performance on some micros and processors. Such is the case of Power Architectures for e200 core. And guess what! Rumors are true and completely functional.   There is a document explaining how to make CW development suites faster and lighter, specifiying step by step the process to rock on programming power architecture features.   This document provides the two sets of options to produce optimal code generation. One set optimizes for speed; another set optimizes for size. You can choose from one of these or apply them both, getting a whole new experience on programming with this useful app note. Are you trying it already? CodeWarrior Build Tools Options for Optimal Performance on the Power Architecture® e200 Core  
View full article
The CodeWarrior C and C++ compilers use the Embedded Warrior Library (EWL) for C to provide and extend the libraries documented in the ISO/IEC standards for C. EWL C also offers facilities described in the POSIX specification and some common application programming iwnterfaces (APIs) from UNIX operating systems.   Intrinsic functions generate in-line assembly code instead of making a call to a library function. Intrinsic functions generate less object code and perform faster than their regular counterparts. In some cases these functions generate just a single assembly instruction.Get the EWL for C   n o w !   For the EWL C++ reference libraries you can also find:   The EWL C++ Library Overview of thismanual describes the language support library that provides components that are required by certain parts of the C++ language, such as memory allocation and exception processing.   “LanguageSupport Library” discusses the ANSI/ISO language support library.   Diagnostics Library elaborates on the diagnostics library that provides a consistent framework for reporting errorsina C++ program, including predefined exception classes.   General Utilities Libraries discusses the general utilities library, which includes components used by other library elements, such as predefined storage allocator for dynamic storage management.   Strings Library discusses the strings components provided for manipulating text represented as sequences of type char, sequences of typewchar_t, or sequences of any other “character-like” type.   ...and so on! Find out what the rest of the libraries have got to give you to improve and update CodeWarrior tools! Check out the manual here!
View full article
Did you know that the CodeWarrior IDE includes assemblers that support several specific processors? Well, it does, and for you, codewarrior programmer this is one of its many cool tools to develop great code!   Today I found this manual that helps us out and explains the corresponding assembly-language syntax and IDE settings for these assemblers, in this case, thesyntax for assembly-language statements that the CodeWarrior assemblers use.   These explanations not only cover simple statements, they also include macros and directives!   You might be thinking, "dude, all the assemblers share the same basic assembly-language syntax!". I won't argue that, it's true, but instruction mnemonics and register names are different for each target processor.   To get the most from this manual, you should be familiar with assembly language and with your target processor, so I'd recommend you to start getting into this whole low-level programming style!   Unless otherwise stated, all the information in this manual applies to all the assemblers, enjoy!   CodeWarrior Development Studio for Microcontrollers V10.x ColdFire Assembler Reference Manual
View full article
How to log an issue in Case system instead CRM (Service request)?     After the merge of Freescale and NXP, technical support cases are answered in a different system. To submit your case into the new system, please follow below steps:    1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.    2) On the bottom of the page under Submit New Issues, click Hardware & Software.    3) Register with your business email to access NXP technical online support.    4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.    5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.   Attached you will find a video explaining the process to follow.
View full article
This project is an example of using the DSC CodeWarrior linker to place code in a different area of memory.  In this case, the FlexNVM flash block is used. The example uses three different methods in the linker command file to force specific code to a different memory segment, see examples below.  For more information on the linker syntax, see the manual installed with CodeWarrior at \CW MCU v10.6.x\MCU\Help\PDF\MCU_DSC_Compiler.pdf     This project was developed for the TWR-56F8400 Tower development board, using CodeWarrior for Microcontrollers v10.6.6.  The project was created using Processor Expert, and blinks an LED using the PIT timer interrupt.     The linker command file is located at \Project_Settings\Linker_Files\FLASH_SDM.cmd.Here are the key changes to the project:     MEMORY {         # Added .p_FlexNVM memory segment         .p_FlexNVM(RWX) : ORIGIN = 0x00068000, LENGTH = 0x00004000 }     # Added .FlexNVM_Code memory section .FlexNVM_Code : {   TI1_c.obj (.text) # Place whole source file in this section   OBJECT (FPE_low_level_init, cpu_c.obj) # Place individual function in this section   * (FlexNVM_code.text) # Place from section defined in source code, see main.c     } > .p_FlexNVM     and in main.c: #pragma define_section FlexNVM_code "FlexNVM_code.text"  RX #pragma section FlexNVM_code begin void main(void) {   /* Write your code here */ } #pragma section FlexNVM_code end
View full article
This document shows a general way how to preserve memory range using target task in CW10.6.   I am using k64 freedom board and Segger J-link in my project as an example. K64 freedom board use MK64FN1M0 MCU which has 1 M size flash.  In my project I divide the flash into two areas in the link file as below:   /* Specify the memory areas */ MEMORY { m_interrupts       (rx) : ORIGIN = 0x00000000, LENGTH = 0x198 m_cfmprotrom       (rx) : ORIGIN = 0x00000400, LENGTH = 0x10 m_text             (rx) : ORIGIN = 0x00000800, LENGTH = 512K m_text2            (rx) : ORIGIN = 0x00080800, LENGTH = 512K - 0x800 m_data         (rwx) : ORIGIN = 0x1FFF0000, LENGTH = 64K                  /* Lower SRAM */ m_data2        (rwx) : ORIGIN = 0x20000000, LENGTH = 192K                 /* Upper SRAM */ } m_text2 is the memory area that I am trying to keep it from being erased while downloading the application to m_text memory area. Here are the steps to do this using target task in CW10.6. Add a target task view by clicking Window -> Show View -> other from menu bar, then select Debug -> Target Tasks view in the popup window. From the Target Tasks view, select “Import” from the context menu. Then select the flash (.xml) file for your target device. In this case I need to select MK64FN1M0.xml file. After that you will see a “MK64FN1M0” task in the list. Double click the task name, you will see there are two actions (“Erase” and “Program and Verify”) in the “Flash Programmer Actions” view.   The default Erase action will mass erase all flash, so I remove this action by unchecking the “Erase” action. I can add erase action in “Program and Verify” action later. Double click the “Program and Verify” action. In the popup dialog, check “Erase sectors before program” option. Check “Restrict to Addresses in this Range” option, and then specify the address range you want to program. The data/code out of this range will be preserved (will not be erased or changed). Click “Update Program Action” button to update the settings of this action. Move to Debug configurations window by clicking Run -> Debug configurations from Menu bar. Select a debug configuration, in this case I select the run configuration for Segger J-Link. Select Download tab which is under Debugger tab. By default, Standard Download will be executed and all the flash will be erased. As I am going to execute target task in this case, so uncheck “Perform Standard Download” and then check “Execute Tasks”. Click “Add” button to add a task. In this case I add K64F1M0M12 task which I created in previous step in target task view. Click “Debug” button, the application will be downloaded to flash but preserved area which was not specified in restrict flash range will not be erased. You can check this from memory view.   With the above steps, you can preserve a specified flash range while downloading application. I am using Segger J-link in my project as an example and the steps also work for other tools like P&E Multilink and USB Tap.
View full article
How to install and use eGit plug-in in CodeWarrior
View full article
This document describes two sets of options and pragmas that can be used with the CodeWarrior tools to produce optimal code for the HCS08 cores. One set optimizes the size of the code; another set optimizes the execution speed.   You can use the build tools options and pragmas described in this document for optimal performance, but the build tools settings must be set according to the application being developed. Don't worry, DebuggerGuys provide you with app notes like this to make the job quickly and easy! Optimal Performance on HCS08 Cores (For more information on the HCS08 Compiler, refer to CodeWarrior Development Studio for Microcontrollers V10.x HC(S)08 web page.)  
View full article
If you mix the great new TAP kit for CodeWarrior with the right Tip, the possibilities of debugging your devices become bigger and more powerful. In this occasion I will show you one more removable probe Tip: the CWH-CTP-BDM-YE, meant for ColdFire processors connects your ColdFire microprocessor/microcontroller target system’s BDM port to the CodeWarrior TAP base unit’s 30-pin target connector.   The compatibility of this Tip and the CodeWarrior TAP CWH-CTP-BASE-HE base unit empowers your creations and helps you lowering costs. Note this Tip is not included within the TAP kit. Check out the cool features:   Features Removable probe tip Low cost and economical to order several spares Allows base unit to work with several different target types   System Requirements ColdFire based target system with BDM header CodeWarrior TAP  
View full article