Overview
The purpose of this document is to provide a guide on how to enable Dual Ethernet with the GKI Development. Reference: How to enable dual ethernet on Android 11
For a better reference how to build Android i.MX image please look at the next chapter 3 Building the Android Platform for i.MX in the Android User's Guide
1. Build the Android Image with the next modifications
The 2nd ethernet port is DWMAC from synopsys and phy used is realtek RTL8211F. To add them into the SharedBoardConfig.mk and remove the camera drivers. diff --git a/imx8m/evk_8mp/SharedBoardConfig.mk b/imx8m/evk_8mp/SharedBoardConfig.mk
index f68eb49e..3e95708e 100644
--- a/imx8m/evk_8mp/SharedBoardConfig.mk
+++ b/imx8m/evk_8mp/SharedBoardConfig.mk
@@ -82,7 +82,12 @@ BOARD_VENDOR_KERNEL_MODULES += \
$(KERNEL_OUT)/drivers/rtc/rtc-snvs.ko \
$(KERNEL_OUT)/drivers/pci/controller/dwc/pci-imx6.ko \
$(KERNEL_OUT)/drivers/net/phy/realtek.ko \
- $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko
+ $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko \
+ $(KERNEL_OUT)/drivers/net/phy/micrel.ko \
+ $(KERNEL_OUT)/drivers/net/pcs/pcs_xpcs.ko \
+ $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/dwmac-imx.ko \
+ $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/stmmac.ko \
+ $(KERNEL_OUT)/drivers/net/ethernet/stmicro/stmmac/stmmac-platform.ko
ifeq ($(POWERSAVE),true)
BOARD_VENDOR_KERNEL_MODULES += \
$(KERNEL_OUT)/drivers/soc/imx/lpa_ctrl.ko \
@@ -219,15 +224,12 @@ BOARD_VENDOR_RAMDISK_KERNEL_MODULES += \
$(KERNEL_OUT)/drivers/perf/fsl_imx8_ddr_perf.ko \
$(KERNEL_OUT)/drivers/cpufreq/cpufreq-dt.ko \
$(KERNEL_OUT)/drivers/cpufreq/imx-cpufreq-dt.ko \
- $(KERNEL_OUT)/drivers/media/i2c/ov5640.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-capture.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-capture.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-hw.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-isi-mem2mem.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-mipi-csi2-sam.ko \
$(KERNEL_OUT)/drivers/dma/imx-sdma.ko \
- $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/basler-camera-driver-vvcam.ko \
- $(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/os08a20.ko \
$(KERNEL_OUT)/drivers/staging/media/imx/imx8-media-dev.ko \
$(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/vvcam-dwe.ko \
$(TARGET_OUT_INTERMEDIATES)/VVCAM_OBJ/vvcam-isp.ko \
To let the Android framework's EthernetTracker and EthernetNetworkFactory know which interfaces to manage, the framework level configure
config_ethernet_iface_regex
config_ethernet_interfaces
must be overlay in device/nxp/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml:
diff --git a/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml b/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml
index 298d50cc..63f6787e 100644
--- a/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml
+++ b/imx8m/evk_8mp/overlay/frameworks/base/core/res/res/values/config.xml
@@ -22,7 +22,12 @@
<resources>
<!--For Android we support eth0 now -->
- <string translatable="false" name="config_ethernet_iface_regex">eth0</string>
+ <string translatable="false" name="config_ethernet_iface_regex">eth\\d</string>
+
+ <string-array translatable="false" name="config_ethernet_interfaces">
+ <item>eth0;12,13,14,15,16,18,19</item>
+ <item>eth1;12,13,14,15,16,18,19</item>
+ </string-array>
<!-- List of regexpressions describing the interface (if any) that represent tetherable
USB interfaces. If the device doesn't want to support tething over USB this should
--
Apply the patch 0001-PATCH-Add-defines-for-ETH-support-drivers.patch
Build the Android Image # Change to the MY_ANDROID Directory
$ source build/envsetup.sh
$ lunch evk_8mp-userdebug
$ ./imx-make.sh -j4 2>&1 | tee build-log.txt
GKI Development
Follow and apply the next community post: Export new symbols of GKI development Android 14
Set the GKI repo
$ repo init -u https://android.googlesource.com/kernel/manifest -b common-android14-6.1
$ repo sync
$ git remote add device https://github.com/nxp-imx/linux-imx.git
$ git remote update
$ git fetch device --tags
$ git checkout android-14.0.0_1.2.0
$ cd ..
#Be sure that symbolic links are created correctly
$ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam
$ ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex
$ BUILD_FOR_GKI=yes
$ BUILD_CONFIG=common/build.config.imx
$ tools/bazel run //common:imx_abi_update_symbol_list
Apply the following changes in the GKI Kernel tree: gki/common: Patch: 0001-PATCH-GKI-Kernel-tree-Drivers-for-the-ETH1-Interface.patch
Build the GKI Image tools/bazel run //common:kernel_aarch64_dist
Follow the build android boot.img and system_dlkm.img $ cp out/kernel_aarch64/dist/boot.img ${MY_ANDROID}/vendor/nxp/fsl-proprietary/
gki/boot.img
$ cd ${MY_ANDROID}
$ TARGET_IMX_KERNEL=true make bootimage
# Change directory to the gki folder
$ cp out/kernel_aarch64/dist/system_dlkm_staging_archive.tar.gz ${MY_ANDROID}/vendor/nxp/fsl-proprietary/gki/system_dlkm_staging_archive.tar.gz
$ cd ${MY_ANDROID}/vendor/nxp/fsl-proprietary/gki
$ tar -xzf system_dlkm_staging_archive.tar.gz -C system_dlkm_staging
$ cd ${MY_ANDROID}
$ make system_dlkmimage
Create the tar.gz file for flash the android image (*.img, *.bat, *.sh, *.bin, *.imx)
Boot the image and type lsmod to ensure the drivers are installed.
Regards,
Mario
View full article