i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Symptoms   Trying to initialize a repo, for example:  $repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml we have the below log: File "/home/username/bin/repo", line 51 def print(self, *args, **kwargs): ^ SyntaxError: invalid syntax   Workaround (1)   The first workaround consist in change the python alternatives (caused when you have installed two or more python versions). NOTE: in my case, the python version that i want to change as first priority is python3.8 $sudo update-alternatives --install /usr/bin/python python /usr/bin/python3.8 1   Then we run: $sudo update-alternatives --config python    To verify if your python priority was changed successfully try: $python --version   You should see the version configured as priority number 1.     Workaround (2)   The workaround is very simple, only we need modify the repo file $ nano ~/bin/repo   and we will change the python interpreter in the first line (from python to python3): ORIGINAL FILE   EDITED FILE   After to do this change, repo will works fine again.     I hope this can helps to you!   Best regards.
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   These are the detailed programming aids for the registers associated with DRAM initialization (DDR3 and LPDDR2) of the MX6DQP (also known as Rev 2 or Dual/Quad Plus), and covers the Sabre_SD boards and DDR3 based Auto Infotainment board. The last work sheet tab in the tool formats the register settings for use with the ARM RealView debugger (.inc) and the DDR Stress Test. It can be manually converted, by the user, to the DS5 .ds format or to a DCD file format used by uboot or other. The programming aids were developed based on NXP development boards and can be customized by the user for their board design. This tool serves as an aid to assist with programming the DDR interface of the MX6DQP and is based on the DDR initialization scripts developed by the R&D team and no guarantees are made by this tool. The following are some general notes regarding this tool: • Refer to the "How To Use" tab in the tool as a starting point to use this tool. • This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance. • The MX6DQP adds a new third party IP called the NoC. The programming for these registers are automatically updated in the tool given a set of user input MMDC parameters and should not be modified manually.
View full article
Hello there. Here is a good way to use U-boot in an efficient way with custom scripts. The bootscript is an script that is automatically executed when the boot loader starts, and before the OS auto boot process. The bootscript allows the user to execute a set of predefined U-Boot commands automatically before proceeding with normal OS boot. This is especially useful for production environments and targets which don’t have an available serial port for showing the U-Boot monitor. This information can be find in U-Boot Reference Manual.   I will take the example load a binary file in CORTEX M4 of IMX8MM-EVK. In my case, I have the binary file in MMC 2:1 called gpio.bin and I will skip those steps because that is not the goal.   First, you need the u-boot-tools installed in your Linux machine: sudo apt install u-boot-tools   That package provide to us the tool mkimage to convert a text file (.src, .txt) file to a bootscript file for U-Boot.   Now, create your custom script, in this case a simple script for load binary file in Cortex M4: nano mycustomscript.scr  and write your U-Boot commands: fatload mmc 2:1 0x80000000 gpio.bin cp.b 0x80000000 0x7e0000 0x10000 bootaux 0x7e0000   Now we can convert the text file to bootscript with mkimage. Syntax: mkimage -T script -n "Bootscript" -C none -d <input_file> <output_file> mkimage -T script -n "Bootscript" -C none -d mycustomscript.scr LCM4-bootscript   This will create a file called LCM4-bootscript (Or as your called it).   A way to load this bootscript file to U-Boot is using the UUU tool, in U-Boot set the device in fastboot with command: u-boot=> fastboot 0 Then in linux with the board connected through USB to PC run the command: sudo uuu -b fat_write LCM4-bootscript mmc 2:1 LCM4-bootscript   Now we have our bootscript in U-Boot in MMC 2:1.   Finally, we can run the bootscript in U-Boot: u-boot=> load mmc 2:1 ${loadaddr} LCM4-bootscript 158 bytes read in 2 ms (77.1 KiB/s) u-boot=> source ${loadaddr} ## Executing script at 40400000 6656 bytes read in 5 ms (1.3 MiB/s) ## No elf image at address 0x007e0000 ## Starting auxiliary core stack = 0x20020000, pc = 0x1FFE02CD...   And the Cortex M4 booted successfully:    I hope this can helps to you.   Best regards.   Salas.  
View full article
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
View full article
We will build a remote debug environmet of Qt Creator in this user guide.   Contents 1 Change local.conf file in Yocto 2 2 Build and deploy Yocto SDK 2 2.1 Build full image SDK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 2.2 Deploy SDK . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 3 Configure QT Kit 2 3.1 Setup device . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2 3.2 Configure QT version . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3 3.3 Configure gcc and g++ manually . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4 3.4 Configure gdb manually . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 3.5 Configure Kit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 3.6 Very important thing!! . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5 4 Test result
View full article
This note show how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real Time protocol is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP.   Prerequisites: MX6x o MX8x board with the L5.10.35 BSP installed. A host PC with either Gstreamer or VLC player installed. Receiving h.264/h.265 Encoded RTP Video Stream on a Host Machine Using GStreamer GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using Host PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC. Sending h.264 and h.265 Encoded RTP Video Stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX 8M Mini Quad/ 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   Using Other Video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L5.10.35 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink      
View full article
Sometime need standalone compile device tree. Only Linux headers and device tree directory are needed.         
View full article
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
View full article
  Question: How can we generate an ARM DS5 DStream format DDR initialization script using the DRAM Register Programming Aid?  Answer: Some RPAs include a  "DStream .ds file" tab for the ARM DS5 debugger specific commands. The i.MX6UL/ULL/ULZ DRAM Register Programming Aids for example already has this supported. However, the user can easily create  the .ds format from the existing .inc format. The basic steps to convert .inc files to .ds format are as follows: 1)  Replace the one instance of setmem /16 with mem set 2)  In that same line, replace 0x020bc000 = with 0x020bc000 16 3)  Use a Replace All command to change setmem /32 with mem set 4)  Use a Replace All command to change = with 32 5)  Use a Replace All command to change // with # 6)  Save as a .ds file.   Question: When using a 528MHz DRAM Controller interface with a DDR memory of a faster speed bin, which speed bin timing options should one use? Answer: For example, let’s assume our MX6DQ design is using a DDR3 memory from a DDR3-1600 speed bin.  However, the maximum speed of the MMDC interface for the MX6DQ using DDR3 is 528MHz.  Should we use the 1600 speed bin (800MHz clock speed) or the 1066 speed bin (533MHz clock speed)?  In short, the user should use the timings rated for the maximum speed (frequency) with which you are running, in this case DDR3-1066 (533MHz).  In some cases, like when using the MX6DL, the maximum DDR frequency is 400MHz.  In this case, you would want to try and use 800 timings found in the AC timing parameters table.  However, most DDR3 devices have speed bin tables that may go only as low as 1066, in which case you would use the closest speed bin to your operational frequency (i.e. the 1066 speed bin table).     Question: Some timing parameters may specify a min and max number, which should I use? Answer: In most cases, you will want to choose the minimum timings.  Some DRAM controllers may have a tRAS_MAX timing parameter, in which case you would obviously use the maximum tRAS parameter given in the DRAM data sheet. Also, for timing parameters tAONPD and tAOFPD, we also want to use the maximum values given in the DDR3 data sheet. These represent the maximum amount of time the DDR3 device takes to turn on or off the RTT (termination), therefore, we should wait at least this amount of time before issuing any commands or accesses.   Question: Some timing parameters state things like “Greater of 3CK or 7.5ns”; which should I use? Answer: This depends on your clock speed.  Say you are running at 533MHz.  At 533MHz, 7.5ns equates to 4CKs.  In this case, 7.5ns at 533MHz is GREATER than 3CK, so we would use the 7.5ns number, or 4CKs. At 400MHz, 7.5ns equates to 3CKs.  In this case, we’d simply use 3CKs.   Question: I have a design that will throttle the DDR frequency (dynamic frequency scaling).  At full speed, I plan to run at 533MHz, and then I plan to throttle down to say 400MHz whenever possible.  Do I need to re-calculate my 400 MHz timing parameters that were initially set for 533MHz? Answer: It is not necessary to re-calculate timing parameters for 400MHz, and you can re-use the ones for 533MHz.  The timings at 533 MHz are much tighter than 400 MHz, and the key here is to NOT violate timings.  Also, it may be a bit of a hassle maintaining two sets of timing parameters, especially if later in the design, you swap DDR vendors that might require you to re-calculate some timing parameters.  It’s easier to do it once and to come up with a combined worse-case timing parameters for 533MHz, which you know will work at 400MHz.  But, if you don’t mind maintaining two sets of timing parameters, and really want to optimize timings down to the last pico-second for 400MHz, then knock yourself out.   Question: Can I use these Register programming aids for both Fly by and T- Topology ? Answer Yes The DDR register programming aid is agnostic to the DDR layout. The same spreadsheet works for both topologies. We recommend running write leveling calibration for both topologies and the values returned by the Write Leveling routine from the Freescale DDR stress test should be incorporated back to the customer specific initialization script. The DDR stress test also has a feature whereby it evaluates the write leveling values returned from calibration and increments WALAT to 1 if the values exceed a defined limit. The DDR stress test informs the user when the Write Additional latency (WALAT) exceeds the limit and should be increased by 1, and reminds the user to add it back in the customer specific initialization script if required.   WALAT - 0 00000000 WALAT: Write Additional latency. Recommend to clear these bits. Proper board design should ensure that the DDR3 devices are placed close enough to the MMDC to ensure the skew between CLK and DQS is less than 1 cycle.     Question: Can I use the DEFAULT Register programming aid values for MDOR when using an Internal OSC instead of the recommended 32.768 KHZ XTAL ? Answer No, NXP recommends reprogramming these values based on the worse case frequency (Max clock) of the internal OSC of the device to guarantee JEDEC timings are met. Please refer to Internal Oscillator Accuracy considerations for the i.MX 6 Series for more details  
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 6/7 Series Family DDR Tools Overview This page contains the latest releases for the i.MX 6/7 series DDR Tools. The tools described on this page cover the following i.MX 6/7 series SoCs: i.MX 6DQP (Dual/Quad Plus) i.MX 6DQ (Dual/Quad) i.MX 6DL/S (Dual Lite/Solo) i.MX 6SoloX i.MX 6SL i.MX 6SLL i.MX 6UL i.MX 6ULL/ULZ i.MX 7D/S i.MX 7ULP The purpose of the i.MX 6/7 series DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.). This process equips the user to then proceed with the bring-up of a boot loader and an OS. Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface. The i.MX 6/7 series DDR Tools consist of: DDR Register Programming Aid (RPA) DDR Stress test _________________________________________________________ i.MX 6/7 Series DDR Stress Test The i.MX 6/7 Series DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational prior for use in u-boot and OS bring-up. The DDR Stress Test tool can be found here: i.MX 6/7 DDR Stress Test Tool Note that the DDR Stress test tool supports all of the above i.MX SoCs, however, some of the supported i.MX SoCs named in the tool support multiple i.MX SoCs as follows: MX6DQ – when selected, this supports both i.MX 6DQ and i.MX 6DQP (Plus) MX6DL – when selected, this supports both i.MX 6DL and i.MX 6S (i.MX 6DLS family) MX6ULL – when selected, this supports both i.MX 6ULL and i.MX6 ULZ MX7D – when selected, this supports both i.MX 7D and i.MX 7S _____________________________________________________________________________ i.MX 6/7 Series DDR Register Programming Aid (RPA) The i.MX 6/7 series DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization script for use with the DDR Stress Test tool. For a history of the previous versions of an RPA, refer to the Revision History tab of the respective RPA. To obtain the latest RPAs, please refer to the following links: i.MX 6DQP i.MX6DQP Register Programming Aids i.MX 6DQ i.MX6DQ Register Programming Aids i.MX 6DL/S i.MX6DL Register Programming Aids i.MX 6SoloX i.MX6SX Register Programming Aids i.MX 6SL i.MX6SL Register Programming Aids  i.MX6SLL i.MX6SLL Register Programming Aids i.MX 6UL/ULL/ULZ i.MX6UL/ULL/ULZ DRAM Register Programming Aids i.MX7D i.MX7D DRAM Register Programming Aids i.MX 7ULP i.MX7ULP DRAM Register Programming Aids _____________________________________________________________________________ DRAM Register Programming Aids FAQ    
View full article
Recently, some customers are using i.MX processor, they want to add raid & LVM function support to the kernel, but they have encountered the problem that the compilation cannot pass. Tested it in L4.14.98, L4.19.35 & L5.4.x, Only L4.14.98 bsp exists the problem. Here are the experimental steps I have done, including the same problems I encountered with the customer, and how to modify the kernel to ensure that the compilation passes. 1. Exporting cross compilation tool chain from yocto BSP (1) Downloading Yocto BSP and compiling it. Following steps in i.MX_Yocto_Project_User's_Guide.pdf, download Yocto BSP and compile it successfully. (2) Exporting cross compilation tool chain Following methods described in i.MX_Linux_User's_Guide.pdf, export cross compilation tool chain from yocto BSP. See Chapter 4.5.12 of the document, please! Then cross compilation tool chain will be like below: (3) Copying linux BSP source code to a new directory # cd ~ # mkdir L4.14.98-2.0.0 # cd L4.14.98-2.0.0 # cp -r ~/imx-yocto-bsp/build-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.14.98- r0/git ./ Then all linux source code has been copied to L4.14.98-2.0.0, which is the top directory of linux kernel source code, I will compile kernel image here. 2. Compiling linux kernel # cd ~/L4.14.98-2.0.0 # source /opt/fsl-imx-fb/4.14-sumo/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make imx_v7_defconfig # make menuconfig Then we will add RAID and LVM modules to linux kernel. In order to reproduce errors, I added all related modules to kernel. See below, please! Device drivers---->Multiple devices driver support (RAID and LVM) After save and exit, began to compile kernel. # make (make –j4) The following errors will occur: ------------------------------------------------------------------------------------------- drivers/md/dm-rq.c: In function ‘dm_old_init_request_queue’: drivers/md/dm-rq.c:716:2: error: implicit declaration of function ‘elv_register_queue’; did you mean ‘blk_register_queue’? [-Werror=implicit-function-declaration] elv_register_queue(md->queue); ^~~~~~~~~~~~~~~~~~ blk_register_queue cc1: some warnings being treated as errors scripts/Makefile.build:326: recipe for target 'drivers/md/dm-rq.o' failed make[2]: *** [drivers/md/dm-rq.o] Error 1 scripts/Makefile.build:585: recipe for target 'drivers/md' failed make[1]: *** [drivers/md] Error 2 Makefile:1039: recipe for target 'drivers' failed make: *** [drivers] Error 2 ------------------------------------------------------------------------------------------- 3. Finding out root cause and solving it (1) elv_register_queue( ) function The function is loaded in dm-rq.c : int dm_old_init_request_queue(struct mapped_device *md, struct dm_table *t) { … … elv_register_queue(md->queue); … … } BUT compiler didn’t find it’s declaration and entity. Searching source code, and found it declared in linux_top/block/blk.h: … … int elv_register_queue(struct request_queue *q); … … It’s entity is in linux_top/block/elevator.c: int elv_register_queue(struct request_queue *q) { … … } (2) Adding declaration and exporting the function --- Declaration Add the line below to dm-rq.c: … … extern int elv_register_queue(struct request_queue *q); … … --- Exporting the function(elevator.c) Add EXPORT_SYMBOL(elv_register_queue); to the end of function, see below. int elv_register_queue(struct request_queue *q) { … … } EXPORT_SYMBOL(elv_register_queue); 4. Re-compiling Linux Kernel The above error will not occur and the compilation will complete successfully.   NXP CAS team Weidong Sun
View full article