eIQ Machine Learning Software Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eIQ Machine Learning Software Knowledge Base

Labels

Discussions

Sort by:
This document will cover some of the most commonly asked questions we've gotten about eIQ and embedded machine learning. Anything requiring more in-depth discussion/explanation will be put in a separate thread. All new questions should go into their own thread as well What is eIQ? The NXP® eIQ™ machine learning (ML) software development environment enables the use of ML algorithms on NXP EdgeVerse™ microcontrollers and microprocessors, including MCX-N microcontrollers, i.MX RT crossover MCUs, and i.MX family application processors. eIQ ML software is made up of several pieces of enablement including inference engines, neural network compilers and optimized libraries. This software leverages open-source and proprietary technologies and is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease. eIQ enablement also enables models to use the new eIQ Neutron NPU found on the MCX-N and i.MX RT700 microcontroller devices and upcoming future NPU enabled embedded devices like i.MX95.    What are the key pieces of eIQ enablement?  eIQ Time Series Studio - PC tool to create and deploy classical machine learning and neural network models for time series analysis eIQ Inference Engines - Included as part of MCUXpresso SDK or Yocto Linux, this software is used to do inferencing of pre-trained neural network models on embedded devices eIQ Neutron SDK - Contains the Neutron Compiler tool for enabling neural network models to be accelerated with eIQ Neutron NPUs eIQ AI Toolkit - Coming Soon! Model optimizations, conversion, and profiling using a docker container on your PC eIQ AI Hub - Coming Soon! Model optimizations, conversion, benchmarking, and profiling through a cloud based interface.  eIQ Model Zoo - browse models tested on NXP silicon eIQ Model Watermarking Extension - Enhance copyright protections on custom models eIQ Model Creator - Partnership with ModelCat for vision-based model development   How much does eIQ cost? eIQ Time Series Studio, eIQ Neutron SDK, and eIQ Inference engines are complimentary and royalty free. eIQ Model Creator has a subscription fee with ModelCat.    What is the development flow for developing and deploying AI/ML models with eIQ? There are two options depending on if already have a model or not, or if interested in Time Series or not: 1) Deploy a neural network model using the eIQ Inference Engines 2) Use eIQ Time Series Studio (TSS) to train and deploy a time series model using a simple C library   eIQ Inference Engines What is the key enablement for using eIQ Inference Engines? 1) The inference engine, like TensorFlow Lite for Microcontrollers, that is included in the MCUXpresso SDK 2) eIQ Neutron Compiler Tool (previously named the Neutron Converter Tool) - located inside the eIQ Neutron SDK package, it is used to convert a quantized TFLite model into a Neutron-accelerated TFLite model. This is only required if using an eIQ Neutron NPU enabled device.    You can use any workflow to create and train your ML model. The model just needs to be exported as TFLite file so it can be converted by the eIQ Neutron Compiler Tool and/or use the TFLM inference engine.    What inference engines are available in eIQ? i.MX apps processors and i.MX RT MCUs support different inference engines. The best inference engine can depend on the particular model being used, so eIQ offers several inference engine options to find the best fit for your particular application.  Inference engines for i.MX: TensorFlow Lite (Supported on both CPU and GPU/NPU) ARM NN (Supported on both CPU and GPU/NPU) OpenCV (Supported on only CPU) ONNX Runtime (Currently only supported on CPU) Inference engines for MCX and i.MX RT TensorFlow Lite for Microcontrollers ExecuTorch (Coming Soon)     What devices are supported by eIQ inference engines? eIQ inference engines are available for the following i.MX application processors: i.MX 8M Plus i.MX 8M i.MX 8M Nano i.MX 8M Mini i.MX 8ULP i.MX 8X i.MX 93 i.MX 95 eIQ inference engines are available for the following MCX MCUs: MCX-N eIQ inference engines are is available for the following i.MX RT crossover MCUs: i.MX RT1180 i.MX RT1170 i.MX RT1160 i.MX RT1064 i.MX RT1060 i.MX RT1050 i.MX RT700 i.MX RT685 i.MX RT595     Can eIQ inference engines run on other NXP MCU devices? There's no special hardware module required to run eIQ inference engines and it is possible to port the inference engines to other NXP devices.    Is eIQ Neutron SDK required to use eIQ inference engines?  eIQ Neutron SDK is required if using a device with an eIQ Neutron NPU as it includes the Neutron Compiler tool which is used to convert a model to be accelerated by the NPU.    What is the eIQ Neutron NPU?  The new eIQ Neutron NPU is a Neural Processing Unit developed by NXP which has been integrated into the MCX N, i.MX RT700, and i.MX95 devices, with many more to come. It was designed to accelerate neural network computations and significantly reduce model inference time. The scalability of this module allows NXP to integrate this NPU into a wide range of devices all while having the same eIQ software enablement.  For more details on the NPU for MCX N see this Community post.  How can I start using the eIQ Neutron NPU?  There are hands-on NPU lab guides available for MCX N or i.MX RT700 that walk through the steps for converting and running a model with the eIQ Neutron NPU. There is also an app note AN14700 - i.MX RT700 eIQ Neutron NPU Enablement and Performance which has more details.    What TFLite operators are supported bythe eIQ Neutron NPU on different devices?  The details and constraints for supported operators can be found in the MCUXpresso SDK documentation.    What happened to the Neutron Converter Tool? Starting in August 2026 the Neutron Converter tool found in eIQ Neutron SDK was renamed to Neutron Compiler. It's the same tool with the same functionality, just has a new name.  What happened to eIQ Toolkit?  The tools previously bundled as part of eIQ Toolkit are now released as standalone packages and eIQ Toolkit will no longer be updated after the eIQ Toolkit v1.17 in Q3 2025. Going forward the tools previously included in eIQ Toolkit can now be found at: eIQ Time Series Studio eIQ Neutron SDK - for the Neutron Compiler Tool eIQ Model Creator - new model creation tool developed by partner ModelCat Netron - For TFLite model visualization  Model optimization and conversion utility coming soon!    Which NXP devices include a Neural Processing Unit (NPU)?  MCX N - eIQ Neutron N1-16 i.MX RT700 - eIQ Neutron N3-64 i.MX 8M Plus - VeriSilicon VIP8000 i.MX 93 - Ethos U65 256 i.MX 95 - eIQ Neutron N3-1024S   eIQ Time Series Studio What is eIQ Time Series Studio (TSS)?   eIQ TSS is software application that provides an automated machine-learning workflow that streamlines the development and deployment of time series-based machine learning models across microcontroller (MCU) class devices such as the MCX portfolio of MCUs and i.MX RT portfolio of crossover MCUs. Time Series Studio supports a wide range of sensor input signals, including voltage, current, temperature, vibration, pressure, sound, time of flight, among others, as well as combinations of these for multimodal sensor fusion. The automatic machine learning capability enables developers to extract meaningful insights from raw time-sequential data and quickly build AI models tailored to meet accuracy, RAM and storage criteria for microcontrollers. The tool offers a comprehensive development environment, including data curation, visualization and analysis, as well as model autogeneration, optimization, emulation and deployment. eIQ Time Series Studio was previously included in eIQ Toolkit but is now available as a standalone installer for both Windows and Linux. A web based version is also now an option which has the same GUI functionality as the PC version.   What devices are supported by the eIQ Time Series Studio?   TSS will generate a C library that can be included in your application and does not require an Deep Learning inference engine, so it can be deployed to a much wider range of NXP devices as it has very minimal flash and RAM requirements.  MCX FRDM-MCXA153 FRDM-MCXC444 FRDM-MCXN947 FRDM-MCXN236 FRDM-MCXW17 FRDM-MCXE247 i.MX RT MIMXRT1060-EVK MIMXRT1170-EVK MIMXRT1180-EVK i.MXRT685 i.MXRT595 i.MXRT700 LPC LPC55S69-EVK Kinetis FRDM-K66F FRDM-KV31F FRDM-K32L3A6 DSC MC56F83000-EVK MC56F80000-EVK i.MX i.MX 6 i.MX 8M Plus i.MX93   Can eIQ Time Series Studio create models that can take advantage of the eIQ Neutron NPU?  Yes, TSS now supports creating both Classical Machine Learning (CML) models as well as Neural Network models. Neural Network models can be accelerated by the NPU. However in many cases it will make more sense to use the CML models for time series applications as they can be just as accurate for many time series datasets but will be much faster and use far less memory due to their smaller model size. Even when using NPU acceleration Neural Network models can be slower than their far smaller CML model counterparts. However in some situations Neural Networks may give better accuracy for complex multi-modal analysis. TSS make it easy to determine if a NN or CML model is the best fit for a particular dataset.  But as many time series applications perform well with CML models then it opens up running time series AI on a wide variety of devices even if they do not have an integrated NPU.  How can I start using the eIQ Time Series Studio tool?  There is a hands-on lab guide available to walk through how to use the tool as well as documentation and guides in the tool itself.    General eIQ Questions How can I get eIQ? For MCU devices: eIQ inference engine libraries and examples are included as part of MCUXpresso SDK for supported devices. Make sure to select the “eIQ” middleware option. eIQ Neutron Compiler Tool that converts your own neural network model to use the Neutron NPU can be found in eIQ Neutron SDK.  eIQ Time Series Studio is available as a standalone installer or web based application.    For i.MX devices: eIQ is distributed as part of the Yocto Linux BSP. Starting with the 4.19 release line there is a dedicated Yocto image that includes all the Machine Learning features: ‘imx-image-full’. For pre-build binaries refer to i.MX Linux Releases and Pre-releases pages.   What documentation is available for eIQ? For i.MX RT and MCX devices:  eIQ MCUXPresso SDK documentation can be found online here.    For i.MX devices: The eIQ documentation for i.MX is integrated in the Yocto BSP documentation. Refer to i.MX Linux Releases and Pre-releases pages. i.MX Reference Manual: presents an overview of the NXP eIQ Machine Learning technology. i.MX Linux_User's Guide: presents detailed instructions on how to run and develop applications using the ML frameworks available in eIQ (currently ArmNN, TFLite, OpenCV and ONNX). i.MX Yocto Project User's Guide: presents build instructions to include eIQ ML support (check sections referring to ‘imx-image-full’ that includes all eIQ features). It is recommended to also check the i.MX Linux Release Notes which includes eIQ details.   For i.MX devices, what type of Machine Learning applications can I create?  Following the BYOM principle described above, you can create a wide variety of applications for running on I.MX. To help kickstart your efforts, refer to PyeIQ – a collection of demos and applications that demonstrate the Machine Learning capabilities available on i.MX. They are very easy to use (install with a single command, retrieve input data automatically) The implementation is very easy to understand (using the python API for TFLite, ArmNN and OpenCV) They demonstrate several types of ML applications (e.g., object detection, classification, facial expression detection) running on the different compute units available on i.MX to execute the inference (Cortex-A, GPU, NPU).   Can I use the python API provided by PyeIQ to develop my own application on i.MX devices? For developing a custom application in python, it is recommended to directly use the python API for ArmNN, TFLite, and OpenCV. Refer to the i.MX Linux User’s Guide for more details.   You can use the PyeIQ scripts as a starting point and include code snippets in a custom application (please make sure to add the right copyright terms) but shouldn’t rely on PyeIQ to entirely develop a product.   The PyeIQ python API is meant to help demo developers with the creation of new examples.   What eIQ example applications are available for MCUs? eIQ example applications can be found in the <SDK DIR>\boards\<board_name>\eiq_examples directory:    How do I recompile the TFLM (TensorFlow Lite for Microcontroller) libraries for MCUs?  Download the Github SDK and then run: west build -p always examples/eiq_examples/tflm_lib --toolchain armgcc --config release -b frdmmcxn947 -Dcore_id=cm33_core0 west build -p always examples/eiq_examples/tflm_lib --toolchain armgcc --config release -b mimxrt700evk -Dcore_id=cm33_core0 west build -p always examples/eiq_examples/tflm_lib --toolchain armgcc --config release -b evkbmimxrt1170 -Dcore_id=cm7 If alternatively you use the MCUXpresso IDE TFLM Library project, make sure to set the optimization level to -O3.    What are Glow and DeepViewRT inference engines in the MCUXpresso SDK?  These are inference engines that were supported in previous versions of eIQ but are now deprecated as new development has focused on TensorFlow Lite for Microcontrollers. These projects are still available in MCUXpresso SDK 2.15 for legacy users, but it is highly recommended that any new projects use TensorFlow Lite for Microcontrollers.     How can I learn more about using TensorFlow Lite with eIQ? There is a hands-on TensorFlow Lite for Microcontrollers lab available. There is also a i.MX TensorFlow Lite Lab that provide a step-by-step guide on how to get started with eIQ for TensorFlow Lite for i.MX devices.    What hands-on labs are available to start learning how to use eIQ? eIQ Time Series Studio Getting Started Lab i.MX RT700 NPU Getting Started Lab MCX N NPU Getting Started Lab MCX N Face Detect Vision Lab TFLite for Microcontrollers Getting Started Lab eIQ Getting Started Guide   What NXP Community Knowledge Base articles are there about eIQ? eIQ FAQ How to Update eIQ Projects with the Latest eIQ Neutron SDK Libraries eIQ TSS Library Integration Guide eIQ Time Series Studio Command Line Interface Using a Camera with FRDM-MCXN947 for Vision AI/ML Using a Camera with i.MX RT700 for Vision AI/ML eIQ Neutron NPU Memory Requirements for MCUs Tips on Importing Custom Models into eIQ MCUXpresso SDK Examples Using the HiFi DSP for Inferencing ML Models on i.MX RT Devices eIQ and MCUXpresso SDK 26.03 with VS Code Known Issues What application notes are available to learn more about eIQ? i.MX RT700 eIQ Neutron NPU Enablement and Performance (AN14700) i.MX RT700 USB Camera Object Detection (AN14718) with software How to Use TSS to Deploy AD Models on MCXA156 (AN14549) Enabling eIQ Core NPU Delegates for i.MX Android Apps (AN14411) Anomaly Detection with eIQ using K-Means clustering in TF-Lite (AN12766) Transfer Learning and Datasets (AN12892) Handwritten Digit Recognition using TensorFlow Lite (AN12603) Caffe Model Development on MNIST Dataset with CMSIS-NN Library (AN12781) Gender Voice Recognition with TensorFlow Lite Inference (AN13065)   What is the advantage of using eIQ instead of using the open-sourced software directly from Github? eIQ supported inference engines work out of the box and are already tested and optimized, allowing for performance enhancements compared to the original code. eIQ also includes the software to capture the camera or voice data from external peripherals. eIQ allows you to get up and running within minutes instead of weeks. As a comparison, rolling your own is like grinding your own flour to make a pizza from scratch, instead of just ordering a great pizza from your favorite pizza place.    Does eIQ include ML models? Do I use it to train a model? eIQ has options to both create model and run pre-existing models so you can Bring Your Own Model (BYOM) and run it on NXP embedded devices. eIQ provides the ability to run your own specialized model on NXP’s embedded devices.  MCUXpresso SDK and the i.MX Linux releases come with several examples that use pre-created models that can be used to get a sense of what is possible on our platforms, and it is very easy to substitute in your own model into those examples. eIQ Time Series Studio can be used to create and deploy time series models eIQ Model Creator is an option to create your own vision based models with our partner ModelCat   I’m new to AI/ML and don’t know how to create a model, what can I do? A wide variety of resources are available for creating models, from labs and tutorials, to automated model generation tools like eIQ Time Series Studio, eIQ Model Creator, Google Cloud AutoML, Microsoft Azure Machine Learning, or Amazon ML Services, to 3 rd party partners like ModelCat, SensiML and Au-Zone that can help you define, enhance, and create a model for your specific application. I’m interested in anomaly detect or time series models on microcontrollers, where can I get started? The eIQ Time Series Studio (TSS) tool is perfect for getting started with time series or anomaly detection models. It allows you to import time series datasets, generate models, and deploy them to NXP microcontrollers.  There is also ML-based System State Monitor Application Software Pack which provides an example of gathering time-series data, in this case vibrations picked up by an accelerometer, and includes Python scripts to use the data that was collected to generate a small model that can be deployed on many different microcontrollers (including i.MX RT1170, LPC55S69, K66F) for anomaly detection. The same concepts and technique can be used for any sort of times series data like magnetometers, pressure, temperature, flow speed, and much more. This can simplify the work of coming up with a customer algorithm to detect the different states of whatever system you're interested in, as you can let the power of machine learning figure all that out for you.  There is also an on-device trained anomaly detection model example that can be found on the Application Code Hub.     Troubleshooting: Why do I get an error when running Tensorflow Lite Micro that it "Didn't find op for builtin opcode"? The full error will look something like this: Didn't find op for builtin opcode 'PAD' version '1' Failed to get registration from op code ADD Failed starting model allocation. AllocateTensors() failed Failed initializing model The reason is that with MCUXpresso SDK, the TFLM examples have been optimized to only support the operands necessary for the default models. If you are using your own model, it may use extra types of operands. To fix this issue, add that operator to MODEL_GetOpsResolver function found in source\model\model_name_ops_npu.cpp Also make sure to also increase the size of the static array s_microOpResolver to match the number of operators.  If the model is converted using the Neutron Compiler tool then a list of all the operators used by that model can be generated by using the --dump-header-file-input or --dump-header-file-output arguments.    Why do I get the error “Internal Neutron NPU driver error 281b in model prepare!” or "Incompatible Neutron NPU microcode and driver versions!" when using the Neutron NPU? The version of the eIQ Neutron Compiler Tool needs to be compatible with the NPU libraries used by your project. You should update the eIQ Neutron Library to match the Neutron Compiler version that was used as described in this Community post on How to Update eIQ Projects with the Latest eIQ Neutron SDK Libraries   Why do I get the warning message "Unable to save model handle, call neutronModelUnprepare() when done" when using eIQ Neutron SDK 3.1.2?  This warning is not relevant for Neutron C devices like RT700 and MCX N and can be ignored as it does not impact inference time or accuracy. It will be fixed in the next eIQ Neutron SDK release.   Why do I get a blank or black LCD screen when I use the eIQ demos that have camera+LCD support on RT1170 or RT1160? There are different versions of the LCD, so you need to make sure you have the software configured correctly for the LCD you have. See this post for more details on what to change.   Older issues involving the deprecated eIQ Toolkit: Sometimes in eIQ Toolkit the Validation page hangs and it stays stuck on "Converting Model". How do I work around this?  On the Validation section of the wizard, you will need to wait for the "Input Data Type" and "Output Data Type" selection boxes to be populated before clicking on the "Validation" button at the bottom. It may take a minute or two for those selection boxes to pop up on the left hand side. Once they do, then click on Validate and it should no longer hang.  How do I use my GPU when training with eIQ Toolkit? eIQ Toolkit 1.10 only supports GPU training on Linux due to the latest TensorFlow versions no longer supporting GPU on Windows.  There is a Javascript error in Time Series Studio when I start the training.  There is a bug in older versions of Time Series Studio where if the eIQ Portal window is closed after opening the Time Series Studio then that error comes up. Try relaunching Time Series Studio but keep the original eIQ Portal window open. Note that this is no longer an issue with the standalone Time Series Studio since mid 2025.  The eIQ Time Series Studio in eIQ Toolkit v1.17 is v1.3.4 but it says there's a newer version?  The eIQ Toolkit v1.17 contains an older version of eIQ Time Series Studio. The latest version can always be found on the eIQ Time Series Studio website.   General AI/ML: What is Artificial Intelligence, Machine Learning, and Deep Learning? Artificial intelligence is the idea of using machines to do “smart” things like a human. Machine Learning is one way to implement artificial intelligence, and is the idea that if you give a computer a lot of data, it can learn how to do smart things on its own. Deep Learning is a particular way of implementing machine learning by using something called a neural network. It’s one of the more promising subareas of artificial intelligence today.   This video series on Neural Network basics provides an excellent introduction into what a neural network is and the basics of how one works.    What are some uses for machine learning on embedded systems? Image classification – identify what a camera is looking at Coffee pods Empty vs full trucks Factory defects on manufacturing line Produce on supermarket scale Facial recognition – identifying faces for personalization without uploading that private information to the cloud Home Personalization Appliances Toys Auto Audio Analysis Wake-word detection Voice commands Alarm Analytics (Breaking glass/crying baby) Anomaly Detection Identify factory issues before they become catastrophic Motor analysis Personalized health analysis   What is training and inference? Machine learning consists of two phases: Training and Inference   Training is the process of creating and teaching the model. This occurs on a PC or in the cloud and requires a lot of data to do the training. eIQ is not used during the training process.   Inference is using a completed and trained model to do predictions on new data. eIQ is focused on enhancing the inferencing of models on embedded devices.   What are the benefits for “on the edge” inference? When inference occurs on the embedded device instead of the cloud, it’s called “on the edge”. The biggest advantage of on the edge inferencing is that the data being analyzed never goes anywhere except the local embedded system, providing increased security and privacy. It also saves BOM costs because there’s no need for WiFi or BLE to get data up to the cloud, and there’s no charge for the cloud compute costs to do the inferencing.  It also allows for faster inferencing since there’s no latency waiting for data to be uploaded and then the answer received from the cloud.   What processor do I need to do inferencing of models? Inferencing simply means doing millions of multiple and accumulate math calculations – the dominant operation when processing any neural network -, which any MCU or MPU is capable of. There’s no special hardware or module required to do inferencing. However specialized ML hardware accelerators, high core clock speeds, and fast memory can drastically reduce inference time.   Determining if a particular model can run on a specific device is based on: How long will it take the inference to run. The same model will take much longer to run on less powerful devices. The maximum acceptable inference time is dependent on your particular application. Is there enough non-volatile memory to store the weights, the model itself, and the inference engine Is there enough RAM to keep track of the intermediate calculations and output   As an example, the performance required for image recognition will be very dependent on the model is being used to do image recognition. This will vary depending on how many classes, what size of images to be analyzed, if multiple objects or just one will be identified, and how that particular model is structured. In general image classification can be done on i.MX RT devices and multiple object detection requires i.MX devices, as those models are significantly more complex.   eIQ provides several examples of image recognition for i.MX RT and i.MX devices and your own custom models can be easily evaluated using those example projects.    How is accuracy affected when running on slower/simpler MCUs? The same model running on different processors will give the exact same result if given the same input. It will just take longer to run the inference on a slower processor.   In order to get an acceptable inference time on a simpler MCU, it may be necessary to simplify the model, which will affect accuracy. How much the accuracy is affected is extremely model dependent and also very dependent on what techniques are used to simplify the model.   What are some ways models can be simplified? Quantization – Transforming the model from its original 32-bit floating point weights to 8-bit fixed point weights. Requires ¼ the space for weights and fixed point math is faster than floating point math. Often does not have much impact on accuracy but that is model dependent. Fewer output classifications can allow for a simpler yet still accurate model Decreasing the input data size (e.g. 128x128 image input instead of 256x256) can reduce complexity with the trade-off of accuracy due to the reduced resolution. How much that trade-off is depends on the model and requires experimentation to find. Software could rotate image to specific position using classic image manipulation techniques, which means the neural network for identification can be much smaller while maintaining good accuracy compared to case that neural network has to analyze an image that could be in all possible orientations.   What is the difference between image classification, object detection, and instance segmentation? Image classification identifies an entire image and gives a single answer for what it thinks it is seeing. Object detection is detecting one or more objects in an image. Instance segmentation is finding the exact outline of the objects in an image.   Larger and more complex models are needed to do object detection or instance segmentation compared to image classification.         What is the difference between Facial Detection and Facial Recognition? Facial detection finds any human face. Facial recognition identifies a particular human face. A model that does facial recognition will be more complex than a model that only does facial detection.      How come I don’t see 100% accuracy on the data I trained my model on? Models need to generalize the training data in order to avoid overfitting. This means a model will not always give 100% confidence , even on the data a model was trained on.   What are some resources to learn more about machine learning concepts?  Video series on Neural Network basics  ARM Embedded Machine Learning for Dummies Google TensorFlow Lab Google Machine Learning Crash Course Google Image Classification Practica YouTube series on the basics of ML and TensorFlow (ML Zero to Hero Series)
View full article
   The eIQ Sample Apps repository hosts Machine Learning applications demos based on the eIQ ™ ML Software Development Environment. The following examples were tested and used for training purposes. To be understandable each application contains a read-me file allowing the user to get started with the eIQ demos.    The eIQ samples apps target the latest eIQ release and are split in labs sections. Before starting with the examples, read the introduction part: eIQ Sample Apps - Introduction Object Recognition using Arm NN This section contains samples for running inference and predicting different objects. It also includes an extension that can recognize any given camera input/object. eIQ Sample Apps - Object Recognition using Arm NN Handwritten Digit Recognition This section focuses on a comparison of inference time between different models for handwritten digits recognition. eIQ Sample Apps - Handwritten Digit Recognition Object Recognition using OpenCV DNN This section uses OpenCV DNN module for running inference and detecting objects from an image. It also includes an extension that can detect any given camera input/object. eIQ Sample Apps - Object Recognition using OpenCV DNN Face Recognition using TensorFlow Lite This section uses a model for running inference and recognizing faces. eIQ Sample Apps - Face Recognition using TF Lite TensorFlow Lite Quantization This tutorial demonstrates how to convert a TensorFlow model to TensorFlow Lite and then apply quantization. eIQ Sample Apps - TFLite Quantization TensorFlow Transfer Learning This lab takes a TensorFlow image classification model and re-trains it to categorize images of flowers.  eIQ Transfer Learning Lab with i.MX 8 To deploy the demos from the eIQ Sample Apps repository to an i.MX8 board, please check: Deploying the eIQ Sample Apps to an i.MX8 board  These labs sections will be updated frequently in order to keep all codes and tutorials up-to-date. Check also: https://community.nxp.com/community/eiq/blog/2020/06/30/pyeiq-a-python-framework-for-eiq-on-imx-processors 
View full article
This lab will cover how to take an existing TensorFlow Lite model and run it on NXP MCU devices using the TensorFlow Lite for Microcontrollers inference engine and the eIQ examples found in MCUXpresso SDK. The labs use a model trained on flower photos but the same concepts could be extended to any type of TFLite model.    This lab was written for i.MX RT1170 but the same concepts can be applied to any eIQ supported board including: FRDM-MCXN947 i.MX RT685-EVK i.MX RT595-EVK i.MX RT700-EVK i.MX RT1050-EVKB i.MX RT1060-EVK i.MX RT1064-EVK i.MX RT1160-EVK i.MX RT1170-EVK i.MX RT1170-EVKB i.MX RT1180-EVK   There is also a supplemental lab for how to use the HiFi4 examples to run models on i.MX RT700 and i.MX RT685.    --- Updated February 2026 to add both VS Code and MCUXpresso IDE lab options
View full article
The attached labs provide a step-by-step guide on how to use the eIQ for Glow Neural Network compiler with a handwritten digit recognition model example. This compiler tool turns a model into an machine executable binary for a targeted device. Both the model and the inference engine are compiled into a binary that is generated, which can decrease both inference time and memory usage. That binary can then be integrated into an MCUXpresso SDK software project.    The eIQ Glow Lab for RT1170.pdf can be used with the i.MX RT1170, RT1160, RT1064, RT1060, and RT1050 The eIQ Glow Lab for RT685.pdf can be used with the RT685.    A step-by-step video is also available You will need to download the Glow compiler tools package as well as the latest MCUXpresso SDK for the board you're using. More details on Glow can be found in the eIQ Glow Ahead of Time User Guide and the Glow website.  Updated August 2023
View full article
Welcome to PyeIQ PyeIQ gathers everything needed by itself. It provides a simplified way to run ML applications, which avoids the user spending time on preparing the environment. PyeIQ Version Release Date Notes tag_v1.0 Apr 29, 2020 - tag_v2.0 - Planned for June i.MX Board BSP Release Building Status 8 QM 5.4.3_2.0.0 passing 8 MPlus 5.4.3_2.0.0 passing This video is currently being processed. Please try again in a few minutes. (view in My Videos) Getting Started with PyeIQ 1. Easy Installation If you prefer to build the package by yourself go to Appendix Section or follow the README file at the PyeIQ repo. 1.1 Copy the PyeIQ pre-built package attached to the board, and then install it by using pip3 tool: 1.2 Check the installation by starting an interactive shell:   1.3 Import PyeIQ and see the version: The output is the PyeIQ latest version installed in the system. (Optional) Install the following package to show downloading status: 2. Easy Running All demos and applications are automatically installed in /opt/eiq. 2.1 To run the demos: 2.2 To run the applications: 2.3 Use help if needed: 3. List of Available Demos and Applications Demo/App Name Demo/App Type i.MX Board BSP Release BSP Framework Inference Status Notes Label Image File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Label Image Switch File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Object Detection SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing Need better model. Object Detection OpenCV SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing Need better model. Object Detection N. GS. SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Object Detection Yolov3 SSD/File QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Object Detection Yolov3 SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Fire Detection File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Fire Detection Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Fire Detection Camera - 5.4.3_2.0.0 PyArmNN 19.08 - - Requires 19.11 Coral Posenet Camera - - - - - Ongoing NEO DLR Camera - - - - - Ongoing 4. Examples 4.1 Fire Detection Image 4.1.1 Non-fire Running Fire Detect Image:     Output: INFO: Created TensorFlow Lite delegate for NNAPI.                                                                        Applied NNAPI delegate.                                                                                                  Inference time: 0:00:00.264853                                                                                           Non-Fire   4.1.2 Fire Running Fire Detect Image: Output: INFO: Created TensorFlow Lite delegate for NNAPI.                                                                        Applied NNAPI delegate.                                                                                                  Inference time: 0:00:00.193055                                                                                           Fire    4.2 Fire Detection Camera Running Fire Detect Camera: Output: PyeIQ also supports training for Fire Detection demo, please refer to PyeIQ - Training and Conversion Support (Keras/TensorFlow Lite) . 4.3 Label Image Switch Running Switch Label Image: Output: Cores Comparison (CPU, GPU and NPU) Check the following graphical plot for Switch Label Image demo: Check the following graphical plot for the other demos: We are currently working to reduce the inference time on Fire Detection demos. Appendix Section The procedures described in this document target a GNU/Linux Distribution Ubuntu 18.04. 1. Software Requirements 1.1 Install the following packages in the GNU/Linux system: 1.2 Then, use pip3 tool to install the virtualenv tool: 2. Building the PyeIQ Package 2.1 Clone the repository: 2.2 Use virtualenv tool to create an isolated Python environment: 2.3 Generate the PyeIQ package: 2.4 Copy the package to the board: 2.5 To deactivate the virtual environment: Contact Feel free to contact us about any issue/bug you might have it. Your feedback is very welcome so we can improve the next version Alifer Moraes diegodorta marcofranchi
View full article
MCUXpresso SDK 2.10 for RT1064 now includes eIQ projects for all eIQ inference engines and so this Knowledge Base article is now depreciated. The instructions are being left up however in case any users using older versions of the SDK before i.MX RT1064 eIQ was fully supported need these steps in the future. Users with a i.MX RT1064 EVK should just use SDK 2.10 or later which has all the eIQ projects natively for i.MX RT1064.        1. Import an i.MX RT1060 project into the SDK. For this example, we'll use the Label Image demo.    2. Right click on the project in the workspace and select Properties.      3. Open the C/C++ Build -> MCU Settings page   4. Change the "Location" of the BOARD_FLASH parameter to 0x70000000 which is where the flash is located on the RT1064. Also adjust the size to be 0x400000. You will need to type it out.      5. Then you need to change the "Driver" parameter so the debugger knows to use the flash algorithm for the RT1064 board. Click on that field and you will see a "..." icon come up. Click on it.      6. Change the Flash driver to MIMXRT1064.cfx     7. Click on OK to close the dialog box, then click on Apply and Close to close the Properties dialog box.        8. Next we need to modify the MPU settings for the new flash address.    9. Open up board.c file. Modify the lines below to change the memory address and the memory size on lines 322 and 323 to start at 0x70000000 and for a 4MB region size.      9. Next, modify the clock settings code to ensure that FlexSPI2 is enabled. The clock setup code in the RT1060 SDK disables FlexSPI2, so we need to comment out that code in order to run the example on the RT1064. Open up clock_config.c file and comment out lines 264, 266, and 268.   10. Finally, open the fsl_flexpi_nor_boot.h file and modify the FLASH_BASE define to use FlexSPI2_AMBA_BASE on line 103     11. Compile and debug the project like normal and this project will now run on the RT1064 board.    Updated July 2021 for SDK 2.10 release. 
View full article
This docker is designed to enable portability to leverage i.MX 8 series GPUs. It enables flexibility on top of the Yocto image and allows the use of libraries available in Ubuntu for machine learning, which is otherwise difficult. Using docker, a user can develop and prototype GPU applications and then ship and run it anywhere using the container. This App note describes how to enable this Docker. The docker is a wrapper that provides an application with the necessary dependencies to execute code on the GPU. This is a significant achievement and has the potential to greatly simplify many customer developments for Linux. We keep the Yocto BSP intact, but customers can develop applications using the widely available neural network frameworks and libraries at the same time leveraging the GPU without compromising on performance. Not quite as straightforward as full up Debian but still should be an easy sell. marcofranchi‌ diegodorta‌
View full article
This Lab 4 explains how to get started with TensorFlow Lite application demo on i.MX8 board using Inference Engines for eIQ Software. eIQ Sample Apps - Overview eIQ Sample Apps - Introduction Get the source code available on code aurora: TensorFlow Lite MobileFaceNets MIPI/USB Camera Face Detection Using OpenCV   This application demo uses Haar Feature-based Cascade Classifiers for real time face detection. The pre-trained Haar Feature-based Cascade Classifiers for face, named as XML, is already contained in OpenCV. The XML file for face is stored in the opencv/data/haarcascades/ folder as well as code aurora. Read Face Detection using Haar Cascades for more details. TensorFlow Lite implementation for MobileFaceNets  The MobileFaceNets is re-trained on a host PC with a smaller batch size and input size to get higher performance. The trained model is loaded as a source file in this demo. Setting Up the Board Step 1 - Download the demo from eIQ Sample Apps and put it in /opt/tflite folder. Then enter the src folder: root@imx8mmevk:~# cd /opt/tflite/examples-tflite/face_recognition/src/ root@imx8mmevk:/opt/tflite/examples-tflite/face_recognition/src# This folder should include these files: . ├── face_detect_helpers.cpp ├── face_detect_helpers.h ├── face_detect_helpers_impl.h ├── face_recognition.cpp ├── face_recognition.h ├── haarcascade_frontalface_alt.xml ├── Makefile ├── mfn.h ├── profiling.h └── ThreadPool.h Step 2 - Compile the source code on the board: root@imx8mmevk:/opt/tflite/examples-tflite/face_recognition/src# make Step 3 - Run the demo: root@imx8mmevk:/opt/tflite/examples-tflite/face_recognition/src# ./FaceRecognition -c 0 -h 0.85 NOTE: -c is used to specify the camera index. '0' means the MIPI/USB camera is mounted on /dev/video0. -h is a threshold for the prediction score. Step 4 - Add a new person to the face data set.  When the demo is running, it will detect one biggest face at real time. Once the face is detected, you can click keyboards on the right of GUI to input the new person's name. Then, click 'Add new person' to add the face to data set.  In brief, 1. Detect face. 2. Input new person's name. 3. Click 'Add new person'. NOTE: Once new faces are added, it will create a folder named 'data' in current directory. If you want to remove the new face from the data set, just delete it in 'data'.
View full article
All the required steps for getting a full eIQ image can be found in the following documentation: NXP eIQ(TM) Machine Learning Enablement. These labs can be applied to all i.MX 8 boards, in this particular tutorial describes the i.MX 8M Mini EVK board. Hardware Requirements i.MX 8MM EVK board USB cable (micro-B to standard-A) USB Type-C to A Adapter USB Type-C 45W Power Delivery Supply IMX-MIPI-HDMI Daughter Card MINISASTOCSI Camera Daughter Card 2×Mini-SAS cable AI/ML BSP flashed into the SDCard Ethernet cable USB Mouse HDMI Cable Monitor Software Requirements For GNU/Linux: minicom or screen. For Windows: PuTTY. Preparing the Board Connect the IMX-MIPI-HDMI daughter card to the Mini-SAS cable and into connector labeled DSI MIPI (J801) and then connect the HDMI monitor cable into it. Warning: Do not hot-plug the Mini-SAS cables and cards or the boards will be damaged! Remove power completely before connecting or disconnecting the Mini-SAS ends. Connect the MINISASTOCSI camera daughter card to the Mini-SAS cable and into connector labeled CSI MIPI (J802). Connect the micro-B end of the supplied USB cable into Debug UART port J901. Connect the other end of the cable to the host computer: For GNU/Linux: Configure minicom or screen with the /dev/ttyUSB port number and set the baud rate to 115200. The port number can be found checking in /dev directory. For Windows: Configure PuTTY with the board COM port number and set the baud rate to 115200. The port number can be found on the Windows Device Manager. NOTE: This board mounts two device port numbers, use the highest number which is used to communicate with Cortex-A. Connect the MicroSD Card to the MicroSD Card Connector J701 in the board back side. In order to Boot the board from the MicroSD Card, change the Boot Switches SW1101 and SW1102 according to the table below: BOOT Device SW1101 SW1102 MicroSD / uSDHC2 0110110010 0001101000 NOTE: The boot device settings above apply to the revision C i.MX 8MM EVK board. Other revisions of the boards may have a different number of boot mode switches and slightly different settings. Please follow the SW1101 and SW1102 values printed on your specific board for booting from the MicroSD Card. Connect the power supply cable to the power connector J302 and power on the board by flipping the switch button SW101. NOTE: For more details on the board peripherals, please consult the i.MX 8MM EVK Getting Started. After these steps, it is all set to start with the eIQ Sample Apps. Go to the eIQ Sample Apps - Object Recognition using Arm NN.
View full article
This Lab 2 explains how to get started with MNIST Handwritten Digit application demo on i.MX8 board using eIQ ™ ML Software Development Environment. eIQ Sample Apps - Overview eIQ Sample Apps - Introduction Get the source code available on code aurora: Handwritten Digit Recognition MNIST Handwritten Digits The MNIST is a large database of handwritten digits commonly used for training various image processing systems. This section provides a comparison of Caffe and TensorFlow models for Handwritten Digit Recognition. The data set used for these applications is from Yann Lecun. This is an MNIST data set sample: Setting Up the Board Step 1 - Create the following folder and grant it permission as it follows: root@imx8mmevk:~# mkdir -p /opt/mnist root@imx8mmevk:~# chmod 777 /opt/mnist   Step 2 - To easily deploy the demos to the board, get the board's IP address using ifconfig command, then set the IMX_INET_ADDR environment variable as follows: $ export IMX_INET_ADDR=<imx_ip>   Setting Up the Host Step 1 - Obtain the eIQ toolchain (3.2.9.Generating the Toolchain) from NXP eIQ(TM) Machine Learning Enablement. Step 2 - Install the toolchain: $ chmod +x <toolchain>.sh $ ./<toolchain>.sh This provides all the needed setup for building ARM64 applications on a x86 machine. Step 3 - Download the application from eIQ Sample Apps. Step 4 - Get the models and dataset. The following command-lines create the needed folder structure for the demos and retrieves the mnist dataset, and the Caffe and TensorFlow models: $ mkdir -p bin data model $ wget -qN https://github.com/ARM-software/ML-examples/raw/master/armnn-mnist/data/t10k-images-idx3-ubyte -P data/ $ wget -qN https://github.com/ARM-software/ML-examples/raw/master/armnn-mnist/data/t10k-labels-idx1-ubyte -P data/ $ wget -qN https://github.com/ARM-software/ML-examples/raw/master/armnn-mnist/model/lenet_iter_9000.caffemodel -P model/ $ wget -qN https://github.com/ARM-software/ML-examples/raw/master/armnn-mnist/model/simple_mnist_tf.pb -P model/ $ wget -qN https://github.com/ARM-software/ML-examples/raw/master/armnn-mnist/model/simple_mnist_tf.prototxt -P model/ $ wget -qN https://github.com/ARM-software/Tool-Solutions/raw/master/ml-tool-examples/mnist-draw/model/optimized_mnist_tf.pb -P model/ Step 5 - Compile the source code using the eIQ toolchain: $ ${CXX} -Wall -Wextra -O3 -std=c++14 caffe_inference.cpp -o caffe_inference -larmnn -larmnnCaffeParser $ ${CXX} -Wall -Wextra -O3 -std=c++14 tensorflow_inference.cpp -o tensorflow_inference -larmnn -larmnnTfParser Step 6 - Deploy the built files to the board: $ scp -r caffe_inference tensorflow_inference data/ model/ root@${IMX_INET_ADDR}:/opt/mnist Inference Comparison Applications Step 1 - At user space, enter the mnist folder which holds the demo files: root@imx8mmevk:/opt/mnist# This is how the mnist folder structure should look like: │... ├── caffe_inference ├── tensorflow_inference ├── data │├── t10k-images-idx3-ubyte │└── t10k-labels-idx1-ubyte ├── model │├── lenet_iter_9000.caffemodel │├── optimized_mnist_tf.pb │├── simple_mnist_tf.pb │└── simple_mnist_tf.prototxt Step 2 - Run the applications: NOTE: For running these applications, please provide the wanted number of predictions, which can vary from 0 to 9999 since the dataset has 10K images. 1 - Handwritten Digit Recognition using Caffe root@imx8mmevk:/opt/mnist# ./caffe_inference 10 [0] Caffe >> Actual: 7 Predict: 7 Time: 0.0336484s [1] Caffe >> Actual: 2 Predict: 2 Time: 0.028399s [2] Caffe >> Actual: 1 Predict: 1 Time: 0.0283713s [3] Caffe >> Actual: 0 Predict: 0 Time: 0.0284133s [4] Caffe >> Actual: 4 Predict: 4 Time: 0.0280637s [5] Caffe >> Actual: 1 Predict: 1 Time: 0.0281574s [6] Caffe >> Actual: 4 Predict: 4 Time: 0.0285136s [7] Caffe >> Actual: 9 Predict: 9 Time: 0.0283779s [8] Caffe >> Actual: 5 Predict: 5 Time: 0.0283902s [9] Caffe >> Actual: 9 Predict: 9 Time: 0.0283282s Total Time: 0.296081s Sucessfull: 10 Failed: 0 2 - Handwritten Digit Recognition using TensorFlow root@imx8mmevk:/opt/mnist# ./tensorflow_inference 10 [0] Tensor >> Actual: 7 Predict: 7 Time: 0.00670075s [1] Tensor >> Actual: 2 Predict: 2 Time: 0.00377025s [2] Tensor >> Actual: 1 Predict: 1 Time: 0.0036785s [3] Tensor >> Actual: 0 Predict: 0 Time: 0.0036815s [4] Tensor >> Actual: 4 Predict: 4 Time: 0.00372875s [5] Tensor >> Actual: 1 Predict: 1 Time: 0.003669s [6] Tensor >> Actual: 4 Predict: 4 Time: 0.00367825s [7] Tensor >> Actual: 9 Predict: 9 Time: 0.0036955s [8] Tensor >> Actual: 5 Predict: 6 Time: 0.00367488s FAILED [9] Tensor >> Actual: 9 Predict: 9 Time: 0.0036025s Total Time: 0.0414569s Sucessfull: 10 Failed: 1 NOTE: The argument 10 refers to the number of predictions for each test. These tests run the inference on the input MNIST dataset images (Actual), showing the inference results (Predict) and how long it took to complete the prediction. The input images for this test are in the binary form and can be found at the t10k-images-idx3-ubyte.gz package from Yann Lecun. By the output results, it is possible to notice that the Caffe model is slower than TensorFlow, however, it is also more accurate than the latter. Change the argument to compare further results between the two models. Go to the eIQ Sample Apps - Object Recognition using OpenCV DNN.
View full article
After setting up an Yocto build environment as described in the L4.19.35_1.0.0 BSP Yocto Project User's Guide, apply the attached patch to the meta-fsl-bsp-release layer: <yocto_dir>/sources/meta-fsl-bsp-release$ git am eiq-sample-apps-Add-recipe.patch To include the applications in the image, add the following line to local.conf: IMAGE_INSTALL_append += "eiq-sample-apps" This will include all applications from the eIQ Sample Apps repository to the built image.
View full article
Convolutional Neural Networks are the most popular NN approach to image recognition. Image recognition can be used for a wide variety of tasks like facial recognition for monitoring and security, car vision for safety and traffic sign recognition or augmented reality. All of these tasks require low latency, great security, and privacy, which can’t be guaranteed when using Cloud-based solutions. NXP eIQ makes it possible to run Deep Neural Network inference directly on an MCU. This enables intelligent, powerful, and affordable edge devices everywhere.   As a case study about CNNs on MCUs, a handwritten digit recognition example was created. It runs on the i.MX RT1060 and uses an LCD touch screen as the input interface. The application can recognize digits drawn with a finger on the LCD.   Handwritten digit recognition is a popular “hello world” project for machine learning. It is usually based on the MNIST dataset, which contains 70000 images of handwritten digits. Many machine learning algorithms and techniques have been benchmarked on this dataset since its creation. Convolutional Neural Networks are among the most successful.   The code is also accompanied by an application note describing how it was created and explaining the technologies it uses. The note talks about the MNIST dataset, TensorFlow, the application’s accuracy and other topics.     Application note URL: https://www.nxp.com/docs/en/application-note/AN12603.pdf (can be found at the documentation page for the i.MX RT1060)   Application code is in the attached zip files: *_eiq_mnist is the basic application from the first image and *_eiq_mnist_lock is the extended version from the second image. The applications are provided in the form of MCUXpresso projects and require an existing installation of the i.MX RT1060/RT1170 SDK with the eIQ component included.   The software for this AN was also ported to CMSIS-NN with a Caffe version of the MNIST model in a follow up AN, which can be found here: https://www.nxp.com/docs/en/application-note/AN12781.pdf 
View full article
This lab will walk through how to use eIQ Time Series Studio (TSS) to create time series models for embedded microcontrollers.  It covers how to import time series data, shows how the tool can generate multiple machine learning (ML) algorithms, and describes how to deploy those generated models to your development board. eIQ Time Series Studio is available as a standalone installer or via a web interface.  This lab uses the FRDM-MCXN947 but the same steps will apply to any of the devices supported by eIQ Time Series Studio. You can also use NXP devices not listed here by selecting the closest related device family while going through the lab: MCX FRDM-MCXA156 FRDM-MCXC444 FRDM-MCXE247 FRDM-MCXN236 FRDM-MCXN947 FRDM-MCXW71 i.MX RT i.MXRT700-EVK i.MXRT685-EVK i.MXRT595-EVK MIMXRT1060-EVK MIMXRT1170-EVK MIMXRT1180-EVK i.MX6 MCIMX6ULL-EVK i.MX8 8MPLUSLPD4-PEVK i.MX9 i.MX93EVK RW FRDM-RW612 LPC LPC55S69-EVK Kinetis FRDM-K66F FRDM-KV31F FRDM-K32L3A6 DSC MC56F83000-EVK MC56F80000-EVK   The labs are written for either VS Code or MCUXpresso IDE, but the same concepts can be used for other IDEs.    You can also view the video below for a quick overview of the Time Series Studio process.  Also check out the ML Universal Datalogger on the App Code Hub for a tool to collect sensor data that can be used with the Time Series Studio, as well as the Time Series Studio examples on App Code Hub. Also see this document for details on how to add TSS libraries to existing projects.  --- Updated September 2026 to clarify supported devices. 
View full article
This Lab 3 explains how to get started with OpenCV DNN applications demos on i.MX8 board using eIQ ™ ML Software Development Environment. eIQ Sample Apps - Overview eIQ Sample Apps - Introduction Get the source code available on code aurora: OpenCV DNN example - File-Based and MIPI Camera OpenCV Inference The OpenCV offers a unitary solution for both neural network inference (DNN module) and classic machine learning algorithms (ML module). Moreover, it includes many computer vision functions, making it easier to build complex machine learning applications in a short amount of time and without having dependencies on other libraries. The OpenCV DNN model is basically an inference engine. It does not aim to provide any model training capabilities. For training, one should use dedicated solutions, such as machine learning frameworks. The inference engine from OpenCV supports a wide set of input model formats: TensorFlow, Caffe, Torch/PyTorch. Comparison with Arm NN Arm NN is a library deeply focused on neural networks. It offers acceleration for Arm Neon, while Vivante GPUs are not currently supported. Arm NN does not support classical non-neural machine learning algorithms. OpenCV is a more complex library focused on computer vision. Besides image and vision specific algorithms, it offers support for neural network machine learning, but also for traditional non-neural machine learning algorithms. OpenCV is the best choice in case your application needs a neural network inference engine, but also other computer vision functionalities. Setting Up the Board Step 1 - Create the following folders and grant them permissions as it follows: root@imx8mmevk:# mkdir -p /opt/opencv/model root@imx8mmevk:# mkdir -p /opt/opencv/media root@imx8mmevk:# chmod 777 /opt/opencv Step 2 - To easily deploy the demos to the board, get the boards IP address using ifconfig command, then set the IMX_INET_ADDR environment variable as it follows: $ export IMX_INET_ADDR=<imx_ip> Step 3 - In the target device, export the required variables: root@imx8mmevk:~# export LD_LIBRARY_PATH=/usr/local/lib root@imx8mmevk:~# export PYTHONPATH=/usr/local/lib/python3.5/site-packages/   Setting Up the Host Step 1 - Download the application from eIQ Sample Apps. Step 2 - Get the models and dataset. The following command-line creates the needed folder structure for the demos and retrieves all needed data and model files for the demo: $ mkdir -p model $ wget -qN https://github.com/diegohdorta/models/raw/master/caffe/MobileNetSSD_deploy.caffemodel -P model/ $ wget -qN https://github.com/diegohdorta/models/raw/master/caffe/MobileNetSSD_deploy.prototxt -P model/   Step 3 - Deploy the built files to the board: $ scp -r src/* model/ media/ root@${IMX_INET_ADDR}:/opt/opencv OpenCV DNN Applications This application was based on: SSD: Single Shot MultiBox Detector. Caffe SSD Implementation. 1 - OpenCV DNN example: File-Based The folder structure must be equal to: ├── file.py ├── camera.py ├── media └── ... ├── model │├── MobileNetSSD_deploy.caffemodel │└── MobileNetSSD_deploy.prototxt This example runs a single picture for example, but you pass as many pictures as you want and save them inside media/ folder. The application tries to recognize all the objects in the picture. Step 1 - For copying new images to the media/ folder: root@imx8mmevk:/opt/opencv/media# cp <path_to_image> .   Step 2 - Run the example image: root@imx8mmevk:/opt/opencv# ./file.py  NOTE: If GPU is available, the example shows: [INFO:0] Initialize OpenCL runtime This demo runs the inference using a Caffe model to recognize a few type of objects for all the images inside the media/ folder. It includes labels for each recognized object in the input images. The processed images are available in the media-labeled/ folder. See before and after labeling: Step 3 - Display the labeled image with the following line: root@imx8mmevk:/opt/opencv/media-labeled# gst-launch-1.0 filesrc location=<image> ! jpegdec ! imagefreeze ! autovideosink 2 - OpenCV DNN example: MIPI Camera This example is the same as above, except that it uses a camera input. It enables the MIPI camera and runs an inference on each captured frame, then displays it in a window interface in real time: root@imx8mmevk:/opt/opencv# ./camera.py 3 - OpenCV DNN example: MIPI Camera improved This example differs from the above due the additional support of GStreamer applied to it. Using the Leaky Bucket algorithm idea, the GStreamer pipeline enables the camera to continue performing its own thread (bucket overflow when full), even if the frame was not processed by the inference thread (bucket water capacity). As a result of this Leaky Bucket algorithm, this demo has smooth camera video at the expense of having some frames dropped in the inference process. root@imx8mmevk:/opt/opencv# ./camera_improved.py Go to the eIQ Sample Apps - Face Recognition using TF Lite.
View full article
This Lab 1 explains how to get started with Arm NN application demo on i.MX8 board using eIQ ™ ML Software Development Environment. eIQ Sample Apps - Overview eIQ Sample Apps - Introduction Get the source code available on code aurora: Arm NN example - File-Based and MIPI Camera Setting Up the Board Step 1 - Create the following folders and grant them permission as it follows: root@imx8mmevk:# mkdir -p /opt/armnn/model root@imx8mmevk:# mkdir -p /opt/armnn/data root@imx8mmevk:# chmod 777 /opt/armnn Step 2 - To easily deploy the demos to the board, get the boards IP address using ifconfig command, then set the IMX_INET_ADDR environment variable as it follows: $ export IMX_INET_ADDR=<imx_ip> Setting Up Arm NN Step 1 - Install TensorFlow on host PC for preparing the model for inference: $ apt-get install python-pip $ pip install tensorflow $ git clone https://github.com/tensorflow/tensorflow.git NOTE: You may need root privileges (sudo) for running the apt-get command. Step 2 - Generate the graph used to prepare the TensorFlow InceptionV3 model for inference: $ mkdir checkpoints $ git clone https://github.com/tensorflow/models.git $ cd models/research/slim/ $ python export_inference_graph.py --model_name=inception_v3 --output_file=../../../checkpoints/inception_v3_inf_graph.pb   Step 3 - Download the pre-trained model and prepare it for inference with the generated graph: $ cd ../../../checkpoints $ wget http://download.tensorflow.org/models/inception_v3_2016_08_28.tar.gz -qO- | tar -xvz # download pretrained model $ python <path_to_tensorflow_repo>/tensorflow/python/tools/freeze_graph.py \ --input_graph=inception_v3_inf_graph.pb --input_checkpoint=inception_v3.ckpt \ --input_binary=true --output_graph=inception_v3_2016_08_28_frozen_transformed.pb \ --output_node_names=InceptionV3/Predictions/Reshape_1 NOTE: <path_to_tensorflow_repo> refers to the cloned TensorFlow path from Step 1. Step 4 - Copy the prepared model inception_v3_2016_08_28_frozen_transformed.pb to /opt/armnn/models: $ scp inception_v3_2016_08_28_frozen_transformed.pb root@<imx_ip>:/opt/armnn/model Step 5 - Find three .jpg images on Google, one containing a dog, one with a cat and one with a shark. Rename them to Dog.jpg, Cat.jpg and shark.jpg accordingly (case sensitive) and copy them to the /opt/armnn/data folder on the device. $ scp Dog.jpg Cat.jpg shark.jpg root@<imx_ip>:/opt/armnn/data NOTE: For the modified demo, download it from eIQ Sample Apps and put it in /opt/armnn folder. 1 - Arm NN example: File-Based Step 1 - At user space, enter the armnn folder which holds the demo files: root@imx8mmevk:~# cd /opt/armnn root@imx8mmevk:/opt/armnn# Here is what the armnn folders should look like: │... ├── data │├── Cat.jpg │├── Dog.jpg │└── shark.jpg ├── model │└── inception_v3_2016_08_28_frozen_transformed.pb │... Step 2 - Run the demo: root@imx8mmevk:/opt/armnn# TfInceptionV3-Armnn --data-dir=data --model-dir=models = Prediction values for test #0 Top(1) prediction is 208 with confidence: 93.5791% Top(2) prediction is 209 with confidence: 2.06653% Top(3) prediction is 223 with confidence: 0.693557% Top(4) prediction is 170 with confidence: 0.210818% Top(5) prediction is 232 with confidence: 0.177887% = Prediction values for test #1 Top(1) prediction is 283 with confidence: 72.4617% Top(2) prediction is 282 with confidence: 22.5384% Top(3) prediction is 286 with confidence: 0.838241% Top(4) prediction is 288 with confidence: 0.0822042% Top(5) prediction is 841 with confidence: 0.05987% = Prediction values for test #2 Top(1) prediction is 3 with confidence: 62.0632% Top(2) prediction is 4 with confidence: 12.8319% Top(3) prediction is 5 with confidence: 1.25482% Top(4) prediction is 154 with confidence: 0.177708% Top(5) prediction is 149 with confidence: 0.116998% Total time for 3 test cases: 2.369 seconds Average time per test case: 789.765 ms Overall accuracy: 1.000 The TfInceptionV3-Armnn demo runs the inference on the three expected input images: one containing a dog, one with a cat and one with a shark. The output shows the top 5 inference results and their confidence percentage. The higher the confidence, the better the input image fits the expected content. There is a chance to get the following result by running the demo: Prediction for test case 0 ( x ) is incorrect (should be y) One or more test cases failed NOTE: ( x ) refers to the ID of the detected object, ( y ) refers to the ID expected object. This is not an execution error. This occurs because the TfInceptionV3-Armnn test expects a specific type of dog, cat and shark to be found so if a different type/breed of these animals is passed to the test, it returns a case failed. The expected inputs for this test are: A_ID Label File Name 208 Golden Retriever Dog.jpg 283 Tiger Cat Cat.jpg 3 White Shark shark.jpg The complete list of supported objects can be found here. Try passing different .jpg images to the test, including the expected types as well as other types and see the confidence percentage increasing when you match the expected breeds. Remember to rename the images according to the expect input (Dog.jpg, Cat.jpg, shark.jpg, case sensitive). To rename a file, use the mv command: root@imx8mmevk:/opt/armnn/data# mv <name>.jpg <new_name>.jpg The next section shows how to modify this demo to identify any object. 2 - Arm NN example: MIPI Camera This section shows how to use the TfInceptionV3-Armnn test from eIQ for general object detection. The list of all object detection supported by this model can be found here. Step 1 - Enter the demo directory and run the demo: root@imx8mmevk:/opt/armnn# python3 camera.py This runs the TfInceptionV3-Armnn test and parses the inference results to return any recognized object, not only the three expected types of animals. Step 2 - Show the provided flash cards to the camera and wait for the detection message: Image captured, wait. The flash cards should not be twisted or curved on this step. Step 3 - After a few seconds, the demo returns the detected object. NOTE: This can return False if the image was not correctly captured. In this case, try showing the flash card again. This video is currently being processed. Please try again in a few minutes. (view in My Videos) Go to the next eIQ Sample Apps - Handwritten Digit Recognition.
View full article
This demo shows a low power smart door running eIQ heterogeneously on i.MX8MMini: Cortex A53 performs face recognition using eIQ OpenCV Cortex M4 performs Key Word Spotting using eIQ CMSIS-NN The demo application is build around the Django framework running on the board. It has two main usage scenarios: The first one is to manage users and inspect the access logs through a dashboard. This dashboard is accesses from a web browser on the host PC. The second use case is the smart door application itself running on the board. The scenario is the following: Cortex A cores and connected peripherals stay in low power mode. Cortex M is active, waiting for the Key Word ‘GO’. When the word is detected, Cortex M sends an MU interrupt to Cortex A and the system wakes up. Now Cortex A performs face recognition and allows access for registered users. In addition to face recognition, the MPUs are able to run a Django server to manage the user’s database, a QT5 application for the graphical interface and perform training on the edge. The algorithm for face recognition running on Cortex A and the one for key word spotting running on Cortex M are both implemented using eIQ. For the MPU eIQ support is integrated in Yocto. For the MCU the support was ported to i.MX8 from the MCU Expresso SDK for RT for the purpose of this demo. Software Environment Ubuntu 16 host PC SD card image with Yocto BSP 4.14.98/sumo 2.0.0 GA for i.MX8MMini platform with eIQ OpenCV AND eIQ heterogenus demo. See detailed steps in Build Yocto Image section CMSIS-NN MCUXpresso SDK version 2.6.0 for i.MX8MMini (SDK_2.6.0_EVK-MIMX8MM-ARMGCC). See detailed build steps in Build Cortex M4 executable section. HW Environment i.MX 8MMini Kit Touch screen display (preferred resolution 1920x1080). Tested with HDMI connection to the board. NOTE: if the display does not support touch, a mouse can be connected to the board and used instead MIPI-CSI Camera module Microphone: Synaptics CONEXANT AudioSmart® DS20921 Ribbon, 4 female-female wires and 60 pins connector to connect mic to board Optional: headphones (used to test recording on M4 - everything recorded by the mic will be played to the headphones). Host PC for remote access to the demo application (used Chrome browser) NOTE: The board and the host PC should be in the same network to communicate. Build Yocto image: Step 1 – Project initialization: $: mkdir imx-linux-bsp $: cd imx-linux-bsp-bsp $: repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_machinelearning.xml $: repo sync Step 2 - Setup Project build: $: MACHINE=imx8mmevk DISTRO=fsl-imx-xwayland source ./fsl-setup-release.sh -b bld-xwayland Step 3 – Download project layer in ${BSPDIR}/sources/: $: git clone https://source.codeaurora.org/external/imxsupport/meta-eiq-heterogenous Step 4 – Add project layer into bblayers: Add the following line into ${BSPDIR}/sources/base/conf/bblayers.conf: BBLAYERS += " ${BSPDIR}/sources/meta-eiq-heterogenous " Step 5 – Enable eIQ and other dependencies. Add the following lines into conf/local.conf: EXTRA_IMAGE_FEATURES = " dev-pkgs debug-tweaks tools-debug \ tools-sdk ssh-server-openssh" IMAGE_INSTALL_append = " net-tools iputils dhcpcd which gzip \ python3 python3-pip wget cmake gtest \ git zlib patchelf nano grep vim tmux \ swig tar unzip parted \ e2fsprogs e2fsprogs-resize2fs" IMAGE_INSTALL_append = " python3-pytz python3-django-cors-headers" IMAGE_INSTALL_append = " opencv python3-opencv" PACKAGECONFIG_append_pn-opencv_mx8 = " dnn python3 qt5 jasper \ openmp test neon" PACKAGECONFIG_remove_pn-opencv_mx8 = "opencl" TOOLCHAIN_HOST_TASK_append = " nativesdk-cmake nativesdk-make" PREFERRED_VERSION_opencv = "4.0.1%" PREFERRED_VERSION_python3-django = "2.1%" IMAGE_ROOTFS_EXTRA_SPACE = "20971520" Step 6 – Bake the image: $: bitbake image-eiq-hetero Build Cortex M4 executable Download MCUXpresso SDK version 2.6.0 for i.MX8MMini (SDK_2.6.0_EVK-MIMX8MM-ARMGCC) OS: Linux, Toolchain: GCC ARM Embedded Components: Amazon-FreeRTOS, CMSIS DSP Library, multicore SDK Version: 2.6.0 (2019-06-14) SDK Tag: REL_2.6.0_REL10_RFP_RC3_4 Download CMIS NN and copy "CMSIS\NN" folder to "$MCUXpressoSDK_ROOT\CMSIS" Got to "$MCUXpressoSDK_ROOT\boards\evkmimx8mm\demo_apps\" Get M4 app from CAF: git clone https://source.codeaurora.org/external/imxsupport/eiq-heterogenous-cortexm4 [Win]: Open ARM GCC console and go to "$MCUXpressoSDK_ROOT\boards\evkmimx8mm\demo_apps\eiq-heterogenous-cortexm4\armgcc\" [Win]: Call "build_ddr_release.bat" to obtain "eiq-kws.bin". Deploy "eiq-kws.bin" to the Yocto image on the boot partition. Prepare the Demo 1.  Connect 12V power supply to the board, switch SW101 to power on the board 2.  Connect a USB cable between the host PC and the J901 USB port on the target board. 3.  Open two serial terminals for A53 core and M4 core with the following settings:     - 115200 baud rate     - 8 data bits     - No parity     - One stop bit     - No flow control 4. Connect display to the board (used 1920x1080 HDMI display connected to the board with an IMX-MIPI-HDMI adapter). NOTE: depending on the display, you might want to change the config in "/etc/xdg/weston/weston.ini". The demo was tested by uncommenting the following section in this file: [output] name=HDMI-A-1 mode=1920x1080@60 transform=90 5.Connect MIPI-CSI camera to the board. 6. Connect Synaptics microphone to the board using a 60 pins connector with a ribbon. SAI3 is used for record and playback on Cortex M4. The following pins are used: Pin 44 (connector) <-> I2S_TX_Data1 (mic board) Pin 43 (connector) <-> I2S_TX_LRCLK (mic board) Pin 41 (connector) <-> I2S_TX_CLK (mic board) Pin 60 (connector) <-> GND (mic board) 7. Using U-Boot command to run the demo.bin file. For details, please refer to "Getting Started with MCUXpresso SDK for i.MX 8M Mini.pdf". 8.  After running the demo.bin, using the "boot" command to boot the kernel on the A core terminal; 9.  After the kernel is boot, using "root" to login. 10.  After login, make sure imx_rpmsg_pingpong kernel module is inserted (lsmod) or insert it (modprobe imx_rpmsg_pingpong). Run the Demo Start Key Word Spotting on Cortex M4: Stop in u-boot and run the eiq-kws.bin executable in DDR: u-boot=>fatload mmc 0 0x80000000 eiq-kws.bin u-boot=>dcache flush u-boot=>bootaux 0x80000000 u-boot=>boot After the boot process succeeds, the ARM Cortex-M4 terminal displays the following information: RPMSG Ping-Pong FreeRTOS RTOS API Demo... RPMSG Share Base Addr is 0xb8000000 During boot the Kernel,the ARM Cortex-M4 terminal displays the following information: Link is up! Nameservice announce sent. Start Face Recognition on Cortex-A: Insert updated rpmsg driver: $: modprobe imx_rpmsg_pingpong After the Linux RPMsg pingpong module was installed, the ARM Cortex-M4 terminal displays the following information: Looping forever... Waiting for ping... Sending pong... 96% go First time only: $: cd ~/eiq-heterogenous-cortexa $: python3 wrap_migrate.py $: python3 wrap_createsuperuser.py Start: $: cd ~/eiq-heterogenous-cortexa $: python3 manage.py runserver 0.0.0.0:8000 --noreload & $: /opt/src/bin/src NOTE: the first instruction will start the django server, the second instruction will show the pin-pad on the display. Browser access from HOST PC: - http://$BOARD_IP:8000/dashboard/😞 Dashboard that facilitates managing users and view access logs - http://$BOARD_IP:8000/admin/: manage users database  
View full article
The tools previously bundled as part of eIQ Toolkit are now released as standalone packages and eIQ Toolkit will no longer be updated after the eIQ Toolkit v1.17 in Q3 2025. Going forward the tools previously included in eIQ Toolkit can now be found at: eIQ Neutron SDK now contains the latest versions of the Neutron Compiler tool (previously called the Neutron Converter tool before Aug 2026) eIQ Time Series Studio can now be found in a standalone package eIQ Model Creator provides an option for vision based model creation eIQ AI Toolkit will provide model optimization functionality (Coming Soon) Netron provides TFLite model viewing functionality This article will remain up for existing users. --------- eIQ Toolkit enables machine learning development with an intuitive GUI (named eIQ Portal) and development workflow tools, along with command line host tool options as part of the eIQ ML software development environment. Developers can create, optimize, debug and export ML models, as well as import datasets and models, rapidly train and deploy neural network models and ML workloads. The eIQ Portal provides output TensorFlow Lite models that seamlessly feed into eIQ inference engines like TensorFlow Lite and TensorFlow Lite for Microcontrollers. Using a tool called Model Runner, eIQ Toolkit can also generate runtime insights to help optimize neural network architectures on i.MX RT and i.MX devices. These labs go over how to use eIQ Portal. It is recommended to do them in the following order: Data Import Lab Model Runner Lab   The labs are written for using a FRDM-MCXN947 and i.MX RT1170-EVK, but other eIQ supported devices can be used as well.  MCX N i.MX RT1050 i.MX RT1060 i.MX RT1064 i.MX RT1160 i.MX RT1170 i.MX RT1180 i.MX RT500 i.MX RT600 For details on the Time Series Studio tool please see the Time Series Studio lab guides. For 
View full article
UPDATE: Note that this document describes eIQ Machine Learning Software for the NXP L4.14 BSP release. Beginning with the L4.19 BSP, eIQ Software is pre-integrated in the BSP release and this document is no longer necessary or being maintained. For more information on eIQ Software in these releases (L4.19, L5.4, etc), please refer to the "NXP eIQ Machine Learning" chapter in the Linux User Guide for that specific release.  Original post: eIQ Machine Learning Software for iMX Linux 4.14.y kernel series is available now. The NXP eIQ™ Machine Learning Software Development Environment enables the use of ML algorithms on NXP MCUs, i.MX RT crossover processors, and i.MX family SoCs. eIQ software includes inference engines, neural network compilers, and optimized libraries and leverages open source technologies. eIQ is fully integrated into our MCUXpresso SDK and Yocto development environments, allowing you to develop complete system-level applications with ease. Source download, build and installation Please refer to document NXP eIQ(TM) Machine Learning Enablement (UM11226.pdf) for detailed instructions on how to download, build and install eIQ software on your platform. Sample applications To help get you started right away we've posted numerous howtos and sample applications right here in the community. Please refer to eIQ Sample Apps - Overview. Supported platforms eIQ Machine learning software for i.MX Linux 4.14.y supports the L4.14.78-1.0.0 and L4.14.98-2.0.0 GA releases running on i.MX 8 Series Applications Processors. For more information on artificial intelligence, machine learning and eIQ Software please visit AI & Machine Learning | NXP.
View full article
This lab will take an existing TensorFlow image classification model and re-train it to categorize images of flowers. This is known as transfer learning. This updated model will then be converted into a TensorFlow Lite file. By using that file with the TensorFlow Lite inference engine that is part of NXPs eIQ package, the model can be ran on an i.MX 8QM-MEK board. This lab can also be used with different i.MX 8 devices.   Please check attached pdf's: 'eIQ Transfer Learning Lab iMX8.pdf': detailed lab instructions 'TransferLearningOverview.pdf': theoretical background of transfer learning and results for customized data set.   Please check also: eIQ Transfer Learning Lab with i.MX RT.
View full article
Transfer learning is one the most important techniques in machine learning. It gives machine learning models the ability to apply past experience to quickly and more accurately learn to solve new problems. This approach is most commonly used in natural language processing and image recognition. However, even with transfer learning, if you don't have the right dataset, you will not get very far.   This application note aims to explain transfer learning and the importance of datasets in deep learning. The first part of the AN goes through the theoretical background of both topics. The second part describes a use case example based on the application from AN12603. It shows how a dataset of handwritten digits can be collected to match the input style of the handwritten digit recognition application. Afterwards, it illustrates how transfer learning can be used with a model trained on the original MNIST dataset to retrain it on the smaller custom dataset collected in the use case.   In the end, the AN shows that although handwritten digit recognition is a simple task for neural networks, it can still benefit from transfer learning. Training a model from scratch is slower and yields worse accuracy, especially if a very small amount of examples is used for training.     Application note URL: https://www.nxp.com/docs/en/application-note/AN12892.pdf 
View full article