S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
***************************************************************************** *Detailed Description: *This example will show you how to configure Wdg_fs23 Driver. *Sbc_fs23_InitDriver, Sbc_fs23_GoToInitState, Wdg_43_fs23_Init, Sbc_fs23_InitDevice initialize the Sbc device and external Wdg in SLOW MODE(This mode can e.g. be used during system startup/initialization phase). *Sbc_fs23_InitDevice release FS0B, according to the configuration in Sbc_fs23 WatchdogConfig tab: Release safety outputs after init *Sbc_fs23_TimeDelay delay for an amount of time, allow Gpt ISR to trigger watchdog externally. *Wdg_43_fs23_SetMode(WDGIF_FAST_MODE); switch Wdg operation mode to FAST MODE(This mode can e.g. be used during normal operations of the ECU). *Wdg_43_fs23_SetTriggerCondition(10000U); sets a new timeout value to 10 seconds, during which Wdg_fs23_Cbk_GptNotification0 continuously refresh the watchdog. *To demonstrate the watchdog timeout, Wdg_43_fs23_SetTriggerCondition was not called again to set a new timeout value, and Wdg_fs23_Cbk_GptNotification0 no longer refreshed the watchdog. *The watchdog error counter(WD_ERR_CNT) continues to increase reached its maximum value(WD_ERR_LIMIT), causing fault error counter(FLT_ERR_CNT) to increment by 1. *FS23 eventually enters fail-safe mode because FLT_ERR_CNT >= max. At this point, it was observed that LEDs V1 (D7), V2 (D8), and V3 (D9) of KITFS23SKTEVM were turned off. *The SPI data between FS23 and S32K311 are captured and attached to the project. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * RTD_WDG_43_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Wdg_43_fs23_TS_T40D34M10I0R0\doc * AUTOSAR_SWS_WatchdogDriver.pdf https://www.autosar.org/fileadmin/standards/R21-11/CP/AUTOSAR_SWS_WatchdogDriver.pdf * This example is migrated from Wdg_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 *****************************************************************************
View full article
This example project will show user how to use and configure the basic functionalities of ICU (WKPU) + DIO (GPIO).   ------------------------------------------------------------------------------ * Test HW: S32K396-BGA-DC1 (SCH-55517 Rev B2) * MCU: S32K396 * IDE: S32DS3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PEMicro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up. This is the simplest WKPU example. Pin PTB19 (WKPU42) is configured for wake-up.  The routine waits for SW8 to be pressed, then turns off LED1, and: Switches core clock to FIRC (Mode C Boot default from Table 125.). Initializes the WKPU instance. Configures WKPU42 (SW4). Enters standby (or fast standby). After pressing SW4, MCU wakes up, resets and polls for SW8 to be pressed again. If FAST_STANDBY is selected, Wkup_FastWkupBootAddress() is entered and both LED2 & LED3 blink before jumping to reset handler for full initialization. This example is provided as is with no guarantees and no support.
View full article
***************************************************************************** *Detailed Description: *This example will show you how to configure Sbc_fs23 Driver. *It initialization of Sbc_fs23 with watchdog window disabled. The Sbc_fs23_InitDevice() must be done within the dedicated 256 ms INIT window. *It Disable regulator V2, then re-enable it again. FS0b pin is asserted due to V2 Undervoltage reaction setting configured in FailSafe Init Configuration tab. *If the example runs without errors, the D12 LED on S32K31XEVB-Q100 will light up Green; otherwise, it will light up Red. *The SPI data between FS23 and S32K311 are captured and attached to the project. *Use the analog input of a logic analyzer or an oscilloscope to monitor the signals of FS23_V2 (TP27) and FS23_FS0 (TP8) on the KITFS23SKTEVM board. *------------------------------------------------------------------------------ *Test HW: * S32K31XEVB-Q100 Board SCH-55131 REV A P32K311HV 0P98C * KITFS23SKTEVM Dev-kit SCH-53096 REV B2 MFS2320BMBB1EP * My S32K31XEVB-Q100 has an onboard PFS2320A0L1W1, but Step 13/14 of AN14041 mention that A0 devices are not supported, so S32K311 communicate with the FS23 on the KITFS23SKTEVM. *Connections: KITFS23SKTEVM | S32K31XEVB-Q100 ------------------------------|-------------------- SPI_CSB J28-2 | J12-5(PTB-17) SPI_MOSI J29-2 | J12-7(PTB-16) SPI_SCK J31-2 | J12-11(PTB-14) SPI_MISO J32-2 | J12.9(PTB-15) VCC J6-1 | J40-15 GND J6-2 | J40-13 - KITFS23SKTEVM: SW1 - position 2-3 , J30 - ON, J26 5-6 ON, J26 9-10 ON . - Connect KITFS23SKTEVM Dev-kit and S32K3 MCU via on-board Arduino headers. *SDK: * S32K3 RTD 4.0.0 (SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip) * FS23 RTD 1.0.0 (S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip) *Debugger: S32DS 3.5.8, OpenSDA/ PEmicro Multilink Universal FX *Target: internal_FLASH *Reference Documentation: * AN14041 FS23 quick start guide (Rev. 2.0 — 23 January 2025) * AN14129 FS23 implementation and behaviors (Rev. 2.0 — 13 December 2024) * FS23, Safety System Basis Chip (SBC) with Power Management, CAN FD and LIN Transceivers Data Sheet (Rev. 8.0 — 30 June 2025) * RTD_SBC_FS23_UM.pdf C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\SW32K3_FS23_R21-11_1.0.0_D2312\Sbc_fs23_TS_T40D34M10I0R0\doc * This example is migrated from Sbc_fs23_example_HLD_S32K344. The method of migrating refers to the video "2.S32DS CT MCAL demo porting K344 to K312 based on RTD500": https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Tools-Part-How-to-port-RTD-s-existing-MCAL-demo-to-other/ta-p/1966315 ***************************************************************************** * Revision History: * Ver Date Author Description of Changes * 0.0 10-26-2025 Robin Shen Initial version * 0.1 11-21-2025 Robin Shen Upgrade FS23 RTD 1.0.0 from S32K3xx_SBC_FS23_R21-11_1.0.0_DS_updatesite_D2402_updated_D250115.zip to S32K3xx_SBC_FS23_R21-11_1.0.0_D2508_DesignStudio_updatesite.zip *****************************************************************************
View full article
**************************************************************************************************** * Detailed Description: * This code demonstrates how to inject an ECC (Error Correction Code) fault into either DTCM0 * (Data Tightly Coupled Memory) or SRAM0 using the EIM (ECC Injection Module). * * When the processor reads corrupted data from DTCM0 or SRAM0, an ECC error is detected, resulting in: * - A Bus Fault exception raised by the core. * - An error report generated by the ERM (Error Reporting Module), which can also trigger an interrupt. * * By default, the ERM interrupt has a lower priority than the Bus Fault exception. In this example, * the Bus Fault exception priority is intentionally lowered so that the ERM interrupt is serviced first. * This ensures the system can respond to the ERM interrupt before the core's Bus Fault handler executes. * * IMPORTANT: The interrupt vector table must not reside in SRAM0 or DTCM0 when injecting an * uncorrectable ECC fault into these memories. Otherwise, the ECC fault would corrupt the vector * table during a fetch, leading to unpredictable behavior. * Always check the VTOR (Vector Table Offset Register) * to confirm the vector table location before performing ECC fault injection. * * Memory Selection: * You can select which memory to inject the ECC fault into using the following macros: * #define SRAM0 * #define DTCM0 *************************************************************************************************** * ------------------------------------------------------------------------------------------------* * Test HW: S32K3X4EVB_Q257 * MCU: S32K344, 0P55A * SDK: NA * Debugger: Lauterbach Trace32 * Target: internal_FLASH ****************************************************************************************************
View full article
Hi everyone, Welcome to the NXP Tech Days 2025 training session AUT-T437: Hands - On Workshop: Explore Ethernet Integration on the S32K3 Microcontroller. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe.   Run the .exe project with administrator rights. Accept the license and install in the desired folder.         Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace.   Select root directory and browse the folder where you downloaded the project.   Select Copy projects into workspace. Then, click Finish.   Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
View full article
This document provides a brief explanation of the Excel-based calculator developed to assist with the computation of TX Arbitration Start Delay as described in the S32K3 reference manual. The tool implements the formula provided in the datasheet, allowing users to input relevant parameters and automatically calculate the delay values. It is intended to support engineers in evaluating CAN transmission timing and optimizing arbitration performance in S32K3-based applications.   1.Fill in the clock and CBT and FDCBT configuration parameters according to your requirements. For example, we fill the parameters according Case 3:  Then we can get the TASD value for non-FD frames is 24.05.   Please note that this summary is not officially released by NXP. It is a personal summary for reference only. If there are any errors, please contact me.
View full article
****************************************************************************************************** * Detailed Description: These demos showcase how to configure the eMIOS module on the S32K3 series, highlighting various operational modes and their implementations using the RTD high-level drivers, commonly known as MCAL drivers. The implementations demonstrated in these examples follow the approach outlined in the community thread:  S32M27x/S32K3 – eMIOS Usage. * Connections:  ******************************************************************************************************* * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Debugger: S32DS 3.6.2, OpenSDA/ PEmicro Multilink Universal FX  * Target: internal_FLASH ******************************************************************************************************* * Important information:  The OPWMT channel does not support the notification function. In this mode, the Sn[FLAG] bit is only set upon an AS2 match, which defines the generation of a trigger event within the PWM period. As a result, OPWMT mode cannot support notifications based on signal edges. A bus exception may occur during the execution of Mcl_Init() if the eMIOS clock is not properly enabled. To avoid this issue, ensure that the eMIOS peripheral clock is activated in the configuration settings under: MCU driver → McuModuleConfiguration → McuModeSettingConf → McuPeripheral *******************************************************************************************************
View full article
**************************************************************************************************** * Detailed Description: * * - CMU errors cannot be injected by any means other than manipulating the CMU thresholds, * except for FXOSC_CLK, which can be physically disrupted on the PCB. * * - CMU_FC_0 (FXOSC_CLK) is configured for **synchronous interrupt** on both LFF and HFF CMU events. * - CMU_FC_3 (CORE_CLK) is configured for **asynchronous destructive reset** triggered only by the LFF event; the HFF event is ignored. * - CMU_FC_4 (CORE_CLK) is configured identically to CMU_3: **asynchronous destructive reset** on LFF only; HFF is ignored. * - CMU_FC_5 (HSE_CLK) can be configured by the HSE_B core only. * Refer to the Reference Manual rev.10, Figure 122. Frequency checking (FC) instances * * - The configuration must be identical in both the MCU MCAL driver and the Clock Configuration Tool (clock details). * - To inject a specific CMU error, define one of the following macros: `INJECT_CMU_0`, `INJECT_CMU_3`, or `INJECT_CMU_4`. * * Behavior After Destructive Reset: * - Following a destructive reset (either `MCU_CORE_CLK_FAIL_RESET` or `MCU_AIPS_PLAT_CLK_FAIL_RESET`), * execution will halt in the `while(wait)` loop. * ------------------------------------------------------------------------------------------------ * Test HW: S32K3X4EVB_Q257 * MCU: S32K344, 0P55A * SDK: RTD 6.0.0 * Debugger: PEMicro Multilink FX * Target: internal_FLASH ****************************************************************************************************
View full article
[S32K3 tool part]:How to use IAR compiler or IAR project to compile MCAL project   1.    Abstract      Through regular observation, it has been found that there are still many customers using platforms such as MCAL+IAR, including those using IAR compilers and those directly using IAR IDEs. In fact, when I was working on industrial MCUs in the past, I also particularly liked IAR IDE for its fast compilation speed, high compilation efficiency, and small code generation. However, when I came to auto MCU, I found that its popularity was not very high, and I also noticed that some customers encountered various problems when importing MCAL into IAR. Therefore, I will directly write a tool article on how to use IAR compiler or IAR IDE project to compile NXP S32K MCAL in combination with EB tresos MCAL. This article uses S32K344 combined with RTD600 to illustrate the compilation of MCAL projects using IAR compiler and the direct import of MCAL into IAR IDE projects 2. IAR Complier with S32K3 RTD MCAL project 2.1 S32K3 HW and SW SW32K3_S32M27x_RTD_R21-11_6.0.0 S32K3X4-EVB Based on Dio_TS_T40D34M60I0R0 IAR:IAR EW for Arm 9.70.1 EB tresos29.0.0 2.2 Compile MCAL project steps using IAR compiler CMD method 2.2.1 Copy one RTD MCAL new project Open path C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins Copy Dio_TS_T40D34M60I0R0 , rename it as Dio_TS_T40D34M60I0R0_IAR Fig 1 2.2.2 Complie EB tresos project Use EB tresos tool open the following EB tresos project : C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject Generate code: Fig 2 2.2.3 Vscode open Dio_TS_T40D34M60I0R0_IAR project Use VS code open the following path folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344 Of course, you can also directly open this folder path using the command line, as long as you ensure that it is in the same layer path as the. mk and makefile scr Fig 3 2.2.4   Project_parameters.mk modification Mainly modify the following points: TOOLCHAIN = iar IAR_DIR = C:/IAR/ewarm-9.70.1 TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_6.0.0/eclipse/plugins The path of IAR must be consistent with the version of IAR software used to ensure that the corresponding IAR compiler can be found. Fig 4 2.2.5   Check_build_params.mk modification Add the following content to check_build_params.mk: else ifeq ($(TOOLCHAIN),iar) ifeq ("$(wildcard $(IAR_DIR)/arm/bin/iccarm.exe)","") $(error Invalid path set to the IAR compiler. \ The provided path: from project_parameters.mk IAR_DIR=$(IAR_DIR) is invalid!) Endif Fig 5 2.2.6        Makefile modification   Makefile need the following 5 points modification: (1)Compilier change ifeq (${TOOLCHAIN},iar) CC := $(IAR_DIR)/arm/bin/iccarm.exe LD := $(IAR_DIR)/arm/bin/ilinkarm.exe AS := $(IAR_DIR)/arm/bin/iasmarm.exe # Intel Hexadecimal Flash image tool GENHEX := $(IAR_DIR)/arm/bin/ielftool.exe HEX_OPTS := --ihex OUT_OPTS := -o endif Fig 6 (2) SRC_DIRS  add TOOLCHAIN SRC_DIRS += $(foreach mod,$(MCAL_MODULE_LIST),$(PLUGINS_DIR)/$(mod)_$(AR_PKG_NAME)/src) \ $(foreach mod,$(MCAL_MODULE_LIST_ADDON),$(PLUGINS_DIR_ADDON)/$(mod)_$(AR_PKG_NAME_ADDON)/src) \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7 \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7/$(TOOLCHAIN) Fig 7 (3) Linker file  modification ifeq ($(LOAD_TO),flash) ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/${TOOLCHAIN}/linker_flash_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_flash_$(DERIVATIVE_LOWER).ld endif else ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).ld endif endif Fig 8 (4) Complier options change ifeq (${TOOLCHAIN},iar) ################################################################################ # iar Compiler options ################################################################################     clib        := $(IAR_DIR)/arm/lib     CCOPT           +=  --cpu=Cortex-M7 \                         -DAUTOSAR_OS_NOT_USED \                         -DUSE_MCAL_DRIVERS \                         --fpu=FPv5-SP \                         --cpu_mode=thumb \                         --endian=little \                         -e \                         -Ohz \                         --debug \                         --no_clustering \                         --no_mem_idioms \                         --do_explicit_zero_opt_in_named_sections \                         --require_prototypes \                         --no_wrap_diagnostics \                         --diag_suppress=Pa050 \                         $(MISRA) \                         -D$(PLATFORM) \                         -D$(DERIVATIVE) \                         -DIAR \                         -DUSE_SW_VECTOR_MODE  \                         -DENABLE_FPU \                         -DD_CACHE_ENABLE \                         -DI_CACHE_ENABLE                             LDOPT           :=  --entry _start \                         --enable_stack_usage \                         --skip_dynamic_initialization \                         --no_wrap_diagnostics \                         --cpu=Cortex-M7 \                         --fpu=FPv5-SP                             ASOPT           :=  $(ASOPT) \                         --cpu Cortex-M7 \                         --cpu_mode thumb \                         -g \                         -r \                         -DMULTIPLE_CORE   endif   Fig 9 Fig  10 So how did these IAR compilation options come about? You can refer to the release note of RTD600, which contains corresponding descriptions Fig 11 (5) Elf related change ifeq (${TOOLCHAIN},iar) %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) $(ODIR)/*.o $(LDOPT) --config $(LINKER_DEF) --map $(ODIR)/ -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" "$(ODIR)/$(ELFNAME).hex" else %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) -Wl,-Map,"$(MAPFILE)" $(LDOPT) -T $(LINKER_DEF) $(ODIR)/*.o -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" $(OUT_OPTS) "$(ODIR)/$(ELFNAME).hex" endif   Fig 12 2.2.7   Build to generate elf Commander: make clean make build to generate the elf files: Fig 13 After generation, the elf can be burned onto the S32K344 EVB board for testing. The test results show that the onboard red light is flashing, indicating that the IAR compiler can work in command-line mode. 3. Import RTD MCAL to IAR IDE project This chapter explains how to create an IAR IDE project and import MCAL drivers to implement S32K3 MCAL combined with EB tresos for running. 3.1 MCAL IAR IDE project 2 methods Difference between two methods and how to import MCAL drivers: (1) Directly copy the RTD MCAL driver to the IAR IDE project directory (2) Connect the IAR IDE project driver to the original RTD driver path Fig 14 3.2 MCAL IAR IDE project import steps 3.2.1 create the new RTD MCAL IAR project folder    Create a new folder, named as:S32K344_DIO_MCAL_RTD600_IAR 3.2.2 create the sub folder for IAR project       Generate:EB tresos project code       Include:app related include file       Mcal: mcal driver copy from RTD       src: project main file       Tresos_Project:EB tresos project Fig 15 3.2.3 create EB tresos project (1) Create the EB tresos project in the followign path:  S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR   (2)Add modules: BaseNXP, Dem, Dio, EcuC, Mcu, Platform, Port, Resource   (3)Copy RTD xdm files in the following path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject\Dio_Example_S32K344\config to: S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR\config   (4)EB tresos Generate project EB tresos code will be generated to folder: S32K344_DIO_MCAL_RTD600_IAR\Generate Fig 16 3.2.4 Copy RTD related drivers to IAR project folder (1) BaseNXP: header, include, src (2)Det:  include, src (3)Dio:  include, src (4)Mcu:  include, src (5)Platform: build_files, include, src, startup (6)Port: include, src (7)Rte: include, src Copy RTD folder to IAR project is one method, if don’t want to copy the file, also can use the linker to add the RTD install path drivers directly. Fig 17 3.2.5 IAR IDE create IAR project   (1) Project->Create new project   (2) In the IAR project, add group   The related folder in project can be structured like the fig 18, which contains:   Generate: Include and src->EB tresos project generate code   Mcal:  Base, Det, Dio, Mcu, Platform, Port, Rte->Mcal driver   Src: Main.c->project main code      (3) Add RTD mcal related drivers to IAR project The RTD MCAL related driver files can be directly downloaded from the RTD installation path or copied to a folder in the IAR project, and both methods yield the same result. Fig 18 (4)IAR project platform folder added result: Fig 19 (5)main code add Main.c can copy from path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\src to S32K344_DIO_MCAL_RTD600_IAR\src Comment:  //#include "check_example.h"  // Exit_Example(TRUE);   3.2.6 IAR project options configuration (1)General options->Target->Device->NXP S32K344 (2)C/C++ Complier->Preprocessor Addional include directories: Use IAR project folder drivers which copied from RTD install path, the directories are: $PROJ_DIR$\Generate\include $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\header $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Mcu_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Rte_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\startup\include $PROJ_DIR$\mcal\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Dio_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Port_TS_T40D34M60I0R0\include $PROJ_DIR$\include If use the RTD install path drivers, use the following directories: $PROJ_DIR$\Generate\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\header C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Mcu_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Rte_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\startup\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Port_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\include   Defined symbols: S32K3XX S32K344 IAR USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Extra options: --no_clustering --no_mem_idioms --do_explicit_zero_opt_in_named_sections --require_prototypes --no_wrap_diagnostics   Languate 1:   Check Require prototypes   Diagnostics Suppress these disgnostics: Pa050 Fig 20 (3)Linker: Two points need to be added: $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\build_files\iar\linker_flash_s32k344.icf Library->Entry symbols: _start Fig 21 (4)Debugger Setup: PE micro, run to main Extra Options: Use command line options: --drv_vector_table_base=__ENTRY_VTABLE Fig 22 3.2.7  Build IAR project Project->Rebuild All Fig 23 3.2.8  Test result Download and debug result: Fig 24 After downloading and running, the red led is blinking on the board, indicating that the IAR IDE MCAL import method project has been successfully run.  
View full article
* ================================================================================================== * Detailed Description: * * This example shows how to implement ADC continuous scan with DMA read. * ADC1 is set to perform continuous scan of 4 channels (S10/S11/S12,S13) with DMA request enabled * for last channel S13. DMA reads respective sequential ADC data registers in one major loop. * * ADC1 channel S10 is connected to board's potentiometer, converted value is used to dim board's LED. * * ================================================================================================== * Test HW: S32K312EVB-Q172 * MCU: S32K312_172LQFP * Compiler: S32DS 3.6.3 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: On-Board Debugger (J40), Lauterbach * Target: Internal_FLASH * ==================================================================================================   Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.  
View full article
Abstract This example presents an use case for complementary PWM outputs with dead-time insertion and hardware ADC triggering using eFlexPWM, TRGMUX, BCTU, SAR-ADC and DMA modules on S32K39-37-36 series based on the RTD low level API to support diverse application needs. Connections: S32K396-BGA-DC1 -> Pin -> Signal -> Label J62-1 -> PTC30 -> siul2_gpio_94 -> GPIO1_GPT J62-5 -> PTD2 -> pwm_0_a, 2 -> PWM1 J62-6 -> PTD3 -> pwm_0_b, 2 -> PWM2 J62-30 -> PTD24 -> pwm_0_a, 0 -> PWMT J62-2 -> PTC31 -> siul2_gpio_95 -> GPIO3_BTCU_Trigger J62-4 -> PTD6 -> siul2_gpio_102 -> GPIO4_BTCU_Watermark J62-24 -> PTB14 -> adc1_s21 -> ADC1 *To use the potentiometer of S32X-MB connect: J62-24 (in S32K396-BGA-DC1) to P26-1 (in S32X-MB)   Note: Following line should be added in project/generate/src/Bctu_Ip_PBcfg.c every time the code is updated in Config Tools: #define DMA_LOGIC_CH_0 ((uint8)0U)   Detailed Description: The Compare Value of GPT eMIOS 0 channel 0 generates a time-out period. Once time-out is reached its eMIOS notification toggles GPIO1. This allows us to observe in scope 2 events, which describe the start and the end of the signal sequence. The eFlexPWM0 module is used for generating PWMs and hardware ADC triggering. The eFlexPWM0 Submodule 2 is employed to generate center-aligned complementary PWM outputs (PWM1 and PWM2) with dead-time insertion. The eFlexPWM0 Submodule 0 generates another independent PWM output (PWMT) and is utilized to generate the trigger signal for analog data capturing within the same PWM period —happens at half the time high in this case—using VAL0 register. The BCTU implements a list for parallel conversions using ADC0 and ADC1. Which is triggered by the eMIOS channel, and the resulting data is stored in FIFO1, as follows: • ADC0: VREFH_ChanNum51 -> BANDGAP_ChanNum48 • ADC1: VREFL_ChanNum50 -> S21_ChanNum45 For debugging purposed the GPIO3 is toggled every BCTU Trigger Notification. Additionally, the GPIO4 is toggled in BCTU Watermark Notification, which happens every time the number of active entries in FIFO exceeds the watermark level, and therefore the data is available for reading. See full signal sequence in Figure 1: Figure 1. Signals of example project When you suspend debug session, in Expressions tab (Figure 2) you can observe results: g_fifo1Result, which corresponds to the BCTU list measurements, meanwhile g_fifo1Volts corresponds to the conversion in volts. Figure 2. Expressions tab of example project   References S32 Design Studio for S32 Platform Real-Time Drivers (RTD) S32K39, S32K37 and S32K36 Data Sheet [S32K39-S32K37-DS] S32K39, S32K37, and S32K36 Reference Manual [S32K396RM] S32K344 to S32K39/S32K37 Migration Guide [AN14301] S32K39/37/36 Electrification Microcontrollers Evaluation Board [S32K396-BGA-DC1] S32X-MB I/O Extension Evaluation Board for Real-Time Domain Control and Actuation [S32X-MB] S32K39-37-36 – eMIOS/BTCU/SAR-ADC/DMA – [RTD600] [S32K Knowledge Base]   Application Software: - S32K396_RTD600_eFlexPWM_TRGMUX_BCTU_SARADC_DMA Example was built and tested using the following IDE and Driver versions: - S32 Design Studio for S32 Platform Version 3.6.3 - S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
View full article
Abstract This example presents an use case for analogue data capturing using eMIOS, BCTU, SAR-ADC and DMA modules on S32K39-37-36 series based on the RTD low level API to support diverse application needs.   Connections: S32K396-BGA-DC1 -> Pin -> Signal -> Label J62-1 -> PTC30 -> siul2_gpio_xx -> GPIO1_GPT (D0) J58-1 -> PTE14 -> emios_0_ch_19_z -> PWM1 J58-2 -> PTG9 -> siul2_gpio_xx -> GPIO2_eMIOS_Trigger J62-2 -> PTC31 -> siul2_gpio_xx -> GPIO3_BTCU_Trigger J62-4 -> PTD6 -> siul2_gpio_xx -> GPIO4_BTCU_Watermark J62-24 -> PTB14 -> adc1_s21 -> ADC1 *To use the potentiometer of S32X-MB connect: J62-24 (in S32K396-BGA-DC1) to P26-1 (in S32X-MB) Note: Following line should be added in project/generate/src/Bctu_Ip_PBcfg.c every time the code is updated in Config Tools: #define DMA_LOGIC_CH_0 ((uint8)0U)   Detailed Description: The Compare Value of GPT eMIOS_0_ch_0 generates a time-out period. Once time-out is reached its Emios Notification toggles GPIO1. This allows us to observe in scope 2 events, which describe the start and the end of the signal sequence. The eMIOS_0_ch_23 channel is configured as global counter bus A. In this setup, it can act as the time base for other eMIOS_0 channels, enabling synchronization between other them—there is just one PWM in this case. This synchronization ensures that channels share the same time base, thereby defining a common period for their operation. The emios_0_ch_19_g channel is configured as OPWMT mode, which offer more flexibility for triggering. An interrupt is requested on every flag event, during which GPIO2 is toggled—happens at half the time high in this case. This flag event, can be configured using Trigger parameter. For more details about eMIOS, please refer to S32M27x/S32K3 – eMIOS Usage, considering differences for porting from S32K3 to S32K39-37-36 in AN14301. The BCTU implements a list for parallel conversions using ADC0 and ADC1. Which is triggered by the eMIOS channel, and the resulting data is stored in FIFO1, as follows: ADC0: VREFH_ChanNum51 -> BANDGAP_ChanNum48 ADC1: VREFL_ChanNum50 -> S21_ChanNum45 For debugging purposed the GPIO3 is toggled every BCTU Trigger Notification. Additionally, the GPIO4 is toggled in BCTU Watermark Notification, which happens every time the number of active entries in FIFO exceeds the watermark level, and therefore the data is available for reading. See full signal sequence in Figure 1: Figure 1. Signals of example project When you suspend debug session, in Expressions tab (Figure 2) you can observe results: g_fifo1Result, which corresponds to the BCTU list measurements, meanwhile g_fifo1Volts corresponds to the conversion in volts. Figure 2. Expressions tab of example project   References S32 Design Studio for S32 Platform Real-Time Drivers (RTD) S32K39, S32K37 and S32K36 Data Sheet [S32K39-S32K37-DS] S32K39, S32K37, and S32K36 Reference Manual [S32K396RM] S32K344 to S32K39/S32K37 Migration Guide [AN14301] S32K39/37/36 Electrification Microcontrollers Evaluation Board [S32K396-BGA-DC1] S32X-MB I/O Extension Evaluation Board for Real-Time Domain Control and Actuation [S32X-MB] S32M27x/S32K3 – eMIOS Usage [S32M Knowledge Base] S32M27x/S32K3 – eMIOS/BTCU/ADC/DMA – [RTD600] [S32M Knowledge Base] S32K39-37-36 – eFlexPWM/TRGMUX/BCTU/SAR-ADC/DMA – [RTD600] [S32M Knowledge Base] Application Software: - S32K396_RTD600_eMIOS_BCTU_SARADC_DMA_Ip_example Example was built and tested using the following IDE and Driver versions: - S32 Design Studio for S32 Platform Version 3.6.3 - S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  FS26 watchdog timer refresh using the SBC_FS26 CDD  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * FS26 : CDD 2.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Please Modify attached code, and add this line of code, in this function Sbc_Wdg_Refresh_Notification  :-- Gpt_StopTimer(GptConf_GptChannelConfiguration_GptChannelConfiguration_0);     This change will make the example work for even starting FS26, driver at 6 msec and above.   Watchdog type :-- NXP eval boards has ASIL-D FS26 part with challenger watchdog. The OTP of FS26 on the board uses challenger watchdog. Change watchdog in code :-- FS26 watchdog is started in disabled mode (means infinite period). Later on we change the watchdog time in the code :--     Array Index for watchdog refresh timing  :-- Example will run once you press switch USER_SW0 connected on PTB26 on the Evaluation board :-- Please add this type of check in your code, during development process so that, avoid any error due to FS26 watchdog mis trigger. When you use Debug FLASH then in that case code goes to flash memory & can cause your MCU to frequent RESET, which caused issue for reprogramming the NEW firmware on the board FLASH memory. If we add this type of check then we can avoid the Faulty FS26 Software to stop misbehaving before flashing new firmware on the board.   In CDD-2.0.0, FS26 goes to INIT_FS state here  :--- Sbc_fs26_InitDevice() --> Sbc_fs26_CheckStateAndGotoInitFS()   In CDD-2.0.0, If we start the Watchdog in enabled mode, watchdog notification function to refresh watchdog is called from this function  :-- Sbc_fs26_InitDevice() --> Sbc_fs26_NormalFSSequence() -->      In CDD 2.0.0, Following function call will exit Debug mode & Release FS0b & FS1B pin :-- Sbc_fs26_InitDevice() --> Sbc_fs26_NormalFSSequence() :--- --> Sbc_fs26_ExitDebugMode() --> Sbc_fs26_ReleaseSequence()   In CDD 2.0.1, Following function call will exit Debug mode & Release FS0b & FS1B pin :-- Sbc_fs26_InitDevice() --> Sbc_fs26_NormalFSSequence() --> Sbc_fs26_ExitDebugMode() ===================== CDD-2.0.1 example ================= RTD used :-- S32K3XX_AASW_4_7_RTM_FS26_2_0_1_DS_updatesite_2311_signed.zip Watchdog started in the Disabled mode (i.e infinite Period) then watchdog period is changed in the code main() function :--   Driver configuration :--   These function get executed :--       One bug in RTD   ---> S32K3XX_AASW_4_7_RTM_FS26_2_0_1_DS_updatesite_2311_signed.zip :-- RTD driver Bug is corrected like this :--   
View full article
******************************************************************************************************* * Detailed Description: These demos showcase how to use eMIOS in Input Capture mode with DMA, utilizing both low-level drivers (Ip) and high-level drivers (MCAL). They demonstrate how timestamp data from captured input signals is stored and how a GPIO toggle provides a simple visual confirmation that the interrupt is being triggered as expected. * Connections:  ******************************************************************************************************* * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Debugger: S32DS 3.6.2, OpenSDA * Target: internal_FLASH ******************************************************************************************************* * Important information:  eMIOS Pwm: Configures EMIOS 0 Channel 1 as OPWMB (Output Pulse Width Modulation Buffered). This channel generates a waveform that will be captured by Channel 9 eMIOS Icu with DMA: Configures EMIOS 0 Channel 9 in ICU_MODE_TIMESTAMP using SAIC (Single Action Input Capture) mode. This channel captures the timestamps of the waveform generated by Channel 1. After a predefined number of captures, a DMA interrupt is triggered. ******************************************************************************************************* Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + RTI (PIT0).  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & PIT for wake-up. The PIT0 instance includes a dedicated RTI (Real Time Interrupt) timer that runs on a separate oscillator clock and can be used for system wakeup. A key feature of this is power saving with a separate input clock for the RTI timer. All other timers share a common core clock. Note: Only PIT_0 supports the RTI feature, and exists in the Standby domain. This example does not poll for a SW press to enter and configure standby; Instead, the main function directly enters the Wkpu_EnterStandby() function which: Switches core clock to FIRC. Initializes and configures WKPU instance and wake-up source 3 (RTI). Initializes and configures PIT0 and PIT0 CH0 as set in Config Tools view. If EN_RUN_ICYCL_DUTY macro is enabled, configures PIT1 for user code before going to standby. Once Pit1_Notification is entered, runFlag is set to FALSE. Turns off LED. Enables RTI channel interrupt (otherwise, MCU cannot be woken up). Finally, sets the timeout value (WKPU_ICYCL_DUTY_TIME macro) and enters standby. This showcases the basic configuration for template on a fast-scanning power saving routine (for example, wake-up, measure ADC, go back to sleep). Keep in mind that power saving depends on the frequency of wake-up events. If MCU spends more time in Run mode rather than in Standby mode, power consumption is affected. The transition time from Standby mode to Run mode is quick. If the MCU only spends 9ms in Run and 1ms in Standby, the average current of the system will be considerably higher than if the MCU was running only 1ms every 1 second. Refer to S32K3 Low Power Management AN and demos for further information. After the period defined with either WKPU_ICYCL_DUTY_TIME, MCU wakes up. After wake-up, MCU resets and the cycle repeats. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + RTC timeout.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & RTC units for wake-up. The RTC is present in always ON domain, hence available in RUN mode as well as in STANDBY mode. The RTC can trigger a single wake-up event (timeout). When the RTC counter reaches a specific, pre-defined alarm time set by the user. RTC timeout is mapped as wake-up source 1. RTC0_CLK source is configured as SIRC_CLK, and SIRC_CLK must be enabled in standby mode. Chapter 69.3.1 RTC explains the functionality of the RTC timer. RTCVAL is updated at the point where no counter match is due as per the previous RTCVAL, the RTCF flag is set when the counter matches the new value. If there is a match when in the low-power mode, then the RTC first generates a wakeup request to force a wakeup to run mode, and then the RTCF flag is set. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches CORE_CLK to FIRC. Initializes the WKPU instance. Configures WKPU1 & WKPU42 (PTB19). Initializes and enables interrupt for RTC. Loads the RTCVAL value to 5000ms.  Starts the counter. Enters standby (or fast standby). After the period defined with RTC_TIME or RTC_PERIOD_DELAY_MS(x) macros defined in Wkpu.h, MCU wakes up. After wake-up, MCU resets and polls for SW5 to be pressed again. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + RTC API.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & RTC units for wake-up. The RTC is present in always ON domain, hence available in RUN mode as well as in STANDBY mode. The chip contains one instance of RTC (Real Time Clock) timer and API (Autonomous Periodic Interrupt) timer, where both can perform 32-bit comparisons. Both RTC and API timers can generate interrupts as well as wake-up from low power modes. The following figure highlights the path for RTC API wake-up. Please refer to Chapter 69.3.2 API functional description from the S32K3XX reference manual (Rev. 12) for further information. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches CORE_CLK to FIRC. Initializes the WKPU instance. Configures WKPU2 & WKPU42 (PTB19). Initializes and enables interrupt for RTC. Enables RTC API and loads the APIVAL to 3000ms.  Starts timer. Enters standby (or fast standby). After the period defined, RTC API generates an interruption and MCU wakes up. After wake-up, MCU resets and polls for SW5 to be pressed again. The RTC API value can be changed with RTC_PERIOD_DELAY_MS(x) macro defined in Wkpu.h. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + LPCMP.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & LPCMP units for wake-up. The S32K3XX's LPCMP can operate in trigger mode in both standby and run mode to continuously scan the input channels. RTC-API and LPCMP must be configured before entering into standby mode as per below shown figure:   See chapters 61.1.5 Comparator Trigger Mode & 61.1.6 Interaction with RTC API to cause wakeup from the S32K3XXRM (Rev. 12) for further information.   The register configurations before entering Standby mode for LPCMP trigger mode operation is the following:   Configure RTC.APIVAL to set the period of the round robin operation. Execute standby mode entry. The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches CORE_CLK to FIRC. Initializes the WKPU instance. Configures WKPU2 & WKPU42 (PTB19). Initializes and enables interrupt for LPCMP. Initializes RTC and sets the timer value (in RTCC - APIVAL) to 100ms. Starts timer. Enters standby (or fast standby). While in standby, PTA0/1/2 are active; if a voltage higher than 2.5V is detected (ICU LPCMP DAC Voltage Level = 127), or SW6 is pressed MCU will wake-up.  After wake-up, MCU resets and polls for SW5 to be pressed again. The RTC timer value can be changed with RTC_PERIOD_DELAY_MS(x) macro defined in Wkpu.h. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + SIUL2 (GPIO).  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS v3.5 & S32DS v3.6.x * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU unit for a GPIO interrupt wake-up. This is the simplest WKPU example. Pin PTB19 (WKPU42) is configured for wake-up.  The routine waits for SW5 to be pressed, then turns off the green LED, and enters Wkpu_EnterStandby() function which: Switches core clock to FIRC. Initializes the WKPU instance. Configures WKPU42 (PTB19). Enters standby (or fast standby). After pressing SW6, MCU wakes up, resets and polls for SW5 to be pressed again. This example is provided as is with no guarantees and no support.
View full article
This example project will show user how to use and configure the basic functionalities of WKPU + FlexCAN.   ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the FlexCAN0 instance for reception. Since RevB2 of the EVB was used for development, CAN TRXCVR used is TJA1443. TJA1443 is initialized in main code (CAN0_STB = 1 & CAN0_EN = 1). FlexCAN bitrate: Bitrate: 500 Kbps Sampling point: 81.25% Individual mask is set to 0x0, meaning all IDs are accepted. Main routine: Waits for SW5 to be pressed, or for FlexCAN interrupt. If SW5 is pressed, turns off green LED, disables FlexCAN and switches CORE_CLK to FIRC. It then configures both PTB19 (SW6) and PTA6 (CAN0_RX) for interrupt wakeups. If either SW6 is pressed or a CAN message is received (edge detect on PTA6), MCU wakes up and will wait for SW5 to be pressed again. FlexCAN is configured for INTERRUPT; If a CAN frame is received, bRxFlag is set to 1 inside the callback, blue LED is toggled, and an ACK frame is sent back. CAN communication can be tested either with another EVB, or with a PCAN analyzer connected to J32. PCAN-View log for dummy and ACK messages: This example is provided as is with no guarantees and no support.
View full article