S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
UART0 communication is supported in the latest version of MPC5746R Bootloader .rbf file (attached below) + Supported UART0/LINFlexD_0: PD13-PD14 pins(Speed: 115200b/s)   Tested on the dev boards:   Development Board MPC5746R-252DC MPC57xx-MOTHERBOARD Processor PPC5746RTMMT5 - 1N83M  
記事全体を表示
So you have created a project in S32DS with target of S32V234 Cortex-A53 APEX2/ISP Linux . You have built the project and now want to execute it on the S32V234-EVB2, which is running the Linux BSP for the VSDK on a microSD card. There are many ways to do this, however, the simplest is to use the built-in support within S32DS to run and/or debug over an Ethernet connection to the Linux BSP OS running on the EVB. In order for S32DS to connect to the Linux BSP OS, the following steps should be followed: 1) First, we must complete the steps in HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP . 2) With the Linux running on the EVB, start a terminal program (for ex. PuTTY) on your PC 3) Set Connection type to Serial 4) Set speed to 115200, Data bits 8, Stop bits 1, Parity None 5) Set Serial line to the COM port associated with the USB port setup in step 1 of this document. (for ex. COM3) 6) Click Open to start the terminal session 7) Press enter key to bring up login prompt 😎 Log into Linux (login name is "root") 9) Get IP address, enter command:    ifconfig       Make note of the IP address 10) Launch S32DS for Vision. From the C/C++ Perspective, select Run->Debug Configurations... 11) From 'C/C++ Remote Application'. Select '<project_name>_Remote_Linux' debug configuration. 12) Select New to create new debug connection. 13) Select SSH 14) Enter the IP address noted earlier 15) Enter user ID as "root". The Linux BSP uses Password based authentication, but by default, no password is set. So the password can be left blank. 16) Select Finish 17) Select Apply, and then if you wish, Debug This connection is stored within the workspace. It can be added to any projects within the workspace. If a new workspace is created, then this connection will not appear in the selection list.
記事全体を表示
Eclipse caches some settings within the workspace directory. After installing a new version of S32DS, some settings in old workspaces may not match the requirement of the new version. The result is often errors reported on new as well as previously existing projects located in an existing workspace which you selected when launching S32DS. The best way to resolve this is to create a new workspace and then import your projects. This will ensure the workspace is created using all the correct settings for the version you have installed.
記事全体を表示
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB2 using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB2 to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the A53 build option. 3) The project is now built, and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the '{project_name}_Remote_Linux' debug configuration is selected and the Connection (see step 3) is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts.   You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial break point is reached in main(), it is almost ready for to start debug on ISP. Click Resume as the A53 must be running before we can attach the ISP debug thread. 😎 Return to the Debug Configurations menu and locate the ISP debug configuration. You will see a debug configuration within the 'S32 Debugger' group (in our example, isp_sonyimx224_csi_dcu_mipi_simple_IPUS0 as shown below). This is the debug configuration we will use, however, it will require some setup.     9) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   10) This is already done for our example, but for your application, it may be necessary to setup the symbols for the ISP engine. Go to the Startup tab and:    a) Check the box for 'Load symbols'    b) Select the option for 'Use file', click Workspace... and locate the object file (.opius) for the ISP engine you wish to debug.   11) Click Apply then Debug. It may take a few moments for the ISP core debug to launch.   12) Wait for the ISP debug launch to complete. You may notice the A53 thread has terminated. This is normal and expected since the camera input cannot be suspended. When the launch completes, the context of the Debug window will switch to the ISP debug thread. 13) Enable Instruction Stepping mode and then step one time to load the object file which was setup in step 6. 14) The ISP debugging is now running and you can step through the ISP engine, look at registers, set a break point, etc. Note: only one hardware break point is supported for ISP.
記事全体を表示
Has this happened to you? You just launched S32DS for Vision and opened a visual graph but the blocks are collapsed onto one another. Probably looks something like this: There is an easy solution. Just click on the 'Arrange All' button and the graph will automatically expand to a manageable state. Here is the result:
記事全体を表示
UART communication is supported in the KEA64 Bootloader .rbf file  + Supported UART0: PTA2-PTA3 pins(Speed: 115200b/s) Tested on the dev board:   Development Board TRK-KEA64 Processor PKEAZN64 MLH 2N22J
記事全体を表示
There are a number of existing ISP Graph diagrams provided within the VSDK. It is possible to import them into S32DS and use them in a new C/C++ project. The steps to do this are detailed within this document. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select File -> New -> S32DS Application Project. 3) Enter a project name, such as: ISP_ISP_Generic_demo 4) Select 'A53 APEX/ISP Linux' 5) Click Next 6) Deselect the APEX2 options and 'ISP Visual Modeling' option. 7) Click Finish 😎 Select File -> New -> S32DS Project from Example. 9) Select isp_generic. 10) Select Finish 11) Open isp_generic in the project explorer 12) Double-click ISP data flow ; isp_generic. The ISP data flow graph will appear in the editor 13) Define a new configuration for emitting code from the graph       a) Right-click in the ISP data flow window and select Emit As -> Emit Configurations...       b) Select ISP Emitter       c) Press New Launch Configuration       d) Enter a name       e) To select the graph, press Browse Workspace       f) Expand each item until you can select the .isp file. Click OK       g) Select the location of the emitted output to the application project, select Browse Workspace       h) Select the name of your application project, then press OK       i) Enter 'A53_gen' to the Dynamic sequences sources folder box. This is the folder within the target project that generated code will be stored. Check the box for Emit host code.       j)Now select the location to store the configuration file. Go to the Common tab, select Shared file and click Browse       k) Select the .launches folder inside ISP_ISP_Generic_demo and click OK       l) Click Apply and Emit. Dialog box will appear when code generation is successful              m) Expand the folders within ISP_ISP_Generic_demo, A53_gen, src and inc, to see the newly generated output files 14) Build the project 'ISP_ISP_Generic_demo' for ISP 15) Open file 'ISP_ISP_Generic_demo/A53_inc/isp_user_define.h', by double clicking on it in the Project Explorer. Change '#define DCU_BPP DCU_BPP_YCbCr422' to '#define DCU_BPP DCU_BPP_24' and change '#define __DCU_BPP' to "#undef __DCU_BPP". Before After 16) Using the method detailed in steps 8 - 10, create the example project 'isp_sonyimx224_csi_dcu'. Take from this project the file 'isp_sonyimx224_csi_dcu/A53_src/main.cpp' and use it to replace the file 'ISP_ISP_Generic_demo/A53_src/main.cpp' in the current project. Then make the following modifications:  On line 36, change <#include "mipi_simple_c.h"> to <#include "isp_generic_c.h">. On line 303, change <gpGraph_mipi_simple> to <gpGraph> AND <gGraphMetadata_mipi_simple> to <gGraphMetadata> On line 330, change <FDMA_IX_FastDMA_Out_MIPI_SIMPLE> to <FDMA_IX_ISP_OUTPUT>. Please see C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\docs\drivers\SDI_Software_User_Guide.pdf for details on what this code is for. 17) In Project Explorer, right-click on "...\A53_gen\src\isp_process.cpp" and select Build path -> Remove from -> A53 18) Select 'ISP_ISP_Generic_demo:A53' in the Project Explorer panel, then Build for A53 19) Run it remotely on the target using the method fromHOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS . Should get results similar to this:
記事全体を表示
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select "New S32DS Project from example" 3) Select isp_sonyimx224_csi_dcu project and click Finish.    In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_sonyimx224_csi_dcu_graph'. Then double click on 'ISP data flow : mipi_simple'. The ISP graph diagram will appear in the editor panel. 5) We are ready to build the project, but first, select isp_sonyimx224_csi_dcu: A53 in the Project Explorer panel 6) Build project for A53  7) Start a debug session using method as described in HOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS, beginning at step 10. 😎 Should get results similar to this:
記事全体を表示
The Vision SDK root is contributed to the Design Studio as a dynamic path variable “S32DS_VSDK_DIR”. Several Design Studio services use this variable to access the resources inside the Vision SDK. By default, this variable points to “${eclipse_home}../S32DS/s32v234_sdk”, i.e. to the Vision SDK shipment bundled with Design Studio. Technically you can change this variable to point to another instance of Vision SDK using the following steps: 1. Go to the main menu "Window -> Preferences" 2. Filter the preference dialog with "sub" keyword or just navigate to "Run/Debug -> String Substitution node. 3. Edit Variable "S32DS_VSDK_DIR" to assign another value to be substituted as Vision SDK root 4. Press OK when changes are complete.
記事全体を表示
One of the many great features of the S32DS is the ability to access the Linux BSP file system on the SD card in the S32V234-EVB. Once connected, you can drag and drop files between your PC and the EVB. Once you have completed HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP  and HOWTO: Setup A Remote Linux Connection in S32DS (S32V234), you are ready to setup the Remote Systems view to connect to the Linux files system to view and access the file system. Prerequisite Before starting this procedure, make sure the BSP is loaded onto the SD Card, the SD Card is inserted into the SD Card Slot, the ethernet cable is connected to both the EVB and the network port, and the EVB is powered up. 1) Go to 'Window -> Show View -> Other' 2) Expand 'Remote Systems', then select "Remote Systems' and click OK 3) Click 'Define a connection to remote system' button OR right-click in the Remote Systems window and select 'New Connection...' from the list Right-click menu 4) Select 'SSH Only' 5) Enter the IP address noted from HOWTO: Setup A Remote Linux Connection in S32DS (S32V234) for Host name, enter a descriptive name for the connection (optional) and click Finish. 6) Right-click on the connection name in the Remote Systems window and select 'Connect' OR expand the folders under the connection name until the login window appears: Connection_name -> Sftp Files -> Root (window appears) 7) Enter "root" for User ID and since the BSP comes with ID root without a set password, leave the password field blank. 😎 Click OK 9) The Linux file system is now visible in the Remote Systems window. You can drag and drop files to and from here. Expand the folders to see the contents.
記事全体を表示
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select 'New S32DS Project from example' 3) Select apex2_fast9 project 4) Click Finish 5) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'. 6) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9. 7) Click Resume  Should see something similar to what is pictured below There are green diamonds at the corners in the image as identified by the fast9 corner detection algorithm
記事全体を表示
Table of Contents 1. Introduction 2. Requirements 2.1 Software Required 2.2 Hardware Required 3. NXP Account Login 4. Installation 4.1 S32K3 FRDM Automotive Board Installation 4.2 FreeMASTER Installation 4.3 AMMCLib Installation 5. Open a Demo from ACH (Application Code Hub) 6. Running a Motor Control Demo from ACH 7. Conclusion 1. Introduction This article aims to help new users prepare and install the necessary software and hardware to use the FRDM-A-S32K312 board with the latest S32K3 FRDM Automotive Bundle and Examples from Application Code Hub (ACH). Note: These steps can also be followed with other NXP Evaluation Board, for example FRDM-A-S32K344. S32K312MINI‑EVB Renamed to FRDM‑A‑S32K312: Now part of the FRDM Automotive Ecosystem under its new name, the board keeps the same hardware and adds full ecosystem compatibility for flexible, scalable development.     2. Requirements   2.1 Software Required S32K3 FRDM Automotive Board Installation Package FreeMASTER Run-Time Debugging Tool Automotive Math and Motor Control Library (AMMCLib) Rev 1.1.44   2.2 Hardware Required FRDM-A-S32K312 Development Board MCSPTE1AK344 Motor Control Kit, which includes: Sunrise motor  DEVKIT-MOTORGD  12V power supply FRDM K64 click shield with Force Click and 4X4 RGB Click USB Type-C cable   3. NXP Account Login Open Software Licensing: Support, make sure you are logged into your NXP Account, and select: Click on My NXP Account. Select Software Licensing and Support. Then click on View accounts: These steps will ensure that you are properly authenticated with your NXP Account before proceeding with any software downloads. Keep the page opened for login to persist.   4. Installation Note: Before proceeding, make sure you have full access to your PC or Laptop. Some installers require local admin rights. Contact your IT department to assist you with installation.   4.1 S32K3 FRDM Automotive Board Installation Navigate to S32K3 FRDM Automotive Bundle The page will open with default selection: FRDM Automotive Board Installation Package    Click on Generate Bundle Installer and then a popup window will appear: Click Next and enter details about Export Control: Click on Submit Export Control, then read the License Agreement: After reading, click on I Accept the terms of the License Agreement Wait for the Generate Bundle Installer to complete and press Done: This will download 2 files on your PC: NXP_Multi_Installer_28.05.26.190715_User_Manual.pdf NXP_Multi_Installer_28.05.26.190715_setup.exe Open  NXP_Multi_Installer_28.05.26.190715_setup.exe : Click Next > and read the License Agreement: After reading press on I Agree Select the type of install: Full and press Next Check the Download folder to your location and press Next Select both options: Launch executable files after download Installation and configuration without any interaction Click on Download Wait for the download to complete, and Installation will begin Wait for the installation process to complete (~10-15 minutes) Click Next to close the window After installation check PEmicro drivers installed on your PC:  Connect the USB cable to your PC and the FRDM Automotive S32K312 board: Open Device Manager to check OpenSDA and the COM port number. OpenSDA - CDC Serial Port → note this COM port number Note: The COM port number may differ on your system.   4.2 FreeMASTER Installation Download the  FreeMASTER Run-Time Debugging Tool:   Open the installer FMASTERSW32.exe Click Next, then select all available products: Use the default installation path: C:\NXP\FreeMASTER 3.2 Wait for the installation to complete.   4.3 AMMCLib Installation First, open the S32 Design Studio 3.6.5 Navigate the Menu to Help -> S32DS Extensions and Updates Search for AMMCLIB and select AMMCLIB for S32K3xx/S32M27x: Click Install/Update 1 item(s) and next Read and Click on I accept the terms and press Finish Select the Authority/Update Site https://www.nxp.com and Trust Selected Select X509 and Trust Selected Restart S32 Design Studio 3.6.5     5. Open a Demo from ACH (Application Code Hub)   Open S32 Design Studio 3.6.5, select Import Project from Application Code Hub This will open a new Window: Click on Search window and enter "brake" Select the Emergency LED-Based Brake Status Monitoring on FRDM-A-S32K312 Click on GitHub link — this will trigger S32 Design Studio IDE to automatically retrieve project attributes, then click Next>. Select main branch and then click Next>. Select your local path for the repo in Destination->Directory window. The S32 Design Studio IDE will clone the repo into this path, click Next>. Select Import existing Eclipse projects then click Next>. Select the project in this repo (only one project in this repo) then click Finish. In Project Explorer, right-click the project and select Update Code and Build Project: This will generate the configuration (Pins, Clocks, Peripherals), update the source code and build the project using the active configuration (e.g. Debug_FLASH ). Make sure the build completes successfully and the *.elf file is generated without errors. Go to Debug and select Debug Configurations. There will be a debug configuration for this project:   Select the FRDM_A_S32K312_BRAKE_MONITORING_Debug_FLASH_PNE configuration and press Debug: Now the perspective will change to the Debug Perspective. Use the controls to control the program flow. Results: The LED strip lights up in different colors to indicate the current voltage level being monitored. Upon startup, all LEDs perform a test sequence to verify functionality. During normal operation, the entire strip changes color based on the measured voltage: green for safe levels, yellow for moderate levels, orange for elevated levels, and red for critical levels, providing real-time visual feedback of the electrical signal being monitored.   6. Running a Motor Control Demo from ACH Open S32 Design Studio 3.6.5, select Import Project from Application Code Hub - Motor Control Open the example: PMSM Motor Control Sensorless dual Shunt FOC on FRDM-A-S32K312   Follow the same steps as above in 5. Open a Demo from ACH (Application Code Hub) After the executable file is downloaded to the board: Disconnect the FRDM-A-S32K312 board from the PC. Insert the DEVKIT-MOTORGD on top of the FRDM-A-S32K312 ensuring proper pin alignment. Plug-in the 12V power supply to the DEVKIT-MOTORGD. Reconnect the USB Type-C cable to the FRDM-A-S32K312   The RGB LED, User Buttons are on top side, Reset Button is on the left side, while the 12V power, Motor Phases and USB Type-C are on the right side.    Open FreeMASTER_control/S32K_PMSM_Sensorless.pmpx project file: This will launch another window with FreeMASTER: Press GO button to connect at 115200 baud. In the App Control Tab, press On and set Speed Required to 1000 RPM: Apply a small mechanical load to the motor (friction force to the motor shaft) and observe the iABC currents: Here is a short video with the steps above explained: 7. Conclusion These steps conclude the Getting Started with the FRDM-A-S32K312 board using the latest S32K3 FRDM Automotive Bundle and examples from Application Code Hub (ACH). For more details, refer to: The corresponding Readme for the selected ACH example. Thank you for your time, Stefan V.
記事全体を表示
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using either the A53 or the TEST_A53 build options. 3) The project is now built and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts. You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial breakpoint is reached in main(), we need to set a breakpoint at the function apu_hal_Enable().    This breakpoint has already been created for you, you just need to enable it! Locate the breakpoint in the Breakpoints view. Due to some known issues with Eclipse CDT, it is necessary to enable->disable->enable the breakpoint so it will work properly. The issue only affects this breakpoint, due to the way it is provided, and will not affect breakpoints which you set elsewhere in the code. 😎 Press Resume twice, so that the breakpoint which was set at apu_hal_enable() is reached for the 2nd time. 9) Open Debug Configurations. You will see a debug configuration within the 'S32 Debugger' group (FAST9COLOR as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.       11) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   12) It may take a moment or two before the APEX2 debug thread launch is complete, see the Thread listed within the <kernel_name>[S32 Debugger] in the Debug window. Also note, a new breakpoint is listed in the Breakpoints view. This breakpoint is set for you at the start of the APEX2 graph function. 13) The debugger context is still on the A53 thread. Press RESUME and then select the APEX2 thread to see that it has stopped on the graph function break point. Now you can step through the graph. 14) To step through a kernel, locate the call to the kernel function in the graph function and set a break point on the line. 15) Press RESUME to advance the program counter to the new break point 16) Press STEP INTO to advance the program counter into the kernel. It may take several steps as the optimizations performed by the compiler produce some synchronization inconsistencies. 17) You may need to help the IDE to locate the source files. Now you can see the kernel wrapper function... and the kernel! 18) Step through, monitor variables and registers and set breakpoints.
記事全体を表示