Table of Contents
1. Introduction
2. Requirements
2.1 Software Required
2.2 Hardware Required
3. NXP Account Login
4. Installation
4.1 S32K3 FRDM Automotive Board Installation
4.2 FreeMASTER Installation
4.3 AMMCLib Installation
5. Open a Demo from ACH (Application Code Hub)
6. Running a Motor Control Demo from ACH
7. Conclusion
1. Introduction
This article aims to help new users prepare and install the necessary software and hardware to use the FRDM-A-S32K312 board with the latest S32K3 FRDM Automotive Bundle and Examples from Application Code Hub (ACH).
Note: These steps can also be followed with other NXP Evaluation Board, for example FRDM-A-S32K344.
S32K312MINI‑EVB Renamed to FRDM‑A‑S32K312: Now part of the FRDM Automotive Ecosystem under its new name, the board keeps the same hardware and adds full ecosystem compatibility for flexible, scalable development.
FRDM-A-S32K312-Details.png
2. Requirements
2.1 Software Required
S32K3 FRDM Automotive Board Installation Package
FreeMASTER Run-Time Debugging Tool
Automotive Math and Motor Control Library (AMMCLib) Rev 1.1.44
2.2 Hardware Required
FRDM-A-S32K312 Development Board
MCSPTE1AK344 Motor Control Kit, which includes:
Sunrise motor
DEVKIT-MOTORGD
12V power supply
FRDM K64 click shield with Force Click and 4X4 RGB Click
USB Type-C cable
3. NXP Account Login
Open Software Licensing: Support, make sure you are logged into your NXP Account, and select:
Click on My NXP Account.
Select Software Licensing and Support.
stefanvlad_4-1766413667183.png
Then click on View accounts: stefanvlad_5-1766413890382.png
These steps will ensure that you are properly authenticated with your NXP Account before proceeding with any software downloads.
Keep the page opened for login to persist.
4. Installation
Note: Before proceeding, make sure you have full access to your PC or Laptop. Some installers require local admin rights. Contact your IT department to assist you with installation.
4.1 S32K3 FRDM Automotive Board Installation
Navigate to S32K3 FRDM Automotive Bundle
The page will open with default selection: FRDM Automotive Board Installation Package stefanvlad_0-1779985423843.png
Click on Generate Bundle Installer and then a popup window will appear: stefanvlad_1-1779984167578.png
Click Next and enter details about Export Control: stefanvlad_2-1779984263930.png
Click on Submit Export Control, then read the License Agreement: stefanvlad_3-1779984364018.png
After reading, click on I Accept the terms of the License Agreement
Wait for the Generate Bundle Installer to complete and press Done: stefanvlad_4-1779984469321.png
This will download 2 files on your PC:
NXP_Multi_Installer_28.05.26.190715_User_Manual.pdf
NXP_Multi_Installer_28.05.26.190715_setup.exe
Open NXP_Multi_Installer_28.05.26.190715_setup.exe : stefanvlad_3-1779986630899.png
Click Next > and read the License Agreement: stefanvlad_4-1779986657860.png
After reading press on I Agree stefanvlad_2-1779986607439.png
Select the type of install: Full and press Next
stefanvlad_5-1779986759079.png
Check the Download folder to your location and press Next stefanvlad_6-1779986834607.png
Select both options:
Launch executable files after download
Installation and configuration without any interaction
Click on Download
Wait for the download to complete, and Installation will begin stefanvlad_8-1779987127107.png
Wait for the installation process to complete (~10-15 minutes) stefanvlad_9-1779987474488.png
Click Next to close the window stefanvlad_10-1779987521122.png
After installation check PEmicro drivers installed on your PC:
Connect the USB cable to your PC and the FRDM Automotive S32K312 board: FRDM-A-S32K312-Connect.png
Open Device Manager to check OpenSDA and the COM port number.
OpenSDA - CDC Serial Port → note this COM port number stefanvlad_2-1766420223283.png
Note: The COM port number may differ on your system.
4.2 FreeMASTER Installation
Download the FreeMASTER Run-Time Debugging Tool:
stefanvlad_3-1766420635579.png
Open the installer FMASTERSW32.exe
Click Next, then select all available products: stefanvlad_3-1766483372281.png
Use the default installation path: C:\NXP\FreeMASTER 3.2 stefanvlad_5-1766483553297.png
Wait for the installation to complete.
4.3 AMMCLib Installation
First, open the S32 Design Studio 3.6.5
Navigate the Menu to Help -> S32DS Extensions and Updates stefanvlad_11-1779987676217.png
Search for AMMCLIB and select AMMCLIB for S32K3xx/S32M27x: stefanvlad_12-1779987760221.png
Click Install/Update 1 item(s) and next stefanvlad_13-1779987884046.png
Read and Click on I accept the terms and press Finish stefanvlad_14-1779987944058.png
Select the Authority/Update Site https://www.nxp.com and Trust Selected stefanvlad_15-1779987973847.png
Select X509 and Trust Selected stefanvlad_16-1779988044438.png
Restart S32 Design Studio 3.6.5
5. Open a Demo from ACH (Application Code Hub)
Open S32 Design Studio 3.6.5, select Import Project from Application Code Hub stefanvlad_1-1780063619713.png
This will open a new Window: stefanvlad_2-1780065330695.png
Click on Search window and enter "brake"
Select the Emergency LED-Based Brake Status Monitoring on FRDM-A-S32K312 stefanvlad_0-1780063360588.png
Click on GitHub link — this will trigger S32 Design Studio IDE to automatically retrieve project attributes, then click Next>.
Select main branch and then click Next>.
Select your local path for the repo in Destination->Directory window. The S32 Design Studio IDE will clone the repo into this path, click Next>.
Select Import existing Eclipse projects then click Next>.
Select the project in this repo (only one project in this repo) then click Finish.
In Project Explorer, right-click the project and select Update Code and Build Project:
stefanvlad_3-1780065674210.png
This will generate the configuration (Pins, Clocks, Peripherals), update the source code and build the project using the active configuration (e.g. Debug_FLASH ). Make sure the build completes successfully and the *.elf file is generated without errors.
Go to Debug and select Debug Configurations. There will be a debug configuration for this project:
stefanvlad_4-1780065730779.png
Select the FRDM_A_S32K312_BRAKE_MONITORING_Debug_FLASH_PNE configuration and press Debug: stefanvlad_6-1780065836787.png
Now the perspective will change to the Debug Perspective. Use the controls to control the program flow.
Results: The LED strip lights up in different colors to indicate the current voltage level being monitored. Upon startup, all LEDs perform a test sequence to verify functionality. During normal operation, the entire strip changes color based on the measured voltage: green for safe levels, yellow for moderate levels, orange for elevated levels, and red for critical levels, providing real-time visual feedback of the electrical signal being monitored.
stefanvlad_5-1780065756598.gif
6. Running a Motor Control Demo from ACH
Open S32 Design Studio 3.6.5, select Import Project from Application Code Hub - Motor Control
Open the example: PMSM Motor Control Sensorless dual Shunt FOC on FRDM-A-S32K312 stefanvlad_17-1779988229433.png
Follow the same steps as above in 5. Open a Demo from ACH (Application Code Hub)
After the executable file is downloaded to the board:
Disconnect the FRDM-A-S32K312 board from the PC.
Insert the DEVKIT-MOTORGD on top of the FRDM-A-S32K312 ensuring proper pin alignment.
Plug-in the 12V power supply to the DEVKIT-MOTORGD.
Reconnect the USB Type-C cable to the FRDM-A-S32K312 K312_MC_KIT.png
The RGB LED, User Buttons are on top side, Reset Button is on the left side, while the 12V power, Motor Phases and USB Type-C are on the right side. K312_MC_KIT_TOP_A.JPG
Open FreeMASTER_control/S32K_PMSM_Sensorless.pmpx project file: stefanvlad_1-1780066630032.png
This will launch another window with FreeMASTER: FreeMASTER_Connect.png
Press GO button to connect at 115200 baud.
In the App Control Tab, press On and set Speed Required to 1000 RPM: FreeMASTER_Running.png
Apply a small mechanical load to the motor (friction force to the motor shaft) and observe the iABC currents: FreeMASTER_Waveforms.png
Here is a short video with the steps above explained:
7. Conclusion
These steps conclude the Getting Started with the FRDM-A-S32K312 board using the latest S32K3 FRDM Automotive Bundle and examples from Application Code Hub (ACH).
For more details, refer to:
The corresponding Readme for the selected ACH example.
Thank you for your time,
Stefan V.
查看全文