S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
For S32 Design Studio v3.5 and earlier, there is a known issue when the S32 Configuration Tools are invoked from command line from a location outside of the S32DS installation directory. The following error is reported: java.lang.reflect.InvocationTargetException at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method) at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance(Unknown Source) at java.base/jdk.internal.reflect.DelegatingConstructorAccessorImpl.newInstance(Unknown Source) at java.base/java.lang.reflect.Constructor.newInstance(Unknown Source) at com.nxp.swtools.common.utils.runtime.SingletonProvider.getSingletonInstance(SingletonProvider.java:46) at com.nxp.swtools.common.ui.utils.swt.internal.SWTFactory.getSingletonInstance(SWTFactory.java:421) at com.nxp.swtools.common.ui.utils.swt.SWTFactoryProxy.getSingletonInstance(SWTFactoryProxy.java:448) at com.nxp.swtools.dcd.controller.DCDController.getInstance(DCDController.java:84) at com.nxp.swtools.dcd.DCDStartup.earlyStartup(DCDStartup.java:23) at com.nxp.swtools.provider.SWToolsPlatform.initializeAllTools(SWToolsPlatform.java:702) at com.nxp.swtools.framework.Application.start(Application.java:475) at com.nxp.swtools.framework.Application.start(Application.java:445) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source) at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source) at java.base/java.lang.reflect.Method.invoke(Unknown Source) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:591) at org.eclipse.equinox.launcher.Main.run(Main.java:1462) Caused by: java.lang.NoClassDefFoundError: javafx/beans/property/SimpleBooleanProperty at com.nxp.swtools.bootimage.controller.ABootController.<init>(ABootController.java:37) at com.nxp.swtools.dcd.dcf.common.DCDCommonController.<init>(DCDCommonController.java:90) at com.nxp.swtools.dcd.controller.DCDController.<init>(DCDController.java:43) ... 24 more Caused by: java.lang.ClassNotFoundException: javafx.beans.property.SimpleBooleanProperty cannot be found by com.nxp.swtools.bootimage_1.0.0.202207251223 at org.eclipse.osgi.internal.loader.BundleLoader.findClass(BundleLoader.java:519) at org.eclipse.osgi.internal.loader.ModuleClassLoader.loadClass(ModuleClassLoader.java:170) at java.base/java.lang.ClassLoader.loadClass(Unknown Source)   Resolution: To resolve the issue: Invoke the command from within the installation directory, for example, from 'C:\NXP\S32DS.3.5\eclipse' OR Change "{S32DS Installation Folder}\eclipse\s32ds.ini" by setting the javafx path from relative to absolute. So, if default installation is used, then: Change -Defxclipse.java-modules.dir=jre/javafx-sdk-11.0.2/lib To -Defxclipse.java-modules.dir=C:/NXP/S32DS.3.5/eclipse/jre/javafx-sdk-11.0.2/lib   In addition, if it is desired to suppress unimportant warning messages: go to {S32DS installation folder}\eclipse\configuration, open logging.properties file and change com.nxp.swtools.level = SEVERE
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.1         Austin, Texas, USA April 4, 2019    The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio v3.1.  Here are some of its major features: NXP GCC toolchains for ARM32 and aarch64 bareboard and Linux targets (GCC version 6.3.1 20170509, build 1574 revision g924fb68) S32 Debug Probe support provided with S32 Debugger and S32 Trace tool for S32V234 S32 Trace tool is integrated to provide software analysis features (profiling, code coverage, and other) P&E Debugger support for S32V23x Lauterbach Trace32® support S32 Flash Tool is delivered to support Flash/SD/MMC memory programming for S32V234 S32 SDK for S32V23x 0.9.0 Beta is integrated. Release notes here. The S32DS Extensions and Updates S32 Configuration Tool framework (EAR7) with the Pin, Clock, Peripheral, DCD, IVT, and DDR Configuration tools S32 Design Studio Versions Versioning convention has changed. The version of this release identified in red box below: Complete S32 Design Studio v3.1 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application package available is Vision S32V2xx  (Other packages are coming soon). The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 2          What is new? Integrated S32 SDK RTM-SR 3.0.1 (see the S32 SDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1 ) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'RSDK 1.3.0 for S32R274 and S32R372' package and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Processing S32 Design Studio v3.4 Update 1 for S32G2         Austin, Texas, USA Apr 30, 2021 The Automotive Processing' Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the  S32 Design Studio v3.4 Update 1 for S32G2 Here are some of major features:​ S32 Configuration Tool framework 1.4 with the Pin, Clock, Peripheral, DCD, IVT, DDR and QuadSPI Configuration tools (SDK/RTD packages required to get support for particular device)  Updates S32 Debugger  Updated S32 Flash Tool Update is available for online install on update site and for download on flexera  S32G2 support: (SW32G2_S32DS_3.4.1_D2104.zip) updated version of header files in accordance with RM Rev 3 Update is available for online install on update site and for download on flexera. Note that Update 1 (S32DS Platform Package version 3.4.1 and S32DS Platform Tools package version 3.4.1) is required for the S32G2 support package. It is included into archive for download. Installation instructions The update is available for online (via Eclipse Updater) or offline installation   online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button   offline installation:   go to S32 Design Studio product download page: S32 Design Studio for S32 Platform -> Downloads, click 'Download' button next to S32 Design Studio 3.4 -- Windows/Linux from the Product Information page, select S32 Design Studio 3.4 Update 1, support for S32G2 family then select 'SW32G2_S32DS_3.4.1_D2104.zip' to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add the downloaded archive as a software site. Click "Add Software Site" and browse to select the archive file downloaded in the prior step        Select from available items and click "Install/Update" button. This will start the update installation process.   Technical Support please use public community for questions https://community.nxp.com/community/s32/s32ds  
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 13          What is new? Integrated Radar SDK RTM 1.5.0 (replacing 1.4.0) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8, Update 10, Update 12)   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file      Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step   Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
This short video is a presentation of DDR tool. It contains a minimum requirement and troubleshooting for starting with DDR and S32G and an initialization training for S32G2-EVB
記事全体を表示
Dear S32DS users, S32 Design Studio for ARM v1.3 Update 1 has been released.  The update is available for online or offline installation. For online installation please select predefined NXP repository in "Help" -> "Install New Software..." dialog and proceed to installation. For offline installation please go to S32 Design Studio product page -> Downloads section and download the "S32 Design Studio for ARM v1.3 - Update 1" file: Then start S32DS and go to Help -> Install New Software... Add a new "Archive" repository, browse to select the downloaded file: Tick all the update items and proceed to installation. The main new feature is beta S32K SDK v0.9.0. Attached are the release notes.
記事全体を表示
This document details how to create a new project in S32 Design Studio and build using the existing code and makefile provided within the NXP Vision SDK example projects. If you are creating a new makefile project with code from any other source, the procedure may be different. Before creating a new makefile project from existing code we need to add some paths to the environment variable PATH and a couple of new environment variables. There are 3 main methods for adding these paths and variables. Which method depends upon your needs. Method 1 The paths and variables can be added to each project individually. This is useful if you only want these changes to affect a small number of projects. Or if your projects require different paths and variables. Note: these changes would be made after the project is created (shown in steps 15 - 17 below) Method 2 The paths and variables can be added to the entire workspace within S32DS . These will not be visible outside of S32DS and therefore will not affect the entire Windows environment. This is useful if you have a large number of projects with common requirements for paths and variables and do not want them visible any tools outside of S32DS. Method 3 The paths and variables can be added globally to the Windows environment and will affect all installed tools. This method is not recommended. Once you have selected a method, add the following paths to the PATH variable (paths shown using the default installation settings for S32DS): C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm32-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-linux\bin C:\NXP\S32DS.3.1\S32DS\build_tools\msys32\mingw32\bin or if within Eclipse (can use variables, which don't need to be updated should the layout of S32DS installation change in a future release) ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} It is also necessary to add the following Windows system variables: Variable Name: S32V234_SDK_ROOT Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\s32v234_sdk Variable Name: APU_TOOLS Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\APUC The following steps demonstrate the procedure based on Method 1 above. 1) Launch S32DS for Vision 2) Click New 3) Select 'Makefile Project with Existing Code' 4) Select Next 5) Enter a name for the project. 6) For 'Existing Code Location',    a) Select 'Browse...' and then select the directory  C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\demos\isp\isp_sonyimx224_rgb_yuv_gs8    b) Click OK 7) For 'Toolchain for Indexer Settings', select the option which matches your desired build configuration. For our example here, we will select 'ARM Linux 64-bit Target Binary Toolchain'. See the Vision Extension Package User Guide for more details on the toolchain options. This sets up some toolchain paths, but later we will set more for the specific needs of the VSDK examples. 😎 Click Finish 9) Right-click on the project from the Project Explorer. Select Properties 10) Go to section 'C/C++ Build' 11) Go to the 'Behavior' tab and in the field next to 'Build', enter:    ISP examples: 'allsub'    APEX examples: 'APU_COMP=nxp allsub' 12) Go to 'Builder Settings' tab, in 'Build location' section change the path for the 'Build directory'. Click on 'Workspace...' button 13) In the Folder selection menu, select the subfolder 'build-v234ce-gnu-linux-d' and click OK 14) Go to section 'Environment' 15) Select the environment variable 'PATH' and click 'Edit...' 16) Add the path variables to the value field, each separated by a comma ';' ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} Click OK 17) Click 'Add...' 18) Click 'Add...' and enter variable name 'APU_TOOLS' and value '${S32DS_APU_TOOLCHAIN_DIR}' Click OK 19) Click OK to close the Properties menu. 20) Click on 'Build' 21) Once the build is complete, the binary file (ELF) will be created
記事全体を表示
A typical debug session will begin by downloading code to Flash and then debugging from main() onwards. However, to explore an already running system a debug connection (attach) can be made to the target MCU without affecting the code execution (at least until the user chooses to halt the MCU!).   Note: Source level debug of a running target is only possible if the sources of the project to be attached exactly match the binary code running on the target.   Click the (Debug As) button on the toolbar, then click Debug Configurations from the drop-down menu. In the left pane of the Debug Configurations dialog box, expand the debugging interface specified in the project settings and click the required launch configuration. After you click the configuration in the left pane, the configuration settings appear in the right pane grouped in tabs. PEmicro Select the Startup tab, then set the ‘Attach to Running Target’ check box as below: When a debug connection is made, the target will continue running until it is paused.   SEGGER J-Link Select the Debugger tab, then set the ‘Connect to running target’ check box as below: Unfortunately, this feature currently not supported.
記事全体を表示
The S32 Design Studio for S32 Platform supports the S32G274A device with the S32 Debugger. This document provides the details on how to setup and begin a debugging session on the S32G274A evaluation board.   Preparation Setup the software tools Install S32 Design Studio for S32 Platform Use the Extensions and Updates menu within S32 Design Studio for S32 Platform to add the S32G2xx Development Package.   Setup the hardware Confirm the setup of the S32G274A evaluation board.  Configure the JTAG. The S32G274A evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.   Procedure Open the Debug Configurations menu, then follow the steps depending on whether an S32 Debugger configuration exists for your project. If the project was created using the New Project Wizard in S32 Design Studio for S32 Platform, and the S32 Debugger was selected as the debugger, then it likely has existing debug configuration(s).     S32 Debugger Configuration(s) Exist If existing S32 Debugger configuration, proceed with probe configuration. Otherwise, skip to the next section. Below is shown the debug configuration which appears for the provided SDK example project 'hello_world_s32g275a'. The suffixes 'debug', 'ram', and 's32debugger' refer to how the project was built and the debugger the configuration is for. Select the debug configuration which corresponds to the project, build type debug, and primary core (if a multicore project) Select the Debugger tab Select the Interface (Ethernet/USB) by which the S32 Debug Probe is connected. If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected via USB to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB) If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address.   S32 Debugger Configuration(s) Do Not Exist There might be no existing debug configuration if the project is being ported from another IDE or was created to use another debugger. Select the S32 Debugger heading and click New Launch configuration (or double click on the S32 Debugger heading, or right click on the S32 Debugger heading and select New from the context menu) A new debug configuration appears with the name set to the name of the active project in the Project Explorer window(this can be set by opening a file from the project or selecting an already opened file from the project in the editor), and the build type which was used to build it. If this is not matching your intended project then it can either be modified to match or deleted and recreated after the active project has been changed to the desired project. Adjust the name of the project as desired. From the Main tab, check that the Project field is set to the correct project name, as listed in the Project Explorer, and that the C/C++ Application is set to the ELF file which was built. If the Project field is not correct, click Browse... and then select the correct project name from the list. If more than one project is open in the workspace, then each will be listed. This shows how, regardless of which project is active in the C/C++ perspective, any available workspace project could be associated. This can be useful when reusing a debug configuration from one project in another. This is not common, but if the C/C++ Application is not correct, click Search Project... and then select the correct binary file (will only work if Project field is correct and project was successfully built). Switch to the Debugger tab, Click 'Select device and core' and then select the correct core from the list. In this case, the M7_0 core is correct. If this is not the primary core, then uncheck the box next to 'Initial core'. This is done only for multi-core projects for the non-boot cores. This causes the scripts to skip the initialization of the core as the boot core will launch the other cores so additional initialization will not be required. Select the Interface (Ethernet/USB) by which the S32 Debug Probe is connected. If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB) If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address. Click Apply Click Debug. This will launch the S32 Debugger. When the debugger has been successfully started, the Debug perspective is opened and the application is executed until a breakpoint is reached on the first line in main().    
記事全体を表示
There are 2 methods to run; GUI, and terminal window. GUI Method 1) Make sure EVB is powered and connected to PC via USB (micro to USB) 2) Launch DDR Stress Test Tool, C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\DDR_Tester.exe 3) Load Image (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\bin\s32v234_ddr_test.bin) 4) Load Init Script (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\scripts\S32V234_LDDR2_MMDC0_2Gb.inc) 5) Select COM port 6) Press Download, then wait for it to complete. (may temporarily show 'not responding') 7) In 32bit Memory Read/Write section, enter address 80000000 in ADDR field. 😎 Change SIZE to 32 WORD 9) Click Read 10) See results 11) In DDR Stress Test section, enter 533 in both Start Freq and End Freq fields 12) Click Stress Test 13) See results 14) Results can be saved (C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\log) Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach AND via USB cable. 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'n' to decline the DDR Calibration 11) Enter 'y' to accept the DDR Stress Test 12) Enter Start and End frequencies (for example, enter 533, as was done in GUI method) 13) Enter 0 to run only once 14) See the results
記事全体を表示
The NXP device S32R45 has accelerators that can be programmed. The S32 Debugger included within the S32 Design Studio for S32 Platform IDE with the S32 Debug Probe provides the ability to debug these accelerators. The accelerator covered in this document: Linear Algebra Accelerator (LAX).      Section map:           Preparation               Setup the software tools                              Setup the hardware             Procedure                Create A New Debug Configuration                             Simulator                             Physical Hardware                Start A Debug Session                             Standalone                             Multi-Core                Debugging LAX Once Debug Session is Started               Multi-thread LAX Debugging: IPPU & VCPU                     Multi-LAX core Debugging                     Preparation   Setup the software tools   Install S32 Design Studio for S32 Platform    Install the S32R4xx development package and the Radar extension package for S32R4xx. Both of these are required for the LAX accelerator.      Setup the hardware   Confirm the setup of the S32R45 evaluation board. Connect the power supply cable   Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable. Connect the S32 Debug Probe to the host PC via USB cable OR via Ethernet cable (via LAN or directly connected and configured for static IP address)  and power supply connected to USB port.   Launch S32 Design Studio for S32 Platform   Open existing project or create a new project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.     Procedure   The procedure for starting a debug session and accessing the associated accelerator-specific registers is detailed here.    Application code executing on the LAX accelerator can be debugged using a simulation as well as on physical hardware.   Debugging using simulation occurs entirely on the PC and no physical hardware is required.      When debugging LAX on physical hardware, this is primarily conducted through one of two methods:   Standalone: the LAX executable is loaded by a debugger over JTAG using a probe and only the LAX core is executed and available for debugging.   Multi-core: the LAX executable is included within A53 executable, the A53 application loads the LAX executable to the LAX core and both A53 and LAX core are available for debugging. The debug connection is made to the two cores through one of two methods:   Baremetal/Bareboard: the debugger connects to both the A53 and LAX cores using the probe over JTAG.   Linux BSP: the debugger connects to the A53 core, which is running Linux BSP, using a remote Linux connection over Ethernet and then connects to the LAX core using the debug probe over JTAG.      Before a debug session can be started a debug configuration must exist.       Create A New Debug Configuration   If the New Project Wizard was used to create the project using the S32DS Application Project option, then there was an opportunity to select the desired debugger from within the wizard. If the desired debugger option was selected at this time, then the needed configuration already exists and will only require adjustments to the hardware connection settings (no hardware settings for LAX Simulator).     If the New Project Wizard was not used to create the project OR the currently desired debugger was not the one selected at the time of project creation, a new debug configuration must be created.       With the existing project selected in Project Explorer, open the Debug Configurations Menu: Run -> Debug Configurations     Having the existing project selected in the Project Explorer view will make the creation of a new launch configuration easier as many settings will be imported from the selected project. To select a project, click on it so it becomes highlighted.   Next, select the debugger for which the new debug configuration will be created.                    Simulator   To create the new configuration, either click on the ‘New launch configuration’ button from the toolbar at the top and to the left, or right-click on the ‘LAX Simulator’ and select ‘New Configuration’ from the menu.     Once the configuration is created it will be displayed and any errors with the configuration will be shown. If the project was selected in the Project Explorer, then the Name of the debug configuration will contain the project’s name and the Project and C/C++ Application fields will be populated as well. The C/C++ Application field will only be populated if the build output executable exists. Confirm these values are correct before moving on.     There is an error showing that the Device core ID is not specified on the Debugger tab. Switch to the Debugger tab and click on the button ‘Select device and core’.     From the Select Target Device and Core window, expand the listing until all cores are listed. Since the LAX Simulator only supports LAX cores on the S32R45, that is all which is listed. Select the desired LAX core and click OK.     Now that the device and core are selected, the only correct initialization script associated with the LAX is selected automatically.     No further changes are required. Click Apply to save the changes or if you are ready to debug with the LAX Simulator, then click Debug and the changes will be saved and the debug session will launch.      Physical Hardware   To create the new configuration, either click on the ‘New launch configuration’ button from the toolbar at the top and to the left, or right-click on the ‘S32 Debugger’ and select ‘New Configuration’ from the menu.     Once the configuration is created it will be displayed and any errors with the configuration will be shown. If the project was selected in the Project Explorer, then the Name of the debug configuration will contain the project’s name and the Project and C/C++ Application fields will be populated as well. The C/C++ Application field will only be populated if the build output executable exists. Confirm these values are correct before moving on.     There is an error showing that the Device core ID is not specified on the Debugger tab. Switch to the Debugger tab and click on the button ‘Select device and core’.     From the Select Target Device and Core window, expand the listing until all cores are listed. Notice that all supported cores on the S32R45 are listed. Select the desired LAX core and click OK.     Now that the device and core are selected, a generic initialization script associated with the LAX is selected automatically, however, this may not be the correct one. If debugging Standalone, meaning only LAX core will be debugged, then the automatic selection   ‘s32r45_generic_bareboard_all_cores.py’ is correct. This script will initialize all of the cores so the LAX can execute properly. If debugging Multicore, meaning both A53 and LAX will be debugged, then the A53 and LAX cores will already be initialized by the time the debugging on LAX begins. So a different script that doesn't initialize all of the cores is needed. Click ‘Browse’ and navigate to ‘{install_dir}\S32DS.3.5\S32DS\tools\S32Debugger\Debugger\scripts\s32r45’ and select the script ‘s32r45_attach.py’. The attach script will allow to start debugging on a core that is already initialized. Refer to the S32 Debugger User Guide, or the document 'README.txt' located in the same folder as these script files for details on all of the provided scripts.     Confirm the setting of the ‘Initial core’ checkbox. This box should be checked within the debug configuration that establishes the first connection to the target device via S32 Debug Probe. When this box is checked, the Debug Probe Connection interface and GDB Server settings become available. The probe connection only needs to be configured once and only one GDB Server needs to be running for each debug session. Therefore, this box should be checked for standalone debugging or for multicore debugging where A53 core is debugged via Remote Linux. If the A53 and LAX cores are debugged via the S32 Debug Probe, then this box should be checked for the A53 debug configuration and should not be checked for the LAX debug configuration.   If this is a standalone debugging of only the LAX core, setup the Debug Probe Connection. Select either USB or Ethernet, depending upon your hardware setup. If USB is selected, the COM port for the S32 Debug Probe will automatically be detected (unless not connected or more than one probe is connected). If Ethernet is selected, then enter either the hostname (fsl + last 6 digits of MAC address) or IP address. It is highly recommended to press the ‘Test connection’ button to confirm the hardware connection is correctly configured. See the included ‘S32_Debug_Probe_User_Guide.pdf’ for more details on the setup of the S32 Debug Probe.     Check that the GDB Client section has the correct path to the LAX GDB executable. It should point to the variable ‘S32DS_R45_GDB_LAX_PATH’.     Startup tab check the following settings   Load image is checked for standalone debugging, NOT checked for multicore debugging. Basically, if it is loaded by A53 core (contained in A53 ELF file), then it does not need to be loaded.   Load symbols is checked. The only time you would not check this box is if there is no project binary containing symbols available.   Set breakpoint at main and Resume are checked for standalone debugging, NOT checked for multicore debugging.     Now you are ready to start debugging. If debugging Standalone, click ‘Debug’. If debugging Multicore, switch to the A53 debug configuration (either C/C++ Remote Application or S32 Debugger) and start the A53 debug session first. Once the A53 debug session is running, advance the program counter to the line just after LAX is initialized.       Start A Debug Session   Starting a LAX debug session are different depending upon whether Standalone or Multi-core debugging is required. The steps for each method are detailed in separate sections below.   For convenience, the example project for S32 Design Studio from the RSDK, ‘RSDK_S32DS_template’, will be used to demonstrate multi-core A53/LAX debugging. Note: Unfortunately, this example project is not setup for standalone debugging because there is no main() executing on LAX to call the    LaxVectorAddGraph(). So the standalone debugging steps will be presented only to highlight the different setup required. For instructions on loading this example project to your workspace, see ‘HOWTO: Create New Project from Example  RSDK_S32DS_template from Radar SDK’.      Standalone   If the standalone bareboard debugging of only LAX core was supported by the RSDK_S32DS_template example, here are the steps which would be required.   Click on the LAX project so it is highlighted, then build it to ensure it builds clean and that the executable exists.     From the menu at the top, select Run -> Debug Configurations…     Select the standalone debug configuration for LAX core. In the case of the RSDK_S32DS_template example project, only the multi-core debug configuration is supported. In this case, the standalone configuration will need to be created. Right click on the multi-core configuration and select Duplicate.  This will create an identical configuration.      Change the name as desired and then select the Debugger tab.     Click Browse next to Initialization script and navigate to the directory   ‘{install_dir}\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32r45’. Select the script  ‘ s32r45_generic_bareboard_all_cores.py’.     Adjust the Debug Probe Connection settings to match your HW setup. Use the Test connection button to confirm.      Select the Startup tab. For standalone debugging the image file will not be loaded by the A53 core, so it must be loaded by the S32 Debugger. Check the boxes for Load image, Set breakpoint at: and Resume.     Click Debug to start the debug session. All of the settings made will be applied and the debug session will be launched.      A53 / LAX Multi-Core   For multi-core debugging, the A53 core is executing an application on the Linux BSP. The EVB should be setup to boot from a flash device which has been loaded with the S32R45 Linux BSP.   Before beginning the debug sessions, be sure to load the driver dependencies (oal_driver, rsdk_spt_driver, and rsdk_lax_driver) as described in the RSDK User Manual, RSDK Offline Example section ‘Running the application’.   Start A53 debug. From the menu at the top, select Run -> Debug Configurations…     In the Debug Configurations menu, from the configuration list, expand the ‘C/C++ Remote Application’ group and select the ‘RSDK_S32DS_template_A53_Debug’ configuration.     On the Main tab, create a new connection for using the IP address of the EVB. The IP address could   be determined either by issuing a Linux command over the serial connection, such as ‘ifconfig’, by accessing the local network connected device list, or perhaps the EVB was setup with a static IP address and it is already known.     Click New… in the Connection section.   Select ‘SSH’ for connection type.   Enter the IP address in Host: field, use ‘root’ in User: field, and leave password field empty        Click Debug to start debugging on the A53 core.     The debugger will launch and execute until the first executable line in main(). See Debugger tab in Debug Configurations menu to adjust this setting.     Now that the A53 is launched, it is necessary to execute the A53 code until just after the LAX core is  initialized and buffers are allocated. Open ‘lax_processing.c’ from the ‘src’ folder in the A53 project and set a breakpoint on line 100. One way is by double-click in the space on the left side of source code editor. This is the executable line just after ‘RsdkLaxInit()’ is called.     Now press ‘Resume’ from the toolbar to advance the program counter to the breakpoint.     Wait for the breakpoint to occur.     Return to the Debug Configurations menu, select the ‘RSDK_S32DS_template_LAX_0_attach’ debug configuration and select the Debugger tab.     Adjust the Debug Probe Connection settings to match your HW setup. Use the Test connection button to confirm.     Click Debug to start the LAX debug session.   Wait for the LAX debug session to launch and stop in the disassembly. Set a breakpoint in the source code. For our example, place one in ‘lax_custom_graph.c’ on line 97, where the kernel ‘ Rsdk_LA_add_VV’ is called.     Select the LAX debug thread and press Resume so it will be ready to run to the breakpoint which was just setup.     Select the A53 debug thread and press Resume to allow execution to resume and then wait for the breakpoint to be reached in the LAX code.       The breakpoint in the LAX code has been reached. Now it is possible to perform some debugging activities on the LAX core.        Debugging LAX Once Debug Session is Started   Once the LAX debug session is started, it will be stopped and only disassembly can be viewed. Select the LAX debug thread to see.     Open the C code source file and set a breakpoint within the kernel of interest.     Press Resume on the LAX debug thread.   Now switch back to the A53 debug thread and press Resume.   The breakpoint you set in LAX will be reached and you can now start stepping through and looking at registers, etc.         Multi-thread LAX Debugging: IPPU & VCPU    Load a project which uses both IPPU and VCPU and start the debug session on LAX using one of the methods provided.   Once the debug session is started on LAX, set a breakpoint on the line containing RSDK function ‘Rsdk_AU_sync_i()’     Press Resume to advance the program counter to the breakpoint. When the breakpoint is reached, the second thread appears. The first thread contains the VCPU and the second thread contains the IPPU.     Select the second thread to see the IPPU disassembly. Now instruction stepping can be performed on the IPPU. Registers can be viewed as well.     To see the opcodes, do not use the codes shown in the disassembly view. The disassembly view does not handle cases where many opcodes are packed into a single address. Instead, use the Memory Spaces view.        If the memory spaces view is not already present, then add it from the menu Window -> Show View -> Memory Spaces.   To add a memory space, right click in the panel on the left or click on the + button at the upper right.      Multi-LAX-core Debugging   The S32R45 device contains 2 LAX cores: LAX_0 and LAX_1. To debug the additional LAX core, simply add a new debug configuration and setup for LAX_1.   Create a new debug configuration for LAX_1 by first duplicating the existing debug configuration for LAX_0.      Rename the configuration to reference LAX_1, but the project name and application file (ELD) will remain the same.     On the Debugger tab, use ‘Select device and core’ button to change the core to LAX_1, change the initialization script to ‘<device>_attach.py’, and uncheck the box next to Initial core.    Depending on how you started the debug session for LAX_0, you may need to adjust the Startup tab. The settings on Startup tab should be set to match the LAX_0 debug configuration.   Start the LAX_0 debug session first, then the LAX_1 debug session. Stepping within each can be conducted independently.
記事全体を表示
In order to improve user experience with S32 Design Studio, in this article you can find some tips and tricks.   Use-Case #1: S32 Design Studio takes to much time to perform some of UI update operations Workaround: Manually update the Eclipse configuration parameters in the s32ds.ini file Use-Case #2: S32 Design Studio takes a lot of time to open waiting for updates checking to finish Solution: Update your environment to use at least Update12 or newer or disable the checking at startup Use-Case #3: Control of package dependencies between RTD and S32DS during install/update flow Solution: Transition to Package Manager as the main/single delivery solution for SW and Tools installation. The concept of “Bundles & Use Cases” guarantee interoperability and come with customer support.    
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 2018.R1         Austin, Texas, USA December 28, 2018   The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio 2018.R1 for S32 Automotive Platform|NXP.  Major features  • NXP GCC toolchains for ARM32 and aarch64 bareboard and Linux targets  (GCC version 6.3.1 20170509, build 1574 revision g924fb68) • S32 Debug Probe support provided with S32 Debugger (support for S32V23x, RAM + FLASH) and S32 Trace tool for S32V23x • S32 Trace tool is integrated to provide software analysis features (profiling, code coverage, and other) • PEMicro® hardware debugger support provided with P&E Debugger • Lauterbach Trace32® support • S32 Flash Tool is delivered to support Flash/SD/MMC memory programming for S32V234 • S32 SDK for S32V23x 0.8.1 EAR is integrated • S32DS Extensions and Updates tool for automatic lookup and on-demand installation of software packages adding support for the NXP Arm® based processor families • S32 Configuration Tool framework (EAR6) with the Pin, Clock, Peripheral configuration tools Complete S32 Design Studio 2018.R1 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application package available is Vision S32V2xx  (Other packages are coming soon). The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
記事全体を表示
Trace functionality is supported in the S32 Debugger for A53 as well as M7 cores on the S32G, RAM-target builds. With Trace, you can record some execution data on an application project and then review it to determine the actions and data surrounding an event of interest.   This document outlines the method to begin using Trace on the S32G2xx device. We start by creating a project on which to execute the trace, however, you may start at step 2, if you are starting with an existing project. Please note, you will need to have debug configurations for the S32 Debugger setup for each core which you intend to capture trace. If you do not already have such configurations, you may copy them from another project and adapt them to the new project as shown in HOWTO: Add a new debugger configuration to an existing project.   Create a new application project, selecting the 'S32G274A_Rev2 Cortex-A53', or the M7 variant. For this example, we are using the A53 screenshots and 'S32 Debugger' options.      There should now be 4 new application projects in your workspace. One for each A53 core. The first core of the S32G274A, A53_0_0, is also a possible boot core, so this project will have build configurations for RAM and FLASH. The other A53 cores (0_1, 1_0, 1_1) will not. Build all projects for Debug_RAM and check that they build clean before proceeding. Building the A53_0_0 project will build all projects and the resulting ELF file will contain the output of all 4. Open 'Debug Configurations...' and select the 'Debug_RAM' configuration for the first core (A53_0_0_Debug_RAM_S32Debug). Switch the initialization from the default s32g2xx_generic_bareboard.py script to s32g2xx_generic_bareboard_all_cores.py in order to make the trace modules accessible. Select the 'Debugger' tab. Enter the Debug Probe Connection settings as appropriate for your hardware setup. Click Apply. Now select the Launch Group configuration for 'Debug_RAM'. It is important to use the launch group to start the debug for each core, not just because it makes it easier, but also because it is necessary to allow for some delay after the first A53 core is started before bringing the other A53 cores from reset to debug state. Press Debug Once the code is loaded to the target and the debugger has started each core and executed to the first line within main(), then it is ready to perform any of the standard debug functions including Trace. Trace does not start automatically, it must be turned on before it will start logging data. To do this, it is necessary to add the view 'Trace Commander'. It can be found by either Window -> Show View -> Other, then search for 'Trace Commander' or enter 'Trace Commander' in the Quick Access field of the toolbar and select Trace Commander from the list. The Trace Commander view will show in the panel with the Console, Problems, etc. Double-click on the tab to enlarge it.  From the dropdown with the XML configuration files, select one matching your debug project name. A configuration is generated if none is present for your debug launch the first time you open it in the debug configuration view. Click on the configure button to change settings.   Click on the Advanced Trace Generators configuration button   For each core to be logged, set the associated ELF file. Select the core, click Add, then '...', and select the elf file for that core. It is recommended to disable all cores that are not required to be traced, as they may funnel in the same buffer, occupying the limited memory. Select Data Streams. Now it is possible to change how the data is captured. Since the buffers have finite memory, they can be set to collect data until full, or to overwrite. If set to One buffer, the data will be collected until the buffer is full, then data collection stops. It is useful to gather data when starting logging from a breakpoint to gather data during execution of a specific section of code. If set to Overwrite, the data collection continues and starts overwriting itself once the buffer is full. This is useful when trying to gather data prior to a breakpoint triggered by a condition.    To turn on the Trace logging, click on the 'Close this trace stream' button. The Trace is now enabled. To collect trace data, the cores must be executing. First double-click the Trace Commander tab to return to the normal Debug Perspective view. Then, one by one, select the main() thread on each core and press Resume to start them all. If collecting from a breakpoint, start the code first with Trace disabled, wait for the breakpoint to be reached, then enable the Trace. Allow the cores to run for a period of time to gather the data, then press Suspend on each one until they are all suspended. Look to the Trace Commander tab to see that the data icon is no longer shaded and click on it to upload the trace data.   A new tab, Analysis Results, has appeared. Double-click this tab to see it better. Click on the arrow next to ETF 0 to show the data collected in the trace buffer. Notice there are 5 separate views on the captured data: Trace (raw data), Timeline, Code Coverage, Performance, and Call Tree. Trace - this is the fully decoded trace data log Timeline - displays the functions that are executed in the application and the number of cycles each function takes, separate tabs for each core Code Coverage - displays the summarized data of a function in a tabular form, separate tabs for each core Performance - displays the function performance data in the upper summary table and the call pair data for the selected function and it's calling function Call Tree - shows the call tree for identification of the depth of stack utilization See the S32DS Software Analysis Documentation for more details on settings, ways to store the logged data, etc.
記事全体を表示
Watchpoints are Breakpoints for Data and are often referred to as Data Breakpoints. Watchpoints are a powerful aid to debugging and work by allowing the monitoring of global variables, peripheral accesses, stack depth etc. The number of watchpoints that can be set varies with the MCU family and implementation. Watchpoints are implemented using watchpoints units which are data comparators within the debug architecture of an MCU/CPU and sit close to the processor core. When configured they will monitor the processor’s address lines and other signals for the specific event of interest. This hardware is able to monitor data accesses performed by the CPU and force it to halt when a particular data event has occurred. The method for setting Watchpoints is rather more hidden within the IDE than some other debugging features. One of the easiest ways to set a Watchpoint is to use the Outline View. From this view you can locate global and static variables then simply select Toggle Watchpoints.     Once set, they will appear within the Breakpoints pane alongside any breakpoints that have been set.    Watchpoints can be configured to halt the CPU on a Read (or Load), Write (or Store), or both. Since watchpoints ‘watch’ accesses to memory, they are suitable for tracking accesses to global or static variables, and any data accesses to memory including those to memory mapped peripherals.  Note : To easily distinguish between Breakpoints and Watchpoints within the Breakpoint view, you can choose to group entries by Breakpoint type. From within the Breakpoints view, click the Eclipse Down Arrow Icon Menu, then you can select to Group By Breakpoint Types as shown below:   As you can see from the above graphic, the option to set a Watchpoint is also available directly from the Breakpoint view.   When set from here, you will be offered an unpopulated dialogue – simply entering an address will cause a watchpoint to be created, monitoring accesses to that location.     Another place to set Watchpoints within the IDE is from the context sensitive menu within a Memory view.   Unfortunately, the conditional watchpoints in S32 Design Studio for S32 Platform 3.3 may not work in some cases.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 8          What is new? Integrated Radar SDK RTM 1.4.0 (replacing RSDK 1.3.0) (see the RSDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
**************************************************************************************** IDE: S32 Design Studio for ARM Version 2.2 Workspace: C:\Projects\S32DS_ARM_22 Project name: S32K142_08_CommandLine Project location: C:\Projects\S32DS_ARM_22\S32K142_08_CommandLine **************************************************************************************** 1. After you finish the edit on your codes, please close S32DS 2. Input the command(as below) at your command_line.bat  3. Run command prompt with Administrator right. 4. Run command_line.bat at command prompt   You will get the *.elf under the folder of C:\Projects\S32DS_ARM_22\S32K142_08_CommandLine\Debug_FLASH   Cheers! Oliver
記事全体を表示
Dear S32DS users, S32 Design Studio for ARM v1.3 Update 2 has been just released. What is new? The main new feature is production grade RTM version of S32K SDK v1.0.0. Attached are the release notes. Installation instructions The update 2 is available for online / offline installation. online installation: select predefined NXP S32 Design Studio update repository in "Help" -> "Install New Software..." dialog and proceed to installation.     offline installation: go to S32 Design Studio product page -> Downloads section and download the "S32 Design Studio for ARM v1.3 - Update 2" file.   Start S32DS and go to Help -> Install New Software... Add a new "Archive" repository, browse to select the downloaded Update 2 file.   Tick all the update items and proceed to installation.  
記事全体を表示
This document shows the step-by-step process to create a simple blinking LED application for the S32G family using the S32 RTD AUTOSAR drivers. This example used for the S32G-VNP-RDB2 EVB, connected via ethernet connection through S32 Debugger. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32G development package and the S32 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_With_AUTOSAR'. The name must be entered with no space characters. Expand Family S32G2, Select S3G274A_Rev2 Cortex-M7 Click Next Click '…' button next to SDKs   Check box next to PlatformSDK_S32XX_2022_07_S32G274A_Rev2_M7_0. Click OK And also, uncheck the other cores Cortex_M7_1 ,  Cortex_M7_2.   Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. Select the overview tab and disable Pins tool. Make sure to overview tab windows shows settings shown as below.  Here, we are disabling pin tools and using MCAL driver from peripheral tools for using AUTOSAR drivers. Now from Overview menu, select peripheral tools and double click to open it. In the driver sections, “Siul2_Port_1 driver” is the non-AUTOSAR version driver and so it must be replaced. Right click on ‘Siul2_Port_1’ and remove it. Keep the osif_1 driver as it is. Click on the ‘+’ next to the MCAL box. Locate and then select the ‘MCU’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Dio’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Port’ component from the list and click OK. Now components tab should show like below : Now we required to configure the different MCAL drivers that we added. Starting with Dio configuration, open the Dio configuration. Now, open the ‘DioGeneral’ tab, and select checkmark as per shown below: Now, open the ”DioConfig” tab. In that, select  “+” sign adjacent to Dio Channel. Then edit Name to Digital_Output_LED and “Dio Channel Id”  to ‘6’ instead of ‘0’. From the schematic for S32G-VNP-RDB2 EVB, we can select signal line based on your choice for the LED color for the multicolor RGB LED. Now, checking for blue user LED from the schematic, channel 6 is connected to blue LED signal, so we use channel 6 signal line to the chip on the blue LED. Similarly, so you can select signal line based on LED color you select. Now Select Port tab for Port configuration. And open the Port Configuration tab, and from that open “PortConfigSet” tab. Change the PortPin Mscr to 6 , PortPin Direction to PORT_PIN_INOUT. After change it should be as below. At the bottom you will find the “UnTouchedPortPin ’’ . Click on “+’’ and add PortPins. Now add 4 port pins as per below configuration. Pins 0, 1, 4, and 5 should be setup. Now configure MCU component. Select Mcu component in MCAL, and then open the Mcu configuration. In Mcu configuration select “McuModesettingConf” from the dropdown menu as shown below. Select ‘McuPartition0Config’ and deselect checkbox for CM7_0 Under MCU Control, CM7_1 Under MCU Control, CM7_2 Under MCU Control as marked below. And it should show as below Now select the Mcupartition1Config and uncheck checkmarks from the selection boxes as shown below Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, Initialize the clock tree and apply PLL as system clock, Apply a mode configuration, Initialize all pins using the Port driver by adding – editing code before write code here comment in main function.          Mcu_Init(&Mcu_Config_BOARD_InitPeripherals);     /* Initialize the clock tree and apply PLL as system clock */     Mcu_InitClock(McuClockSettingConfig_0);     /* Apply a mode configuration */     Mcu_SetMode(McuModeSettingConf_0);     /* Initialize all pins using the Port driver */     Port_Init(NULL_PTR); Now replace the logic of for loop as shown below code section, which will enable the LED blinking for 10 times: First define the variable volatile uint8 level; globally above the main function. You also need to declare and initialize the loop variable uint8 i = 0U. Then replace the code as below: while (i++ < 10) {       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_HIGH);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000);       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_LOW);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000); } Before the 'main' function, add a delay function as follows: void TestDelay(uint32 delay); void TestDelay(uint32 delay) {     static volatile uint32 DelayTimer = 0;     while(DelayTimer<delay)     {         DelayTimer++;     }     DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_with_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. And make selection as shown in screenshot below. You need to select the ethernet connection for S32 debugger and provide its IP address Click Debug To see the LED blink, click ‘Resume' This code as it is will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
記事全体を表示