S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 1          What is new? S32 SDK for Power Architecture 0.8.2 EAR (Early Access Release) for MPC574x-B-C-G and MPC574xP derivatives (see attached release notes for more details) MPC5744B, MPC5745B, MPC5746B MPC5744C, MPC5745C, MPC5746C - 1N84S (Cut 2.1), MPC5747C, MPC5748C MPC5746G, MPC5747G, MPC5748G - 0N78S (Cut 3.0) MPC5741P, MPC5742P, MPC5743P, MPC5744P - 1N15P (Cut 2.2B) S32 SDK  Power Architecture v0.8.2 Examples - "Create S32DS Project from Example" Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
This document shows the step-by-step process to create a simple blinking LED application for the S32G family using the S32 RTD AUTOSAR drivers. This example used for the S32G-VNP-RDB2 EVB, connected via ethernet connection through S32 Debugger. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32G development package and the S32 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_With_AUTOSAR'. The name must be entered with no space characters. Expand Family S32G2, Select S3G274A_Rev2 Cortex-M7 Click Next Click '…' button next to SDKs   Check box next to PlatformSDK_S32XX_2022_07_S32G274A_Rev2_M7_0. Click OK And also, uncheck the other cores Cortex_M7_1 ,  Cortex_M7_2.   Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. Select the overview tab and disable Pins tool. Make sure to overview tab windows shows settings shown as below.  Here, we are disabling pin tools and using MCAL driver from peripheral tools for using AUTOSAR drivers. Now from Overview menu, select peripheral tools and double click to open it. In the driver sections, “Siul2_Port_1 driver” is the non-AUTOSAR version driver and so it must be replaced. Right click on ‘Siul2_Port_1’ and remove it. Keep the osif_1 driver as it is. Click on the ‘+’ next to the MCAL box. Locate and then select the ‘MCU’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Dio’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Port’ component from the list and click OK. Now components tab should show like below : Now we required to configure the different MCAL drivers that we added. Starting with Dio configuration, open the Dio configuration. Now, open the ‘DioGeneral’ tab, and select checkmark as per shown below: Now, open the ”DioConfig” tab. In that, select  “+” sign adjacent to Dio Channel. Then edit Name to Digital_Output_LED and “Dio Channel Id”  to ‘6’ instead of ‘0’. From the schematic for S32G-VNP-RDB2 EVB, we can select signal line based on your choice for the LED color for the multicolor RGB LED. Now, checking for blue user LED from the schematic, channel 6 is connected to blue LED signal, so we use channel 6 signal line to the chip on the blue LED. Similarly, so you can select signal line based on LED color you select. Now Select Port tab for Port configuration. And open the Port Configuration tab, and from that open “PortConfigSet” tab. Change the PortPin Mscr to 6 , PortPin Direction to PORT_PIN_INOUT. After change it should be as below. At the bottom you will find the “UnTouchedPortPin ’’ . Click on “+’’ and add PortPins. Now add 4 port pins as per below configuration. Pins 0, 1, 4, and 5 should be setup. Now configure MCU component. Select Mcu component in MCAL, and then open the Mcu configuration. In Mcu configuration select “McuModesettingConf” from the dropdown menu as shown below. Select ‘McuPartition0Config’ and deselect checkbox for CM7_0 Under MCU Control, CM7_1 Under MCU Control, CM7_2 Under MCU Control as marked below. And it should show as below Now select the Mcupartition1Config and uncheck checkmarks from the selection boxes as shown below Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, Initialize the clock tree and apply PLL as system clock, Apply a mode configuration, Initialize all pins using the Port driver by adding – editing code before write code here comment in main function.          Mcu_Init(&Mcu_Config_BOARD_InitPeripherals);     /* Initialize the clock tree and apply PLL as system clock */     Mcu_InitClock(McuClockSettingConfig_0);     /* Apply a mode configuration */     Mcu_SetMode(McuModeSettingConf_0);     /* Initialize all pins using the Port driver */     Port_Init(NULL_PTR); Now replace the logic of for loop as shown below code section, which will enable the LED blinking for 10 times: First define the variable volatile uint8 level; globally above the main function. You also need to declare and initialize the loop variable uint8 i = 0U. Then replace the code as below: while (i++ < 10) {       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_HIGH);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000);       Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_LOW);       level = Dio_ReadChannel(DioConf_DioChannel_Digital_Output_LED);       TestDelay(2000000); } Before the 'main' function, add a delay function as follows: void TestDelay(uint32 delay); void TestDelay(uint32 delay) {     static volatile uint32 DelayTimer = 0;     while(DelayTimer<delay)     {         DelayTimer++;     }     DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_with_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. And make selection as shown in screenshot below. You need to select the ethernet connection for S32 debugger and provide its IP address Click Debug To see the LED blink, click ‘Resume' This code as it is will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 12          What is new? Integrated S32 SDK for Power Architecture RTM 3.0.3 (replacing 3.0.2) Integrated AMMCLIB 1.1.21 This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8, Update 10)   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file      Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step   Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.     This will start the update installation process.
記事全体を表示
1. Modify your application to be compatible with RAppID BL tool. Add memory space for delay and application key in linker file (modified hello world project is in attachment):   Add data for this sections in your app (for example in main.c file): 2. Flash MPC5744P.rbf file into MCU. You can create new empty project or use existing one. Start debug Configurations and Browse MPC5744P.rbf file (located in [YOUR_RAPPID_INSTALL_FOLDER]\RBF_Files. Start debug session.  3. Modify your EVB - add jumper wire from J3-4 to J2-16  and J3-2 to J2-14. RAppID uses UART0 and to USB is connected UART1.   4. Start RAppID BL tool, select COM port where EVB is connected,  choose your s-record file and Start Boot Loader:
記事全体を表示
This document describes, how to add software site and how to install update from the 3rd party software site. 1) In S32DS, click Help->Install New Software 2) Click Available Software Sites. 3) Select required site, if available. 4) Select required site in Work with line: 5) Available updates will appear in the window below. Check GNU E200 PEMicro Interface Debugging Support 6) Click Next and new window will appear. Select required software and click Next. 7) Accept the license terms and click Finish. New software will be downloaded and installed. Hope it helps. Martin
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Vision v2.0          Austin, Texas, USA September 15, 2017 The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Vision  v2.0. The S32 Design Studio enablement simplifies and accelerates the deployment of ADAS vision and neural network solutions in automotive, transportation and industrial applications. Release Content Eclipse Neon 4.6 Framework GNU Tools for ARM® Embedded Processors (launchpad) build (4.9.3 20150529) ARM64: Linaro GCC 4.9-2015.05 Libraries included: newlib, newlib-nano and ewl2 (ewl and ewlnano) NXP Array Processor Unit (APU) Compiler P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) Fully integrated Vision SDK release v.1.0.0. (for the details on the feature set of SDK please refer to Reference Manuals) New Project wizard to create application, library and Visual Graph projects for supported devices Visual Graph tools to support ISP and APU/APEX2 program development Peripherals Register View DDR configuration and validation tools Lauterbach debugger support by new project wizard Kernel Aware debugging for FreeRTOS, OSEK. Devices supported: S32V234 Complete S32 Design Studio for Vision v2.0 release notes are available here. Installation To download the installer please visit the S32 Design Studio product page downloads section or click the direct here. The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. For more information about the product installation see S32DS Vision 2.0 Installation Manual.   Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
記事全体を表示
PE Micro is not able erase unused FLASH block - typically if your application resist in Large block and Low/Mid block is used for data storage. As a workaround you can flash empty s-record into desired area.  Create new empty project for MPC5777C for flashing custom .srecord Copy empty s-record (in attachment) into project folder. If you need different address range or s-record values - feel free modify attached python script and generate your own s-record.  Open debug configuration and modify C/C++ Application to empty s-record Add custom flash algorithm nxp_mpc5777c_1x32x64k_eeprom_highspeed.pcp via Debug -> Advanced Options. Scripts are lcated in [S32DS_INSTALL_DIR]\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.3.201803261737\win32\gdi\P&E\ Start debug session. You can check if memory is rewritten properly (in this case I write zeroes to Low/Mid block): 
記事全体を表示
You can use a project that was created in an earlier version of S32 Design Studio, but it requires changes to the build configuration settings and the project structure. Migrating ISP Application Project The following explains how to configure your ISP application project. Click File > Import... > General > Existing Projects into Workspace, then click Next. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish. Remove all VSDK specific settings from the build configuration settings: Right-click the project in the Project Explorer view and click Properties on the context menu. Open C/C++ Build > Settings and remove the following settings for the A53 build configuration: Standard S32DS C Compiler/Standard S32DS C++ Compiler > Preprocessor: Remove VSDK_UMAT_USE_OPENCV from the Defined symbols list. Standard S32DS C Compiler/Standard S32DS C++ Compiler > Includes: Remove all the ${S32DS_VSDK_DIR} paths from the Include paths list. Standard S32DS C++ Linker > Libraries: Remove all libraries from the Libraries and Library search paths lists. Click SDKs on the left pane of the project properties, then attach VSDK_MODULE_WIN to the A53 build configuration. Remove typedefs.h from the A53_inc folder. Migrating APEX2 Application Project The following explains how to configure your APEX2 application project. Click File > Import... > General > Existing Projects into Workspace, then click Next. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish. Remove some build configuration settings: Right-click the project in the Project Explorer view and click Properties on the context menu. Open C/C++ Build > Settings and remove the following settings for the A53 and TEST_A53 build configurations: Standard S32DS C Compiler/Standard S32DS C++ Compiler > Preprocessor: Clear the Defined symbols and Undefined symbols lists. Standard S32DS C Compiler/Standard S32DS C++ Compiler > Includes: Remove all the ${S32DS_VSDK_DIR} paths from the Include paths list. Standard S32DS C++ Linker > Libraries: Clear the Libraries and Library search path lists. Remove the following settings for the APU build configuration: APU C Compiler/APU C++ Compiler > Preprocessor: Clear the Defined symbols lists. APU C Compiler/APU C++ Compiler > Includes: Remove all the ${S32DS_VSDK_DIR} paths from the Include paths list and clear the Include files list. APU C++ Linker > General: Remove the script file. APU C++ Linker > Libraries: Clear the Libraries and Library search path lists. Remove the following settings for the EMU and TEST_EMU build configurations: Cross G++ Compiler > Preprocessor: Clear the Defined symbols list. Cross G++ Compiler > Includes: Remove all paths except the ${ProjDirPath} ones from the Include paths list. Cross G++ Linker > Libraries: Clear the Libraries and Library search path lists. Replace the Project_Settings/Scripts/gen_apu_load.tcl file with a copy from any APEX2 project created in new S32 Design Studio. Remove typedefs.h from the A53_inc folder and S32V_APU.lcf from Project_Settings/ Linker_Files . Right-click the project in the Project Explorer view and click SDKs on the context menu. Attach VSDK_MODULE_WIN to all build configurations. Emit the source code from the updated Visual Graph Tools projects. If you want to debug your application using APEX2 Emulator, update the debug configuration settings: Right-click the project in the Project Explorer view and click Debug As > Debug Configurations... on the context menu. In the left pane, open the configuration under C/C++ Application. In the right pane, go to the Environment tab. Edit the PATH value: ${S32DS_GCC_TOOLCHAIN_DIR};${S32DS_OPENCV_DIR}/x86/mingw/bin  Then select the Replace native environment with specified environment check box. Go to the Debugger tab and update the GDB debugger location: ${S32DS_GCC_TOOLCHAIN_DIR}/gdb.exe Migrating APEX2 Graph Project The following explains how to update your APEX2 graph diagram. Click File > Import... > General > Existing Projects into Workspace, then click Next. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish. Open the graph diagram. In the Palette pane, drag Add Kernels and drop it to the canvas. Select the kernel used in your old project. You can start typing the kernel name in the search box or use the filtering button to specify the kernel location. Click OK. Remove your old kernel and connect the Input and Output elements with the respective ports of the newly added kernel. Repeat the 5-7 steps for each kernel on the diagram. Right-click the canvas and click Validate diagram on the context menu. If a validation problem was found, the Problems view displays an error or warning. The element that caused the error is marked on the diagram with a red cross icon, so you can easily find and fix it. Migrating APEX2 Program Project The following explains how to update your APEX2 program diagram. Click File > Import... > General > Existing Projects into Workspace, then click Next. Click Browse... and browse to the project location, click OK, select the Copy projects into workspace option, then click Finish. Open the program diagram. In the Palette pane, drag Process from Graph and drop it to the canvas. Select the updated graph. Click OK. Remove your old process and connect the Inlet and Outlet elements with the respective ports of the newly added process. Repeat the 5-7 steps for each process on the diagram. Right-click the canvas and click Validate diagram on the context menu. If a validation problem was found, the Problems view displays an error or warning. The element that caused the error is marked on the diagram with a red cross icon, so you can easily find and fix it.
記事全体を表示
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the device reference manual. The Python scripts used for this task are designed and tested to work on the EVBs, where EEPROM hardware is connected via I2C.(Serial EEPROM is not implemented on all boards).   The RCON can be set by the following:    Fuses (internal to the device)  Parallel (GPIO pins/DIP Switches on EVB)  Serial (EEPROM connected via I2C)    The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.  The images shown throughout this document are of the S32G274A device implementation and are provided for illustration purposes.               Preparation    Install S32 Design Studio IDE  Use the S32DS Extensions and Updates menu to install the Development Package for the device subject to debugging. This is important as the Development Packages add the S32 Debugger support which provides access to the EEPROM programming capabilities via I2C of the S32 Debug Probe.  Connect the S32 Debug Probe to the EVB and the host PC containing S32 Design Studio installation.  Set BOOTMOD pins to boot from RCON    Set BOOT_CFG[8]=1 on the EVB, for serial RCON mode   Procedure    Depending on the way the device used and how the {device name}_i2c_RCON.py is edited, user must use the old procedure on the new one. Both detailed below. To choose between the Old procedure and the new procedure, you must check in the {device_name}_i2c_RCON.py if variables like “INTERACTIVE_MODE” and “RCON_DATA” exist. The {device_name}_i2c_RCON.py can be found in: {INSTALL_DIR}…S32DS/tools/S32Debugger/Debugger/scripts/{device_name}/ {device_name_part_name}_i2c_RCON.py If the variables exist, please use the old procedure. If the variables were removed, please use the new procedure. I.  Old procedure ( If “INTERACTIVE_MODE” variable still exists)   Open cmd window to the S32 Debugger folder where the device-specific scripts are located. ../S32Debugger/Debugger/Scripts/{device_name/part_number} Set Python path so correct version is used (if not already set in env vars)   set PYTHONPATH=C:\NXP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\N XP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages   Edit the python script to adjust the value to be programmed to RCON, {device_name}_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application.   Adjust RCON_DATA for the configuration you wish to program. Do not adjust RCON_ADDR. Adjust S32DBG_IP for the IP address of your S32 Debug Probe. Adjust INTERACTIVE_MODE i. Set True, if desired to be prompted in the command window to enter RCON_DATA      ii. Set False, if desried to have script automatically enter RCON_DATA, based on the value set     within the file. Adjust _SOC_NAME as appropriate for the specific device you are using. The valid options are defined in {device_name}_context.py Enter the command to start GDB, passing in the RCON Python script:   Windows OS: ../ S32DS\tools\gdb-arm\arm32-eabi\bin/arm-none-eabi-gdb-py.exe -x {device_name}_i2c_RCON.py OR ../ S32DS\tools\gdb-arm\arm64-eabi\bin/arm-none-eabi-gdb-py.exe -x {device_name}_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x {device_name}_i2c_RCON.py   If everything worked properly, then the value you programmed will be displated to the screen.   To exit GDB, enter ‘quit’. II.  New Procedure ( If “INTERACTIVE_MODE” variable was deleted)   Set Python path so correct version is used (if not already set in env vars)  set PYTHONPATH=C:\NXP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\N XP\S32DS.3.5\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages  Start GDB Server. (…\S32Debugger\Debugger\Server\gta\gta.exe)   Start Command Prompt and enter the command to start GDB with python: Example:   C:\NXP\S32DS.3.5_230912_devpck\S32DS\tools\gdb-arm\arm32eabi\bin\arm-none-eabi-gdb-py.exe Linux OS: arm-none-eabi-gdb-py     In s32rcon.py ( C:\NXP\S32DS.3.5_230912_devpck\S32DS\tools\S32Debugger\Deb ugger\scripts\gdb_extensions\rcon\s32rcon.py😞 Edit connection parameters (Probe IP, GDB server port, JTAG speed, etc.) Edit _RCON_SCRIPT parameter with absolute path to the desired I2C RCON script for the desired board: Example: _RCON_SCRIPT = " C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Deb ugger/scripts/s32g2xx/ s32g274a_i2c_RCON.py"      c. Source s32rcon.py in GDB. Example: source C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Deb ugger/scripts/gdb_extensions/rcon/s32rcon.py     d. Run command py rcon() in GDB. OBS:  Steps a, b can be done after c directly from GDB, using GDB py commands: Examples:  py _GDB_SERVER_PORT=45000  py _RCON_SCRIPT="C:/NXP/S32DS.3.5_230912_devpck/S32DS/tools/S32Debugger/Debu gger/scripts/s32g2xx/ s32g274a_i2c_RCON.py"   User can now use the available commands, like rcon_help, rcon_read, rcon_write to interact with the EEPROM.   User can write [command] -h for more information and mandatory parameters of the command.   User can write ‘quit’ to exit the S32 RCON services.
記事全体を表示
Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below: For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted. To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.  The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix. In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK. Now the problem should be resolved.
記事全体を表示
In recent releases of S32DS (Power v2017.R1, ARM v2.0, Vision v2.0) is new feature - you can add custom example into example list by copy example folder into [S32DS_INSTALL]\S32DS\examples path:  If you select New project from example - you can see your recently added project in User Examples folder. You can filter all examples by name or MCU model (for example all examples for S32K148):  Another useful improvement is possibility rename project before is inserted into active workspace. It allows you to have more projects based on the same example: If in your project folder is present description.txt file - the content of the file is shown in Create project dialog:
記事全体を表示
This document shows the step-by-step process to create a simple blinking LED application for the S32R45 family using the S32 RTD AUTOSAR drivers. This example used for the S32R45 EVB, connected via ethernet connection through S32 Debugger. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32R45 development package and the S32R45 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_With_AUTOSAR'. The name must be entered with no space characters. Expand Family S32R45, Select S32R45 Cortex-M7 Click Next Click '…' button next to SDKs   Check box next to PlatformSDK_S32RXX_4_0_0_S32R45_M7_0. (or whichever latest SDK for the S32R45 is installed). Click OK And also, uncheck the other cores Cortex_M7_1 ,  Cortex_M7_2.   Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. Select the overview tab and disable Pins tool. Make sure to overview tab windows shows settings shown as below.  Here, we are disabling pin tools and using MCAL driver from peripheral tools for using AUTOSAR drivers. Now from Overview menu, select peripheral tools and double click to open it. In the driver sections, “Siul2_Port_1 driver” is the non-AUTOSAR version driver and so it must be replaced. Right click on ‘Siul2_Port_1’ and remove it. Keep osif_1 driver as it is. Click on the ‘+’ next to the MCAL box. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Dio’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Mcu’ component from the list and click OK. Click on the ‘+’ next to the MCAL box again, and Locate and then select the ‘Port’ component from the list and click OK. Now components tab should show like below : Now we required to configure the different MCAL drivers that we added. Starting with Dio configuration, open the Dio configuration. Now, open the ‘DioConfig’ tab, and Edit Dio Port id to 3 as shown below: Now, in “Dio Configuration” window only, Select  “+” sign adjacent to DioChannel. Then Edit Name to “Digital_Output_LED” and Dio Channel Id to ‘5’ instead of ‘0’. From the schematic for S32GR45 EVB, checking for user LED from the schematic, channel 5 is connected to user LED signal, so we use channel 5 signal line to the chip for the user LED. So, we select the singal line for Dio channel Id 5 for the user LED connected on the S32R45 EVB. Now Select Port tab for Port configuration. And open the Port Configuration tab, and from that open “PortConfigSet” tab. Change the PortPin Mscr to ‘53’ and slew rate to ‘SRE_208MHZ_1_8V_166MHZ_3_3V’ and, PortPin Direction to PORT_PIN_INOUT as shown below: Now, at the bottom you will find the “UnTouchedPortPin ’’ . Click on “+’’ and add PortPins. Now add port pins 0, 1, 2, 3 as per below configuration Now configure MCU component. Select Mcu component in MCAL, and then open the Mcu configuration. In Mcu configuration click on MCUModuleConfiguration and then select “McuModesettingConf” from the dropdown menu as shown below. From McuModeSettingConf, select McuPartitionConfiguration tab. Then open the “McuPartition0Config” tab. And under the McuCore0Configuration or “McuCoreClockEnable” select checkbox and for “McuCoreResetEnable” uncheck the checkbox. Similarly, And under the McuCore1Configuration for “McuCoreClockEnable” select checkbox  and for “McuCoreResetEnable” uncheck the checkbox. Similarly, And under the McuCore2Configuration for “McuCoreClockEnable” select checkbox and for “McuCoreResetEnable” uncheck  the checkbox. After modification it should be as shown below: Now open the “McuPartition1Config” tab. for " Partition1 Clock Enable" select checkmark to true and for " Partition1 Clock Reset Enable" uncheck the checkmark for " CA53 CORE 0 cluster0 Core Clock Enable" select checkmark to true and for " Cortex-A53 Core 0 cluster 0 Clock Reset Enable" uncheck  the checkmark In the McuCore1Configuration, and for " Cortex-A53 Core 1 cluster 0 Clock Reset Enable" uncheck the checkmark In the McuCore2Configuration, for " Cortex-A53 CORE 0 cluster 1 Core Clock Enable" select checkmark to true and for " Cortex-A53 CORE 0 cluster 1 Clock Reset Enable" uncheck the checkmark In the McuCore3Configuration, for " Cortex-A53 CORE 0 cluster 1 Clock Reset Enable" uncheck the checkmark After modification it should be as shown below: Now open the “McuPartition2Config” tab. for " Partition2 Clock Enable" select checkmark to true and for " Partition2 Clock Reset Enable" uncheck the checkmark Now open the “McuPartition3Config” tab. for " Partition3 Clock Enable" select checkmark to true and for " Partition3 Clock Reset Enable" uncheck the checkmark Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, Initialize the clock tree and apply PLL as system clock, Apply a mode configuration, Initialize all pins using the Port driver by adding – editing code before write code here comment in main function.        /* Initialize the Mcu driver */        Mcu_Init(&Mcu_Config_BOARD_InitPeripherals);        /* Initialize the clock tree and apply PLL as system clock */        Mcu_InitClock(McuClockSettingConfig_0);        /* Apply a mode configuration */        Mcu_SetMode(McuModeSettingConf_0);        /* Initialize all pins using the Port driver */        Port_Init(NULL_PTR); Now replace the logic of for loop as shown below code section in the main function, which will enable the LED blinking for 10 times: You also need to declare and initialize the loop variable uint8 i = 0U; . Then replace the code as below after write your code comment: /*Logic for blinking LED 10 times*/ while (i++ < 10) {           /* Get input level of channels */           Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_HIGH);           TestDelay(3000000);           Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED, STD_LOW);           TestDelay(3000000); } Before the 'main' function, add a delay function as follows: void TestDelay(uint32 delay); void TestDelay(uint32 delay) {      static volatile uint32 DelayTimer = 0;      while(DelayTimer<delay)      {             DelayTimer++;      }      DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_with_AUTOSAR_Debug_RAM'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. And make selection as shown in screenshot below. You need to select the ethernet connection for S32 debugger and provide its IP address Click Debug To see the LED blink, click ‘Resume' This code as it will blink the LED 10 times, you can make changes in for loop condition to blink it infinitely.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 1          What is new? Integrated Radar SDK RTM 1.3.0 (see the Radar SDK release notes) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'RSDK 1.3.0 for S32R274 and S32R372' package and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
Requirements: PC machine with telnet client (for Windows you can use Putty - Download PuTTY - a free SSH and telnet client for Windows ) DHCP server running on your PC machine or network connection with DHCP server How to install DHCP server on Linux https://www.ostechnix.com/install-dhcp-server-in-ubuntu-16-04/  DHCP server for Windows - Open DHCP Server download | SourceForge.net      S32 debug probe connected to network (with DHCP server) and visible for your PC machine   separate network using static IP addresses (or direct connection between PC and S32 debug probe). The scenario is similar like on this picture:  Procedure:   Connect power to S32 debug probe with already connected ethernet cable and wait until green LED (RX/TX) starts blink.Connect to S32 debug probe by telnet client. You can use default domain name FSLXXYYZZ where XXYYZZ are last 6 digits from S32 debug probe MAC address or assigned IP address: Static IP address can be set by netparam static_ip_address ADDRESS:NETMASK command. Make sure that you are choosing IP address from range of your Embedded network. My network uses standard 192.168.1.xxx here is mt setings:  netparam static_ip_address 192.168.1.100:255.255.255.0 You also need to set boot config from DHCP to Static: netparam bootconfig static Turn OFF and ON again S32 debug probe and check the settings by telnet with static IP address - in my case 192.168.1.100: We are done. 
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 7          What is new? MPC574xx SDK BETA 1.9.0 S32R SDK BETA 1.9.0  Radar SDK for S32R274 & S32R372 RTM 1.1.1 AMMCLib 1.1.13 for MPC560xB, MPC560xP, MPC564xL, MPC567xF, MPC567xK, MPC574xC, MPC574xG, MPC574xP, MPC574xR, MPC577xC, MPC577xK,  MPC577xM This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
There are a number of existing ISP Graph diagrams provided within the VSDK. It is possible to import them into S32DS for Vision and use them in a new C/C++ project. The steps to do this are detailed in this document. 1) Launch S32DS for Vision 2) Select File -> New -> S32DS Application Project or select "S32DS Application Project" from the toolbar. 3) Enter a project name, such as: ISP_ISP_Generic_demo 4) Select 'A53 APEX/ISP Linux' 5) Click Next 6) Unselect the APEX2 options and 'ISP Visual Modeling' option. 7) Click Finish 😎 Select File -> New -> S32DS Project from Example or select "S32DS Project from Example" from the toolbar. 9) Select isp_generic. 10) Select Finish 11) Open isp_generic in the project explorer 12) Double-click ISP data flow ; isp_generic. The ISP data flow graph will appear in the editor 13) Define a new configuration for emitting code from the graph       a) Create a folder in the application project to receive the emitted code. Right-click on the application project and select New -> Folder.       b) Enter a name for the folder and click Finish       c) Right-click in the ISP data flow window and select Emit As -> Emit Configurations...       d) Select ISP Emitter       e) Select New Launch Configuration       f) Enter a name       g) Select the graph, Browse Workspace       h) Expand each item until you can select the .isp file. Click OK       i) Select the location of the emitted output to the application project, select Browse Workspace       j) Select the name of your application project, then OK       k) Write A53_gen to the Dynamic sequences sources folder box. This is the folder within the target project that generated code will be stored. Check the box for Emit host code.       l)Now select the location to store the configuration file. Go to the Common tab, select Shared file and click Browse       m) Select the folder name you created earlier inside ISP_ISP_Generic_demo and click OK       n) Click Apply and Emit. Dialog box will appear when code generation is successful              o) Expand the folders within ISP_ISP_Generic_demo, A53_gen, src and inc, to see the newly generated output files 14) Change to C/C++ perspective, click on ‘C/C++ Development’ 15) Build the project 'ISP_ISP_Generic_demo' for ISP 16) Open file 'ISP_ISP_Generic_demo/A53_inc/isp_user_define.h' and change '#define __DCU_BPP' to "#undef __DCU_BPP" 17) Using the method detailed in steps 8 - 10, create the example project 'isp_sonyimx224_csi_dcu'. Take from this project the file 'isp_sonyimx224_csi_dcu/A53_src/main.cpp' and use it to replace the file 'ISP_ISP_Generic_demo/A53_src/main.cpp' in the current project. Then make the following modifications:  On line 40, change <#include "mipi_simple_c.h"> to <#include "isp_generic_c.h">. On line 303, change <gpGraph_mipi_simple> to <gpGraph> AND <gGraphMetadata_mipi_simple> to <gGraphMetadata> On line 330, change <FDMA_IX_FastDMA_Out_MIPI_SIMPLE> to <FDMA_IX_ISP_OUTPUT>. Please see C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\docs\drivers\SDI_Software_User_Guide.pdf for details on what this code is for. 18) In Project Explorer, right-click on "...\A53_gen\src\isp_process.cpp" and select Build path -> Remove from -> A53 19) Select 'ISP_ISP_Generic_demo:A53' in the Project Explorer panel, then Build for A53 20) Run it remotely on the target using the method fromHOWTO: Create A53 Linux Project in S32DS for Vision. Should get results similar to this:
記事全体を表示
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.3   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.3 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family       Major Features for S32 Design Studio 3.6.3 Installer S32 Design Studio 3.6.3 is delivered with all public NPI's in a single 3GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.3 using Extension and Updates.     Added optional driver installation where user can customize the debugging functionalities.   Platform IDE and UI The latest release of Platform IDE introduces several enhancements and a wide range of bug fixes to improve stability and usability: S32 Config Tools can now generate Real Time Drivers code directly from the main S32 Design Studio perspective. A new context menu option, "Update Code and Build Project", has been added next to "Build Project" in the main S32DS perspective. When selected, this option automatically launches S32CT, triggers RTD code generation, and prepares the project for building—all without requiring the user to switch views. This enhancement significantly improves usability and streamlines the workflow between S32CT and RTD inside S32DS. In headless mode, the SDK_PATH environment variable is automatically set, with clear error reporting if any issues occur. As a result, projects with an attached SDK (such as RTD projects) that build successfully in S32 Design Studio IDE will also build from the command line without requiring manual configuration of SDK_PATH. The S32 Debugger configuration now offers an improved user experience by automatically selecting the appropriate launch configuration based on the currently selected project, rather than defaulting to the previously used one. This enhancement reduces the configuration time and the overall debugging process for users. Based on internal customer feedback, all SoC families are now kept collapsed by default in the New Project Wizard. Users can expand only the desired SoC family, resulting in a cleaner interface and more efficient use of space. Debugger performance has been improved when stepping over with registers expanded in the Watch Registers view. Previously, background operations in this view could create the impression that the debugger was stuck. This problem has now been resolved, resulting in a smoother debugging experience.   Major Features for NPIs S32K3 Family Added S32K356 phantom with supported toolchains in the S32K3xx development package. Enabled debug functionalities for S32K356 with Lauterbach and S32Debugger(blind). Enabled semihosting functionality on Lauterbach for multicore debug scenarios. S32R45 Family New version of Radar Extension Package 1.6.1 with new LAX Compiler b432 built with MSVC 2022.   This release is available for download on: S32 Design Studio 3.6.3 can be found on:  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6  Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.3 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.3, available on nxp.com , in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.3 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds  
記事全体を表示
Hi,     With S32DS and multilink, you can try the follow steps to dump flash or RAM data into file.  1. Attach    (https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375) 2. Export the data which you need    (https://community.nxp.com/t5/S32-Design-Studio/S32DS-how-to-properly-dump-RAM-in-debug-session/m-p/649974#M1089) Cheers! Oliver
記事全体を表示
The S32 Design Studio for S32 Platform supports the S32R45 device with the S32 Debugger. This document provides the details on how to setup and begin a debugging session on the S32R45 evaluation board.   Preparation Setup the software tools Install S32 Design Studio IDE   Use the Extensions and Updates menu within S32 Design Studio for S32 Platform to add the S32R4xx Development Package.   Setup the hardware Confirm the setup of the S32R45 evaluation board.  Configure the JTAG. The S32R45 evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.     Procedure Open the Debug Configurations menu, then follow the steps depending on whether an S32 Debugger configuration exists for your project. If the project was created using the New Project Wizard in S32 Design Studio for S32 Platform, and the S32 Debugger was selected as the debugger, then it likely has existing debug configuration(s).       S32 Debugger Configuration(s) Exist If existing S32 Debugger configuration, proceed with probe configuration. Otherwise, skip to the next section. Below is shown the debug configuration which appears for the provided SDK example project 'hello_world_s32r45'. The suffixes 'debug', 'ram', and 's32debugger' refer to how the project was built and the debugger the configuration is for. Select the debug configuration which corresponds to the project, build type debug, and primary core (if a multicore project) Select the Debugger tab Select the Interface (Ethernet/USB) by which the S32 Debug Probe is connected. If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected via USB to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB) If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address.   S32 Debugger Configuration(s) Do Not Exist There might be no existing debug configuration if the project is being ported from another IDE or was created to use another debugger. Select the S32 Debugger heading and click New Launch configuration (or double click on the S32 Debugger heading, or right click on the S32 Debugger heading and select New from the context menu) A new debug configuration appears with the name set to the name of the active project in the Project Explorer window(this can be set by opening a file from the project or selecting an already opened file from the project in the editor), and the build type which was used to build it. If this is not matching your intended project then it can either be modified to match or deleted and recreated after the active project has been changed to the desired project. Adjust the name of the project as desired. From the Main tab, check that the Project field is set to the correct project name, as listed in the Project Explorer, and that the C/C++ Application is set to the ELF file which was built. The name of the project can be customized, but '_' must be used instead of spaces. If the Project field is not set or incorrect, click Browse... and then select the correct project name from the list. If more than one project is open in the workspace, then each will be listed. This shows how, regardless of which project is active in the C/C++ perspective, any available workspace project could be associated. This can be useful when reusing a debug configuration from one project in another. If the C/C++ Application is not set or incorrect, click Search Project... and then select the correct binary file (will only work if Project field is correct and project was successfully built). Switch to the Debugger tab, Click 'Select device and core' and then select the correct core from the list. In this case, the M7_0 core is correct. If this is not the primary core, then uncheck the box next to 'Initial core'. This is done only for multi-core projects for the non-boot cores. This causes the scripts to skip the initialization of the core as the boot core will launch the other cores so additional initialization will not be required. Select the Interface (Ethernet/USB) by which the S32 Debug Probe is connected. If connected via USB and this option is selected for interface, then the COM port will be detected automatically (in the rare event where 2 or more S32 Debug Probes are connected to the host PC, then it may be necessary to select which COM port is correct for the probe which is connected to the EVB) If connected via Ethernet, enter the IP address of the probe. See the S32 Debug Probe User Manual for ways to determine the IP address. Click Apply Click Debug. This will launch the S32 Debugger. When the debugger has been successfully started, the Debug perspective is opened and the application is executed until a breakpoint is reached on the first line in main().  
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 5          What is new? Service Pack WCT101xS. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示