S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
There are 2 errors which produce the FNP error 0 message for which we have identified solutions:   1) That activation request yields no right to a license If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution.     This issue is due to a recent event. On October 1st, 2019, Flexera made this change. Since NXP uses Flexera for product activations, we were affected.   The solution to the issue is to enable support for TLS 1.2 within your Internet Properties.   2) com.acresso.activation.handler.ServerException If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution. This issue is known to occur on older releases of S32 Design Studio.   image.png   The version of FlexNet Publisher (FNP) used to activate the S32 Design Studio on your PC has an issue on some users machines. While we don't fully understand what change is happening to cause this issue, we have determined that an update to the version of FNP will resolve it. We have incorporated a newer version in the 3.5 release of S32 Design Studio.   Attached is a package of files (Activation.7z) which will allow you to update the version of FNP on your machine.   Enter the following command replacing the paths as noted. It should be possible to execute from CMD window located at any path. Make sure to use the ‘/’ instead of ‘\’ and if you have any paths with spaces, then enclose the full path with “.   For 64-bit OS: C:/NXP/S32DS.3.5/jre/bin/java  -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/x64"  -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   For 32-bit OS: C:/NXP/S32DS.3.5/jre/bin/java -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/i86" -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   If you have no existing S32DS installation from which to use Java, then please use the attached package (CLL_FNP.11.18.0.2.zip) and follow the instructions in the included .txt file. This package only works on Windows OS 64-bit.
記事全体を表示
This tutorial walks a user through the steps to create a new application for the S32V234 MCU using S32DS for Vision and the built in ISP Visual Graph tool. The completed application will take an image from camera, processes it on ISP and put the processed image in DDR buffers. Once the image is in DDR buffer, host (A53 core running Linux) will direct the display control unit (DCU) to display it on screen. Prerequisites: Some knowledge of the S32V234 System on a Chip (SoC) Have an understanding of the ISP architecture Be familiar with the NXP Vision SDK software Looking for Interactive Tutorial? You can view this tutorial as a video: S32 Design Studio: Getting Started – ISP Graph Tool Tutorial
記事全体を表示
Application based on FreeRTOS S32DS example performs prinf/scanf functionality in FreeRTOS. Application runs in two modes - standard run-time mode with two tasks maintained by scheduler and command mode implementing basic memory monitor. Application was tested with putty terminal (http://www.putty.org/). Putty serial terminal settings: 115200 8N1, no HW control. USAGE: In run-time mode is green LED blinking and on terminal are shown task counter values. To enter into COMMAND MODE - press button (next to LED diode). LED light switches to red and you can enter commands. Available commands: =================== F show free heap memory A set memory address V print value on address M set address to main() P previous mem page N next mem page ? help X Exit from command mode Putty configuration: Terminal output:
記事全体を表示
Dear S32DS users, S32 Design Studio for ARM v1.3 Update 1 has been released.  The update is available for online or offline installation. For online installation please select predefined NXP repository in "Help" -> "Install New Software..." dialog and proceed to installation. For offline installation please go to S32 Design Studio product page -> Downloads section and download the "S32 Design Studio for ARM v1.3 - Update 1" file: Then start S32DS and go to Help -> Install New Software... Add a new "Archive" repository, browse to select the downloaded file: Tick all the update items and proceed to installation. The main new feature is beta S32K SDK v0.9.0. Attached are the release notes.
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 2018.R1         Austin, Texas, USA December 28, 2018   The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio 2018.R1 for S32 Automotive Platform|NXP.  Major features  • NXP GCC toolchains for ARM32 and aarch64 bareboard and Linux targets  (GCC version 6.3.1 20170509, build 1574 revision g924fb68) • S32 Debug Probe support provided with S32 Debugger (support for S32V23x, RAM + FLASH) and S32 Trace tool for S32V23x • S32 Trace tool is integrated to provide software analysis features (profiling, code coverage, and other) • PEMicro® hardware debugger support provided with P&E Debugger • Lauterbach Trace32® support • S32 Flash Tool is delivered to support Flash/SD/MMC memory programming for S32V234 • S32 SDK for S32V23x 0.8.1 EAR is integrated • S32DS Extensions and Updates tool for automatic lookup and on-demand installation of software packages adding support for the NXP Arm® based processor families • S32 Configuration Tool framework (EAR6) with the Pin, Clock, Peripheral configuration tools Complete S32 Design Studio 2018.R1 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application package available is Vision S32V2xx  (Other packages are coming soon). The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
記事全体を表示
Hello,   The new official release of S32DS for Power Architecture v1.1 is available now! You can download it from S32DS product web page: S32 Design Studio IDE|NXP       This release requires the product activation! Please enter the Activation code from the notification email (it is sent after you click on S32DS download button) into the installer dialog (see the screenshots below). The Activation code is valid for both versions (Windows/Linux).     S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB) and other open-source software to offer designers a straightforward development tool with no code-size limitations. This release supports Windows 7/8/8.1/10 (32/64 bit) and Linux versions as well.   S32DS Power v1.1 main features Free of charge tool with no code size limitation (no license file required - Only acti) Eclipse Luna 4.4 Framework GNU Build Tools for e200 processors supports VLE and BookE ISA, LSP, SPE/SPE2 based on gcc 4.9.2, binutils 2.24 and gdb 7.8.2 Libraries included: newlib, newlib-nano and Freescale EWL2 (ewl and ewl-nano) P&E Multilink (with P&E GDB Server) Graphical tool for creating SPT algorithms SDK management included (FreeMASTER for 560xP, AMMCLIBs) GreenHills and Diab compilers support by new project wizard Lauterbach, iSystem** and PLS debuggers support by new project wizard Kernel Aware Debugging FreeRTOS, eCOS, OSEK. "New S32DS project from” added to support project creating from examples Devices supported MPC56xx MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A MPC5643L MPC5676R MPC57xx MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B MPC5744P, MPC5743P, MPC5742P, MPC5741P S32 S32R274   Host Operating System Support Microsoft Windows 7/8/8.1/10 32-bit and 64-bit (Home and Pro Editions) Linux versions Ubuntu 12.04/14.04, Debian 8, CentOS 7   Technical Support S32 Design Studio is supported on NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes (product & GCC build tools)   * Red items are the new features ** iSystem plugin integration with the project wizard will be available in S32DS PA v1.2   Regards, Stan
記事全体を表示
This instruction details the steps to create an image vector table, then subsequently generate a blob image which can be written to external flash on the S32R45 EVB. For this, the 'hello_world_s32r45' example project from the S32R45 SDK installed to S32 Design Studio IDE. This instruction shows the process for QSPI, however, SD, MMC, and eMMC are also supported.   The Image Vector Table (IVT) image is a set of pointers to other images which are required by the BootROM. It typically contains the following images, though not all are required to create a valid IVT image: DCD Self-Test DCD HSE Application Bootloader   The IVT Tool enables configuration and generation of the IVT image as specified in the BootROM reference manual.   Prerequisites Before using the IVT Tool, it will be useful to have already generated the binary image from your application project, it will be an input to the IVT. It may also be necessary to include a DCD image, for example, to initialize the SRAM. For application bootloader image, follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file, selecting 'Raw binary' option. For DCD image, follow the steps in HOWTO: Use DCD Tool To Create A Device Configuration Data Image .     Procedure With desired project open in project explorer (C/C++ perspective), switch to IVT perspective. Click on 'Open IVT'. In the Boot Configuration section, check that the correct Boot Target is selected. For the demonstration here, M7_0 is the correct selection. Check the 'Interface selection' section. If your intended boot device is SD, MMC or eMMC, then change the setting from QuadSPI Serial Flash. If your intended boot device is QuadSPI AND you do not have a QuadSPI parameter file to specify, then uncheck the box for 'Configure QuadSPI parameters'. QuadSPI parameters change some flash registers' settings away from the default setting and are generally required for larger memory sizes (for ex. applications over 1 MB in size, for some supported devices). From the Image Table section, depending on your configuration, turn off all unused images. For the demonstration here, the following will be changed to Reserved: Self-Test DCD, Self-Test DCD (backup), DCD (backup), Application bootloader (backup). The following images will remain enabled: DCD, Application bootloader. In DCD section of the Image Table, click 'Browse File' and select the DCD binary file. Ignore the red shading on the Start address and Size in bytes fields for now. Now the red shading should be resolved. This is appearing because when the DCD section was enabled, it added a block to the Memory Layout map. But the other blocks in the map are unchanged resulting in overlaps. To resolve this, click on the ‘Align’ button from within the Automatic Align section.. After the Memory Map has been aligned, a confirmation message will be displayed and the red shading will disappear. In Application bootloader section, again use  'Browse File' and select the application binary. When the application boot image is loaded, the tool processes the file to check if it contains the header for the application bootloader image. If the header is not found, it means that the file is only the raw code (the bin generated by S32 Design Studio) and it will be necessary to provide the values for RAM start & entry addresses (code length is automatically calculated), as noted with the expanded view and red shading. To set the RAM start pointer and entry pointer addresses, from to the C/C++ perspective: From Project Explorer on the C/C++ perspective, open the linker file (hello_world_s32r45\Project_Settings\Linker_Files\S32R45_common_ram.ld) and locate the RAM start address and enter it in both the RAM start pointer AND RAM entry pointer fields in the IVT Tool. Since the application binary file which was loaded is just a raw binary file, it is necessary to generate the full application bootloader image. The Export Image function takes the values entered for the RAM start & entry pointers and Code length, then generates the Application bootloader header. This header is added to the raw binary file producing a new image, the full application bootloader image file. Within the Application bootloader section, click 'Export Image' and enter a meaningful name for the image file. In addition to being a necessary source component of the IVT image, this file can more easily be shared or re-used to as an input to other IVT images. After the file has been generated, you will notice that the address settings section has collapsed. This is because it has replaced the file you originally selected with the newly generated one and the tool has recognized that the file contains the required header information. Click 'Export Blob Image' to generate the blob image file. This is what will be flashed to the target. Now that the Blob Image is generated, the 'Flash Image' button could be used to program the image to the target over serial connection, use the S32 Flash Tool, or over the JTAG connection using the Flash Programmer within the S32 Debugger (QSPI only).
記事全体を表示
Please note: AMMCLib SDK is standalone from S32/MPC SDK, it is intended for users who will not use the S32/MPC SDK. The AMMCLib SDK does not support all toolchains listed in S32DS new project wizard. For the toolchains it does support, It does not support all versions. The available SDKs will vary depending upon the toolchain which is selected. When creating a new S32DS Application Project, you may have noticed the S32K14x_AMMCLib_xxx SDK option in the Select SDK menu. This is the standalone version of the AMMCLib. If you plan to use one of the S32/MPC SDKs, then it most likely contains an integrated version of the AMMCLib. For this integrated case, the AMMCLib is accessed like any other S32/MPC SDK component and you would not need to add the standalone version. To add the AMMCLib SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the SDK from the list and then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', causing it to disappear. It should also be noted that there exist example projects which demonstrate usage of the AMMCLib, though these show usage of the S32/MPC SDK integrated version. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer view to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy math coding with AMMCLib!
記事全体を表示
S32 Design Studio for S32 Platform - 3.6.x releases   Date Version Release content/NPI support Download link Notes November 28, 2025 S32DS 3.6.5   S32K3 S32K1 S32M2 S32G S32ZE S32N S32R41 S32R45 S32R47 SAF8xxx S32J nxp.com Flexera Win/Linux installer for S32DS 3.6.5 with all public NPI's  integrated September 30, 2025 S32DS 3.6.4   S32K3 S32K1 S32M2 S32G S32ZE S32N S32R41 S32R45 S32R47 SAF8xxx nxp.com Flexera Automotive Software Package Manager Win/Linux installer for S32DS 3.6.4 with all public NPI's  integrated July 31, 2025 S32DS 3.6.3 S32K3 S32K1 S32M2 S32G S32ZE S32R41 S32R45   nxp.com Flexera Automotive Software Package Manager Win/Linux installer for S32DS 3.6.3 with all public NPI's  integrated May 30, 2025 S32DS 3.6.2 S32K3 S32K1 S32M2 S32G S32ZE S32R41 S32R45   nxp.com Flexera Automotive Software Package Manager Win/Linux installer for S32DS 3.6.2 with all public NPI's  integrated March 31, 2025 S32DS 3.6.1 S32K3 S32K1 S32M2 S32G S32ZE S32R41 S32R45 nxp.com Flexera Automotive Software Package Manager Win/Linux installer for S32DS 3.6.1 with all public NPI's  integrated Nov 29, 2024 S32DS 3.6.0 S32K3 S32K1 S32M2 S32G S32ZE S32R41 S32R45 nxp.com Flexera Automotive Software Package Manager Win/Linux installer for S32DS 3.6.0 with all public NPI's  integrated   S32 Design Studio for S32 Platform - 3.5.x releases   Date Version Release content/NPI support Download link Notes July  29, 2022 S32DS 3.5 base/platform package Flexera Win/Linux installer for S32DS 3.5  Sep 30, 2024 S32DS 3.5.14 Update 14 with support for S32Z2/E2 SPF2 Add-On 1.5.0 download offline package installable on previous S32DS 3.5.x installations via S32DS Extensions and Updates (see installation Note* from below) Jul 31, 2024 S32DS 3.5.13 Update 13 with support for: S32R45 Development Package 3.5.13 S32Z2/E2 Development Package 3.5.13 S32K3xx Development Package 3.5.13 S32K39x Development Package 3.5.13 S32M2xx Development Package 3.5.13 S32R45 Radar Extension 1.5.0 S32R45 BBE32 Add-On 1.5.0 S32Z2/E2 SPF2 Add-On 1.4.0 download May 31, 2024 S32DS 3.5.12 Update 12 with support for: S32N5 Development Package 3.5.12 SAF85xx and SAF86xx Development Package 3.5.12 SAF85xx Radar Extension Package 1.2.0 SAF85xx and SAF86xx BBE32 Add-On 1.3.0 download Mar 29, 2024 S32DS 3.5.11 Update 11 with support for: S32Z2/E2 SPF2 Add-On 1.3.0 SAF86xx Development Package 3.5.11 SAF86xx BBE32 Add-On 1.2.0 download Jan 31, 2024 S32DS 3.5.10  Update 10 download Dec 20, 2023 S32DS 3.5.9  Update 9 download Nov 29, 2023 S32DS 3.5.8 Update 8 with support for: S32K3xx Development Package 3.5.8 S32M2xx Development Package 3.5.8 download Sep 29, 2023 S32DS 3.5.6 Update 6 with support for: S32Z2/E2 Development Package 3.5.6 S32Z2/E2 SPF2 Add-on package for  1.2.0 S32K39x Development Package 3.5.6 download Aug 31, 2023 S32DS 3.5.5 Update 5 with support for: S32R45 Development Package 3.5.5 Radar Extension and BBE32 Add-on package for S32R45 1.4.0 S32V2 Development Package 3.5.5 download Jul 31, 2023 S32DS 3.5.4 Update 4 with support for: S32K1 Development Package 3.5.4 download Jun 30, 2023 S32DS 3.5.3 Update 3 with support for: S32Z27/E27 Development Package S32R41 Development Package S32R41 Radar Extension Package S32R41 BBE32 Add-on download Feb 28, 2023 S32DS 3.5.2 Update 2 with support for: S32G, S32R41, S32V2 Development Packages download (Note*) Installation procedure for platform update/development/extended/add-on packages: Install S32 Design Studio v3.5 (base/platform) version using Win/Linux installer Download the archive files for platform/dev/ext/add-on package. Start S32 Design Studio v3.5 and install the application package. Go to  Help > S32DS Extensions and Updates. In the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to  S32DS Extensions and Updates and can use this dialog to select desired packages. Q: How to install S32DS 3.5.6 ? A: install S32DS 3.5 base/platform using Win/Linux installer and apply Update 6 or apply Update 6 on existing S32DS 3.5.1-5 installation S32 Design Studio for S32 Platform - legacy versions   S32 Design Studio for S32 Platform 3.4 (Windows/Linux) S32 Design Studio for S32 Platform 3.4 Update 1 (for S32G2) S32 Design Studio for S32 Platform 3.3 (Windows/Linux)  S32 Design Studio for S32 Platform 3.2 (Windows/Linux)  S32 Design Studio 3.2 - Update 191226 S32 Design Studio 3.2 - Update 191219 S32 Design Studio 3.1 (Windows/Linux) S32 Design Studio 3.1 - Update 2    S32 Design Studio 3.1 - Update 190708  S32 Design Studio 3.1 - Update 190508  S32 Design Studio 2018.R1 (Windows/Linux)   Development packages S32K1 Service Pack 1 (S32 Design Studio 3.4) S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 (S32 Design Studio 3.3) Extension packages Vision Extension Package for S32V234 1.2.0 (S32 Design Studio 3.3) Vision Extension Package for S32V2xx 1.0.0 (for S32 Design Studio 3.1)   S32DS for Arm S32 Design Studio for Arm 2.2 (Windows/Linux)  S32 Design Studio for Arm 2.2 - Update 1 S32 Design Studio for Arm 2018.R1 (Windows/Linux)  S32 Design Studio for Arm 2018.R1 - Update 11  S32 Design Studio for Arm 2018.R1 - Update 10  S32 Design Studio for Arm 2018.R1 - Update 9  S32 Design Studio for Arm 2018.R1 - Update 8  S32 Design Studio for Arm 2018.R1 - Update 7 S32 Design Studio for Arm 2018.R1 - Update 6  S32 Design Studio for Arm 2018.R1 - Update 5 S32 Design Studio for Arm 2018.R1 - Update 4  S32 Design Studio for Arm 2018.R1 - Update 3 S32 Design Studio for Arm 2018.R1 - Update 2 S32 Design Studio for Arm 2018.R1 - Update 1 S32 Design Studio for Arm v2.0 (Windows/Linux) S32 Design Studio for Arm v2.0 - Update 3 S32 Design Studio for Arm v2.0 - Update 2 S32 Design Studio for Arm v2.0 - Update 1 S32 Design Studio for Arm v1.3 (Windows/Linux)  S32 Design Studio for Arm v1.3 - Update 3 & 4 S32 Design Studio for Arm v1.3 - Update 2 S32 Design Studio for Arm v1.3 - Update 1 S32 Design Studio for ARM v1.2 (Windows/Linux)    S32DS for Power S32 Design Studio for Power Architecture v2.1 (Windows/Linux)  S32 Design Studio for Power Architecture v2.1 - Update 14 S32 Design Studio for Power Architecture v2.1 - Update 13 S32 Design Studio for Power Architecture v2.1 - Update 12 S32 Design Studio for Power Architecture v2.1 - Update 10  S32 Design Studio for Power Architecture v2.1 - Update 8  S32 Design Studio for Power Architecture v2.1 - Update 7  S32 Design Studio for Power Architecture v2.1 - Update 2  S32 Design Studio for Power Architecture v2.1 - Update 1  S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux)  S32 Design Studio for Power Architecture 2017.R1 - Update 11  S32 Design Studio for Power Architecture 2017.R1 - Update 10  S32 Design Studio for Power Architecture 2017.R1 - Update 9 S32 Design Studio for Power Architecture 2017.R1 - Update 8 S32 Design Studio for Power Architecture 2017.R1 - Update 7  S32 Design Studio for Power Architecture 2017.R1 - Updates 5 and 6  S32 Design Studio for Power Architecture 2017.R1 - Update 4 S32 Design Studio for Power Architecture 2017.R1 - Update 3  S32 Design Studio for Power Architecture 2017.R1 - Update 2 S32 Design Studio for Power Architecture 2017.R1 - Update 1 S32 Design Studio for Power v1.2 (Windows/Linux)   S32 Design Studio for Power v1.2 - Update 3 S32 Design Studio for Power v1.2 - Update 2 S32 Design Studio for Power v1.2 - Update 1 S32 Design Studio for Power v1.1 (Windows, Linux)  S32 Design Studio for Power v1.1 - Update 1 S32 Design Studio for Power v1.0 (Windows)    Other Hot Fixes S32 Design Studio Offline activation issue hot fix 
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 8          What is new? S32K1xx SDK BETA 2.9.2 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7 ) Installation instructions The update is available for  (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
Problem description When installing S32 Design Studio using the offline activation method (Offline activation on S32 ) the installer may pop up an error dialog: " Error: "Invalid offline response, ResponseType"." This typically occurs on the computers that have no previous installation of S32 Design Studio.   Affected versions S32DS for ARM v1.1, v1.2, v1.3 S32DS for Power v1.1 S32DS for Vision v1.0 Newer versions should include the fix already. Solution Option A) Easiest solution is to use online method instead of offline. But in some cases it may not be possible (LAN restrictions, computer is not connected to the Internet or there is some other network obstacle etc.) Option B) Apply the hot fix attached. See the instructions below how to proceed for Windows and Linux (Ubuntu) users   Windows users Download and extract the attached archive file "licfix.zip" to your local machine (same package for Windows and Linux) Run "clean.bat" to reset trusted storage  Run "setts.bat" to run the activation fix and enter your activation ID for the product you need to activate Select offline activation type and save generated "request.xml" file Submit generated "request.xml" to your nxp.com account offline activation section and generate activation response "activation.xml" Save the created activation response, refresh the Activation response dialog and select the saved file The script is then successfully terminated and now you should be able to install S32 Design Studio Linux (Ubuntu) users Download and extract the attached archive file "licfix.zip" to your local machine (same package for Windows and Linux) Add the executable right to configure.sh script chmod 777 configure.sh Run the script as admin with parameter "install" to install appropriate libraries sudo ./configure.sh install Run the script as admin with parameter "reset" to reset trusted storage into its initial state  sudo ./configure.sh reset Run the script as admin with parameter "activate" to proceed to activation process sudo ./configure.sh activate Enter your activation ID for the product you need to activate Select offline activation type and save generated "request.xml" file Submit generated "request.xml" to your nxp.com account offline activation section and generate activation response "activation.xml" After this step the script should be terminated without any error message.   Now you should be able to install S32 Design Studio on your computer. Special thanks to Denis Robert and zhongzheng liu for your help with fix testing and to all of you who reported this nasty issue. Thank you!!! Stan
記事全体を表示
Installation & Activation HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio HOWTO: Install IAR Eclipse plug-in into S32 Design Studio for ARM  HOWTO: Activate S32 Design Studio     Getting Started HOWTO: Create a New Project in S32 Design Studio for ARM  HOWTO: Create S32DS Project from Example 'Hello World' for S32K144 (w/o SDK)    Build tools & Standard libraries  HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio  HOWTO: Add a static library file into S32 Design Studio GCC project HOWTO: Place custom data into flash memory  HOWTO: Link a binary file(s) into the application project using GNU build tools HOWTO: Execute a library function from RAM memory using GNU build tools  NEW!   Debug  & Flash Programming HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  HOWTO: Update OpenSDA Firmware on EVB Using GDB Server Monitor Commands from Eclipse GDB Console  HOWTO: Debug multiple elf files in S32 Design Studio with GDB  HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface) Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse   https://community.nxp.com/docs/DOC-345344  HOWTO: Program multiple memory types in single debug session NEW!   S32 SDK & Other SDKs HOWTO: Create FreeRTOS project in S32 Design Studio How to change package on S32DS Processor Expert  HOWTO: Create the Blinking LED example project using S32K144 SDK  HOWTO: Show FreeRTOS Threads in Eclipse Debug View with Segger J-link and NXP S32 Design Studio  Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1  Using custom FreeRTOS with S32K SDK and OSIF for ARM | MCU on Eclipse  Implementing FreeRTOS Performance Counters on ARM Cortex-M | MCU on Eclipse  HOWTO: Change the CPU Derivative in an SDK-Based Application Project  HOWTO: Working with AMMCLib SDKs  HOWTO: Working with FreeMASTER SDKs  HOWTO: Add custom SDK into existing project   HOWTO: Use SDK based example code as standalone (usable for GIT, SVN...)  NEW!   General Usage HOWTO: S32 Design Studio Command Line Interface  HOWTO: Add user example into S32DS HOWTO: Generate S-Record/Intel HEX/Binary file  HOWTO: Update S32 Design Studio  HOWTO: Set project optimization level  HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)  NEW!   Troubleshooting Troubleshooting: PEmicro Debug Connection: Target Communication Speed  Troubleshooting: Indexer errors on header file  S32 Design Studio Offline activation issue hot fix  Troubleshooting: Installer rolls back immediately following activation code entry  Troubleshooting: Activation fails with error message FNP ERROR 0 
記事全体を表示
Getting started with APEX2 S32DS: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS: Getting Started - ISP Graph Tool Tutorial 
記事全体を表示
Online update In standard situation update can be started by clicking on message box appeared after S32DS Launch: If you don't see such message - you can check for updates/update your S32DS Installation manually. On main menu bar click on Help -> S32DS Extensions and Updates  Select from available items, then click "Install/Update" button  Offline update   Download update package from Updated/Patches (for S32DS 3.x - S32 Design Studio | NXP , for ARM S32DS - S32 Design Studio IDE for Arm® based MCUs|NXP, for Power Architecture S32DS - S32 Design Studio IDE for Power Architecture based MCUs | NXP ). Click on Help -> S32DS Extensions and Updates and choose Go to Preferences.   Click Add... Click Archive... and locate the zip file you downloaded and click OK Select the packages and updates then start the installation with the Install/Update button. 
記事全体を表示
The ability to reset target MCU via debugger (also known as "in-target reset") is one of the essential feature when it comes to e.g. debugging of a code that is getting into an Exception/Fault Handler or situations like "...why my code works fine in the debugger, but fails without debug..." S32 Design Studio offers this feature for all Pemicro debug interfaces (Multilink Universal/FX, OpenSDA) and it is available in all S32 Design studio flavors (S32DS ARM, S32DS Power, S32DS Vision) Reset button icon is active only in the active debug session (debug perspective) and in the root debug context only.  By default the reset icon is inactive during project debugging: To activate the reset icon change the Debug view context to the root one. After reset is completed the execution stops at the application reset vector and the information about reset that has just occurred is displayed in GDB server console. It is also possible to execute initialization script (.mac) which is triggered by the reset action. The reset script can be selected in the  Debug Configuration (Debugger Tab -> Advanced Options -> Enable Initialization Script) For more information about initialization scripting capabilities please contact www.pemicro.com
記事全体を表示
  The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via the S32 Debugger. Note: currently only QSPI flashing is supported. Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for performing the flash programming operations. DanielBarbu_0-1729686203356.png   Open the application project containing the application to be programmed to the flash memory device. Follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file , selecting the 'Raw Binary' option. Build the project, generating the binary executable. This will be our application binary input to the IVT Tool. The IVT Tool must be used to generate the BLOB image which can be programmed to flash memory device and loaded to the RAM by the BootROM. Follow the steps in HOWTO: Use IVT Tool To Create A BLOB Image S32G274A. The resulting BLOB image file is what can be flashed to the device.   Procedure Open Debug Configuration menu Select 'S32 Debugger Flash Programmer', then right-click and select New. Enter an name for the new configuration and click Add... to add the file to be flashed. Click Browse... to select the project from the workspace where the application binary is located Select the project and click OK By default, the ELF file is found. Click Search in project to select the binary file. Select the .bin file and click OK Now we must enter the base address. Typically, this could be 0, but you may have other requirements. Click OK. Just the memory required by the new image needs to be cleared, so only check the box 'Erase all flash memory' if truly needed. Now we are ready to configure the debugger connection settings. Click on the Debugger tab. Starting from the top and working our way down, click on Select device. Select the device and click OK The correct Initialization script will automatically be set. Set the Debug Probe Connection settings to match your setup. When done, click Apply To start the flashing, click Debug When complete, the Debug perspective will show at terminated thread. DanielBarbu_0-1727863610078.png   Happy flashing with GDB!   Note, to debug this application since it will be subsequently started by the BootROM: use 's32gxx_attach.py' in the Initialization script field on the debugger tab of the Debug Configurations menu Make the following adjustments on the Startup tab within the Debug Configurations menu: Uncheck "Load image"  Check "Set program counter at:" and enter the value "Reset_Handler"  
記事全体を表示
There are a number of existing ISP Graph diagrams provided within the VSDK. It is possible to import them into S32DS for Vision and use them in a new C/C++ project. The steps to do this are detailed in this document. 1) Launch S32DS for Vision 2) Select File -> New -> S32DS Application Project or select "S32DS Application Project" from the toolbar. 3) Enter a project name, such as: ISP_ISP_Generic_demo 4) Select 'A53 APEX/ISP Linux' 5) Click Next 6) Unselect the APEX2 options and 'ISP Visual Modeling' option. 7) Click Finish 😎 Select File -> New -> S32DS Project from Example or select "S32DS Project from Example" from the toolbar. 9) Select isp_generic. 10) Select Finish 11) Open isp_generic in the project explorer 12) Double-click ISP data flow ; isp_generic. The ISP data flow graph will appear in the editor 13) Define a new configuration for emitting code from the graph       a) Create a folder in the application project to receive the emitted code. Right-click on the application project and select New -> Folder.       b) Enter a name for the folder and click Finish       c) Right-click in the ISP data flow window and select Emit As -> Emit Configurations...       d) Select ISP Emitter       e) Select New Launch Configuration       f) Enter a name       g) Select the graph, Browse Workspace       h) Expand each item until you can select the .isp file. Click OK       i) Select the location of the emitted output to the application project, select Browse Workspace       j) Select the name of your application project, then OK       k) Write A53_gen to the Dynamic sequences sources folder box. This is the folder within the target project that generated code will be stored. Check the box for Emit host code.       l)Now select the location to store the configuration file. Go to the Common tab, select Shared file and click Browse       m) Select the folder name you created earlier inside ISP_ISP_Generic_demo and click OK       n) Click Apply and Emit. Dialog box will appear when code generation is successful              o) Expand the folders within ISP_ISP_Generic_demo, A53_gen, src and inc, to see the newly generated output files 14) Change to C/C++ perspective, click on ‘C/C++ Development’ 15) Build the project 'ISP_ISP_Generic_demo' for ISP 16) Open file 'ISP_ISP_Generic_demo/A53_inc/isp_user_define.h' and change '#define __DCU_BPP' to "#undef __DCU_BPP" 17) Using the method detailed in steps 8 - 10, create the example project 'isp_sonyimx224_csi_dcu'. Take from this project the file 'isp_sonyimx224_csi_dcu/A53_src/main.cpp' and use it to replace the file 'ISP_ISP_Generic_demo/A53_src/main.cpp' in the current project. Then make the following modifications:  On line 40, change <#include "mipi_simple_c.h"> to <#include "isp_generic_c.h">. On line 303, change <gpGraph_mipi_simple> to <gpGraph> AND <gGraphMetadata_mipi_simple> to <gGraphMetadata> On line 330, change <FDMA_IX_FastDMA_Out_MIPI_SIMPLE> to <FDMA_IX_ISP_OUTPUT>. Please see C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\docs\drivers\SDI_Software_User_Guide.pdf for details on what this code is for. 18) In Project Explorer, right-click on "...\A53_gen\src\isp_process.cpp" and select Build path -> Remove from -> A53 19) Select 'ISP_ISP_Generic_demo:A53' in the Project Explorer panel, then Build for A53 20) Run it remotely on the target using the method fromHOWTO: Create A53 Linux Project in S32DS for Vision. Should get results similar to this:
記事全体を表示
While the S32V234-EVB2 comes shipped with an SD card preloaded with a Linux Board Support Package(BSP), it does not support the Vision Software Development Kit(VSDK). This you will have to load yourself. There are two methods for installing the S32V234 BSP for VSDK to your SD card: 1) Download the image file from your Software Account on nxp.com and write the file to the SD card, or 2) Create the image on the SD card from ubuntu installed on a PC or virtual machine Download the image file and write it to SD card This is the simplest method, but does not allow for much customization. It is an excellent choice for those users who do not have much experience with Linux or just need something quick to get up and running with S32 Design Studio, try out the application examples, etc. Procedure 1) Login to your account on NXP.COM (if you do not already have an account, then just register for one) 2) Go to Vision SDK Software  3) Accept the license agreement 4) Select the version of VSDK you wish to use 5) Check the box next to 'VisionSDK RTM x.x.x pre-built SD Card image based on Yocto rootfs' and click 'Download selected files'. This will download the .gz file to your PC. 6) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar.gz archive file 7) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar archive file 😎 Navigate to the '\build_content\v234_linux_build\s32v234evb' folder, then unpack the sdcard-evb.tar.bz2 file 9) Unpack the sdcard-evb.tar file 10) The resulting file is sdcard-evb.img. You can use an image writing tool (such as Win32 Disk Imager download | SourceForge.net) to write this image file to the SD card. You will need to use the SD card adapter to insert the microSD card into the SD card slot on your PC, if available. If you do not have an SD card slot on your PC, there are many SD card-to-USB adapters available on the market. 11) The SD card is now ready to inserted into the SD card slot on the S32V234-EVB2 SD card slot. Create the image on SD card from ubuntu This is a better choice for more advanced users who wish to customize the BSP. To prepare an SD card for a Linux boot, it is necessary to connect the SD card to a machine with Linux OS. If a Linux OS machine is not available, then a virtual machine installed to a Windows OS machine may be used. If you have access to a Linux OS machine, skip to step 4. Procedure 1) Download and install a virtual machine VMware Workstation Player Virtual Box 2) Download Ubuntu. This tutorial uses the Ubuntu version 14.04.5.  The image will be ubuntu-14.04.5-desktop-amd64.iso. 3) Launch VMware or Virtual Box and create a new virtual machine Use downloaded Ubuntu image when requested for installer disc image file Hit Next and select Linux as the guest operating system and select Ubuntu for the version. Hit Next and name your virtual machine and specify where you want to store it. Increase the disk size to 40 GB Hit Finish and install VMware Tools for Linux, if asked 4) Within C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\os extract 'build_content.tar.gz', then extract 'build_content.tar' and navigate to the 'v234_linux_build' folder 5) Start virtual machine May need to manually connect USB-mounted SD card reader Log in to virtual machine 6) In files, go to 'Home' directory and create a folder "VSDK" 7) Within VSDK folder, copy the files image, u-boot.s32, s32v234-evb.dtb, and rootfs.tar from the 'v234_linux_build' folder.  Note: The file s32v234-evb.dtb and u-boot.s32 will have names with XXXXX-suffix for the schematic number printed on the evaluation board (EVB) you are using. Be sure to use the files which correspond to your EVB. 😎 Load the card into the reader. If you are using a virtual machine, it is recommended to use a USB adapter instead of a built-in reader in the PC. 9) Within the virtual machine, launch the terminal program 10) Within the terminal program, enter command 'cat /proc/partitions' to view the names of the partitions and identify the names of the partitions on your SD card. Perhaps it is named 'sdb'. 11) Delete all existing partitions.    a) Enter command 'sudo fdisk /dev/sdb'.    b) Enter command 'd' and then the number of the partition to delete. Repeat as necessary until all partitions have been deleted 12) Create new partitions    a) Enter command 'n' for new    b) Enter 'p' (or just hit <enter>, as this is the default) for primary    c) Enter '1' (or just hit <enter>, as this is the default) for partition number 1.    d) Press <enter> to select the default value for the First sector    e) Enter '+255M' to set the size    f) Enter command 'n' again, for partition number 2, however, press <enter> to select the default value for the 'Last sector' 13) Set the partition type    a) Enter command 't' for type    b) Enter '1' for partition number 1    c) Enter 'c' for partition type FAT32    d) Enter command 't' again, for partition number 2, however, enter '83' for partition type LINUX If you get error 16: Device or resource busy, as shown above, use commands 'umount /dev/sdb1' and 'umount /dev/sdb2' to free the pre-existing partitions. Then try again and should be ok now 14) Write the new configuration, enter 'w' 15) Try to setup the filesystems. Enter 'sudo mkfs.vfat -n boot /dev/sdb1'. If you get the error '/dev/sdb1 contains a mounted filesystem', you will need to unmount the partition first. To save time, unmount both /dev/sdb1 and /dev/sdb2. Enter 'umount /dev/sdb1' and then 'umount /dev/sdb2' Now try 'sudo mkfs.vfat -n boot /dev/sdb1' again 16) It worked, so now enter 'sudo mkfs.ext3 -L rootfs /dev/sdb2'. It will take a minute or two for this to complete. Wait until you get the command prompt again. 17) Now it's time to load the BSP content from the VSDK. But first, change the directory to the one we created earlier for the BSP files. Enter 'cd /home/user/VSDK' or 'cd VSDK'. Enter the following commands: sudo dd if=u-boot.s32 of=/dev/sdb bs=512 seek=8 conv=fsync sudo cp Image /media/user/boot sudo cp s32v234-evb.dtb /media/user/boot 18) Now we need to extract the root filesystem, change the directory to its location 19) Enter command 'sudo tar -xvf /home/user/VSDK/rootfs.tar' 20) Once the files are extracted, enter command 'sync'   Now the SD card is ready to be used in the S32V234-EVB.
記事全体を表示
There are three methods to run the configuration tool; from S32DS, from Terminal and JTAG, and from command line. S32DS Method 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach 2) Launch S32DS for Vision 3) File -> New -> S32V DDR Configuration Project 4) Enter a name for the project, for example 'DDR_Config_test'. Click Next 5) Expand 'S32V' and select 'S32V_234' 6) Click Finish to generate the project with default settings OR if you wish, to view or adjust more project settings, click Next. For this demonstration, we click Next. a. Select which DDR controller to which the settings will be applied. For this demonstration, we leave it at default (1st DDR Controller) b. There is an option to import settings from a file c. Board setting allows you to select from a list of predefined configurations, one for each of the NXP S32V234 evaluation boards i. S32V234_EVB is for LPDDR2 (SCH28899 and SCH28292(old board)) ii. X_TR_DVAL_625 is for DDR3 (SCH28662(old board)) iii. S32V234_NXP_EVB is for SCH29288 (S32V234-EVB2) iv. Custom allows for more options to be selected. See user manual for more detail d. For this demonstration, we select S32V234_EVB e. Click Finish 7) It will take a couple minutes to generate the project. You will get a prompt to pen the S32V DDR Configuration perspective. Click Yes. 😎 Now the project is generated and you can see it listed in the Project Explorer 9) Notice the Components and Component Inspector views of the S32V DDR Configuration perspective. 10) Select the component 'MMDC_0:Init_MMDC from the Components view 11) In the Component Inspector window you can see all of the configuration settings. You can modify the settings here. Changes made to some of the high-level settings may also cause changes to some of the low-level settings. There are some consistency checks that are run automatically after settings are changed which will trigger an error message in the case of an invalid configuration. a. For an example of high-level settings affecting low-level settings, try changing the 'Memory type' from LPDDR2 to DDR3. You can see the Burst Length, Column Address Width, and Row Address Width have changed. b. For an example of a consistency check on an invalid configuration, try changing the CAS Read Latency value (MDCFG0) from 8 to 12 (valid range as displayed with mouse hover tooltip shows 3-11), you will see the error appear. Change back to 8 and error is gone. 12) Open Configuration Registers view. Window -> Show View -> Other -> Processor Expert -> Configuration Registers. This shows how the settings will appear in the memory map. As you change the settings, the values will update here and the affected rows will be highlighted. Try it by changing Column Address Width in MDCTL of the Component Selector window. Likewise, you can try changing the value manually in the Configuration Registers view and see the setting in the Component Selector window update as well. *Hint: enter the name of the view in the search bar to find it quicker 13) Once all changes to the settings are complete, code can be generated. Press the 'Generate Processor Expert Code' button in the Components view. The generated .c and .h file will appear in the 'Generated_Code' folder of the Configuration project. These can be copied into your application project. OR 14) Back in the Component Inspector view, there are tabs for Import and Export settings. The Import settings tab will allow you to import existing settings files, as was also shown in the new project wizard. From the Export settings tab, you can generate a settings file for storage or sharing. The settings files for MMDC_0 and MMDC_1 for each of the supported NXP EVBs are included and can be located in 'C:\NXP\S32DS_Vision_v2.0\eclipse\ProcessorExpert\Optimization\resources\S32V\Boards' and then select the folder for the specific board. The CodeWarrior Register Text format is recommended for these files. 15) Now select the 'Validation' tab (some views, such as Configuration Registers, can be minimized for better view). Here we can execute a validation of the configuration settings we've made. Now is a good time to double check the hardware connections. 16) Select the connection method (either PEMicro or Lauterbach, depending on your setup). We will use System: S32V234; PEMICRO 17) Press 'Connect to Target' 18) Check a box for one of the scenarios. For example, select 'Read Delay Calibration' 19) Select the 'Choose Tests' tab 20) You can select tests from a list. To see the script behind the test, simply double-click on the name. For faster operation, ELF file versions are also provided. 21) Select the tests you wish to execute and press 'Start Validation'. For example select 'Write-Read-Compare-Elf', 'Walking Ones Elf', and 'Walking Zeros Elf'. 22) These tests will try different values and to determine which will work and which will not. After the test is finished, the best values are chosen and written back to the project configuration settings. To see the values change, go to the Properties tab and find 'PHY Read delay-lines Configuration' or restore the 'Configuration Registers' view and see the values changed. 23) For each test, you can see the errors which occurred in the 'Summary' tab, Test results section. There is also Updated configuration registers section which shows the register and the new value which was written to it. For more details on the errors, there is a Log tab which displays the log for each test which was run. Finally there is a Scripts tab which shows the script for each test containing the test settings. Each test box is colored to reflect the result of the test. Clicking on different ones causes the display below to change and show the results for that test. 24) The Write Delay Calibration test scenario is very similar to the Read Delay Calibration test scenario, but instead, the Write delay-lines Configuration will be updated. 25) The Operational DDR Tests run the same tests, but no value in the configuration is changed. You can set it to run for many repetitions to test for stability. Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach (to load test application) AND serial communications via USB cable(for terminal access). 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'y' to accept the DDR Calibration 11) Enter 'y' to accept the DDR frequency of 533MHz 12) Wait and watch while the test completes. 13) When the test completes, the results are shown. You will have to manually update your settings from the information displayed. 14) Next you will have the option to run the DDR Stress Test.
記事全体を表示
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the TEST_A53 build option. 3) Start debug on A53 core. Project is now built, ELF file is read to be loaded to EVB for execution. 4) Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 5) Select the debug drop-down menu and click Debug Configurations     6) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     7) The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts. You may get an error message on the first try, this is normal. Just try it again and it will work. 😎 Once the Linux GDB has started on A53 core and the initial breakpoint is reached in main(), we need to set a breakpoint at the function apu_hal_Enable().    This breakpoint has already been created for you, you just need to enable it! Locate the breakpoint in the Breakpoints view. Due to some known issues with Eclipse CDT, it is necessary to enable->disable->enable the breakpoint so it will work properly. The issue only affects this breakpoint, due to the way it is provided, and will not affect breakpoints which you set. 9) Press Resume twice, so that the breakpoint which was set at apu_hal_enable() is reached for the 2nd time. 10) Open Debug Configurations. You will see a debug configuration within the 'S32 Debugger' group (FAST9COLOR as shown below). This is the debug configuration we will use, however, it will require some setup.     11) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.       12) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   13) It may take a moment or two before the APEX2 debug thread launch is complete, see the Thread listed within the <kernel_name>[S32 Debugger] in the Debug window. Also note, a new breakpoint is listed in the Breakpoints view. This breakpoint is set for you at the start of the APEX2 graph function. 14) The debugger context is still on the A53 thread. Press RESUME and then select the APEX2 thread to see that it has stopped on the graph function break point. Now you can step through the graph. 15) To step through a kernel, locate the call to the kernel function in the graph function and set a break point on the line. 16) Press RESUME to advance the program counter to the new break point 17) Press STEP INTO to advance the program counter into the kernel. It may take several steps as the optimizations performed by the compiler produce some synchronization inconsistencies. 18) You may need to help the IDE to locate the source files. Now you can see the kernel wrapper function... and the kernel! 19) Step through, monitor variables and registers and set breakpoints.
記事全体を表示