S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 13          What is new? Integrated Radar SDK RTM 1.5.0 (replacing 1.4.0) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8, Update 10, Update 12)   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button image.png offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file      image.png Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step   image.png Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   image.png This will start the update installation process.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.3 Vision Extension Package for S32V234 1.2.0          What is new? Integrated VSDK 1.6.0   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button image.png offline installation:   go to S32 Design Studio for S32 Platform product page -> Downloads section or use direct link to download the update archive zip file        image.png Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link image.png And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step       image.png Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   image.png This will start the update installation process.
View full article
UART communication is supported in the KEA64 Bootloader .rbf file  + Supported UART0: PTA2-PTA3 pins(Speed: 115200b/s) Tested on the dev board:   Development Board TRK-KEA64 Processor PKEAZN64 MLH 2N22J
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 12          What is new? Integrated S32 SDK for Power Architecture RTM 3.0.3 (replacing 3.0.2) Integrated AMMCLIB 1.1.21 This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8, Update 10)   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button image.png offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file      image.png Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step   image.png Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.     image.png This will start the update installation process.
View full article
IVT - short for Image Vector Table, is an image with a set of pointers to other images which are required at boot by the embedded BootROM. This video will explain using S32V chip how IVT tool works and covers create and flash SDK's PIT example.
View full article
This short video is a presentation of DDR tool. It contains a minimum requirement and troubleshooting for starting with DDR and S32G and an initialization training for S32G2-EVB
View full article
DCD(short for Device Configuration Data) is the configuration information that BootROM uses to configure the peripherals on the device. This video will explain using S32V how DCD works and create a simple example to have RUN1 as default run mode.
View full article
Pin muxing is the process of assigning a peripheral function to a physical pin. This video will explain how fast and easy is to a configured pin muxing using Pins Tool from S32 Configuration Tool suite. Example is a UART project from S32V microcontroller SDK.
View full article
Has this happened to you? You just launched S32DS for Vision and opened a visual graph but the blocks are collapsed onto one another. Probably looks something like this: There is an easy solution. Just click on the 'Arrange All' button and the graph will automatically expand to a manageable state. Here is the result:
View full article
Create From Example 1 | Create an ISP Project from Example A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio. 2 | Create an APEX2 Project from Example A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Create New Project 3 | Create a New ISP Project A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio. 4 | Create a New APEX2 Project A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio. https://www.nxp.com/support/training-events/getting-started-with-s32-design-studio-ide-for-vision-2018.r1:TIP-S32DS Debug 5 | ISP Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 6 | APEX2 Debugging w/ S32 Debug Probe A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe. 7 | APEX2 Debugging with Emulator A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio. 8 | Debug a bare-board APEX2 Project A demonstration of how to debug a bareboard APEX2 image processing application project in the S32 Design Studio with Lauterbach TRACE32. 9 | Debug a Linux A53 Project A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code. 10 | Debug a bare-board A53 Project A demonstration of how to debug a bareboard A53 image processing application project in the S32 Design Studio for Vision version 2.0 using PEMicro GDB interface. The example shown also includes code for APEX, but currently PEMicro only supports debug of the A53 code.
View full article
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the A53 build option. 3) Start debug on A53 core. Project is now built, ELF file is read to be loaded to EVB for execution. 4) Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 5) Select the debug drop-down menu and click Debug Configurations     6) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     7) The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts.   You may get an error message on the first try, this is normal. Just try it again and it will work. 😎 Once the Linux GDB has started on A53 core and the initial break point is reached in main(), it is almost ready for to start debug on ISP. Click Resume as the A53 must be running before we can attach the ISP debug thread. 9) Locate the ISP debug configuration from the Debug Configurations menu. You will see a debug configuration within the 'S32 Debugger' group (in our example, isp_sonyimx224_csi_dcu_ISP as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   11) This is already done for our example, but for your application, it may be necessary to setup the symbols for the ISP engine. Go to the Startup tab and:    a) Check the box for 'Load symbols'    b) Select the option for 'Use file', click Workspace... and locate the object file (.opius) for the ISP engine you wish to debug.   12) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   13) Wait for the ISP debug launch to complete. You may notice the A53 thread has terminated. This is normal and expected since the camera input cannot be suspended. When the launch completes, the context of the Debug window will switch to the ISP debug thread. 14) Enable Instruction Stepping mode and then step one time to load the object file which was setup in step 6. 15) The ISP debugging is now running and you can step through the ISP engine, look at registers, set a break point, etc. Note: only one hardware break point is supported for ISP.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 9          What is new? S32 SDK for Power Architecture 2.0.0 RTM supporting  MPC5741P, MPC5742P, MPC5743P, MPC5744P, MPC5744B, MPC5745B,  MPC5746B, MPC5744C, MPC5745C, MPC5746C, MPC5747C, MPC5748C, MPC5746G, MPC5747G, MPC5748G, S32R274, S32R372 (see the S32 SDK release notes) AMMCLIB version 1.1.14 (see the AMMCLIB MPC574xP example release notes) Radar SDK RTM, version 1.2.0 (see the RSDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the ability to access the flash programming and debugging of the S32 Debug Probe via GDB command line. This document provides only the necessary commands specific to launching a debug session on NXP devices. It does not cover general GDB command line operations, these are covered in detail in the GNU communities and other public websites which are not associated with NXP.   Preparation Setup the software tools Install S32 Design Studio for S32 Platform  Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores. Setup the hardware Confirm the setup of the S32G274A evaluation board.  Configure the JTAG. The S32G274A evaluation board supports both 10- and 20- pin JTAG connections. The default board configuration is set to 20-pin, change the position of the jumper J59 from 2-3(default)  to 1-2, if you are using the 10 Pin JTAG interface. Both are supported by the S32 Debugger and S32 Debug Probe. Connect the power supply cable Setup the S32 Debug Probe Connect the S32 Debug Probe to the evaluation board via JTAG cable. Refer to the S32 Debug Probe User Manual for installation instructions. Use the JTAG connection as was confirmed in the previous step. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard. DanielBarbu_0-1719826642815.png     Procedure As separate debug threads need to be started for each core to be debugged, and the method for launching a debug thread differs depending upon whether it is a primary core or secondary core and if the executable image will be loaded or if the executable is already running and the debugger just needs to be attached. These scenarios will be covered by the following 3 sections: Primary Core Load Image and Run: The application image will be loaded directly to memory by the debugger and then initialized and started. The primary core will launch any secondary cores used by the application. Secondary Cores: The primary core has launched a secondary core, it is now running and the debugger will connect through the attach method. Primary Core Image Already In Memory and Running: The primary core has already been initialized and launched by other means, such as via a Linux OS on the target, so the debugger will connect through the attach method without initializing or loading the image to memory.   Please proceed with the section which applies to the core for which you are starting a debug thread.   Primary Core Load Image and Run Prepare the initialization script for the core(s) to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_generic_bareboard_all_cores.py Uncomment the following lines: #_JTAG_SPEED = 16000 #_PROBE_IP = "10.112.101.91" #_GDB_SERVER_PORT = 45000 #_CORE_NAME = 'M7_0' #_RESET_TYPE = "default" #_RESET_DELAY = 1 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True This file is used by the S32 Debugger within the S32 Design Studio IDE where the settings are provided from the GUI, so these lines are commented out in order to allow the GUI settings to have control. The commented lines are provided so the script could more easily be run by the command line method. Update the IP address line (_PROBE_IP) to match the IP address of the S32 Debug Probe which is connected to your PC. See the user guide for the S32 Debug Probe for details on how to obtain the IP address.  Update the core name (_CORE_NAME), if necessary. See s32g2xx_context.py for complete list of supported cores. Save the file with a new name to preserve the original. For example, s32g2xx_gen_bb_all_c_my_probe.py. This ensures the S32 Debugger will still function correctly. DanielBarbu_2-1729678829471.png   Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe  Should see a window appear like this: DanielBarbu_0-1729678503840.png   Ensure Environment Variable for Python is set. From command prompt, run the command:  set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages DanielBarbu_1-1729678711096.png   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: DanielBarbu_3-1729679065676.png   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_gen_bb_all_c_my_probe.py This specifies the script for initialization. py board_init() This initializes the board. It should only be called for the initial core. In a multicore debugging workflow, the debugger launch for additional cores would omit this step. py core_init() This initializes the core specified in the initialization script in step 1. DanielBarbu_4-1729679180416.png   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\New_S32G_Project\\New_S32G_Project_M7_0\\Debug_RAM\\New_S32G_Project_M7_0.elf load DanielBarbu_5-1729679752298.png   Secondary Cores After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. Some additional steps will need to be performed from within the primary core GDB session, enter the following commands: set *0x34100000 = 0x34200000  set *0x34100004 = 0x34100025 set *0x34100024 = 0xFFFEF7FF set *0x34200000 = 0x34300000 set *0x34200004 = 0x34200025 set *0x34200024 = 0xFFFEF7FF b main c DanielBarbu_10-1729681111292.png   These lines prepare the environment for launching debugging on secondary cores. This will allow for multicore debugging in the case of separate ELF files for each core. These can be found in the Run Commands field of the Startup tab on the Debug Configuration for the primary core within S32 Design Studio IDE, of any multicore project created from the New Application Project Wizard. Note: If there is just one ELF file for all cores, then these 'set *0x... = 0x...' commands should be skipped. In general, it will be correct to set the break-point at main, as shown, but this might need to be changed depending on when the secondary cores are started within the project. Prepare the initialization script for the secondary core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True #_SOC_NAME = "S32G274A" Make the following changes to the lines: _JTAG_SPEED = 14000 ->  None _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> None _CORE_NAME = 'M7' -> 'M7_1' (this should be set to match the name of the core to be debugged, see s32g2xx_context.py for complete list) _RESET_DELAY = 1 _CMD_TIMEOUT = 7200 _REMOTE_TIMEOUT = 60 _IS_LOGGING_ENABLED = True _SOC_NAME = "S32G274A" Save the file with a new name to preserve the original. For example, s32g2xx_attach_my_probe_core1.py. This ensures the S32 Debugger will still function correctly. DanielBarbu_9-1729680896856.png The existing GTA server is used, so do not launch a new one. Open an new command window and follow similar steps as done for the primary core. Setup the Python environment variable, if not done globally set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: DanielBarbu_8-1729680717892.png   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_attach_my_probe_core1.py This specifies the script for initialization. We will not execute the py board_init() as this was already done for the primary core. py core_init() This initializes the core specified in the initialization script in step 2. DanielBarbu_7-1729680182207.png   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32G_MultiCore\\S32G_MultiCore_M7_1\\Debug_RAM\\S32G_MultiCore_M7_1.elf load DanielBarbu_6-1729679991000.png   Repeat 3-6 for each additional core. Primary Core Image Already in Memory and Running The core is running and does not need to be initialized. Prepare the initialization script for the core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\s32g2xx_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: #_JTAG_SPEED = 14000 #_GDB_SERVER_PORT = "127.0.0.1:45000" #_RESET_TYPE = "default" #_PROBE_IP = "s32dbg:10.222.24.64" #_CORE_NAME = 'M7' #_RESET_DELAY = 1 #_CMD_TIMEOUT = 7200 #_REMOTE_TIMEOUT = 60 #_IS_LOGGING_ENABLED = True #_SOC_NAME = "S32G274A" Make the following changes to the lines: _JTAG_SPEED = 14000 _GDB_SERVER_PORT = "127.0.0.1:45000" -> 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg:10.222.24.64" -> (enter the IP address of your probe) _CORE_NAME = 'M7' -> 'M7_0' (this should be set to match the name of the core to be debugged, see s32g2xx_context.py for complete list) _RESET_DELAY = 1 _CMD_TIMEOUT = 7200 _REMOTE_TIMEOUT = 60 _IS_LOGGING_ENABLED = True _SOC_NAME = "S32G274A" Save the file with a new name to preserve the original. For example, s32g2xx_attach_my_probe_core0.py. This ensures the S32 Debugger will still function correctly. DanielBarbu_0-1729682595628.png   Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this: DanielBarbu_1-1729682669901.png   Ensure Environment Variable for Python is set. From command prompt, run the command: set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages DanielBarbu_2-1729682760898.png   Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: DanielBarbu_3-1729682914844.png   From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32g2xx\\s32g2xx_attach_my_probe_core0.py This specifies the script for debugger initialization. Do not execute the py board_init() as this will initialize the board, and reset the currently executing application, which is not desired for this case. py core_init() This initializes the debugger connection to the core specified in the initialization script in step 1. DanielBarbu_4-1729683233854.png   Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32G_Multicore\\S32G_Multicore_M7_0\ \Debug_RAM\\S32G_Multicore_M7_0.elf load DanielBarbu_5-1729683397223.png   After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. See section ‘Secondary Cores’ for each additional core to be debugged.
View full article
Condition: Enable Stopindebug bit for PIT and STM module. Counter could be stop when debug project, but when i set debug mode on, counter not count, project can't be run. Analysis: In order for PIT timer to count when a FRZ bit is enabled, all cores on S32V23x devices need to be running. The reason why it does not work out of the box with current plugin configuration, is because we halt all device cores, which is especially necessary for RAM based projects. Solution: We created a start-up macro to keep all cores running when S32V232M80 or S32V234M100 debug sessions are launched. In order to use it, please go to the following directory without your S32DS3.2 IDE: eclipse\plugins\com.pemicro.debug.gdbjtag.pne_4.2.8.201909091700\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx. Please rename S32V234M100_All_Cores_Running.mac or S32V232M80_All_Cores_Running.mac to default macro names, saving existing default macros in renamed form, or a separate location: S32V234M100.mac or S32V232M80.mac.separate location: S32V234M100.mac or S32V232M80.mac.
View full article
So you've just installed the S32DS for Vision and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started.   1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click Finish 7. Change to C/C++ perspective, click on 'Switch to C/C++ Development' 8. Build the project for Debug 9. Project is now built, ELF file is read to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP. 10. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 11. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 12. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 13. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 14. The executable file is copied to Linux file system and gdbserver starts. 15. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
View full article
This document shows the step-by-step process to create a simple 'Blinking_LED' project. There is also a video which demonstrates the same steps. This project uses the S32K144EVB-Q100 EVB, connected to a PC through USB (OpenSDA) connection. 1. New S32DS Project OR 2. Provide a name for the project, for example 'S32K144_Blinking_LED'. The name must be entered with no space characters. 3. Expand Family S32K1xx, Select S32K144 4. Click Next 5. Click '…' button next to SDKs 6. Check box next to S32K144_SDK. 7. Click OK 8. Click Finish, wait for project generation wizard to complete 9. Notice Processor Expert views have opened. 10. Make sure the project is selected in Project Explorer view, then from the Components - S32K144_Blinking_LED view, select: Components -> pinmux:PinSettings 11. From the Routing tab, select the GPIO pin routing group and scroll the list until PTD Pin 15 and Pin 16 are visible 12. Click on the fields in the Pin/Signal Selection and Direction columns to set the following:       a. Row: Pin 15, Pin/Signal Selection: PTD15, Direction: Output       b. Row: Pin 16, Pin/Signal Selection: PTD16, Direction: Output 13. Click Save 14. Project -> Generate Processor Expert Code OR, click the button from the Components view 15. The main.c file from 'Sources' folder should be already open, if not, then in the project window click to expand the project folder then Sources, and finally double click the main.c file to open it. 16. Expand the clock_manager component in the Components Window, then locate CLOCK_DRV_Init 17. Drag and drop the CLOCK_DRV_Init function into main, after the comment 'Write your code here' 18. Now we need to supply an argument so the CLOCK_DRV_Init() function knows what clock settings to use. With clockMan1:clock_manager selected in the Components view, look at the Components Inspector and locate the name of the only clock configuration listed, 'clockMan1_InitConfig0'. 19. Enter the name of the clock configuration, with address operator, to the input arguments of CLOCK_DRV_Init(). Notice the name is shaded grey and a mouse-hover reveals the definition. 21. Expand the pin_mux:PinSettings component  in the Components Window 22. Drag and drop the PINS_DRV_Init function into main, below the clock configuration  24. Drag and drop the PINS_DRV_SetPinsDirection function into main immediately after PINS_DRV_Init 25. Drag and drop the PINS_DRV_SetPins function into main 26. Drag and drop the PINS_DRV_ClearPins function into main 27. For each of the PINS_DRV functions, there are 2 arguments, first is always PTD (which is macro defined in SDK), the second is defined as follows: PINS_DRV_SetPinsDirection: OR-ing of LEDRGB_RED and LEDRGB_GREEN = 1 << 15U | 1 << 16U PINS_DRV_SetPins: Bit shift of LEDRGB_RED = 1 << 15U PINS_DRV_ClearPins: Bit shift of LEDRGB_GREEN = 1 << 16U 28. Include an infinite loop after these functions 29. Drag and drop the PINS_DRV_TogglePins function in to main, and place it inside the 'for' loop. 30. Again, the first argument will be PTD and the second is the same as for PINS_DRV_SetPinsDirection above. 31. Within the 'for' loop, and prior to the PINS_DRV_TogglePins function, add a delay of 720000 cycles int cycles = 720000; while(cycles--); 32. Build 'Blinking_LED_S32DS'. Select the project name in 'C/C++ Projects' view and then press 'Debug_RAM'. Or you can build for Debug_FLASH, but programming RAM won't overwrite anything you already have in FLASH. 33. After the build completes, check that there are no errors. 34. Open Debug Configurations and select 'Blinking_LED_S32DS_Debug_RAM' OR 35. Check the Debugger settings and ensure that 'OpenSDA Embedded Debug - USB Port' is selected for interface. Or select the settings which are appropriate for your hardware configuration. 36. Click Debug 37. Set breakpoint on PINS_DRV_TogglePins. Double-click on the blue shaded area at left on the line of code to set breakpoint. 38. Step through initialization calls 39. To see the output register bits change, go to 'EmbSys Registers' tab and expand 'GPIO', then 'PTD' and 'PDOR'. Double-click on PDOR to enable reading of the values. 40. Click resume to advance to the breakpoint, see the LED on board change color. 41. Click resume again and see LED change to other color
View full article
Build your project and choose Debug Configuration option  On the left side select Launch Group of your choice (Flash/RAM) and press Debug button Wait while debug session is fully started. If you left default startup configuration - all cores has active break-point at the beginning of main() function. You can chose any core for debugging just by clicking on the core's thread. Sometimes are init functions - including startup of other cores - inside main() of boot core (for S32R274 is boot core Z4). In this case you should let boot core perform init sequence first and then try debug other cores. On next picture are all cores halted.  On this picture are core 1 (Z4) and 2 (Z7_0) running - and third one is stopped. You can perform any debug operation on this core (memory/registers view, instruction step...) without effect on other cores.  On the last picture are running cores 1 (Z4) and 3 (Z7_1) and second core (Z7_0) is stopped and any debug operation can be performed on this core. 
View full article
Requirements: SD card with installed Linux image connected to EVB (https://community.nxp.com/docs/DOC-335023 ) Serial link connection between PC and EVB (HOWTO: Setup A Remote Linux Connection in S32DS for Vision )  EVB connected to network   Procedure: Turn on EVB and connect to EVB via serial link using putty or any other terminal (115200 baud, 8N1). Login as the root user. Edit network interfaces configuration file by command vi /etc/network/interfaces and modify (press INS key to switch vi editor to edit mode) the file by the way as shown on next screenshot. Set IP address from range of your PC machine network settings.      The vi /etc/network/interfaces string is cutoff, because the OS acts during typing. The OS-printed line. [    29.817839] random: nonblocking pool is initialized (it varies with each boot). is written automatically by the OS a few seconds after login.  These characters do not make a difference.  Just enter the string as instructed and press Enter.  You will see the screen as follows.   Save new settings by :w command (press ESC key to switch vi editor to command mode) and exit from vi by :q command.   Restart network by command /etc/init.d/networking restart         Check the IP address by command ifconfig and try ping to your PC machine.        Troubleshooting: If you can't ping to PC machine and IP address is the same as you requested - check IP address on PC side and cable connection. If the IP address on EVB is different than you requested - check if you commented out the dhcp configuration. You may also try to reboot EVB instead of restarting network only.
View full article
This document shows, how to set optimization level for whole project and how to edit single files with different optimization level. As soon as the project is created, it has set optimization level to 0 by default. This means, compiler do neither size optimization nor speed optimization. Optimization level can be set for every project according to the project requirements. 1) Optimization level set Right click the project and select project properties. Click C/C++ Build ->Settings->Standard S32DS C Compiler ->Optimization. You can see, optimization level is none -O0. Click the arrow on the right side of the list and choose the required optimization level. There are five options you can choose. Details description of the options are included in S32DS reference manual. Chosen optimization is used for all files in the project. 2) Change optimization level for single file in the project If you want to change optimization level for single file and do no affect another files, select required file, right click on it and select properties. As you can see, there are limited possibilities to set the file itself. Select required optimization level, click apply and close the window. Now, selected file has different options than the rest of the project. Hope it helps. Martin
View full article
Example introduction: After startup - uninitialized RAM is set to 0 by startup code (startup_S32K144.S). If you need access to data stored in the RAM after reset is performed, you can  add these variables into .noinit section. You need to update your linker file and add .noinit section aligned to 1024 bytes before _RAM_START is defined:  In code assign your variable into .noinit section:  Example usage:  Import attached example into S32DS for ARM, build in and start debug session. Resume target and suspend program execution:  In semihosting debug console you can see that noinit_data are set to 0. The board is in state after power ON: Reset board and let's check if data remains in RAM memory:  After resume, you can see in semihosting console (or expressions view), that data remains unchanged:
View full article