S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
S32DS for Vision contains many example projects from which you can learn how S32DS for Vision can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS for Vision. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed. 1) Launch S32DS for Vision 2) Select 'New S32DS Project from example' 3) Select apex2_fast9 project 4) Click Finish 5) Change to C/C++ perspective, click on 'Switch to C/C++ Development' 6) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'. 7) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9. 😎 Click Resume  Should see something similar to what is pictured below There are green diamonds at the corners in the image as identified by the fast9 corner detection algorithm
記事全体を表示
This document describes a way, how to place custom constant data into specific flash memory area. Create a custom linker section in the linker file (.ld), where custom data should be placed into. Use the KEEP keyword in case you would like to avoid dead stripping if and object is not referenced. add the __attribute__ section statements to the custom data definition. Map file should looks like this way Hope it helps. Martin
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 9          What is new? S32K1xx SDK RTM 3.0.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148  (S32K1xx SDK release notes) AMMCLIB version 1.1.15  (AMMCLIB S32K14x release notes) Segger J-Link drivers v6.42a (J-Link release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
Sometimes you would like to share sources between projects and - even better - between platforms. Let's say that we are developing software with the very same functionality for S32K144 and MPC5744P. In this case, we can identify platform independent functions - generic, platform specific functions - not related to MCU itself, but related to the way some peripheral works (for example different ADC result range) - and MCU dependent functions like clock init. In attachment is a very simple SDK which can be shared with S32K144 and MPC5744P (each in different S32DS editions).  Unzip my_sdk.zip archive (for example C:\NXP folder). You can import example projects, but instead let's start from the beginning. Create a new S32DS Application project and choose MCU: You can use default project configurations and click through to finish: Right click on project name -> Properties and select SDKs -> Add Complete the Name, Version and Description fields in New SDK dialog and click on Change button next to Location field. In Change SDK Location dialog, leave Define new variable setting selected, click Browse and find the my_sdk path: Now we can select files (sources, headers...) from selected SDK, you can select all available files. If you select a folder, then all files in that folder will be selected as well. Don't forget to select header files too: If you choose Copy - the files will be copied into project folder and you can do local changes. Without this option (default) - changes will be shared between all projects depended on this particular SDK. The ability to individually select the files to be included from the SDK as well as to copy into the project folder, provides much flexibility to customize SDK usage in your projects. Click on OK, then Attach/Detach... to attach this SDK into your project:  If you like to use your SDK for newly created projects (as an option in SDK select list) - click on Make global button: Now you can see changes in your project: As well, the SDK can be viewed in SDK Explorer (Window -> Show View -> Other...), where functions and macros are available for drag and drop functionality into your code: Platform specific code is filtered by preprocessor-defined macro. So - let's define if we are working with S32K144 or MPC5744P. Right click on project name -> Properties -> C/C++ Build -> Settings -> <Standard S32DS C Compiler OR name of your compiler> -> Preprocessor: We are done - now we can use SDK functions - S32K144:  and MPC5744P (enabling interrupts is default part of empty project for MPC5744P - that's only difference):
記事全体を表示
The Vision SDK root is contributed to the Design Studio as a dynamic path variable “S32DS_VSDK_DIR”. Several Design Studio services use this variable to access the resources inside the Vision SDK. By default, this variable points to “${eclipse_home}../S32DS/s32v234_sdk”, i.e. to the Vision SDK shipment bundled with Design Studio. Technically you can change this variable to point to another instance of Vision SDK using the following steps: 1. Go to the main menu "Window -> Preferences" 2. Filter the preference dialog with "sub" keyword or just navigate to "Run/Debug -> String Substitution node. 3. Edit Variable "S32DS_VSDK_DIR" to assign another value to be substituted as Vision SDK root
記事全体を表示
Eclipse caches some settings within the workspace directory. After installing a new version of S32DS, some settings in old workspaces may not match the requirement of the new version. The result is often errors reported on new as well as previously existing projects located in an existing workspace which you selected when launching S32DS. The best way to resolve this is to create a new workspace and then import your projects. This will ensure the workspace is created using all the correct settings for the version you have installed.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 2          What is new? This update adds bare-board device support for S32K118 and some minor fixes. This is a cumulative update - it includes all the content of previous Update 1 Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
Example show one of the methods how to create and use shared memory with symbols between cores. In source code shared_mem.c are variables which can be seen by each core. This file is built once (during s32r274_shmemZ7_0 project compilation) and is linked to other core's elf file by linker into shared_mem section (see linker file for each core) starting on the very same address for each core. Hardware semaphores are used for access shared memory. Lock/Unlock functions are implemented in the shared_func.c (build once during s32r274_shmemZ7_0 project compilation too) file and the object is linked into .text section. Each core has it's own instance of shared functions. There is counter in the shared memory for each core increased each time when shared memory can be accessed by particular core.
記事全体を表示
Example contains modified startup code to be able run in BookE only mode. For GNU gcc and as you need to add -mno-vle parameter in project properties:  For debugging with PE Micro you need to use modified Initialization script in Advanced options: Please note that there is no STD C BookE only library available:
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 8          What is new? Integrated Radar SDK RTM 1.4.0 (replacing RSDK 1.3.0) (see the RSDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2.2  Update 1          What is new? SDK S32K1xx RTM SR 3.0.3 (Patch for SDK S32K1xx RTM 3.0.0) AMMCLIB version 1.1.19 for KEAx, for S32K11x, for S32K14x AMMCLIB version 1.1.20 for KEAx, for S32K11x, for S32K14x Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  online installation: go to menu "Help" -> "S32DS Extensions and Updates" dialog check boxes next to "S32K1xx development package", "S32K1xx SDK 3.0.3 pakage" and "S32 Design Studio for ARM Devices development package" click "Install/Update 3 item(s)" offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file go to menu "Help" -> "S32DS Extensions and Updates" dialog select "Go to Preferences" Add a new Software Site Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step check boxes next to "S32K1xx development package" and "S32 Design Studio for ARM Devices development package" click "Install/Update 2 item(s)" This will start the update installation process.
記事全体を表示
There are often errors displayed after the indexer completes building its data base following the creation of a new project or the opening of a project not already in the workspace and again just before building. Some of these errors can be due to settings in the Eclipse Indexer settings. In one scenario, a project which builds clean, that is, no compiler or IDE errors, will mark code lines in a source file which includes a large header file as 'cannot resolve symbol xxxx'. In this case, the header file is larger than 17 MB. In the Eclipse Indexer settings, there are settings 'Skip files larger than' and 'Skip included files larger than'. These settings, by default, are set to 8 MB. This would be too low for the header file in this example. In order to resolve the issue, the setting should be increased to allow for the large header file to be indexed.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 10          What is new? S32K1xx SDK RTM-SR 3.0.1 introducing support for three new pin variants: S32K142 - 48LQFP, S32K144 - 48LQFP, S32K148 - 100LQFP and for two new TJA devices: TJA1101HN (NXP) Production and TJA1102HN (NXP) Production  (S32K1xx SDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8, Update 9 ) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB2 using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB2 to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the A53 build option. 3) The project is now built, and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the '{project_name}_Remote_Linux' debug configuration is selected and the Connection (see step 3) is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts.   You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial break point is reached in main(), it is almost ready for to start debug on ISP. Click Resume as the A53 must be running before we can attach the ISP debug thread. 😎 Return to the Debug Configurations menu and locate the ISP debug configuration. You will see a debug configuration within the 'S32 Debugger' group (in our example, isp_sonyimx224_csi_dcu_mipi_simple_IPUS0 as shown below). This is the debug configuration we will use, however, it will require some setup.     9) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   10) This is already done for our example, but for your application, it may be necessary to setup the symbols for the ISP engine. Go to the Startup tab and:    a) Check the box for 'Load symbols'    b) Select the option for 'Use file', click Workspace... and locate the object file (.opius) for the ISP engine you wish to debug.   11) Click Apply then Debug. It may take a few moments for the ISP core debug to launch.   12) Wait for the ISP debug launch to complete. You may notice the A53 thread has terminated. This is normal and expected since the camera input cannot be suspended. When the launch completes, the context of the Debug window will switch to the ISP debug thread. 13) Enable Instruction Stepping mode and then step one time to load the object file which was setup in step 6. 14) The ISP debugging is now running and you can step through the ISP engine, look at registers, set a break point, etc. Note: only one hardware break point is supported for ISP.
記事全体を表示
The document describes the steps that need to be done in order to place and execute a library function from a custom memory section - typically RAM using GNU Build tools. The instructions are applicable to any GNU tool-chain. It is demonstrated on a New S32DS Project created in S32 Design Studio for ARM. Lets assume that we'd like to execute memcpy() function from the standard library (NewLib). 1) The first step is to exclude specific library object file(s) from the input section (using EXCLUDE_FILE) so they will not be linked into the standard .text* flash section.  The input section associated with EXCLUDE_FILE shall not interfere with the same input section used later in section list (e.g. with *(.text*) input section deleted from the list below). EXCLUDE_FILE in behaves the same was as *.(text*) rule - it only exclude selected file(s) but places all the remaining (non-excluded) input data. /* The program code and other data goes into internal flash */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ /* Exclude file(s) from NewLib libc.a from .text.* section */ *(EXCLUDE_FILE (*libc.a:lib_a-memcpy-stub.o) .text*) *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 2) Now let's place the memcpy object into a code_ram section which is already defined in the project .ld file. This section is dedicated to a code that shall be executed from RAM (startup routine initializes this section). For more details see HOWTO: Run a routine from RAM in S32 Design Studio  . The following line places the code (.text* section) from the object file (lib_a-memcpy-stub.o) from the standard NewLib (libc.a)  *libc.a:lib_a-memcpy-stub.o (.text*)‍ into .code section: .code : AT(__CODE_ROM) { . = ALIGN(4); __CODE_RAM = .; __code_start__ = .; /* Create a global symbol at code start. */ __code_ram_start__ = .; *(.code_ram) /* Custom section for storing code in RAM */ *libc.a:lib_a-memcpy-stub.o (.text*) /* add memcpy from the NewLib library here*/ . = ALIGN(4); __code_end__ = .; /* Define a global symbol at code end. */ __code_ram_end__ = .; } > m_data‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ After building the project you can check the map file to confirm memcpy is indeed placed into .code section in RAM memory: .code 0x1fff881c 0x18 load address 0x00000d90 0x1fff881c . = ALIGN (0x4) 0x1fff881c __CODE_RAM = . 0x1fff881c __code_start__ = . 0x1fff881c __code_ram_start__ = . *(.code_ram) *libc.a:lib_a-memcpy-stub.o(.text*) .text.memcpy 0x1fff881c 0x16 C:/NXP/S32DS_ARM_v2018.R1/Cross_Tools/gcc-6.3-arm32-eabi/arm-none-eabi/newlib/lib/thumb/v7e-m\libc.a(lib_a-memcpy-stub.o) 0x1fff881c memcpy 0x1fff8834 . = ALIGN (0x4) *fill* 0x1fff8832 0x2 0x1fff8834 __code_end__ = . 0x1fff8834 __code_ram_end__ = . 0x00000da8 __CODE_END = (__CODE_ROM + (__code_end__ - __code_start__)) 0x00000da8 __CUSTOM_ROM = __CODE_END‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note If you are placing a function into RAM always consider to add sub-functions called by that function (typically located in a different object file).
記事全体を表示
The attached file is an example project based on KEA128 for LED flashing by toggle GPIO signals. It was developed   on S32 Design Studio for ARM 1.0.
記事全体を表示
On reset, all module registers have default values. These settings are typically not ideal for achieving optimal system performance. Also, some peripherals must be configured before they can be used. DCD is the configuration information contained in the DCD image that BootROM uses to configure peripherals on the device. BootROM determines the location of the DCD table from the associated pointer in the IVT.   The main functionality of the DCD Tool is to generate the Device Configuration Data (DCD) image using the format and constraints as specified in the Boot ROM reference manual.   In the steps below, an example process for creating the DCD binary for initializing SRAM is shown. To initialize the SRAM, a logic '1' must be written to the INITREQ bit within the PRAMCR register of the SRAMC and SRAMC_1 peripherals.   Procedure With a project open in project explorer (C/C++ perspective), switch to DCD perspective. Click on the arrow next to the 'Open S32 Configuration' button and select 'Open DCD'. Check that correct project is selected  In DCD Commands panel, select Command Type 'Write', then click 'Set' Click 'Add Register', then set the following settings. Can start typing the names to filter the list for faster setting selection.   For Peripheral setting, select 'SRAMC'. You can search for it by typing the name. Register setting, select 'PRAMCR'. The list is short, so it is not necessary to type the name. In Bitfields, select 'INITREQ' Now click on the highlighted bit to set it. Again using 'New Command' box, repeat settings of steps 3 & 4, however, this time select Peripheral 'SRAMC_1'. If everything was done correctly, in the DCD Binary panel to the right, should appear as shown. If so, click 'Export'. The generated DCD file will be displayed. By default, C format is selected. Select Binary format and click OK. Select a location to save the file (such as the project folder in the workspace directory) and give it a meaningful name. Click Save. You are done! DCD image file is created in binary format and ready to be imported to IVT Tool.  
記事全体を表示
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using either the A53 or the TEST_A53 build options. 3) The project is now built and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts. You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial breakpoint is reached in main(), we need to set a breakpoint at the function apu_hal_Enable().    This breakpoint has already been created for you, you just need to enable it! Locate the breakpoint in the Breakpoints view. Due to some known issues with Eclipse CDT, it is necessary to enable->disable->enable the breakpoint so it will work properly. The issue only affects this breakpoint, due to the way it is provided, and will not affect breakpoints which you set elsewhere in the code. 😎 Press Resume twice, so that the breakpoint which was set at apu_hal_enable() is reached for the 2nd time. 9) Open Debug Configurations. You will see a debug configuration within the 'S32 Debugger' group (FAST9COLOR as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.       11) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   12) It may take a moment or two before the APEX2 debug thread launch is complete, see the Thread listed within the <kernel_name>[S32 Debugger] in the Debug window. Also note, a new breakpoint is listed in the Breakpoints view. This breakpoint is set for you at the start of the APEX2 graph function. 13) The debugger context is still on the A53 thread. Press RESUME and then select the APEX2 thread to see that it has stopped on the graph function break point. Now you can step through the graph. 14) To step through a kernel, locate the call to the kernel function in the graph function and set a break point on the line. 15) Press RESUME to advance the program counter to the new break point 16) Press STEP INTO to advance the program counter into the kernel. It may take several steps as the optimizations performed by the compiler produce some synchronization inconsistencies. 17) You may need to help the IDE to locate the source files. Now you can see the kernel wrapper function... and the kernel! 18) Step through, monitor variables and registers and set breakpoints.
記事全体を表示
So you've just installed the S32DS and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started. Prerequisite Before following the steps in this HOWTO, ensure you have the S32V2xx development package installed to S32DS. 1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click the '...' next to the SDKs field 7. Check the box next to 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS and click OK. 8. Click Finish 9. Build the project for Debug 10. Project is now built, ELF file is ready to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP. 11. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234)  12. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 13. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 14. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 15. The executable file is copied to Linux file system and gdbserver starts. 16. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2, Update 2             What is new? AMMCLIB v1.1.9 support for MPC56xx (MPC560xB, MPC560xP, MPC5643L, MPC567xF, MPC567xK) and for MPC57xxx (MPC574xC, MPC5748G, MPC574xP, MPC574xR, MPC577xC, MPC577xK, MPC577xM) updated PEmicro Eclipse Plugin Update v1.6.9 which fixes HSM mass erase problem for MPC5748G (see e.g.MPC5748G can not attach JTAG )   Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite  select all available items and click "Next" button   offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 2" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 2 archive file: Select all available items and click "Next" button.
記事全体を表示