S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
Condition:  I am trying FreeRTOS using S32K118 EVB and run in DEBUG mode. When I set the break point in vTaskDelay and press Resume for the first time, there is a smooth stop at the break point. The second time I press Resume, the debugger should enter the same break point again, but there is no response. Then I press Suspend and can't press Resume again, at this point I can only leave. However, I am free to run this project with no problem, what's wrong? Analysis: This is due to an access of DDR memory region which is not initialized by default project settings. Solution: To resolve it, a macro initializing the DDR memory should be selected to run at the beginning of a debug session. A user should go to Advanced Options dialog and check "Enable initialization script". Our DDR init macros can be found at the following location within S32DS3.2 layout: eclipse\plugins\com.pemicro.debug.gdbjtag.pne_4.2.8.201909091700\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR3_EVB29288.mac. Please note that the type of the macro might depend on the revision of the board and S32V23x device one is working with. I am also attaching a picture of debug configuration and Advanced Options dialog with all the settings in place.
記事全体を表示
The following article describes how to add FreeRTOS thread aware debugging to the Eclipse Debug view using SEGGER J-Link: Show FreeRTOS Threads in Eclipse Debug View with SEGGER J-Link and NXP S32 Design Studio | MCU on Eclipse  I hope this is useful, Erich
記事全体を表示
This application demonstrate integration Processor Expert (PE) RAppID Suite for  MPC5777M initialization tool with S32 Design Studio for Power v1.1. There is a separate RAppID project and RAppID Workspace folder included in this project:       This multicore project first initializes the device (PinMux, Clocks, PIT timer). Each core toggles with one LED with different time period. Z4_0 core: LED1...GPDO[0] Z7_0 core: LED2...GPDO[1] Z7_1 core: LED3...GPDO[2]     Yo can adjust the device initialization in PE RappID (open included workspace), generate the code and finally rebuild the project in S32DS.   Note:  Do not let generate PE_Types.h file since it includes some non-vle instructions mixed with VLE ones - this cannot be built by S32DS compiler. linker command file generation needs to be disabled otherwise it generates HighTec specific keywords that S32DS GCC linker does not understand.    Test HW:       MPC5777M-512DS, MPC57xx Motherboard MCU:             PPC5777MQMVA8 0N78H Debugger:    PeMicro USB-ML-PPCNEXUS Target:           Debug (internal flash) EVB connection:  USER LED1 connected to P8.0, LED2 connected to P8.1 LED3 connected to P8.2
記事全体を表示
Hello,   The new official release of S32DS for Power Architecture v1.1 is available now! You can download it from S32DS product web page: S32 Design Studio IDE|NXP       This release requires the product activation! Please enter the Activation code from the notification email (it is sent after you click on S32DS download button) into the installer dialog (see the screenshots below). The Activation code is valid for both versions (Windows/Linux).     S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB) and other open-source software to offer designers a straightforward development tool with no code-size limitations. This release supports Windows 7/8/8.1/10 (32/64 bit) and Linux versions as well.   S32DS Power v1.1 main features Free of charge tool with no code size limitation (no license file required - Only acti) Eclipse Luna 4.4 Framework GNU Build Tools for e200 processors supports VLE and BookE ISA, LSP, SPE/SPE2 based on gcc 4.9.2, binutils 2.24 and gdb 7.8.2 Libraries included: newlib, newlib-nano and Freescale EWL2 (ewl and ewl-nano) P&E Multilink (with P&E GDB Server) Graphical tool for creating SPT algorithms SDK management included (FreeMASTER for 560xP, AMMCLIBs) GreenHills and Diab compilers support by new project wizard Lauterbach, iSystem** and PLS debuggers support by new project wizard Kernel Aware Debugging FreeRTOS, eCOS, OSEK. "New S32DS project from” added to support project creating from examples Devices supported MPC56xx MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A MPC5643L MPC5676R MPC57xx MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B MPC5744P, MPC5743P, MPC5742P, MPC5741P S32 S32R274   Host Operating System Support Microsoft Windows 7/8/8.1/10 32-bit and 64-bit (Home and Pro Editions) Linux versions Ubuntu 12.04/14.04, Debian 8, CentOS 7   Technical Support S32 Design Studio is supported on NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes (product & GCC build tools)   * Red items are the new features ** iSystem plugin integration with the project wizard will be available in S32DS PA v1.2   Regards, Stan
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 11          What is new? S32 SDK for Power Architecture RTM 3.0.0 supporting  S32R274, S32R372, MPC574x-B-C-G, MPC574x-P, MPC574x-R and MPC577x-B-E-C (see the S32 SDK release notes) Integrated Radar SDK RTM 1.2.1 (see the Radar SDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8, Update 9, Update 10  ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Updates 5 and 6          What is new? S32 SDK for Power Architecture 1.0.0 RTM supporting MPC574xx.  Service Pack supporting MPC5775 B/E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
Please note: AMMCLib SDK is standalone from S32/MPC SDK, it is intended for users who will not use the S32/MPC SDK. The AMMCLib SDK does not support all toolchains listed in S32DS new project wizard. For the toolchains it does support, It does not support all versions. The available SDKs will vary depending upon the toolchain which is selected. When creating a new S32DS Application Project, you may have noticed the S32K14x_AMMCLib_xxx SDK option in the Select SDK menu. This is the standalone version of the AMMCLib. If you plan to use one of the S32/MPC SDKs, then it most likely contains an integrated version of the AMMCLib. For this integrated case, the AMMCLib is accessed like any other S32/MPC SDK component and you would not need to add the standalone version. To add the AMMCLib SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the SDK from the list and then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', causing it to disappear. It should also be noted that there exist example projects which demonstrate usage of the AMMCLib, though these show usage of the S32/MPC SDK integrated version. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer view to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy math coding with AMMCLib!
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v1.2, Update 3            September 21, 2017   What is new? S32 SDK EAR 0.8.1 supporting MPC5748G & MPC5748C. The new project wizard now offers the new version of S32 SDK: "New S32 Project from Example" offers additional demos and examples. The complete S32 SDK EAR 0.8.1 release notes attached below. Installation instructions This is a cumulative installer - all previous updates (except previous version of S32 SDK EAR 0.8.0) are included so you do not need to install any previous update. The update is available for online (Eclipse Updater) or offline (direct download link) installation. online installation go to menu "Help" -> "Install New Software..." dialog  select predefined NXP S32 Design Studio update repository select all available items http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite click "Next" button offline installation  go to S32 Design Studio product page -> Downloads section or use the direct download linkand download the "S32 Design Studio for Power v1.2 - Update 3" file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 3 archive file Select all available items and click "Next" button.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 8          What is new? S32K1xx SDK BETA 2.9.2 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7 ) Installation instructions The update is available for  (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 8          What is new? S32 SDK for Power Architecture 1.8.0 EAR supporting MPC5777C, MPC5775B, MPC5775E, MPC5746R, MPC5745R, MPC5743R This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7 ). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 7          What is new? MPC574xx SDK BETA 1.9.0 S32R SDK BETA 1.9.0  Radar SDK for S32R274 & S32R372 RTM 1.1.1 AMMCLib 1.1.13 for MPC560xB, MPC560xP, MPC564xL, MPC567xF, MPC567xK, MPC574xC, MPC574xG, MPC574xP, MPC574xR, MPC577xC, MPC577xK,  MPC577xM This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2, Update 1 1            What is new? The S32 Software Development Kit (S32 SDK v0.8.0 EAR) which is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP Power MPC5748G and MPC5746C microcontrollers. Release notes are available here: http://www.nxp.com/docs/en/release-note/C55_SDK_EAR_0.8.0-RN.pdf  Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite  select all available items and click "Next" button offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 1" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 1 archive file: Select all available items and click "Next" button.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 3          What is new? S32 SDK 1.8.8 EAR (Early Access Release) for S32K118. This is a cumulative update - it includes all the content of previous updates ( Update 1, Update 2) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 10          What is new? Service Pack for S32R264 This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8 ) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
Installation & Activation HOWTO: Activate S32 Design Studio  HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio  Create a New Project  HOWTO: Create APEX2 Project From Example in S32DS for Vision  HOWTO: Create An ISP Project From Example in S32DS for Vision  HOWTO: Create A53 Linux Project in S32DS for Vision  HOWTO: Create An ISP Project From Existing VSDK Graph in S32DS for Vision  HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project   HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio  HOWTO: Create A53 APEX2 and/or ISP Linux Project in S32DS for Vision DDR Configuration & Validation and Stress Test Tools HOWTO: Use DDR Configuration and Validation Tool  HOWTO: Use DDR Stress Test Tool  Hardware Setup HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP HOWTO: Prepare and boot S32V234 EVB from eMMC  HOWTO: Setup static IP address for S32 debug probe  Debugging HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP  HOWTO: S32V234-EVB debugging with Linux and gdbserver on target machine  HOWTO: Start Debug on an ISP Application Project with S32 Debugger and S32 Debug Probe  HOWTO: Start Debug on an APEX2 Application Project with S32 Debugger and S32 Debug Probe  Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse   VSDK HOWTO: Change Vision SDK root in S32DS for Vision  HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project  HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK  Linux HOWTO: S32V234 EVB Linux - Static IP address configuration  HOWTO: S32V234 EVB Linux - DHCP IP address setup  HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK  HOWTO: Access Linux BSP file system on S32V234-EVB from S32DS for Vision HOWTO: Setup A Remote Linux Connection in S32DS for Vision  General Usage HOWTO: S32 Design Studio Command Line Interface  HOWTO: Add user example into S32DS  HOWTO: Generate S-Record/Intel HEX/Binary file  HOWTO: Update S32 Design Studio  Troubleshooting Help! I just relaunched S32DS for Vision and my visual graph is collapsed!  Help! I just updated to new version of S32DS and now my projects have errors and I can't build!  Troubleshooting: PEmicro Debug Connection: Target Communication Speed  Troubleshooting: Indexer errors on header file  S32 Design Studio Offline activation issue hot fix  https://community.nxp.com/docs/DOC-345238 
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 7          What is new? Integrated S32 SDK for Power Architecture RTM 3.0.2 (see the S32 SDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2 ) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
Hello, the new release of S32DS for ARM v1.3 is available now in the download section of S32DS web page: http://www.nxp.com/s32ds   The Activation code is required to install the product. The activation code is different to previous versions (v1.1/1.2). You should get the appropriate Activation Code by a notification email which is send automatically when you proceed to the downloading: What is new?  New device supported: S32K144 v2.0 ARM64: Linaro GCC 4.9-2015.05 Fully integrated S32 SDK for S32K144 EAR release v0.8.2. including PinMuxing and Processor Expert configuration. FreeMASTER Serial Communication driver for S32K144 family  Highly Assembly Optimized version of Automotive Math and Motor Control Libraries for KEA and S32K devices v1.1.6  IAR debugger support by new project wizard Updated SEGGER and P&E debug plugins to the latest and greatest versions Reset functionality added with P&E debugger for single core projects (KEA, S32K devices) and A5 core for MAC57D54H Flash configuration supported for S32V234 Header files for KEA and MAC57D54H updated Advanced FreeRTOS kernel aware debug support Bug fixes Project Explorer updated to correctly show active build configuration resources     Note: The plugins to support GreenHills, IAR, iSystem, Lauterbach are not included and have to be installed from corresponding update site or installation.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 2          What is new? This update adds bare-board device support for S32K118 and some minor fixes. This is a cumulative update - it includes all the content of previous Update 1 Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 8          What is new? Integrated Radar SDK RTM 1.4.0 (replacing RSDK 1.3.0) (see the RSDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
The attached file is an example project based on KEA128 for LED flashing by toggle GPIO signals. It was developed   on S32 Design Studio for ARM 1.0.
記事全体を表示