S12 / MagniVマイクロコントローラ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 / MagniV Microcontrollers Knowledge Base

ラベル

ディスカッション

ソート順:
The package contains of AN5327_SW ported to S12ZVML-MINIBRD hardware. Just minor changes are introduced, such as removing a button control, moving the LED light to another pin and using internal oscillator. This is just a working version, it is NOT an official release!!! AN5327_SW_CW11_MINIBRD.ZIP CodeWarrior 11.0 and AMMCLib 1.1.13 or higher is required to run this example. If you are not sure about the AMMCLib version, please download the general AN5327_SW from the www.nxp.com/automcdevkits first, install it and then unzip and use the example above.
記事全体を表示
This example shows a few possible configurations of the S12PWM8B8CV2 PWM module. Five PWM channels are configured with different clock source, polarity, alignment, period and duty-cycle.   Four clock sources (A, B, SA, SB) are derived from bus clock using dividers.   Selected polarity of PWM channel determines the duty-cycle whereas the alignment determines the period of the PWM signal.   Four 8-bit channels (4-5, 6-7) are concatenated into two 16-bit channels. Channels 4 and 6 become high-order channels while channels 5 and 7 become low-order channels. These low-order channels (5 and 7) are the output channels routed to a port  and they configure the clock, polarity, alignment and enablement of the PWM signal.  Period and duty-cycle of the signal are configured with both the low-order and high-order channels.   The period registers (PWMPERx) and the duty-cycle registers (PWMDTYx) are double buffered. When they are rewritten while the channel is enabled, the change will not take effect until one of the following occurs: 1. The effective period ends 2. Counter resets 3. The channel is disabled
記事全体を表示
AN12086 Simple Serial Bootloader for S12Z AN12086 SW     AN5330 Migration Guide for S12ZVM Devices AN5330       AN5327 Three-phase Sensorless Single-Shunt Current-Sensing PMSM Motor Control Application with MagniV MC9S12ZVM AN5327       AN5264 Emulating I2C Master Mode AN5264 SW     AN5207 Hardware Design Guidelines for S12ZVM Microcontrollers AN5207       AN5190 S12ZVM Derivatives Configuring PMF Module AN5190 SW     AN5168 Using the ADC Module in S12ZVM AN5168 SW     AN5135 3-phase Sensorless PMSM Motor Control Kit with MagniV MC9S12ZVM AN5135       AN5122 Using Freescale’s LIN Driver with the MagniV Family AN5122 SW     AN5084 Hardware Design Guidelines for S12ZVL Microcontrollers AN5084       AN5082 MagniV in 24V Applications AN5082       AN4975 Using MSCAN on the MagniV Family AN4975 SW     AN4912 Tuning 3-Phase PMSM Sensorless Control Application Using MCAT Tool AN4912       AN4867 Hardware Design Guide lines for S12ZVC AN4867       AN4852 Using the SENT Transmitter Module in S12ZVC Devices AN4852 SW     AN4842 S12ZVL LIN Enabled RGB LED Lighting Application AN4842 SW     AN4841 S12ZVL LIN Enabled Ultrasonic Distance Measurement AN4841 SW     AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers AN4731       AN4723 S12Z MagniV Bootloader AN4723 SW     AN4722 Real Time Counter (RTC) on the S12ZVH Family AN4722       AN4721 S12ZVH: Hardware Design Guidelines AN4721       AN4718 3-Phase BLDC Hall Sensor Application Using S12ZVM AN4718 SW     AN4704 3-phase Sensorless BLDC Motor Control Kit with the S12 MagniV MC9S12ZVM AN4704       AN4680 PMSM Electrical Parameters Measurement AN4680       AN4643 S12VR - Hardware Design Guidelines AN4643       AN4642 Motor Control Application Tuning (MCAT) Tool for 3-Phase PMSM AN4642       AN4618 Sensorless BLDC Motor Control Using S12G240 Based on HVAC Platform AN4618       AN4617 HMI Design Using HVAC Platform AN4617       AN4616 Flap Motor Control Based On HVAC Platform AN4616       AN4558 3-phase Sensorless BLDC Motor Control Development Kit with MC9S12G128 MCU AN4558 SW     AN4540 Comparison Between the MC9S12VR and MM912_634 AN4540       AN4506 Software Analysis in CodeWarrior for MCU AN4506       AN4505 Safety Considerations S12G-Family AN4505       AN4483 Emulated EEPROM Routines for the S12P Family AN4483 SW     AN4455 MC9S12G128_A240 Demonstration Lab Training AN4455 SW     AN4448 MC9S12VR Family Demonstration Lab Training AN4448 SW     AN4418 MC9S12G64 Demonstration Lab Training AN4418 SW     AN4388 Quad Flat Package (QFP) AN4388       AN4364 Glucose Meter Fundamentals and Design AN4364 SW     AN4320 Introduction to the 16-bit Tower Boards Using the MC9S12GN32 AN4320       AN4303 Light control and diagnostics using a MC9S12GN32 MCU AN4303 SW     AN4302 Introduction to the S12G Family EEPROM AN4302 SW     AN4283 Migrating Software Applications from the S12 (XEXSP) and S08 to S12G Microcontrollers AN4283       AN4268 Three-phase Sensorless BLDC Motor Control Kit with the Qorivva MPC5604P AN4268       AN4263 Modification of the eGUI (D4D) Driver for char Displays (D4CD) AN4263 SW     AN4258 Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Technology AN4258 SW     AN4236 MC9S12XHY-Family Demonstration Lab Training AN4236 SW     AN4143 Migrating from the 16-bit S12XE to 32-bit MPC5604B Family of Microcontrollers AN4143       AN4058 BLDC Motor Control with Hall Effect Sensors Using the 9S08MP AN4058       AN4024 High Speed Stall Detection on the S12HY Family AN4024 SW     AN4021 MC9S12HY-Family Demonstration Lab Training AN4021 SW     AN3961 EEPROM Emulation for the MC9S12XS and MC9S12P Families Using AN2302 as a Reference AN3961 SW     AN3937 MC9S12P-Family Demonstration Lab Training AN3937 SW     AN3936 How to install and run Classic CodeWarrior products on 64-bit Windows 7 PC AN3936       AN3832 Sensorless BLDC Motor Control Using MC9S08AC16 AN3832 SW     AN3784 Understanding the Memory Scheme in the S12(X) Architecture AN3784       AN3743 Emulated EEPROM Quick Start Guide AN3743       AN3624 S12X Temperature Sensor AN3624       AN3622 Comparison of the S12XS CRG Module with S12P CPMU Module AN3622       AN3613 Using the MC9S12XS Family as a Development Platform for MC9S12P Family AN3613       AN3589 Optically-Isolated Multilink BDM Interface for the S08-S12 Microcontrollers AN3589       AN3555 Investigating XGATE Software Errors AN3555       AN3510 S12HZ and S12XHZ Family Compatibility AN3510       AN3497 S12XS Family Compatibility Considerations AN3497       AN3493 TFT display AN3493 SW     AN3490 Overview of the MC9S12XE Emulated EEPROM AN3490       AN3469 S12 and S12XE Family Compatibility AN3469       AN3458 Debugging XGATE Code AN3458       AN3419 System Integrity Techniques for the S12XE AN3419       AN3391 LFAE Bootloader Example and Interface for use with AN2546 (CAN bootloader for S12XE) AN3391       AN3333 Implementing CAN and LIN Signal Level Gateway AN3333 SW     AN3330 Introduction to the Stepper Stall Detector Module AN3330 SW     AN3328 HCS12XD Family Compatibility Considerations AN3328       AN3327 Using the S12XE-Family as a Development Platform for the S12XS-Family AN3327       AN3300 General Soldering Temperature Process Guidelines AN3300       AN3298 Solder Joint Temperature and Package Peak Temperature AN3298       AN3292 XGATE Library SCI Emulation AN3292 SW     AN3291 How to Use IIC Module on M68HC08, HCS08, and HCS12 MCUs AN3291       AN3289 Low-Power Techniques for the S12X Family AN3289       AN3275 S12 All-Access Bootloader for the HCS12 Microcontroller Family AN3275 SW     AN3262 Designing Hardware for the HCS12X D-Family AN3262       AN3257 Meeting IEC 60730 Class B Compliance with the MC9S08AW60 AN3257       AN3253 XGATE Library Load Measurement AN3253 SW     AN3242 S12XD and S12XE Family Compatibility AN3242       AN3226 XGATE Library ATD Average AN3226 SW     AN3225 XGATE Library PWM Driver AN3225 SW     AN3224 Tutorial Introducing the XGATE Module to Consumer and Industrial Application Developers AN3224       AN3219 XGATE Library TN STN LCD Driver AN3219 SW     AN3208 Crystal guide AN3208       AN3153 USB - HID - ZSTAR AN3153 SW     AN3145 XGATE Library Using the Freescale XGATE Software Library AN3145       AN3144 Using XGATE to Implement a Simple Buffered SCI AN3144 SW     AN3034 Using MSCAN on the HCS12 Family AN3034 SW     AN3031 Temperature Sensor for the HCS08 Microcontroller Family AN3031 SW     AN3015 Using the XGATE for Manchester Decoding AN3015 SW     AN2974 Quick Start for Beginners to Drive a Stepper Motor AN2974       AN2881 Mapping Memory Resources on HCS12 Microcontrollers AN2881       AN2880 Using Backdoor Access Capability to Unsecure HCS12 MCUs AN2880 SW     AN2836 Web Server Development with MC9S12NE64 and OpenTCP AN2836 SW SW2 SW3 AN2764 Improving the Transient Immunity Performance of MCU-based Applications AN2764       AN2759 Implementing an Ethernet Interface with the MC9S12NE64 AN2759 SW     AN2734 HCS12X Family Memory Organization AN2734       AN2732 Using XGATE to Implement LIN Communication on HCS12X AN2732       AN2727 Designing Hardware for the HCS12 D-Family AN2727       AN2726 XGATE Library CAN Driver AN2726 SW     AN2724 Using the HCS12X PIT as a 24-bit Elapsed Timer AN2724       AN2720 A Utility for Programming Single FLASH Array HCS12 MCUs, with Minimum RAM Overhead AN2720 SW SW2   AN2708 An Introduction to the External Bus Interface on the HCS12X AN2708       AN2700 Basic Web Server Development with MC9S12NE64 and CMX-MicroNetT TCP-IP Stack AN2700 SW     AN2692 MC9S12NE64 Integrated Ethernet Controller AN2692       AN2685 How to Configure and Use the XGATE on S12X Devices AN2685       AN2678 Using the HCS12 NVM Standard Software Drivers with the Cosmic Compiler AN2678       AN2624 Basic Web Server Development with the CMX-MicroNet TCP-IP Stack AN2624 SW     AN2617 A Software Piority Interrupt Scheme on HCS12 Microcontrollers AN2617 SW     AN2615 HCS12 and S12X Family Compatibility AN2615       AN2612 PWM Generation Using HCS12 Timer Channels AN2612 SW     AN2597 Using the MC9S12E128 to Implement an IrDA Interface AN2597 SW     AN2573 LINkits LIN Evaluation Boards AN2573       AN2554 Clearing and Disabling Interrupt Flags AN2554       AN2552 Configuring the System and Peripheral Clocks in the MC9C12E128 AN2552 SW     AN2548 Serial Monitor Program for HCS12 MCUs AN2548 SW     AN2546 HCS12 Load RAM and Execute Bootloader User Guide AN2546 SW     AN2485 HCS12 Software Stationery AN2485 SW     AN2461 Low Power Management using HCS12 and SBC devices AN2461       AN2438 ADC Definitions and Specifications AN2438       AN2434 Input-Output Pin Drivers on HCS12 Family MCUs AN2434       AN2433 5V to 3V Design Considerations AN2433       AN2429 Interfacing to the HCS12 ATD Module AN2429       AN2428 An Overview of the HCS12 ATD Module AN2428       AN2408 Examples of HCS12 External Bus Design AN2408       AN2400 HCS12 NVM Guidelines AN2400       AN2396 Servo Motor Control Application on a LIN AN2396 SW     AN2342 Opto Isolation Circuits For In Circuit Debugging of 68HC9(S)12 and 68HC908 Microcontrollers AN2342       AN2321 Designing for Board Level Electromagnetic Compatibility AN2321       AN2318 Using the I2C Bus with HCS12 Microcontrollers AN2318 SW     AN2304 Implementation of a UDP-IP (User Datagram Protocol) Stack on HCS12 Microcontrollers AN2304 SW     AN2302 EEPROM Emulation for the MC9S12C32 AN2302 SW     AN2295 Developer's Serial Bootloader for M68HC08 abd HCS08 MCUs AN2295       AN2287 HCS12 External Bus Design AN2287       AN2283 Scalable Controller Area Network (MSCAN) Interrupts AN2283       AN2263 PC Master Software: Creation of Advanced Control Pages AN2263       AN2255 MSCAN Low-Power Applications AN2255       AN2250 Audio Reproduction on HCS12 Microcontrollers AN2250 SW SW2 SW3 AN2221 MI Bus Software Driver for the MC9S12DP256 AN2221 SW     AN2216 MC9S12DP256 Software Development Using Metrowerk's Codewarrior AN2216       AN2213 Using Cosmic Software's M68HC12 Compiler for MC9S12DP256 Software Development AN2213       AN2204 Fast NVM Programming for the MC9S12DP256 AN2204 SW     AN2201 Low Battery Cranking Pulse in Automotive Applications AN2201       AN2189 Using the Clock Generation Module on the HC12 D Family AN2189       AN2153 A Serial Bootloader for reprogramming the MC9S12DP256 FLASH Memory AN2153 SW     AN2104 Using Background Debug Mode for the M68HC12 Family AN2104       AN2103 Local Interconnect Network (LIN) Demonstration AN2103       AN2011 The MSCAN on the MC9S12DP256 compared with the MSCAN on the HC12 family AN2011       AN1954 MPXY8000 Series Tire Pressure Monitoring Sensor AN1954       AN1837 Non-Volatile Memory Technology Overview AN1837       AN1798 CAN Bit Timing Requirements AN1798       AN1783 Determining MCU Oscillator Start-up Parameters AN1783       AN1775 Expanding Digital Input with an AD converter AN1775       AN1771 Precision Sine-Wave Tone Synthesis Using 8-Bit MCUs AN1771       AN1716 Using M68HC12 Indexed Indirect Addressing AN1716       AN1705 Noise Reduction Techniques for Microcontroller-Based Systems AN1705       AN1284 Transporting M68HC11 Code to M68HC12 Devices AN1284       AN1280 Using and Extending D-Bug12 Routines AN1280       AN1263 System Design and Layout Techniques with Single-Chip Microcontrollers AN1263       AN1259 System Design and Layout Techniques for Noise Reduction in MCU-Based Systems AN1259       AN1058 Reducing A_D Errors in Microcontroller Applications AN1058       AN1051 Transmission Line Effects in PCB Applications AN1051       AN1050 Designing for Electromagnetic Compatibility (EMC) with HCMOS Microcontrollers AN1050       AN5389 S12Z MagniV LIN Bootloader AN5389 SW     AN11967 S12ZVM Family in 48 V Applications AN11967      
記事全体を表示
I would like to mention some of the many programming/debugging possibilities by this document. Possibilities for production We have no solution for mass production such as stand-alone programmers, you have to turn to the third party products. CodeWarrior (CW) Simulator/Debugger tool Hiwave: After entering into the debug mode in the CW, we can see the "True-Time Simulator & Real-Time Debugger" window which is Hiwave. Also, the Hiwave can be launched by hiwave.exe independently from the CodeWarrior which is located in the Prog folder in the CW install directory: \Prog\hiwave.exe However, we need to use it together with PEmicro BDM. PROG12Z- Flash Programmer software: PROG12Z | 68HC(S)12(X) Flash/EEPROM Programmer Software | PEmicro  Also, includes the command-line version of the programmer software - CPROG12Z. But we need to use it together with PEmicro BDM. USB Multilink Universal: USB-ML-UNIVERSAL Compatible with ARM devices from many manufacturers as well as NXP's Kinetis, LPC, S32, ColdFire V1/+V1, ColdFire V2-4, MPC55xx/56xx/57xx, HCS08, RS08, HC(S)12(X), S12Z. For more information look at the link: MULTILINK | Debug Probe | PEmicro 1 Stand-alone programmer, test & debug interface: The CYCLONE_UNIVERSAL  supports a wide variety of ARM Cortex devices from many manufacturers as well many non-Arm based devices including from NXP (S32, Qorivva (MPC5xxx), MPC5xx/8xx, S12Z, RS08, S08, HC08, HC(S)12(X), Coldfire, Kinetis, LPC),  Note: The Cyclone Pro is no available. It has been replaced by the Cyclone Universal and Cyclone Universal FX production programmers. These programmers support all of the devices supported by Cyclone PRO CYCLONE | In-System Flash Programmers | PEmicro  Or LFBDMPGMR: Lead-Free BDM Flash Programmer for S08, S12x|NXP  As a low-cost solution can be used: Open Source BDM interface: OSBDM  Or USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.  In the chapter Device Characteristics and links to documentation, can be found supported devices by USBDM and useful links for the USBDM devices where are described, for example, compatible IDEs and other useful information.   And one of the advanced tool TRACE32: LAUTERBACH DEVELOPMENT TOOLS 
記事全体を表示
Here is a SW example demonstrating measurement of the bandgap voltage featured on a microcontroller. The bandgap voltage is routed to an internal ATD channel. ATD converter measures the input voltage and stores it to a variable located in Flash memory. The SW example project is made in CodeWarrior v5.1 for MC9S12XEP100 device.
記事全体を表示
Officially we offer two S12ZVM motor control kits: MTRCKTSBNZVM128: 3-phase Sensorless BLDC Development Kit with S12 MagniV S12ZVM MTRCKTSPNZVM128: 3-phase Sensorless PMSM Development Kit with S12 MagniV® MC9S12ZVML128 MCU     In fact, the kit contents are the same - S12ZVML12EVBLIN board and LINIX 45ZVN24-90 motor. The LINIX motor is BLDC type, but their characteristics are rather close to the PMSM type. So, the difference is just in used software and jumper settings.   Since the current web pages are slightly confused, I would like to place here links for the main 4 types of software for MTRCKTSBNZVM128 and MTRCKTSPNZVM128 kits.   3-Phase Sensorless BLDC S12ZVM Application – six step driving https://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVM128QSG.pdf https://www.nxp.com/docs/en/application-note/AN4704.pdf https://www.nxp.com/webapp/Download?colCode=MTRCKTSBNZVM128_SW&appType=license    3-Phase Hall Sensor BLDC S12ZVM Application – six step driving https://www.nxp.com/docs/en/user-guide/MTRCKTSBNZVMHQSG.pdf https://www.nxp.com/docs/en/application-note/AN4718.pdf https://www.nxp.com/docs/en/application-note-software/AN4718SW.zip   3-phase Sensorless Dual-Shunt PMSM S12ZVM Application – FOC driving https://www.nxp.com/docs/en/user-guide/MTRCKTSPNZVM128QSG.pdf https://www.nxp.com/docs/en/application-note/AN5135.pdf https://www.nxp.com/webapp/Download?colCode=MTRCKTSPNZVM128-SW&appType=license    3-phase Sensorless Single-Shunt PMSM S12ZVM Application – FOC driving https://www.nxp.com/docs/en/user-guide/AN5327-QSG.pdf Note: please be aware that there is still typo error in this document (already reported) – the jumpers J57 and J60 should be in position 2-3. https://www.nxp.com/docs/en/application-note/AN5327.pdf https://www.nxp.com/docs/en/application-note-software/AN5327SW.zip   EDIT: Additionally, we may use a cost-effective S12ZVM Mini Board or Mini Kit evaluation platform. The software refers to the above mentioned, but with small modification for S12ZVML-MINBRD board.    I hope it helps you.
記事全体を表示
Dear reader,   There is extended information provided in the attached document. it contains detailed description "how-to", example design, detailed memory maps and code examples.   Also tested example projects created under CodeWarrior are attached.   I believe the document as well as SW examples will help you in the design and avoid mistakes we have met under our work in the S12(X) support team.   Yours sincerely,   Ladislav
記事全体を表示
S12(X) S12 MagniV DOCUMENTS CAN setup calculator for S12(X) and MagniV devices  S12(X) MCU Security  S12(X) devices reference schematics  Useful documents for building own CAN bootloader  How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method)  DOCUMENTS S12Z constant, variable, code allocation in CodeWarrior   BLDC 6-step control speed scaling using S12ZVM  MagniV Power Dissipation Calculator  MTRCKTSBNZVM128 vs MTRCKTSPNZVM128 kit motor  S12ZVM configuration for the motor control applications  Software for S12ZVM motor control kits  DEVKIT-ZVL128 EVB review  S12 family devices - COP recognition consideration calculator  MagniV PLL calculator  Bus-Off Handling in MSCAN   EXAMPLES CAN Standard ID and CAN Extended ID for S12(X) and MagniV devices, memories refreshment  S12XD, S12XE - External BUS design - Addendum To AN2708  S12X Examples Pack  TIC-S12-XDP512-FLASH-E_W-CW47  S12X_Interrupt_catcher (catch all unexpected interrupts)  API example code for S12G  Read paged const in S12  EXAMPLES How to get device ID and write program once field without programming application to the S12Z device in the CodeWarrior (Eclipse)  CAN Standard ID and CAN Extended ID for S12(X) and MagniV devices, memories refreshment  S12Z Protection Override  S12ZVC IFR Program Once Field  S12Z: Simulating ECC errors at EEPROM by cumulative write  S12Z: Simulating ECC errors at RAM by debug access  S12Z: Simulating ECC errors at Flash by cumulative write  S12Z SW example of COP Watchdog Reset  S12Z Interrupt catcher for unexpected interrupts  S12Z voltage measurement  S12Z EEPROM example code  S12Z Flash example code  Autonomous Clock Trimming SW example for MagniV devices  BATS Voltage Supply Sense example code for MagniV devices  High-Voltage Input (HVI) SW examples for MagniV devices  SW examples for MagniV S12ZVC and S12ZVL devices  PWM example code for S12ZVL  S12ZVL-TIM-FrequencyMeasurement-V1_0-CW106-TIC-EXAMPLE  SW example of Security feature with Backdoor Access Key option for S12ZVL  Example S12ZVL ADC0 triggered by TIM0 OC updates PWM duty cycle  S12ZVM clock module and PLL configuration - SW examples  Low power mode example code for S12ZVC  Single / double bit RAM ECC error example code at S12ZVC  S12ZVML-MINIBRD software ported from AN5327  Example: S12ZVC192-ACMP-POT-CW107  Example codes form "Easily Develop LIN-based Actuator Applications with Mixed-signal MCUs" webinar     
記事全体を表示
Interrupt catcher example code catches all unexpected interrupts. It can be used for debugging or directly in the application software. The Machine Exception routine is used here as example of expected interrupt.   A few notes: 1. For each expected interrupt you must remove a code line for given interrupt     from the part of the code "A Set of unimplemented interrupts" and     create your own service routine as it is, for example, made     for interrupt 5 void Machine_Exception_ISR(void)   2. All interrupt vectors have 32bit size, however, addresses have only 24bit,     therefore the most significant byte in interrupt vector is not used.     Definitions with the keyword "interrupt XX" where XX represents vector     order in the interrupt vector is used to define interrupt service function.      3. Interrupt number 0 is assigned to POR reset vector,                      1 is assigned to Unimplemented page1 op-code trap vector                      2 is assigned to Unimplemented page2 op-code trap vector                      3  ...                      4  ...     Interrupt number = (0x1FC-Vector Address)/4. See Table 1-11. Interrupt     Vector Locations at RM(page 62-65).     For Example: Interrupt number of SCI0 = (0x1FC-0x19C)/4 = 0x18 = 24.     So you can use either form                interrupt VectorNumber_Vsci0 void SCI0_isr(void)     or                interrupt 24 void SCI0_isr(void)     or                interrupt ((0x1FC-0x19C)/4) void SCI0_isr(void)       Note: VectorNumber_Vsci0 is defined in mc9s12zvl32.h      
記事全体を表示
Based on S12G128,  Firstly, placed some const at PAGE_0B,  Secondly, place the same data at NON_BANKED  Finally, you can check whether reading result of paged const is right. Of course, they are the same.  Cheers !
記事全体を表示
The bold blue links below provide direct download of SW example packs for MagniV devices based on S12Z core.   S12ZVC Getting Started Exercises (REV 1.0) This file contains four hands-on exercise where you can find basic setup code to enable a quick development in different areas. The file includes CodeWarrior projects demonstrating usage of peripheral modules such as: - Digital-to-Analog Converter (DAC), - Controller Area Network (CAN), - Pulse Width Modulation (PWM), - Timer (TIM).   Getting started with S12ZVL32 - S12 MagniV Example Codes (REV 0) The MC9S12ZVC device integrates a battery level (12V) voltage regulator and supply voltage monitoring. This zipped file includes four CodeWarrior examples demonstrating - Overcurrent protection on EVDD pin, - low power STOP mode with API timer and wake-up feature, - Pulse Width Modulation (PWM) - Serial Peripheral Interface (SPI) communication.   Many of these examples can be used on various MCU families across the MagniV product line. Check the appropriate device guide for list of modules and its versions.
記事全体を表示
Hello Community user, This post is intended to show how to recovery from Bus-Off state using the MSCAN and CANPHY modules in the MagniV devices. This example is focused on S12ZVC due to the internal CANPHY so it makes easier to create a quick example. What is Bus-Off condition? The bus-off condition is a catastrophic condition where the node in this state does not transmit anything on the bus. How to enter in Bus-Off state? A node enters in this state if any of the two error counters, Transmit Error Counter (TEC) and Receive Error Counter (REC) raises above 255. How to recovery from Bus-Off? A note is permitted to become error-active (no longer bus-off) when its error counters both set to 0 after 128 occurrences of 11 consecutive recessive bits have been monitored on the bus. The MSCAN module implements two ways to recover from the fault, the automatic and the manual. The automatic bus-off recovery method puts the node into the error-active state after monitoring 128 occurrences of 11 consecutive bits on the bus. It's important to note that the CANPHY also reports errors on the bus so, the proper error flags must be clear to assure the correct functionality of the node if CANPHY is being used. The manual bus-off recovery method (which is used in this example) puts the note into the error-active state after both independent events have become true in any order: 128 occurrences of 11 consecutive recessive bits on the CAN bus have been monitored. (Cannot be consecutive). CANMISC[BOHOLD] bit has been cleared by the user. Implementation The project contains a header file called  "common.h" which contains three defines that are used to set the CAN nodes. Just one define must be active per node. NODE0_TX and NODE1_TX are transmitting messages on the CAN bus and the NODE_RX is receiving the messages. #define NODE0_TX #define NODE1_TX #define NODE_RX‍‍‍‍‍‍ All nodes are blinking the green led indicating the communication is stable and no errors have occurred. At this point, you should generate the bus-off condition. A way to generate a bus-off condition is grounding one of the two CAN lines (CAN_High or CAN_Low) which will cause a bus-off condition to the transmitters nodes. When the node is in the bus-off state, the yellow led is toggled. At this point, you should not be any message being transmitted on the bus due to the transmitter node is in bus-off. The bus-off condition is detected by the application in the bus-off interrupt (refers Events.c file) which triggers the yellow led toggling. void CAN0_OnBusOff(void) { /* Get CAN bus status */ CAN0_GetError(&gCANErrpr); /* If bus error is set, inform to the application*/ if(gCANErrpr.errName.BusOff){ gBusOffState = PENDING; } CAN0RFLG_CSCIF = 1; // Clear flag }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ In the main.c file when the node transmitters are selected, there is a routine asking for a push-button event. This event triggers the bus-off recovery request by setting the CANMISC[BOHOLD]. At that point, the 128 occurrences of 11 consecutive recessive bits on the CAN bus should have passed and the green led will toggle again indicating the communication is stable again and no errors have occurred. At this point, you should see the messages on the CAN bus again. /* Read button to recovery from bus off condition*/ if(PushButton3_GetVal()){ CAN0_BusOffRecoveryRequest(); // Request get out of bus off gBusOffState = NONPENDING; /* Clear bus off LED indicator */ LED_YEL_OFF; }‍‍‍‍‍‍‍‍‍‍‍‍‍‍ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note: The VLG-MC9S12ZVC was used for this example and the push button that must be pressed is SW12. Best Regards, Atzel Collazo
記事全体を表示
Interrupt catcher you can use for debugging or directly in your software. Few notes: 1. You should replace lines for expected interrupt by your interrupts routines as in example of SCI0 interrupt routine. 2. All interrupt vectors are only 16bit addresses, therefore all your interrupt routines must be placed in non banked memory (for example by #pragma commands) 3. Interrupt number 0 presents POR reset vector, 1 is CM reset, 2 is COP reset, … , 119 is Spurious Interrupt. Interrupt number = (0xFE-Vector Address)/2. See Table Interrupt Vector Locations at RM. For Example: Interrupt number of SCI0 = (0xFE-D6)/2 = 0x14 = 20.
記事全体を表示
Tested on: DEVKIT-S12ZVC MCU: S12ZVC192 Development tool: CodeWarrior 10.7 This example shows ACMP - analog comparator,  which compares voltage from potentiometer and voltage from DAC. DAC is set at 2.5V and uses the positive input of the comparator. Potentiometer uses the negative input in the range of 0V - 5V. When the potentiometer is moved, the output from ACMP will be changed.  If the voltage at the non-inverting (positive) input > the voltage at the inverting (negative) input, the output result is in the logic level 1 and the red LED is on.
記事全体を表示
******************************************************************************** Detailed Description: TIM0_Ch2 OC triggers ADC measurements on AN2 (DEVKIT S12ZVL32, potentiometer) every 50ms. ADC interrupt updates duty-cycle (0-100%) of 3 PWM signals that are shifted by 90°. ADC can work either in Trigger or Restart mode. PWM signals are routed to RGB LEDs (DEVKIT S12ZVL32). --------------------------------------------------------------------------------------------- Test HW: DEVKIT-S12ZVL32 MCU: S12ZVL32 Debugger: CW11 Target: internal_FLASH ********************************************************************************
記事全体を表示
Abstract The paper describes basic scaling procedure of a six-step BLDC motor control application with focus on S12ZVM MCU devices.  Abstract Introduction BLDC six-step control Speed scaling Timing Commutation periods Speed calculation Application note links Calculation accuracy Real applications Resources Introduction Based on the various questions regarding the BLDC speed calculation, I've decided to write this document to make the scale calculation clear. Please use it for your reference and comment in case there is something to be explained in more details. BLDC six-step control This document is linked with the six-step control of BLDC motors, known for the trapezoidal back-EMF shaped voltage. The key is to create a torque using DC current in two phases while the third phase is not connected. As the rotor is moving, the phases are switched (commutated) to keep the stator flux ahead the rotor flux. The principles are well described in many application notes, such as AN4718 or AN4704. The instant of the commutations can be driven by Hall sensors or by the back-EMF signal monitoring (so-called "sensorless"). For field-oriented control, please refer to the PMSM control discussed in AN5135 or AN5327. Speed scaling It's more benefitial to describe in details the sensorless algorithm over the hall-sensor-based control. However, the approach is almost the same. Timing The motor speed is calculated based on the zero-cross detection of BEMF voltage on a non-active phase. These zero-cross events times are measured by capturing a timer (TIM0CNT) register at the time the ADC routine detects a zero-cross (or when the Hall sensor commutation event occurs). That means, the time is scaled by the timer TIM0 settings. There is no general guidance how to set up the timer. However, the timer should be set to cover some reasonable number of ticks between two commutations (which is linked to the speed precission at high speeds) and should be able to cover two commutations "far away" from each other at very low speeds, without the timer overflow. A good practice would be: at least 100 timer ticks between two commutations maximum 16bit = 65535 ticks between two commutations The same aproach can be followed using the Hall-sensor events. Commutation periods In the application, zero-cross (or hall-sensor) periods are captured with periodZC_F_PhA, periodZC_R_PhA, etc. or periodZC[6], defined as tU16 (16 bit unsigned). The periods are captured using a timer, as mentioned above. In electric motor theory, we recognize "electrical" and "mechanical" speed. The "electrical" speed is linked with the rotational field. The mechanical speed is connected directly with the rotor speed. The relation between these two speeds is determined by number of poles or pole-pairs: (1)   mechanical speed = electrical speed / number of pole-pairs = electrical speed / ( number of poles / 2 ) In the following text, 3-phase BLDC motor is discussed. Speed calculation To calculate one "electrical" revolution of a motor = 6 commutations (or 6 zero-crosses), all the 6 commutation time periods shall be summed. For that case, the resulting "period6ZC" is defined, formated as tU32 (or unsigned long) to prevent an overflow if all six 16-bit zero-cross periods are summed. If you sum all the 6 zero-cross periods, you'll get the number of timer ticks per single "electric" revolution. That means, if the motor is 2-pole motor ( = 1 pole-pair motor), it would be the time per single "mechanical" revolution of the rotor. In thsi case: (2)   mechanical speed = electrical speed; You can easily get the time per mechanical revolution for higher-pole motor simply by multipling it by number of pole-pairs. (3)   time per mechanical revolution = period6ZC * number of pole-pairs  The period per 6 zero-crosses "period6ZC" is calculated within the control loop, usually in the 1 ms timer interrupt routine. Since the speed (rotor frequency) is just an inverted time period, we can use following code line to calculate the actualSpeed: (4) actualSpeed = SPEED_CALC_NUMERATOR / period6ZC; Now, how to read it's scale and what is the SPEED_CALC_NUMERATOR? Let's assume the "actualSpeed" is tFrac32 (1.31 formated signed 32bit number). It would mean the maximal fraction number is 1.0, which is represented by its integer value 2^31 = 2,147,483,648. Why to use 32-bit number over 16-bit is obvious - since the period6ZC is 32-bit value, the result should be of the same resolution or width. The task is to find the right SPEED_CALC_NUMERATOR. Let's consider the S12ZVM device and the timer TIM0 used to capture the zero-cross events times. The prescaler is set to 16 (TIM0TSCR2_PR = 4) and the bus clock is 12.5MHz, the timer tick is 12.5MHz / 16 = 781.25 kHz, in time scale it is 1.28us. Let's assume the maximum mechanical speed of the motor is 10,000 RPM and the motor has 6-pole-pairs. That would give us (5)   (10,000 RPM) / (60 seconds) = 166.67 revolutions per second, (6)   166.67*(6 pole-pairs) = 1000 electrical revolutions per second, so (7)   1000 * (6 commutations) = 6000 commutations/zero-crosses per second. (8)   That would make 1/6000 = 166.67us per one commutation. (9)   Ticks per one period at max speed = 166.67 us / 1.28us = 130.28 With our 1.28us timer, we can catch upto 130 periods at maximal speed. For maximal speed of the motor 10,000 RPM, we can simply rearrange the "actualSpeed" calulation shown in (4) into (13) and (14), assuming that: (10)   actualSpeed = FRAC32(1.0) = 2,147,483,648 (11)   period6ZC = 6 periods * 130 = 780 (rounded down, since the value is still an integer) In case of S12ZVM device, it is more convenient to use 16-bit (tFrac16) calculations than 32-bit. Hence, we can do a trick with the scaling to use 32-bit actualSpeed to prevent an overflow use the same 32-bit number as 16-bit number just by scaling it correctly benefit from the 16bit calculation, which is good enough and fast enough at the same time The trick is hidden in the casting of the actualSpeed from Frac32 to Frac16: (12)   speedErr = requiredSpeed - (tFrac16) actualSpeed; That means, only the lower 15 bits are considered the speed (assuming the actualSpeed will never exceed 32767 so the 16th "sign" bit will always be zero). For maximum speed and the SPEED_CALC_NUMERATOR determination, the "actualSpeed" should be 32767 (which is the range of signed tFrac16). Equation (4) can be used to calculate the SPEED_CALC_NUMERATOR as follows: (13)   32767 = SPEED_CALC_NUMERATOR / 780 (14)   SPEED_CALC_NUMERATOR  = 780 * 32,767 = 25,558,260 Thus  #define SPEED_CALC_NUMERATOR 25558260 Using the equation (4), the speed for the minimum period6ZC would be: (15)   actualSpeed = SPEED_CALC_NUMERATOR / period6ZC = 25,558,260 / 780 = 32,767; Masking that value by lower 15 bits and casting it to tFrac16 would give us 1.0. Since the speed scale has been determined by the maximum speed of the motor 10,000 RPM, we can calculate the real speed simply by: (16)   RealScaleSpeedRPM = (tFrac16)actualSpeed / 32,767 * MAX_SPEED = (tFrac16)actualSpeed / 32,767 * 10,000. Application note links In the application note AN4704, there are several macro constants used to control the application. These constants should be calculated using following definitions, with a little help of the SPEED_SCALE - floating point representation of the real scale of the speed. #define SPEED_SCALE 10000.0  // Used for correct calculation of the following: #define REQUIRED_RUN_SPEED FRAC16(2000.0/SPEED_SCALE) // 2000 rpm #define MIN_SPEED FRAC16(500.0/SPEED_SCALE) // 500 rpm minimal speed for Down button control (should be min 10% of nominal motor speed) #define MAX_SPEED FRAC16(5000.0/SPEED_SCALE) // 5 krpm maximum speed for Up button control #define SPEED_STEP FRAC16(100.0/SPEED_SCALE) // 100 rpm, Up/Down step for button controls   If the application uses FreeMASTER to display or control, the scales shall be updated in the FreeMASTER project as well. The new FM scales for AN4704 are: Variable name Variable watch settings requiredSpeed Real type transformation: Linear: a = SPEED_SCALE = 10,000; b = 0 actualSpeed Signed int, Size = 4 Show as: REAL Bit fields maks with: word (0xffff) Real type transformation: Linear: a = SPEED_SCALE / 32767.0 = 0.3051851; b = 0  Calculation accuracy Now, let's have a look on the speed resolution (or accuracy): At the full speed, if one period changes by 1 tick, then you'll get the period6ZC from 780 to 781 at max speed, which makes 12.8041 RPM difference. The higher the SPEED_SCALE is, the higher the error is. If the assumption would be a change in all of the 6 periods (thus the period6ZC would change from 780 to 786), the resulting change to the speed would be 76.336 RPM. That makes the speed error 10,000 RPM +- 76, which is 0.76%. In terms of accuracy, it makes sense to set the maximum speed (or the SPEED_SCALE) to the maximal speed of the application instead of copying some high number from the datasheet of the motor. Well, the max speed of the application should not exceed the max speed of the motor, but it doesn't help if the speed scale is unnecessarily high. Real applications In real applications, the calculated speed (actualSpeed) reflects all the deviations and changes of the period6ZC. Therefore, it is a good practice to do some kind of filtering of the period6ZC, either by averaging or using a low-pass filter. In case of one or more zero-crosses are lost, there should a mechanism to process and detect if the motor is stalled (mechanical speed loses lock with the commutation) or if it is just a disturbance to the signal. The stall detection or the Hall-signal fault/damage detection is one of the challenges towards high quality application. Resources S12ZVM MCU - NXP main S12ZVM page AutoMCDevKits - NXP Automotive Motor Control Development Solutions AN4718 - 3-Phase BLDC Hall Sensor Application Using S12ZVM AN4704 - 3-phase Sensorless BLDC Motor Control Kit with the S12 MagniV MC9S12ZVM AN5201 - Integrating the LIN driver with BLDC sensorless motor controller In the S12ZVM128 device AN5330 - Migration Guide for S12ZVM Devices
記事全体を表示
You can find here two example codes for API timer. G240-API-CW51.ZIP contains example code for trimming API timer to 10kHz (API isn't factory trimmed). G240-API+STOP-CW51.ZIP contains example code for enter to stop mode and periodical wakeup by API interrupt
記事全体を表示
The S12Z MCU has linear address space therefore constant, variable, code placement is easier in compare with older S12 or S12X MCUs. But still, there are several ways and potential issues.   The object placement is made by Smart Linker. The linker configuration is defined by settings in project *.prm file and also by linker command line options (menu - Project – Properties – C/C++ Build – Settings – S12Z Linker). The detail information about linker options may be found in MCU_Build_Tools_Utilities.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_Build_Tools_Utilities.pdf"   We may define memory segments in *.prm linker file. The default prm file contains segments for RAM, EEPROM, and ROM (Flash). The sizes of these segments typically reflect our MCU derivative physical memory map, but we may redefine that and use more virtual segments per our needs. The physical/virtual segments definition in prm linker file is located at: SEGMENTS // segments definition END‍‍‍‍‍‍   The general data placement may be divided into two main approaches: Manual – the programmer will specify fix address for some of the data Automatic – the placement will be driven automatically by Smart Linker   Manual placement The first option is an exact specification of specific content at a specific address. This may be managed for a small amount of data by FILL linker command in *.prm linker parameter file. For example: SEGMENTS //… ROM_CONST       = READ_ONLY   0xFE0000 TO 0xFE0000 FILL 0x5A;  //insert 0x5A value at address 0xFE0000 //… END‍‍‍‍‍‍‍‍‍‍ Such placement isn’t very comfortable, but it might be simply used for some configuration data out of project code. Note: you may use more than one bytes (e.g. FILL 0x0A 0x34). If segment size is bigger than a number of specified bytes, the bytes will be used as a pattern for filling whole target segment. Note: The potential linker placement will overlap such defined data.   The next option is using address specification by an @ qualifier directly in C code. For example: unsigned const int rom_const @0xFE0100 = 0x5AA5;‍‍ This may be used also for more complex types than simple byte – typically arrays,...   Since such type of placement is still manual, the linker parameters must be configured for avoiding possible overlapping. Be aware! The default CW project has disabled memory overlapping warnings. So, we must exclude target memory area from linker using. For example, in the *.prm file: SEGMENTS //… ROM_1           = READ_ONLY   0xFE0000 TO 0xFE00FF //ROM_CONST  = READ_ONLY   0xFE0100 TO 0xFE0101;            //we use the 0xFE0100 byte for rom_const ROM_2           = READ_ONLY   0xFE0102 TO 0xFFFDFF //… END‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note: We use qualifiers for define memory access type. READ_ONLY is used for Flash, READ_WRITE for RAM and NO_INIT for RAM where we do not want to initialize data after reset. Sections placed in an NO_INIT segment should not contain any initialized variables (variable defined as int c = 8).   Note: The manual placement may be also implemented by assembler code. For example: XDEF MyVariable MyVariable: equ $1100‍‍‍‍ However, also in this case, we must exclude target memory area from linker use like in the case of @ qualifier for avoiding memory overlapping.   Automatic placement by linker The PLACEMENT block allows us to physically place each section from the application in a specific memory area (segment). The sections specified in a PLACEMENT block may be linker-predefined sections (like DEFAULT_ROM, DEFAULT_RAM, COPY, SSTACK,…) or user sections specified in one of the source file building the application (like MY_RAM,…). PLACEMENT // section(s) INTO segment(s); MY_CODE INTO ROM_1; END‍‍‍‍‍‍‍‍ Note: Since the linker is case sensitive, the name of the section names specified in the PLACEMENT block must be valid predefined or user-defined section names. Note: There is quite mess in ELF/Freescale section/segment terminology. Please take this information as simplified as possible. Please look at MCU_Build_Tools_Utilities.pdf for more details about predefined segments/sections. Note: We may place a various number of sections into a various number of segments. The “,” is used as section/segment delimiter. Note: In general, the placement order is given by simple list order (first specified section will be allocated from first specified segment, after that next section …). But, there are still few limitations for sections list order. The error is generated in the case of wrong list order – for example: ERROR L1122: only checksum section may be behind .copy in the section list.   The default variable/constant/code placement may be changed by #pragma commands. Note: Most of these pragma commands are not limited to the single file. Therefore, we should keep it in complementary pairs. An example of placing code into specific section: #pragma CODE_SEG MY_CODE void f(void) { //… } #pragma CODE_SEG DEFAULT‍‍‍‍‍‍‍‍‍‍‍‍ The #pragma DATA_SEG modifies variable placement. For example: #pragma DATA_SEG MY_RAM unsigned int counter; //… #pragma DATA_SEG DEFAULT‍‍‍‍‍‍‍‍   The #pragma CONT_SEG modifies variable placement. For example: #pragma CONT_SEG MY_ROM const unsigned int my_parameter; //… #pragma CONT_SEG DEFAULT‍‍‍‍‍‍‍‍   Note: The shorter option for directly allocating variables in a named segment, rather than using a #pragma may be used. For example: unsigned int counter@"MY_RAM";‍‍ However, even in such case, the #pragma command like #pragma DATA_SEG MY_RAM must be used at least once prior that variable declaration.   Note: The S12Z compiler/linker allows to use also already predefined sections like DEFAULT_ROM, DEFAULT_RAM or ROM_VAR as target sections in #pragma commands (not possible in the case of older S12(X) compiler/linker).     More details about #pragma commands may be found in MCU_S12Z_Compiler.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_S12Z_Compiler.pdf" Data alignment Sometimes we need to keep allocated data aligned. This is for example typical requirement for ADC command and result list where DMA is used for transfer data between ADC module and memory. The simplest method is using alignment attribute. For example: volatile unsigned long adc0_cmdlist[NR_A_CH] __attribute__ ((aligned (4))); //max 256 bytes = 64 commands per 4-byte entries volatile unsigned int adc0_results[NR_A_CH] __attribute__ ((aligned (4)));  //max 128 bytes = 64 results per 2-byte entries‍‍‍‍ I hope it helps you. Best regards Radek
記事全体を表示
Since there isn't a CAN based bootloader developed for S12X device family, here are some useful documents that might be of help for creating such bootloader:   - The AN3312 is an application note of a BootLoader that uses CAN but it is targetted for our DSC family of devices. These devices have the FlexCAN module (the silicon that handles CAN Communications is different to the one in the MC9S08DZ60). However this document can be used as a reference on how to build a loader. https://www.nxp.com/docs/en/application-note/AN3312.pdf    - Following document explains how to use the msCAN module for communications. It provides basic examples on how to send and receive data through the port. https://www.nxp.com/docs/en/application-note/AN3034.pdf    - Next document provides the source code and documentation for an assembly-written Bootloader. This software loads the code through the serial port and burns it into flash. This document can help you understand the specific details of the bootloader implementation. This code is available for a lot of S08 families included the MC9S08DZ60 device. https://www.nxp.com/docs/en/application-note/AN2295.pdf  - Serial booloader for S12(X) family: https://www.nxp.com/docs/en/application-note/AN4258.pdf    With the information in these documents you can design your loader and plan how to solve the 5 main challenges of a loader application:   ++Memory Protection++ The Boot Loader handles the non-volatile memory of the microcontroller. The developer must plan how much memory is needed for the loader and protect it. Memory protection provides a guideline of the final system memory organization. A section of memory is used for the loader and another section for the application. Applications that will be executed with a loader are affected by how the loader manages memory and interrupt vectors.   ++Burning Flash++ Programming and Erasing non-volatile memory requires special attention as the procedure must be executed in RAM. The process of handling NVM may vary between devices. We have source code that provides routines to write Flash and that solves the problem of executing in RAM.   ++Vector Redirection+ Interrupt vectors should be shared between the application and the users code. Hardware vector redirection is supported by the microcontrollers but with some limitations. It is necessary to decide how vector redirection will be implemented. Software and hardware methods can be used to redirect vectors.   ++Data Interface++ Different applications required different interfaces to receive s-record information. Serial Ports are used widely for this purpose although the bootloader implementation should allow exchanging interfaces in a simple way. For your case you want CAN interface. CAN frames support up to 8 bytes of data per frame. This requires the developer to fully design a protocol or a data structure mounted over the CAN frames to be able to send the complete frames to the device that will be reprogrammed.   ++Mode Selection++ The Boot Loader is the owner of the reset vector. Upon startup the Boot Loader should select if the User code will be executed or if the Boot Loader mode should execute. The applicaton determines the best way to select between User/Loader mode. It might be a simple GPIO or a CAN frame or any input that can be recognized by the application and Loader to be able to set the loader mode when needed. Developing a loader is not easy, but hopefully this information will be of a great help.
記事全体を表示