NXP Tech Blog - Page 13

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Tech Blog - Page 13

PetrKraus
NXP Employee
NXP Employee

The Kinetis Design Studio support has been phased out. The latest SDK version 2.4 doesn’t support this toolchain. The SDK builder always builds new SDK packages from the latest SDK version supporting the selected device/board/kit. That is the reason why KDS is not on the list of the available toolchains now.

Read more...

More
0 0 2,697
SowmyanKousthub
NXP Employee
NXP Employee

Attached is a sample source code for OTP programming in NXP LPC54018 MCU.

Brief about the example:

The example programs 4 words of data each into OTP bank 1 and OTP bank 2. The example uses LPC54018 SDK drivers. The complete SDK for LPC54018 can be downloaded from Welcome | MCUXpresso SDK Builder .

Read more...

More
0 0 2,912
csmgsarma
Contributor IV

I was surprised to learn MQX(Ver 4.2) does not support SPI Slave configuration.

Reference

There are many workarounds in the community but the information is in bits and pieces. So i decided to write this note.

I wanted to configure SPI0 Channel on MK64FX512VLQ12 board as Slave driven by interrupt in which can call MQX APIs. I have MQX Ver 4.2 installed.  My base BSP is derived from TWR-K64 board BSP given by MQX. IDE is KDS.f Reference hardware is TWR-K64 board. 

Read more...

More
1 0 3,355
omar_cruz
NXP Employee
NXP Employee

If you are searching for a high-performance, power efficient, yet cost sensitive MCU for your designs, then here is the exciting news: NXP recently introduced the LPC51U68 MCU.

Read more...

More
2 5 7,697
MeganHansen
NXP Employee
NXP Employee

NXP has released new updates to the MCUXpresso suite of software and tools. These updates include support for new Kinetis, LPC and i.MX RT devices based on the Arm Cortex-M core, along with improved features and functionality.

Read more...

More
3 1 3,891
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v4.1 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

Read more...

More
1 0 3,159
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v10.2.0 (build 759) is now available.

This is a major new version of the IDE, and contains many new features and enhancements over the previous v10.0 and v10.1 releases. The attached presentation, recommended viewing for all users (new or experienced),  provides an overview of many of the major changes, as well as things to be aware of when upgrading from an earlier release

Read more...

More
1 0 23.6K
brendonslade
NXP TechSupport
NXP TechSupport

@jennymplunkett from the Arm mbed team just posted a great tutorial using the LPCXpresso54608 touch screen on her blog... check it out at https://os.mbed.com/blog/entry/How-to-LPCXpresso54608-touch-panel/

Read more...

More
1 0 2,312
brendonslade
NXP TechSupport
NXP TechSupport

The LPC800-DIP board is now being sold by Coridium for just $10:

http://www.coridium.us/coridium/shop/boards/bd07-special

Read more...

More
1 0 1,899
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v10.1.1 (build 606) is now available.

 

This is a minor update to the MCUXpresso IDE v10.1.0 release, the main changes being to fix a small number of SDK handling related issues.

Read more...

More
0 0 17.3K
lpcxpresso_supp
NXP Employee
NXP Employee

Now updated to v201

We have updated the attached document detailing various features relating to using the iMXRT1050-EVK(B) evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.x.

 

Read more...

More
7 1 28.1K
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v4 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

Read more...

More
1 0 2,776
randylathropade
Contributor I

I have the OM13086 Cloud Connectivity Kit
I have been following the ZentriOS "Quickstart Guide".
As part of the Zentri OS Quickstart procedures, I chose "Custom Install", so instead of using the "Zentri IDE", I'm uisng LPCXpresso 8.2.2, with the Zentri SDK plugin

Read more...

More
0 1 4,516
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v10.1.0 (build 589) is now available.

 

This incorporates many new features, as well as enhancements based on feedback that we have received since the original MCUXpresso IDE v10.0.0 launch back in March.

Read more...

More
1 0 15.2K
brendonslade
NXP TechSupport
NXP TechSupport

Today we announced the new LPC8N04, NFC-enabled MCU. We will be demonstrating the board at ARM Techcon in San Jose, and the lucky first 100 visitors to the NXP booth can exchange their business card for a free board!

Read more...

More
1 0 2,713
brendonslade
NXP TechSupport
NXP TechSupport

You may be interested to know that we recently released a new set of debug firmware and Windows 7 drivers for our boards that feature the LPC11U3x MCU as a debug probe (so all the "MAX" boards). The new firmware can be found under the Software & Tools tab of the board page you are using  http://www.nxp.com/demoboard/omxxxxx (where xxxxx is the board part number, such as om13071, om13097, etc.

Read more...

More
1 3 15.3K
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE v10.0.2 (build 411) is now available.

Read more...

More
2 0 65.7K
Daniel_Popa
NXP Employee
NXP Employee

Win a S32K144 or MPC5744P Development Kits. Do you want to know how ? Follow this topic for the next weeks and you'll find out more details.

 

Let us start by giving you a few hints:

- it is big event

- it has to do with Model Based Design

- it is something we build from scratch for that event based on S32K and MPC5744P

Read more...

More
1 16 7,737
ckphua
NXP Employee
NXP Employee

For the low pin count and small memory footprint LPC800 family, NXP offers free LPCOpen Driver Code and Example Code Bundles. 

The LPCOpen Driver Code for LPC81x/82x/83x series, is an Application Programming Interface (API) base. For users who are not too concerned with overall code size, LPCOpen provides the ease of use without diving into details of each peripheral registers, and it is easy to migrate from LPC8xx to LPC11xx family. 

Read more...

More
1 1 7,072
BlackNight
NXP Employee
NXP Employee

The link below is a step-by-step tuturial how to use the LPC800-DIP board with the MCUXpresso IDE

Read more...

More
0 0 13.4K
BlackNight
NXP Employee
NXP Employee

The MCUXpresso IDE has flexible ways how to use 'disconnect' and 'terminate'. Read more about this in

MCUXpresso IDE: Terminate and Disconnect a Debug Session | MCU on Eclipse 

Read more...

More
0 0 2,036
justinbmortimer
NXP Employee
NXP Employee

Nice project from Kevin Townsend showing off capabilities of LPC824 with it's state configurable timer to drive Neopixel and IR distance application.

 

Read more...

More
1 0 2,023
justinbmortimer
NXP Employee
NXP Employee

I love seeing how our LPC community uses our microcontrollers ... keep sharing what you create and let's continue to support and invest in each other.  

 

Read more...

More
1 0 1,663
ericding
NXP Employee
NXP Employee

Hi LPC fans,

 

We have very good news to share with you today.

As you know, one of the major roadmap for LPC this year is the LPC546xx release.

And it will be coming soon~~~, as you all expected.

For this new and hot product, the LPC SE team has prepared a serial of training slides covering almost every peripheral and aspects of LPC546xx.

Read more...

More
3 1 90K
BlackNight
NXP Employee
NXP Employee

I have completed an article (external link) describing how existing Kinetis Design Studio projects can be imported and used in the MCUXpresso IDE

Read more...

More
1 0 58.6K
BlackNight
NXP Employee
NXP Employee

The following article (external link) shows how to install the Eclipse Market Client into the MCUXpresso IDE

Read more...

More
0 1 2,847
BlackNight
NXP Employee
NXP Employee

The following article (external link) shows how to genereate S-Records (.s19), Intel Hex (.hex) and Binary (.bin) files:

MCUXpresso IDE: S-Record, Intel Hex and Binary Files | MCU on Eclipse 

 

Enjoy!

Erich

More
1 0 9,368
BlackNight
NXP Employee
NXP Employee

If you have already Kinetis Design Studio v3.x installed on Linux, then you might run into a P&E driver installation problem while installing MCUXpresso IDE v10.0.0 build 344.

Read more...

More
0 0 3,849
BlackNight
NXP Employee
NXP Employee

The following blog post gives a tour through some of the features in the NXP MCUXpresso IDE:

MCUXpresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse 

Read more...

More
0 0 1,660
justinbmortimer
NXP Employee
NXP Employee

I am humbled and energized after spending a week with 30,000+ engineers at this year’s Embedded World!

Amazing.  That’s the only way to describe the passion and enormity of our LPC FANS across Europe.  LPC is deep-rooted in the hearts of many and I am lucky to be a part of this inspired, tightknit community.    Embedded World has a strong place in the heart of LPC. 

My personal highlights from the event .... LPC FANS, What's Popular, MCUXpresso & Geoff.

Read more...

More
1 2 13.3K