Overview of using the MIMXRT1050-EVK(B) with MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overview of using the MIMXRT1050-EVK(B) with MCUXpresso IDE

lpcxpresso_supp
NXP Employee
NXP Employee
7 1 25.9K

Now updated to v201

 

We have updated the attached document detailing various features relating to using the iMXRT1050-EVK(B) evaluation board with MCUXpresso IDE v10.2.1 and SDK v2.4.x.

 

Also attached are the following:

 

  • a connect script file (RT1050_SDRAM_Init.scp) to enable the on board SDRAM
    • This LinkServer connect script can be used to enable the on-board SDRAM prior to debug operations directly to this memory region. Please see the attached document for more details.
  • a connect script file (RT1050_Debug_Connect.scp)
    • this LinkServer connect script may assist users who experience problems obtaining debug control of this board. Again, please see the attached document for more details.
  • a folder containing the required header source files to enable boot from QSPI
    • these files are only for use with boards modified to use the onboard QSPI device

 

Yours,

 

MCUXpresso IDE Support

1 Comment