OM13086 ZentriOS Device Setup failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13086 ZentriOS Device Setup failure

randylathropade
Contributor I
0 1 4,955

I have the OM13086 Cloud Connectivity Kit
I have been following the ZentriOS "Quickstart Guide".
As part of the Zentri OS Quickstart procedures, I chose "Custom Install", so instead of using the "Zentri IDE", I'm uisng LPCXpresso 8.2.2, with the Zentri SDK plugin

I've left the LPCXpresso43S67 board jumpers in the default configuration, please see attached photos.
I connected the LPCXpresso43S67 + LPC General Purpose Shield boards to my laptop with 2 USB cables.
When I follow the Quickstart instruction "Running the ZentriOS Setup Device Wizard", it fails, with these messages:

 

Setting up the device for SDK development ...
03:27:16.165 [INFO] Verifying DMS credentials ...
03:27:17.904 [INFO] DMS credentials valid
03:27:17.946 [INFO] Retrieving available platforms from DMS ...
03:27:18.515 [INFO] 4 platforms available
03:27:18.517 [INFO] Probing for connected device ...
03:27:18.517 [INFO] Discovering device connected to local computer ...
03:27:19.36 [INFO] Starting OpenOCD server for AMW106 ...
03:27:23.365 [INFO] Starting OpenOCD server for AMW004 ...
03:27:27.786 [INFO] Starting OpenOCD server for AVN4343 ...
03:27:31.823 [ERROR] Is the device connected and correctly enumerated?
03:27:31.823 [ERROR] Exception: No devices found
03:27:33.391 [INFO] Ensure the device is connected via USB to the computer and that the USB is correctly enumerated.

<img src="https://docs.zentri.com/resources/wifi/sdk/setup-device/sdk-connecting-an-nxp-device1.png" width="539" height="192" />

More information here: <a target="_blank" href="https://docs.zentri.com/wifi/sdk/latest/user-guide/getting-started#setting-up-the-zentrios-device" >Connecting NXP Hardware</a>
03:27:35.292 [INFO] Is the device connected and correctly enumerated?
03:27:35.293 [INFO] Checking for solution ...
03:27:35.295 [INFO] Retrieving driver nodes ...
03:27:35.638 [INFO] NXP driver repair available
03:27:36.805 [INFO] Attempting to repair NXP driver issue
tools/makefiles/standard_platform_targets.mk:38: recipe for target 'setup' failed

1 コメント