MCUXpresso IDE v10.2.1 Now Available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso IDE v10.2.1 Now Available

lpcxpresso_supp
NXP Employee
NXP Employee
0 0 7,182

We are pleased to announce that MCUXpresso IDE v10.2.1 (build 795) is now available.

 

This is a maintenance release that builds upon the previous MCUXpresso IDE v10.2.0 release, and we recommend that all existing users download and install this new version.

 

To download the installers for all platforms, please login to our download site via:

 
Summary of Changes - version 10.2.1 - July 2018

  • Fixed issue in New Project Wizard when switching between a board and a generic device (or vice versa)
  • Fixed issue with floating point settings when importing SDK example projects for Cortex-M7 based MCUs
  • Fixed issue with notification of missing dependencies when Add/Remove Component used with SDK v2.4 packages
  • Improved options to handle part selection when project importing in cases where associated SDK is not installed
  • Fixed issue which could prevent a renamed project from being debugged in some circumstances
  • Resolved various issues with user interface of GUI Flash Tool
  • Resolved issue with workspace preferences when trying to configure the Debug perspective to be used for debugging projects (instead of the default Develop perspective)
  • Improved reliability of LinkServer debug sessions via enhancements to the way the IDE connects to the server process, as well as enhancements in the server itself
  • Improved the IDE's display of the LinkServer "RedlinkServer" console
  • Fixed issue with LinkServer "Disconnect behavior" always using "cont", even when configured to use another disconnect option
  • Option to terminate debug session added to IDE's LinkServer error dialog
  • Fixed issue with handling of number formats for entries in Global Variables view
  • Live Global Variable graphing no longer inserts spurious zero entry when target paused
  • Fixed issue with enumerated bitfield handling in the Peripheral Register viewer
  • Fixed issue with display of PriMask, BasePri, FaultMask and Control special registers in Registers view for LinkServer debug sessions. This change also now allows these registers to be edited
  • Fixed issue with LinkServer erroneously setting VTOR in some circumstances after programming flash
  • Fixed issue with zoom function on SWO Interrupt Trace view
  • Fixed issue with Instruction Trace view, which could prevent profile information being displayed in source and disassembly views in some circumstances
  • Fixed issue with Instruction Trace Config view, which prevented a modified configuration being saved
  • Preliminary LinkServer SPI flash drivers that self-configure using JEDEC SFDP information read from the device are now included for i.MX RT1020 (QSPI) and RT1050 (QSPI and Hyperflash)
  • Example device specific flash driver projects provided for i.MX RT1020 and RT1050. These can be used as a starting point for writing flash drivers for custom boards fitted with flash devices that do not support SFDP information
  • Updated FreeRTOS TAD plugin to v1.0.6
    • Fixed issues with Pause button
    • Added more verbose log for determining heap type
    • Removed problematic heap identification from available variables
  • Fixed issue which prevented the P&E Micro plugin updating from the P&E update server
  • Upgraded to a later version of the P&E Micro plugin (v3.5.6)
  • Upgraded to a later version of the SEGGER software (v6.32h)