MCUXpresso Config Tools v4 Now Available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Config Tools v4 Now Available

petrstruzka
NXP Employee
NXP Employee
1 0 2,855

We are pleased to announce that MCUXpresso Config Tools v4 are now available.

 

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

Features:

  • Available as Web and Desktop application
  • Kinetis SDK v2 support
  • Multicore support
  • Localized for English and Simplified Chinese
  • Mostly Connected: On-Demand device data download
  • Integrates with any compiler and IDE

 

V4_Pins_Tool.png

 

 

Currently there are the following tools available: 

V4_ico_peripherals.pngV4_ico_pins.pngV4_ico_clocks.pngV4_ico_cloner.png

  • Peripherals
  • Pins                  
  • Clocks
  • Project cloner

 

To download the installer for all platforms, please login to our download site via: 

 

Please refer to MCUXpresso Config Tools documentation for installation and quick start guides.

 

For online version, login into MCUXpresso site:

 

Overview of Changes - version 4

  • Peripherals Tool added

  • Project Generator replaced by Project Cloner

  • Added ability to import configuration from existing MEX file (for selected tools)

  • If the MEX file is stored within toolchain project, the tool reports missing SDK component in that project, that are required by the tool

  • Open configuration command verifies that the configuration matches with sources detected from toolchain project

  • Added common Functions group toolbar across all tools

  • Added option to not generate YAML

  • Pins tool: multiselect in Routed pins view supported

  • Syntax coloring supported in Sources view

  • Export sources wizard simplified

  • Several bug fixed and performance improved

  • Quick start guide added

 

Community

MCUXpresso Config Tools