NXPモデルベース・デザイン・ツールナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Model-Based Design Tools Knowledge Base

ディスカッション

ソート順:
General Tip of the day Tip of the day  Model Reference Model referencing in i.MX RT Toolbox  Peripherals FLEXCAN How to set i.MX RT FlexCAN receive message buffer Mask for range of IDs ?   LPI2C How to use LPI2C in transfer mode in i.MX RT  LPUART Questions about i.MX RT LPUART driver  Apps
記事全体を表示
  Product Release Announcement Automotive Embedded Systems NXP Model-Based Design Toolbox for S32M2 – version 1.1.0   The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32M2 version 1.1.0. This release supports automatic code generation for S32M2 peripherals and applications prototyping from MATLAB/Simulink for NXP S32M2 Automotive Microprocessors. This product adds support for S32M41, S32M242, S32M43, S32M244, S32M274, S32M276 MCUs and part of their peripherals, based on RTD MCAL components (ADC, AE, DIO, CAN, Can_Trcv, DPGA, GDU, GPT, LIN, LIN_Trcv, MCL, PWM, MCL, MCU, PORT, QDEC, SPI, UART). In this release, we have also added support for FreeMASTER, AMMCLib, and MATLAB support for the latest versions. The product comes with over 85 examples, covering all supported peripherals, and Simulink simulation modes Software-in-the-Loop, Processor-in-the-Loop, and External Mode. Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=6481361 Technical Support: NXP Model-Based Design Toolbox for S32M2 issues will be tracked through the NXP Model-Based Design Tools Community space. Release Content: Automatic C code generation from MATLAB® & Simulink® for NXP S32M2 derivatives: S32M241 S32M242 S32M243 S32M244 S32M274 S32M276 Support for the following peripherals (MCAL components): ADC AE CAN CAN_Trcv DIO DPGA GDU GPT ISR LIN LIN_Trcv MCL MCU MEMORY PROFILER PWM PORT QDEC SPI UART Profiler in PIL mode Provides 2 modes of operation Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tool or EB Tresos to configure peripherals/pins/clocks Provides Motor Control examples MBDT for S332M2 1.1.0 provides examples for PMSM sensorless, open loop and closed-loop hall sensors motor control applications, supporting S32 Configuration Tools. Each of them has a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. Integrates the Automotive Math and Motor Control Library version 1.1.38 All functions in the Automotive Math and Motor Control Functions Library v1.1.38 are supported as blocks for simulation and embedded target code generation. Integration with FreeMASTER MBDT for S332M2 1.1.0 delivers several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications. Support for Custom Default Project MBDT for S332M2 1.1.0 provides support for users to create their own custom default project. This could be very useful when having a custom board design – the configuration for it needing to be created only once. After that configuration is saved as a custom default project, it can be used for other models that are developed. Support for custom board initialization MBDT for S332M2 1.1.0 generates the components’ peripherals initialization function calls as configured in the Board Initialization window, which can be customized to each Simulink model. This feature allows users to set a custom order for the components initialization, the insertion of the Custom code sequences, or share the custom initialization with multiple Simulink models via the Export and Import functionality. Integration with S32 Config Tools version v1.7 Integration with S32 Design Studio MBDT for S332M2 1.1.0 automatically generates the <model_name>_Config folder, next to the Simulink model location, providing user the opportunity to easily import the generated code from Simulink into S32 Design Studio. Each time the code is generated, the  <model_name>_Config folder is updated with the new changes. Toolbox also provides a mechanism to launch an S32 Design Studio instance, with the imported generated code project in the Project Explorer tab from S32DS. Simulation modes       Toolbox provides support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode      Support for application execution profiling Custom Linker File and Startup Code Users can choose to use custom files for this process, from the Build Options group which can be found in the Target Hardware Resources, as illustrated in the image below. Examples for every peripheral/function supported       We have added over 60 examples, including: CDD Blocks (Ae, Dpga, Gdu, Mcl, Qdec) Communication (Can, Lin, Spi, Uart) AMMCLib IO Blocks (Adc, Dio, Pwm) ISR Blocks (Hardware Interrupt Handler) MCAL Blocks (Gpt) Utility Blocks (FreeMASTER, Memory, Profiler, Registers) Software-in-the-Loop / Processor-in-the-Loop / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached. MATLAB® Integration Support for MATLAB® versions R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b   The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32M2 MCUs and evaluation board solutions out-of-the-box with:   Target Audience This release (MBDT for S32M2 1.1.0) is intended for technology demonstration, evaluation purposes, and prototyping of S32M2 MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt DEMO Motor Control Rapid Prototyping on NXPs S32M2 with MathWorks and the Model-Based Design Toolbox This training shows how to design and develop motor control algorithms with Simulink® (MathWorks) and the Model-Based Design Toolbox for S32M2. Presentation introduces NXP’s S32M2 family, an integrated solution for 12V Motor Control and show how to access and configure the MCU peripherals making the Simulink® model hardware-aware and ready to generate, build and deploy the application on the target. The FreeMASTER software tool is used to control and monitor the algorithms running on the S32M2. First application focuses on a simple scalar control (also known as open-loop control or Volts per Hertz control) algorithm for a permanent magnet synchronous motor (PMSM). Second application shows how MATLAB and Simulink works together with the MBDT for S32M2 focusing on a workflow of implementing a predictive maintenance motor control application. Toolbox is used to acquire data from an accelerometer mounted on the motor. The motor is spinning at various speeds, and the vibrations are monitored using FreeMASTER. Data is transferred to MATLAB, where is preprocessed and a Support Vector Machine is trained. Then the resulted classifier is transferred to Simulink where together with the Model-Based Design Toolbox for S32M2 code is generated and deployed on the MCU. For more details about the demo mentioned above, please check this webinar a full demo description.        
記事全体を表示
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.3.0 EAR   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.3.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K311, S32K312, S32K314, S32K322, S32K324, S32K341, S32K342, S32K344, S32K358 and S32K396 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A and MC33772C battery cell controllers (& MC33665PHY). In this release, we have also updated S32 Configuration Tools, RTD, AMMCLib, and MATLAB support for the latest versions. The product comes with over 115 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13957417   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K311 S32K312 S32K314 S32K322 S32K324 S32K341 S32K342 S32K344 S32K358 S32K396   Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A and MC33772C battery cell controllers & MC33665PHY The toolbox provides support for the MC33775A, MC33772C, and MC33665. The MC33775A and MC33772C are lithium-ion battery cell controller ICs designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33665 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high-speed isolated communication network. The ready-to-run examples provided with the MBDT for S32K3 show how to communicate between the S32K344 and the MC33775A and MC33772C via the MC33665 transceiver. For the MC33775A, the examples show how to configure the battery cell controller to perform Primary and Secondary chains conversion, and read the cell voltages conversion results from the MC33775A, while for the MC33772C the examples show how to configure the Battery cell controller to read current. All the converted values are displayed to the user over the FreeMaster application.       Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.       Support for component restore to default settings The toolbox allows users to restore the configuration of a component (for models which use the EB Tresos configuration tool) to the settings corresponding to the Default Configuration Template the model uses. This allows reverting changes (if made) to the default values.   Support for AUTOSAR blockset (SW-C deployment) New RTD version supported  (v3.0.0 CD04) – only for S32K311, S32K358 and S32K396 New S32 Configuration Tools version supported (v1.6) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.31: All functions in the Automotive Math and Motor Control Functions Library v1.1.31 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b   S32Design Studio Integration We provide a simple mechanism for the users to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.     Board initialization: The Model-Based Design Toolbox for S32K3xx generates the component’s peripherals initialization function calls as configured in the Board Initialization window. The toolbox provides a default configuration including function calls for initializing the clocks, followed by pins and a custom order for the rest of the peripherals which have been configured in the project associated to the model.     Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 115 examples, including: Battery Management Systems examples Motor control applications (including eTPU example on S32K396) Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.3.0 is fully integrated with MATLAB® environment in terms of installation:         Target Audience This release (1.3.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt                
記事全体を表示
This page summarizes all Model-Based Design Toolbox tutorials and articles related to DSC MCUs Product Family.
記事全体を表示
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.0.0 RTM       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.0.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K344 MCU and part of its peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, GPT). It also adds support for FreeMASTER, AMMCLib, and Simulink simulation modes – Software-in-Loop, Processor-in-Loop, and External mode. Moreover, this release adds the option to configure everything (pins/peripherals/clock) via an external configuration tool - S32 Configuration Tools or EB Tresos. The product comes with over 70 examples, covering everything that is supported, including a motor control application demo. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=12747097 Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K344 Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI GPT DIO Support for profiling execution times Support for register R\W and memory R\W operations Provides 2 modes of operation: Basic User Mode – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced User Mode – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.24 for: All functions in the Automotive Math and Motor Control Functions Library v1.1.24 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a S32Design Studio Integration We added a simple mechanism to provide users the opportunity to export the generated code from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project, as well as for debugging purposes.   Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode   Examples for every peripheral/function supported: We have added over 70 new examples, including: Motor control application Communication (SPI, CAN) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.0.0 is fully integrated with MATLAB® environment in terms of installation: Target Audience This release (1.0.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.    Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt    
記事全体を表示
Introduction This article is going to show how to use the IMXRT117X board in co-simulation mode to run a Deep Learning application of facial recognition. Given that a development board has limited resources, the deployment of a Deep Learning application should be done as efficiently as possible. For now, since the latest version of Matlab (2021a) does not offer support for CNN optimization for Arm Cortex-M processors, we will restrict to developing an application in co-simulation mode. That means that while the data will be provided by the target board, the actual processing will take place in a Matlab environment. By running in co-simulation mode, we will exploit both hardware and the Matlab software capabilities.  The goal of this article is for the user to be able to: use a pre-trained CNN model from Matlab; use the MBDT IMXRT Board Object for co-simulation; develop a standard facial recognition application; Hardware overview For the development of this application, the i.MX RT1170 Evaluation board was used with a MIMXRT1176 CPU, and the attached ON Semiconductor OV5640 camera. Additionally, the RK055AHD091 LCD panel can be used to visualize the frames from the camera. The i.MX RT1170 EVK provides a high-performance solution in a highly integrated board. It consists of a 6-layer PCB with through hole design for better EMC performance at a low cost, and it includes key components and interfaces. Some of the i.MX RT1170 EVK main features are: MIPI camera sensor connector and MIPI LCD connector JTAG connector and On-board DAP-Link debugger Connectivity: 2x Micro-USB OTG connectors, Ethernet (10/100/1000M) connector, Ethernet (10/100M) connector, SIM card slot, CAN transceivers 5V Power Supply connector For a more comprehensive view and a more detailed description regarding hardware specifications and user guides, please check the documentation here. For this example, we are going to make use of the following peripherals and components hence make sure you have all of them available and you are familiar with their intended scope: ON Semiconductor OV5640 camera used for capturing the frames from the board; A CAT-5 ethernet cable will be used for getting video frames from the IMXRT on-board camera to be processed in MATLAB; Mini/micro USB cable for downloading the executable on the target; (Optional, if LCD is used) 5V power supply Software overview Software delivered by MathWorks: MATLAB (version 2021a) (we assume you have already installed and configure this). As a hint, please make sure the MATLAB is installed in a path with empty spaces; MATLAB Embedded Coder is the key component that allows us to generate the C code that will be cross-compiled to be executed on the target; Deep Learning Toolbox allows us to use pre-trained networks or re-train and re-purpose them for other scenarios; Image Processing Toolbox for preprocessing the images before training the network; Computer Vision Toolbox for performing face detection using the Viola-Jones algorithm; Software delivered by NXP: NXP MBDT IMXRT Toolbox as IMXRT embedded target support and plug-in for MATLAB environment to allow code generation and deployment. Make sure you install this toolbox in MATLAB 2021a. Deep Learning – Facial recognition Facial recognition is the process of verifying a person’s identity through their facial features in order to grant access to a service, application, or system. Recognition needs to be performed in 2 steps: 1) face detection – so identifying and isolating the face area from an image and 2) face recognition – analyzing the features of the image and classifying them. In this example, face detection is performed with the CascadeObjectDetector, from the Matlab Computer Vision Toolbox, which is based on the Viola-Jones algorithm, and face recognition will be performed with AlexNet, a pre-trained neural network specialized for object classification. source: https://test.neurohive.io/en/popular-networks/alexnet-imagenet-classification-with-deep-convolutional-neural-networks/ 1.Datasets In order to train the network for our application, custom datasets will need to be generated containing the faces of the people we want to recognize. A challenge that arises regarding the dataset are the changes that occur to a person’s appearance: during the day the mood of a person can change, which may affect their facial expressions; also, the lighting of the room can affect the features, by enhancing or diminishing them; nevertheless, the appearance of a person might vary depending on make-up, hairstyle, accessories, facial hair, etc. Thus, this is something that needs to be taken into consideration when creating the dataset used in training. A recommendation for better performance would be to take samples of a person's appearance multiple times during the day and in different lighting conditions. Another challenge is dealing with the category of unknown people since it is impossible to have and use a picture of every unknown person. A possible approach is to use a threshold value for classifying the pictures so that a person is accepted as “known” only over a certain probability.  Another solution would be to create an additional dataset for the “Unknown” category, which should contain various faces of different people. This way the model should be able to generalize and differentiate between known and unknown people. One of the datasets that can be used for this purpose is the Flickr-Faces-HQ Dataset (FFHQ) which contains over 70,000 images with a high variety in terms of ethnicity, age, emotions, and background. For this example, 6 classes were used, 5 of them representing known people and 1 for unknown people. In order to generate a dataset using the attached OV5640 camera, the Matlab client will connect to the Board Object on the target, it will request frames from the camera and it will save them as BMP files. %% Establish communication with the target board board_imxrt = nxpmbdt.boardImxrt('162.168.0.102', 'Video', 'GET'); %% Request frames from the camera and save them as bmp images count = 0; while (1) % Camera snapshot img = board_imxrt.step(); imwrite(img, [num2char(count) '.bmp']) end The next step is to extract the face area from an image and resize it to 227x227x3 so that it can be given as input to AlexNet. For that, we can create a directory with all the images that we want to train/test the network with and run the following script, which will perform face detection, then crop and resize the images to the desired dimensions. All the scripts and code snippets presented are also included in the attached archive. % Create Face Detector Object faceDetector = vision.CascadeObjectDetector; inputFolder = 'datastorage/to_process'; outputFolder = 'datastorage/processed/'; pictures = dir(inputFolder); for j = 3 : length(pictures) imgName = pictures(j).name; img = imread([inputFolder '/' imgName]); % Perform face detection bboxes = step(faceDetector, img); if(sum(sum(bboxes)) ~= 0) detectedFace = imcrop(img, bboxes(1, :)); % Resize image to fit AlexNet requirements detectedFace = imresize(detectedFace, [227 227]); imwrite(detectedFace, [outputFolder imgName]); end end       2.Training the network For training the network, we need to modify the output layer of the AlexNet network to match the number of classes we use, in this example 6. To improve the results for the case where we might not have enough input data, we can augment the images, and for that, we use the imageDataAugmenter from Matlab, where we set the images to be flipped horizontally and/or vertically, and rotated with a random angle between -90 and 90 degrees. This will help the model to avoid overfitting and generalize better. allImages = imageDatastore('datastorage', 'IncludeSubfolders', true,... 'LabelSource','foldernames'); % Split into train and validation sets [imgSetTrain, imgSetTest] = splitEachLabel(allImages, 0.7, 'randomized'); augmenter = imageDataAugmenter('RandXReflection', true,... 'RandYReflection', true,... 'RandRotation', [-90 90]); augimds_train = augmentedImageDatastore([227 227], imgSetTrain,... 'DataAugmentation', augmenter); augimds_test = augmentedImageDatastore([227 227], imgSetTest,... 'DataAugmentation', augmenter); Set the training options, these can be configured by the user as they wish, for this example, we have used a learning rate of 0.001 and batch size of 64, and have run the model for 7 epochs. opts = trainingOptions('sgdm', 'InitialLearnRate', 0.001,... 'Shuffle', 'every-epoch', ... 'MaxEpochs', 7, 'MiniBatchSize', 64,... 'ValidationData', augimds_test, ... 'Plots', 'training-progress'); trained = trainNetwork(augimds_train, layers, opts); save('trained_50_50_ep7_6classes', 'trained'); Save the trained network into a .mat file. It will be used for classifying the frames received from the camera. 3.Setup For the installation and usage of the MBDT IMXRT Toolbox please refer to this article. Running in co-simulation mode means that the target board is able to communicate with the host (in this case, Matlab) through the TCP/IP protocol, thus exploiting both hardware and Matlab software capabilities. The logic of the application is presented in the following figure: the attached camera will send the captured frames to the computer through an Ethernet connection; there, the frame will be processed using a Matlab script, which will perform Face detection and be further sent to the AlexNet trained classifier, which will return a label and the probability of that label being correct. Then, based on whether the person was recognized or not, a signal will be sent to the IMXRT board to toggle the USER LED. In order to create the executable that will act as the server part of our application, we will create a new Simulink model containing the IMXRT Board Object. For this example, the Board Object is sufficient for creating the co-simulation environment and running the application, for it makes use of both Camera and LWIP functionalities: The next step would be to configure the Board Object in order to be able to communicate with the host: open the Block Parameters window and input the IP address and port number you want to use. In the case of the server, it does not matter whether it is configured in SEND or GET mode, because it will wait for commands from the client. Then the model’s Ethernet parameters need to be configured. Open the Configuration Parameters window from Simulink, select Hardware Implementation from the left menu and then go to the Ethernet tab: here insert the values of the board IP address, subnet mask, and the gateway address.   Connect the board through USB to the computer. Go to the Download tab and select the drive you want to download the executable to. More information about this process is presented here. Also, please make sure that you have selected the NXP MIMXRT117Xxxxxx Hardware Board. The selection of the MIMXRT117X Hardware Board should copy the default ConfigTool MEX file which you can modify, but you can also create or use another MEX file as long as it has the name <model_name>_<core>Config.mex. In the MEX file are configured the peripherals and pins settings, in this case the Camera peripheral and the GPIO User LED. For better performance, we recommend using a low-resolution for the Camera. Build the model and the generated executable will be copied on the target board. Restart the board. Next step is to connect to the target board from Matlab and start receiving frames from the attached camera. For this, we will use a Matlab script that will create a board object configured to request frames from the target. The nxpmbdt.boardImxrt object is the same type as the one used in the previous Simulink model: here we can use it as a function call in a script, so we need to configure it accordingly. For information about how to use the Board Object, use the following command:  The Matlab script that will run in co-simulation and will connect to the target board: load trained_50_50_ep7_6classes.mat trained; faceDetector = vision.CascadeObjectDetector; board_imxrt = nxpmbdt.boardImxrt('162.168.0.102', ... 'Video', 'GET'); while (1) img = board_imxrt.step(); bboxes = step(faceDetector,uint8(img)); if (sum(sum(bboxes)) ~= 0) es = imcrop(img, bboxes(1,:)); es = imresize(es, [227 227]); [label, ~] = classify(trained, es); if ~strcmp(char(label), 'Unknown') board_imxrt.led_on(); else board_imxrt.led_off(); end else board_imxrt.led_off(); end end When running simulation mode from a Matlab script, please make sure that the configuration structure (the script mscripts\target\imxrt_code_gen_config) is configured accordingly with the desired hardware. After the application has received the camera frame from the board, it can start the preprocessing required for classification. We create a face detector object using the CascadeObjectDetector, to which we will input the camera frame and we receive in exchange the margins of the box where it detected a face. In the case a face was detected, we crop the image and resize it to 227x227x3, which is the size the AlexNet network requires, and we classify the image using the loaded model. The USER LED on the board will be switched on if the person was identified. The script also provides a Matlab UI Figure for better visualization.   Conclusions The NXP MBDT Toolbox provides a solution for developing Computer Vision applications targeted for Arm Cortex-M processors. This aims to be a temporary approach until the Matlab support required for generating CNN optimized C code is added.
記事全体を表示
Product Release Announcement EDGE PROCESSING  NXP Model-Based Design Toolbox for i.MX RT Crossover MCUs – version 1.2.0     The Edge Processing Tools Team at NXP Semiconductors is pleased to announce the release of the Model-Based Design Toolbox for i.MX RT 1xxx Series version 1.2.0. This release supports automatic code generation for peripherals and applications prototyping from MATLAB/Simulink for NXP’s i.MX RT 117x, 106x & 101x Series of crossover MCUs.   NXP Download Location https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   MATHWORKS Download Location https://www.mathworks.com/matlabcentral/fileexchange/81051-nxp-support-package-imxrt1xxx   Version 1.2.0 Release Content Automatic C code generation based on MCUXpresso SDK 2.9.1/2.9.2 drivers and MCUXpresso Configuration Tools 9.0 initializations from MATLAB®/Simulink® for: i.MX RT 1176: MIMXRT1176DVMAA,MIMXRT1176AVM8A,MIMXRT1176CVM8A i.MX RT 1175: MIMXRT1175DVMAA,MIMXRT1175AVM8A,MIMXRT1175CVM8A i.MX RT 1173: MIMXRT1173CVM8A i.MX RT 1172: MIMXRT1172DVMAA,MIMXRT1172AVM8A,MIMXRT1172CVM8A i.MX RT 1171: MIMXRT1171DVMAA,MIMXRT1171AVM8A,MIMXRT1171CVM8A i.MX RT 1061: MIMXRT1061CVJ5A,MIMXRT1061CVL5A,MIMXRT1061DVJ6A,MIMXRT1061DVL6A i.MX RT 1062: MIMXRT1062CVJ5A,MIMXRT1062CVL5A,MIMXRT1062DVJ6A,MIMXRT1062DVL6A i.MX RT 1064: MIMXRT1064CVJ5A,MIMXRT1064CVL5A,MIMXRT1064DVJ6A,MIMXRT1064DVL6A i.MX RT 1011: MIMXRT1011CAE4A,MIMXRT1011DAE5A   Multiple options for configuration of MCU packages, Build Toolchain and embedded Target Connections are available via Simulink Model Configuration UI       Multiple MCU peripherals and Drivers supported. The following subsystems highlighted in red as supported in Simulink environments in various forms: blocks, files, options i.MX RT 117x derivatives   i.MX RT 106x derivatives i.MX RT 101x derivatives     Basic and Advanced Simulink Block configuration modes via MCUXpresso Configuration Tools 9.0 UIs for Pins, Clocks, and Peripherals       MATLAB/Simulink versions 2019a – 2021b are supported for Design, Simulation, Code Generation, and Deployment of applications on i.MX RT 117x,106x & 101x Series. Other i.MX RT devices will be supported in future versions of the toolbox. Support for Software-in-Loop (SiL), Processor-in-Loop (PiL), and External Mode; RTCESL – Real-Time Control Embedded Software Motor Control and Power Conversion Libraries (limited support designed for Motor Control applications). A future update will enhance the number of functionalities supported by Simulink.     Simulink Example library with more than 190 models to showcase various functionalities:   Integrated PMSM Motor Control Sensor/Sensor-less application for both IMXRT1060-EVK and IMXRT1170-EVK:     Target Applications with MATLAB/Simulink This release of the Model-Based Design Toolbox can be used to design, build, and test applications from multiple domains: INDUSTRIAL AC Meters Motion Control Robotics HMI SMART CITY/HOME Video Surveillance Identification Appliances Speakers   AUTOMOTIVE HVAC ECU     Target Audience This release is intended for technology demonstration, evaluation purposes, and prototyping for i.MX RT 1xxx MCUs and their corresponding Evaluation Boards: EVK-MIMXRT1170 EVK-MIMXRT1060 EVK-MIMXRT1064 EVK-MIMXRT1010   Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt Technical by System Tools: https://web.microsoftstream.com/channel/618ab630-c8da-4fa8-ade8-5aa70a353124    
記事全体を表示
This page summarizes all Model-Based Design Toolbox topics related to the DSC Product Family. Model-Based Design Toolbox for DSC- Release Notes: Rev 1.0.0 - NXP Model-Based Design Toolbox for DSC MC56F8x MCUs - version 1.0.0 
記事全体を表示
This page summarizes all Model-Based Design Toolbox videos related to DSC MCUs Product Family.
記事全体を表示
Model-Based Design Toolbox supporting Kinetis-V Series. System modeling, simulations, automatic code generation, validation, and verification MATLAB & Simulink workflows are now available on the Kinetis V microcontrollers by reusing MCUXpresso ecosystem: MCUXpresso SDK MCUXpresso Configuration Tool MCUXpresso IDE,GCC
記事全体を表示
1. Introduction This article shows how to develop an application for the UCANS32K1SIC evaluation board in MATLAB ® and Simulink ® and NXP ® ’s Model-Based Design Toolbox.  1.1. General purpose The UCANS32K1SIC is a CAN signal improvement capability (SIC) evaluation board designed for both automotive (ADAS, Body Control Units etc.) and industrial applications (Building Control, Servos, Mobile Robotic, etc.) In total, there are three UCANS32K1 evaluation boards: UCANS32K146-01 UCANS32K1SCT UCANS32K1SIC In this article, we choose to focus only on one of them, the UCANS32K1SIC evaluation board. The UCANS32K1SIC provides two CAN SIC interfaces and is based on the S32K146 (32-bit Arm ®  Cortex ® -M4) from the S32K microcontroller family. Also, the UCANS32K1SIC features EdgeLock ®  SE050 secure element for authentication and encryption development. For complete details, please access the following link 1.2. Block Diagram     2. The UCANS32K1SIC application example model The UCANS32K1SIC application example proposed in this article (ucans32k1sic_mbd_4_3_0) implements the following actions: Controls the RGB LED (GPO) Reads the Switch state  (GPI) Displays  messages on the LCD screen (“Red Led On”, “Green Led On”, “Blue Led On”) using the I 2 C communication protocol Adds FreeMASTER communication via UART protocol Configures  both instances of the CAN communication protocol (CAN0 and CAN1) and sends/receives messages 2.1. Prerequisite Software For the development of this application, the following software is required: MATLAB ® and Simulink ® (minimum 2020a) Stateflow ® MATLAB Coder ™ Simulink Coder™ Embedded Coder ® Support Package for ARM Cortex-M Processors Model-Based Design Toolbox for S32K1xx 4.3.0 FreeMASTER Run-Time Debugging Tool 3.2 2.2. Prerequisite Hardware For the development of this application, the following hardware is required: UCANS32K1SIC evaluation board DCD-LZ-ADAPT debug adapter with cable, which provides breakout connectors for SWD/JTAG Debugger and FTDI USB-UART CAN Bus Terminator (DRONE-CAN-TERM) with MicroUSB cable CAN cable terminated on both ends OLED Display 128x64 pixels JLink Debug Probe (or any other compatible SWD probe) IXXAT USB-to-CAN V2 (or any other canAnalyser )   3. Simulink model implementation and blocks configuration After the NXP Model-Based Design Toolbox for S32K1xx is installed, the next step is to open the library and drag and drop the necessary blocks. The MCU configuration with MBD_S32K1xx_Config_Implementation block   The first step is to add the MBD_S32K1xx_Config_Information into our Simulink model. This action makes the model aware that it will generate code for the S32K1 microcontroller. Once opening the block, the user needs to choose the processor family inside the MCU tab. For this particular board, the processor is S32K146. Then the system clock frequency (MHz) must also be specified: Clock Frequency Value (80 MHz) External Crystal clock - 8 MHz (check the schematics or other materials)     In the Target Connection tab, the following settings are required: The download interface JTAG and SEGGER JLink software. In our case, the kit comes with the SEGGER JLink so we are selecting this one. In case the JLink software is installed at a different location than the default one, the correct path shall be indicated in the “SEGGER JLink installation path” field.       3.1. Reads the Switch state (GPI) In this application, each push of the button selects which color of the RGB LED is lighten up. So, to be able to control that, the state of the button needs to be read. A variable named “counter” stores the values corresponding to each state (0-RED, 1-GREEN, 2-BLUE). The pin corresponding to the SW button reading must be configured (using the schematic for the UCANS32K1SIC evaluation board).                   With each execution of the main step in the model, the GPI Read block triggers the subsystem where the states of the LED are changed.   3.2. Controls the RGB LED (GPO) When the counter is incremented, the LED changes its state (RED-GREEN-BLUE). This is implemented using the GPO Write blocks. The pins corresponding to each LED color must be configured according to the schematic.   After identifying each pin, they must be set in GPO write blocks as follows: To turn on one of the LEDs colors, set the pin to 0 and to turn it off set it to 1. This is because the LED anode is routed to 3V3 and the cathode is connected to the pin. When the application requires to turn on only one color, the others must be turned off, as might be seen in the screenshots below.                            3.3. Displays messages on the LCD screen (“Red Led On”, Green Led On”, “Blue Led On”) using the I 2 C communication protocol For this example, the OLED display used is 128 x 64 pixels. The LCD communicates with MCU via LPI2C0 (P4). So, in order to communicate with the OLED display, the LPI2C instance must be first configured. LPI2C0 block configuration: The pins corresponding to LPI2C0 instance must be configured according to the schematic.                   Next, the OLED block  needs to be configured as follows:   After the LPI2C0 and OLED blocks are configured, messages can be displayed on the LCD screen using the LCD Write String block. LCD Write String block configuration:           To display the other messages (GREEN LED ON and BLUE LED ON), the steps are the same. To clear the LCD screen and  display another message, the LCD Clear Screen must be used.       3.4. FreeMASTER project via UART protocol FreeMASTER is a user-friendly real-time debug monitor and data visualization tool that enables runtime configuration and tuning of embedded software applications. The FreeMASTER block configuration from NXP MBDT for the S32K1xx library uses the following communication interfaces: UART CAN In this example, we used the LPUART1 interface to send/receive messages from the FreeMASTER application. The pins corresponding to LPUART1 (they are routed to the P6 connector) instance must be configured according to the schematic.                              The RxD and TxD pins required routed in the schematics are PTC6 and PTC7. Another parameter that must be configured is the Baud Rate (maximum number of bits per second to be transferred). For this application, the Baud Rate is 115200 kbps.     3.5. Configures of both instances of the CAN communication protocol (CAN0 and CAN1) and sends/receives messages In this subchapter, the goal is to show how to receive/send messages on both CAN instances (CAN0 and CAN1). CAN0 instance First, CAN0 instance needs to be configured. For this action, the CAN configuration block is required. In the General tab, the following settings are: Module: 0 (for the CAN0 instance) Operational Mode: Normal mode Max number of MBs (1-32): 16 The RxD and TxD pins required are: PTE4 and PTE5 (according to the schematic)           In the Bit rate tab, the default Bitrate is 1000Kbit/s, but it depends on the case.     The next step is to choose the operating mode for the CAN transceiver (for UCANS32K1SIC, the CAN transceiver is TJA1463). The TJA1463 is a member of the TJA146x family of transceivers that provide an interface between a Controller Area Network (CAN) or CAN FD (Flexible Data rate) protocol controller and the physical two-wire CAN bus. Control pins STB_N and EN are used to select the operating mode. To simplify the application, the Normal mode has been selected to be set for the entire execution of the application. HIGH-level state on pin STB_N and pin EN selects Normal mode. According to the schematic, for the instance of CAN0, the corresponding pins for STB_N and EN are PTE11 and PTA10. For checking the correctness of the configuration of the settings and application, the transceiver outputs CAN_H and CAN_L are connected to CAN Analyzer, while messages are sent from the PC.           A numeric sequence with the ID 0x3FF is sent continuously while a  message received with ID 0x3FE toggles the PTD15 (Red LED) on each receive. To receive a CAN message asynchronous with the application, the CAN receive interrupt must be used. When a message is received, it triggers the subsystem Rx_0x3FE.     The fcan_s32l_receive block configuration is: Module: 0 Mode: Non-blocking Message Buffer: 14 ID: 3FF ID mask: FFFFFFFF         To send a message with the ID 0x3FF on CAN0, in the fcan_s32l_send block, the following settings are required: Module: 0 Mode: Blocking Timeout (ms): 50 Message Buffer: 15 ID: 3FF       CAN1 instance For the instance of CAN1, the steps are the same as above (the configuration of CAN0), but this time a numeric sequence with ID 0x2FF is sent continuously and a received message with ID 0x3FF will toggle the PTD16 (Green LED) on each receive. A CAN Analyzer is needed to analyze and collect data from the CAN bus and display them on the PC. To use both CAN instances on the same  CAN Analyzer, a hardware connection is needed between CAN0A and CAN1A (or any CAN0 with CAN1). This can be seen in the following diagram:     In this application, the  CAN Analyzer used is IXXAT USB-to-CAN V2 and the software interface is IXXAT canAnalyser3 Mini, but of course, any other CAN Analyzer can be used.       4. Model overview The application is structured in 3 categories as follows: Input (green area): Hardware-dependent blocks that read/receive values from peripherals Algorithm (blue area): Hardware-independent blocks that process the values received from Input blocks, runs the algorithm and controls the outputs. Output (pink area): Hardware-dependent blocks which receive the processed values from the Algorithm blocks.     After all the steps have been followed, the code can be generated, compiled, and deployed on the target. To do so, Go to Simulink -> Apps -> Embedded Coder then click on the Build button.     In the Diagnostic Viewer, the process can be analyzed if there is any error and if the download was successfully completed on the target as in the image below:       The following figure shows the setup:     Conclusion In this article we explained how to use the NXP Model-Based Design Toolbox for S32K1xx to handle the UCANS32K1SIC evaluation board. Access to all the board's peripherals was possible in Simulink by using the Model-Based Design Toolbox, an addon which connects the MATLAB and Simulink high level world with the NXP Tools and Hardware. In this application, we have shown how to control the RGB LED and read the state of the switch; how to display messages on the LCD screen and configure both instances of the CAN communication protocol for sending and receiving messages. We have also added the FreeMASTER communication to monitor or fine-tune the algorithms running on the UCANS32K1SIC board, while the model is available down below.   EdgeLock and NXP are trademarks of NXP B.V. All other product or service names are the property of their respective owners. © 2023 NXP B.V. Arm, Cortex are trademarks and/or registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere. The related technology may be protected by any or all of patents, copyrights, designs and trade secrets. All rights reserved. MATLAB, Simulink, Stateflow and Embedded Coder are registered trademarks and MATLAB Coder, Simulink Coder are trademarks of The MathWorks, Inc. See mathworks.com/trademarks for a list of additional trademarks.
記事全体を表示
        Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for HCP – version 1.1.0 RFP       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for HCP version 1.1.0. This release supports automatic code generation from MATLAB/Simulink for S32G2xx, S32S2xx, and S32R41 MPUs. This new product adds support for running Processor-in-Loop and Software-in-Loop simulation on S32R41 (ARM Cortex-A53).   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/product?child_plneID=683951   Technical Support: NXP Model-Based Design Toolbox for HCP issues will be tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32G2xx derivatives: S32G274A Automatic C code generation from MATLAB® for NXP S32S2xx derivatives: S32S247TV Automatic C code generation from MATLAB® for NXP S32R4x derivatives: S32R41 Supported Evaluation Boards GoldBox Development Platform (S32G-VNP-RDB2 Reference Design Board) GreenBox II Development Platform X-S32R41-EVB Development Board Support for MATLAB versions: R2020a R2020b R2021a R2021b Simulation mode: We provide support for Software-in-Loop (SIL) and Processor-in-Loop (PIL) simulation mode with code execution profiling:   Includes the HEV demo (S32G2xx, S32S2xx):   Includes the RADAR demo - MFSK Radar Range and Speed Estimation on Multiple Targets (S32R41), in collaboration with Gamax Laboratory Solutions Kft.:   Includes an Example library with 16 examples that cover: Software-in-Loop (SIL), Processor-in-Loop (PIL)   GUI to help you setup the toolbox and the evaluation board :     For more details, features and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32G2xx, S32S2xx, and S32R41  processors and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for HCP version 1.1.0 (RFP) is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.1.0 RFP) is intended for technology demonstration, evaluation purposes and prototyping S32G2xx, S32S2xx, and S32R41 and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt    
記事全体を表示
Check this short video to see the cool stuff you can do with an S32K144 DevKit. NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
General Installer and Setup Installation Troubleshooting  TPL Communication TPL communication troubleshooting TPL Communication with multiple BCCs FreeMASTER Configuration FreeMASTER not detected on the HVBMU Board  TD Handler TD Handler indexing 
記事全体を表示
This video explains how to use a three phase inverter to control the voltage applied on PMSM using various PWM Modulation techniques like: bipolar modulation unipolar modulation sinusoidal modulation space vector modulation third harmonic injection The goal of this video is to cover the topic of Space Vector Modulation and PWM generation that represents the basics for applications we are going to develop throughout https://community.nxp.com/thread/464336 .
記事全体を表示
1. INTRODUCTION    This article presents how to use NXP’s Model-Based Design Toolbox (MBDT) to implement an Air Quality Monitor that integrates multiple sensors, which will be configured to run on the 3S32K144 EVB.    The Model-Based Design Toolbox offers a solution for deploying complex applications on NXP hardware directly from Simulink. It incorporates hardware-optimized software, including drivers, libraries, and tools, allowing users to concentrate solely on algorithm development. The toolbox manages the hardware integration, ensuring the applications are hardware-aware. By integrating with the MathWorks ecosystem, the Model-Based Design Toolbox leverages the model-based design paradigm. This enables a programming process based on models, where users create logical diagrams using Simulink blocks for dedicated functions, eliminating the need to write C code for their designs.     This article aims to show how this tool can be used for designing and deploying on an S32K144 Evaluation board an air quality monitor application. Therefore, the steps meant to accomplish this are parted in the following sections:       II. General purpose – what is the aim of the application;       III. Application overview – how the application works and how the sensors are integrated;      IV. Hardware design – the description of the components used;       V. Software design – the execution flow of the application and the model implementation explained in detail;      VI. Conclusion – results of the application.    2. GENERAL PURPOSE    This application shows how easily an Air Quality Monitor can be implemented when using the MBD toolbox for S32K1xx, which helps the users simplify their job by providing the means to use a graphic and visual way to put their idea into use and generate the C code from it, which will be uploaded on the EVB.    3. APPLICATION OVERVIEW     The application displays in FreeMASTER the values of temperature, humidity, dust density, pressure, and the values of eCO2 and TVOC. Those values are read from the sensors connected to the EVB and computed using the algorithms from the libraries corresponding to each sensor, such as Adafruit’s libraries for BMP280 and CCS811, Sparkfun library for HTU21D and the GP2Y1010AU0F library, which are then adapted in Simulink logic. The application will be split into four subsystems, each covering a sensor and its algorithm.    BLOCK DIAGRAM                                                        Figure 1: Block Diagram     4. HARDWARE DESIGN     4.1. Hardware components   The required components for this application are:  S32K144 Evaluation Board  HTU21D, temperature and humidity sensor CCS811, eCO2 and TVOC sensor  BMP280, pressure sensor  GP2Y1010AU0F, dust density sensor        1) S32K144 Evaluation Board  The S32K144EVB is a low-cost evaluation and development board for general-purpose industrial and automotive applications. The board represents the main part of the application as it collects the data from the sensors and applies the algorithm to compute the values shown in FreeMASTER.  For more information about the board, access the following NXP page.      2) Temperature and humidity sensor HTU21D  The HTU21D is an easy-to-use, digital sensor for measuring humidity and temperature levels. It utilizes the I2C communication protocol, making it suitable for various applications, such as an Air Quality Monitor.     3) eCO2 and TVOC sensor CCS811  The CCS811 sensor precisely monitors indoor air quality, measuring TVOCs and carbon dioxide levels in real time. Using the I2C communication protocol, it is easily integrated into air quality monitor applications.     4) Pressure sensor BMP280  The BMP280 sensor accurately measures atmospheric pressure using the I2C communication protocol.     5) Dust density sensor GP2Y1010AU0F  The GP2Y1010AU0F sensor is utilized for the measurement of dust density with high precision. Utilizing an analog output mechanism, it delivers reliable data for comprehensive air quality assessments.    4.2. Electrical schematic    Apart from the components described above (HTU21D sensor, CCS811 sensor, BMP280 sensor and GP2Y1010AU0F sensor), a resistor and a capacitor will be needed.   The following electrical schematic is an example of how the sensors can be connected:                                                             Figure 2: Electrical schematic    5. SOFTWARE DESIGN    5.1. Prerequisite software  To be able to follow the next steps presented in this article, the following software will be necessary:  Matlab® and Simulink® (2021a or newer), including Stateflow ®, MATLAB® CoderTM, Simulink® CoderTM, Embedded Coder®  NXP Support Package S32K1xx    5.2. Model overview   The application uses the Simulink environment to implement the algorithms for computing the data read from the sensors connected to the S32K144 EVB. The model is organized into two big sections: initialization and sensors’ algorithms. For the sensors part, each sensor has its subsystem where the algorithm is implemented.                                                     Figure 3: Application’s model    5.3. INITIALIZATION  The initialization holds the blocks required for our model to work. On the first line, from left to right, the following can be found:        1) The Configuration block for S32K1xx processor family. The required settings of the processor configuration block are the default ones, except for the processor family and the download interface.                           Figure 4: Configuration block for S32K1xx family of processors        2) The LP2IC Configuration block. Here the functioning mode (master or slave) can be changed, and the pins used for communication can be chosen. This application has three sensors that use this communication protocol:  BMP280, whose address is 0x76  CCS811, whose address is 0x5A HTU21D, whose address is 0x40                                            Figure 5: Configuration block for LPI2C        3) The FreeMASTER configuration block. Here the communication interface, the baud rate, and long interrupt serial communication can be set. This component facilitates communication between the S32K144 EVB LPUART1 instance and the FreeMaster tool, via the microUSB serial port.                                Figure 6: Configuration block for FreeMASTER        4) The configuration block for ADC. The ADC converter number and the resolution mode can be selected from here.     Figure 7: Configuration block for ADC    On the second line, the data stores for the variables used in this project can be found. The data type and size for the data stores can be found in the following table:     VARIABLE NAMES  DATA TYPE  SIZE / DIMENSION  SENSOR  aux_temp  uint8  3  BMP280  aux_press  uint8  3  BMP280  BMP280_Temp  uint8  6  BMP280  BMP280_Press  uint8  18  BMP280  BMP280_T  uint16  1  BMP280  BMP280_T2  int16  2  BMP280  BMP280_P  uint16  1  BMP280  BMP280_P2  int16  8  BMP280  raw_press  int32  1  BMP280  raw_temp  int32  1  BMP280  Pressure  double  1  BMP280  buf  uint8  8  CCS811  TVOC  uint16  1  CCS811  eCO2  uint16  1  CCS811  temperature  double  1  HTU21D  humidity  double  1  HTU21D  hum_raw  uint16  1  HTU21D  temp_raw  uint16  1  HTU21D  humcomp  default  default  HTU21D  dustDensity  default  default  GP2Y1010AU0F    Figure 8: Variables    Note! It is important, for the variables to be visible in FreeMASTER, to go to Apps -> Embedded Coder -> Code Interface -> Default Code Mappings -> Data Stores and set all the variables to Volatile.    Figure 9: Embedded Coder selection    Figure 10: Default Code Mappings    5.4. ALGORITHM   The second part of the model consists of every sensor’s subsystem. In each subsystem, the necessary algorithm for computing the data is implemented.   Let’s look at every subsystem and algorithm.       5.4.1. BMP 280 Pressure sensor   For this sensor’s initialization, BMP280_Temp and BMP280_Press will  be used. Top down, five subsystems can be found: Global Initialization Sensor, Temp Calib, read16LE – temp, Press Calib, read16LE – press.     Figure 11: BMP280 subsystems    The purpose of the Global Initialization Sensor is to prepare the sensor for subsequent data reading. This involves transmitting specific data to the sensor using the LPI2C Master Transmit block. These data include values such as 0xF5 and 108, as well as 0xF4 and 111, which serve to configure and calibrate the sensor for upcoming tasks. Having multiple sensors connected using I2C communication protocol, the way the sensor can differentiate between them is by their address. Therefore, the data will be sent to the 0x76 address, which corresponds to the address of the pressure sensor.  Figure 12: Pressure sensor initialization    In Temp Calib subsystem, data is read from the temperature's memory location and placed into the BMP280_Temp data store mentioned earlier. The addresses from which data needs to be read are sequential, so reading begins from the 0x88 address and 6 bits of data are requested, resulting in reading from address 0x88 to address 0x8C inclusively.  Figure 13: I2C Master Multi Transfer    In read16LE – temp subsystem, the add operation is utilized to perform an OR bit operation for calibrating the data and placing it into the BMP280_T data store and the BMP280_T2. LE stands for Little Endian.    Figure 14: Temperature data calibration    For the Press Calib and read16LE – press subsystems, the same operations described previously are performed, but for a greater number of bits. After the initialization is completed, the Else subsystem is entered, where the computing takes place. An auxiliary temperature is computed, which is required for the pressure's formula. For this purpose, the data store named aux_temp will be used. Within this subsystem, there are 2 further subsystems: READ TEMP REGISTER and RAW TEMP.  In READ TEMP REGISTER, data is read from the 0xFA address using an LPI2C Master Multi Transfer, and 3 bits of data are transferred into the aforementioned aux_temp data store.  In RAW TEMP, the raw_temp necessary for the pressure calculation formula is computed.  Similar to the temperature calculation, the pressure calculation data is read from the 0xF7 address into the data store named aux_press, and then the raw_press required for the formula is computed.  For the actual computation of the pressure, an S-Function block with C code inside is utilized, where the algorithm found in the Adafruit Library for BMP280 is included. [1] [functions float Adafruit_BMP280::readTemperature() and float Adafruit_BMP280::readPressure()].  Figure 15: convertPressure S-Function       5.4.2. CCS811 TVOC & eCO2 sensor  For this sensor, during initialization, the same procedure as before is followed: specific data is sent to the sensor using the LPI2C Master Transmit to notify it of the upcoming data reading. Specifically, the predefined data 0xF4 and 0x01, 16 is now transmitted.   Figure 16: Initialization for eCO2 and TVOC sensor    In the Else subsystem, 8 bits of data are read and placed into the buf variable using the LPI2C Master Multi Transfer block. Subsequently, after the necessary data is retrieved from the sensor, the required values are computed, with their formulas sourced from the Adafruit Library for the CCS811 sensor [2]:  _eCO2 = ((uint16_t)buf[0] << 😎 | ((uint16_t)buf[1]);  _TVOC = ((uint16_t)buf[2] << 😎 | ((uint16_t)buf[3]);    Figure 17: Compute data for eCO2 and TVOC values       5.4.3. Humidity & Temperature subsystem  For this sensor, another library [3] will be utilized to obtain the necessary formulas and the algorithm. Initially, for both temperature and humidity readings, the LPI2C Master Multi Transfer block will be employed to retrieve the required values. Specifically, the command to trigger temperature readings is 227, and for humidity, it is 229. Each reading will consist of 3 bits, from which only the most significant bit and the least significant bit will be utilized for temperature and humidity, respectively.  For both of them, the raw values need to be computed. The formulas needed are:  For temperature:  uint16_t rawValue = ((uint16_t) msb << 😎 | (uint16_t) lsb;  temp_raw = rawValue & 0xFFFC;       2. For humidity:  uint16_t rawValue = ((uint16_t) msb << 😎 | (uint16_t) lsb;  hum_raw = rawValue & 0xFFFC;    The temperature is computed using the following formula:  Temperature = temp_raw * (175.72 / 65536.0) – 46.85;    Figure 18: Temperature computing    The humidity is computed using the following formula:  Humidity = (-6) + 125 * (hum_raw / 65536.0) + (25 – Temperature) * (-0.15);    Figure 19: Humidity computing    Figure 20: Temperature and humidity subsystem       5.4.4. Dust Pm2.5 subsystem  For this final sensor, an additional library [4] will be employed to implement our model-based design algorithm for measuring and computing the PM2.5 levels in our surroundings.   In this scenario, the GPIO Write block will be utilized to activate and deactivate the infrared LED on the sensor. Following activation, a 0.28ms delay will be introduced before employing the ADC to read the data, which will then be computed using the provided formula:  dustDensity = (170 * 5 / 1024 – 0.1) * Voltage      Figure 21: Formula applied for dust density    After applying the above-mentioned formula, another delay of 0.04ms will be used and then the LED will be turned off.      Figure 22: Dust Pm2.5 subsystem    5.5. FREEMASTER  To visualize the results from the application, a FreeMASTER project can be created. Once created, the .elf file of the built application can be added by navigating to Project -> Resource files -> "pack" directory setup -> MAP Files -> Default symbol file.  Variables can be added to the Variable Watch section. For this project, the most important ones are Pressure, eCO2, TVOC, humidity, temperature, and dustDensity.    Figure 23: Variable watch section    5.6. HARDWARE SETUP  A possible example for hardware setup is represented in the below picture:  Figure 24: Hardware setup    6. CONCLUSION    The application covers the steps of developing an air quality monitor that monitors how the pressure, TVOC, eCO2, humidity, temperature, and dust density evolve in a room, using the Model-Based Design Toolbox for S32K1 MCUs. It can be a good academic study for how to use the S32K1XX EVB and sensors using the MBDT and for how to adapt C code and use it in a graphic programming environment such as Simulink to simplify your work.      Bibliography:   [1] https://github.com/adafruit/Adafruit_BMP280_Library  [2] https://github.com/adafruit/Adafruit_CCS811  [3] https://github.com/sparkfun/SparkFun_HTU21D_Breakout_Arduino_Library  [4] https://github.com/mickey9801/GP2Y1010AU0F       NXP is a trademark of NXP B.V. All other product or service names are the property of their respective owners. © 2024 NXP B.V. MATLAB, Simulink, and Embedded Coder are registered trademarks of The MathWorks, Inc. See mathworks.com/trademarks for a list of additional trademarks.   
記事全体を表示
This video presents the system block diagram for BLDC speed closed loop control and how to map the application block diagram over the existing hardware. We discuss about: - What is a BLDC motor and how is made - How a BLDC motor works with electronic commutation - What is needed to construct a speed control loop - Mapping the SW and HW together NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
記事全体を表示
  Product Release Announcement Analog & Automotive Embedded Systems NXP Model-Based Design Toolbox for S32K3 – version 1.7.0     The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3 version 1.7.0. This release supports automatic code generation for S32K3 peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3 Automotive Microprocessors. This new product adds support for S32K310, S32K311, S32K312, S32K314, S32K322, S32K324, S32K328, S32K338, S32K341, S32K342, S32K344, S32K348, S32K358, S32K364, S32K366, S32K374, S32K376, S32K388, S32K394 and S32K396 MCUs, and part of their peripherals, based on RTD MCAL components (ADC, CAN, DIO, FEE, GPT, I2C, ICU, LIN, MEM, MCL, PWM, SPI, UART), and support for the GD3162 Gate Driver based on the S32K396 GD3162 Software. In this release, we have also updated the RTD, S32 Configuration Tools, AMMCLib, FreeMASTER, and MATLAB support for the latest versions. The product comes with over 180 examples, covering all the features and functionalities of the toolbox, including new demos for motor control applications.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=7608021   Technical Support: NXP Model-Based Design Toolbox for S32K3 issues will be tracked through the NXP Model-Based Design Tools Community space.   Release Content: Automatic C code generation from MATLAB® for NXP S32K3 derivatives: S32K310 S32K311 S32K312 S32K314 S32K322 S32K324 S32K328 S32K338 S32K341 S32K342 S32K344 S32K348 S32K358 S32K364 S32K366 S32K374    S32K376    S32K388    S32K394  S32K396   Support for the following peripheral components and functions: ADC CAN DIO eTPU FEE GD3162 GPT I2C ICU LIN MCL (including DMA support) MEM Memory read/write PWM Profiler Registers read/write SPI UART   New RTD version supported (6.0.0)   Integrates S32K396 GD3162 v2.0.2 The toolbox enables access to the GD3162 gate driver for S32K396 derivatives from Simulink models, by delivering a library block (Gd3162) that generates code on top of GD3162 components API.   New S32 Configuration Tools version supported (2024.R1.8)😎   Integration with EB tresos v29.0.0   Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB tresos to configure peripherals/pins/clocks   Default Configuration Project Templates targeting all the supported S32K3 derivatives The toolbox delivers default configuration projects, available in both S32 Configuration Tools and EB tresos, covering an initial enablement of the on-board peripherals, pins, and clocks, for all the supported S32K3 derivatives. The desired template, which represents the starting point for enabling the hardware configuration of the application, can be selected via a dropdown widget.   Support for creating and using Custom Project Templates The toolbox provides support to use and create custom project templates. This could be very useful when having a custom board design – offering the possibility to create the configuration for it only once. After it is saved as a custom project template, it can be used for every model that is being developed.   Such custom projects, addressing specific hardware designs are offered inside the current version of the toolbox to integrate the following EVBs: MCTPTX1AK324 S32K344-WB S32K396-BGA-DC1 MR-CANHUBK344, alongside a set of examples specifically created to target this hardware design and a series of articles (available on NXP Community) demonstrating how to use the toolbox features and functionalities for creating applications for custom boards.   The toolbox has been tested and validated on the official NXP Evaluation Boards     S32K31XEVB-Q100     S32K312EVB-Q172     XS32K3X2CVB-Q172     XS32K3X4EVB-Q257     XS32K3XXEVB-Q172     MR-CANHUBK344             S32K3X4EVB-T172      S32K344-WB        XS32K3X8CVB-Q172     S32K388EVB-Q289             XS32K396-BGA-DC     XS32K396-BGA-DC1   Integrates the Automotive Math and Motor Control Library release 1.1.41 All functions in the Automotive Math and Motor Control Functions Library v1.1.41 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   S32 Design Studio integration We provide the feature of importing the code generated from a Simulink model inside the S32 Design Studio IDE. This functionality can be useful if the model needs to be integrated into an already existing project or for debug purposes.   Simulation modes We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) including AUTOSAR SW-C deployment External mode   GD3162 Applications To demonstrate the integration and support of the GD3162 gate driver IC, we have included a reference Simulink application that configures six GD3162 devices in   a daisy-chain topology using SPI communication. The setup enables sequential initialization, configuration, and status monitoring of each GD3162 device using the S32K396 as a controller MCU.   Motor Control Applications The toolbox provides examples for 1-shunt and 2-shunt PMSM and BLDC motor control applications, supporting both S32 Configuration Tools and EB  tresos. Each of the examples provides a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. The toolbox also demonstrates the integration of the Motor Control Blockset in developing such applications.   For demonstrating the S32K3 eTPU Software integration, we have included a PMSM application where the FOC algorithm runs on the main CPU of the S32K396 MCU, while the analog sensing, software resolver, and PWM signals generation are offloaded to the eTPU co-processor.   The motor control applications were developed and validated on the MCSPTE1AK344 and MCSPTR2AK396 Motor Control kits.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b R2025a   Examples for every peripheral/function supported More than 180 examples showcasing: I/O Control Timers and scheduling Communication (CAN, I2C, LIN, SPI, UART) Memory handling Motor Control applications (BLDC and PMSM) AMMCLib FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3 MCUs and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for S32K3 version 1.7.0 is fully integrated with MATLAB® environment.   Target Audience: This release (1.7.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3 MCUs and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
記事全体を表示