NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
This video shows how to program the GPIO with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system.   We discuss about: - How to implement a simple program to read data from the GPIO - How to test in real time with FreeMaster - How to transform GPI pulses into a speed reference data that represents the rpm. - How to implement from scratch a Simulink model to cover the GPIO functionality NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video presents the hardware and software setup used for Motor Control Class. It shows: - MPC5744P DevKit main hardware features - MotorGD DevKit main hardware features - How to install the Model Based Design Toolbox for MPC5744P revision 2.0.0 - How to generate a license - How to setup a compiler toolchain using S32 Design Studio for Power Architecture - How to add the Model Based Design Toolbox for MPC5744P into the Simulink Standard Libraries - How to validate the software installation by generation C code for the first time NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
General Tip of the day Tip of the day  Licensing MBDT license missing error  Toolbox functionality Registers, Linkers not displaying options  Profiler/Execution S32k144 Simulation Time and Profiler  Peripherals How to put MCU into sleep? Apps Motor Control
View full article
1. Introduction   This article demonstrates how to control a 4-wire server fan based on temperature or user input, using the Model-Based Design Toolbox for S32K1 MCUs. The Model-Based Design Toolbox represents a solution which allows the complex applications deployment on NXP hardware directly from Simulink. By incorporating hardware optimized software, such as drivers, libraries, and tools, the Model-Based Design Toolbox allows the users to focus only on the algorithm development, while making such applications hardware-aware is handled by the toolbox. By the integration with the MathWorks ecosystem, the MBDT leverages the model-based design paradigm, thus enabling a programming process based on models - users to not need to write C code for implementing their designs, but create logical diagrams using Simulink blocks performing dedicated functions. In this article, we will demonstrate how this tool can be used for designing and deploying on an S32K146 Evaluation board a fan speed control application. Thus, the steps proposed for achieving this are described thorughout the article, in the following sections: II. Application overview – how the application works and the links between the components; III. Hardware design – the description of the components used and the electrical diagram; IV. Software design – the application execution flow and the model implementation explained in more detail; V. Conclusion – the results of the application.   2. Application overview   The application has 2 operating modes: automatic and manual. To switch between operating modes, we need to press the SW2 button on the S32K146 board. When starting, the application is in automatic operating mode (the RGB LED of the board lights up green): this means the fan adjusts its speed according to temperature. In manual mode (the RGB LED of the board lights up blue), the fan changes its speed depending on the value supplied by the potentiometer. The graphs and values of fan speed, acceleration, ambient temperature will be displayed in FreeMASTER. Block diagram   Figure 1: Block diagram   3. Hardware design   A. Hardware components The required hardware components are:  S32K146 Evaluation board  Thermistor NTC100K  4-wire PC fan   12V power supply AC-DC.   1) S32K146 Evaluation board The S32K146EVB serves as an affordable evaluation and development board designed for a wide range of industrial and automotive uses. The board is the “brain” of the application, as it collects data from various sensors (e.g.: temperature sensor) and uses the algorithm to regulate the actuators (e.g.: the BLDC motors found in fans).  For more information about the board, please read from here.   2) Thermistor NTC100K A thermistor is a resistor whose resistance is dependent on temperature. The temperature value is calculated using the Steinhart-Hart equation. The Steinhart-Hart coefficients A, B, C vary depending on the type and model of thermistor and the temperature range of interest. To find these coefficients, we use three values of resistance data for three known temperatures. For example, from NTC100K Thermistor Datasheet we get for the temperatures of 15℃, 25℃ and 45℃, corresponding resistance values of 156407 Ω, 100000 Ω and 43659 Ω. It results, according to the equation (2), that the coefficients have the following values:  So, the steps to determine the temperature are to get the thermistor resistance using a voltage divider converter along with an analog-to-digital converter (ADC) and calculate the temperature from the resistance.    3) 4-wire PC fan The fan has 4 pins, being used especially for processors with high power consumption. The simplest fan has 2 pins, one for power and one for ground. The 3-wire fan has an extra pin called “tachometer”, which indicates the speed of the fan (one/two impulses are received for each rotation). With 2-wire and 3-wire fans, the speed is controlled by increasing/decreasing the voltage on the power pin. Instead, the 4-wire fan has a control pin and uses PWM (Pulse Width Modulation) to control the speed.  Before using the fan, we must find out information such as the maximum speed, the number of impulses per rotation given by tachometer and the minimum operating speed if necessary. These things can be looked up in the fan’s datasheet or can be determined experimentally if we have an unknown fan, and we cannot find its datasheet.  The values of the fan used as an example in this article were determined experimentally and we got an approximate maximum speed of 300 rotations per second (18000 rpm), two impulses per rotation and a minimum operating speed of 80 rotations per second (4800 rpm).    4) 12V power supply AC-DC The power supply converts alternating current (AC) electrical energy into direct current (DC) electrical energy with an output voltage of 12 volts. In our application, it will supply the power for the fan.   B. Electrical schematic There are multiple hardware configurations for the fan speed control application. We will use, in addition to the hardware components mentioned above (fan, 12V power supply, thermistor), the potentiometer, the SW2 button and the RGB LED of the S32K146EVB.  We propose the following electrical schematic:  Figure 2: Electrical schematic Note! It is important that all components are connected to the same ground.   C. Hardware setup A possible hardware setup may look like in the following picture:  Figure 3: Hardware setup example   4. Software design   A. Prerequisite software To be able to follow the next steps in this article, the following software is necessary: MATLAB ®  and Simulink ®  (2021a or newer), including Stateflow ® , MATLAB ®  Coder TM , Simulink ®  Coder TM , Embedded Coder ® Model-Based Design Toolbox for S32K1xx 4.3.0   B. Flow chart The application execution flow is based on a state machine, according to the following diagram. Figure 4: State machine The architecture of the application is a closed-loop system, which uses a feedback signal to adjust the fan speed. The current fan speed and the fan acceleration update their values with each tachometer pulse. The difference between the reference speed (set using temperature or potentiometer) and the current speed, alias error signal, is the input to the closed-loop control system, such as a proportional-integral-derivative (PID) controller. The PID controller applies a correction based on proportional, integral, and derivative coefficients to a control function, in our case, it determines the PWM duty cycle to control the fan speed.  Figure 5: Application's model   C. Model Overview From top to bottom (Figure 5), we have 4 big sections:  Initialization Switching between operating modes The operating modes which set the reference speed The control algorithm. Let’s take each section to dive further into the details.    1) Initialization  Figure 6: Initialization section We have on the first line, from left to right, the Configuration block for S32K1xx processor family, the FreeMASTER Configuration Block and two ADC Configuration Blocks. On the second line, we have the pull-up resistance on the tachometer pin and two mapping functions from the temperature value and the ADC potentiometer value to the reference speed. Also, there are variables for current operating mode, temperature value, reference speed, current speed, duty cycle and some other auxiliary variables.  The required configurations of the processor configuration block are the default ones, except for the processor model and the download interface (Figure 7).  For the FreeMASTER configuration block, we set the communication interface (e.g.: LPUART1), the baud rate (e.g.: 19200) and long interrupt serial communication. This component provides an interface where relevant data such as current speed, ambient temperature and many others are displayed. In the ADC configurations blocks, used for reading temperature and potentiometer value, we select the ADC converter number and the resolution mode (e.g.: 10-bit conversion).   Figure 7: Configuration block for S32K1xx family of processors   2) Switching between operating modes We configure the pin PTC12 (SW2) to generate a falling edge interrupt on each button press, using the GPI ISR block. Figure 8: Switching mode section When an interrupt is generated, the value of the operation mode variable is toggled and the color of the LED corresponding to the operating mode lights up (automatic mode – green, manual mode – blue). It also enables/disables the PIT (Periodic Interrupt Timer) interrupt which triggers the ADC reading of the temperature sensor at each one second (Figure 10).  Figure 9: The function called when the interrupt is generated.  Figure 10: Enable/disable PIT interrupt for ADC temperature reading; RGB LED in Automatic & Manual mode   3) Operation modes  Figure 11: Operation modes section Depending on the operating mode, the reference speed is set by the temperature value or the ADC value of the potentiometer. a) Automatic mode In this mode, the PIT block is enabled, and the ADC value of the thermistor is read once per second. The resolution of the ADC is 10 bits. So, it can take values between 0 and 1023, which corresponds to voltage values between 0V and 5V. Let’s assume Vout is the output voltage on the pin PTB13. Also, according to the electrical schematic from Figure 2, we have a voltage divider: We can find out the value of thermistor resistance: And then, we can get the temperature value using the Steinhart-Hart equation (1).  Based on the temperature, we can map a value for reference speed. We can define for this mapping a linear function or whatever we need.  Figure 12: Automatic mode   b) Manual mode In manual mode, the ADC value of the potentiometer is read and mapped to reference speed.  Figure 13: Manual mode   4) The control algorithm  Figure 14: The control algorithm section In this section, the closed loop of the system is implemented using the PID (Proportional-Integral-Derivative) controller. We must tune the coefficients of the PID controller (Kp, Ki, Kd) to produce the optimal control function. There are several methods for tuning: manual, Ziegler-Nichols or using software specialized tools. For this application, the Ziegler-Nichols method was used, and, for fine adjustment, manual tunning was applied. After applying this method, we get the following values: KP = 0.003, KI = 0.003, KD = 0.001.  Figure 15: PID controller configuration With the PWM signal from the PID controller, we control the fan speed via the PWM pin, using the FTM PWM Config block. We configure the block as follows:  Figure 16: Parameters of FTM PWM Config block According to the electrical schematic (Figure 2), the pin used to control the fan speed is PTC1, which corresponds to FTM0_CH1. This means we need to configure the channel 1 from the module 0 of FTM (FlexTimer Module). To get the fan current speed, we need to know the period between two pulses from the tachometer. This can be determined using the FTM Input Capture block, which returns the timestamp in microseconds. Remember that there are two pulses per rotation. We measure the speed once every 10 milliseconds. So, the acceleration has the following value:  Figure 17: Calculation of fan speed and acceleration   D. FreeMASTER To visualize the results of the application, you can create a FreeMASTER project. Add the .elf file of the built application to Project – Resource files – “pack” directory setup – MAP Files – Default symbol file. You can add variables to the Variable Watch section, such as operation mode, current speed, reference speed, temperature (Figure 19). Also, you can create a graph, as in Figure 18, using the FreeMASTER oscilloscope with the current speed and reference speed. In the following figure, we can observe that the system is initially in automatic mode: temperature is about 28 Celsius degrees, which corresponds to an approximate reference speed of 110 rotations per seconds. Then, when SW2 button is pressed (at second 685 on the graph), the system goes into manual mode and the reference speed is set about 236 rotations per second, which is mapped according to the value read from the potentiometer. The current speed (red line) is tracking the reference speed imposed (green line).  Figure 18: Graphic with reference speed and current speed Also, we can track values such as operation mode - boolean value (0 for automatic mode and 1 for manual mode), temperature in Celsius degrees, reference speed and current speed measured in rotations per second, acceleration or the PWM duty cycle used for controlling the fan speed.  Figure 19: Variable watch section   5. Conclusion   In conclusion, the application consists in controlling the fan speed depending on the temperature or the potentiometer value, using the Model-Based Design Toolbox for S32K1 MCUs. It combines notions from systems theory, electronics, and embedded systems, representing an academic study on the use of fans for temperature control in different applications like servers, routers, switches, etc.   Useful links:   1. S32K146EVB:   https://www.nxp.com/document/guide/getting-started-with-the-s32k146-evaluation-board-for-general-purpose:NGS-S32K146EVB  2. NTC100K Thermistor: https://www.tme.eu/Document/f9d2f5e38227fc1c7d979e546ff51768/NTCM-100K-B3950.pdf  https://en.wikipedia.org/wiki/Steinhart%E2%80%93Hart_equation#Steinhart%E2%80%93Hart_coefficients  3. 4-wire fan:  https://www.electroschematics.com/4-wire-pc-fan/  https://www.nidec.com/en/product/search/category/B101/M111/S100/NCJ-V40S-E5-57/  4. PID coefficients:  https://control.com/textbook/closed-loop-control/p-i-and-d-responses-graphed/  https://en.wikipedia.org/wiki/Proportional%E2%80%93integral%E2%80%93derivative_controller    NXP is a trademark of NXP B.V. All other product or service names are the property of their respective owners. © 2024 NXP B.V. MATLAB, Simulink, and Embedded Coder are registered trademarks of The MathWorks, Inc. See mathworks.com/trademarks for a list of additional trademarks.  
View full article
This video shows: - how to download the Model Based Design Toolbox; - how to generate a license from your account; - how to setup the environment; - quick tour of the toolbox, supported functionalities and available examples;
View full article
This video discuss about how to mix together the ADC and GPIO models to obtain a common speed reference for the BLDC speed closed loop control system.   We discuss about: - How to use analog and digital inputs - How to create a variable that can be changed in real time via Freemaster - How to test the final application - Finalize the Speed Reference Block - Short Quiz NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we implement Simulink models for reading the hall sensors directly via GPIO or based on Hall transitions interrupts via eTimer Capture.   We discuss about: - How to build simple hall reading application using the available MBD Toolbox GPIO blocks  - How to enhance this simple model by adding interrupt service routines capabilities to read the hall sensors only when there is a transitions - How to count the number of hall transitions - How to validate the applications with FreeMASTER NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we show how to build, simulate and test a speed estimator based on Hall Sensors for a BLDC motor. The estimator is first tested under Matlab Simulink environment and then ported into the Open Loop Control Simulink model and tested on the MPC5744P Development Kit with FreeMASTER over CAN interface.   We discuss about: - How to compute the speed; - How to build a speed estimator based on Hall sensors; - Step-by-step model building an enhancements; NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
  Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.2.0 RTM   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.2.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K312, S32K314, S32K322, S32K324, S32K341, S32K342, and S32K344 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, GPT). To enable BMS applications development, we have added support for MC33775A and MC33772C battery cell controllers (& MC33665PHY). In this release, we have also updated FreeMASTER, AMMCLib, and MATLAB support for the latest versions. The product comes with over 130 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=13593437   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K312 S32K314 S32K322 S32K324 S32K341 S32K342 S32K344     Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI UART GPT DIO   Support for MC33775A and MC33772C battery cell controllers & MC33665PHY The toolbox provides support for the MC33775A, MC33772C, and MC33665. The MC33775A and MC33772C are lithium-ion battery cell controller ICs designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33665 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high-speed isolated communication network. The ready-to-run examples provided with the MBDT for S32K3 show how to communicate between the S32K344 and the MC33775A and MC33772C via the MC33665 transceiver. For the MC33775A, the examples show how to configure the battery cell controller to perform Primary and Secondary chains conversion, and read the cell voltages conversion results from the MC33775A, while for the MC33772C the examples show how to configure the Battery cell controller to read current. All the converted values are displayed to the user over the FreeMaster application.           Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.         Support for component restore to default settings The toolbox allows users to restore the configuration of a component (for models which use the EB Tresos configuration tool) to the settings corresponding to the Default Configuration Template the model uses. This allows reverting changes (if made) to the default values.   Support for AUTOSAR blockset (SW-C deployment) New RTD version supported  (v2.0.0) New S32Config Tools version supported (v1.5) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.29: All functions in the Automotive Math and Motor Control Functions Library v1.1.29 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.     Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a R2021b R2022a   S32Design Studio Integration We provide a simple mechanism to let users the opportunity to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.          Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 130 examples, including: Battery Management Systems examples Motor control applications Communication (SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode   For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.2.0 is fully integrated with MATLAB® environment in terms of installation:         Target Audience This release (1.2.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt            
View full article
This page summarizes all Model-Based Design Toolbox videos related to BMS. Speed-Up BMS Application Development with NXP's High-Voltage Battery Management System Reference Design and Model-Based Design Toolbox (MBDT) Link to the recording here  This webinar shows how to design and develop Battery Management Systems, with NXP's High-Voltage BMS Reference Design and Model-Based Design Toolbox for S32K3xx, with Simulink® and Embedded Coder. During this webinar, we will introduce the ASIL D High Voltage Battery Management System Reference Resign that comprises a Battery Management Unit (BMU), Cell Monitoring Units (CMU), and a Battery Junction Box (BJB). NXP's HV-BMS Reference Design is a robust and scalable solution including hardware designs, production-ready software drivers, and safety libraries, as well as extensive ISO 26262 Functional Safety documentation. The design significantly reduces the development effort and enables an improved time to market with the latest chipset innovations. Speed Up Electrification Solutions Using NXP Tools Link to the recording here  This video provides an overview of the NXP Software and Tools solutions, designed to help customers to speed up application development with design, simulation, implementation, deployment, testing, and validation. During this session, you will learn about all the steps required to build complete solutions like battery management systems with NXP in-house solutions and NXP Model-Based Design Toolbox with simulation and code generation.
View full article
In this video we discuss about Open Loop Control strategy and for the first time in this course we will put together all the models we have created so far and build the Simulink model that will allow us to rotate the BLDC motor. We discuss about: - Open Loop Control diagram; - Step-by-step model building an enhancements; - Test the open loop control system on the BLDC motor;   NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we enhance a Simulink model to allow the reading of hall sensors after processor reset to get the initial position of the rotor.   We discuss about: - How to build a special initialization routine to read the halls once in the beginning - How to use StateFlow programming - How to mix the direct read of GPIOs with ISR based on hall transition readings NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows how to build a simple S32K application with NXP's Model-Based Design Toolbox that consists in: Read the SW2 push button state at each 0.1 seconds Switch on/off the Blue LED Record the value of the push button and display its state via serial communication in FreeMASTER
View full article
  Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K1xx – version 4.3.0 Austin, Texas, USA - September 13, 2022   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K1xx version 4.3.0. This release supports automatic code generation for S32K1xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K1xx Automotive Microprocessors. This new release adds support for RDDRONE-772B  Battery Management Systems (support for MC3377xC), Code deployment directly from Simulink via JTAG/SWD (OpenSDA, PeMicro Probe, or SEGGER JLink), SIL/PIL support for the latest MATLAB versions, new community and customer requested features (Enhanced support for SBC, FCAN Blocks, UART Blocks, I2C Blocks) and many other various new functionalities to help customers with rapid prototyping with NXP S32K1xx microcontrollers.   FlexNet Location: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Activation link: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Technical Support: NXP Model-Based Design Toolbox for S32K1xx issues are tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation based on S32K SDK 4.0.0 RTM drivers from MATLAB® for NXP all S32K1xx derivatives: S32K142W MCU Packages with 48/64 LQFP (*updated) S32K144W MCU Packages with 48/64 LQFP (*updated) S32K116 MCU Packages with 32QFN and 48LQFP (*updated) S32K118 MCU Packages with 48/64 LQFP (*updated) S32K142 MCU Packages with 48/64/100LQFP (*updated) S32K144 MCU Packages with 48/64/100LQFP and 100BGA (*updated) S32K146 MCU Packages with 64/100/144LQFP and 100BGA (*updated) S32K148 MCU Packages with 144/176LQFP and 100BGA/QFP (*updated) Multiple options for packages and clock frequencies are available via Model-Based Design Toolbox S32K Simulink Main Configuration Block       Added Support for RDDRONE-BMS772         We added examples for the RDDRONE-BMS772. This is a standalone BMS reference design suitable for mobile robotics such as drones and rovers, supporting 3 to 6-cell batteries. MBDT examples cover applications like BMS, LCD, CAN and SBC.       Battery Management System (BMS) support for MC3377xC – examples, documentation and FreeMASTER UI are available Special Simulink Blocks have been added to simplify the way a user can initialize such a controller, read vital parameters (like cell voltage, stack voltage, temperature, current), and manage the whole system. The entire suite of blocks is easily integrated within the new Battery Management Toolbox from Mathworks, so users can leverage these algorithms on top of our blocks.       Enhanced FCAN Support We improved the FCAN communication support by addressing the following: FCAN communication is now fully functional when external SBC is configured (for both UJA113x and UJA1169) The user is able to retrieve the ‘Error Status’ of an ongoing transfer and abort it in case something is wrong. The ‘Receive’ and ‘Send’ blocks for FCAN now allow the user to specify when the initialization for the message buffers should be executed (during Model Initialization, at each execution of the block, or none). If the ‘NONE’ option is selected, a newly added block ‘FCAN_MBConfig’ can be used to configure the message buffer. The FCAN messages ID can also be provided via an input port for both ‘Send’ and ‘Receive’ operations.   Multiple S32K1xx peripheral support. The peripheral coverage for each of the S32K1xx derivatives is shown below:   S32K116 S32K118       S32K142   S32K144         S32K146 S32K148       Added support for JTAG deployment directly from Simulink We added support for deployment over JTAG directly from Simulink. In the main Config block, under Target Connection, the JTAG option must be selected. Following this action, the JTAG Interface selection becomes active. Here is the following selection: OpenSDA Embedded Debug – the EVB Embedded Debugger is used. USB Multilink PEmicro – an external PEmicro probe is used. SEGGER JLink – this action requires the external selection of the SEGGER JLink     Extended support for MATLAB versions We extended support for our toolbox to cover a wider range of MATLAB releases – starting from R2016a and going up to R2022a. This way we want to avoid locking out users that have constraints regarding MATLAB versions.   New community-requested features In our efforts to make  NXP’s Model-Based Design Toolbox for S32K1xx version 4.3.0 fit the needs of the users, we have added the following requested features/updates: Added OSIF Time Delay Block Added Code Size Report Added NONE option for the SPI SIN/SOUT pins Enabled support for more than one ADC Interleave Block Updated Profiler functionality Updated FCAN Blocks Updated I2C Blocks Updated LPUART Blocks Fixed Registers dropdowns not displaying options on some machines   100% S32K1xx supported peripheral coverage with examples. Approximately 300 examples are available as part of the toolbox that exercises all the functionalities supported.     For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K1xx MCUs and evaluation boards solutions out-of-the-box with: NXP Support Package for S32K1xx Online Installer Guide Add-on allows users to install the NXP solution directly from the MathWorks website or directly from MATLAB IDE. The Support Package provides a step-by-step guide for installation and verification. NXP Model-Based Design Toolbox for S32K1xx version 4.3.0 is fully integrated with MATLAB® environment in terms of installation, documentation, help and examples:       Target Audience This release (4.3.0) is intended for technology demonstration, evaluation purposes, and prototyping for S32K116, S32K118, S32K142, S32K144, S32K146, S32K148, S32K142W, and S32K144W MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
1. Introduction The NXP HCP Toolbox enables automatic code generation for applications prototyping from Simulink for NXP’s S32G2xx and S32S2xx MPUs. This article details the steps to build, deploy, and run the HEV demo on S32G2xx, and also collect telemetry data using AWS IoT Greengrass. 2. Hardware overview The following hardware components are needed for running the HEV demo: an S32G274A RDB2 Evaluation Board Configure the evaluation board to boot from the SD card. a microSD card We'll flash and boot the GoldVIP Linux from this card a micro USB cable Connect the cable to the UART0 port and your host machine. This connection will be shown in Windows as a serial port and we'll use it to connect from a terminal emulator for the initial Linux setup. two Ethernet cables Connect another Ethernet cable to the P3A port and to your LAN network. This connection will be used for AWS data telemetrics. Connect one Ethernet cable to the P3B port and to your LAN network. This connection will be used for PIL communication between MATLAB and the application running on the board. a Logitech F310 or compatible gamepad Connect the gamepad to your host machine before opening the HEV model. We'll use it to drive the car in the virtual 3D environment: to steer, accelerate, and brake. The following figure shows the USB, UART, CAN and power connectors on the S32G2 RDB2 evaluation board. The following figure shows the Ethernet connectors on the S32G RDB2 evaluation board. 3. Software overview To run the HEV demo we must perform the following steps to install the required software. 3.1 Mathworks MATLAB and Add-Ons Install the following software from Mathworks required to build and run any model that uses the NXP Model-Based Design Toolbox for HCP : MATLAB 2020a or newer MATLAB Embedded Coder, the key component that allows us to generate the C code that will be cross-compiled to be executed on the target Embedded Coder Support Package for ARM Cortex-A Processors Install the following additional toolboxes from Mathworks required to build and run the HEV demo: Powertrain Blockset Vehicle Dynamics Blockset Automated Driving Toolbox Simulink 3D Animation Mapping Toolbox All these toolboxes can be installed from MATLAB, by opening Get Add-Ons window and searching for each of these toolboxes.   3. 2 NXP Model-Based Design for HCP Toolbox Install NXP MBDT HCP Toolbox to add the HCP target support to the MATLAB environment to allow code generation and deployment. Following are the steps to install NXP’s Model-Based Design Toolbox for HCP Series of MPUs: 1. Go to nxp.com and sign in to your NXP account. If you don't have an NXP account, create one from the Registration page. Toolbox is for free but an account is required to download the tool and access training & support on NXP Model-Based Design Toolbox Community). 2. Go to NXP Model-Based Design Toolbox (MBDT) page, select the DOWNLOADS tab and press the Download page, which will open the Model-Based Design Toolbox download page. 3. From the Model-Based Design Toolbox download page select the Model-Based Design Toolbox for HCP 1.0.0, and then on the next page, you will be asked if you agree to the Software Terms and Conditions. 4. On the Model-Based Design Toolbox for HCP download page, download the following files: SW32_MBDT_HCP_1.0.0_EAR_D2111.mltbx, the toolbox installer MBDToolbox_HCP_1.0.0_S32S2xx_Tools.zip, the S32G2xx build toolchain Some browsers will download the .mltbx file as .zip file.  To avoid that, please press right click on the download link and select Save link as. 5.  Open MATLAB, navigate to where you downloaded the toolbox installer, and run the installer (press double click or right-click and select Install). 6. After a few minutes (~4-5min), the NXP’s Model-Based Design Toolbox should be visible as a new add-on in the Add-On Manager. 7. The Model-Based Design Toolbox uses the toolchain mechanism exposed by the Simulink to build the  code generated with Embedded Coder toolbox. By default, the toolchain is configured for the MATLAB R2020a / R2020b / R2021a releases. For any other MATLAB release, the user needs to execute a toolbox m-script to generate the appropriate settings for his/her installation environment. This is done by running the mbd_hcp_path.m script.     >> mbd_hcp_path No compatible target currently available for NXP S32G2xx. Creating one.. Creating folders for the target 'NXP S32G2xx' in the folder 'C[…]\NXP_MBDToolbox_HCP\mbdtbx_hcp\codertarget\2021b\s32g2'... Creating the framework for the target 'NXP S32G2xx'... Registering the target 'NXP S32G2xx'... Done. No compatible target currently available for NXP S32S2xx. Creating one.. Creating folders for the target 'NXP S32S2xx' in the folder 'C[…]\NXP_MBDToolbox_HCP\mbdtbx_hcp\codertarget\2021b\s32s2'... Creating the framework for the target 'NXP S32S2xx'... Registering the target 'NXP S32S2xx'... Done. Successful.       3.3 Gold Vehicle Integration Platform (GoldVIP) In the case of S32G2 at the start of the PIL simulation a Linux application is cross-build on the MATLAB host machine, deployed to the evaluation board via SSH, and executed inside a Linux operating system running on that board. We'll use the Linux image from Gold Vehicle Integration Platform (GoldVIP) package that supports telemetry to cloud using AWS IOT Greengrass. Telemetry statistics are fetched from the device, calculated and sent to the cloud counterpart of the application. Statistics received in the cloud are then displayed into user-friendly graphs. The statistics include but may not be limited to: Networking accelerator usage statistics, Realtime cores load, Domain-0 VCPU load and Domain-0 Memory utilization statistics. The GoldVIP is a reference software platform for a vehicle service-oriented gateway running on NXP vehicle network processors like the S32G274A. Following figure shows the GoldVIP high-level architecture. NOTE: GoldVIP is available upon NXP approval as an Early Access Release. Please contact your NXP sales representative for more information. Once you get the approval, go to the GoldVIP download page and download the following files: GoldVIP-0.11.0-binaries.zip GoldVIP-0.11.0_User-Manual.pdf Next we unzip the GoldVIP-0.11.0-binaries.zip archive and  we'll find the Linux image fsl-image-goldvip-s32g274ardb2.sdcard in GoldVIP-0.11.0-binaries\binaries folder. 5. Toolbox setup NXP Model-Based Design Toolbox for HCP offers a Setup GUI to select which toolchain to use, flash the Linux image card, configure and test the network connection. After the installation of the toolbox has finished the GettingStarted.mlx file is opened. To run it go to the LIVE EDITOR tab and push the Run button. Running it will open the Setup GUI that will help you configure the toolbox. 5.1 Select Target We are going to select S32G274A and push the Next button. 5.2 Setup Toolchain  Select I need to acquire the toolchain and push the Next button. In case you already have the toolchain the steps are a subset of the one below. 5.3 Download Toolchain Next download the S32G2xx toolchain by following the steps from 3.2, step 4, if you haven't already done so, and then select the path to the downloaded toolchain archive. Then select the folder to where the archive should be unzipped. Next press the Unzip button to unzip the selected toolchain archive. This step will take around 10 minutes. If the toolchain archive is unzipped successfully, the Next button is enabled. 5.4 Validate build toolchain Select the toolchain folder using the Browse button to verify it. Push the Validate button. If everything is alright the message is Toolchain is valid, otherwise the message is Toolchain is not valid. If the toolchain is valid the Next button is enabled and should be pushed to continue the configuration 5.5 Write Linux on the microSD card This page helps you to write the Linux on a microSD card. First, insert the microSD card, then push the Refresh button to actualize the drive list. If the microSD is available in Windows the list should be not empty. Select a drive from the list and push the Next button. Select the Linux image using the Browse button. Finally, push the Write button to write the Linux image. 5.6. Get additional software In order to connect to the S32G2 board we'll need to install additional software. You can use Terminal Emulator familiar to you, such as Tera Term, Putty or other. Also install FTDI CDM WHQL driver for serial configuration from FTDI chip, otherwise you will not be able to connect to the board using the serial port. 5.7 Connect Hardware Connect the board using the following instructions: 1. Remove the memory card from the host computer and insert into the S32G2 board micro SD card slot. 2. Connect two Ethernet cables to S32G2 board, one to P3A port and another one to P3B port. Connect the other ends of the cables to your LAN or HOME network. 3. Connect an USB cable between the UART0 port on the S32G2 board and your host computer. 4. Connect the 12 V power supply to the S32G2 board and power on the board. 5. Open the terminal emulator (e.g. putty) to connect to the board and configure the network settings. Select the serial port added to Ports (COM & LPT) in Device Manager when the micro USB cable is connect to the host machine, and select 115200 as the baud rate. If you didn't install the FTDI driver in the previous steps, a new COM port will not be added when you connect the USB cable. Once you connect over the serial to the board, you will be asked to log into Linux in the terminal emulator. The default username is root, without a password.  If your network assigns IP address automatically via DHCP, you don't need to do any network configuration on Linux. Otherwise, you will have to configure the network settings for pfe2 interface. Run ifconfig pfe2 to get the IP address that we'll use for PIL simulation. The field that we are looking for is inet, and in the bellow output the IP address is 192.168.2.152.     root@s32g274ardb2:~# ifconfig pfe2 pfe2: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500 inet 192.168.2.152 netmask 255.255.255.0 broadcast 192.168.2.255 inet6 fe80::6da:49da:68c3:24d9 prefixlen 64 scopeid 0x20<link> ether 00:01:be:be:ef:33 txqueuelen 1000 (Ethernet) RX packets 190 bytes 14318 (13.9 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 186 bytes 18928 (18.4 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 device memory 0x46000000-46ffffff     Copy this IP address as we'll need it in the next step of the toolbox setup. 5.8. Setup network connection Fill in the Device Address, Username, Password, and Download folder, and then push the Test Connection button. This tests if the device address is valid, and also if the a SSH commands can be run. For the Device Address use the IP address copied from the output of ifconfig pte2. Default username is root, and no password is set. Default download folder is the home folder of the root use, /home/root. 5.9. Setup done Congratulations! You are ready to use the Model-Based Design for HCP toolbox. Note: Press the Finish button to save the toolchain path and network connection settings. 7. GoldVIP setup By default, the GoldVIP deliverable includes Xen hypervisor. Xen is a type 1 hypervisor (bare metal) that makes possible running multiple instances of the same operating system seamlessly on the hardware. Xen allows creation of virtual machines from the command line or automatically at startup. Xen virtualizes CPUs, memory, interrupts and timers, providing virtual machines with virtualized resources. Two types of virtual machines are defined by Xen: Privileged (Dom0 or Domain-0): The first machine that runs natively on the hardware and provides access to the hardware for unprivileged domains. Unprivileged (DomUs): Virtual machines spawned by Dom0. These machines use the hardware resources allocated from the privileged domain (CPU, Memory, Disk, Network). In the GoldVIP, two virtual machines are started by default, before the user logs in: Domain-0, which has access to all the system resources and creates a network bridge for the unprivileged guest. This bridge, namely xenbr0 is the network interface that forwards packets to the DomU; v2xdomu, unprivileged domain, which has access only to a limited number of resources. The HEV demo will run in Domain-0, in the privileged domain. Telemetry data is collected from Domain-0 and passed to v2xdomu through a TCP client-server communication. To switch to v2xdomu type: xl console v2xdomu The username on the v2xdomu is root without a password. To exit from v2xdomu press Ctrl + ] 7. AWS setup 7.1 Prerequisites You will need an AWS account with SSO enabled. Follow the steps in this guide to enable SSO: https://docs.aws.amazon.com/singlesignon/latest/userguide/getting-started.html Enabling SSO will grant you access to the SSO console. SSO is also required to use the SiteWise Dashboard. 7.2 AWS IAM Permissions A policy for an AWS IAM user, it contains the necessary permissions for the deployment and use of the telemetry use case:     { "Version": "2012-10-17", "Statement": [ { "Effect": "Allow", "Action": [ "cloudformation:*", "cloudwatch:*", "iot:*", "lambda:*", "logs:*", "s3:*", "greengrass:*", "sns:*", "iotsitewise:*", "iam:*", "sso:*", "sso-directory:*" ], "Resource": "*" } ] }     AWS IAM documentation: https://docs.aws.amazon.com/IAM/latest/UserGuide/getting-started_ create-delegated-user.html 7.3 Deployment of the Telemetry Stack in AWS 1. Go to the AWS SAR console: https://console.aws.amazon.com/serverlessrepo/ 2. Go to Available applications tab; then to Public applications and search for goldvip. 3. Check Show apps that create custom IAM roles or resource policies to see the application. 4. Click on nxp-goldvip-telemetry. You can modify the application parameters. 5. Check I acknowledge that this app creates custom IAM roles. 6. Click Deploy. The deployment will take a few minutes. You will be redirected to another page. The name of the stack is on the top of the page, starting with serverlessrepo-, if you changed the application name you will need this name in the next step. You can go to the Deployments tab and see the status of the deployment. Wait for the status to change from Create in progress to Create complete. Note: you may need to refresh the page to see the status change. This CloudFormation stack creates on your account: A Greengrass V2 telemetry component, this is a python function which runs on v2xdomu and sends data to AWS IoT Core. The provisioning script described in chapter 7.4. Connecting the board to AWS creates a Greengrass V2 continuous deployment which will run the telemetry component on your board. A SiteWise Portal with multiple Dashboards; after the board is connected to AWS a live visual representation of the telemetry data received via the Greengrass V2 component is displayed in these. 7.4. Connecting the board to AWS 1. Log into the v2xdomu virtual machine using the command: xl console v2xdomu 2. Configure environment variables for Greengrass provisioning script: From the v2xdomu console, set the AWS credentials as environment variables:     $ export AWS_ACCESS_KEY_ID=<access key id> $ export AWS_SECRET_ACCESS_KEY=<secret access key>     One way of obtaining your AWS credentials is the following: From the AWS SSO console select your account and retrieve the environment variables by clicking on Command line or programmatic access. From section macOS and Linux copy the variables and paste them on your board. Use Option 1: set the AWS credentials as environment variables. Please check the AWS documentation for additional information: https://docs.aws.amazon.com/cli/latest/userguide/cli-configure-envvars.html Note: IAM credentials should never be used on a device in production scenario. These variables are temporary and are erased at reboot. 3. Run the Greengrass provisioning script on your board:     $ python3 ~/cloud-gw/greengrass_provision.py --stack-name <stack-name> --region-name <region-name>     Where <stack-name> is the name of the deployed stack. If you did not change the application name you do not need to specify this parameter. In <region-name> put the region you have selected from the supported ones: us-west-2 or eu-west-1. This will setup the network interface, start the Greengrass V2 Nucleus, and create a Greengrass V2 continuous deployment, which will run the telemetry component created by the Telemetry Stack. Note: the provisioning script will try to setup the internet connection using the eth0 network interface by default. To get more details about the script parameters use:     $ python3 ~/cloud-gw/greengrass_provision.py -h     The board is now connected to your AWS account and it will begin to send telemetry data. 7.6. Accessing the SiteWise dashboard 1. Go to the SiteWise console: https://console.aws.amazon.com/iotsitewise/ 2. Click on Portals from the list on the left. 3. Click on the name of your portal, it starts with SitewisePortal_serverlessrepo. 4. Click on Assign administrators. 5. Add your account and any other you want to have access to the SiteWise Dashboard. 6. Click Assign administrators. 7. Click on the Portal’s Url (or Link). 8. Close the Getting started pop up window. 9. Click on one of the dashboards to visualize the telemetry. You will now see the live telemetry data from your board. For more information check the GoldVIP User Manual. 8. Running HEV demo 1. A Logitech F310 gamepad is needed to control the car. Connect the gamepad before opening the model. 2. We recommend to make a copy of the HEV demo folder from HCP toolbox in another working folder. Run the following command in Matlab to navigate to S32G2xx examples folder.     cd(fullfile(mbd_find_hcp_root(), 'HCP_Examples', 's32g2')     Copy the HEV_P4_Ext_TV to another working folder, e.g. C:\workspace\. 3. Open the HEV_P4_ExternalDriver_v3_TV_v4_fixedStep.slx model. The HEV demo is already configured for PIL simulation mode. 3. Run the PIL simulation by pressing the Start button from . Simulink generates the code for the model, compiles it, downloads it on the board, and then starts the simulation.  
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to i.MX RT Product Family Facial Recognition Application in Co-Simulation mode for IMXRT117X Sensor application for IMXRT1060
View full article
This page summarizes all Model-Based Design Toolbox videos related to i.MX RT Product Family
View full article
  Product Release Announcement Analog & Automotive Embedded Systems NXP Model-Based Design Toolbox for S32K3 – version 1.7.1 img_0-1713952962606.png     The Automotive Embedded Systems, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3 version 1.7.1. This release supports automatic code generation for S32K3 peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3 Automotive Microprocessors. This new product adds support for S32K310, S32K311, S32K312, S32K314, S32K322, S32K324, S32K328, S32K338, S32K341, S32K342, S32K344, S32K348, S32K358, S32K364, S32K366, S32K374, S32K376, S32K388, S32K394 and S32K396 MCUs, and part of their peripherals, based on RTD MCAL components (ADC, CAN, DIO, FEE, GPT, I2C, ICU, LIN, MEM, MCL, PWM, SPI, UART), and support for the GD3162 Gate Driver based on the S32K396 GD3162 Software. In this release, we have also updated the RTD, S32 Configuration Tools, AMMCLib, FreeMASTER, and MATLAB support for the latest versions. The product comes with over 180 examples, covering all the features and functionalities of the toolbox, including new demos for GD3162 Gate Driver applications.   Target audience: This product is part of the Automotive SW – Model-Based Design Toolbox.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=7846241   Technical Support: NXP Model-Based Design Toolbox for S32K3 issues will be tracked through the NXP Model-Based Design Tools Community space.   Release Content: Automatic C code generation from MATLAB® for NXP S32K3 derivatives: S32K310 S32K311 S32K312 S32K314 S32K322 S32K324 S32K328 S32K338 S32K341 S32K342 S32K344 S32K348 S32K358 S32K364 S32K366 S32K374    S32K376    S32K388    S32K394  S32K396   Support for the following peripheral components and functions: ADC CAN DIO eTPU FEE GD3162 GPT I2C ICU LIN MCL (including DMA support) MEM Memory read/write PWM Profiler Registers read/write SPI UART   New RTD version supported (6.0.0)   Integrates S32K396 GD3162 v2.0.2 The toolbox enables access to the GD3162 gate driver for S32K396 derivatives from Simulink models, by delivering a library block (Gd3162) that generates code on top of GD3162 components API.   New S32 Configuration Tools version supported (2024.R1.8)😎   Integration with EB tresos v29.0.0   Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB tresos to configure peripherals/pins/clocks   Default Configuration Project Templates targeting all the supported S32K3 derivatives The toolbox delivers default configuration projects, available in both S32 Configuration Tools and EB tresos, covering an initial enablement of the on-board peripherals, pins, and clocks, for all the supported S32K3 derivatives. The desired template, which represents the starting point for enabling the hardware configuration of the application, can be selected via a dropdown widget.   Support for creating and using Custom Project Templates The toolbox provides support to use and create custom project templates. This could be very useful when having a custom board design – offering the possibility to create the configuration for it only once. After it is saved as a custom project template, it can be used for every model that is being developed.   Such custom projects, addressing specific hardware designs are offered inside the current version of the toolbox to integrate the following EVBs: MCTPTX1AK324 S32K344-WB S32K396-BGA-DC1 MR-CANHUBK344, alongside a set of examples specifically created to target this hardware design and a series of articles (available on NXP Community) demonstrating how to use the toolbox features and functionalities for creating applications for custom boards.   The toolbox has been tested and validated on the official NXP Evaluation Boards     S32K31XEVB-Q100     S32K312EVB-Q172     XS32K3X2CVB-Q172     XS32K3X4EVB-Q257     XS32K3XXEVB-Q172     MR-CANHUBK344             S32K3X4EVB-T172      S32K344-WB        XS32K3X8CVB-Q172     S32K388EVB-Q289             XS32K396-BGA-DC     XS32K396-BGA-DC1   Integrates the Automotive Math and Motor Control Library release 1.1.42 All functions in the Automotive Math and Motor Control Functions Library v1.1.42 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications. S32 Design Studio integration We provide the feature of importing the code generated from a Simulink model inside the S32 Design Studio IDE. This functionality can be useful if the model needs to be integrated into an already existing project or for debug purposes.   Simulation modes We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) including AUTOSAR SW-C deployment External mode   GD3162 Applications The toolbox provides examples for configuring and accessing the external GD3162 gate driver device via SPI communication to demonstrate Dynamic Gate Strength and DC Link Discharge features, supporting both S32 Configuration Tools and EB tresos. Each of them has a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. The examples provided in this release include the following topics: - GD3162 Dynamic Gate Strength - GD3162 DC Link Discharge   Motor Control Applications The toolbox provides examples for 1-shunt and 2-shunt PMSM and BLDC motor control applications, supporting both S32 Configuration Tools and EB  tresos. Each of the examples provides a detailed description of the hardware setup and an associated FreeMASTER project which can be used for control and data visualization. The toolbox also demonstrates the integration of the Motor Control Blockset in developing such applications.   For demonstrating the S32K3 eTPU Software integration, we have included a PMSM application where the FOC algorithm runs on the main CPU of the S32K396 MCU, while the analog sensing, software resolver, and PWM signals generation are offloaded to the eTPU co-processor.   The motor control applications were developed and validated on the MCSPTE1AK344 and MCSPTR2AK396 Motor Control kits.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b R2023a R2023b R2024a R2024b R2025a R2025b   Examples for every peripheral/function supported More than 180 examples showcasing: I/O Control Timers and scheduling Communication (CAN, I2C, LIN, SPI, UART) Memory handling GD3162 Gate Driver applications (DC Link Discharge and Dynamic Gate Strength) Motor Control applications (BLDC and PMSM) AMMCLib FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes and Quick Start Guides documents attached.   MATLAB® Integration: The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3 MCUs and evaluation board solutions out-of-the-box. NXP Model-Based Design Toolbox for S32K3 version 1.7.1 is fully integrated with MATLAB® environment.   Target Audience: This release (1.7.1) is intended for technology demonstration, evaluation purposes, and prototyping S32K3 MCUs and Evaluation Boards.   Useful Resources: Examples, Trainings, and Support: https://community.nxp.com/community/mbdt      
View full article
  Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.4.0 RFP   The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.4.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K310, S32K311, S32K312, S32K314, S32K322, S32K324, S32K328, S32K338, S32K341, S32K342, S32K344, S32K348, S32K358 and S32K396 MCUs and part of their peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, UART, LIN, GPT). To enable BMS applications development, the toolbox offers support for MC33775A and MC33772C battery cell controllers (& MC33665PHY). In this release, we have also updated RTD, AMMCLib, and MATLAB support for the latest versions. The product comes with over 120 examples, covering everything that is supported, including demos for battery cell controllers (BCC) and motor control.   Target audience: This product is part of the Automotive SW – S32K3 Standard Software Package.   FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=14146527   Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K310 S32K311 S32K312 S32K314 S32K322 S32K324 S32K328 S32K338 S32K341 S32K342 S32K344 S32K348 S32K358 S32K396   Support for the following peripherals (MCAL components): ADC PWM MCL LIN CAN SPI UART GPT DIO   Board initialization: The Model-Based Design Toolbox for S32K3xx generates the component’s peripherals initialization function calls as configured in the Board Initialization window. The toolbox provides a default configuration including function calls for initializing the clocks, followed by pins and a custom order for the rest of the peripherals which have been configured in the project associated to the model. Moreover, the toolbox provides the option to save and export the initialization sequence to a file which can be later used for other models as well – in this way, the customization of the board initialization sequence can be done only once, even if applicable for other models as well. Such a file can be then imported as an external Board Initialization Template.   Custom Linker Files and Startup Code: The toolbox allows the selection of custom linker files and startup code to be used during the build process. By enabling the Use Custom Linker or/and Use Custom Startup Code checkboxes, this feature is activated, allowing the users to Browse for specific files.   Support for Referenced Configurations The Model-Based Design Toolbox for S32K3xx enables the usage of Referenced Configurations, a Simulink feature which allows users to share the configuration of an application with multiple models.   Support for MC33775A and MC33772C battery cell controllers & MC33665PHY The toolbox provides support for the MC33775A, MC33772C, and MC33665. The MC33775A and MC33772C are lithium-ion battery cell controller ICs designed for automotive applications which perform ADC conversions of the differential cell voltages and battery temperatures, while the MC33665 is a transceiver physical layer transformer driver, designed to interface the microcontroller with the battery cell controllers through a high-speed isolated communication network. The ready-to-run examples provided with the MBDT for S32K3 show how to communicate between the S32K344 and the MC33775A and MC33772C via the MC33665 transceiver. For the MC33775A, the examples show how to configure the battery cell controller to perform Primary and Secondary chains conversion, and read the cell voltages conversion results from the MC33775A, while for the MC33772C the examples show how to configure the Battery cell controller to read current. All the converted values are displayed to the user over the FreeMaster application.       Support for AUTOSAR blockset (SW-C deployment) New RTD version supported  (3.0.0) Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tools or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.32: All functions in the Automotive Math and Motor Control Functions Library v1.1.32 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2021a R2021b R2022a R2022b R2023a   S32Design Studio Integration We provide a simple mechanism for the users to export the code generated from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project or for debugging purposes.   Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the configuration for it once. After it is saved as a custom default project, it can be used for every model that is being developed.   Support for component restore to default settings The toolbox allows users to restore the configuration of a component (for models which use the EB Tresos configuration tool) to the settings corresponding to the Default Configuration Template the model uses. This allows reverting changes (if made) to the default values.   Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode     Examples for every peripheral/function supported: We have added over 120 examples, including: Battery Management Systems examples Motor control applications (including eTPU example on S32K396) Communication (LIN, SPI, CAN, UART) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached. MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.4.0 is fully integrated with MATLAB® environment in terms of installation:       Target Audience This release (1.4.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings, and Support: https://community.nxp.com/community/mbdt          
View full article
Four-Part How-To Series Model-Based Design Toolbox (MBDT) is an integrated development environment and toolchain for configuring and generating all the necessary software automatically to execute complex applications. The MBDT includes integrated Simulink® embedded target for NXP processors, peripheral device blocks and drivers, the Math and Motor Control library set, and bit-accurate simulation results. Watch on-demand each of our Model-Based Design Toolbox four-part How-To series and learn the basics of MBDT, also its SPI and CAN communication and its PWM control blocks.   Session 1/4 = Get to Know the User-Friendly NXP MBDT for Application Development in MATLAB/Simulink dumitru-daniel.popa‌ will show you how to configure and use the MBDT, engineered to help you speed up application development in MATLAB/Simulink Environment for NXP hardware. Get to know its main features and capabilities through the creation, simulation, built, deployment, and validation of a basic "hello world" type of application on theS32K144EVB.  Session 2/4 = Introducing the SPI Communication Blocks from NXP MBDT nxf46081‌ will highlight the key aspects of communication in the automotive industry while showing you how to configure and use designated blocks that implement the SPI communication inside the MATLAB/Simulink Environment for creating a quick and easy data transfer application using MBDT and the S32K144EVB. Session 3/4 = Introducing the CAN Communication Blocks from NXP MBDT constantinrazvan.chivu‌ will highlight the key aspects of communication in the automotive industry while showing you how to use MBDT and the S32K144EVB to simplify CAN applications with only a few blocks: configuration, transmit, and receive. Session 4/4 = Introducing the PWM Control Blocks from NXP MBDT mariuslucianandrei‌ will showcase how to start using PWM, its features and functionalities while showing you how to build a first application able to generate different types of PWM signals using MBDT and the S32K144EVB; also, learn to sample the external signals to determine the key values: duty-cycle, period, among others.   Your software development processes can speed up by using the free-of-charge NXP Model-Based Design Toolboxes for MATLAB and Simulink development environments, providing full integration, an out-of-the-box configuration, and action blocks for basic/advanced features for designing complex automotive solutions.
View full article