Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
如何在 i.MX RT1050 上从多个启动地址运行同一个启动加载程序? 嗨,恩智浦社区、 我正在开发一个i.MX RT1050项目,其单个引导加载程序目前位于闪存中的 0x60000000。我希望能够在运行时选择启动加载程序从哪个起始地址运行,本质上是从两个不同的位置(例如,出厂启动模式和工作启动模式)执行相同的引导加载程序。 限制和设置: 闪存中只有一个引导程序映像。 我想在运行时从RAM 中运行它,以选择不同的起始地址。 引导加载程序目前与位置无关 (PIC)。 我已经分配了足够的 RAM(0x80000000,大小为 2 MB)来容纳引导加载程序。 我知道有这样一种做法: 将启动加载程序从闪存复制到 RAM。 将 SCB->VTOR 设置为新的 RAM 位置。 将 MSP 设置为新引导加载程序的堆栈指针。 跳转到 RAM 中的 RESET 处理程序。 我的问题是 如果 i.MX RT1050没有编译成 PIC,能否安全地从 RAM 执行引导加载程序? 要使引导加载程序与位置无关,需要做哪些修改? 是否有为固件插槽实施运行时可选择引导加载程序启动地址的最佳实践? 任何指导、示例或参考都会非常有帮助。 启动 ROM | 启动配置 | 闪存 核心与内存 MCXC Re: How to run the same bootloader from multiple start addresses on i.MX RT1050? 你好@sachin13t、 请查看以下可能对你有用的链接:在 i.MX RT10xx 系列上实现第二个引导加载程序 + master 上的 sbl/元器件/secure/semifunc/hab_rvt.c · nxp-mcux presso /sb l · GitHub 有关位置无关代码的更多信息,可以参考以下链接:适用于 ARM Cortex-M 的带有 GCC 的 位置独立代码 | Eclipse 上的 MCU。 BR, IsaulO.
View full article
Enable C99 on Codewarrior 10.6 Good morning, I would like to enable C99 for CW 10.6 v. I use the micro mc9s08ac32, I looked in the manual and used the directive both ‘#pregma c99 on’ and ‘#define EWL_C99 1’, in both cases I found no success. I probably need to enable it from the settings, but I couldn't find any option to enable it. I went to properties>C/C++ Build>Tool settings but i didn't see about C99, only HS08 compiler.  Could you give me some advice? Re: Enable C99 on Codewarrior 10.6 Hello Transidico  Unfortunately CodeWarrior v11 also C90 compliance. So far NXP doesn't have an IDE for HCS08 supporting C99. Best Regards, Jun Zhang Re: Enable C99 on Codewarrior 10.6 Good morning, thank you for your kind reply. I would be interested in using the C99 somehow for this micro, is there no way I can use it? I understand that the compiler does not support it, is there no other compiler that is compatible? If I install CodeWarrior 11.1v does it not support C99? Or is there not something that converts C99 to C90 for me? Thanks Re: Enable C99 on Codewarrior 10.6 Hello Transidico, HCS08 compiler Compliants with C90 standards. C99 is not supported. Thanks, Jun Zhang
View full article
FS85 SPI communication error Hi, I ported the FS8x_S32K144_WatchdogExample this demo in the part about SPI read and write FS85 registers, now the cycle read register M_FLAG, deviceStatus = 0xF0,readData = 0xF014. the specific errors are Wrong number of clock cycles ( <32 or >32) and Error detected in the SPI CRC The CRC8 uses the same function provided by DEMO, why is there an error? How to solve these two errors? Reading register FS_STATES, readData = 0x2003, the state machine corresponding to 03 was not found. FS85 &FS84 回复: FS85 SPI通信报错 Hello  Osker The FS_STATE =5 indicates that RSTB is not released to high, can customer check the RSTB pin level ?    The OV/UV related flag registers are not active at this moment. Any other questions, please let me know. Brs CIndy Wen 回复: FS85 SPI通信报错 Hi, did you follow up on the SPI communication problem with the first chip to find out what caused it. 回复: FS85 SPI通信报错 Hi xuxin User should clear FS_OVUVREG_STATUS by writing all bits to '1',if the faults are triggered again, that is real OV UV fault.  As in FS8510D3 OTP ,ABIST1 is assigned to all the monitors. So if VCOREMON or VMON1~4 reported UV, the   state machine is stuck at ABIST1 state, and can not go to INIT_FS state.  VCOREMON should be connected to BUCK1, VMON1~4 should used to monitor regulators in your schematic. Please refer to the FS85 DEMO board. Please contact local DISTI FAE for more help if debugging support is needed. Brs Cindy Wen 回复: FS85 SPI通信报错 Hi Xuxin Please read the FS_OVUVREG_STATUS register.  Please check if VCOREMON is connected to BUCK1 output.  Check whether the VDDIO voltage is the  level defined by OTP.   Check whether VMON1~4 are 0.8V. Which part number are you using? If you are using specific OTP defined by your company , please share the OTP file to me .  Brs Cindy Wen 回复: FS85 SPI通信报错 Hi Cindy, I just asked my hardware engineer to measure the PGOOD and RSTB pins and both are low, the hardware engineer said that pull-up resistors have been added but did not succeed in pulling them high. Do I need to configure any registers in software next? Or is it simply a hardware issue? 回复: FS85 SPI通信报错 Hi Xuxin If FS state can not enter INIT_FS,I think the PGOOD/RSTB are not released due to some faults.  Please check whether the PGOOD/RSTB are released to high or not? If they are low, please check if there is OV/UV faults on board. Brs Cindy Wen 回复: FS85 SPI通信报错 Hello Cindy. I followed your suggestion and read the following registers after writing 1 to the corresponding bit of M_FLAG, and MISO returned the data as shown, and FS_STATS is still 0x2003. 回复: FS85 SPI通信报错 Hello Xuxin Could you clear these below bits by writing ‘1’  to these bits and see if the faults will be triggered again.  If these faults were triggered only when power on reset, we can ignore them, as they will not happen during the normal operation.   Brs Cindy Wen 回复: FS85 SPI通信报错 Hello, Tomas. Here is the SPI waveform I read from the SPI waveform from FS_STATES register. 1 is CLK, 2 is CS, 3 is MOSI, 4 is MISO. the MOSI I parsed from the waveform is 0xAC,00,00,F4, and the MISO is 0x70,20,03,14. it's really not 0x2006. does it have something to do with the fact that I'm in debug mode all the time? 回复: FS85 SPI通信报错 Hello Xuxin, Good to know that the original error disappeared. I am not aware of the fail-safe state machine state code of 0x03. It should be indeed 0x06. Could you please share a scope shot illustrating the read of the FS_STATES register? BRs. Tomas 回复: FS85 SPI通信报错 Hi Tomas, After I replaced a new FS85 chip, the Wrong number of clock cycles ( <32 or >32) and Error detected in the SPI CRC disappeared. I wrote DBG_EXIT in the FS_STATES register, but when I read the FS_STATES register, readData = 0x2003, not 0x2006, what does this 03 stand for? How to enter INIT_FS state? 回复: FS85 SPI通信报错 As shown, 1 is MOSI, 2 is CLK, 3 is CS, 4 is MISO. i read the FS_DIAG_SAFETY register, and the MOSI is 0xA8,0x00,0x00,0xF2. the MISO values are 0xF0,0x04,0x29,0xD9. 0xF2 and 0xD9 are the CRC values, which are the same as the ones i calculated with the CRC8 tool! the same as the values I calculated with the CRC8 tool. Also, I don't know how to confirm the values in table100. 回复: FS85 SPI通信报错 Hello Xuxin, If you have an oscilloscope or a logic analyzer, could you please share screenshots illustrating both SPI write and read transactions? Also please double check that all SPI timing requirements as shown in Table 100 of the datasheet are met. BRs, Tomas  回复: FS85 SPI通信报错 SPI configuration is as follows: clock 20Mhz, chip select low active, MSB transmission, clock idle low, sampling on the second edge of the clock, SPI frame length is 32 bits, baud rate is 1000000
View full article
将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 您好,NXP团队: 我们从 NXP 网站上获得了 MC33771C 和 MC33772C 的 BCC SW 驱动程序包。 我们正在尝试将这些示例项目迁移到 S32 平台的 S32 设计工作室(版本:3.5)。 我们按照以下链接中的迁移程序进行操作: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Video-Migrating-S32K1-projects-from-S32DS-for-ARM-and-SDK-3-0-x/ta-p/1296239 。 但是,代码没有正确迁移,我们无法确定原因。 请帮助我解决这个问题。 顺祝商祺! 哈里什 回复:将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 你好@Hareesh 恐怕 S32DS v3.5 的迁移功能不如 S32DS v3.4 那样全面。我们建议迁移到 S32DS v3.4。 我会将这个问题告知相应的团队。带来不便敬请谅解。 回复:将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 你好@Hareesh 正如我在之前的回复中提到的。所采取的步骤与所分享的视频中提供的步骤相同。完成代码迁移步骤后,出现的错误与库包含有关,可以使用我上一篇文章中提供的信息来解决。
View full article
IMX8MP spread spectrum Hello, I wanna add spread spectrum for my IMX8MP LVDS screen signal. I find that the feature is available for 8QuadMax and i.MX 8QuadXPlus Display but not for i.MX 8MP. Do you know when this will be available or there is already a patch to add it ? Thanks. Re: IMX8MP spread spectrum It works, thank you. Re: IMX8MP spread spectrum Hi @clemntnxp,  Thank you for contacting NXP Support. On our i.MX8MP EVK the enablement of Spread Spectrum Clocking is via software. We don't have any code example to apply the required changes. Here is a description of Spread Spectrum enablement for LVDS interface. The LVDS interface doesn't have an integrated PLL such as MIPI or USB interface, therefore, LDB (LVDS Display Bridge) module uses VIDEO_PLL1 as root clock and VIDEO_PLL1 support SSCG (Spread Spectrum Clock Generator). Here is a block diagram of LVDS interface on iMX8M Plus. To enable the Spread Spectrum Clocking for LVDS interface you will need to write on VIDEO_PLL1 control register. You will need to set SSCG_EN and the other parameters (MFR, MRR, SEL_PF, SEL_PF) with U-Boot. For a proper setting up, please have a look to the section 5.1.5.4.4 SSCG and Fractional PLLs on the i.MX8MP Reference Manual. Have a great day!
View full article
ls1028ardb 更改DDR和pinmux配置,参考文件? 为了准备定制电路板,我正在尝试更改 LS1028ARDB 电路板上的 DDR 设置和 pinmux。 我的第一个目标是禁用内存上的 ECC(以加快启动时间)。 显然,实现这一目标的方法是通过 codewarrior。 我可以找到如何为这些东西创建一个项目。但我找不到有关主板设置的任何参考。如果能够从 LS1028ARDB 板已经正确的设置开始,那就方便多了。 有这样的文件吗? 另外,codewarrior 提供了从内存转储加载这些内容的选项。但是,例如,在使用“md”转储 u-boot 中的寄存器内容后,在 codewarior 中加载这些内容后的结果完全是假的。似乎没有任何文档描述如何创建 codewarrior 所需的文件。 回复:ls1028ardb 更改 DDR 和 pinmux 配置,参考文件? 让它有点工作了。 从 codewarrior 创建了十六进制转储。尝试读一遍,确实有效。 获取我已经创建的 u-boot 内存转储,并编写了一个 python 脚本将其转换为与 hexdump 相同的格式。 它会接受这个文件。生成了 DDR 设置,从而创建了无法在 ATF 中使用的无用文件。 做出更改并再次生成。使用差异工具比较文件,然后手动将这些更改修补到 ATF 代码中。 回复:ls1028ardb 更改 DDR 和 pinmux 配置,参考文件? 我有可用的图像、软件、Yocto 和所有东西,但我并不寻求这些。我还完全清楚,当我使用 Yocto 构建东西时,DDR 运行得非常好。 我一直在您提供的链接上寻找,但没有找到任何与我所寻找的东西有点相似的东西。 我正在寻找可以输入 CodeWarrior 的东西,以便它可以为 LS1028ARDB 创建 DDR 代码。 我尝试过内存转储(来自 u-boot 的各种格式),但 codewarrior 不接受它们并且抱怨格式。 回复:ls1028ardb 更改 DDR 和 pinmux 配置,参考文件? 我一直在您提供的链接上寻找,但没有找到任何与我所寻找的东西有点相似的东西。 我正在寻找可以输入 CodeWarrior 的东西,以便它可以为 LS1028ARDB 创建 DDR 代码。 我尝试过内存转储(来自 u-boot 的各种格式),但 codewarrior 不接受它们并且抱怨格式。 回复:ls1028ardb 更改 DDR 和 pinmux 配置,参考文件? 我的问题是关于如何获得工作推荐。 当我选择 LS1028 时,它默认出现的 DDR 配置与 LS1028ARDB 板不匹配。一个明显的区别是 ECC 处于关闭状态。 我想要的是 LS1028ARDB 的配置。 其余的事情我想我可以自己解决。
View full article
Re: How can i configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @PavelL, @alejandro_e  I am Trying to Implement VLAN for Sending Two different Streams such as stream1, stream 2 so for that on top of Existing Configuration I am trying to include VLAN for that General Parameters Table  TPID = 34984 TPID2 = 33024 L2 Lookup Table  I changed the MASK to  0x1FFFFFFFFFFFFFFFF for including VLAN, IOTAG MACADDR = 0x4C4C36454143 SRCPORT = 3 DSTPORT = 1,2,5 CB Sequence Generation and Individual Recovery Table REPLACE_PORT = 1,2 TAG_PORT = 1,2 CB Tag Replacement Table  REPLACEVLANID - ENABLE VLANID = 1 RTAG_RESERVED = ENABLE Second VLAN Integration  L2 Lookup Table  I changed the MASK to  0x1FFFFFFFFFFFFFFFF for including VLAN, IOTAG MACADDR = 0x112233445566 SRCPORT = 4 DSTPORT = 1,2,3 CB Sequence Generation and Individual Recovery Table REPLACE_PORT = 1,2 TAG_PORT = 1,2 CB Tag Replacement Table  REPLACEVLANID - ENABLE VLANID = 2 RTAG_RESERVED = ENABLE Added VLAN Lookup Table for both stream  VMEMB_PORT = 1,2,3,5 BC_DOMAIN = 1,2,3,5 TYPE_ENTRY[0]  = ENABLE TYPE_ENTRY[1] = ENABLE This was the change I was planning to have a Separate VLAN ID for this Two Different MAC Address Computation for that I am trying to Implement VLAN? whether this configuration Satisfy the configuration of VLAN or what are the other changes need to be made for Configuring VLAN ? Re: How can I configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @PavelL  SWITCH - 1 Initially Created a Default VLANID  VLANID = 0 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Disable all Ports BC_DOMAIN = Disable all Ports TAG_PORT = Disable all Ports TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 0 VLANID = 1 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4 -- ENABLE BC_DOMAIN = Port 1,2,3,4 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 1 VLANID = 2 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4,5 -- ENABLE BC_DOMAIN = Port 1,2,3,4,5 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 2 MAC Configuration Table  Port 1 --> VLANPRIO = 7 VLANID = 1 Port 2 --> VLANPRIO = 7 VLANID = 2 Port 3 --> VLANPRIO = 7 VLANID = 3 Port 4 --> VLANPRIO = 7 VLANID = 4 Port 7 --> VLANPRIO = 3 VLANID = 2 SWITCH - 2 VLANID = 0 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Disable all Ports BC_DOMAIN = Disable all Ports TAG_PORT = Disable all Ports TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 0 VLANID = 1 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4 -- ENABLE BC_DOMAIN = Port 1,2,3,4 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 1 VLANID = 2 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4,7 -- ENABLE BC_DOMAIN = Port 1,2,3,4,7 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 2 MAC Configuration Table  Port 1 --> VLANPRIO = 7 VLANID = 1 Port 2 --> VLANPRIO = 7 VLANID = 2 Port 3 --> VLANPRIO = 7 VLANID = 3 Port 4 --> VLANPRIO = 7 VLANID = 4 Port 5 --> VLANPRIO = 3 VLANID = 2 I made the configuration changes above  my CAN packets are getting Lost and CAMERA packets are getting streamed  so what would be the root cause for packet loss even after configuring VLANID  So what would be the ideal scenario to overcome the issue of Packet loss i understand CAMERA packets are flooding How to overcome this issue  Regards Abrar Re: How can I configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @Abrar_23 , UDP is fine for traffic testing. 30Mbps is also fine. Up to ~90% of max traffic load (in this case - egress queue) there should be no traffic drop. I apologize for late responses, I have to prioritize my tasks. Due to limited resources, customers which are using generic email accounts such as gmail.com or qq.com or similar have lower priorities. Please ensure that you use your company email address when communicating with NXP so that we can prioritize your question accordingly. Thank you for your understanding. Best regards, Pavel Re: How can I configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @PavelL  SWITCH - 1 Initially Created a Default VLANID  VLANID = 0 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Disable all Ports BC_DOMAIN = Disable all Ports TAG_PORT = Disable all Ports TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 0 VLANID = 1 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4 -- ENABLE BC_DOMAIN = Port 1,2,3,4 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 1 VLANID = 2 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4,5 -- ENABLE BC_DOMAIN = Port 1,2,3,4,5 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 2 MAC Configuration Table  Port 1 --> VLANPRIO = 7 VLANID = 1 Port 2 --> VLANPRIO = 7 VLANID = 2 Port 3 --> VLANPRIO = 7 VLANID = 3 Port 4 --> VLANPRIO = 7 VLANID = 4 Port 7 --> VLANPRIO = 3 VLANID = 2 SWITCH - 2 VLANID = 0 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Disable all Ports BC_DOMAIN = Disable all Ports TAG_PORT = Disable all Ports TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 0 VLANID = 1 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4 -- ENABLE BC_DOMAIN = Port 1,2,3,4 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 1 VLANID = 2 VING_MIRR = Disable all Ports VEGR_MIRR = Disable all Ports VMEMB_PORT = Port 1,2,3,4,7 -- ENABLE BC_DOMAIN = Port 1,2,3,4,7 -- ENABLE TAG_PORT = Port 1,2 TYPE_ENTRY[1] = ENABLE TYPE_ENTRY[0] = ENABLE VLANID = 2 MAC Configuration Table  Port 1 --> VLANPRIO = 7 VLANID = 1 Port 2 --> VLANPRIO = 7 VLANID = 2 Port 3 --> VLANPRIO = 7 VLANID = 3 Port 4 --> VLANPRIO = 7 VLANID = 4 Port 5 --> VLANPRIO = 3 VLANID = 2 can you give me a right way for the above one what are the VLANID need to be configured in MAC Configuration table and VLAN Lookup table  Same VLANID can be mentioned in MAC Configuration Table and the VLANID also need to be configured in L2 Lookup table   These VLANID are used in L2 lookup table were for some MAC Address we utilized VLANID = 1 and for other MAC Addresses used VLANID = 2 in this configuration with respect to stream of VLANID = 1 is working fine able to Transmit and receive Message whatever the VLANID getting mentioned in Port 3 & Port 4 is configured that Configuration of Message is working fine  Say suppose when i configure VLANID = 1 in Port 3 at the time the configuration with respect to that is working but the configuration with respect to VLANID = 2 is not working when i do vice versa its working fine  The stream 2 is an UDP stream, which is coming around 30Mbps speed what is the root cause of the issue ? Re: How can I configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @Abrar_23 , let's start with the CB.  If you want to isolate the CB traffic from the other traffic by adding a VLAN tag to it, you have to do the following: Add VLAN entry to VLAN Lookup Table  // no mirroring VING_MIRR = 0x0 VEGR_MIRR = 0x0 // vlan port membership, add ports used for CB // for switch 1 this would be e.g. port 2, 3 and 4 VMEMB_PORT = 0x1C VLAN_BC = 0x1C // keep the VLAN tag at egress TAG_PORT = 0x1C // VLAN type this entry is eligible for TYPE_ENTRY[1] = 1 TYPE_ENTRY[0] = 1 // VLAN ID VLANID = 100 Edit the respective L2 Lookup Table entry // add VLAN ID 100 to the lookup VLANID = 100 VLANIDMASK = 0xfff where VLANIDMASK is a part of MASK, you already have set up. If you want to keep VLAN tag on egress, select port in TAG_PORT (VLAN lookup table). If you want to add VLAN tag on ingress, VLANID shall be set on MAC configuration table for the requested port. I think that L2 policing table shall be also set - please check AN12925, chapter 5.3.1 L2 policing. Your idea with VLAID priority as the flow shaper might work. BTW, how do you generate your streams? How much traffic (Mbps) do you generate? Bets regards, Pavel Re: How can I configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @PavelL  So, for my setup I am having two Stream say stream 1 & stream 2 when i enable both the stream same time i am losing the stream 1 Packets  so, in order to overcome this issue i am planning to add VLAN to overcome this issue by the reference from document i read when VLAN is added we will have a Separate queue for Processing each stream since separate VLANID is assigned  I want to add tag on the Egress  Yes, I want to Isolate the CB Stream Traffic from other traffic by adding VLAN tag to it   I tried the above implementation i checked the ethernet Frame where the VLAN ID is tagged but its unable to overcome the issue of Packet loss of Stream 1 when both the stream is append running  assigned different VLANID and VLAN(Priority) different but the still packet loss is happening  How to overcome this issue  Regards Abrar  Re: How can i configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @Abrar_23 , I went through your setup. I apologize but I'm not sure what do you want. Could you please be more specific? Do you want to tag ingress? Keep tag on egress? Do you want to isolate the CB traffic from the other traffic by adding a VLAN tag to it? Thank you. Best regards, Pavel Re: How can i configure IEEE802.1CB Frame Replication and Elimination for Redundancy (FRER) in SJA11 Hello @Abrar_23 , I moved the post to the thread. I hope I will come with answer this week. Thank you for your understanding. Best regards, Pavel
View full article
How to use iseled library at s32k116 Hello, I use s32 design studio for ARM ver. 2018.r1 and processor is fs32k116lit0vfmt. I changed MCU package 48pin(default at s32k116 pjt) to 32pin. But how to use iseled library. it's version is indicated as s32k144_sdk01. I choose SDK_S32K1xx_15/timing_pal when it added. so can't choose data & clk pin match on s32k116_32. What can I do for using correct iseled library version at s32k116_32? Re: How to use iseled library at s32k116 Hi @kimmk, It is necessary to install corresponding S32K1xx SDK before installing ISELED SDK. There is description about how to match version between S32K1xx SDK and ISELED SDK in the “S32K1_ISELED_RTM_x.x.x_ReleaseNotes.pdf”, which is included in ISELED SDK package. Best regards, Julián
View full article
在 FRDM-MXCN947 板上同时使用以太网和摄像头 在 MCXNx4x 中,SmartDMA 可用于实现摄像头接口。 根据 MCXNx4x 数据表,以太网和 SmartDMA 的 Pinmux 分配有冲突。因此,我认为以太网和摄像头不能同时使用。 但是,FRDM-MCXN947 板用户手册 (UM12018) 规定了以下内容: > 如果在使用摄像机时仍然需要以太网功能, ,将 SJ16 和 SJ26 跳线从默认位置移开。 有没有办法同时使用以太网和摄像头? 开发板 MCX N Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 你好@dubian1shu 我重新检查了文件内容,确认文件中的描述存在问题。 我们将及时修改文件。 可以同时使用SmartDMA (EZH_CAMERA) 和以太网 (ENET),但需要找到一些不共享的引脚供摄像头使用。 您可以参考这篇文章。 MCX N947:同时实现以太网和摄像头功能 - NXP 社区 希望能帮到你。 BR 挂 Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 感谢@Harry_Zhang的检查和回复 由于 SmartDMA 支持 P1_X 和 P3_X,我认为 MCXNx4x 可以同时使用 SmartDMA 和以太网功能。 但使用 FRDM-MCXN947 能否使用 SmartDMA 和以太网功能? FRDM-MCXN947 的 J9(摄像头接头)有七个引脚与以太网引脚冲突。FRDM-MCXN947 主板用户手册 (UM12018) 中描述的 P1_4 的解决方案仅解决了其中一个问题,没有提及其他六个冲突。 例如,P1_5、P1_13 和 P1_15 在 SmartDMA 和以太网之间存在冲突。从原理图文件(SCH-90818)来看,似乎没有解决这一冲突的办法。 有办法在 FRDM-MCXN947 上同时使用 SmartDMA (EZH_CAMERA) 和以太网 (ENET) 吗? Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 你好@dubian1shu 我查看了MCXNx4x 数据表,确实有一些引脚以太网与 SmartDMA 冲突。但如果你想同时使用以太网和 SmartDMA,可以选择一些以太网和 SmartDMA 不冲突的引脚。 例如,可以选择 P3_X 作为 SmartDMA 引脚,选择 P1_X 作为以太网引脚。 然后参照 FRDM-MCXN947 主板用户手册 (UM12018) 移动跳线。 希望能帮到你。 BR 挂
View full article
S32G-VNP-RDB32 (SJA1110) スイッチのレジスタアクセス こんにちは、 レジスタに値を書き込む方法を探しています 読み書きの完全な住所を教えていただけますか? 住所 名前 アクセス リセット 説明 8Ch DYN_BE_LKP_ エントリー0 読み取り/書き込み 0h (FFFFFFFEh) 8chより前のベースアドレスは何でしたか? 例えば0x3fc0008cになりますので、この動的エントリテーブルには完全なアドレスがあります。完全なアドレスを教えていただけますか? 8Ch DYN_BE_LKP_ エントリー0 読み取り/書き込み 0h (FFFFFFFEh) 90時間 DYN_BE_LKP_ エントリー1 読み取り/書き込み 0h 94時間 DYN_BE_LKP_ エントリー2 読み取り/書き込み 0h 98時間 DYN_BE_LKP_ エントリー3 読み取り/書き込み 0h 9Ch DYN_BE_LKP_ エントリー4 読み取り/書き込み 0h A0h DYN_BE_LKP_ エントリー5 読み取り/書き込み 0h A4h DYN_BE_LKP_CTRL 読み取り/書き込み 0h (FF800000h) レジスター内の動的エントリを構成するための完全なアドレスを教えていただけますか? この実装はSJA1110 スイッチで行う必要がある Re: Register Access in S32G-VNP-RDB32 (SJA1110) Switch こんにちは@Atkinson 、 最初は簡単ではないと思われるかもしれませんが、コンセプトは実際には非常にシンプルです。 最終的なレジスタ アドレスは、アクセス方法 (AHB 経由の M7 コア経由で内部的にアクセスしているか、SPI_AP インターフェース経由で外部的にアクセスしているか) によって異なります。ベース アドレスはアクセス ポイントによって異なります。 レジスタ アドレスは、UM11107 の表 2 に示されているベース アドレスを使用して計算されます。たとえば、スイッチ サブシステムの場合、ベース アドレスは SPI_AP アクセスの場合は0x00000000 、AHB アクセスの場合は0xFF000000です。 あなたのCASE、レジスタ0x8C (DYN_BE_LKP_ENTRY0) は、AHB 経由でアクセスすると0xFF00008Cになります。 ここで混乱が生じる可能性があります。SDK ドライバは次のように定義します。 #define SJA1110_L2_ART_LE_ADDR ( 0x3fc00023 ) /**< l2ArtLockedEntryレジスタのアドレス *   SWITCH_DRV_Write ルーチンは、内部 (AHB) アクセスのためにアドレスを 2 ビット (<< 2) 左にシフトします。SPI 転送 (カスケード スイッチ セットアップで使用される) の場合、シフトは適用されません。SO、 0x3fc00023 << 2 は0xFF00008Cになります。   上記の説明で理解が深まったかと思います。   よろしくお願いいたします。 パベル
View full article
关于 ADC 通道分配 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,社区 在数据表 99 中分配给 ADC1_IN0 至 ADC1_IN3。 另一方面,在《参考手册》的 ADC 存储器映射中,ADC1 有 CH_A 到 CH_D。 是否可以将通道 0 指定为 CHA_SEL,通道 1 指定为 CHB_SEL,通道 2 指定为 CHC_SEL,通道 3 指定为 CHD_SEL,以支持以下操作? IN0-CH_A IN1-CH_B IN2-CH_C IN3-CH_D 顺祝商祺! 请访问 i.MX7 双核 About ADC channel assignment 你好,伊戈尔帕季科夫。 这是一个解决方案,但我不明白,所以我有一个问题。 根据数据手册中的引脚分配,ADC1_IN0 至 ADC2_IN3 共有八个物理输入端。 在参考手册中,adcx_ch_A_CFG1 的 CHA_SEL 的范围从 0 到 15。 ADC1_INx 和 Channelx 对应的是什么? 还是它们互不相关? 应如何设置 ADC2_IN0? 顺祝商祺! Re: About ADC channel assignment <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 后藤 是的,这是可能的。如第 14.1.1 节所述概述 i.MX 7Dual 应用处理器参考手册 "ADC 最多支持五个逻辑组(ChA / ChB / ChC / ChD / SW)的转换。每组可从 0 - 15 个物理通道中选择一个通道 。" 问候 igor ----------------------------------------------------------------------------------------------------------------------- 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。Thank you! -----------------------------------------------------------------------------------------------------------------------
View full article
Clarifications Required for i.MX RT1170 EVKB Dear NXP Team, Greetings! We are planning to use the i.MX RT1170 MCU, starting with the EVKB board, for one of our upcoming projects. The project will involve integration of a 4G data module, Ethernet, camera, audio, and display. I have a few technical queries and would appreciate your guidance on the following: 1. 4G Data Module Configuration We would like to use a 4G module with the EVKB board. Is it correct to insert the SIM card into the on-board slot and connect a 4G modem (e.g., Quectel EC25) via the M.2 interface? Which interfaces (e.g., UART, USB) are internally connected between the EVKB, SIM slot, and the M.2 connector? Are there any SDK examples or application notes available for configuring and communicating with a 4G module through this interface? 2. Camera Interface and Remote Monitoring Our requirement involves using a camera to stream video remotely, similar to a CCTV system. Can the i.MX RT1170 EVKB support this use case? What are the supported camera interfaces (MIPI-CSI, USB, etc.), and is there any reference code or documentation for camera integration and remote streaming? 3. Display Integration We intend to use a display with either RGB-to-LVDS or MIPI-DSI interface to show full-screen videos, animations, and text. Are there any SDK examples or reference guides for interfacing LVDS/MIPI-DSI displays? What are the hardware/software requirements for rendering smooth video and graphics? 4. Audio Playback The system should play voice prompts example like “Hello” or “Good Morning.” We are considering using either an audio codec with the SAI interface or a DFPlayer module over UART. Which method would be more reliable or recommended for this platform? Are there any SDK examples available for SAI + codec configuration? I would greatly appreciate your support and any reference documentation or sample projects you could share. Looking forward to your kind assistance. Thank you in advance. Best regards, Pandiyan T. Re: Clarifications Required for i.MX RT1170 EVKB 1. Unfortunately, we do not have a test case to confirm this as the examples are for Wifi and Bluetooth. So I cannot confirm that inserting the SIM card will work with a 4g modem via M.2 interface.  The board schematic shows that SIM card is directly connected to the RT1170. M.2 connector interfaces with UART and SDIO. 2. Yes, that application can be used however there is no example of streaming video. There are examples to acquire video through MIPI-CSI and trough USB. Developing a simple UVC device based on i.MX RT1050 i.MX 8/RT MIPI DSI/CSI-2 3. Yes, please refer to the display examples on the SDK, as well as lvgl examples. Please refer to this application note: AN12940: Use Case of RT1170 LCD Display System based on MIPI DSI – Application Note Regarding the requirements, it may vary as the resolution would require certain amount of data. 4. I don't know your requirements to choose which one to use, however, we have useful examples of SAI with the onboard codec. Please refer to any of SAI examples of the SDK, they use SAI along with the EVK codec. BR, Omar
View full article
在 VSCode CMake 环境中将 LVGL 与 RT1060 Matter 开发集成 你好,我正在使用 RT1060 开发 Matter。 我目前使用 VSCode 和 CMake 开发环境。 我需要将 LVGL 集成到这个设置中。 请提供指导。 Re: Integrating LVGL with RT1060 Matter Development in VSCode CMake Environment 你好,我是@pooisonner、 感谢您对 NXP MIMXRT 系列的关注! 虽然没有官方的 LVGL 移植指南,但 SDK 中包含 LVGL 示例,您可以从 lvgl_demo_benchmark 开始。 为了与开发环境保持一致,还需要使用 MCUXpressoForVscode 插件来导入演示程序。 致以最诚挚的问候, Gavin
View full article
IMXRT1170-EVKBのデュアルイーサネット構成 こんにちはチーム、 あいさつ! 私はIMXRT1170-EVKBボードに取り組み、デュアルイーサネット(ETH0とETH1)を実装して、100Mと1Gの速度で同時に動作するようにしています。 まず、同じワークスペース内でスタンドアロンモードで正常に動作するSDKサンプル「evkbmimxrt1170_lwip_ping_bm_cm7」をインポートしました。イーサネットポートの選択は、次のものを使用して制御されます。 - 「BOARD_NETWORK_USE_100M_ENET_PORT(1U)」 - 「BOARD_NETWORK_USE_100M_ENET_PORT(0U)」 ただし、両方のイーサネットポート(100Mと1G)を同時に有効にする必要があります。これを達成するために、私は持っています: - lwIP を使用して 2 つのイーサネット インターフェイス (100M と 1G) を設定および初期化しました。 - 一意のMACアドレス、PHYリソース、およびクロック構成を割り当てました。 - 各インターフェースに「netif_100M」と「netif_1G」の構造体を作成しました。 ドライバーと設定ファイルの変更: 1. opt.h の "IP_FORWARD" を有効にしました。 2. 両方のイーサネットインターフェイスのping初期化をイネーブルに。 3.「lwipopts.h」を更新しました。 - 「LWIP_SINGLE_NETIF = 0」を設定すると、複数のインターフェイスが許可されます。 - 「LWIP_NUM_NETIF = 2」を設定して、ネットワークインターフェースの最大数を定義します。 これらの変更を統合すると、両方のイーサネット入力に対して ping を正常に送信できます。ただし、「1G イーサネット (ETH1) が応答する」だけで、「100M イーサネット (ETH0) は応答を受信しません」。 参照用に、ターミナルのスクリーンショットと完全に変更されたプロジェクト「evkbmimxrt1170_lwip_ping_bm_cm7」を添付しました。私の構成を確認し、この問題の原因となっている可能性のある不足している手順を提案していただけませんか? ご指導を楽しみにしています。 お手数ですが、よろしくお願いいたします。 よろしくお願いいたします クマール王子 Re:IMXRT1170-EVKBのデュアルイーサネット構成 こんにちはサム、 迅速な対応ありがとうございました。 提案どおりに変更を加えました。削除/コメント "netif_set_default(&netif_100M);」しかし、それでも同じ問題が発生します。たとえば、100Mからではなく、1Gからのみ応答を取得するpingのようなものです。 B.R.、 クマール王子
View full article
56F8300プログラミングソフトウェア こんにちは。56F8323からファームウェアを読み出す必要があります。そのタスクに使用されるソフトウェアについて説明できる人はいますか? そのために 56800E フラッシュ プログラマー ユーザーガイドを使用できますか?   Re: 56F8300 programming software MCU のクローン作成に関する情報をいくつか追加しました。568323 から 2 つのファイルのみを読み出す必要があります。 1)fflash 568323_flash.cfg プログラム flash.S -rp0x00000:0x03FFF -p0x378 2)fflash 568323_flash.cfg ブートフラッシュ.S -rp0x20000:0x20FFF -p0x378 私の理解では、データフラッシュ領域(0x01000 0x01FFF)はSO必要ありません Re: 56F8300 programming software こんにちは@Fduch 、それを聞いてとても嬉しいです。新しい問題がある場合は、新しい投稿を作成してください。 Re: 56F8300 programming software ついに解決しました!CodeWarrior for 56800E デジタル・シグナル・コントローラ v8.3.exe をインストールする必要があります+ FLSHPROGRAMMER_V1.2_WIN32.exe を次のディレクトリに移動します。 C:\Program Files\Freescale\FlashProgrammer v1.2\bin>fflash 568323_flash.cfg 1623 0_p.S -rp0x0:0xfff -s -p0x378 56800E フラッシュプログラマー v1.1 プログラムの実行日: 2025 年 7 月 21 日月曜日 14:45:06 ローカルCCSサーバーにコネクテッド ポートLPT1でパラレルコマンドコンバータを使用するように構成 使用構成ファイル: 568323_flash.cfg 設定ファイルで定義された 3 つのフラッシュ ユニット。 チップID: 0x01f4001d コアID: 0x02211004, 1 - 通常モード デバイスをデバッグ モードにしています。お待ちください... 読書メモリ: ****************、完了 デバイスをユーザー モードにリセットしています... 初期化: 2907ms、メモリ読み取り: 3297ms、デバッグ終了: 921ms、合計: 7125ms Re: 56F8300 programming software OSはWinXPです。そして、CodeWarrior をインストールしていませんでした。アーカイブ 56800E フラッシュ プログラマー ユーザー ガイドから 56800E Flash Programmer.exe と FFLASH.exe のみ。CodeWarrior をインストールする必要がありますか? Re: 56F8300 programming software 56F8300 プログラミング ソフトウェアのバージョンは何ですか。また、このソフトウェアは CodeWarrior のどのバージョンのプラグインですか。また、Windows OS は何ですか? ログに「 CCCSClient::Open: 接続が拒否されました」と記録されていることに気付きました。 CCS に関係するかも知れませんので、参考にして下さい。Windows 7/10: CodeWarrior for DSC で USB TAP を使用する - NXP コミュニティ Re: 56F8300 programming software さて、正しい CMD と、私があなたの *cfg で持っているものは次のとおりです: C:\JtagV2>fflash 568323_flash.cfg 16230_x.S -rx0x0:0xfff -p0x378 56800E フラッシュプログラマー v1.0 プログラムの実行日: 2025 年 7 月 21 日月曜日 13:48:18 CCCSClient::Open: 接続が拒否されました C:\JtagV2> Re: 56F8300 programming software こんにちは。Codewarrior v8.3 で別の 56F8323 構成ファイルを見つけました。もう一度試していただけますか? Re: 56F8300 programming software さて、いくつかのアクション: C:\JtagV2>flashJtagLoader 568323_flash.cfg 16230_x.S -rX0x0:0xfff -p0x378 DSP56F801x フラッシュローダー。2006年11月3日18:00:59にコンパイルされました。 バージョン アルファ 2.0 (c) Freescale, TIC, 2006 ウィリアム・ジャン 部分著作権 2000-2002、Zloba Alexander I/Oポートドライバが起動しました アドレス 0x378 のプリンタ ポートを使用しています。 チップID: 0x01f4001d プログラミング時に部品をリセットすると、JTAG パスは次のようになります。 JTAG IRパス長: 8 JTAG DR パス長: 1 (BYPASS) コアID: 0x02211004 コアステータス: 0x0d - デバッグ プログラミング時に部品のコアTAPを選択した後、JTAGパスが変更されます。 今!!! JTAG IRパス長: 4 JTAG DR パス長: 1 (BYPASS) デバッグ要求ステータス: 0xd - デバッグ OnCEステータスを有効にする: 0xd - デバッグ OnCE の有効化に成功しました。ターゲット チップはデバッグ モードです。 緩和発振器のトリムが成功しました!、トリム値 = 0x026c チップが保護されていません フラッシュ構成ファイルコマンドが無視されました: target_code_sets_hfmclkd 1 フラッシュ構成ファイルコマンドが無視されました: set_hfm_config_base 0x003FF7 フラッシュ構成ファイルコマンドが無視されました: set_hfm_programmer_base 0x2F800 フラッシュ構成ファイルコマンドが無視されました: set_hfm_prog_buffer_base 0 フラッシュ設定ファイルコマンドが無視されました: set_hfm_prog_buffer_size 512 設定ファイルで定義された 3 つのフラッシュ ユニット。 コードのダウンロードに失敗しました。PRAMベースアドレスを確認してください。 C:\JtagV2> どうしたの? Re: 56F8300 programming software こんにちは!戻ってきました...そして、その操作には flash.cfg ファイルが必要であることがわかりました。しかし、56800E Flash Programmer.exeには*cfgファイルがありません どこで入手できますか?正確に言えば - flash8323.cfg Re: 56F8300 programming software こんにちは@Fduch 、 これは LPC チャネルなので、その他の DSC 関連の質問については、 デジタル・シグナル・コントローラ - NXPコミュニティに新しい投稿を作成してください。 あらかじめご了承ください。 よろしくお願いいたします。 セレステ Re: 56F8300 programming software 後で必ず質問が出るでしょう。それについては調査が必要です Re: 56F8300 programming software こんにちは@Fduch 、 サポートありがとうございます。 はい、 56800E フラッシュ プログラマ ユーザーガイドを使用して、56F8323 からメモリを読み取ることができます。 56F8XXXFPソフトウェアをダウンロードしてください: MC56F832xおよびMC56F812x DSC用EVK | NXP Semiconductors 次に、ファイル56800EFPUGを開き、「2.2.3 メモリの表示」セクションの手順に従います。 お役に立てれば幸いです。 よろしくお願いいたします。 セレステ ------------------------------------------------------------------------------------------------------------------- 注: この投稿が質問の答えである場合は、「解決策として承認」ボタンをクリックしてください。ありがとう! -------------------------------------------------------------------------------------------------------------------
View full article
S32DS for ARM 2018R1 ライセンス こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1のライセンスの有効期限が切れました。 延長していただけますか? アクティベーションコード00B2-2243-F93D-50F1 よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: 0255-52A3-B9BE-AB0C よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM V2.2 のライセンスが 13 日後に期限切れになります。確認して延長を手伝っていただけますか? Arm用S32 Design Studio アクティベーションID: 97B6-8CB8-3FC0-851A 評価日数: 13 機能バージョン: 2.2 機能のステータス: 評価 (13 日間) ありがとうございます。 Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license はい、うん Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ARM V2.2 ライセンスの有効期限が切れました。 ライセンスを延長していただけますか? アクティベーションID: DD5C-6F03-8AE4-7ECA SOありがとう。 Re: S32DS for ARM 2018R1 license S32 プラットフォーム 3.4 の S32DS のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます。アクティベーションコード C5A1-5B94-2A38-9034 Re: S32DS for ARM 2018R1 license こんにちは: おはようございます!S32dsのライセンスが期限切れです。ライセンスの延長をお願いできますか?ソフトウェアバージョンは2.2です。 本当にありがとうございます!あなたの助けが必要です! Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード:349D-19F8-FFD7-7F10 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード592C-8B75-D563-0CAE Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license S32DS for ARM 2018R1 のライセンスの有効期限が切れました。延長をお願いしたいです。どうもありがとうございます。 コード9DD9-3E3B-4AA1-1DE3 S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DE17-8B75-A725-CBC3 Re: S32DS for ARM 2018R1 license S32DS for Power Win32 v2017 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか?「このライセンスを返却することはできません」というヒントです。返品しようとすると、「 よろしくお願いします。 Re: S32DS for ARM 2018R1 license S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?アクティベーションコード D429-1EC2-B799-7507 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは: S32 Design Studio for Power Architecture ® v2.1 - Windows/Linuxのライセンス IDE の有効期限が切れました。確認と延長を手伝っていただけますか? アクティベーションコード DDD9-023A-976E-CD88 ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認と延長を手伝っていただけますか?アクティベーションコード DDD9-023A-976E-CD88 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license こんにちは、S32 Design Studio for ARM v2.2 ライセンスの有効期限はすでに切れています。延長してもらえますか? ありがとうございます! アクティベーションコード: 2D6B-DC21-07CF-F125 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは: 私の免許証 S32DS for Arm v2.2 IDE の有効期限がもうすぐ切れます。確認して延長していただけませんか? ありがとうございます。 アクティベーションコード: BC11-7022-0D21-E460 回复: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 4777-90EB-DAF6-AE57 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018 R1 のライセンスが期限切れです。延長してもらえますか? アクティベーションコード: 6EC6-15B7-7227-97F6 ありがとうございます。 カルロ 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM V1.3 のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license 問題は解決しました。ありがとうございます Re: S32DS for ARM 2018R1 license S32DS ライセンスの拡張を手伝ってください。アクティベーションコード: FF84-9C7B-EFCB-6595。ありがとうございます! Re: S32DS for ARM 2018R1 license こんにちは、 あなたのアカウントを確認しましたが、すべてのライセンスは有効でアクティブ化されています。S32DS PA では異なるアクティベーション キーを使用しましたが、問題はありません。 Re: S32DS for ARM 2018R1 license ソフトウェアフィードバック:(ライセンスがありません) Re: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限がすでに切れていますが、延長することはできますか? ありがとうございます! アクティベーションコード: 77FC-3B94-A7DC-54EE Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: FF84-9C7B-EFCB-6595 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。ARM 2018R1 用に S32DS を再インストールしました。 オフラインでアクティベートすると、activation.xml に「ライセンスを生成CANません。すでに期限が切れています」と表示されます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスが期限切れになりました。延長していただけますか? アクティベーションコード: FC1A-4C29-3203-9C08 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v3.5 のライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8A8B-9E9B-F34E-2603 回复: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Arm v2.2 ライセンスはすでに期限切れです。延長してもらえますか? ありがとうございます! アクティベーションコード: D0BA-0474-25E0-F056 S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます!アクティベーションコード: 3EF3-981A-CE8D-45C3 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 3EF3-981A-CE8D-45C3 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: C617-86A4-65B7-F3D9 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 0384-6363-91F6-CB8E Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8238-B154-F160-0911 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 516A-3379-0522-6A9D どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 0D34-286B-9EE6-E692 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: DE63-F9AF-C189-5399 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 ========================================== 商品の説明S32 Design Studio 注文番号S32DS_2018_R1_100931407 注文番号 ライセンスの総数:100 アクティベーションコード C625-7579-0C28-63DC 製品に適用されるライセンス: バージョンの説明 R1 2018 S32 Design Studio (EULA を表示) 3.1 S32 Design Studio (EULA を表示) 100個入手可能       Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM v2.2 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード F1B3-2017-8F0D-17BE よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @acirillo さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32S 2018のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @linxwhut さん、 両方のライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @Detective さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: C819-045E-F1F8-61B7 Re: S32DS for ARM 2018R1 license こんにちは。私と同僚の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限が切れてしまいました。ライセンスの延長を手伝っていただけますか?ありがとう アクティベーションコード:82DF-FC84-F43A-1EF0 アクティベーションコード:5EBA-DE62-DCF0-02A9 Re: S32DS for ARM 2018R1 license こんにちは、ホーガンさん。 有効期限を2027年まで延長しました。現在のコードで再度アクティブ化してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとうございます Re: S32DS for ARM 2018R1 license よろしくお願いします。 Re: S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとう 。 Re: S32DS for ARM 2018R1 license こんにちは、 @J_Garyさん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: E971-3802-1E3D-5BA6 Re: S32DS for ARM 2018R1 license こんにちは、 @liamtsenさん、 あなたのライセンスを2028年12月末まで延長しました。 使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちはサラさん ライセンスが延長されました。アクティベーション コードをもう一度試してください。 よろしくお願いします、 マイク 回复: S32DS for ARM 2018R1 license こんにちは、 @Hanshengさん あなたのライセンスを2027年末まで延長しました。使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1 ライセンスの有効期限がすでに切れています。延長にご協力いただけませんか? ありがとうございます! アクティベーションコード: B7B1-173F-51BA-13A2 よろしくお願いいたします。 サラ Re: S32DS for ARM 2018R1 license こんにちは、 @1772137309 。 あなたのライセンスを2028年末まで延長しました。 S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: B0A4-688C-2AD6-79EE Re: S32DS for ARM 2018R1 license こんにちは、 @ScreenUserさん、 ライセンスの有効期限を 2027 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 6C82-9208-D1F2-C38F Re: S32DS for ARM 2018R1 license こんにちは、 ライセンスの有効期限を 2026 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは: S32DS_Power_Win32_v2.1 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 Re: S32DS for ARM 2018R1 license どうもありがとうございます。今はすべて正常に動作しています。改めて感謝申し上げます。 Re: S32DS for ARM 2018R1 license こんにちは、ハオさん あなたの免許を3年間延長しました。S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは、 @Jaydenyzhu 私はこの権利を2026年まで延長しました。 新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 - メフル・パテル S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコードD5D0-D801-AB24-58DF よろしくお願いします。 Re: S32DS for ARM 2018R1 license My S32 Design Studio for Arm 2018_R1 の有効期限が 4 日後に切れますが、延長してもらえますか?ありがとう; アクティベーションID: 799E-5E79-910F-6C57 Re: S32DS for ARM 2018R1 license こんにちは、Gen Liさん あなたの免許を3年間延長しました。 現在のアクティベーション コードを使用して再度アクティベーションしてください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license おはよう、 S32 Design Studio for Power Architecture バージョン 2.1 IDE のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード DBA1-317C-5265-7E4F よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、Mehul_Patelさん S32DS が動作するようになりました。ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん あなたのライセンスを2026年12月末まで延長しました。 アクティベーションを更新してください。 ありがとう。敬具。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 アクティベーションコードはD876-C313-75B1-2E1B です。ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 @cjgyf さん、 あなたの権利を2025年12月末まで延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん ライセンスを再アクティブ化できるように、 S32DS for Arm v2018のアクティベーション コードを共有していただけますか。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license 私のライセンスも期限切れ(9DE8-C6AE-8B6B-952B)なのですが、延長していただけますか?よろしくお願いいたします! Re: S32DS for ARM 2018R1 license こんにちは、NXPの専門家の皆さん。 S32DS for Arm v2018 のライセンスの有効期限が切れ、ライセンスが返却されましたが、現在ライセンスが欠落していることが示されています。ライセンスの延長にご協力ください。どうぞよろしくお願いいたします。 デビッド Re: S32DS for ARM 2018R1 license こんにちは、マイク 遅れてごめんなさい。どうもありがとうございます。今はすべて正常に動作しています。 敬具 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。同じコードで再度アクティベートしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 09D2-DE37-6529-87FB よろしくお願いします。 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 この権限のサーバー ログを確認しました。返却されたライセンスの最大数に達したことが報告されています。カウントをリセットした、SO今は動作するはずです。同僚にもう一度試してもらってください。 また、同僚が次のリンクを使用して NXP.com アカウントにログインすると、独自のライセンスを取得できることにも注意してください。 https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、マイク 再アクティベーションは現在私の PC では機能していますが、以前は同じライセンスが機能していた同僚の他の PC では機能しなくなりました。同僚にもライセンスを拡張することは可能ですか?それとも、新しいライセンスを取得することは可能ですか?NXP アカウントは次のとおりです。 [email protected] [email protected] よろしくお願いします。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license 本当にありがとう、マイク。 敬具 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 あなたの権利を延長しました。新しい有効期限を受け取るSOライセンスを更新してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう。 S32DS for ARM 2018R1 のライセンスが期限切れになります。延長していただけますか?添付ファイルでご覧いただけます。 ありがとうございます。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは、 私はこの権利を2025年まで延長しました。新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 4F70-F0A3-101C-3C96 本当にSOありがとう。 Re: S32DS for ARM 2018R1 license ありがとう、マイク。 良い一日を! Re: S32DS for ARM 2018R1 license こんにちは、 両方の権利は2025年まで延長されました。インストールを再アクティベートするには、アクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は B361-6887-8BBF-ED12 さらに、私の同僚のアンナ・ダレッシオにも: E735-6A42-FED4-6005 本当にSOありがとう。 アニタ Re: S32DS for ARM 2018R1 license こんにちは@zhanglei327さん、 あなたの権利を2025年まで延長しました。インストールをライセンス サーバーと同期するには、[ヘルプ] -> [NXP ライセンス] メニューにある [更新] ボタンを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、 私の免許証はもうすぐ期限切れになります。 Re: S32DS for ARM 2018R1 license おはよう! 問題は解決しました! よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 サーバー側からライセンスを手動で返却しました。ライセンスの返却のオファーを受け取ったら、「はい」を選択してください。場合によっては、適切にリセットされない設定があり、強制的にリセットされることがあります。この後、ライセンスを返却すれば、問題なくアクティベートできるはずです。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 同じライセンス番号で再アクティブ化を試みましたが、ライセンスは別の機能用であるというメッセージが表示され続けます。ただし、最初のエラーの後、戻り値の回数を超えたことに関する 2 番目のエラーは再び発生しません。 助けていただけますか? よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 ライセンスサーバーを確認しました。返品の最大数を超えたと報告されました。返品カウントをリセットしました。これで問題は解決されるはずです。もう一度お試しください。 Mike Re: S32DS for ARM 2018R1 license おはよう、 以前と同じ番号でライセンスを再度アクティブ化しようとしましたが、ライセンスは別の機能用であると表示されます。その後、「戻る」をクリックすると、エラー メッセージが表示されます (添付ファイルを参照)。 助けていただけますか? よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。[ヘルプ] -> [NXP ライセンス] メニューから更新するか、以前と同じアクティベーション コードを使用して再アクティベーションしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 S32DS for Arm 2018R1 IDEs のライセンスが期限切れになりました。延長していただけますか? 添付ファイルで、現在のライセンスの有効期限が切れていることをCAN確認できます。 よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは、 あなたの権利を延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 Mike
View full article
i.MX8/9 の Apple CarPlay Ultra こんにちは、 i.MX8 または i.MX9 シリーズ プロセッサで Apple CarPlay Ultra のサポートが計画されていますか?もしSOなら、予想されるタイムラインは何ですか? i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Re: Apple CarPlay Ultra on i.MX8/9 これはプロサポートチームから得た情報です。また、プロサポートのメンバーの1人がApple CarPlay Ultraについて次のように話していました。 「現時点ではサポートしていませんし、FUTURE的にもサポートする予定はないと思います。これはアナ・ワーシー氏から始まる議論です。」
View full article
IMX SM (システムマネージャ) を使用した IMX95 ハードウェアのパーティショニングとアイソレータ こんにちは、 IMX95 verdin evkボードを使用したプロジェクトに取り組んでいます ハードウェア (A55 コア) をパーティション分割して、それぞれで異なる重要度のアプリケーションを実行する 4 つの別個の分離された Linux を実行したいと考えています。私たちは、プロトタイプ作成のために SM を使用してボードを素早く分割し、生産に近づいたときに PikeOS に移行することを望んでいました。 SM ドキュメントでは、A55 パーティションを構成する方法についてはあまり説明がありませんでした。それが可能だといいのですが、間違っていたら訂正してください。 理想的には、パーティション分割された A55 を含む参照構成と、コメントとコンポーネントの説明を含む参照構成が必要であり、何がどこにあり、なぜであるかを理解できるようになります。Linux を実行するために必要な最小限の A55 LM 構成の例もいただければ幸いです。 私たちが望むものの例 - コンポーネントの説明と時折の説明コメントを含む完全な構成:   PD_A55P start=2, stop=8, test #power delivery to A55 package PD_A55C0 stop=7 #power delivery to A55 core 0 - only stop because of ... PD_A55C1 stop=8 #power delivery to A55 core 1 ... A55P OWNER, sema=0x442313F8 #A55 package - must be owned by LM2 because ..., sema means ... ... FLEXSPI1_MEM EXEC, begin=0x000000000, end=0x0FFFFFFFF #only needed if ... OCRAM_C EXEC, begin=0x001000000, end=0x001017FFF #used for ..., minimum size ... OCRAM EXEC, begin=0x0204C0000, size=96K #used for ..., minimum size ... GPU DATA, begin=0x04D900000, end=0x04DD7FFFF #only on LM that owns GPU, minimum size ... DDR EXEC, begin=0x088000000, end=0x089FFFFFF #ddr partition 1, used for ... DDR EXEC, begin=0x08E000000, end=0x87FFFFFFF #ddr partition 2, used for ... 適切に文書化された構成ファイルを 1 つ用意しておくと、望ましい結果を得るために何を変更する必要があるかを理解するのに大いに役立ちます。上記の例では、A55P は A55 パッケージを意味すると推測しましたが、確信を得る方法はありません。また、1 つの LM の下にメモリの DDR セクションが 2 つある (さらにセキュア A55 セクションに 1 つある) 理由もわかりません。また、すべての A55 LM にこれらすべてが必要かどうかもわかりません。 また、複数の LM で同時に同じ Linux イメージを起動できるCANかどうか、また各 LM に異なる Linux イメージをロードできるCANかどうか、またそれをどのように設定するかについても興味があります。 最後に知りたいのは、シリアル DBG ポートにコネクテッドする LM を選択する方法と、(使用しない) M7 のデバッグ COM ポートを別の A55 LM で上書きできるかどうかです。 ありがとうございます。ご返信をお待ちしております。 ウラジミール
View full article
i.Mx8MP:启动动画后,Android 14.1.2.0 电路板支持包中的 ENG 版本无法渲染 GUI 你好 我们已经使用用户调试版本(安卓 14.1.2.0 电路板支持包)测试了我们的硬件,所有接口都能正常工作。但是,在 eng 版本中,启动动画之后 GUI 无法完全呈现——屏幕保持黑色。userdebug 和 eng 版本的完整源代码是相同的。 启动动画开始时会出现重复的日志打印。 [43.895856][ T1] 启动:控制信息:Could not find 'aidl/activity' for ctl.interface_start from pid: 210 (/system/bin/servicemanager) [ 43.913409][ T685] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)试图将 aidl 服务活动作为懒服务启动,但无法启动。通常这种情况发生在未安装服务的情况下,但如果服务是作为懒人服务使用的,则可能是配置不正确。 [ 44.895921][ T210] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)由于无法找到 "activity",因此尝试将其作为懒惰的 AIDL 服务启动。(如果未配置为懒惰服务,则可能会卡住启动或仍在启动)。 [ 44.939268][ T1] 启动:控制信息:Could not find 'aidl/activity' for ctl.interface_start from pid: 210 (/system/bin/servicemanager) [ 44.955168][ T687] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)尝试将 aidl 服务活动作为懒服务启动,但无法启动。通常这种情况发生在未安装服务的情况下,但如果服务是作为懒人服务使用的,则可能是配置不正确。 [ 45.935838][ T210] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)由于无法找到 "activity",因此尝试将其作为懒惰的 AIDL 服务启动。(如果未配置为懒惰服务,则可能会卡住启动或仍在启动)。 [ 45.963901][ T1] 启动:控制信息:Could not find 'aidl/activity' for ctl.interface_start from pid: 210 (/system/bin/servicemanager) [ 45.979228][ T688] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)尝试将 aidl 服务活动作为懒服务启动,但无法启动。通常这种情况发生在未安装服务的情况下,但如果服务是作为懒人服务使用的,则可能是配置不正确。 [ 46.963765][ T210] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0) 由于无法找到 "activity",因此尝试将其作为懒惰的 AIDL 服务启动。(如果未配置为懒惰服务,则可能会卡住启动或仍在启动)。 [ 46.987934][ T1] 启动:控制信息:Could not find 'aidl/activity' for ctl.interface_start from pid: 210 (/system/bin/servicemanager) [ 47.000965][ T689] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)尝试将 aidl 服务活动作为懒服务启动,但无法启动。通常这种情况发生在未安装服务的情况下,但如果服务是作为懒人服务使用的,则可能是配置不正确。 [ 47.987624][ T210] servicemanager:调用者(pid=463,uid=1041,sid=u:r:audioserver:s0)由于无法找到 "activity",因此尝试将其作为懒惰的 AIDL 服务启动。(如果未配置为懒惰服务,则可能会卡住启动或仍在启动)。 此电路板支持包中的工程版本需要进行任何具体更改吗? 致以最崇高的敬意, Maruti Naik Android 图形与显示 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 感谢您的更新。 请确认一下,你能在 ENG 模式下完全启动到 Android GUI(主屏幕)吗? 如果你能分享设置 > System > About > 内部版本号的屏幕截图以供参考,那将很有帮助。 顺祝商祺! Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 您指的是哪个图形用户界面?我可以在 ENG 模式下使用 GPU 加速启动安卓动画。 此致 Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 感谢您确认版本。 澄清一下——你能否确认在使用工程模式二进制文件时 GUI 加载/渲染是否正确? 此致 Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 是的,它在 EVK 中版本得很好。 此致 Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 亲爱的@Bio_TICFSL 感谢您的澄清。 是的,我知道优化的代码在使用ENG版本时表现更好,但是两个版本的功能都应该可用。 你能否确认一下,在运行 Android 14 和 en g 版本的 i.MX8MP EVK 上,GUI 是否可以正常呈现而没有任何问题? 顺祝商祺! Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 是的,我确认当您使用 ENG 时,您的代码会得到更好的优化,但在两种选择下,您应该都能使用它。 此致 Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 我多次尝试闪存 eng 图像,但问题依然存在。 有趣的是,在 userdebug 版本中,相同的日志消息出现大约 4-5 次,然后停止,之后 GUI 成功呈现。但是,在 eng 版本中,这些消息不断循环出现,GUI 永远不会完全加载。 请确认在eng 模式下是否有任何特定配置或限制会影响图形用户界面的渲染? Re: i.Mx8MP : GUI Not Rendering with ENG Build in Android 14.1.2.0 BSP After Boot Animation 你好 最好重新版本然后烧掉你的板然后再试一次,因为 Android 开发中的 " 找不到 “aidl/activity” " 错误可能表明编译系统无法在 aidl 目录结构中找到名为 act ivity 的 AIDL 文件 。 这通常意味着 AIDL 文件或目录结构缺失或配置不正确。 要解决此问题,请确保 AIDL 文件(例如 activity.aidl )存在于正确的位置,并且编译系统配置为可识别 AIDL 文件。     以下是潜在问题的分类和解决方法: 1.AIDL 文件丢失或放错位置: 检查文件: 验证是否存在 activity.aidl 文件。 检查目录: 确保 activity.aidl 文件位于 Android 项目的 src/main/aidl 目录中,如果使用自定义源码集,则位于相应的源码集中。 代码包结构: AIDL 文件的代码包声明(例如, 代码包 com.example.app.aidl; )必须 与其所在的目录结构相匹配。 如果文件位于 src/main/aidl/com/example/app/ 中,则代码包声明应为 package com.example.app.aidl;。     2。版本系统配置(Android Gradle 插件): 启用 AIDL: 确保在 app/ 版本 d.gradle 文件中启用 aidl 编译功能。   代码   android { buildFeatures { aidl true } } 源代码集: 如果使用自定义源代码集,可能需要在 sourceSets 块中指定 AIDL 文件的源代码目录。   代码   android { sourceSets { main { aidl { srcDirs 'src/main/aidl' } } } } 3.清洁和重建: 更改 AIDL 文件或 版本配置后,清理并重建项目,确保更改生效。 在 Android Studio 中,转到 版本 > Clean Project ,然后转到 版本 > 重建项目 。   。增量版本(安卓工作室): Android Studio 的增量版本通常可以高效处理 AIDL 文件,但如果你遇到问题,可以尝试完全重建。       5.稳定的 AIDL: 如果您使用的是稳定版 AIDL,请确保您的 AIDL 接口的所有依赖项也定义为稳定版 AIDL。 通过直接在 AIDL 文件中定义包裹体结构,将任何包裹体转换为稳定包裹体。   示例:   假设您有一个名为 IMyInterface 的 AIDL 接口,您想在活动中使用它。   创建 IMyInterface.aidl : 代码   // IMyInterface.aidl package com.example.app.aidl; interface IMyInterface { void doSomething(); } 将其放在 src/main/aidl/com/example/app/ 中 :     代码   my_app/ ├── src/ │ └── main/ │ ├── aidl/ │ │ └── com/ │ │ └── example/ │ │ └── app/ │ │ └── IMyInterface.aidl 在 app/ 版本.gradle 中启用 AIDL:     代码   android { buildFeatures { aidl true } } 清洁和重建。     按照这些步骤,您应该能够解决"无法找到 'aidl/activity'" 错误,并在 Android 项目中成功使用 AIDL 接口。     此致
View full article
小さな非セキュアパーティションとセキュアパーティションを持つmcuboot用のファームウェアを生成する こんにちは、 このテストには frdm_rw612 ボードを使用しています。私の IDE は、MCUxpresso プラグインを備えた vscode です。私はファームウェアを「mcuboot 対応」になるようにコンパイルしようとしています。つまり、それを使用して OTA を実行できるようにしたいと考えています。 まず、このチュートリアルに従いました: https://community.nxp.com/t5/Zephyr-Project-Knowledge-Base/Zephyr-app-with-MCUboot-in-VS-Code/ta-p/2089541 期待通りに動作しています。現在のパーティション構成は、boards\nxp\frdm_rw612\frdm_rw612_common.dtsi ファイルで確認したとおりです。 partitions { compatible = "fixed-partitions"; #address-cells = <1>; #size-cells = <1>; /* * Partition sizes must be aligned * to the flash security sub-region size of 128KB. */ boot_partition: partition@0 { label = "mcuboot"; reg = <0x00000000 DT_SIZE_K(128)>; }; slot0_partition: partition@20000 { label = "image-0"; reg = <0x00020000 DT_SIZE_K(640)>; }; slot0_ns_partition: partition@C0000 { label = "image-0-non-secure"; reg = <0x000C0000 DT_SIZE_M(3)>; }; slot1_partition: partition@3C0000 { label = "image-1"; reg = <0x003C0000 DT_SIZE_K(640)>; }; slot1_ns_partition: partition@460000 { label = "image-1-non-secure"; reg = <0x00460000 DT_SIZE_M(3)>; }; storage_partition: partition@760000 { label = "storage"; reg = <0x00760000 (DT_SIZE_M(57) - DT_SIZE_K(384))>; }; }; 私の理解では、hello-world の例は非常に小さいSO、小さな (640kB) セキュア パーティション内に収まります。 残念ながら、現在のファームウェア (Wi-Fi、Bluetooth など) で同じことを実行すると、パーティションがオーバーロードされるというメッセージが表示され、コンパイルできません。 [...]/arm-zephyr-eabi/bin/ld.bfd.exe: zephyr\zephyr_pre0.elf section `rodata' will not fit in region `FLASH' [...]/arm-zephyr-eabi/bin/ld.bfd.exe: region `FLASH' overflowed by 1682828 bytes 総括する: mcuboot をコンパイルしてフラッシュCAN。また、hello-world の例を正しくフラッシュすることもCAN (UART からこの hello-world アプリを正しくロードできることを確認できます)。一方、「大きな」ファームウェアをコンパイルすることはできません。 メインファームウェアが配置される非セキュア領域にのみジャンプする、最小限のセキュアパーティションを持つイメージを生成するにはどうすればよいでしょうか? FUTUREこの安全なパーティションを使用する予定なので、現在のパーティション構造を維持したいと考えています。 ありがとうございました。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ さん、お元気ですか。 パーティションのサイズを変更する場合は、パーティションの場合と同様にオーバーレイ ファイルで行うことができますが、MCUboot が対象のパーティション内のイメージを認識できるように構造を維持する必要があります。 さらに、フラッシュ パーティションを共有して使用する場合、これは TF-M スタックで使用することを意図しており、TF-M スタックでも MCUboot をセキュア ブートローダーとして使用して、安全な環境でイメージを検証およびロードすることになるため、注意してください。 保護されたストレージの詳細については、Zephyr リファレンス ドキュメントの「Secure Storage」を参照してください。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition 少しは進歩しました。短期的な解決策として、frdm_rw612_common.dtsi ファイル内の slotx_partition を slotx_ns_partition と反転し、より大きなセキュア パーティションをコンパイルしてCAN使用します。 オーバーレイ ファイルでこれを変更すると、コンパイルはCANますが、実行時に mcuboot はイメージにジャンプできなくなります。mcuboot が生成されると、現在のプロジェクトではオーバーレイ ファイルが使用されないと思われます。 とにかく、セキュアなパーティションと非セキュアなパーティションの違いがよく分かりません。ファームウェア全体をセキュアパーティションに格納することには、何か欠点がありますか? このプロジェクトに PSA_protected_storage を追加する方法がまだわかりません。この機能を追加すると、どのパーティションがこの機能に使用されますか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 問題はあなたのサンプルと同じです。フラッシュ サイズ 640kB (デフォルトのセキュア パーティション サイズ) を超えるとすぐに、コンパイル時に次のエラーが発生します。 領域「FLASH」が15872バイトオーバーフローしました このsmp_svrサンプルにBTとUDPのサポートを追加すると、エラーが表示されます。 SO、私のこれまでの質問はすべて、私の問題を理解し解決するために残っています。 メインファームウェアが配置される非セキュア領域にのみジャンプする、最小限のセキュアパーティションを持つイメージを生成するにはどうすればよいでしょうか? これら両方のパーティションを処理するファームウェアを生成するにはどうすればよいでしょうか? psa_protected_storage を使用する場合、暗号化されたデータはどこに保存されますか?この機能を使いたいです。 さらに、ファイル用のカスタムの不揮発性パーティションが必要になりますが、これは common.dtsi のパーティション テーブル定義の現在の storage_partition ですか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 。 MCUboot を使用して OTA を実行する必要がある場合は、「smp_svr」サンプルを使用することをお勧めします。このサンプルの主な目的は、MCUmgr プロトコルで使用するファームウェアの更新を行い、Bluetooth、UDP、UART などを介して更新を可能にすることです。このサンプルは MCUboot と連携して、適切に署名されたバイナリを確認し、MCU に更新します。 サンプルをテストするには、ファームウェアのアップデートを行うために MCUmgr クライアントをダウンロードする必要があり、最初に MCUboot を個別にビルドしてフラッシュし、次に smp_svr サンプルの prj.conf ファイルに必要なマクロを追加して smp_svr サンプルをビルドしてフラッシュする必要があります (これは、使用する OTA トランスポートによって異なります)。これが完了すると、システムは MCUmgr クライアントと適切に通信して、アップロードされたイメージのリストを確認し、新しいイメージをロードできるようになります。 MCUboot の新しい有効なイメージをロードするには、ロードするサンプルの prj.conf ファイルに次の構成を追加することをお勧めします。 CONFIG_HEAP_MEM_POOL_SIZE=2048 次のようにすると、サンプルをビルディングするだけで、MCUboot の有効な署名付きイメージを生成できます。 CONFIG_MCUBOOT_SIGNATURE_KEY_FILE=" /root-rsa-2048.pem" CONFIG_MCUBOOT_GENERATE_CONFIRMED_IMAGE=y CONFIG_BOOTLOADER_MCUBOOT=y これがあなたにとって有効であり、あなたの要件を満たしているかどうかを教えてください。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こちらの投稿を読みました: https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Zephyr-MCUBoot-TFM-Demo-using-RW612/ta-p/2047528 tfm 構造をより深く理解するために、「psa_protected_storage」サンプルもダウンロードしましたが、イメージをどのようにパーティション分割するかはまだよくわかりません。 たとえば、psa_protected_storage の場合、暗号化されたデータを保存するために使用されるパーティションはどれですか?それは「storage_partition」にありますか? 上記の投稿では、fw_storage パーティションについて言及しています。このパーティションはありませんが、Wi-Fi は使用できます。 最新のドキュメントはどこにありますか?何か特別なことをしようとしているわけではなく、mcuboot を使用して OTA を実行できるようにしたいだけですが、その方法を理解するための正しいドキュメントを見つけるのに苦労しています。 ご回答をよろしくお願いします。 アーサー Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 正直に言うと、分かりません。最初の投稿で述べたように、frdm_rw612 パーティション分散が推奨される方法であると思われるため、それに従うことにしました。 まだプロトタイプなので、現時点では安全な機能は使用していませんが、間もなく製品版に取り組む予定であり、後で問題になるような選択を今日はしたくありません。 FRDM_RW612 には、640kB のセキュア パーティションと 3MB の非セキュア パーティションがあります。 現在のアプリケーションのサイズは 2.3 MB です (最適化はまったく行われていません)。 これら両方のパーティションを処理するファームウェアを生成するにはどうすればよいでしょうか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ さん、お元気ですか。 ご希望のパーティション配分をご確認ください。小さくて安全でないパーティションと大きくて安全なパーティションですか、それともその逆ですか?さらに、アプリケーションのサイズも共有していただけますか? いずれのCASEでも、各パーティション サイズ 128kB の配置を考慮して、オーバーレイ ファイルを使用してパーティション サイズを変更できるはずです。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition 親愛なるローマンへ 私の質問に答えてくれないので、完全に理解するのは困難です。 「ただし、構造を維持する必要があります」と言うとき、最初にセキュアなパーティションがあり、その後に非セキュアなパーティションがあることを意味しますか? このプロジェクトに PSA_protected_storage を追加する方法がまだわかりません。この機能を追加すると、どのパーティションがこの機能に使用されますか? メインファームウェアが配置される非セキュア領域にのみジャンプする、最小限のセキュアパーティションを持つイメージを生成するにはどうすればよいでしょうか? これら両方のパーティションを処理するファームウェアを生成するにはどうすればよいでしょうか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 ありがとう、よく理解できました。 このリンクはエンジニアリング チームによって作成されたものですか?https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Zephyr-MCUBoot-TFM-Demo-using-RW612/ta-p/2047528 それでも SDK をこのように変更する必要がありますか?「非セキュア イメージの変更」セクションで説明されているように、非セキュア イメージを変更できないためです。nxp_zephyr\zephyr\に「build」フォルダが存在しません さらに、frdm_rw612_rw612_ns.dts ファイルには、frdm_rw612_common.dtsi ですでに構成されているすべてのパーティションを削除する行があります。パーティション構造を維持するというアイデアには従いません。 とにかく、非セキュアボードを使用すると、ストレージパーティションを使用しているためコンパイルされず、/delete-node/行でストレージパーティションが存在しなくなります。 &w25q512jvfiq { /delete-node/ partitions; partitions { compatible = "fixed-partitions"; #address-cells = <1>; #size-cells = <1>; slot0_ns_partition: partition@080C0000 { label = "image-0-non-secure"; reg = <0x080C0000 DT_SIZE_M(3)>; }; /* This partition is reserved for connectivity firmwares storage * and shouldn't be moved. */ fw_storage: partition@400000 { label = "fw_storage"; reg = <0x400000 0x280000>; read-only; }; }; }; 「開発は独自で行う必要がある」とおっしゃるのは、TF-M を公式にサポートしていないということですか?それで、SDK を手動で変更する必要があるのですか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 。 はい、そのガイドは当社のエンジニアリングチームによってZephyrバージョン4.0.0で使用するために作成されました。ただし、おっしゃるとおり、それ以降のバージョン (現時点では 4.2.0 および 4.3.0) では、ガイドに示されている TFM の例に BL2 統合 (セキュア ブートローダとしての MCUboot) がデフォルトで含まれているため、このガイドは必要ありません。したがって、バージョン 4.2.0 ダウンストリームおよびアップストリーム、および 4.3.0 では、この機能はすでにサポートされています。 これで疑問が解消されることを願っています。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 わかりました。理解が深まりました。 frdm_rw612_rw612_ns.dts ファイルでこれを削除すると、tfm を使用してファームウェアをコンパイルできます。 &w25q512jvfiq { /delete-node/ partitions; partitions { compatible = "fixed-partitions"; #address-cells = <1>; #size-cells = <1>; slot0_ns_partition: partition@080C0000 { label = "image-0-non-secure"; reg = <0x080C0000 DT_SIZE_M(3)>; }; /* This partition is reserved for connectivity firmwares storage * and shouldn't be moved. */ fw_storage: partition@400000 { label = "fw_storage"; reg = <0x400000 0x280000>; read-only; }; }; }; パーティション ノードを削除する目的がわかりません。 とにかく、「tfm_merged.hex」をフラッシュすると、次のような出力が得られます: [INF] Starting bootloader [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [INF] PSA Crypto init done, sig_type: EC-P256, using builtin keys [INF] Image index: 1, Swap type: none [INF] Image index: 0, Swap type: none [INF] Bootloader chainload address offset: 0x20000 [INF] Image version: v0.0.0 [INF] Jumping to the first image slot Booting TF-M v2.2.0+g9a6c6f958 [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [Sec Thread] Secure image initializing! [INF][PS] Encryption alg: 0x5500100 [INF][Crypto] Provision entropy seed... [INF][Crypto] Provision entropy seed... complete. bl2 は正常に起動しているように見えますが、その後何も起こりません。安全でないファームウェアが起動しません。 ファイル zephyr_ns_signed.hex もフラッシュしようとしましたが、結果は同じでした。 私がそう思うのは間違っているだろうか boot_partitionはbl2(mcuboot)があるパーティションです slot0_partitionはtfm(psa)のパーティションです slot0_ns_partitionはファームウェアのパーティションです   この安全でない構成は、sysbuild を有効にして mcuboot をビルドすることと互換性がないことを確認しますか?ここで説明されているように: https://community.nxp.com/t5/Zephyr-Project-Knowledge-Base/Zephyr-app-with-MCUboot-in-VS-Code/ta-p/2089541 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 。 TF-MとBL2を使ってアプリケーションをビルドしてフラッシュする際に、どのような手順を踏んでいるのか教えていただけますか?MCUbootのビルドにはsysbuildを使用していますか? さらに、パーティションはおっしゃるとおり、セキュア パーティションは TF-M のセキュア サービスをホストするためのもので、非セキュア パーティションは非セキュア アプリケーション用になります。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition sysbuild の場合: tfm用に変更したプロジェクトでsysbuildを有効にし、このCmake Extra Args SB_CONFIG_BOOTLOADER_MCUBOOT='y'を追加します。 「純粋なビルド」をすると、さまざまなものがコンパイルされます 最後にこのメッセージが表示される image.py: sign the payload image.py: sign the payload Usage: imgtool.py sign [OPTIONS] INFILE OUTFILE Try 'imgtool.py sign -h' for help. Error: Image size (0x1ed91c) + trailer (0x1b0) exceeds requested size 0xa0000 image.py: sign the payload Batch file failed at line 12 with errorcode 2 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 sysbuild を使用するとさらに悪くなります。これは、hello_world の例 (つまり、mcuboot もパーティション分割も使用しない) から作成した現在のプロジェクト (Wifi、Bluetooth、イーサネット などの多くの機能がすでに実装されている) で行っていることです。 デバッグ構成では、ボードを frdm_rw612 から frdm_rw612/rw612/ns に変更します。そして、DTC_OVERLAY_FILE='boards/frdm_rw612.overlay' を明示的に設定します(現在のプロジェクトで使用しているオーバーレイファイルと同じものを保持するため)。 prj.confに以下の内容を追加します 前回のメッセージでお伝えした内容をfrdm_rw612_rw612_ns.dtsファイルから削除します プロジェクトを右クリックして「選択したターゲットをフラッシュ」し、tfm_merged.hexを選択します。 prj.confに追加する内容 CONFIG_BUILD_WITH_TFM=y CONFIG_WIFI_NXP=y CONFIG_NXP_RW610=y CONFIG_ETH_DRIVER=y # stack size CONFIG_SHELL_STACK_SIZE=6144 CONFIG_SYSTEM_WORKQUEUE_STACK_SIZE=2048 CONFIG_NET_MGMT_EVENT_STACK_SIZE=4608 CONFIG_NET_TCP_WORKQ_STACK_SIZE=2048 CONFIG_MAIN_STACK_SIZE=4096 CONFIG_IDLE_STACK_SIZE=1024 コンソールに表示される内容: [INF] Starting bootloader [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [INF] PSA Crypto init done, sig_type: EC-P256, using builtin keys [INF] Image index: 1, Swap type: none [INF] Image index: 0, Swap type: none [INF] Bootloader chainload address offset: 0x20000 [INF] Image version: v0.0.0 [INF] Jumping to the first image slot Booting TF-M v2.2.0+g9a6c6f958 [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [Sec Thread] Secure image initializing! [INF][PS] Encryption alg: 0x5500100 [INF][Crypto] Provision entropy seed... [INF][Crypto] Provision entropy seed... complete. 出力結果から判断すると、すでにブートローダーが存在するため、sysbuild を有効にしませんでした。 何が間違っているのか教えていただけますか? ご協力の程、よろしくお願い申し上げます。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 私が何を間違っているのか教えてもらえますか?今週ファームウェアを公開するためには、解決策を見つけることが私にとって非常に重要です。 ご協力いただきありがとうございます Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 、遅くなってごめんなさい。 BL2 を搭載した TF-M で基本ファームウェアを生成してみましたが、正常に動作しています。frdm_rw612_rw612_ns.dts ファイルから、ご指摘のセクションを削除する理由は理解できますが、このオーバーレイはボードの非セキュア「バージョン」で TF-M が使用するパーティション構造を設定するものであるため、この手順は必須です。これを削除すると、互換性のない構造が生成され、アプリケーションが MCUboot の既知のアドレスにロードされない可能性があります。 プロジェクトで生成された dts ファイルを共有していただけますか?それとも、dts のパーティション セクションのスクリーンショットでしょうか?プロジェクト内の次のパスに配置する必要があります: debug/zephyr/zephyr.dts ご辛抱いただきありがとうございます。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 申し訳ありませんが、まだ同じ質問があります。 1. sysbuild を有効にする (および SB_CONFIG_BOOTLOADER_MCUBOOT="y" を設定する) 必要がありますか? 2. prj.conf に追加している内容は正しいですか? 3. すべてがコンパイルされたら何をフラッシュする必要がありますか? パーティション ノードの削除を維持する必要があると言われています。次に、このシナリオにおける私の問題点は次のとおりです。 現在のファームウェアでは、common.dtsi で定義された storage_partition を使用しています。非セキュア構成を使用すると、すべてのパーティションが削除されるため、storage_partition が定義されなくなり、コードをコンパイルできなくなります。4. この非セキュア構成で storage_partition を使用するにはどうすればよいですか? common.dtsi で定義された同じパーティション構造を維持する必要があると明示的に述べられました。5. では、なぜ fw_storage パーティションは 0x400000 に配置されているのでしょうか?common.dtsi 構造を調べてみると、これは slot1_partition にあります。 6. ところで、この fw_storage パーティションとは何でしょうか?なぜ「標準」の安全な構成ではないのですか? あまり時間がないのは承知していますが、私の 6 つの質問にご回答ください。それが私の理解を深め、自立するのに役立ちます。 storage_partition と Wifi/BLE コネクティビティを使用して標準ファームウェアをコンパイルおよびフラッシュするための、ステップバイステップの TF-M と BL2 の例を共有していただければ完璧です。ありがとう PS: 現状では意味をなさないため、DTS のパーティション セクションは共有しませんでした。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 。 sysbuild を有効にする (および SB_CONFIG_BOOTLOADER_MCUBOOT="y" を設定する) 必要がありますか? いいえ、TF-M ビルド システムにはデフォルトで MCUboot が含まれているため、sysbuild を使用する必要はありません。 prj.conf に追加している内容は正しいですか? はい、観察してみると、ボードの非セキュア バージョン用のプロジェクトを作成するときに、「CONFIG_BUILD_WITH_TFM」がデフォルトで設定されます。 すべてがコンパイルされたら何をフラッシュする必要がありますか? それは状況によりますが、TF-M ビルド システム Zephyr ドキュメントのスクリーンショットには、生成された各ファイルのユーティリティに関する詳細な説明があります。 ただし、初めて使用する場合、MCUboot ブートローダ、TF-M セキュア イメージ、および非セキュア アプリケーションのマージを含む tfm_merged.hex ファイルをフラッシュする必要があることに注意してください。 この安全でない構成でストレージ パーティションを使用するにはどうすればよいですか? TF-M 構成のフラッシュ レイアウトではこのストレージ用のスペースが予約されているため、ユーザーは TF-M が提供する安全なストレージ サービスを使用することが予想されます。 ところで、この fw_storage とは何でしょうか? fw_storage パーティションは、Wi-Fi、BLE、および 802.15.4 ファームウェア ストレージ用に予約されています。 この情報があなたの開発に役立つことを願っています。ご辛抱いただきありがとうございます。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 明日ファームウェアを公開しなければならないのですが、返信を期待できますか?それとも、まだあなたの側で準備ができていないので、プラン B を見つける必要がありますか? ご回答をよろしくお願いします。 アーサー Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 フィードバックありがとうございます。パーティション構造に関する質問には回答しませんでした 5. では、なぜ fw_storage パーティションは 0x400000 に配置されているのでしょうか?common.dtsi 構造を調べてみると、これは slot1_partition にあります。 1.この fw_storage は重要と思われますが、なぜ「セキュア」構成で言及されないのでしょうか? 2. このパーティションに必要なファームウェアを配置するには、何か特別な操作を行う必要がありますか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ さん、お元気ですか。 ご質問にお答えすると、Wifi ファームウェアは自動的にロードされるものと予想されます。ただし、この問題については社内で確認中です。 ご辛抱いただきありがとうございます。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 コンパイルしてフラッシュしてみました(tfm_merged.hex)基本サンプル用。zephyr/samples/hello_world を使用すると次のようになります: [INF] Starting bootloader [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [INF] PSA Crypto init done, sig_type: EC-P256, using builtin keys [INF] Image index: 1, Swap type: none [INF] Image index: 0, Swap type: none [INF] Bootloader chainload address offset: 0x20000 [INF] Image version: v0.0.0 [INF] Jumping to the first image slot Booting TF-M v2.2.0+g9a6c6f958 [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [Sec Thread] Secure image initializing! [INF][PS] Encryption alg: 0x5500100 [INF][Crypto] Provision entropy seed... [INF][Crypto] Provision entropy seed... complete. *** Booting Zephyr OS build nxp-v4.1.0-23883-g5fbcfde7cfc2 *** Hello World! frdm_rw612/rw612/ns SO、すべてが期待どおりに機能しているようです。 ただし、zephyr/samples/net/wifi/shell のような WiFi を使用する例を使用すると、ファームウェア (WiFi と BLE を使用) と同じ出力が得られます。 [INF] Starting bootloader [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [INF] PSA Crypto init done, sig_type: EC-P256, using builtin keys [INF] Image index: 1, Swap type: none [INF] Image index: 0, Swap type: none [INF] Bootloader chainload address offset: 0x20000 [INF] Image version: v0.0.0 [INF] Jumping to the first image slot Booting TF-M v2.2.0+g9a6c6f958 [WRN] This device was provisioned with dummy keys. This device is NOT SECURE [Sec Thread] Secure image initializing! [INF][PS] Encryption alg: 0x5500100 [INF][Crypto] Provision entropy seed... [INF][Crypto] Provision entropy seed... complete. したがって、問題の根本的な原因は Wi-Fi にあり、ファームウェア パーティションに関する私の質問に関連している可能性があります。Wifi と tf-m を使用してサンプルをコンパイルする手順を共有していただけますか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ 。 ホリデーシーズンのため、返答にかかるおおよその時間をお伝えすることはできませんが、何か分かり次第お知らせいたします。 ありがとう。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 ご協力いただきありがとうございます。到着予定時間はどれくらいですか?数日ですか、それとも数週間ですか? Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは@_arthur_ さん、ありがとうございます。あなたにとっても 2026 年が幸せな年になりますように! このマターに関して社内チームからの返答をまだ待っていますので、返答が届き次第お知らせします。 Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、ローマン。 2026年もNXPとあなたの成功を祈っています このトピックに関して何かニュースはありますか? ありがとうございました。 アーサー Re: Generate a firmware for mcuboot with a small non secure partition and a secure partition こんにちは、 @_arthur_ さん。この件についてお待たせして申し訳ありません。 ZephyrのWi-Fi ShellサンプルをTF-Mでビルドした際に、アプリケーションが正しく起動しないという問題が発生していた件について、prj.confファイルに以下の設定を追加してみてください。 # General CONFIG_HEAP_MEM_POOL_SIZE=122880 # TF-M S CONFIG_TFM_BL2=y CONFIG_BUILD_WITH_TFM=y CONFIG_TFM_PROFILE_TYPE_NOT_SET=y # Update the flash base address of ns image CONFIG_FLASH_BASE_ADDRESS=0x80C0000 # TF-M IPC CONFIG_TFM_IPC=y CONFIG_TFM_ISOLATION_LEVEL=2 # TF-M NS CONFIG_HWINFO=y # Networking (TF-M NS) CONFIG_NETWORKING=y CONFIG_NET_L2_ETHERNET=y CONFIG_NET_SOCKETS=y CONFIG_NET_DHCPV4=y CONFIG_NET_IPV4=y CONFIG_NET_TCP=y CONFIG_DNS_RESOLVER=y CONFIG_ETH_DRIVER=n CONFIG_WIFI=y # NXP Networking (TF-M NS) CONFIG_WIFI_NXP=y CONFIG_NXP_RW610=y CONFIG_NET_MGMT_EVENT_QUEUE_SIZE=20 CONFIG_NET_BUF_DATA_SIZE=1744 CONFIG_NET_SOCKETS_POLL_MAX=12 CONFIG_ZVFS_OPEN_MAX=30 CONFIG_PSA_CRYPTO_ENABLE_ALL=y これらの設定により、シェルアプリケーションが正常に起動するはずです。しかしながら、現在社内チームで確認中の動作として、「wifi scan」コマンドを使用するとアプリケーションがハードフォルト状態になるという問題があります。したがって、「wifi scan」の代わりに「nxp_wifi scan」コマンドを使用して、近くのネットワークをスキャンしてください。ただし、以下に示すように、デフォルトの「wifi connect…」コマンドを使用すれば、ネットワークに接続できるはずです。 これがあなたにとって有効かどうか教えてください。
View full article