1959710_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1959710_en-US

1959710_en-US

Enable C99 on Codewarrior 10.6

Good morning,

I would like to enable C99 for CW 10.6 v. I use the micro mc9s08ac32, I looked in the manual and used the directive both ‘#pregma c99 on’ and ‘#define EWL_C99 1’, in both cases I found no success.

I probably need to enable it from the settings, but I couldn't find any option to enable it. I went to properties>C/C++ Build>Tool settings but i didn't see about C99, only HS08 compiler. 

Could you give me some advice?

Re: Enable C99 on Codewarrior 10.6

Hello Transidico 

Unfortunately CodeWarrior v11 also C90 compliance.

So far NXP doesn't have an IDE for HCS08 supporting C99.

Best Regards,

Jun Zhang

Re: Enable C99 on Codewarrior 10.6

Good morning, thank you for your kind reply.
I would be interested in using the C99 somehow for this micro, is there no way I can use it?
I understand that the compiler does not support it, is there no other compiler that is compatible?

If I install CodeWarrior 11.1v does it not support C99? Or is there not something that converts C99 to C90 for me?

Thanks

Re: Enable C99 on Codewarrior 10.6

Hello Transidico,

HCS08 compiler Compliants with C90 standards. C99 is not supported.

Thanks,

Jun Zhang


Tags (1)
No ratings
Version history
Last update:
‎11-22-2025 05:56 AM
Updated by: