Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
RT1020 BSP for RT-Thread RTOS        该软件包为RT-Thread RTOS配套的BSP板级支持包,默认支持官方开发板MIMXRT1020-EVK,用户可以针对该BSP移植到自己的prototype上面,当前RT1020_EVK板级包在RT-Thread v3.1.3版本编译通过并运行测试成功。使用时,需要将附件源码解压后拷贝到\rt-thread\bsp\imxrt路径下。 Products Product Category NXP Part Number URL MCU MIMXRT1021 i.MX RT1020 Crossover MCU with Arm® Cortex®-M7 core    Tools NXP Development Board URL i.MX RT1020 Evaluation Kit MIMXRT1020-EVK: i.MX RT1020 Evaluation Kit  SDK SDK Version URL RT-Thread_v3.1.3 https://github.com/RT-Thread/rt-thread/tree/v3.1.3  SDK_v2.6.1 mcuxpresso.nxp.com Industrial
記事全体を表示
Using TWR-SER2 with TWR-K70F120M for Ethernet TWR-K70F120M running MQX and RTCS can work with the Dual Phy on TWR-SER2. Below I list the modifications I did to the default BSP: 1) I add phy_dp83xxx.c and phy_dp83xxx.h to the bsp_twrk70f120m build project. These files are with MQX in /mqx/source/io/enet/Phy 2) I modify the BSP to use DP83xxx PHY for the Ethernet MACNET: in the /mqx/source/bsp/twrk70f120m/init_enet.c: #include "phy_dp83xxx.h" const ENET_IF_STRUCT ENET_0 = {      &MACNET_IF,      //&phy_ksz8041_IF,      &phy_dp83xxx_IF,      MACNET_DEVICE_0,      MACNET_DEVICE_0,      BSP_ENET0_PHY_ADDR,      BSP_ENET0_PHY_MII_SPEED }; 3) MDIO line requires an external pull up resistor, per DP83849I Data sheet. As I didn't have one at the moment, I enable internal pull up on MCU pin PTB0. in the /mqx/source/bsp/twrk70f120m/init_gpio.c: //pctl->PCR[0] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK; /* PTB0, RMII0_MDIO/MII0_MDIO   */ /* PTB0, RMII0_MDIO/MII0_MDIO   */ /* internal pull up enabled on MDIO */ pctl->PCR[0] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK; With these changes, the RTCS applications work over TWR-SER2 Dual PHY channel A. On TWR-SER2, J8 and J9 are un-shunted, SW1 = 11000000, SW2 = 10100000 on TWR-K70F120M, J18 is configured to disable 50 MHz OSC, as I use 50 MHz clock source from TWR-SER2 U504 50 MHz output. This clock is used to provide reference clock for the MCU (EXTAL), as well as for the Dual PHY X1 input (RMII reference clock). Real-Time TCPIP Communications Suite Re: Using TWR-SER2 with TWR-K70F120M for Ethernet Hi Hafiz, I have successfully used TWR-SER and TWR-SER2 cards with MQX4.1 Ethernet applications for the TWR-K70F120M independently (i.e. only using one tower serial card at a time and not using both cards simultaneously). Both TWR-SER and TWR-SER2 are running RMII and using the clock source from the respective TWR-SER(2) card to clock both the Ethernet PHY and the MCU which synchronizes the clock domains. I can just swap the cards and run the same application code. Note that when using the TWR-SER2 card I am only using one of the Ethernet ports ETH_A/J12. Regards, David Re: Using TWR-SER2 with TWR-K70F120M for Ethernet Hi I had made it work on BSP for TWR-K53N512, besides jumper settings listed above, I just applied changes mentioned in step 3. Thanks and Best Regards, Kan Re: Using TWR-SER2 with TWR-K70F120M for Ethernet Hi I had successfully run my Ethernet Driver on TWR-SER board for TWR-K70F120M but not working on TWR-SER2. 1. Is Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M?  According to this link, (Line: 241) it is not supported? 2. If supported, then is there any change in signal settings like (MDC, MDIO, CRS_DV, RXDn, RXErr, TXDn, TXEN and RMII_REF_CLK) as compared to TWR-SER board? Regards
記事全体を表示
FRDM-K64 Interrupt basic example using mbed Here you can find the code and project files for the Interrupt example, in this example 2 KBI interrupts are enabled, one assigned to SW2 and another to SW3, during the main routine the blue led is turned on, when the interrupt routines are triggered the blue led is turned off and the red or green led blink once, the interrupt was configured to detect falling edges only. Code: #include "mbed.h" DigitalOut Red(LED1); DigitalOut Blue(LED3); InterruptIn Interrupt(SW2); void blink() {     wait(.4);     Red=1;     Blue=0;     wait(.4);     Blue=1;     wait(.4); } int main() {     Interrupt.fall(&blink);     Blue=1;     while (1)     {         Red=!Red;         wait(.4);     } } Freedom Development Platform Kinetis K Series MCUs
記事全体を表示
Troubleshooting: Quick Fix Option in Problems View Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below: For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted. To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.  The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix. In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK. Now the problem should be resolved. Eclipse IDE Usage and Settings General Re: Troubleshooting: Quick Fix Option in Problems View Thanks for the sharing! The warning of the type "S32 project version problem" and "The hardware settings required for project" can be fixed by referring to this article.
記事全体を表示
TSN(Time-Sensitive Networking)とイーサネットによる車載ネットワークの構築 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このプレゼンテーションでは、主要なTSN(Time-Sensitive Networking)規格と、それらが自動車の要件とどのように関連しているかについて説明します。関連するIEEE® 802.1 TSN規格の概要と、これらを自動車環境で適用および使用する方法の例を示します。このセッションの終わりまでに、参加者はネットワークのユースケースに基づいて必要な機能を理解し、選択できるようになります。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このプレゼンテーションでは、主要なTSN(Time-Sensitive Networking)規格と、それらが自動車の要件とどのように関連しているかについて説明します。関連するIEEE® 802.1 TSN規格の概要と、これらを自動車環境で適用および使用する方法の例を示します。このセッションの終わりまでに、参加者はネットワークのユースケースに基づいて必要な機能を理解し、選択できるようになります。
記事全体を表示
FTF-MHW-N1923 超小型单芯片 Qi 低功耗无线发射器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 无需插入充电线即可为智能手机充电,增加了便利性,并可在公共场所进行移动充电。第一代无线充电器由 100 多个组件组成,价格过于昂贵,无法被大众市场采用。NXQ1TXH5 是一款单芯片 Qi 低功耗无线充电发射器,集成了 Qi 无线充电器的所有数字、模拟和电源功能。高集成度使得元件数量非常少,并且易于设计无线充电器。这也将无线充电器的成本降低了 3 倍。NXQ1TXH5 是一个真正的数字即插即用平台,无需外部模拟设计工作。您所需要的只是一块 2 层 PCB,其顶层具有信号和电源布线,底层采用全铜以实现热性能。在输入端连接电源和去耦器,在输出端连接 LC 电路以将电力传输到接收器,您的无线充电器就可以使用了! 观看视频演示 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 无需插入充电线即可为智能手机充电,增加了便利性,并可在公共场所进行移动充电。第一代无线充电器由 100 多个组件组成,价格过于昂贵,无法被大众市场采用。NXQ1TXH5 是一款单芯片 Qi 低功耗无线充电发射器,集成了 Qi 无线充电器的所有数字、模拟和电源功能。高集成度使得元件数量非常少,并且易于设计无线充电器。这也将无线充电器的成本降低了 3 倍。NXQ1TXH5 是一个真正的数字即插即用平台,无需外部模拟设计工作。您所需要的只是一块 2 层 PCB,其顶层具有信号和电源布线,底层采用全铜以实现热性能。在输入端连接电源和去耦器,在输出端连接 LC 电路以将电力传输到接收器,您的无线充电器就可以使用了! 观看视频演示 安全移动 | 医疗保健和可穿戴设备
記事全体を表示
AMF-AUT-T2348 - NXP 音频视频桥接 (AVB) 堆栈 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由于车辆不同端点之间的媒体、通信和 ADAS 流增加,以太网在新 OEM 平台中的应用正在加速。所需的服务质量和同步通常是通过实施音频视频桥接 (AVB) 规范或 AVB 的衍生产品来实现的。NXP 在市场上占据着独特的地位,因为我们有能力为汽车中的 AVB 提供完整的解决方案,包括端点(MPU 和 MCU)、PHY、交换机以及所需的软件堆栈。此外,软件堆栈功能齐全,包括关键但经常被遗忘的组件,例如媒体时钟恢复。了解 AVB 技术的基础知识,以及 NXP 如何帮助您在产品中部署 AVB。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由于车辆不同端点之间的媒体、通信和 ADAS 流增加,以太网在新 OEM 平台中的应用正在加速。所需的服务质量和同步通常是通过实施音频视频桥接 (AVB) 规范或 AVB 的衍生产品来实现的。NXP 在市场上占据着独特的地位,因为我们有能力为汽车中的 AVB 提供完整的解决方案,包括端点(MPU 和 MCU)、PHY、交换机以及所需的软件堆栈。此外,软件堆栈功能齐全,包括关键但经常被遗忘的组件,例如媒体时钟恢复。了解 AVB 技术的基础知识,以及 NXP 如何帮助您在产品中部署 AVB。
記事全体を表示
環境契約およびセキュリティのためのNXPプロセッサ <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> <meta http-equiv="Content-Type" content="text/html; charset=utf-8" />
記事全体を表示
SMI-N2003 Make Your Own 3D Printer with NXP Technology This class will show the benefits of NXP devices for 3D printing technology. The lecture will look at using microcontrollers, analog products, MOSFETs and other standard products as well as software algorithms like BLDC motor control to create a 3D printer. This class will show the benefits of NXP devices for 3D printing technology. The lecture will look at using microcontrollers, analog products, MOSFETs and other standard products as well as software algorithms like BLDC motor control to create a 3D printer. Smart Machinery & Industrial Automation
記事全体を表示
AUT-N1888 功率 MOSFET 在汽车应用中增强可靠性,提高效率 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次培训将讨论分立式功率MOSFET在动力总成、安全、底盘和车身控制等汽车应用中的使用,向将参会者介绍恩智浦最佳、最新的硅片和封装技术。 重点介绍采用电机控制燃料、机油和水泵的解决方案。 观看视频演示 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次培训将讨论分立式功率MOSFET在动力总成、安全、底盘和车身控制等汽车应用中的使用,向将参会者介绍恩智浦最佳、最新的硅片和封装技术。 重点介绍采用电机控制燃料、机油和水泵的解决方案。 观看视频演示 安全互联汽车和自动化汽车
記事全体を表示
USB ホスト大容量記憶クラス (MSC) の例 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> NXP SemiconductorsとOnChip Technologiesは提携して、USBホスト機能を備えたLPC1000、LPC2000、およびLPC3000ファミリのマイクロコントローラにUSBHostLiteソフトウェアを提供しています。これらには、LPC17xxシリーズ、LPC23xxシリーズ、LPC24xxシリーズ、LPC29xxシリーズ、LPC31xxシリーズ、およびLPC32xxシリーズのマイクロコントローラのメンバーが含まれます。USBHostLite は、OS レス環境で実行するための最小限のコードで USB 大容量ストレージ クラスのサポートのみを含む、簡素化された USB ホスト スタックです。USBHostLiteは、USBホストポートに接続されたUSBペンドライブ、USBハードディスクドライブなどのUSB大容量ストレージデバイス上のファイルにアクセスするための簡単なソリューションを提供します。 特長 USBHostLite は、次の機能をサポートしています。 オペレーティングシステムなしで動作 小さなメモリフットプリントが含まれています ソースコードはANSI Cで書かれており、IDEから独立しています 制御および一括転送をサポート FAT16ファイルシステムをサポート シンプルなファイルAPIにより、ファイルの読み取りおよび書き込み操作が可能 よく構造化され、理解しやすいソースコード 制限 NXPの無料のUSBHostLiteソフトウェアには、次の制限があります。 USBHostLiteは現在、Embedded ArtistsのLPC2468 OEMボードとKeilのMCB1760ボードにのみ移植され、テストされています。 大容量ストレージ以外のクラスはサポートされていません。 大容量記憶装置インターフェースは、最初の構成に存在する必要があります。 0 より大きい最大論理ユニット番号 (LUN) はサポートされていません。 FAT16 以外のファイルシステムはサポートされていません。 長いファイル名はサポートされていません。 ルートディレクトリ以外のフォルダにあるファイルにはアクセスできません。 アプリケーションで使用するバッファ・サイズは、4 KB を超えてはなりません。 注:このアプリケーションノートでは、USBHostLiteスタック全般と、特にEmbedded Artists LPC2468 OEMボードでのアプリケーションについて説明します。 ソフトウェア LPCソースコード用のUSBHostLiteは、NXPのお客様が無料で使用でき、NXPのLPC2000およびLPC3000ファミリのマイクロコントローラでのみ使用できます。USBHostLiteソフトウェアをダウンロードまたは使用することにより、これらのNXPマイクロコントローラーでのみ使用することに同意したことになります。Hitex LPC2939ボード上の LPC293x デバイスに移植されたUSBHostLiteスタック: LPC293x用のUSBHostLite VBeta 0.01 (2009/07/28) - 添付 Embedded Artists LPC2468 OEM ボード上の LPC2468 デバイスに移植された USBHostLite スタック: LPC23xx/LPC24xx用USBHostLite V1.00 (2010年1月4日) Keil MCB1760評価ボード上の LPC1768 デバイスに移植されたUSBHostLiteスタック: LPC17xx用のUSBHostLite VBeta 0.01 (2009/07/14) - 添付 OnChip Technologies LLCは、フル機能と量産品質の組み込みUSBスタックを必要とするお客様のアプリケーション向けに、USB仕様に完全に準拠し、優れた安定性と構成可能性を提供する組み込みUSBホスト/デバイス/OTGスタックを提供しています。 詳細情報 免責事項 このソフトウェアは、NXP Semiconductorsから現状のまま提供されます。NXP Semiconductorsは、情報提供以外の目的で、ここに含まれるソフトウェアをサポートまたは保証しません。サポートオプションやその他の組み込みUSBホスト/デバイス/OTGスタックなど、さらなる支援についてはOnChip Technologies LLCにお問い合わせください。 さらにサポートが必要な場合 オンチップテクノロジーズLLC LPC3000、LPC2000、およびLPC1000ファミリー向けのその他のプロフェッショナルUSBホストスタックソリューション CMXシステムCMX-USBホスト HCC組み込みUSB(EUSB)HostLiteスタック micrium μC/USBホスト マイクロデジタル smxUSBH Quadros RTXCusb ソフトウェア Thesycon組み込みUSBホストスタック
記事全体を表示
USBウェイクアップを備えた低電力モード <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Kinetisファミリには、豊富な低消費電力モードがあります。お客様は、低電力モードからウェイクアップする別の方法を理解するのに混乱する可能性があります。 1) VLPR では、VLPW: NVIC は割り込みの影響を受け続けるため、割り込みはすべて処理されます。 2)停止、VLPSでは、デバイスは USB ウェイクアップ割り込みによってのみウェイクアップできます。 3)LLSでは、VLLSx:デバイスはどの USB ソースから もウェイクアップ できません。 4) LLWUは ウェイク アップに使用されるため、お客様は利用可能なLLWU ウェイク アップソースのいずれかから ウェイク アップできます。 USBモジュールに関しては 、 USB 再開イベントには2つの異なる割り込みがあります。1つは、 USB ライン の状態の変化によって トリガーされる低電力モードから ウェイクアップ できるようにするための非同期です。もう 1 つは同期しており、K 状態 (フル スピードの場合は D+ = 0、D- = 1) を検出してから 2.5 us 後にのみトリガーされます。アプリケーションは、必要なときにいつでも低電力モードに移行する責任があり、この目的のために 、USB スタックによって報告されたデバイスの状態を確認する必要があります。バス で サスペンド状態が検出されると、SLEEP割り込みがトリガーされ、スタックの状態がサスペンドに変わります。その後、アプリケーションは低電力モードに移行します。この SLEEP 割り込みが発生すると、非同期 ウェイク 割り込みが有効になり、トリガーされると無効になります (これは、モジュールが割り込みをクリアするために必要です)。通常の状態では、同期再開割り込みまたはリセット割り込みが後でトリガーされ、スタックの状態が中断以外に遷移します。その後、アプリケーションは通信が再びアクティブになったことを認識し、再び低電力モードに入るのを回避できます。
記事全体を表示
FlexIOによるLEDパネル制御 [1] <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このプロジェクトの目的は、Kinetis K82マイクロコントローラに搭載されているFlexIOペリフェラルを使用してRGB LEDパネルを制御することです。 FlexIOペリフェラルは、GPIOビットバンギングやPWM + DMAを使用した他の制御方法と比較して、LEDの色と輝度情報を更新する過程で CPUをアンロード するという大きな利点を提供します。私は別の方法を使用します。 パネルは、WS2812BコントローラーとLEDストライプを使用します。また、アプリケーションを開発するためのシミュレーションプラットフォームも用意します。 ハードウェア: 30 x16 LED WS2812Bパネル マルチプレクサボード FRDM-K82の Uctronics QVGAディスプレイ ソフトウェア: IAR Workbench 7.50.1 (英語) SDK 1.3 for the Kinetis K82 FreeRTOS eGUIグラフィックライブラリ LEDパネルが機能している状態でビデオを見ることができます。 ビデオリンク : 4707 パート1:LEDパネルの構築 パート2:FlexIOを使用したLED制御方法 パート3:LEDパネルエミュレーション用ソフトウェア パート4:パネル制御用ソフトウェア モバイル Re:FlexIOによるLEDパネル制御[1] <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるグレイ、 ページが更新されましたので、ぜひご覧ください。 Re:FlexIOによるLEDパネル制御[1] <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるグレイ、 私たちは、ここで共有できるようにソフトウェアの更新に取り組んできましたが、現時点では、適切なライセンスを追加するまで、ソフトウェア以外のバージョンのみを共有することができます。更新されたソフトウェアが手に入り次第、オンラインにします。 参考までに、ここでも同様のプロジェクトがありますが、FlexIO:Kinetis K20によって駆動されるLEDビデオパネルは使用していません Re:FlexIOによるLEDパネル制御[1] <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。このプロジェクトに感謝します。さまざまなドキュメントにアクセスできないようです。私は得ています: 不正 この場所またはコンテンツへのアクセスが制限されています
記事全体を表示
テクニカルレポート 裏野Brazil.pdf <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ブラジル代表の浦野チームによるフリースケールカップWWファイナルズのテクニカルレポート <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ブラジル代表の浦野チームによるフリースケールカップWWファイナルズのテクニカルレポート Re:テクニカルレポート裏野Brazil.pdf <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちはルーカス、私たちはそれらを強制するために最善を尽くしています...確かに、英語が一番です。 Re:テクニカルレポート裏野Brazil.pdf <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> テクニカルレポートは英語でなければならないと思いましたか? ルールは明確ですが、尊重されていませんか? それともエラーですか? よろしくお願いいたします
記事全体を表示
Microwave Heating at 915 Mhz Presented by tiefengshi Presented at DwF RF Solutions - Chengdu - 9 April 2015 Presented by Tiefeng Shi Presented at DwF RF Solutions - Chengdu - 9 April 2015 RF
記事全体を表示
下载 .sdcard使用 MFGTool 的 i.MX6sx SabreSDB 图像 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我遵循 Yocto 培训直到任务#4 - 部署和测试......但我被困在这里。 我无法下载 .sdcard图像到我的 SD 卡。我需要先格式化它吗?它是全新的。 由于sudo dd if=core-image-base -imx6solosabresd .sdcard of=/dev/sdb1 bs=1M对我不起作用,我无法从主板上的 SD 卡启动。主板开关设置为从 SD4 卡启动。imx6solosabresd 是用于 solox 的正确 MACHINE 吗?我尝试在 local.conf 文件中设置 MACHINE=imx6sxsabersd,但收到了错误消息(任务 #2)。 这就是我想要尝试 MFGTool 的原因。我已将主板设置为从 SD3 启动,以便它可以进入“下载模式”。当我浏览 MFGTool 时,它显示没有设备连接,尽管出现了符合 HID 的供应商定义的设备。 本文件是根据以下讨论生成的:
記事全体を表示
I2C NCSWの使用例 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> NCSW(NetCommソフトウェア)は、フリースケールのPowerQUICCおよびQorIQプロセッサ・プラットフォームでの開発を迅速化するためのパッケージです。これには、NCDD(NetComm Device Drivers)およびその他のコンポーネントが含まれています。ここでは、バージョンGA_4.7でサポートされているP3041 I2Cを例にとり、NetCommソフトウェアの構造とデバイスドライバの使用状況を分析します。CW PA 10.3 は、ユースケースコードと互換性を持つために使用されます。
記事全体を表示
APF-ACC-T1551の <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、オートモーティブ・アプリケーションに最適なFreescale i.MX 6シリーズのアプリケーション・プロセッサの多くのインタフェースについて説明します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、オートモーティブ・アプリケーションに最適なFreescale i.MX 6シリーズのアプリケーション・プロセッサの多くのインタフェースについて説明します。
記事全体を表示
启动 LS1046A 当闪存为空或镜像损坏时,如何启动板卡?当根据需求修改 RCW 后,如何从各种启动模式启动板卡?本文档将以全新的 LS1046ARDB 板卡为例介绍相关功能(文档中所有目标板均为 LS1046ARDB)。 内容 通过 CodeWarrior TAP 启动 LS1046A 从 SD 卡启动 从 RCW 源文件编译 PBL 二进制文件 将 PBL 二进制文件编译为固件 将固件编程到目标板(LS1046ARDB) 从QSPI启动 从 RCW 源文件编译固件 将固件编程到目标板(LS1046ARDB) 从eMMC启动 启用板载 eMMC 从 RCW 源文件编译固件 将固件编程到目标板(LS1046ARDB) QorIQ LS1设备
記事全体を表示
[Sharing/i.MX8MP]Download image via USB OTG2 on i.MX8MP On i.MX8MP EVK, image is downloaded into eMMC/SD via OTG1, if customer wants to enable USB OTG2 on i.MX8MP for uuu tool. Pls find modification as attached. Linux Re: [Sharing/i.MX8MP]Download image via USB OTG2 on i.MX8MP How to use the files?
記事全体を表示