Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
Pull RTSP stream failed on i.MX 8MP hi,  community # iMX 8MP @ Harvey021 I missed an issue during pull rtsp stream. The "RTSP_URL" has has been verified using VLC. Video coding: H264 command: gst-launch-1.0 rtspsrc location=$RTSP_URL queue ! rtph264depay ! v4l2h264dec ! autovideosink target image version: linux6.6.36 full target machine: i.MX 8mp Re: Pull RTSP stream failed on i.MX 8MP Hi, Is there more information? Best Regards, Zhiming Re: Pull RTSP stream failed on i.MX 8MP The video's fps is 10. The following is the detailed information. Re: Pull RTSP stream failed on i.MX 8MP Hi @noway  If you want to decode video for 60FPS, the maximum resolution is 1080p, the gstreamer has limited maximum resolution. The performance will decrease as the resolution increases on VPU. For the opencv, you can try below configuration. gst = f"rtspsrc location={RTSP_URL} protocols=tcp latency=50 ! " \ f"rtph265depay ! h265parse config-interval=-1 ! " \ f"decodebin ! videoconvert ! video/x-raw,format=BGR ! " \ f"queue max-size-buffers=1 leaky=downstream ! " \ f"appsink drop=true max-buffers=1 sync=false" cap = cv2.VideoCapture(gst, cv2.CAP_GSTREAMER) Best Regards, Zhiming Re: Pull RTSP stream failed on i.MX 8MP Thank you for your reply, the decoding is now working. However, I still have two issues: When I change the video resolution from 1080p to 2K, it cannot decode          Please refer to the attached file "pull.log" for the log.       2. When decoding with Python, I found it takes 0.4 seconds to get one frame of data - why is it so slow? Please refer to the attached file "rtsp.py" for the code. Re: Pull RTSP stream failed on i.MX 8MP Hi, Please try below command to split audio and video configuration. gst-launch-1.0 -v rtspsrc location=xxxxx name=src protocols=tcp latency=100 \ src. ! queue ! application/x-rtp,media=video,encoding-name=H264,payload=96 ! rtph264depay ! h264parse ! v4l2h264dec! videoconvert ! autovideosink \ src. ! queue ! application/x-rtp,media=audio,encoding-name=MPEG4-GENERIC,payload=97 ! rtpmp4gdepay ! aacparse ! avdec_aac ! audioconvert ! audioresample ! autoaudiosink Best Regards, Zhiming Re: Pull RTSP stream failed on i.MX 8MP He indicated that the avdec_h264 was not found.  And then I try the v4l2h264dec, Nor was it successful. Please refer to the attachment for the error log. trying command:  gst-launch-1.0 -v rtspsrc location=$RTSP_URL protocols=tcp latency=100 ! rtph264depay ! v4l2h264dec ! autovideosink > pull.log 2>&1 Re: Pull RTSP stream failed on i.MX 8MP Hi, Please try to use below command. gst-launch-1.0 -v rtspsrc location=$RTSP_URL protocols=tcp latency=100 ! rtph264depay ! avdec_h264 ! autovideosink Best Regards, Zhiming
記事全体を表示
某些处理器的示例未在 2.16.100 中构建,但在 2.16.000 中可以运行。 我正在尝试构建这个示例: evkmimx8ulp/multicore_examples/rpmsg_lite_str_echo_rtos 它使用 SDK 2.16.000构建,但在2.16.100中失败并出现以下错误: middleware_multicore_rpmsg_lite dependency does not meet, please check middleware/multicore/set_middleware_multicore.cmake. 该错误似乎是由提交“应用 2.16.100 发布更新” 中对 mcuxsdk-middleware-multicore 存储库中的 set_middleware_multicore.cmake 文件所做的更改引起的。请参阅此处的差异。 当CONFIG_DEVICE_ID或CONFIG_BOARD的值不属于受支持值列表之一时,就会触发我收到的错误消息。在2.16.000中, middleware_multicore_rpmsg_lite依赖项允许82 个可能的CONFIG_DEVICE_ID值和27 个可能的CONFIG_BOARD值,但在2.16.100中,这个数字减少到只有15 个可接受的CONFIG_DEVICE_ID值和9 个CONFIG_BOARD值。 这感觉是无意的。为什么小版本会放弃对超过 80% 的设备的支持?2.16.100的发行说明将mcux-sdk-middleware-multicore列为“没有源更改,只有清单版本更改” 。 生成这个.cmake的过程中是否出了问题2.16.000和2.16.100之间的文件?为什么在发行说明中没有提及的情况下大幅减少了支持的设备和主板? 如果有人能仔细看看这个我会很感激。 更多详情: 我使用以下命令从最初为空的目录中检索 SDK: 对于 2.16.000: west init -m https://github.com/nxp-mcuxpresso/mcux-sdk --mr "MCUX_2.16.000" west update 对于 2.16.100: west init -m https://github.com/nxp-mcuxpresso/mcux-sdk --mr "MCUX_2.16.100" west update 然后,在每种情况下,我进入示例的armgcc文件夹并运行build_release (Windows 上为.bat ,Linux 上为.sh )。 它可以使用2.16.000正常构建,但不能使用2.16.100正常构建。 回复:某些处理器的示例无法在 2.16.100 中构建,但在 2.16.000 中可以运行。 正如我在原始消息中指出的那样,SDK 2.16.000可以工作。因此,解决方案是:暂时使用 SDK 2.16.000而不是最新版本。
記事全体を表示
在 Windows 11 物联网企业版中获取 imx93evk 的 CPU 温度 你好,我正在使用 imx93-evk 板查询 Windows 11 IoT 上的 CPU 温度。 但是,无论使用命令还是第三方软件,我都无法查询温度。 如何查询 CPU 温度? #imx93 Re: Get CPU temperature on imx93evk in Windows 11 IoT Enterprise 嗨,KirkHsu: 我建议您 与 [email protected] 的物联网团队联系 。 此致 丹尼尔
記事全体を表示
i.MX95 decoder performance Hello. I have a question about the performance of the i.MX95 chip. We are planning to decode and output more than 16 channels of 640×480 @ 30 fps, 600 kbps video on the i.MX95. (1) Is this possible, and what is the maximum number of channels it supports? When we used the i.MX8QuadMax, its VPU only supported up to eight simultaneous decoders. (2) Does the i.MX95 also have a fixed number of hardware decoders like the QuadMax, or is its capacity determined dynamically by overall VPU performance? Also, with the i.MX8QuadMax we could only use GStreamer (no native decoder API was provided). (3) Does the i.MX95 offer a dedicated decoder API, or—like the QuadMax—must it be used solely through GStreamer? Thank you. Re: i.MX95 decoder performance Hi, For video decoding, the h264 decoder support 4k60 max or up to 32 streams. For VPU  simultaneous decoders number, it's decided by maximum DDR bandwith and maximum resolution. No native decoder API was provided. Best Regards, Zhiming
記事全体を表示
S32K344 CAN FD 当我使用 PCAN-USB pro 从 S32K344 接收 64 字节数据时。 PCAN-USB pro 只收到了前 8 个字节,剩下的 56 个字节丢失了。 当我使用 PCAN-USB pro 向 S32K344 传输 64 字节数据时。 S32K344 成功接收 64 字节数据。 Re: S32K344 CAN FD 平台:S32DS3.5 SDK:PlatformSDK_S32K3_S32K344_M7-5.0.0 我将示波器的通道 1 连接到 S32K344 的 CAN H,将通道 2 连接到 S32K344 的 CAN L,得到了以下波形。 我已经将 CAN 有效载荷设置为 64 字节,但是示波器上显示的 DLC 仍然是 8 而不是 64 字节。 Can_43_FLEXCAN-CanConfigSet-CanControllerCan_43_FLEXCAN-CanConfigSet-CanController Can_43_FLEXCAN-CanConfigSet-TRANSMITCan_43_FLEXCAN-CanConfigSet-TRANSMIT Can_43_FLEXCAN-CanConfigSet-RECEIVECan_43_FLEXCAN-CanConfigSet-RECEIVE Re: S32K344 CAN FD 您好, 尝试在发送信息后删除 Can_43_FLEXCAN_SetControllerMode 调用。不知道你为什么要停止/启动控制器。 BR, Petr Re: S32K344 CAN FD 我再次上传文件。 Re: S32K344 CAN FD 您好, 我无法查看/下载项目。因此,请务必根据需要更新 Can_PduInfo。 BR, Petr Re: S32K344 CAN FD 我正在使用MCAL来版本这个项目。 在上一条信息中,我附上了我的项目。 Re: S32K344 CAN FD 您好, 您是否正确设置了 tx_info 参数,以使用具有所需有效载荷大小的 CAN FD 帧? BR, Petr
記事全体を表示
MPC5744P ADC 在现场停止工作 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 我希望有人能紧急帮助我解决这个问题。 我们现场有一款产品,ADC 突然停止工作,ADC 值被冻结。这个问题只在现场出现,我们无法在测试实验室复制。我查阅了处理器手册,但没有找到任何可以在没有任何警告的情况下停止 ADC 转换的源代码。在 CPU 硬 RESET 后,ADC 开始正常工作。 我们还对 CPU 内部温度进行了监控,结果显示了同样的情况。 请解释一下造成这种现象的原因。是否可以在不重新启动 ADC 模块的情况下重新启动 ADC 模块? 谢谢! 此致, 阿里-梅拉伊 概述 Re: MPC5744P ADC stop working in the field 你好,我们也遇到了类似的问题。我们的芯片是 MPC5675K,使用 ADC 收集三个通道的数据。然而,不知从什么时候开始,数据不再同时工作了。我们已经在实验室测试了我们的设备是否有电子转账,但一直无法重现这个问题。对于 ADC 的突然冻结,我们目前束手无策。您有什么新的解决方案吗? Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 对不起,我想说我们不能重新启动。 我们进行了一些高分辨率示波器测量,发现当 HV 接通时,ADC 输入电压会在几微秒内超过 5V,然后才重新稳定下来。我们正在实验室密切关注这一问题,电子团队正在努力缓解这一问题。 我同意你的所有观点。 一旦我从实验室得到了一些范围图,我将向你们提供最新信息,并可能向你们提供更多有关我们发现的信息。 非常感谢彼得。 此致, 阿里-梅拉伊 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 问题在于我们可以 RESET 微型,因为这些 ADC 故障不会影响控制,但会限制产品功能。 你能还是不能?因为只有一种方法可以 RESET ADC模块和PBRIDGE(寄存器所在的位置),那就是系统 RESET。这也是我与设计部门讨论的结果。 此外,如果微波干扰与 EMI(900V 开关),我认为这对微波的整体概念也至关重要。 如何在如此严重的干扰下保证功能安全,从而使ADC模块停止工作。 其他模块也可能受到影响,如 FCCU、STCU 或类似模块,这些模块在 micro 运行期间并不一直在使用。 你看到的只是 ADC 问题,因为它一直在运行。 如果在微处理器处理 IVOR 或 FCCU 例程时开启高压,会对系统造成严重影响。 以上只是我的一些假设。 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 感谢您的测试。 问题在于我们可以 RESET 微型,因为这些 ADC 故障不会影响控制,但会限制产品功能。 产品已经交付给客户,我们可以对其进行任何修改,但我们正在进行内部调查,研究如何将 EMI 对 Mirco 的影响降至最低,以便对产品进行修改。临时解决办法是在现有产品出现故障时,以某种方式重新启动 ADC,使其重新联机。 所以我想你是在建议唯一的解决方案是 RESET Mirco 但没有其他方法可以让 ADC 恢复活力? 你是否建议先让 ADC 掉电,然后禁用时钟,然后重新启动时钟,然后重启 ADC 你认为这会再次重启 ADC 转换吗? 非常感谢彼得的帮助。 此致, 阿里-梅拉伊 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, PCTLx 将切断 ADC 的时钟。 请参阅参考手册: 59.3.52 ADC_0 外围设备控制寄存器(MC_ME_PCTL237) 但我刚刚进行了测试,它不会擦除 ADC 寄存器。(它们位于 PBRIDGE 上),因此在恢复 ADC 的时钟后,寄存器的值是相同的。 我想重置ADC寄存器的唯一方法是触发微型RESET。 如果你用子卡保护 ECU 免受 EMI 影响会发生什么?问题仍然存在吗? 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 我通过将掉电位设置为 1 来关闭 ADC 的电源,然后等到 ADC 状态更改为掉电然后重启它。我附上了 ADC 重新启动的代码。 我使用 SCAN 模式进行正常转换,而不是 CTU 模式。 因此,在代码启动时,通过将 NSTART 位设置为 1 来启动 ADC 一次,然后直接从 CDATA 读取数据 我附上了 ADC 配置和 ADC 每 1ms 读取一次的代码 希望这能解释 ADC 的设置方法。 为什么要停止转换?这是一个随机问题,因为它主要发生在接通高压(800V)电源时。这个问题与 EMI 有关,但它锁定了 CDATA 注册。我怎么能再次触发转换,因为我认为在扫描模式下不需要触发信号。 从 CDR 数据中提取数据时,有效位应该清零,但 CPU 处于该状态时,有效位不会清零。 您提到 PCTL 寄存器,请提供更多关于使用 PCTL 寄存器重启 ADC 的信息。 如果您需要更多信息,请告诉我。 此致, 阿里-梅拉伊 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 重启 ADC 模块并没有解决问题,因为即使尝试重启 ADC 模块,ADC 值仍然被冻结。 您是如何重启 ADC 模块的?您是否在 PCTL 寄存器中将其关闭,然后将模式转换到 RUNx 再返回? 能否请您帮助我了解 CDR 注册锁定的原因? 看来 ADC 转换已经完成,新的转换尚未启动。 (因此,ADC 不会卡住,而是处于定义状态并等待新的转换触发信号,无论是 SW 还是 CTU) 这我就不知道了,因为我对 ADC 的使用方法了解有限。 此致, Peter 注:如果在 ADC 转换卡住后通过调试器手动启动 ADC 转换,会发生什么情况?它会继续转换吗? Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 希望你一切顺利。 我有一个更新 重启 ADC 模块并没有解决问题,因为即使尝试重启 ADC 模块,ADC 值仍然被冻结。 我有注册快照,可以更深入地了解这个问题。 出现此问题时,ADC 模块工作正常,ADC 状态在状态 4 和 6 之间切换,但 CDATA 注册被冻结为固定值 CDR 寄存器 因此,它们都锁定为十进制 1171(十六进制 0x493)的相同值,有效位保持高电平 CPU 和 BandGap 显示了相同的行为。 能否请您帮助我了解 CDR 注册锁定的原因? 谢谢! 此致, 阿里-梅拉伊 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 好的,彼得,谢谢。我会记录 ADC 的状态,如果有更新,我会给您回复。 谢谢您, 阿里 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 很难说、 我从没试过这样做。 但是,如果时钟丢失,就无法从 PBRIDGE 上的寄存器中读取任何信息,而 ADC 也在该寄存器中。 但由于您能读取结果,我怀疑 ADC 转换未处于扫描模式,而是处于 IDLE 状态。 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 发生故障时,我会尝试将 ADC 状态保存在闪存中。 如果是时钟问题,那么你认为让 ADC 掉电并重启会恢复时钟吗? 此致, 阿里 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗯 最重要的是查看 ADC 是否仍在转换,但结果寄存器没有更新。 当 ADC 转换卡住时,测试 SW 应检查 ADC 状态并将其存储。 由于是扫描模式,我想只有时钟丢失才会导致这种情况。 但首先让我们看看出现问题时 ADC 是否仍在转换。 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 主要问题是我无法在 LAB 中复制故障,因此不确定 ADC 状态寄存器在现场的状态如何。 我已经准备了一个测试软件,可以在ADC值停滞时执行ADC RESET,所以我希望这能解决这个问题。 我尝试过将ADC电源置于3.3V以下,但随后MCU RESET,因此这不是导致问题的原因,因为我们在现场看不到CPU RESET。我还尝试改变 ADC 的参考电压,但这并不能阻止 ADC 模块工作。 是否有办法强制解决 ADC 硬件上的任何特定问题,使其卡住,例如您提到的 ADC 校准丢失? 如果出现电压问题,我将检查 FCCU 的故障反应,我认为该问题未配置为执行 RESET。 谢谢! 阿里 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 好吧,这些都是假设。 如果 ADC 功率下降或突破低压检测/HVD 阈值,则设备将执行通知并在启用后 RESET。 它可能导致ADC电容失准,或停滞在逻辑电平上,或许多其他原因。 如何启用和禁用 ADC? ADC 卡住时的状态是什么? 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 当发生这种情况时,计数被冻结在 1373 个计数上,再也无法恢复,因此我们必须执行电源循环。主要发生在高压电源启动时,但有时是随机的,在功能运行时也会发生。 我们已经在HV实验室测试了这些板,发现HV开启时ADC_HV和ADC_Ref出现峰值,但是ADC不会停止工作,它只发生在我假设电磁干扰水平很高的现场。HV 接通后,ADC_HV 和 ADC_ref 电压很快就会稳定下来。 您知道 ADC 在断电或出现噪音时会自动进入什么特定状态吗?重启 ADC 会有帮助吗? 此致, 阿里 Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 好吧,因为只有在接通 900V 时才会出现这种情况,所以我怀疑可能是电磁干扰问题。 出现这种情况时,ADC 电压测量值是多少?ADC ref 或 ADC_HV 是否存在尖峰? 测量的线路电压如何? 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,彼得、 谢谢您的答复。 我使用的是 SCAN(扫描)模式,时钟频率为 80Mhz。 我在启动任务中启动转换,该任务只执行一次。 只要应用程序需要,我就会从 CDATA Reg 中收集转换后的数据。 我们有自己的控制板用于测试。 当开启高压电源(即 900 伏直流)时,会出现此问题。因此可能与电磁干扰有关,但 ADC 始终无法恢复,并不断报告 1373 计数。这种情况只发生在现场,因为我们无法在高压实验室复制这个问题。 以下是 ADC 设置和读取的代码 谢谢! 阿里 ADC_0.MCR.B.OWREN = 1U; /* 启用结果覆盖 */ ADC_0.MCR.B.CTUEN = 0U; /* CTU 模式未启用 */ ADC_0.MCR.B.模式 =cdd_adc_continious_scan_conversion; ADC_0.MCR.B.ADCLKSEL = 1U; /* 80 Mhz 模式 */ ADC_0.MCR.B.PWDN = 0U; /* 启用 ADC0(将其从掉电模式中释放) */ /* NSTART 应该是设置的最后一个寄存器位 */ ADC_0.MCR.B.NSTART = 1; /* 启动正常模式 */ 读取 ADC 转换后的数据                                                                        Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,阿里、 从你提供的非常简短的描述来看,它可以是任何东西,从处理顶级任务到总线权限,再到未服务的 ADC 触发信号或时钟故障。 如果能告诉我们您如何使用 ADC(CTu 或 CPU 模式?) 如何触发转化 如何提供转换后的数据 因为它看起来真的像你的 SW 设计中没有服务的角落案例。 您的软件在恩智浦 EVB 上运行正常吗? 此致, Peter Re: MPC5744P ADC stop working in the field <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 谁能帮我解决这个问题? 此致, 阿里
記事全体を表示
S32K344 CAN FD MCAL Hi, NXP. EVB: S32K344 Environment: S32DS RTD 5.0.0 I am building the CAN FD project using MCAL. Is there any sample project i can refer to? Thanks. Re: S32K344 CAN FD MCAL Hi @IanHsueh You can refer to the examples in the RTD. They are the same as shown in this training presentation: S32K3XX COMMUNICATION MODULES: FLEXCAN WITH RTD AND LOW-LEVEL DRIVERS. These projects are configured for loopback, so you will need to enable normal/user mode and initialize the transceiver output pins (CAN_H & CAN_L). There are also some community posts with examples: Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMA test S32DS3.5 RTD400 - NXP Community Solved: S32K344 EVB With MCAL FLEXCAN TJA1153 - NXP Community Best regards, Julián
記事全体を表示
RT1166/RT1170 MIPI-CSI data convert between RGB888/RGB565 Hi We want to use RT1166/RT1170 to process MIPI-CSI RGB565 16-bit data, we want to receive the RGB56 data to RAM. Reference data:  AN13573  Reference thread: https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/iMXRT1176-MIPI-CSI2-to-UVC-reducing-the-frame-bu...   Method1: Sensor RGB565(A) output --> MIPI RGB565 --> RGB888 MIPI controller will save RGB888 to XRGB8888 PXP can convert XRGB8888 to RGB565(B). I think RGB565(B) should be same as RGB565(A) if we don't modify it between format converts. These conversions will not cause any difference between RGB565(A) and RGB565(B). Is it correct? Methold2: Can RT1166/RT1170 bypass the MIPI-CSI RGB565 data to RAM directly without RGB888 format convert? Regards Ken Re: RT1166/RT1170 MIPI-CSI data convert between RGB888/RGB565 @kensu  Method1: Sensor RGB565(A) output --> MIPI RGB565 --> RGB888 MIPI controller will save RGB888 to XRGB8888 PXP can convert XRGB8888 to RGB565(B). I think RGB565(B) should be same as RGB565(A) if we don't modify it between format converts. These conversions will not cause any difference between RGB565(A) and RGB565(B). Is it correct? A: Good question, I assume it should be correct. I don't have the hardware enviroment, but I suggest that you can refer to this example to setup and print them out.  https://github.com/nxp-mcuxpresso/mcux-sdk-examples/tree/main/evkbmimxrt1170/driver_examples/csi/mipi_rgb/cm7  Methold2: Can RT1166/RT1170 bypass the MIPI-CSI RGB565 data to RAM directly without RGB888 format convert? A: No, it can't. Please see Errata(116x), Erra(117x) to find below info, 'Due to an issue in the Video Mux Controller (VIDEO_MUX), raw data and YUV422 (10 bit) formats to the MIPI_CSI2 block are not supported ', it means: if the input data format is  RGB565, the MIPI_CSI converts it to RGB888 internally and sends to CSI. In other words, the CSI input data bus width is 24-bit. The CSI saves the frame as 32-bit format XRGB8888.' 
記事全体を表示
在 i.MX93 FRDM 上操作 ov2740 摄像头的设置 你好, 我正在尝试在 IMX93 FRDM 板上操作 OV2740 摄像头模块。 当我尝试捕获一帧时,v4l2-ctl 会挂起: root @imx93frdm:~# v4l2-ctl-d /dev/video0--set-fmt-video=width=1932,height=1092,pixelFormat=ba10--stream-mmap= 4--stream-count=1--stream-to=test_capture.raw--ver bose VIDIOC_QUERYCAP:ok VIDIOC_G_FMT:ok VIDIOC_S_FMT:ok 格式视频捕获多面: 宽度/高度:1932/1092 像素格式:''BA10''(10 位拜耳 GRGR/BGBG) 字段:无飞机数量:1 标志: 色彩空间:sRGB 传输功能:默认 YCBCR/HSV 编码:ITU-R 601 量化:全程平面 0:每行字节数:3864 大小图片:4219488 VIDIOC_REQBUFS 返回 0(成功)VIDIOC_QUERYBUF 返回 0(成功)VIDIOC_QUERYBUF 返回 0(成功) VIDIOC_QUERYBUF 返回 0(成功) VIDIOC_QUERYBUF 返回 0(成功)VIDIOC_ G_FMT 返回 0(成功)VIDIOC_QBUF 返回 0(成功) VIDIOC_QBUF 返回 0(成功)VIDIOC_QBUF 返回 0(成功) VIDIOC_QBUF 返回 0(成功)媒体图看起来像没事吧: root@imx93frdm:~# media-ctl -p 媒体控制器 API 版本 6.6.36 媒体设备信息 -------------------------------------------- 驱动程序 mxc-md 型号 FSL 捕获媒体设备串行总线信息平台:42800000.bus: camera hw revision 0x0 驱动程序版本 6.6.36 设备拓扑 -实体 1:mxc_isi.0(16 个焊盘,2 个链接,0 条路线) 类型 V4L2 子开发子类型未知标志 0 p ad0:水槽 <-" mxc-mipi-csi2.0 ": 4 [已启用] p ad1:水槽垫3:水槽垫 3:水槽垫板 5:水槽 垫 7:水槽垫 8:水槽垫 10:水槽 垫 11:水槽垫 12:来源-> " c_isi.0.capture ": 0 [已启用] pad13:来源 pad 14:来源 pad15:水槽 -实体 18:mxc_isi.0.捕获(1 个焊盘,1 个链接) 类型节点子类型 V4L 标志 0 设备节点名称 /dev/ video0 pad0:Sink <-" mxc_isi.0 ": 12 [已启用] -实体 22:mxc-mipi-csi2.0(8 个焊盘,2 个链接) 类型节点子类型 V4L 标志 0 设备节点名称 /dev/v4l-subdev0 pad0:Sink <-" ov2740 2-0036 ": 0 [启用,不可变] pad1:Sink p ad3:Sink pad4:来源-> " mxc_isi.0 ": 0:0 [ENABLED] pad5: Source pad6:来源 pad7: 来源 -实体 31:ov2740 2-0036(1 个焊盘,1 个链接,0 条路由) 类型 V4L2 子开发子类型传感器标志 0 设备节点名称 /dev/v4l-subdev1 pad0:来源 [stream: 0 fmt: sgrbg10_1x10/1932x1092 字段:无 crop.boundes 😞 0,0) /1932 x1092 crop:(0,0)/1932x1092] -> " mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE] My DTS : & clk { assigned-clocks =<& clk IMX93_CLK_CCM_CKO3>; assigned-clock-parents =<& clk IMX93_CLK_24M>; assigned-clock-rate =<24000000>; }; ov2740_mipi: ov2740_mipi@36{ 兼容 ="ovti,ov2740" ; reg =<0x36> ; pinctrl-names ="默认" ; pinctrl-0 =<& pinctrl_cam_mclk> ; clocks =<& clk IMX93_CLK_CCM_CKO3> ; assigned-clocks =<& clk IMX93_CLK_CCM_CKO3> ; 分配的时钟频率 =<24000000> ; 时钟名 ="xclk" ; 时钟频率 =<24000000> ; reset-gpios = < & pcal6524 22 GPIO_ACTIVE_LOW >; csi_id =<0> ; mipi_csi; 旋转 =<0> ; 方向 =<2> ;   status ="okay" ;   端口 { ov2740_mipi_ep:端点 { remote-endpoint =<& mipi_csi_in_ep> ; 总线类型 = <4>; data-lanees =<1 2> ; 时钟-非连续; link-frequencies = /bits/ 64<360000000> ; }; }; &cameradev { status ="okay" ; };   &isi_0 { status ="okay" ;   cap_device { status ="okay" ; }; };     &mipi_csi { status ="okay" ; FSL,RX-lanees =<2> ; csis-hs-settle =<16> ;   /* 端口 0:来自传感器的水槽 */ 端口@0 { reg =<0> ; mipi_csi_in_ep: 端点 { remote-endpoint =<& ov2740_mipi_ep> ; data-lanees =<2> ; cfg-clk-range =<28> ; hs-clk-range =<0x16> ; 总线类型 = <4>; 时钟-非连续; }; }; }; 驱动程序是来自 linux-imx scargapth 的 ov2740 驱动程序。我修改了它以匹配 DT,并更改了 PLL 配置以匹配 24MHz 时钟: 以下是摄像机数据表: www.elinfor.com/pdf/OmniVision/OV2740-OmniVision.pdf 请注意,我的模块稳压器连接到 3.3 伏电压,因此我没有在 DTS 中定义稳压器,如有任何建议 BR Basel Re: Settings to operate ov2740 camera on i.MX93 FRDM 嗨,@BaselHn! 您可以通过以下链接申请定制驱动程序: https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and-microcontrollers:PREMIUM-SUPPORT 致以最崇高的敬意, Chavira Re: Settings to operate ov2740 camera on i.MX93 FRDM 你好@Chavira 在这种情况下,有哪些支持选项? BR Basel Re: Settings to operate ov2740 camera on i.MX93 FRDM 嗨,@BaselHn! 遗憾的是,i.MX93 平台不支持 OV2740 摄像头模块。当前的 Linux 电路板支持包、设备树配置和驱动程序未设置为可与该传感器配合使用,这可以解释您在帧捕获 1 期间遇到 v4l2-ctl 挂起的问题。 为了获得最佳的兼容性和性能,我们建议在 i.MX93-FRDM 板上使用经过验证的摄像头模块之一。这些模块在电路板支持包中经过测试和支持,可确保更顺畅的集成和功能。 如果您仍希望继续使用 OV2740,则需要自定义驱动程序开发和设备树修改,这不属于标准支持的范围。 致以最崇高的敬意, Chavira Re: Settings to operate ov2740 camera on i.MX93 FRDM 你好@Chavira 哪些驱动程序未配置为与之配合使用? 我们需要打什么补丁才能使它们与该相机模块配合使用? BR Basel Re: Settings to operate ov2740 camera on i.MX93 FRDM 你好@BaselHn、 遗憾的是,iMX93 平台不支持该相机。当前的 Linux 电路板支持包、设备树和驱动程序未配置为可与之配合使用。 致以最崇高的敬意, Chavira Re: Settings to operate ov2740 camera on i.MX93 FRDM 嗨 @Chavira 你 是什么意思它不受支持,为什么? 这是否意味着它没有在板上进行测试? RPI 凸轮与 ISP 配合使用,但在我们的应用中却不需要。 BR Basel Re: Settings to operate ov2740 camera on i.MX93 FRDM 您好@BaselHn! 感谢您联系恩智浦支持中心! 遗憾的是,i.MX93 处理器目前不支持您所说的摄像头。我们建议改为在 i.MX93-FRDM 板上使用经过验证的摄像头模块。 一个不错的选择是RPI-CAM-MIPI,它已通过测试,并确认可与该平台可靠配合使用。 顺祝商祺! 查维拉
記事全体を表示
在 EB Tresos 工作区升级 RTD 驱动程序 你好,团队、 我目前正在使用 LLCE CAN 驱动程序(v1.0.2)和 RTD 驱动程序(以太网、端口、平台等)版本 2.0.0 在 S32G274A 板上进行一个正在运行的项目。用于这些驱动程序的 EB Tresos 配置工作区在 CAN 和以太网模块上都能成功运行。 我现在计划将 RTD (MCAL) 驱动程序从 2.0.0 版升级到 5.0.0 版。我想了解使用 EB Tresos 更新驱动程序版本和重新生成模块的过程,最好以现有工作区为基础。 能否请您指导我执行此升级的建议步骤或最佳做法? 谢谢! Re: Upgrading RTD Drivers in EB Tresos Workspace 你好,@PZK 谢谢您的帖子。 你曾经使用的版本已经很旧了,对于这种主要版本的更新,我建议重新生成代码/配置,你可以先选择以下组合作为参考: LLCE1.0.10、RTD5.0.0QLP03 和其他(如需要)(HSE FW0.2.64、PFE 1.6.0)、因为这种组合在正式版本之前已经过测试。 然后更改参考您先前工作的设置,并为接下来的构建和测试生成新的代码/配置。 BR 切宁
記事全体を表示
MCX-A346: プログラム開始時のコア状態 Cortex-M33 コアは実際には MCX-A346 のリファレンス・マニュアルには記載されていませんが、Arm の対応する技術リファレンス・マニュアルを参照できるため、記載されているものと思われます。けっこうだ。しかし、プログラムが制御を取得したときに発生するコアの状態 (アドレス 0x4 の初期 PC 値) は、ARM のマニュアルでリセット状態として定義されているものとは異なります。コアハードウェアが仕様通りに実装されていると仮定すると、非適合状態を残すのはブートROMコードであると考えられます[1]。 この初期のコア状態は文書化されていますか? 文書化されている場合、どこにありますか?ありがとう。 [1] 例: 1) プリマスク = 1 2) FPU は有効になっていますが、さらに悪いことに、CONTROL.FPCA = 1、つまり、コードの実行前に FPU 命令が使用されることを示しています。現在、Thread モードのすべての例外がこのフラグによって汚染されており、コードが FPU 命令を使用していない場合でも、FPU レジスタを含む拡張スタック フレームが生成され、スタック メモリが浪費されます (遅延スタックのおかげで、実行時のオーバーヘッドは最小限に抑えられます)。 もちろん、これらの問題は両方とも初期化コードでCAN解決できます。このCASE、そしておそらく私がまだ「発見」していない他の同様のCASEも文書化しておくと役立つでしょう。 コアとメモリ MCXA Re: MCX-A346: Core State at Program Start こんにちは、ハリー。私が言いたいのは、コアの状態が Arm マニュアルに記載されていないため、NXP による対応するドキュメントを期待しているということです。私が説明した 2 つのCASEをブート ROM チームに確認したいとのことでした。 しかし、いずれにせよ、非準拠が見つかった場合は、初期起動コードで MCU を ARM で文書化された状態にリセットするだけです。ありがとう。 Re: MCX-A346: Core State at Program Start こんにちは@ygrayne これがあなたが探しているものかどうかわかりません。添付のドキュメントまたは次のリンクの B1.6 の章を確認してください。 Arm Cortex-M33 デバイスの汎用ユーザーガイド r0p4 MCXA リファレンス マニュアルには、ユーザー イメージ ヘッダーを含む表 112 があり、ここにも役立つ情報が含まれている可能性があります。 PC に関しては、アドレス 0x4 を調べている場合、これは初期プログラム カウンターであり、リセット後に常にコア PC レジスタにロードされます。この値は、MCU やその他の変数によって異なります。 これが役に立つことを願います。 BR ハリー Re: MCX-A346: Core State at Program Start こんにちは@ygrayne ブートROMがPRIMASKとCONTROL.FPCAの状態を変更したかどうかについては、 ROM チームに確認する必要があります。 BR ハリー
記事全体を表示
Freemaster3.2版本使用过程中出现崩溃无法正常使用 我这边开发过程中一直使用Freemaster3.2版本进行程序辅助开发,最近在使用过程中每次打开后无任何反应,使用任务管理器查看后展开列表-显示Project-FreeMATER"无响应",如图片所示(卸载后重新安装问题也没有解决,麻烦社区给予支持  谢谢了 )
記事全体を表示
NT3H2111 Capability Container byte2, LAST_NDEF_BLOCK How should they be configured       1. The range of LAST_NDEF_BLOCK is from 1h to 37h, and the corresponding NFC page range is from 4h to DCh. Based on the given information, the calculated byte size is D9 * 4. This means that from the starting page to the last page corresponding to LAST_NDEF_BLOCK, the entire data area contains D9 NFC pages (each NFC page is 4 bytes) 2. According to NFC Forum Type 2 Tag specification, the value of byte 2 of the CC multiplied by 8 equals the data area byte size. the data area byte size as D9 * 4  (D9 * 4) / 8 = 217 / 2 = 108.5. As byte 2 of the CC is an 8 - bit data (1 byte), its value should be an integer.  it becomes 108 in decimal, and converting it to hexadecimal gives 6C. So, according to the specification, the CC should be set to  :Byte0:0xe1 , Byte1:0x10  Byte2:0x6c Byte3:0x00  right? 回复: NT3H2111 Capability Container byte2, LAST_NDEF_BLOCK How should they be configured   I found out why: the NDEF data area contains data in non-NDEF format   回复: NT3H2111 Capability Container byte2, LAST_NDEF_BLOCK How should they be configured after set CC and LAST_NDEF_BLOCK the session bytes FEh: 0~7 byte value: 0, 0x37, 0xf8, 0x48, 0x8, 0x1, 0x0, 0x0 the i2c block0 0~15 value:  0x4, 0xa9, 0x35, 0x12, 0xf0, 0x71, 0x80, 0x0, 0x44, 0x0, 0x0, 0x0, 0xe1, 0x10, 0x6c, 0x0 Not clear why the TagInfo cannot detect NDEF information   
記事全体を表示
SPI NORフラッシュの他の場所からT1022を起動する 皆さん、こんにちは。 私はカスタムT1022子ボードを持っており、プロセッサはSPI NORフラッシュに保存されているubootから起動します。上記のNORフラッシュに複数のubootを保存して、この子ボードがマウントされている親ボードに従ってプロセッサが起動するようにする予定です。だから私の質問は: 1) 可能ですか?(現在、場所間でubootをコピーしてみましたが、遅すぎます) 2) .cmm によるファイルの場合、uboot は常に 0 の場所に格納されます。それはどうしてですか。この場所をどこかで変更して、ユーザーにubootの場所を尋ねることはできますか? これに関する提案は大歓迎です。 よろしくお願いいたします。 スービック Re:SPI NORフラッシュの他の場所からT1022を起動します どういたしまして。 Re:SPI NORフラッシュの他の場所からT1022を起動します よろしくお願いします。 Re:SPI NORフラッシュの他の場所からT1022を起動します IFC NORとは異なるRCWをフェッチする必要があるため、IFC NORに向かうアドレス行を操作する必要があります。例 - IFC NORは仮想銀行に分割されており、特定の銀行を選択するためのロジックがあります。これについては、ハードウェア設計ガイドを一度確認できます。そのため、CPLDまたはIFC NORでバンクを切り替えるための外部コントローラーが必要になります。そのため、異なるバンクに存在する異なる RCW は、そのロジックを使用して PBL でフェッチできます。そのため、ハードウェア設計の変更が必要です。 Re:SPI NORフラッシュの他の場所からT1022を起動します 偵知。 Re:SPI NORフラッシュの他の場所からT1022を起動します わかりました。ありがとうございます。道筋がわかりました。 最後の質問。PBL が IFC NOR の別の場所からフェッチされるようにするには、どうすればよいですか?フェッチ場所を設定したフィールドが見つかりませんでした。 Re:SPI NORフラッシュの他の場所からT1022を起動します チャイルドボードのGPIOとSERDESの構成を変更したいですよね?次に、子ボードのIFC NORに3つの異なるRCWを保持する必要があります。 RCWはPBLによって取得されます。UbootはPBLステージより遅れて来るため、Ubootはこれを処理できません Re:SPI NORフラッシュの他の場所からT1022を起動します あなたに戻ってきます Re:SPI NORフラッシュの他の場所からT1022を起動します この場合、IFC NOR FLASHを子カードではなく親ボードに保持する必要があります。私は正しいですか? 代わりに子カードにNORフラッシュを保持している場合、RCWが異なるパーティションからロードされるようにするにはどうすればよいでしょうか。パーティションの場所は、SPIフラッシュに保存されているubootに書き込むことができますか? Re:SPI NORフラッシュの他の場所からT1022を起動します だからここにあなたが必要とするものがあります:- RCW には gpio と serdes の設定があります。したがって、3つの親カードに応じて、目的の構成を持つ3つの異なるRCWが必要です。 パワーオン リセット時に、PBL[Pre-bootloader] は、目的の不揮発性ソース [IFC NOR、eSDHC、NAND フラッシュ] の 1 つからこの RCW をフェッチし、このコンフィギュレーションをロードします。考えられる解決策の1つは、IFC NORをソースとして使用することです。 IFC NORには、3つの異なるメモリパーティションに3つの異なるRCWがあります。 親カードは、次のように設計する必要があります。 子ボードが親カードAに接続されている場合、RCWはIFC NORのパーティションAからフェッチされます。 子ボードが親カードBに接続されている場合、RCWはIFC NORのパーティションBからフェッチされます。 3枚目の親カードも同様です。 Re:SPI NORフラッシュの他の場所からT1022を起動します AEチームと話し合います。 Re:SPI NORフラッシュの他の場所からT1022を起動します 「その特定のdtbでイメージをロードできる」と言うとき、親カードはそれぞれのdtbを保持し、プロセッサが起動すると親カードに保存されているdtbをロードするということですか?私が理解したことが正しければ、dtbがserdesの設定を変更することができる場合、これは可能な解決策の代替手段になる可能性があります。 私の場合、親カードAがあり、SRDS_PRTCLが0x86である必要があり、別の親カードBがあり、SRDS_PRTCLが0x81する必要があり、プロセッサの子カードが1つあるとします。プロセッサが各ボードのSRDS_PRTCLsに従って起動することをどのように確認できますか。私の意見では、dtbのフェッチはubootが実行された後に開始されます。ただし、親カードに従ってubootを変更する必要があります。 Re:SPI NORフラッシュの他の場所からT1022を起動します 親カードによってGPIO構成が異なる3つの異なるデバイスツリーバイナリを作成することはできませんか?また、必要に応じて、その特定のdtbで画像をロードできます。 これらの3つの親カードは、同じアプリケーションプロセッサで構築されていますか? Re:SPI NORフラッシュの他の場所からT1022を起動します わかりました。 Re:SPI NORフラッシュの他の場所からT1022を起動します AEチームからの以下の最新情報をご参照ください。 NORフラッシュ内の複数のUbootについて。NORフラッシュに2つのUbootが必要な理由について、要件についてもう少し詳しく教えてください。「プロセッサは、この子ボードがマウントされている親ボードに従って起動します」 -- これについて詳しく教えてください。 Re:SPI NORフラッシュの他の場所からT1022を起動します 私はこのケースをAEチームにエスカレーションしましたので、今彼らからのフィードバックを待っています。 Re:SPI NORフラッシュの他の場所からT1022を起動します AEチームと話し合う。
記事全体を表示
how to check image CRC I have an image built using the MCUXpresso Secure Provisioning Tool. It's a plain image with a CRC, and the offsetToExtendedHeader field(address 0x00000028) contains the 4bytes CRC checksum value. Now, I want to check the CRC before writing it to flash. I tried to calculate it using these settings, but I cannot match the CRC with the offsetToExtendedHeader field. (ref: Kinetis Bootloader v2.0.0 Reference Manual) Is there any tool available to calculate the image CRC (like nxpimage and blhost)? Alternatively, where can I find more details about calculate the image CRC? Boot ROM|Booting | Flash MCXA 回复: how to check image CRC Hi Marek I found the Mbi_ExportMixinCrcSign function and the CRC algorithm in the nxpimage tool, which is part of SPSDK. Based on the above algorithm, I created a python program to verify the image CRC, and it works. Thanks for your support. Re: how to check image CRC Hi Victor, SEC tool uses SPSDK application nxpimage to build a CRC bootable image. You can see generated build script to find, how the nxpimage tool is used. See main menu > Help > SPSDK Online Documentation for nxpimage documentation. SPSDK is opensource, so you can find implementation details in GitHub.
記事全体を表示
ArduinoのPortenta X8ハードウェアのサポート 私が関わっている研究プロジェクトでは、NXPのMIMX8MM6CVTKZAA SoCをベースにしたArduinoのPortenta X8モジュールを利用したカスタムハードウェアを作成することが決定しました。 https://docs.arduino.cc/hardware/portenta-x8/  プロジェクトの要件により、Arduinoのファームウェアを使用できません(使用したくもありません)。これまで、NXPのピン構成ツールを使用してmex構成ファイルの作成を開始することができましたが、ここからどのように進めるかがわからなくなります。 質問1:NXPプロセッサのJTAGを介したフラッシュオプションは何ですか?MCU-Link Debug ProbeはこのSoCで動作しますか? 質問2:これはEVK開発ボードではないため、ミニマリストのLinuxビルド(yocto)を作成するためのサポートを見つけるのに苦労しています。これにはどのようなサポートがありますか?portenta X8で実行できる新しいLinuxベースのプロジェクトを作成するにはどうすればよいですか? Re:ArduinoのPortenta X8ハードウェアのサポート MIMX8MM6CVTKZAAの内部メモリに画像をフラッシュする方法はありませんか?許してください。私はSWDでマイクロコントローラを操作することに慣れています。 Re:ArduinoのPortenta X8ハードウェアのサポート X8からX8のSTマイコンをフラッシュするための独自のソリューションを生成する必要があることは理解していますが、今はそれについて尋ねているわけではありません。私の質問は次のとおりです。 NXPは、EVKボードがなくてもこのNXPプロセッサにイメージをフラッシュできるようにするために、どのようなデバッグまたはプログラミングハードウェアを提供していますか?たとえば、NXPのMCU-LinkデバッグプローブはNXPデバイスをフラッシュするために機能しますか?
記事全体を表示
如何配置LPC845 BRK ADC2和ADC3? 我正在使用 LPC845 BRK,需要配置 ADC2 和 ADC3 来测量来自 pin27 和 pin8 的电压水平。 示例项目是lpc845breakout_lpc_adc_basic。ADC0 在这个项目中运行没有任何问题。 尝试扩展项目以像这样使用 ADC2 和 ADC3, ADC_DoSelfCalibration(ADC2_BASE,频率)); ADC_DoSelfCalibration(ADC3_BASE,频率)) ; ADC_Init(ADC2_BASE,&adcConfigStruct); ADC_Init(ADC3_BASE,&adcConfigStruct); 如果将 ADC0 定义为 ADC 基地址,那么 ADC2 和 ADC3 的基地址是多少? #定义ADC0_BASE(0x4001C000u)//在LPC845.h中 我希望您能分享一个如何成功配置 ADC2 和 ADC3 的示例。 非常感谢, 奥西 LPC800 回复:如何配置 LPC845 BRK ADC2 和 ADC3? 感谢 frank_m 的澄清, 现在我清楚了 回复:如何配置 LPC845 BRK ADC2 和 ADC3? > 我正在使用 LPC845 BRK,需要配置 ADC2 和 ADC3 来测量来自 pin27 和 pin8 的电压水平。 我自己没有/不使用 LPC845。 但是,阅读数据表后,我认为你错了。该MCU只有一个ADC,最多可以有12个独立通道。 要使用这些通道,您需要初始化相应的 GPIO 引脚,类似于通道 0(我认为提到的示例提供了)。 > ADC_DoSelfCalibration(ADC2_BASE,频率)); 并且校准是针对整个 ADC 单元进行的,而不是针对单个通道。
記事全体を表示
NFC USB 加密狗 - 写入期间显示数据 大家好, 我有兴趣了解是否有方法可以检索发送到 NFC USB 加密狗的数据。目前,我已经通过启用#define CARDEMU_SUPPORT成功执行了“C”示例。我既可以向加密狗写入数据,也可以从加密狗读取数据。然而,在写入过程中,我正在寻找一种方法让应用程序捕获写入器发送的数据记录。任何有关此事的帮助都将不胜感激。 我正在使用的特定加密狗可以在这里找到: https://www.mikroe.com/nfc-usb-dongle 回复:NFC USB 加密狗 - 写入期间显示数据 我正在使用 PN7150 NFC USB 加密狗并尝试与我的手机通信。我运行了示例包 SW4335 中提供的 NXP-NCI_Windows_example.exe。应用程序成功启动,命令提示符显示: 等待设备发现当我将手机靠近加密狗时,它会成功检测到它,并显示以下消息:监听模式:已从远程读取器激活---已发送 NDEF 记录紧接着,显示以下消息:读取器已断开连接 我最初怀疑这可能是驱动程序问题,但根据您的文档,不需要任何驱动程序。我已经在多台笔记本电脑和手机上测试了这种行为,但问题仍然存在。 您能帮我理解为什么发送 NDEF 记录后读取器会断开连接吗?我已附上命令提示符下的日志供您参考 回复:NFC USB 加密狗 - 写入期间显示数据 已解决
記事全体を表示
freeRTOS stack size configuration I am currently learning FreeRTOS on the LPC51U68 development board (OM40005). I have created 7 tasks for testing and am using the RTOS task list monitor provided by MCUXpresso IDE. I noticed that the stack sizes displayed in the task list don't match the configurations I set. Could this be related to memory alignment? Where can I check the rules for configuration differences? Below is the code I modified from the freertos_hello example. /* * Copyright (c) 2015, Freescale Semiconductor, Inc. * Copyright 2016-2017 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ /* FreeRTOS kernel includes. */ #include "FreeRTOS.h" #include "task.h" #include "queue.h" #include "timers.h" /* Freescale includes. */ #include "fsl_device_registers.h" #include "fsl_debug_console.h" #include "pin_mux.h" #include "board.h" #include /******************************************************************************* * Definitions ******************************************************************************/ /* Task priorities. */ #define hello_task_PRIORITY (configMAX_PRIORITIES - 1) /******************************************************************************* * Prototypes ******************************************************************************/ static void task1(void *pvParameters); static void task2(void *pvParameters); static void task3(void *pvParameters); static void task4(void *pvParameters); static void task5(void *pvParameters); static void task6(void *pvParameters); static void task7(void *pvParameters); /******************************************************************************* * Code ******************************************************************************/ /*! * @brief Application entry point. */ int main(void) { /* Init board hardware. */ /* attach 12 MHz clock to FLEXCOMM0 (debug console) */ CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH); BOARD_InitBootPins(); BOARD_InitBootClocks(); BOARD_InitDebugConsole(); if (xTaskCreate(task1, "task1", configMINIMAL_STACK_SIZE + 50, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task2, "task2", configMINIMAL_STACK_SIZE + 100, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task3, "task3", configMINIMAL_STACK_SIZE + 160, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task4, "task4", configMINIMAL_STACK_SIZE + 161, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task5, "task5", configMINIMAL_STACK_SIZE + 170, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task6, "task6", configMINIMAL_STACK_SIZE + 200, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } if (xTaskCreate(task7, "task7", configMINIMAL_STACK_SIZE + 300, NULL, hello_task_PRIORITY, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; } vTaskStartScheduler(); for (;;) ; } /*! * @brief Task responsible for printing of "Hello world." message. */ static void task1(void *pvParameters) { for (;;) { PRINTF("Hello world.\r\n"); vTaskSuspend(NULL); } } static void task2(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } static void task3(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } static void task4(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } static void task5(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } static void task6(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } static void task7(void *pvParameters) { for (;;) { PRINTF("H\r\n"); vTaskSuspend(NULL); } } Re: freeRTOS stack size configuration Hi @Relas  In FreeRTOS, the stack size specified in xTaskCreate() is measured in words (not bytes). For the LPC51U68, which uses a 32-bit word size, each word is 4 bytes. For instance, if you specify configMINIMAL_STACK_SIZE + 50, this translates to (configMINIMAL_STACK_SIZE + 50) * 4 bytes of stack space. The alignment adjustments by FreeRTOS or the compiler can cause discrepancies between the requested stack size and the actual allocated size. BR Hang
記事全体を表示
LPC860 MCU的LPCXpresso860-MAX开发板 使用2块LPC860 MCU的LPCXpresso860-MAX开发板, 通过 keil 分别运行 demo 程序i3c_interrupt_b2b_transfer_master 和 i3c_interrupt_b2b_transfer_slave, master 程序在SDR read 的阶段, 在MCTRL 写入 0x6180(ADDR:0x30 slaver DDA, DIR:0x01 read, IBIRESP:0x10 ACK with * mandatory byte)后, MERRWARN 值立即变为0x00000004 (I3C_MERRWARN_NACK_MASK:Not acknowledge (NACK) error), MSTATUS 值立即变为0x00009923 ,导致后续 master 接收不到 slaver 的SDR数据. 我真的不知道接下来该怎么做. 提供帮助将感激不敬. Re: LPC860 MCU的LPCXpresso860-MAX开发板 Hi @Zahi  是的 我对照了我的开发板之间的连线与你的一样。 我用的IDE 为了MCUXpresso IDE,SDK版本为2.15. 您是否可以换这个IDE尝试一下。 BR Harry Re: LPC860 MCU的LPCXpresso860-MAX开发板 是的, 烧录程序后, 关闭keil, 尝试过使用台式机或笔记本标准USB口, 未经任何hub转换, 未处于调试模式, 结果跟doc文档不一致, 均卡在 SDR READ 阶段. 请问有没有任何值得怀疑的地方呢?因为您那边看起来结果是OK的. Re: LPC860 MCU的LPCXpresso860-MAX开发板 Hi @Zahi  请问您是两个板子都是全速运行代码么? 我尝试运行一下代码,是没有问题的。 BR Harry Re: LPC860 MCU的LPCXpresso860-MAX开发板 @Harry_Zhang  调试过程如下 : Re: LPC860 MCU的LPCXpresso860-MAX开发板 Hi @Harry_Zhang  感谢回复 我用的是官方示例 然后代码调试看到 master 在SDR read 阶段 发送 I3C_MasterTransferNonBlocking 中, 给MCTRL写值后MERRWARN就变为0x00000004了 Re: LPC860 MCU的LPCXpresso860-MAX开发板 Hi @Zahi  请问您是用运行官方SDK的 I3C demo出现这个问题么? BR Harry
記事全体を表示