Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
替代设备 MMA7361L <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, ,我需要购买 50 个传感器 MMA7361L,用于替换已有的一个系统。你们有类似的产品吗? 加速度传感器 Re: Alternative device MMA7361L <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,吉尔贝托、 如您所知,MMA7361L 没有任何引脚兼容的替代品。但是,我们确实有 FXLN83xxq 系列的模拟加速度计可以取代mma73xxL。 请参阅AN4992,其中提供了从 MMA73xxL 加速计过渡到 FXLN83xxQ 加速计的实用技巧。 顺祝商祺! 托马斯
View full article
i.MX8M plus, single channel ddr on channel B Is it possible to use a single channel lpddr4 16bit that is only connected on channel B with the i.MX8M plus? We have a design where A is connected to B and B to A, will this design work if swapping to a single channel lpddr4? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8M plus, single channel ddr on channel B Hi @johan_carlsson, Thank you for contacting NXP Support! Based in iMX8MP Hardware design guide, iMX8MP datasheet and iMX8MP Reference Manual. No. NXP neither documents nor validates a single‑channel LPDDR4 (16‑bit) design connected only to Channel B on the i.MX 8M Plus. The single‑channel configuration assumed in the documentation and reference designs is on Channel A. A design with A <-> B crossed (A wired to B and B wired to A) is not supported. Best Regards, Chavira Re: i.MX8M plus, single channel ddr on channel B HI Chavira, are you sure about this? the TRM says this, so shouldn't changing DqLnSel registers allow (per byte lane / slice) to be changed from A to B? Re: i.MX8M plus, single channel ddr on channel B Hi @dav1, I noticed some misunderstanding here. According to the Reference Manual: "Supports mapping of PHY dq to DRAM dq within a byte (swizzle)… per‑dbyte… each register in a byte’s set of DqLnSel must have a unique value…” This means the PHY lets you undo board level bit to bit scrambling inside a single 8‑bit slice (dbyte). For example, if PHY lane 3 routes to DRAM DQ0 within that same dbyte, you set Dq0LnSel = 3 for that dbyte. This helps things like MRR binary counters return correct values after the swizzle is logically undone. Re: i.MX8M plus, single channel ddr on channel B would it be possible to do this workaround - setup the DDR as 2 channels - configure it so that it doesn't interleave across A and B - define only the B section as valid Re: i.MX8M plus, single channel ddr on channel B HI @dav1, At this time, this configuration has not been validated and is not expected to be possible. While you may attempt to test it, please note that this is outside the intended functionality of the RAM PHY, and therefore reliable operation is not expected. Best Regards, Chavira Re: i.MX8M plus, single channel ddr on channel B If there is anything wrong with my reply, please point it out. If there isn’t any problem and this post gets deleted again like the previous times, then I will post this on Facebook. But Why the RPA tool shows, it can do swap. MX8M_Plus_LPDDR4_RPA_v10.xlsx https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352 Re: i.MX8M plus, single channel ddr on channel B did you try it?         Re: i.MX8M plus, single channel ddr on channel B @dav1 If a swap issue occurs, the table will turn red and show a warning. However, when Channel A and Channel B are swapped, this RPA tool still shows green, and the corresponding registers are also modified. Therefore, there are only two possibilities: The RPA tool is wrong. The Reference Manual is wrong. One of two must be true. This is what @Chavira  needs to clarify/answer.
View full article
iMXRT HAB 使用存储在 PKI 服务器上的密钥签署图像 你好, ,我正在使用 iMXRT 10xx 做一个项目。我需要使用存储在 PKI 服务器上的私钥为 MCU 生成 HAB 签名镜像,用于对二进制文件进行签名。让二进制文件由私钥签名的唯一方法是创建一个脚本,将文件发送到服务器并对其进行签名。 恩智浦用于签名的工具将签名作为最终程序映像的一部分。 您是否有任何文件解释最终程序映像中包含的签名的正确格式? 我需要让 PKI 服务器对二进制文件进行签名,并以 MCU 的 HAB 可以理解的方式将签名添加到最终图像中。 此致, 伦纳德 Re: iMXRT HAB signed image using a key stored on a PKI server 嗨,@CLEO、 我刚刚就您的问题咨询了专家,请您发表如下意见: RT10xx 尚不支持该功能,但将在 26.03 版本中提供。 客户仍然可以探索它在适用于其他设备的 高效密码学标准\\(SEC\\) 工具中的工作原理——参见此处的文档:https://docs.mcuxpresso.nxp.com/secure/latest/07_generic_workflows.html#signature-provider-workflow 返回到 1. 如果客户与恩智浦签订了保密协议,我们可以提供抢先体验版本 现在,有关高效密码学标准(SEC)工具解决方案的更多细节——需要客户方编写小型脚本。我们提供了将密钥存储在磁盘上的 python 示例(请参阅文档),但也可以很容易地将其调整为任何客户的解决方案。尽管高效密码学标准(SEC) 工具不直接支持 PKCS #11,但它可以在客户端实施。 希望对你有所帮助、 祝您愉快, Kan ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"标记正确" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请打开一个新主题并参考已关闭的主题。 -------------------------------------------------------------------------------
View full article
JTAG security in S32K311 about Security levels and Mass erase Hi,  May I know about the steps for locking and unlocking process. Is it possible to mass erase and unlocking mechanism in S32K311 microcontroller ? Re: JTAG security in S32K311 about Security levels and Mass erase Hello @truptikavadi1 , Thanks for your post.  No, S32K1xx works exactly as you described, however, S32K3xx does not. If you would like to obtain more information related to S32K3xx security, please note that since this is a K32L channel, that product is beyond the scope of my support. I recommend creating a new post on S32K - NXP Community, where the appropriate supporters will be able to assist you further. Thanks for your understanding. BR Celeste   ---------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! ----------------------------------------------------------------------------------------------------------------------
View full article
RT1170 以太网中的自由缓冲区超出范围问题 您好, 我正在尝试从自定义板上的自定义项目中执行基本的以太网测试。作为该项目(该项目集成了不同的模块,如SD卡、CAN、GPIO、ADC、以太网和EEPROM)的一部分,基本的以太网发送和接收有待验证。但我在 ping 发送前遇到"freed buffer out of range 错误" 。我已经完成了与以太网有关的所有基本初始化和配置。我看到出现错误的原因是函数"ethernetif_rx_free" (enet_ethernetif_kinetis.c) 中的 LWIP_ASSERT("Freed buffer out of range", ((idx>= 0)&& (idx< ENET_RXBUFF_NUM))); 其中的 idx 值为负数。这一完整的功能可在 EVK 套件上使用。 还能缺少什么?请提出建议。 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 大家好 这个问题也发生在我的 RT1024 客户板上,当我在某个地方放了一个断点然后它就停止了,然后恢复正常运行更有可能导致这个错误。 此致敬礼! Ping Re: Freed Buffer out of Range Issue in Ethernet for RT1170 如果示例项目在您的自定义板中运行良好,则问题似乎出在软件方面。 您使用的不是 FreeRTOS 对吗? 似乎有什么东西干扰了示例的行为,可能是缺少某些配置,或者只是示例流程受到应用程序其他部分的影响。 我建议你尝试使用最新的软件开发工具包版本,即2.15.000。如果您的问题在此版本中仍然出现,那么恐怕您的应用程序流程出现了问题。 此致, 丹尼尔 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 您好, 是的,在自定义板中实现合并的源代码时会出现问题。但是,没有与其他接口合并的 Ethernet_PING 的单个来源在自定义板中运行良好。当以太网的单个源与其余接口合并时,就会出现问题。 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 如果我没有理解错的话,当您运行 SDK 示例时,它是可以工作的。但当您添加自定义应用程序时,问题就出现了。你能确认吗? 此致, 丹尼尔 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 您好, 实际上,以太网的各个源代码在自定义板中运行良好。当我尝试集成代码时,以太网无法正常工作。我观察到EIR 寄存器的第 25 (RXF)、26 (TXB) 和 27 (TXF) 位被设置为 0,RDAR 寄存器的第 24 位被更新为 0,但在以太网的工作代码中,这些寄存器被设置为 "1"。 我怀疑这些寄存器更新是由中断处理的,但我无法在自定义项目代码库中找到负责这些更新的特定处理程序。请帮帮我。 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 请仔细检查是否有任何外围更改(例如:......)。为了让 EVK 示例在您的定制硬件中运行,您的项目中需要哪些外围实例? 如果您已经验证了这一点,看来问题出在硬件方面。 您是否已经用 HDG 验证了您的设计? 此致, 丹尼尔 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 您好, 我使用的是 SDK 11.6.1 版。我正在尝试测试 lwip_ping_bm_cm7 示例。在 EVK 中运行正常。 但是,当尝试将所有源代码与以太网连接时,它在自定义板上不起作用。如果我们面临"Freed Buffer out of range" ,可能会出现什么问题?请帮我解决这个问题。 Re: Freed Buffer out of Range Issue in Ethernet for RT1170 您好, 您使用的是哪个版本的 SDK? 您用来测试的 SDK 示例是什么? 如果我理解正确,应用程序在 EVK 中运行正常,对吗? 此致, 丹尼尔
View full article
PCIe: i.MX 95: 複数の MSI IRQ ベクトルを割り当てる こんにちは、 PCIe2 インスタンス経由でコネクテッドされた i.MX95 ベースのシステムで ATH12K Wi-Fi モジュールを使用しています。 linux-imx lf‑6.12.y ベースのカーネルではこのセットアップは失敗しますが、lf‑6.6.y ベースのカーネルでは期待どおりに動作します。 カーネル ドライバは 16 個の MSI 割り込みを正常に要求し、受信します。しかし、その後、Wi-Fi モジュールの起動に失敗します。 [ 5.888139] ath12k_pci 0001:01:00.0:iommuグループ5に追加 [ 5.888506] ath12k_pci 0001:01:00.0:BAR 0 [mem 0xa10000000-0xa101fffff 64bit]: 割り当て済み [ 5.888553] ath12k_pci 0001:01:00.0:有効化デバイス (0000 -> 0002) [ 5.889315] ath12k_pci 0001:01:00.0:MSIベクター: 16 [ 5.889334] ath12k_pci 0001:01:00.0:ハードウェア名: wcn7850 hw2.0 [ 6.475718] ath12k_pci 0001:01:00.0:チップID 0x2 チップファミリー 0x4 ボードID 0xff soc_id 0x40170200 [ 6.475743] ath12k_pci 0001:01:00.0:fw_version 0x110cffff fw_build_timestamp 2025-06-25 09:26 fw_build_id QC_IMAGE_VERSION_STRING=WLAN.HMT.1.1.c5-00302-QCAHMTSWPL_V1.0_V2.0_SILICONZ-1.115823.3 [ 7.647106] ath12k_pci 0001:01:00.0:制御応答完了、ポーリングを受信できませんでした。 [ 8.675241] ath12k_pci 0001:01:00.0:サービス接続タイムアウト [ 8.681002] ath12k_pci 0001:01:00.0:HTTへの接続に失敗しました: -110 [ 8.692180] ath12k_pci 0001:01:00.0:コアの起動に失敗しました: -110 カーネルメーリングリスト[1]では別のPCIeデバイスに関する関連した議論がありましたが、まだ私たちのシステムで動作する構成には至っていません。 どうすれば最善の進め方でしょうか? 再開まで今しばらくお待ちください。 最大 [1] https://lore.kernel.org/all/1819305.VLH7GnMWUR@steina-w/ Re: PCIe: i.MX 95: Allocate Multiple MSI IRQ Vectors こんにちは、 i,MX95 はまだ初期段階であり、一部の構成はデザインされていません。しかし、PCIe2経由でATH12Kを搭載したi.MX95は lf-6.12.y ですが、 lf-6.6.y で作業中ですこれは、新しいカーネルの PCIe または Wi-Fi スタックにおける回帰またはドライバー相互作用の変更を示唆しており、PCIe パワーマネージメント (ASPM)、MSI マッピング、または ATH12K の特定の PCIe エンドポイントの癖に関係している可能性があります。多くの場合、カーネル パッチを適用するか、新しいカーネルのブート引数で ASPM を無効にすることで解決できます。dmesg で PCIe エラーを確認し、デバイスツリーを比較し、NXP/Linux カーネル メーリング リストで関連するコミットを探します。  考えられる原因とトラブルシューティングの手順を次に示します。 1. カーネルログを確認する ( dmesg ) PCIe エラーを探す: 障害が発生した lf-6.12.y カーネルの dmesg で、「PCI」、「MSI」、「ATH12K」、「Error」、「Firmware」、または「Timeout」メッセージを検索します。 ファームウェアのロード: ath12k ファームウェアが正しくロードされているかどうか、および初期化中にエラーが発生していないかどうかを確認します。  2. PCIe電源管理(ASPM) 一般的な問題:新しいカーネルでは、多くの場合、Active State パワーマネージメント (ASPM) がデフォルトで有効になっています。これにより、組み込みシステム上の ATH12K などの PCIe デバイス、特に古いファームウェア/ハードウェアで問題が発生する可能性があります。 ASPM を無効にしてみてください:カーネル ブート引数 (U-Boot または GRUB など) に pcie_aspm=off を追加して、再度テストします。  3. Devicetree/DTBの違い DTB の比較:両方のカーネル ( .dtb ファイル) で使用されるデバイス ツリー BLOB (DTB) を生成して比較します。特に割り込み、電源ドメイン、または互換性プロパティに関連する、 pci2 の PCIe ノードの変更を探します。  4. カーネルドライバー/ファームウェアの回帰 特定のコミット: ATH12K ドライバ ( ath12k )、 mac80211 、または lf-6.12.y のコア PCIe/Arm コードによって、セットアップを壊す変更が導入された可能性があります。 メーリング リストを検索: ath12k 、 i.MX95 、およびそれ以降のカーネル (6.12+) に関するパッチやディスカッションについては、Linux カーネル メーリング リスト (LKML) および NXP のリストを確認してください。  5. MSIの取り扱い 割り込み再マッピング:割り込みを受信すると、その処理方法 (MSI-X と MSI、割り込み再マッピング) が微妙に変わる場合があります。 proc/interrupts で割り込みをチェックします。カーネル間で割り込みの分布またはカウントが異なるかどうかを確認します。  6. ファームウェアブロブ ファームウェア バージョン:新しいカーネルのドライバと互換性のある、ATH12K 用の正しいファームウェアを使用していることを確認します。新しいドライバには新しいファームウェアが必要になる場合があります。  要約すると、 dmesg から始めてASPMを無効にしてみてください。これらは、組み込みプラットフォームの新しいカーネルでPCIe Wi-Fiの障害が発生する最も一般的な原因です。   よろしくお願いします。 Re: PCIe: i.MX 95: Allocate Multiple MSI IRQ Vectors 提案は問題をデバッグするための良い指針でしたが、解決策を見つけることができませんでした。つまり、すべての MSI IRQ ベクトルがドライバ内の IRQ ルーチンをトリガーしたわけではありません。 最終的には、ath12k ドライバーを変更して、1 つの MSI IRQ のみを要求するようにすることで、この問題を回避しました。 現在の Linux マスターにはこの問題は発生しないことに注意してください。 よろしくお願いします。 最大
View full article
Mram probe is not working in uboot Hi I have nvram compatible = "everspin,mr25h40"; for imx6q board .In the uboot 2020 i have configured the pad setting in board file like below :- static iomux_v3_cfg_t const ecspi5_pads[] = {     MX6_PAD_SD1_CLK__ECSPI5_SCLK | MUX_PAD_CTRL(SPI_PAD_CTRL),     MX6_PAD_SD1_DAT0__ECSPI5_MISO | MUX_PAD_CTRL(SPI_PAD_CTRL),     MX6_PAD_SD1_CMD__ECSPI5_MOSI | MUX_PAD_CTRL(SPI_PAD_CTRL),     MX6_PAD_SD1_DAT1__ECSPI5_SS0 | MUX_PAD_CTRL(NO_PAD_CTRL), };   In the uboot2024 as it is strictly needs a dts entry for the probe and working i have added the dts entry like below :- &ecspi5 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_ecspi5>; status = "okay";   mram@0 { #address-cells = <1>; #size-cells = <1>; compatible = "spi-device"; spi-max-frequency = <30000000>; reg = <0>; }; };   pinctrl_ecspi5: ecspi5grp {  fsl,pins = < MX6QDL_PAD_SD1_DAT0__ECSPI5_MISO 0x1b0b1 MX6QDL_PAD_SD1_CMD__ECSPI5_MOSI 0x1b0b1 MX6QDL_PAD_SD1_CLK__ECSPI5_SCLK 0x1b0b1 MX6QDL_PAD_SD1_DAT1__ECSPI5_SS0 0x1b0b1 >; };    when i build the uboot 2024 with these changes and booted the device im seeing when i execute the dm tree command it shows as not probed . So please help me to how to configure in uboot 2024 dts so that my mram probe happens and works, i have tried using gpio also as a chip select still faced same issue. i.MX6Quad Re: Mram probe is not working in uboot Hello, Please try to change the compatible property with: compatible = "everspin,mr25h40", Regarding max frequency, please note that the SPI subsystem just can divide the clock in integers. For example, in this case the clock used by SPI is 80MHz, so, dividing by: 80/1 = 80MHz 80/2 = 40MHz 80/3 = 26.66MHz 80/4 = 20MHz The driver proximate the configured clock on the command with its divider and will not get exactly 30MHz but is under the 40MHz supported by your device. Try to use GPIO as a chip select considering above. Could you please share the kconfig options that you are using for U-boot? Best regards. Re: Mram probe is not working in uboot Hi JorgeCas , I have attached my uboot .config below and i see there is no driver which tells compatible = "everspin,mr25h40", in uboot 2024 source code, please guide me what all the changes needed completely inorder to make this up ,dts changes and any driver changes needed. Re: Mram probe is not working in uboot Hello, Thank you for the information, I do not see issues in your kconfig options. If you do not need a custom driver, you can take a look in this device tree configuration: https://github.com/nxp-imx/uboot-imx/blob/4ddbad60eff308a5b356fb9ab8734ac382ddd692/dts/upstream/Bindings/mtd/jedec%2Cspi-nor.yaml#L4 Best regards. Re: Mram probe is not working in uboot Hi JorgeCas , I have attached the defconfig below please review and guide any changes needed 
View full article
電源構成とRESET_Bの問題 – MCXN546VKLT 現在、NXP MCXN546VKLT マイクロコントローラ (HLQFP パッケージ) を使用したカスタム PCB 設計に取り組んでおり、初期のボード立ち上げ時に問題が発生しています。このデバイスのPower Architectureとリセット動作についてご指導いただければ幸いです。 1. VDD_SYS電源の理解 VDD_SYS 電源ドメインが内部でどのように動作し、VDD_CORE (~1.0 V) の生成にどのように寄与するかを明確にしていただきたいと思います。具体的には、以下の点についてご確認をお願いいたします。 VDD_SYS、VDD、VDD_Px、VDD_ANA、およびVDD_COREの正しい外部電源構成 VDD_CORE を外部電源で駆動するか、またはデカップリングのみを行うか MCXN546VKLT の推奨電源投入シーケンス。 2. 電源投入時のRESET_Bピンの問題 RESET_B ピンに関連する問題も発生しています。 ボードの電源投入時に、RESET_B は低いままになります。その結果、MCU は実行を開始しないように見えます。 理解したいこと:パワーオンリセット中のRESET_Bの内部動作、不適切なVDD_SYSまたはVDD_COREのランプアップによりRESET_Bが低レベルに保持されるかどうか これらの問題を解決するのに役立つ可能性のある、MCXN546VKLT に固有の参考回路図、アプリケーションノート、または電源/リセット構成ガイドラインをご提供ください。 どうぞよろしくお願いいたします。弊社の取締役会の成功に向けて皆様のご指導を期待しております。 B よろしくお願いいたします マニッシュ・アガルワル MCX N Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT こんにちは@ma0208 MCXN546VKLTマイクロコントローラのハードウェア設計については、以下を参照してください。 https://www.nxp.com/webapp/Download?colCode=UG10343&isHTMLorPDF=HTML このユーザー ガイドは MCXN236 用に書かれていますが、MCXN546VKLT にも適用されます。   電源投入シーケンスについては、MCXN546のデータシートを参照してください。 これらの文書を確認した後でも質問がある場合は、お気軽にお問い合わせください。 よろしくお願いします。 BR アリス Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT 親愛なるアリスへ PFA 回路図。 よろしくお願いします。 マニッシュ Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT 親愛なるアリスへ 情報をありがとうございます。 共有されたハードウェアデザインガイドに従って電源デザインをチェックしましたが、問題はありません。使用している構成は LDO モードです。カスタム ボードの電源を入れると、Reset_b ピンが Low にアサートされ、High になりません。リセット回路は、ハードウェア設計ガイドで推奨されているものとまったく同じです。これには何が原因として考えられますか。できるだけ早くお知らせください。 B よろしくお願いいたします マニッシュ・アガルワル Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT こんにちは@ma0208 回路図を共有してください。問題の確認をお手伝いします。 よろしくお願いします。 BR アリス Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT こんにちは@ma0208 あなたの回路図を確認しました。 DCDC_LXピンをフローティングにしてください。 以下の点にご注意ください:DCDCを無効にするには、DCDC_LXをフローティング状態に保ち、VDD_DCDCピンに電源を供給してください。ソフトウェアでもDCDCを無効にする必要があります。 もう一度、前回言及したアプリケーション ノートを参照して、それに応じて回路図を確認してください。   よろしくお願いします。   BR アリス Re: Power Supply Configuration and RESET_B Issue – MCXN546VKLT 親愛なるアリスへ 現在は動作していますが、はんだが乾燥していたため VBAT に電力が供給されていませんでした。 皆様のサポートに感謝いたします。 B よろしくお願いいたします マニッシュ
View full article
[RTD600 IP] S32K3X4EVB-T172 RTI Cycle Wake-up This example project will show user how to use and configure the basic functionalities of WKPU + RTI (PIT0).  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 (SCH-53148 REV B2) * MCU: S32K344 * IDE: S32DS3.5 & S32DS3.6 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example routine configures the WKPU & PIT for wake-up. The PIT0 instance includes a dedicated RTI (Real Time Interrupt) timer that runs on a separate oscillator clock and can be used for system wakeup. A key feature of this is power saving with a separate input clock for the RTI timer. All other timers share a common core clock. Note: Only PIT_0 supports the RTI feature, and exists in the Standby domain. This example does not poll for a SW press to enter and configure standby; Instead, the main function directly enters the Wkpu_EnterStandby() function which: Switches core clock to FIRC. Initializes and configures WKPU instance and wake-up source 3 (RTI). Initializes and configures PIT0 and PIT0 CH0 as set in Config Tools view. If EN_RUN_ICYCL_DUTY macro is enabled, configures PIT1 for user code before going to standby. Once Pit1_Notification is entered, runFlag is set to FALSE. Turns off LED. Enables RTI channel interrupt (otherwise, MCU cannot be woken up). Finally, sets the timeout value (WKPU_ICYCL_DUTY_TIME macro) and enters standby. This showcases the basic configuration for template on a fast-scanning power saving routine (for example, wake-up, measure ADC, go back to sleep). Keep in mind that power saving depends on the frequency of wake-up events. If MCU spends more time in Run mode rather than in Standby mode, power consumption is affected. The transition time from Standby mode to Run mode is quick. If the MCU only spends 9ms in Run and 1ms in Standby, the average current of the system will be considerably higher than if the MCU was running only 1ms every 1 second. Refer to S32K3 Low Power Management AN and demos for further information. After the period defined with either WKPU_ICYCL_DUTY_TIME, MCU wakes up. After wake-up, MCU resets and the cycle repeats. This example is provided as is with no guarantees and no support.
View full article
IMX8MP DDR4 カスタム ボード :: 緊急モードです。 こんにちは、 i.MX8M Plus DDR4カスタムボードを使用しています。Image.gzを読み込んでいます。DTBおよびrootfs (cpio.gz)SD カードから DDR にコピーし、カーネルとルート ファイル システムを DDR から起動します。 ルート ファイルシステムをロードした後、次のメッセージが表示されます。 緊急モードです。ログイン後、「journalctl -xb」と入力して詳細を確認してください。 メンテナンスのためにEnterキーを押してください (または、Ctrl + D キーを押して続行します): [ 12.946854] ランダム: crng init が完了しました。 参考までに、完全なブート ログを添付しました。 以下は、SD カードから DDR にイメージをロードするために使用している U-Boot コマンドです。 =================== SD カードから DDR にロード ================== fatload mmc ${mmcdev} :1 ${loadaddr}イメージ.gz ファットロード mmc ${mmcdev} :1 ${fdt_addr} imx8mp-ddr4-evk.dtb ファットロード mmc ${mmcdev} :1 ${initrd_addr} cpio.gz setenv bootargs コンソール= ${console} 、 ${baudrate} earlycon= ${earlycon} 、 ${baudrate} rdinit=/sbin/init ブーティ${loadaddr} ${initrd_addr} ${fdt_addr} ============================================================== 私の質問は次のとおりです: 次のような通常のルート ログイン プロンプトを取得するにはどうすればよいですか: root @imx 8mp-ddr4 -evk :~ 緊急モードに入るのを避けるために、ブート引数に必要な推奨変更はありますか? あらゆるご指導やご提案をいただければ幸いです。 よろしくお願いいたします。 バードワジ。 Re: IMX8MP DDR4 Custom board :: You are in emergency mode. こんにちは、 ログ全体を共有していただけますか? よろしくお願いいたします。 Re: IMX8MP DDR4 Custom board :: You are in emergency mode. こんにちは@JorgeCas 、 参考までに、以下のログ全体を添付します。 よろしくお願いします。
View full article
LS1021A 物联网网关参考设计 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> LS1021A 物联网网关参考设计 包含在套件中 Linux BSP和OpenWRT 参考设计(提供原理图、布局和BOM) 硬件快速入门指南和用户指南 如果您符合以下情况,您可能对该产品感兴趣: 需要一个随时可用的高性能物联网网关参考平台 需要内置 WiFi 和 Arduino 连接 想要一个可立即制造的硬件设计 主要硬件特点: 1 Gb QSPI NOR闪存 1 GB DDR3L SDHC 插槽 — 最大支持 32 GB,已安装 4 GB 1x 1 Gb/s以太网(SGMII) 1x 1 Gb/s以太网(RGMII) 2x mini PCIe (x1) slots 1x mSATA插槽 1x 终端(USB转UART) x 四线 LP-UART 至 Arduino 连接器(Thread、ZigBee、蓝牙等) • 多路复用 LCD/QE 接口 24 位 LVDS LCD 接口 QE UART 至 PROFIBUS 或 RS485 接头(需要外部收发器) • USB 3.0 2x 端口 - USB-A 2x 端口至 mini PCIe 插槽 • 13x GPIO 或 8x FTM (PWM) • 6x 中断 • 1 个 SPI • I 2 C1 总线板 EEPROM 启动 EEPROM Arduino 连接器传感器/PHY 等,待定 • I 2 C2 GPIO 扩展 ADC 传感器/PHY 等,待定 认证:FCC B类和CE 本产品的全部内容 产品图 点击此处购买 LS1021A 物联网网关参考设计 物联网物理组件 网关 SOC: QorIQ LS1021A 主板/模块: QorIQ LS1021A IoT网关参考设计 FRDM-KW24D512 软件: Linux BSP OpenWRT 通信基础设施
View full article
RD56F8300LCSM:采用恩智浦DSC的低成本软调制解调器参考设计 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Overview 特性 结构框图 电路板 设计资源 Overview 该参考设计展示了软调制解调器设计的简单性、它占用的处理器资源的少以及它在美国平均线路上的良好性能。该设计省略了标准电信Codec,而是采用PWM作为输出,ADC作为输入。 由于这两种外设都可以在一个56F8300/100系列器件上使用,并且具有比单核更高的处理能力,所以该设计是一个真正的单芯片、单核系统,具有电信功能,可以提供更多的系统功能。 非常适合高级运动控制、家用电器、医疗监控、消防和安全系统、电源管理、智能继电器和 POS 终端。 特性 混合架构有利于实现 V.21 和 V.22bis 调制解调器、控制和信号处理功能集成在一个芯片中 仅消耗 调制解调器功能运行速度为 7.5 MIPS - 完整的调制解调器应用程序和测试工具仅包含 15K 字的 Flash 高性能、安全的闪存消除了对外部存储设备的需求 扩展的温度范围允许非易失性存储器在恶劣环境下运行 EEPROM 的闪存仿真消除了对外部非易失性存储器的需求 具有16位代码密度的32位性能 片上稳压器和电源管理降低了整体系统成本 片外存储器扩展功能允许与外部设备的额外存储器进行无缝连接,而不会降低性能 直接从闪存引导,提供额外的应用灵活性 具有可编程故障功能的高性能PWM简化了设计并促进了安全法规的合规性 PWM和ADC模块紧密耦合以减少处理开销; 每个调制解调器仅使用其中的一个模块 通用输入/输出(GPIO)引脚支持特定应用的需求 通过增强型OnCE或串行通信简化应用中的闪存编程 结构框图 电路板 设计资源 传统设计 回复:RD56F8300LCSM:采用 NXP DSC 的低成本软调制解调器参考设计 在线购买管道材料时,必须验证规格以确保其满足您的项目需求。查找详细的产品描述,包括尺寸、材料和温度等级。
View full article
Slackware 上的所有 NFS 板块 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 网络文件系统 (NFS) 设置主机 1-在主机上安装 NFS 服务,输入: 您的 slackware linux 可能已经安装了某个版本的 nfs-utils,但如果没有,您可以从以下位置下载 nfs-utils: [1] 然后以 root 身份: #安装pkg nfs-utils-1.0.7-i386-1.tgz 2 – 设置导出输入: $sudo kedit /etc/exports 并添加以下行: /tftpboot/ltib/*(rw,no_root_squash,异步) 3 – 重新启动 NFS 服务器: $sudo /etc/rc.d/rc.rpc restart $sudo /etc/rc.d/rc.nfsd restart 现在主机已准备好使用 NFS。 设置目标 Linux 映像以使用 NFS 1-运行LTIB配置输入: $./ltib -c 2 - 在第一页菜单中,转到“目标图像生成->选项”,如下图所示。 3 – 选择仅 NFS 选项并退出 LTIB 配置以使用新配置进行编译。 4 - LTIB 应该开始新的编译并在 / /rootfs/boot/zImage 上创建一个新的 Linux 映像 5 - 将 / /rootfs/boot/zImage 上创建的图像复制到 /tftpboot/zImage 6 – 系统已准备好运行 NFS。目标上的根 文件 系统将位于主机上的 / /rootfs/
View full article
i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) 和 i.MX7ULP1 PRC2(Beta2) 发布公告 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 适用于 i.MX6 的 Linux L4.9.11_1.0.0 RFP(GA) 发布文件现已在www.nxp.com上提供 可用文件: # 名称 描述 1 L4.9.11_1.0.0-ga_图像_MX6QPDLSOLOX.tar.gz i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files 2 L4.9.11_1.0.0-ga_图像_MX6SLEVK.tar.gz i.MX 6Sololite EVK Linux Binary Demo Files 3 L4.9.11_1.0.0-ga_图像_MX6UL7D.tar.gz i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 4 L4.9.11_1.0.0-ga_图像_MX6SLLEVK.tar.gz i.MX 6SLL EVK Linux二进制演示文件 5 L4.9.11_1.0.0-ga_图像_MX7ULPEVK.tar.gz i.MX 7ULP EVK Linux二进制演示文件 6 L4.9.11_1.0.0-ga_mfg-工具.tar.gz 适用于 Linux 的 i.MX 制造工具包 L4.9.11_1.0.0 BSP 7 L4.9.11_1.0.0-ga_gpu-工具.tar.gz L4.9.11_1.0.0 i.MX VivanteVTK file 8 bcmdhd-1.141.100.6.tar.gz 适用于 i.MX Linux L4.9.11_1.0.0 BSP 的 Broadcom 固件包。 9 imx-aacpcodec-4.2.1.tar.gz 适用于 L4.9.11_1.0.0 的 Linux AAC Plus 编解码器 10 fsl-yocto-L4.9.11_1.0.0.tar.gz 适用于 Linux BSP 文档的 L4.9.11_1.0.0。包括发行说明、用户指南。   目标板: i.MX 6QuadPlus SABRE-SD 开发板和平台 i.MX 6QuadPlus SABRE-AI 开发板 i.MX 6Quad SABRE-SD 主板和平台 i.MX 6DualLite SABRE-SD 主板 i.MX 6Quad SABRE-AI电路板 i.MX 6DualLite SABRE-AI 板 i.MX 6SoloLite EVK 板 i.MX 6SoloX SABRE-SD电路板 i.MX 6SoloX SABRE-AI电路板 i.MX 7Dual SABRE-SD 开发板 i.MX 6UltraLite EVK 板 i.MX 6ULL EVK 板 i.MX 6SLL EVK 板 i.MX 7ULP EVK 板(Beta 质量)   新功能/功能: 请查阅发行说明。 已知问题 有关已知问题和更多详细信息,请参阅发行说明。 有关变更的更多信息,请参阅: 自述文件: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/README?h =imx-morty 变更日志: https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/tree/ChangeLog?h =imx-morty i.MX6_全部 i.MX6DL i.MX6 双核 i.MX6DualPlus6QuadPlus i.MX6 四核 i.MX6S i.MX6SL i.MX6SoloX i.MX6UL i.MX7 双核 i.MX7 单核 i.MX7ULP Linux 回复:i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) 和 i.MX7ULP1 PRC2(Beta2) 发布公告 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 供您参考: 如果您从官方 IMX7D Sabre 板下载 L4.9.11_1.0.0-ga_images_MX6UL7D.tar,并尝试刷新 SD 卡映像,则无法启动。(uboot错误) 旧图像 L4.1.15_1.2.0-ga_images_MX7DSABRESD.tar.tz 至少具有可运行的 uboot。 当然,您可以将正确的 uboot.imx 闪存到 SD 卡上(然后就可以工作了,因为其余数据都没问题),但这对于 EVK 图像来说并不是特别用户友好。 Re: i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) and i.MX7ULP1 PRC2(Beta2) Release Announcement Qt为什么不是5.9呢,能不能升级到5.9 Qtwayland相对完善 回复:i.MX 6/7D Linux L4.9.11_1.0.0 RFP(GA) 和 i.MX7ULP1 PRC2(Beta2) 发布公告 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> mfgtool 在 WIN10 下使用,检测到设备后,mfgtool 停止
View full article
LPC11u37h NFC 读卡器库移植指南(Ver 5.12)- 移植 NfcrdlibEx1_BasicDiscoveryLoop <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最新的 NFC 阅读器库支持 lpc1769,这是一个带有 LPCopen lib 支持的 cortex M3 控制器,因此理论上,它应该支持 LPCopen 支持的其他控制器,但我们必须对此进行测试,因此我们选择例如 lpc11u37(一个基于 cortex M0 的控制器)进行此移植。 本次移植的平台: LPC11u37h-Xpresso Rev A: CLRC663 加上基于 CLEV663B Blueboard 3.0。有关详细信息,请参阅准备 CLEV663B 板以进行 NFC 读取器库移植。 它们通过 LPCXpresso 端口连接。 现在我们可以开始移植了,本次移植使用的IDE是MCUXpresso 10.1.1 1. 下载并导入 CLEV6630B 的最新 NFC 读取器库,因为它支持 CLRC663 plus。 有关如何导入项目,请参阅https://www.nxp.com/docs/en/application-note/AN11211.pdf 。 2.下载适用于 LPC11u37h 的 LPCopen 并将其导入。 3.现在我们可以在NFC阅读器库中选择一些演示,例如NfcrdlibEx1_BasicDiscoveryLoop,并为lpc11u37h创建新的构建配置。 4.选择正确的MCU 5.修改构建设置 这里我们发现 LPC1769RC663 被定义了,所以我们必须在代码中找到与这个定义相关的内容并改变它/它们。 幸运的是,这样的人并不多。您可能会发现它们仅与板头文件或类似的东西有关,因此修改它们并不困难。 6.为新的板定义添加新的头文件 7.添加新的板定义 8.由于我们现在使用 LPCopen lib 来代替 LPC11u37h,所以我们必须更改包含路径。 由于 LPC11u37h 基于 Cortex M3,因此我们必须设置 FreeRTOS 以支持 M0: 并添加构建源代码: 9.更改链接库和包含路径 10.设置正确的参考项目以将 LPCopen 用于 LPC11u37h。 11.LPCopen 库中的一些变化: 1)启用半主机调试 2)为演示添加启动源代码,该C文件可以从某些lpcopen项目中重用/导入。 12.完成上述步骤后,我们还要更改DAL中的源代码: 您知道,由于 LPCopen 库的版本不同,某些函数定义可能会发生变化,并且不同的 LPCXpresso 板与 LPCXpresso 端口的引脚连接也不同,因此建议检查电路板原理图和 lpcopen 项目中的示例,找到适当的函数调用来实现 DAL 文件夹中的源代码。完成后,移植就完成了。 13.由于最终图像大小大于128K,我们启用了尺寸优化。 14.Demo test ok. 现在,我们知道lpc11u37可以被最新的NFC读取器库支持,因此移植也应该适用于其他Cortex M0控制器,并且建议使用具有较大内部闪存容量的控制器,最好大于128K,但无论如何,在此移植中,我没有启用LPCopen库的大小优化,因此最终可能会有更小尺寸的图像...... NFC 前端解决方案 NFC读卡器库
View full article
MPC5777C CSE CSE_ECR=0X02 命令序列错误 大家好, 客户目前正在做CSE密钥加载&擦除(用for循环,先加载密钥再擦除密钥约10000次)测试实验。 但是经过10000次测试后,再次打开MCU电源,密钥无法再加载或擦除,并且CSE_ECR = 0x02报告命令序列错误,并且其他CSE命令发送到CSE时也会出现此错误。CANCEL 是 CSE 唯一会接受且不会出现 0x02 错误的命令。此问题与此工单相同,但没有正确答案: https://community.nxp.com/t5/MPC5xxx/MPC5777C-CSE-Problem/mp/589107#M4239 所以问题是如何处理这个问题,因为在这种情况下密钥不能再被加载或擦除,并且 CSE 命令也不能被 CSE 核心接受。 我比较了正常芯片(在 EVB 上用新芯片替换)和问题芯片,发现 SR_BFN 位和 CSE_ECR 位不同,SR_BFN 位表示安全启动完成,但我没有在问题芯片上启用安全启动。 错误一: 正常一个: 回复:MPC5777C CSE CSE_ECR=0X02 命令序列错误 Hi Lukas, 听起来很有道理,如果这一点应该注意Key擦除,那么应该在文档中弄清楚,因为在我们正常的调试过程中,在调用DEBUG_CHAL + DEBUG_AUTH时,我们可能会意外重启或再次打开电路板。 回复:MPC5777C CSE CSE_ECR=0X02 命令序列错误 Hi Lukas, 有没有任何文档提到这一点? 回复:MPC5777C CSE CSE_ECR=0X02 命令序列错误 Hi @Zhongling_Lang  最有可能的是,这是由于意外重置或 MCU 电源循环之前的超时时间太短造成的(在闪存上执行的擦除周期越多,擦除闪存所需的时间就越长)。 如果由 DEBUG_CHAL+DEBUG_AUTH 命令触发的擦除操作因意外重置而终止,则会导致 CSE 无法使用并且无法恢复。 无论如何,这不是实际应用中预期的用例。DEBUG_CHAL+DEBUG_AUTH 应该只在开发期间使用,而不是在现场使用。 此致, Lukas
View full article
星型拓扑中的 PCA9615 Hi, 我正在开发基于 4 个 I2C 传感器和 PCA9615 的系统,它们通过星型拓扑中的 CAT5 电缆连接,如图所示(电缆长度以米为单位)。 如果我连接 3 个或更少的传感器,系统就能正常工作,连接第 4 个传感器后,所有通信都会中断。我检查了较短的电缆(每根约 20 厘米),其行为是一样的。当在 MCU 端使用两个 PCA9615 时,每个 PCA9615 连接 2 个传感器,通信没有问题(第二张图) PCA9615 应该在这样的拓扑结构中工作吗?什么原因会导致这些问题? 一些细节: 整个系统在 3.3V 下运行,传感器由 CAT5 电缆供电(VDDA 和 VDDB 短路) 在 MCU 和每个传感器上我使用终端电阻 R2=100ohm、R1=390ohm,取自 Sparkfun 设计(PCA9615 数据表建议 R2=120ohm、R1=600ohm(5V)) I2C速度为100KHz RJ45 分离器是无源的,它们只是将信号从一个端口分离到另一端的两个端口 非常感谢您的帮助,谢谢。 回复:星型拓扑中的 PCA9615 Hi Karol, 没关系。很高兴能帮上忙。祝你今天过得愉快。 最诚挚的问候, Jozef 回复:星型拓扑中的 PCA9615 感谢您的快速回复! 我将根据提供的计算结果更改终端电阻,现在对我来说看起来更加清晰了。 我已经看到了文档中提供的示意图,它们都假设总线拓扑在 MCU 端和总线的另一端终止。我将仅使用一个带终端的传感器和其他不带终端的传感器来测试我的系统(文档指出要使电缆尽可能短,但我无法使它们短于 1-2 米)。 我怀疑星型拓扑结构的所有端点终止都应该被考虑在内,并且电阻的计算方式与仅有 2 端点的电阻计算方式不同。但我更像是嵌入式软件工程师而不是电子专家,因此对于该原型而言,任何工作设计都可以。 回复:星型拓扑中的 PCA9615 Hi Karol, 对于多目标 dI2C 设计,请参阅图 8 和图 9。取决于您是否要通过电缆布线 VDD 和 VSS。 有关终端电阻的计算,请参阅下面应用工程师对另一位客户的详细回答。 di2c 的外部电阻器经过精心选择,以便在整个线路上提供至少 200 mV(最大接收器阈值)的偏置。 上拉电阻 (R1) 和下拉电阻 (也称为 R1) 应始终保持相等的阻值。这可为驱动器提供对称负载。终端电阻 Rb(从端电缆终端电阻)的选择应使其与双绞线电缆的特性阻抗 (ZO) 匹配。如果终端电阻与线路匹配,即 Rb = ZO,则不会产生反射。 在电缆的另一端,R2 和两个 R1 电阻的等效电阻也应与线路的特性阻抗匹配。在这种情况下,R2 与 R1 和 R1 并联 (R2//(R1 + R1))。为了使该等效电阻与线路匹配,R2 必须大于 ZO。R2 通常比 ZO 大 10Ω 到 20Ω,但实际值取决于 R1 和 R1 的值。 故障安全偏置 (Vfsb) 是线路上的压降,Rb 与 R2 并联 (Req = Rb // R2)。因此,故障安全偏置只是 Req、R1 和 R1 之间的分压器。 对于此示例,假设电缆的特性阻抗(ZO)为 120Ω,这是一个典型值。 步骤 1. 假设 R2 和 Rb 相等,并且选择与 ZO 匹配。 R2 = Rb = ZO = 120Ω 步骤2.计算R2//Rb的等效并联电阻。 R2 // Rb = 120Ω // 120Ω = 60Ω 步骤 3. 计算上拉和下拉电阻值,已知 FAILSAFE 偏压为 200 mV,VCC = 3.3V。 Vfsb = VCC(Req/(R1 + Req + R1)) 求解 R'(定义为 R1 + R1) R' = ((Req)VCC/Vfsb) − Req R' = ((60Ω)3.3V/0.2V) − 60Ω = 930Ω 由于R1和R1相等,因此R1 = R1 = 930Ω/2 = 465Ω 步骤4.重新计算R2//(R1 + R1)的等效电阻。 R2//(R1+R1)=120Ω//(465Ω+465Ω)=106Ω 由于等效电阻不在电缆特性阻抗 (ZO) 的 10% 范围内,因此需要进一步调整电阻值。R2 的匹配值可以通过将以下公式代入 ZO 并求解 R2 来计算。 ZO = R2 // (R1 + R1) ∴Rc=138Ω 现在等效电阻(Req = R2 // Rb)变为 138Ω // 120Ω = 64Ω,与原来的 60Ω 足够接近。 在重新计算故障安全偏置电位之前,可以替换标准电阻值,以简化电阻选择、降低成本并提高可用性。使用 5% 容差表,我们找到以下标准电阻值:R1 = 470Ω,Rb = 120Ω,R2 = 130Ω,R1 = 470Ω 为了验证所选值是否符合标准,应完成以下计算: 1. R2//(R1 + R1)=ZO 130Ω//(470Ω+470Ω)=114Ω(由于等效电阻在电缆特性阻抗(ZO)的10%以内,因此不需要进一步调整电阻值)。 2. Req=Rb//R2 120Ω//130Ω=62Ω(更接近原来的60Ω)。 3. Vfsb = VCC (Req/(R1+Req+R1)) 3.3V(62Ω/(470Ω+62Ω+470Ω))=204毫伏 总结: R1 = 470Ω,R2 = 130Ω,R1 = 470Ω,应该适合您的应用。 最诚挚的问候, Jozef Re: PCA9615 in star topology 我知道这已经是两年前的事情了,但我想从 Virage 了解一下,它是作为星形系统在所有四个传感器上都装有终端电阻器,还是在其中一个传感器上装有终端电阻器? 此致, 戴维
View full article
基于 RDB2 v2.0 板上的 SDK BSP40 的 EMMc 写入失败 Hi, 最近尝试在RDB2 v2.0板上测试基于SDK BSP40的EMMc启动案例。但是当我尝试将 fip.s32 图像写入 EMMc 时,电路板重置,如以下日志所示: root@nxp-s32g:~# flashcp -v fip.s32-qspi-bsp40 /dev/mtd0 擦除块:18/18(100%) 写入数据:1106k/1106k (100%) 验证数据:1106k/1106k (100%) root@nxp-s32g:~#重启 注意:复位状态:上电复位 注意:BL2:v2.5(发布):bsp40.0-2.5 通知:BL2:建造时间:2024 年 3 月 21 日 08:41:20 注意:BL2:启动 BL31 U-Boot 2022.04+gd482def7e3+p0(2024 年 3 月 21 日 - 08:40:56 +0000) SoC:NXP S32G274A 修订版。2.0 CPU:ARM Cortex-A53 r0p4 @ 最高 1000 MHz 型号:NXP S32G274A-RDB2 动态随机存取存储器:3.5 GiB 核心:305 个设备、25 个 uclass、设备树:board MMC: FSL_SDHC: 0 从 SPIFlash 加载环境...SF: 检测到 mx25uw51245g,页面大小为 256 字节,擦除大小为 64 KiB,总计 64 MiB 好的 s32cc_serdes_phy serdes@40480000:对SerDes子系统使用模式0 pci_s32cc pcie@40400000: 无法设置设备 ID pci_s32cc pcie@40400000:配置为 RootComplex pci_s32cc pcie@40400000: 无法建立链接 输入:serial@401c8000 输出:serial@401c8000 错误:serial@401c8000 主板修订版:RDB2/GLDBOX 修订版 C PCIe:BusDevFun VendorId DeviceId 设备类 子类 ________________________________________________________________________ pcie@40400000 根复合体 | `-- 01:00.00 0x1957 0x4002 桥接设备 0x04 网络:eth0:ethernet@4033c000 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 按任意键停止自动启动:0 => mmc 重新扫描 => mmc 列表 FSL_SDHC: 0(eMMC) => FSL_SDHC: 0(eMMC) => DHCP ethernet@4033c000 等待 PHY 自动协商完成.......完成 BOOTP广播1 BOOTP 广播 2 *** OFFER/ACK 中未处理的 DHCP 选项:43 *** OFFER/ACK 中未处理的 DHCP 选项:43 DHCP 客户端绑定到地址 128.224.35.131(282 毫秒) 使用以太网@4033c000设备 来自服务器 128.224.161.77 的 TFTP;我们的 IP 地址是 128.224.35.131;通过网关 128.224.34.1 发送 文件名“undionly.kpxe”。 加载地址:0x8a080000 加载中: ##### 6.3 MiB/秒 完毕 传输的字节数 = 72763(11c3b 十六进制) => 设置环境服务器 IP 128.224.34.193 => 设置环境网关 IP 128.224.178.1 => => 设置环境网络掩码 255.255.254.0 => => => => => 运行 loadtftpimage 使用以太网@4033c000设备 来自服务器 128.224.34.193 的 TFTP;我们的 IP 地址是 128.224.35.131 文件名“图像”。 加载地址:0x8a080000 正在加载:##################################################################### ############# ## 9.2 MiB/秒 完毕 传输的字节数 = 1134464(十六进制 114f80) => setexpr loadaddr${loadaddr} + 0x1000 => setexpr n_b 0 00 00 => setexpr n_blocks 0x114f80 / 0x200 => 优先块 n_blocks=8a7 => setexpr n_blocks${n_blocks} - 7 => 优先块 n_blocks=8a0 => mmc 重新扫描 => mmc 列表 FSL_SDHC: 0(eMMC) => mmc 写入${loadaddr} 8${n_blocks} MMC 写入:设备 # 0,块 # 8,计数 2208。注意:复位状态:上电复位 注意:BL2:v2.5(发布):bsp40.0-2.5 通知:BL2:建造时间:2024 年 3 月 21 日 08:41:20 注意:BL2:启动 BL31 U-Boot 2022.04+gd482def7e3+p0(2024 年 3 月 21 日 - 08:40:56 +0000) SoC:NXP S32G274A 修订版。2.0 CPU:ARM Cortex-A53 r0p4 @ 最高 1000 MHz 型号:NXP S32G274A-RDB2 动态随机存取存储器:3.5 GiB 核心:305 个设备、25 个 uclass、设备树:board MMC: FSL_SDHC: 0 从 SPIFlash 加载环境...SF: 检测到 mx25uw51245g,页面大小为 256 字节,擦除大小为 64 KiB,总计 64 MiB 好的 s32cc_serdes_phy serdes@40480000:对SerDes子系统使用模式0 pci_s32cc pcie@40400000: 无法设置设备 ID pci_s32cc pcie@40400000:配置为 RootComplex pci_s32cc pcie@40400000: 无法建立链接 输入:serial@401c8000 输出:serial@401c8000 错误:serial@401c8000 主板修订版:RDB2/GLDBOX 修订版 C PCIe:BusDevFun VendorId DeviceId 设备类 子类 ________________________________________________________________________ pcie@40400000 根复合体 | `-- 01:00.00 0x1957 0x4002 桥接设备 0x04 网络:eth0:ethernet@4033c000 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 发现PFE版本0x50300(S32G2) ELF 文件太大,大小:4294836224 PFE 固件文件“ @0x030a0000: ”加载失败:-27 按任意键停止自动启动:0 => => 首先,我尝试将 fip-qspi.s32 映像写入 qspi flash,然后从 qspi flash 启动,并在 uboot 阶段写入 fip.s32-sdcard图像到 EMMc。此时,电路板按上述方法重置。 您能帮忙检查一下这个问题吗? 谢谢! Zhantao 回复:基于 RDB2 v2.0 板上的 SDK BSP40 导致 EMMc 写入失败 Hi @chenyin_h , 感谢您的回复。 您的回复非常有帮助,该问题可以按照您的建议解决。 谢谢! Zhantao 回复:基于 RDB2 v2.0 板上的 SDK BSP40 导致 EMMc 写入失败 Hello, @hittzt 我已经在本地 RDB2 REVC(配备 2.0 硅片)上重现了它,并发现可以通过禁用 u-boot 配置中的以下选项来修复它:MMC_IO_VOLTAGE,您可以尝试一下。 我也与内部团队讨论过这个问题,并确认这里的主要问题与 Silicon 2.0 无关,而与主板修订有关,RDB2 REVC 上 eMMC 的默认电压供应为 3.3V,但 BSP40 的默认模式使用 1.8v,这可能是问题的根本原因。 希望对您有帮助。 顺祝商祺! 陈银 回复:基于 RDB2 v2.0 板上的 SDK BSP40 导致 EMMc 写入失败 Hello, @hittzt 感谢您的反馈。 很高兴听到该问题似乎仅存在于采用 2.0 芯片的 RDB2 上。 抱歉,我们团队中没有基于 2.0 硅片的开发板,请让我检查一下其他团队是否有,在获得进一步结果后会进行更新。 很抱歉给您带来不便。 顺祝商祺! 陈银 回复:基于 RDB2 v2.0 板上的 SDK BSP40 导致 EMMc 写入失败 Hi @chenyin_h , 谢谢你的回复。 我在 RDB2 v2.0 和 RDB3 v1.1 板上测试了该情况,并且 RDB3 v1.1 与 EMMc 启动模式配合良好。 而且我手里没有 RDB2 v2.1 板。 您能帮忙检查一下您那边 RDB2 v2.0 板的状态吗? 谢谢! Zhantao 回复:基于 RDB2 v2.0 板上的 SDK BSP40 导致 EMMc 写入失败 Hello, @hittzt 感谢您的提问。 抱歉,我没有在本地重现该问题,这里的细微差别是我使用的是带有 2.1 芯片的 RDB2。您是否在其他论坛上遇到过类似的问题? 附上日志供您参考。 顺祝商祺! 陈银
View full article
iMX8M QuadでのDRMサポート Hello, iMX8M QuadがDRM、Widevineをサポートしているかどうか教えてください。 もしそうなら、DRMサポートのためにNXPとのライセンス契約が必要ですか? ありがとうございます。 よろしくお願いいたします。 Andy Re:iMX8MクワッドのDRMサポート Hello, i.MX8Mは、AndroidでWidevineレベル1をサポートできます。この点については、NXPプロフェッショナルサービスを通じて取り扱われていますが、いくつかの作業が行われているため、共有できる価格に関する公開情報はありません。(i.MX8MはLinuxでもサポートできるはずです) 詳細については、NXPプロフェッショナルサービスにお問い合わせください。 https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE よろしくお願いします。
View full article
将 AUTOSAR OS 生成从 EB tresos 导入 S32 工具 MBDT 尊敬的恩智浦同事们: 我正在将 EB tresos 配置导入 S32 工具 .mex电机控制示例项目 S32K396_MBDT_BASED_MC_0_9_0 的文件。 所以我已经导入了所有的.epc文件(Resource.epc 除外)放入 S32 工具中,但仍然有错误。我可以在哪里获取 EBT 项目的这些信息来修复错误。 尝试导入 Resource.epc 时出错 S32工具中的错误列表 我附加了 .mex包含所有 .epc 文件已加载。 谢谢, 阿古斯丁。 @Irina_Costachescu 回复:将 AUTOSAR OS 生成从 EB tresos 导入到 S32 工具 MBDT 你好@Irina_Costachescu , 感谢您提供详细的示例和介绍,指导如何将 mbdt 演示中使用的 EB 项目导入 S32DS IDE。干得好! Hi @agus_idiada, 我将列出有关 mbdt 演示中使用的 DMA 通道的信息,还包括一些与 DMA 通道使用相关的注释。 演示中使用的 DMA 通道概览: 实例 1, 通道6~7,用于将处理后的SDADC结果(在Dspss中)传输到Etpu进行旋转变压器计算, 通道8与通道6联动,用于传输激励信号触发。 详细配置如下图所示: Overview 通道6 通道7 8频道 上面的快照列出了生成的配置。另外需要注意的是,DMA通道仍然需要配置源地址和目标地址。请检查文件 common/etpu_motor/motor_bsp/mbd_user_init.c 中的代码 void Dma_User_Config(void) 。该函数在配置板初始化部分被调用,详情请参阅演示指南。这里列出了函数代码并附带注释。 因此,请检查并确保生成后 Dma_User_Config() 中使用的宏/定义是正确的。 谢谢! 文森特 回复:将 AUTOSAR OS 生成从 EB tresos 导入到 S32 工具 MBDT Hello @agus_idiada  请查看附件中的 .mex文件没有错误。我已经测试过,按下“更新代码”按钮时它会成功生成配置代码,我想对您遇到的问题添加一些评论。   一般来说,将配置从 EB Tresos 迁移到 S32 配置工具的过程并非完全自动化。这意味着,即使 .epc文件导入到 .mex 中文件,还必须进行一些手动更改以确保配置没有任何错误。   要导航到导致在问题视图中显示错误的设置,您可以双击该特定问题,GUI 将打开包含未按预期配置的项目的特定配置选项卡。将鼠标悬停在错误上可以提供有关驱动程序方面预期的详细信息。因此,将来请注意,此过程可以帮助您找出错误的原因。     我按照这种方法所做的工作如下所述:   1.我已经删除了 I2C、LIN、ICU 和 CAN 组件,因为它们没有在演示中使用,因此没有在 EB Tresos 项目中配置。由于 MCU 和 MCL 组件的配置与工具箱提供的默认配置不同,因此缺少讨论中的组件的一些设置(例如,Lin 外围参考时钟(未在 MCU 中配置)、I2C FlexIO 通道(需要在 MCL 中启用 - 这只是两个示例)。   2. 由于为 AdcHwUnits 3 和 4 启用了 ADC_DMA,因此该工具也需要在配置中启用 DMA 通道。由于 EB Tresos 工具内的驱动程序似乎没有实现此约束,我恳请@Vincent_Deng在此提供更多信息,说明每个配置的 SDADC 实例应该使用哪个通道。目前,我刚刚允许他们修复错误   3. S32CT 环境中的 MCU 组件设置需要与时钟工具中启用的设置相匹配。由于 Mcu 组件是从 EB Tresos 项目导入的,包含应用程序所需的设置,因此我已更新时钟工具设置以匹配 Mcu 中的设置。为了执行此操作,您可以检查 Mcu 组件中的错误设置,然后转到时钟工具并在那里进行相应的更新。所需的修改意味着:   - 更改时钟源 - 可以通过双击相应的时钟分频器并选择适当的源来完成     - 启用时钟源分频器 - 双击相应的分频器块并从右侧选项中选择适当的选项   此搜索栏可帮助您找到时钟工具内必要的 MUX 和设置。   请让我们知道此配置是否也适用于您的设置。   谢谢! Irina
View full article