Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
CSCI E-251,2012 年秋季 - 最终项目演示 - Kate Fischl <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 哈佛大学继续教育学院 CSCI E-251,2012 年秋季:操作系统原理 最终项目展示 凯特·菲舍尔 (Kate Fischl) 演讲 (在 “我的视频” 中查看) 学生项目
View full article
使用 KDS 在 FRDM-KL46 板上进行反应测量游戏 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> KDS 中的反应游戏   说明:   在 KDS 中制作的一个项目,使用 FRDM-MKL46Z256VLL4 板的 LCD 屏幕和两个开关 SW1 和 SW3,创建一个反应测试游戏。 用两个拇指握住电路板的两个开关上方。 出现“rdy”(就绪)后,屏幕将显示“left”(左)、“righ”(右)或“both”(两者),您必须按下相应的按钮。 然后它将以毫秒为单位显示您的反应时间。 您最初有 1000 毫秒的时间做出反应,每得分一分,反应时间就会减少 25 毫秒,最少为 500 毫秒。 每正确回答一次可得 1 分。 如果您反应不够快,或者按了错误的按钮,您就会输掉游戏。 一旦您输了,您的分数就会显示出来,然后游戏将重置回“rdy”,并有 1000 毫秒的时间做出反应。   问题: 您可以通过每次按下两个按钮来作弊,但这不会 100% 有效。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> KDS 中的反应游戏   说明:   在 KDS 中制作的一个项目,使用 FRDM-MKL46Z256VLL4 板的 LCD 屏幕和两个开关 SW1 和 SW3,创建一个反应测试游戏。 用两个拇指握住电路板的两个开关上方。 出现“rdy”(就绪)后,屏幕将显示“left”(左)、“righ”(右)或“both”(两者),您必须按下相应的按钮。 然后它将以毫秒为单位显示您的反应时间。 您最初有 1000 毫秒的时间做出反应,每得分一分,反应时间就会减少 25 毫秒,最少为 500 毫秒。 每正确回答一次可得 1 分。 如果您反应不够快,或者按了错误的按钮,您就会输掉游戏。 一旦您输了,您的分数就会显示出来,然后游戏将重置回“rdy”,并有 1000 毫秒的时间做出反应。   问题: 您可以通过每次按下两个按钮来作弊,但这不会 100% 有效。 概述
View full article
VsetとVregの違い Vset:電圧を設定します。LINモードでは、レギュレーションvoltageはLINRXフレームによって設定されます。设定调节电压。LIN调节模式下,Vset为LIN协议RX帧设定的调节电压值;默认模式下,Vset为OTP中写入的默认调节电压。 Vreg:レギュレーション電圧。デバイスが調整する実際の値。温度補償または LIN タイムアウト中、Vreg は Vset と等しくありません。//调节电压。芯片实际工作中调节的目标电压值。温度补偿或者LIN超时,实际的调节电压Vreg会不等于Vset。 オルタネータ・レギュレータ
View full article
PCT2075 - Temperature data streaming using UTICK timer on the LPC55S06-EVK Hi Everyone, In this document I would like to present a very simple example code I created for the PCT2075. This I2C digital temperature sensor offers a resolution of 0.125°C with an accuracy of ±1°C over -25°C to 100°C range. It operates with a single supply from 2.7V to 5.5V and has three address pins, allowing up to 27 devices to operate on a single I2C bus without address collisions. The device also includes an open-drain output (OS) which becomes active when the temperature exceeds the programmed limits. NXP offers the PCT2075DP Arduino Shield and GUI for easy evaluation of this temperature sensor. However, I have decided to pair this demo board with the LPC55S06-EVK and create a simple example code in the MCUXpresso IDE using Config tools (Pins, Clocks and Peripherals). The connection is very straightforward. The PCT2075DP-ARD daughter board is inserted to J9, J10, J12 and J13 connectors located on LPC55S06-EVK development board. Both SDA pin (J1-5) and SCL (J1-6) lines are connected through the on-board 5.6K pull-up resistors to the FlexComm1 SDA (PIO0_13, J13_9) and SCL (PIO0_14, J13_11) pins on the LPC55S06-EVK board. The VCC pin (J6-4) is connected to the 3.3V supply voltage and the GND pin to common ground. The address select pins A0, A1 and A2 are connected to GND using jumpers between pins 2 and 3 of J7, J8 and J9, resulting in a 7-bit I2C slave address of 0x48. I created a new project in MCUXpresso IDE v11.3.0 based on SDK_2.8.2_LPCXpresso55S06 using the New project wizard: It was not necessary to make any changes to the project and I named it LPC55S06 PCT2075 Temp reading using I2C in the wizard: Let’s start with the Pins Config tool...: ...to configure PIO0_13 and PIO0_14 for their I2C functions (I2C_SDA and I2C_SCL, respectively). Simply search for each pad in the Pins view: In the diagram above, I already have PIO0_13 routed for I2C function (it is showing green). However, you may want to check the checkbox in the first column to mark the pin for routing. A dialog pops up, offering you all the possible pin multiplex functions for the pad. Scroll down through the list and select FlexComm1’s SDA function: When you put a checkmark (“tick”) in the FC1_CTS_SDA row, the Pins Config tool routes the pad and you will see a new entry (in yellow) in the Routed Details view at the bottom of the perspective: Follow the same procedure to route PIO0_14 for function FC1_SCL. That is already done in the screen-grab above, so I am ready to move to the Peripherals Config tool.  Use the Peripherals icon to switch to the Peripherals perspective: The Peripherals Config tool identifies that I have set up the pads/pins for FlexComm1 to be used as I2C. But I have not yet set up the I2C peripheral, and so the tool reports a Warning: There is a very simple fix, proposed by the tool. Select the FLEXCOMM1 warning line, and right-click to bring up a context menu: Selecting “Initialize FLEXCOMM1 peripheral” opens a dialog where I can select the desired function for FlexComm1… in this case I want I2C configuration. So I select I2C and click [OK]: The Peripherals Config tool displays the Flexcomm Interface I2C configuration screen. This shows all of the ‘top level’ settings for the I2C module. I configured it as follows: As the PCT2075 does not have a data ready interrupt, I use the MicroTick (UTICK0) timer to read the Temp register periodically at a fixed rate of about 10Hz since the temp-to-digital conversion is executed every 100 ms. The UTICK0 is configured in the Peripherals Config tool as follows: I am ready to move to the final, Clocks Config tool: I chose to use the BOARD_BootClockFRO12M() functional group: Then I enabled the clock to FlexComm1, since this is the FlexComm module that I use for I2C. I used the fro_12m as the clock source for FlexComm1 I2C: Finally I enabled the fro_1m and attached the fro_1m to the UTICK timer: All the configuration is now complete. I can click “Update Code” at the top of the screen to generate all of the necessary configuration code, accept the changes, and return to the C/C++ Develop perspective. In the UTICK0_Callback function, the Temp register is read and then the real temperature in °C is calculated as shown below. For more information on how to convert the raw values from the Temp register to real values in °C, please refer to the PCT2075 data sheet (Chapter 7.4.3). This screenshot shows the two bytes read of the Temp register (0x00).  The calculated temperature can be watched either in the "Global Variables" window on the top right of the Debug perspective...: ...or in the Console window: Attached you can find the complete project developed in the MCUXpresso IDE v11.3.0. If there are any questions regarding this simple application, please feel free to ask below. Regards, Tomas
View full article
Smart Peephole Overview Features Use Cases Block Diagram Products Overview Smart, integrated building systems empower users to improve energy efficiency, lower maintenance costs, and conveniently control environments from smartphones and advanced HMIs. Their interconnected features house a platform of big data to make smarter, environmental-friendly decisions while ensuring maximum comfort and performance. Features Smart Peephole implement camera capture and LCD display function at the same time. Touch screen to trigger JPEG compression and storage. User can take it as a reference for basic framework for video transfer. Optional WiFi & BLE module to transmit the captured information to the user. Use Cases Home secure. Supervising children and pets. Loss prevention. Locating bugs and pests. Vandalism deterrence. Block Diagram Products Category MCU Product URL i.MX RT1050 Crossover MCU with Arm® Cortex®-M7 core  Product Description The i.MX RT1050 is the industry's first crossover MCU and combines the high-performance and high level of integration on an applications processors with the ease of use and real-time functionality of a microcontroller. Category RTC Product URL PCF85063TP: Tiny Real-Time Clock/calendar  Product Description The PCF85063TP is a CMOS Real-Time Clock (RTC) and calendar optimized for low power consumption. Category Wireless Product URL 1 QN902X: Ultra low power Bluetooth LE system-on-chip solution  Product Description 1 QN902x is an ultra-low power, high-performance and highly integrated Bluetooth LE solution. Product URL 2 88W8801: 2.4 GHz Single-Band 1x1 Wi-Fi® 4 (802.11n) Solution  Product Description 2 The 88W8801 is a highly integrated, single-band (2.4 GHz) Wi-Fi 4 1x1 System-on-Chip (SoC), specifically designed to support High Throughput (HT) data rates. Block Diagrams Smart Home
View full article
Sensor Toolbox GUI インストーラ Rev.4.2.0.8 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 以下は、Sensor Toolbox GUIのリビジョン4.2.0.8のインストーラーファイルです <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 以下は、Sensor Toolbox GUIのリビジョン4.2.0.8のインストーラーファイルです 加速度センサ 圧力センサ タッチ・センサ
View full article
POS Printer Overview Block Diagram Recommended Products Documentation Overview NXP ®  offers PowerQUICC ® . and ColdFire ® . processors and a large selection of 8-bit MCUs that support common point-of-sale (POS) printer applications for retail and services industry customer receipts. Benefits include Low cost and complexity OS support to control print-heads, paper handling, character management, scanner inputs Management of digital/analog inputs and controls Multiple connectivity options Flexibility to address multiple mixed-feature applications Block Diagram Recommended Products Category Name MCU and MPU 32-bit Microprocessor with USB On-The-Go, Ethernet, PCI, DDR2/DDR controller and Encryption | NXP  32-bit MPU, 10/100 ETH, USB OTG, PCI. i.MX258 Processors|Point of Sale (POS) | NXP  400 MHz Arm9®, SVGA, 10/100 ETH, CAN, tamper detection, <1W i.MX28 Applications Processors: Integrated Power Management Unit (PMU), Arm9™ Core | NXP  454 MHz Arm9®, SVGA, 10/100 ETH, CAN, PMU, <1W i.MX 6Solo Applications Processors | Single Arm® Cortex®-A9 @ 1GHz | NXP  1 GHz Arm® Cortex™-A9, 2xWXGA, graphics, video, 10/100/1000 ETH, CAN, PCIe, PMU 8-bit Flexis QE MCUs | NXP  Flexis Low-Power 8-bit MCU 4-128K Flash. Category Name Power Management 3.0A 1.0MHz DDR Switch-Mode Power Supply | NXP  Li-Ion Battery Charger, DDR Switch-Mode Power Supply (3.0A, 1MHz). Category Name Signal Conditioning MC33972 | MSDI with Suppressed Wakeup | NXP  Switch Detector 22 contacts. MSDI | NXP  Switch Detector 22 contacts. Category Name Print Sensor 0 - 10kPa Integrated Pressure Sensor | NXP  Sensor On-Chip Signal Conditioned, Temperature Compensated and Calibrated. Category Name Motor Driver MC33880 | Octal Serial Switch with SPI | NXP  Configurable Octal Serial Switch (LSS / HSS) for Motor Drive. MC34931 | H-Bridge, Brushed DC Motor Driver | NXP  H-Bridge Brushed DC Motor Driver, 5-28V, 5A, 11kHz MC34932 | H-Bridge, Brushed DC Motor Driver | NXP  H-Bridge Brushed DC/Stepper Motor Driver, 5-28V, 5A, 11kHz MC33886 | H-Bridge, Brushed DC Motor Driver | NXP  H-Bridge Brushed DC Motor Driver, 5-28V, 5A, 10kHz MC33926 | H-Bridge, Brushed DC Motor Driver | NXP  H-Bridge Brushed DC Motor Driver, 5-28V, 5A, 20kHz Dual H-Bridge Motor Driver 2-8.6 V 1.4 A 200 kHz | NXP  H-Bridge Brushed DC/Stepper Motor Driver, 2-8.6V, 1.4A, 200kHz H-Bridge DC Motor Driver 2-15 V 3.8 A 200 kHz | NXP  H-Bridge Brushed DC Motor Driver, 2-15V, 3.8A, 200kHz Documentation Application Notes: Simplified EHCI Data Structures for the High-End ColdFire ®  Family USB Modules https://www.nxp.com/docs/en/application-note-software/AN3522.pdf Block Diagrams Smart City
View full article
KDS - FRDM KL25Z 上的简易空中鼠标 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 根据 Erich 的HID 鼠标教程,这是一个简单的符合 HID 标准的空中鼠标,其指针由板载加速度计控制。     关于如何制作该项目的完整教程可以在 Zip 中的“FRDM KL25Z 上的简单空中鼠标.pdf”中找到。旨在全面解释在 KDS 中构建项目的过程、如何设置板以进行 HID 交互以及如何设置加速度计。   感谢 Erich Styger 提供的原始教程和见解,以及他非常方便的组件库。   如果我造成了混淆或者忘记记录某些事情(毫无疑问我会有),请不要害怕给我留言让我知道,我会更新相关文件。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 根据 Erich 的HID 鼠标教程,这是一个简单的符合 HID 标准的空中鼠标,其指针由板载加速度计控制。     关于如何制作该项目的完整教程可以在 Zip 中的“FRDM KL25Z 上的简单空中鼠标.pdf”中找到。旨在全面解释在 KDS 中构建项目的过程、如何设置板以进行 HID 交互以及如何设置加速度计。   感谢 Erich Styger 提供的原始教程和见解,以及他非常方便的组件库。   如果我造成了混淆或者忘记记录某些事情(毫无疑问我会有),请不要害怕给我留言让我知道,我会更新相关文件。 概述
View full article
How use USB as both gadget mode and host mode usb USB_OTG Q:How use USB as both gadget mode and host mode usb USB_OTG? A: Hardware: imx6 sabresd board usb otg diagram, as follow Software: You can use USB OTG port for both host mode and device gadget mode. There are 2 signals you should care: - USB_OTG_ID - USB_OTG_MODE (control power for usb vbus in host mode, this is EIM_D22 pin) In device tree: reg_usb_otg_vbus: regulator@0 {                         compatible = "regulator-fixed";                         reg = <0>;                         regulator-name = "usb_otg_vbus";                         regulator-min-microvolt = <5000000>;                         regulator-max-microvolt = <5000000>;                         gpio = <&gpio3 22 0>;                         enable-active-high;                 };   pinctrl_usbotg: usbotggrp {                         fsl,pins = <                                 MX6QDL_PAD_GPIO_1__USB_OTG_ID           0x17059                                 MX6QDL_PAD_EIM_D22__GPIO3_IO22           0x80000000                         >;                 }; &usbotg {         vbus-supply = <&reg_usb_otg_vbus>;         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_usbotg>;         disable-over-current;         srp-disable;         hnp-disable;         adp-disable;         dr_mode = "otg";                 status = "okay"; };  With above config, one can use OTG port for mouse, usb stick in host mode, and gadget mode for ADB... https://community.nxp.com/message/943460  i.MX6_All
View full article
零部件选择——自动驾驶汽车成败的关键 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 车辆成为物联网中最复杂的节点,驾驶辅助功能最终将融入自动驾驶汽车。越来越多的消费电子组件被应用到汽车中,对前所未有的计算性能的需求正在重新定义汽车的“高端”。恩智浦数十年来一直是汽车领域的领导者,也是最高端计算网络解决方案的领导者。本次会议将重点介绍德国电子工业协会 (ZVEI) 行业工作组确定的汽车和消费电子零部件之间可能普遍存在的 66 个关键差异,例如影响车辆的可靠性、质量和寿命。我们将展示恩智浦在所有产品领域和性能范围内的功能如何解决您的许多隐藏风险,为您的自动驾驶汽车提供良好的起点。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 车辆成为物联网中最复杂的节点,驾驶辅助功能最终将融入自动驾驶汽车。越来越多的消费电子组件被应用到汽车中,对前所未有的计算性能的需求正在重新定义汽车的“高端”。恩智浦数十年来一直是汽车领域的领导者,也是最高端计算网络解决方案的领导者。本次会议将重点介绍德国电子工业协会 (ZVEI) 行业工作组确定的汽车和消费电子零部件之间可能普遍存在的 66 个关键差异,例如影响车辆的可靠性、质量和寿命。我们将展示恩智浦在所有产品领域和性能范围内的功能如何解决您的许多隐藏风险,为您的自动驾驶汽车提供良好的起点。
View full article
面向医疗和工业市场的传感器产品 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 传感器是使您的产品在市场上脱颖而出的关键,并增加了情境感知、篡改检测、强大的用户界面和准确的媒体兼容性。本课程将逐步介绍医疗和工业市场中一些使用运动和压力传感器的关键领先应用以及一些新兴应用。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 传感器是使您的产品在市场上脱颖而出的关键,并增加了情境感知、篡改检测、强大的用户界面和准确的媒体兼容性。本课程将逐步介绍医疗和工业市场中一些使用运动和压力传感器的关键领先应用以及一些新兴应用。
View full article
LS1088ARDB/LS1088ARDB-PB - SDカードのU-Bootバイナリを更新する方法 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このハウツートピックは、LSDK 18.09以前のリリースにのみ適用されます。LSDK 18.12 以降のリリースについては、「LS1088ARDB-PB - SD カードに TF-A バイナリをデプロイする方法」を参照してください。 SDカード上のU-Bootバイナリを更新するには、次の手順に従ってください。 前提条件 LSDK 18.06 または LSDK 18.09 の U‑Boot バイナリをビルドするには、Linux ホストマシンに Ubuntu 18.04 64‑bit をインストールしておく必要があります。   U‑Boot バイナリのコンパイル u-boot リポジトリをクローンします。 $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b LSDK-. たとえば、「 $ git checkout -b LSDK-18.09 LSDK-18.09 」のように入力します $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean 適切な defconfig ファイルを実行します。 LS1088ARDBの場合:$ make ls1088ardb_sdcard_qspi_defconfig LS1088ARDB-PBの場合:$ make the ls1088ardb_pb_sdcard_qspi_defconfig 必要に応じて、U-Bootファイルに変更を加えてください。 $ 作る make コマンドで "*** Your GCC is older than 6.0 and is not supported" というエラーが表示された場合は、LSDK 18.06 または LSDK 18.09 の U‑Boot バイナリをビルドする際に Ubuntu 18.04 64‑bit を使用していることを確認してください。 コンパイルされた U-Boot イメージ u-boot-with-spl.bin は  u-boot/ から入手できます。 U‑Boot バイナリの SD カード開始ブロック番号 イメージ SD カードの開始ブロック番号 U-Boot バイナリ 0x00800 = 2048 すべての LSDK ファームウェア イメージの SD カード開始ブロック番号の完全なリスト については、 PPA を使用したブート フローのフラッシュ レイアウト – LSDK 18.09 以前のリリース を参照してください 。    U‑Boot バイナリを SD カードに書き込む SD カードを Linux ホストに挿入します。 Linuxホストで次のコマンドを実行します。 $ sudo dd if=u-boot-with-spl.bin of=/dev/sdX bs=512 seek=2048 conv=fsync cat /proc/partitions コマンドを使用して、デバイスとそのサイズの一覧を表示します。 正しいデバイス名が選択されていることを確認してください。 Linux PC の SDHC ストレージドライブは /dev/sdX として検出されます。X は a、b、c などの文字です。必ず正しいデバイス名を選択してください。このデバイス上のデータは上書きされます。 Linux ホストマシンが追加の SDHC カードリーダーなしで SDHC カードの読み書きを直接サポートしている場合、そのデバイス名は通常 mmcblk0 になります。    LinuxホストマシンからSDカードを取り外してください。 LS1088ARDB/LS1088ARDB-PB で、スイッチが SD カードからボードを起動するように設定されていることを確認します。 SDカードから起動する場合、 SW1[1:8] + SW2[1] = 0010_0000_0  SDカードをボードに接続し、ボードをUbuntuで起動します。 U‑Boot が SD カード上で LSDK を検出できない場合、SD カードに保存された lsdk_linux_arm64_tiny.itb から TinyDistro を起動します。 QorIQ LS1デバイス 日時:LS1088ARDB / LS1088ARDB-PB - SDカード上のU-Bootバイナリを更新する方法 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 素晴らしいガイド、ありがとう!
View full article
Model-Based Design Toolbox for Panther (MPC574xP) プロセッサ 2.0 ファミリ <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> PANTHER (MPC574xP) プロセッサ ファミリ 2.0 のモデルベース デザイン ツールボックス   モデルベースデザインツールボックス Panther (MPC57xP) version 2.0に対応したMATLAB/Simulinkの提供を開始しました。   この製品は 無料で 、一般に公開されています。 ダウンロード モデルベースデザインツールボックス MBDTの    リリースハイライト – Panther(MPC574xP)向けモデルベースデザインツールボックス 新しいPanther XDEVKIT-MPC5744Pボード(ARDUINOスタイル)をサポートし、新しいシャーシXDEVKIT-MOTORGDと連携してモータ制御アプリケーションに対応します。 最新の Automotive Math and Motor Control Library リリース1.1.7の組み込み。 64ビットを含む 最新のMATLABバージョン のサポート (2015/2016 a/b) 新しい DMA ブロックにより、ADCのサンプル・データをDMAモジュールを介してCPUの介入なしにメモリに転送できます。 シリアル通信をサポートするための新しい LINFlexD ブロックにより、UARTを介したデータの送受信操作が可能になりました。 新しい メモリ読み取り/書き込み ブロックが追加され、任意のメモリ ゾーンの読み取り/書き込みに使用できるようになりました。 新しい Custom Initialization ブロックが追加され、モデルの最初の手順の前に、既定のセットアップ以外の任意のモジュールの構成を拡張するために使用できます。 S32 Design Studio for Power Compiler v1.1、新しいコンパイラバージョンであるWind River DIAB v5.9.4.8、Green Hills MULTI for PowerPC v2015.1に対応 新しい Advanced Motor Control ブロックが追加され、 Track Observer や Back EMF Observer などの新機能が Simulink ブロックとして提供されるようになりました。 20MHzから80MHzまでの ADCクロック周波数 (最大速度)にアライメント。 新しい ADCチャネル構成 ブロックは、ADCチャネルのサンプリングなしで構成できるように再設計され、転送のDMAシナリオが可能になりました。 新しい 診断 パネルを使用して、複数の整合性チェックを有効/無効にできます。 UART1 通信をサポートする新しい ブートローダー ビルド。 FreeMASTERリリース2.0.2と同期してサポート。 新機能!!! ホットフィックス: S32 Design Studio for Power v1.2  でリリースされた最新の e200 コンパイラのサポートを追加。 MBD Toolbox を最新の e200 コンパイラで動作させるには、 HotFix_3 セットアップを参照してください。   コミュニティサポートが利用可能 NXPコミュニティを通じて利用可能なサポート: https://community.nxp.com/community/mbdt Re: Model-Based Design Toolbox For Panther (MPC574xP) プロセッサ ファミリ 2.0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちはchandan24、 たぶんただの不具合だったんでしょうね。それでもうまくいかない場合は、次の直接リンクを使用してください https://nxp.flexnetoperations.com/control/frse/product?child_plneID=683951&cert_num=284425987  又は モデルベースデザインの公式ページを使用して、ダウンロード先にアクセスします: Model-Based Design Toolbox|NXPの  これがお役に立てば幸いです! ダニエル書 Re: Model-Based Design Toolbox For Panther (MPC574xP) プロセッサ ファミリ 2.0 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ツールボックスのダウンロードリンクが機能しない
View full article
示例 MPC5777C 渐进时钟切换 GHS716 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 本示例演示了从全 PLL 时钟进行的渐进时钟切换 * 256MNHz 降至 200MHz。 * * ------------------------------------------------------------------------------------------------------------- * 测试硬件:MPC57xx * 掩模组:3N45H * 目标:FLASH * 系统频率:256 MHz PLL * ******************************************************************************** 修订历史: 1.0 Aug-04-2016 b21190(Vlna Peter) 初始版本 1.1 2017 年 9 月 5 日 b21190(Vlna Peter)增加了 FCCU 故障清除 1.2 2018年5月7日 nxa13250(Vlna Peter)PLL 从 256->200MHz 切换 ********************************************************************************************/ <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 本示例演示了从全 PLL 时钟进行的渐进时钟切换 * 256MNHz 降至 200MHz。 * * ------------------------------------------------------------------------------------------------------------- * 测试硬件:MPC57xx * 掩模组:3N45H * 目标:FLASH * 系统频率:256 MHz PLL * ******************************************************************************** 修订历史: 1.0 Aug-04-2016 b21190(Vlna Peter) 初始版本 1.1 2017 年 9 月 5 日 b21190(Vlna Peter)增加了 FCCU 故障清除 1.2 2018年5月7日 nxa13250(Vlna Peter)PLL 从 256->200MHz 切换 ********************************************************************************************/
View full article
如何使 Android 的显示屏以纵向模式工作。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 有时需要当物理面板处于横向模式时使显示以纵向模式工作。 setprop persist.demo.rotationlock真的 setprop persist.demo.remoterotation肖像 上述代码可以在init.rc中设置,以便在android启动时生效。
View full article
TARS_里程碑_1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在本视频中,您将能够看到我们为完成里程碑 1 所包含的任务而设计的电子方案。您还将能够看到传感器测量的环境参数以及通过模拟各种情况而测量的参数。 (在 “我的视频” 中查看) 2017 年 Linux 嵌入式挑战赛
View full article
i.mx6UL从引导加载程序启动APP <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的,   我们想从引导加载程序启动应用程序,我们有以下问题: 我们使用I.MX6UL bootrom启动BootLoader,需要使用mkimage.sh,编译生成bin文件,然后转换成可执行文件。 如果需要使用Bootloader运行应用程序,应用程序镜像是否也需要通过mkimage.sh进行转换? mkimage.sh转换后的文件是压缩文件。不知道它的格式,起始地址怎么样,如何实现地址跳转,有例子吗?谢谢。  
View full article
INS-N2013 i.MX と新しいNXPプラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、i.MX アプリケーションプロセッサが新しいNXPポートフォリオとどのようにインターフェースするかについて説明します。i.MX プロセッサファミリと、それらをNXPコンポーネントに接続して完全な車載プラットフォームを作成する方法を確認します。 ビデオプレゼンテーションを見る <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、i.MX アプリケーションプロセッサが新しいNXPポートフォリオとどのようにインターフェースするかについて説明します。i.MX プロセッサファミリと、それらをNXPコンポーネントに接続して完全な車載プラットフォームを作成する方法を確認します。 ビデオプレゼンテーションを見る インサイト&イノベーション
View full article
Kinetis® MCU Security Technology As connected edge devices gain momentum with consumers, the security approaches and assumptions of the past will fail and create new threats and vulnerabilities to consumer safety and privacy. Additionally, the cost for security in mobile phones, tablets, and PCs will present a challenge for applications such as occupant sensors and heart rate monitoring patches. Lastly, the teams of security experts in connected industries do not yet exist at suppliers who are connecting products to the network. Join this session to learn how industries are providing cost effective, highly secure, certified hardware that can hasten the learning cycle for emerging edge node applications, bring solutions for security, drive down costs, and limit the supplier specific required expertise. As connected edge devices gain momentum with consumers, the security approaches and assumptions of the past will fail and create new threats and vulnerabilities to consumer safety and privacy. Additionally, the cost for security in mobile phones, tablets, and PCs will present a challenge for applications such as occupant sensors and heart rate monitoring patches. Lastly, the teams of security experts in connected industries do not yet exist at suppliers who are connecting products to the network. Join this session to learn how industries are providing cost effective, highly secure, certified hardware that can hasten the learning cycle for emerging edge node applications, bring solutions for security, drive down costs, and limit the supplier specific required expertise.
View full article
HMB-N1826 为物联网应用设计高性能电源转换器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将深入介绍降压调节器的性能及其可靠性方面。降压调节器是应用最广泛的拓扑结构。一旦计算出系统功率需求,确定正确的电源管理芯片对于项目的成功至关重要。会议参与者应该能够识别和审查关键的 DC-DC 转换器规格,并根据他们的需要选择最佳的电源解决方案。讨论了计算/选择降压调节器周围的无源元件和分立元件以创建稳健的设计。最后,分享了确保热稳定性和环路稳定性的关键参数的测量。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将深入介绍降压调节器的性能及其可靠性方面。降压调节器是应用最广泛的拓扑结构。一旦计算出系统功率需求,确定正确的电源管理芯片对于项目的成功至关重要。会议参与者应该能够识别和审查关键的 DC-DC 转换器规格,并根据他们的需要选择最佳的电源解决方案。讨论了计算/选择降压调节器周围的无源元件和分立元件以创建稳健的设计。最后,分享了确保热稳定性和环路稳定性的关键参数的测量。 智能家居和智能建筑
View full article