Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
MIMXRT1180 how to output a pwm signal on the pin M16 - GPIO_AD_27 Hi guys,  I have a MIMXRT1189CVM8C. I am not able to output a simple PWM signal from the pin M16 - GPIO_AD_27. I have attached the screenshots of the MCUXpresso Config Tool which I set. Can someone help me, please? Re: MIMXRT1180 how to output a pwm signal on the pin M16 - GPIO_AD_27 Hi @silvio-vallorani , Thank you so much for your interest in our products and for using our community. I suggest you can refer to SDK demo "evkmimxrt1180_pwm_cm33". 1: Pin Configuration : In MCUXpresso Config Tools, set pin M16 (GPIO_AD_27) to function as PWM2_B (submodule 1). 2: Add PWM Initialization Code Follow the SDK demo for PWM setup. The demo project uses PWM1 submodule 0, submodule 1, and submodule 2 to generate waveforms. You can adapt the same method for PWM2 Submodule 1.   Best Regards MayLiu Re: MIMXRT1180 how to output a pwm signal on the pin M16 - GPIO_AD_27 My new related question is about a function I need to implement, but I can't figure out how to do it cleanly and possibly totally in hardware. I have a periodic square signal generated by my application. I need to generate a new periodic square signal that is 8 time more fast and that perfectly sync with the signal above, every it's rise edge. In the Reference Manual I saw this block diagram: However, going into more detail about the behavior of PWM_EXT_SYNC I found this block diagram: It seems that the PWM peripheral is unable to simultaneously generate the PWM signal and synchronize with the external signal, is this true? Can you help me to find a good solution for my needs? Thank you very much, Silvio Re: MIMXRT1180 how to output a pwm signal on the pin M16 - GPIO_AD_27 Thank you @mayliu1 for your reply. I found the problem, it was related to the "fault disable" signals. I tryed to disable the beahviour that involve faults, using the "MCUX Config Tool" is not possible: if I uncheck all the "fault disable" signals, the generated code totally remove the PWM_SetupFaultDisableMap() call and the "fault disable map" register stay to it's all enabled by default. I think this is a buggy beahviour of the tool, beacouse if I uncheck all the "fault disable" signals from the tool and then I manually add the PWM_SetupFaultDisableMap() call with "0" as the mask, I obtain the expected behaviour. Anyway, on my code I finally leave enabled all the "fault disable" signals and I added XBAR signals to route "InputLogicHigh" on "Flexpwm2Faultx" signals and that's works fine. Now I have a new question, but I ask it as a separate message below. Re: MIMXRT1180 how to output a pwm signal on the pin M16 - GPIO_AD_27 Hi @silvio-vallorani , Thanks for your updated information. Q: It seems that the PWM peripheral is unable to simultaneously generate the PWM signal and synchronize with the external signal, is this true?   A: The FlexPWM module on i.MX RT1180 can simultaneously generate PWM outputs and synchronize its counter to an external signal. For more detailed information, I suggest you can refer to this Application Note : AN14196: Flex Pulse Width Modulator (FlexPWM) Usage on MCX N Series | NXP Semiconductors, especially Section 3.2.2 “Counter Synchronization”, which describes how the FlexPWM counter can be synchronized across modules or via external sources. Best Regards MayLiu
記事全体を表示
S32N55: GM として動作している場合の gPTP ブリッジ デバイスのシーケンス ID こんにちは、チームの皆さん gPTP の例でブリッジ デバイスの動作をテストしていました。私はGrayVIP_1_0_22_0を使用しています。 ユーザー マニュアルによると、ブリッジがStartupTimeoutS後に Sync メッセージを受信しない場合は、GM として動作を開始する必要があります。ただし、この状況では、同期フレームと同期フォローアップ フレームの両方のシーケンス ID が 1024 のまま増加しないことがわかりました。 関連コードを確認したところ、ブリッジが GM モードに移行すると、同期メッセージの生成に使用されるシーケンス ID が、スレーブ ポートのprSyncMachines [ prDomain -> u8SlaveMachineId ]. u16SequenceIdから取得されることがわかりました。 スレーブ ポートが Sync メッセージを受信していない場合、この値は更新されず、マスター ポートから送信された Sync メッセージ内のシーケンス ID は変更されません。 この動作は、このメカニズムではブリッジが GM として適切に機能できないことを示しています。 なぜこの橋がこのように動作するように設計されているのか、説明していただけますか? BR、 ブリジット GPTP_STACK Re: S32N55: sequence ID in gPTP bridge device when acting as a GM こんにちは@Bridget 、 チームはケースを取り上げ、できるだけ早く回答を提供します。 よろしくお願いします、 ラドゥ Re: S32N55: sequence ID in gPTP bridge device when acting as a GM こんにちは@Bridget 、 私たちは問題を再現するために取り組んでおり、チーム内で今後の手順について話し合う予定です。折り返しご連絡いたします。 ありがとう、 ルーカス Re: S32N55: sequence ID in gPTP bridge device when acting as a GM @ブリジット、 実際のところ、gPTP ブリッジのこの動作は意図されたものであり、802.1as 標準に準拠しています。 ブリッジは、マスター ポートで受信したシーケンス ID を中継することになります。グランド マスターが失われた場合、シーケンス ID は実際に更新されなくなります。これは、ダウンストリーム デバイスが GM が失われたことを検出できる方法の 1 つです。 そもそも GM が存在しないブリッジの場合、シーケンス ID は標準ごとにランダムになります。ランダム性の解釈は、シーケンス ID については何も保証されない、または想定されるべきではないということです。ハードコードされた 1024 はこれに準拠していると見なされます (他の数値でもかまいません)。 シーケンス ID がアプリケーションで問題を引き起こしていますか?ご存知のとおり、エンドポイントはシーケンス ID に関係なく、ブリッジと完全に同期できます。 長くかかってしまい申し訳ありません。不明な点がございましたらお知らせください。 BR、ルーカス
記事全体を表示
「xio」ドライバのソースコードをお探しですか?NXPのボードに属している こんにちは。私はNXP PNX8543/TV543をエミュレートしようと試みてきました 私はこれを実現するためにオープンソース プロジェクト QEMU と、PNX8550 の基本的な割り込みソリューションを含む Linux カーネル ソースを使用しました ( https://git.riwo.eu/Opensource/linux-toradex-kernel/-/tree/9c9ab76c48ffc48648c8e5da40d57965fc65c030/arch/mips/pnx8550/common )これはこのボードで使用されているチップ(NXP PNX8543)と十分に類似しています。 しかし今、私は行き詰まっています。 xio と呼ばれるドライバに関連するコード (<6>xio ドライバがロードされました) により、カスタム QEMU ソリューションでカーネル パニックが発生します。通常、xio は何らかのベンダー システムに属していると言えますが、xio は Google でソース コードを簡単に見つけることができない NXP ドライバに関連していると考える理由があります。 もし私が適切な場所にいない場合は、遠慮なく私に教えてください。 私は xio のソース コードを見つけようとしていますが、Linux カーネル ソースには存在せず、NXP 製品に属していると思うのですが、見つけるのが困難であり、どこを探せばよいかわかりません。 (一般情報) Vmlinux でエミュレートしようとしているソース: NAND ダンプからの Sony KDL-32BX300 2010 年代の TV。 (何か確認したい方がいらっしゃれば、vmlinux と抽出した rootfs を送信できます。) Re: Looking for "xio" driver source code? Belongs to a NXP board もし私が間違っていて、xio が NXP によって配布されるものに属していない場合は、お詫び申し上げます。 しかし、xioがnxps組み込みソフトウェアに属するものであると私が考えるのは、vmlinuxの文字列「pnx85xx-xio」です。
記事全体を表示
S32K344 : PMIC[MFS2613] 控制源代码或示例代码 S32K344 白板已配备 PMIC[MFS2613]。 我想获得SPI控制源代码[示例代码]。 Re: S32K344 : PMIC[MFS2613] control source or example code HI 请注意,在圣诞假期期间,我们的支持响应时间可能会比平时长。在某些情况下,您的请求可能会在新年后得到处理。感谢您的理解。 请点击下载 FS26 RTD S32K3 标准软件-> 汽车软件-SBC/PMIC-实时驱动程序-> SBC FS26 R21-11 5.0.0 虽然这些示例并非基于 S32K344-WB(注意 SPI 引脚的不同),但随附的 S32K3 RTD 是相对较新的 RTD 6.0.0。 或下载S32K344_Whiteboard_Example(LLD)_RTM_1.0.0.zip 文件。不幸的是,S32K3 RTD 的版本已经很老了:S32K3_RTD_2_0_0_D2203 C:\NXP\S32K344_Whiteboard_Example(LLD)_RTM_1.0.0\S32K344_Whiteboard_Example(LLD)_RTM_1.0.0\s32k3_wb_fs26 C:\NXP\S32K344_Whiteboard_Example(LLD)_RTM_1.0.0\S32K344_Whiteboard_Example(LLD)_RTM_1.0.0\s32k3_wb_self_test 祝好, Robin ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"ACCEPT AS SOLUTION" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请另开新主题,并参考已关闭的主题。 ------------------------------------------------------------------------------- Re: S32K344 : PMIC[MFS2613] control source or example code 不幸的是,s32k3_wb_fs26使用 MCAL 的Sbc_fs26在 S32DS 外围设备工具. s32k3_wb_self_test不使用 MCAL 的Sbc_fs26。 S32DS 外围设备工具但该项目包含 /s32k3_wb_self_test/ExternalDevices/FS26_Drv。 或者,您也可以参阅Sbc_fs26_example_IP_S32K344,了解如何使用Sbc_fs26_Ip在 S32DS 外围设备工具. Re: S32K344 : PMIC[MFS2613] control source or example code 亲爱的@Robin_Shen 我将查看 Sbc_fs26_example_IP_S32K344 ,了解如何使用 Sbc_fs26_Ip 顺便问一下,我在哪里可以获得[s32k3_wb_self_test] 的代码?   Re: S32K344 : PMIC[MFS2613] control source or example code 亲爱的@Robin_Shen 感谢您的支持。 恐怕您提到的示例文件是空的。 请再次检查。 ============================================================== 或下载 S32K344_Whiteboard_Example(LLD)_RTM_1.0.0.zip.遗憾的是,S32K3 RTD 版本已相当老旧:S32K3_RTD_2_0_0_D2203 Re: S32K344 : PMIC[MFS2613] control source or example code 亲爱的@Robin_Shen 所有代码都基于 Tresos AUTOSAR。 是否有任何非 Autosar 基础板示例或 PMIC SPI 驱动程序? Re: S32K344 : PMIC[MFS2613] control source or example code 请解压此 .zip 文件文件,然后安装 .exe锉刀 Re: S32K344 : PMIC[MFS2613] control source or example code 在此附上我的代码。请看一看。 Re: S32K344 : PMIC[MFS2613] control source or example code 亲爱的@Robin_Shen 感谢您的回复。 我曾尝试版本 WB_Self_Test 但遇到了一些错误,我不知道如何修复它。 请帮帮我。
記事全体を表示
HAB Error on IMX8MP processor Dear all, Trying to validate HAB signatures on the i.MX8MP board I am getting these errors HAB Configuration: 0xf0, HAB State: 0x66 --------- HAB Event 1 ----------------- event data: 0xdb 0x00 0x14 0x45 0x33 0x0f 0xc0 0x00 0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00 0x00 0x00 0x00 0x50 STS = HAB_FAILURE (0x33) RSN = HAB_INV_INDEX (0x0F) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB Event 2 ----------------- event data: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x42 0x5a 0x00 0x00 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB Event 3 ----------------- event data: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x00 0x40 0x40 0x00 0x00 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) They come from this development environment U-Boot SPL 2023.04-lf_v2023.04+g1e5b6c6bf2 Can someone give me an advice on this topic ? Thanks in advance Re: HAB Error on IMX8MP processor any chance you got this fixed , i have the same issue , when i try to change from srk1 to srk2  Re: HAB Error on IMX8MP processor Hi, RSN = HAB_INV_INDEX (0x0F) tells wrong key at given index or target index for installed key not available. To have a check the csf files. To refer to the HAB API where you'll find more details for these errors. The API is with CST tool that you download for signing. Regards Harvey
記事全体を表示
S32K344-使用内置 CRC 引擎计算 FS26 CRC-8 正如标题所暗示的那样,我想知道是否有可能在我的 S32K344 上使用内置的 CRC 引擎来生成 SPI 与 FS26 进行通信所需的 CRC-8 校验和。 根据恩智浦公开的 AN14492,这里定义了种子和多项式: 我已经写了自己的 CRC 驱动程序但我注意到参考手册 S32K3XXRM " 5 8.3.2 CRC 计算" 没有定义计算 8 位 CRC 的方法。 是否可以使用 CRC 引擎生成 8 位校验和? Re: S32K344 - Using built-in CRC engine to compute FS26 CRC-8 HI 感谢您的耐心等待。 S32K3 中的 CRC 支持 16 位或 32 位模式。这意味着 CRC-8 无法通过硬件实现。 我建议您下载 FS26 的 RTD,因为其 API 已包含 CRC-8 软件实现。单击 S32K3 标准软件-> 汽车软件-SBC/PMIC-实时驱动程序 请注意,在圣诞假期期间,我们的支持响应时间可能会比平时长。在某些情况下,您的请求可能会在新年后得到处理。感谢您的理解。 祝好, Robin ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"ACCEPT AS SOLUTION" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请另开新主题,并参考已关闭的主题。 -------------------------------------------------------------------------------
記事全体を表示
SC18IS606 桥接器在尝试读回缓冲区时返回值总是 00 大家好, 我正试图使用恩智浦 SC18IS606-EVB 驱动 I2C 至 SPI 桥接器 SC18IS606。 目前使用示波器检查各点是否正常: * 通过 I2C 总线对恩智浦桥进行读写访问 * 可通过 SPI 写入板载 ATMEL EEPROM(寄存器和内存) * SPI 时钟速率为 1.875 kHz,我可以看到 SPICLK 在 I2C 总线上接收 STOP 序列(SDA + SCL)时运行良好 * SPI 写入工作正常(在 MOSI 上观察到写入数据) * SPI 读取(MISO 上的预期数据) BUT...... 读取桥接缓冲区(ST + 51 + data1 +... + daTan + SP)时,所有接收到的字节均为 00(注意:十六进制芯片地址为 50)。 例如,以下序列 : a) ST 50 02 06 SP ==> 设置板载 EEPROM 的写使能锁存器 (WEL) b) ST 50 02 05 FF SP == > 02 是 EEPROM 地址(SS1 为 CS),05 是读取状态寄存器(FF 是一个额外字节)—— 有了示波器,人们可以在 MOSI 上看到 05,然后在 MISO 上看见 02,这意味着这两个交换没问题。 c) ST 51 00 00 00 00 SP ==> 读取 SC18IS606 桥接缓冲器的返回值始终为 00 如果我没猜错,预期内容应该是 05 FF 02。 出了什么问题? 感谢您的帮助。 顺祝商祺! 欧盟委员会 Re: SC18IS606 bridge returns always 00 when trying to read back its buffer 你好,拉法、 日安,新年快乐! 以下是你要求的捕获和我附带的解释: 目前的总体目标是从I2C总线读取嵌入在恩智浦评估板(SC18IS606-EVB)上的SPI ATMEL EEPROM的状态寄存器。 在 I2C 总线上,这按以下顺序排列: ST -> 启动条件 50-> 设备写入权限(50h = 恩智浦网桥的目标地址) 02 -> 启用 SS1 的网桥功能 ID(选择 EEPROM)。 05 -> 发送至 EEPROM 的指令代码(05 = RDSR,读取 STATUS 寄存器) FF-> 允许在 MISO 上通过 SPI 传输一个字节的填充字节 SP -> STOP 条件 scope_1 至 scope_4 是该序列的照片。 由于我只有四向示波器,我无法同时捕获 5 个信号(SCL、SDA、SPICLK、MOSI 和 MISO)。这就解释了为什么绿色信号有时是 SDA,有时是 SPICLK。 最后,scope_5 的照片显示了问题所在:对网桥缓冲区(I2C 目标地址为 51h,读/W 位 = 1)的读取权限仅返回空字节。 感谢您的关注。 欧盟委员会 Re: SC18IS606 bridge returns always 00 when trying to read back its buffer 预期(缺失的)捕获...
記事全体を表示
LS1021A-IoT: SDKとオリジナル8GB SDカードイメージのリクエスト こんにちは、みんな、 LS1021A-IoT ボードに関するサポートを求めています。 しばらく前にこのデバイスを購入しましたが、残念ながら元の SD カード イメージを紛失してしまいました。ボードを工場出荷時の状態に戻そうとしましたが、次の公式ダウンロードリンクが見つかりません。 LS1021A-IoTに同梱されていたオリジナルの8GB SDHCカードの画像 このプラットフォームで使用される対応するSDK / BSP NXP の Web サイト、ドキュメント、コミュニティ リソースを検索しましたが、リンクは利用できなくなっているか、削除されているようです。 NXP またはコミュニティの誰かがアドバイスをお願いします: LS1021A-IoTの公式SDKsはどこで入手できますか? オリジナルの SD カード イメージがまだダウンロード可能かどうか (または非公開で共有CANかどうか) ボードを元の動作状態に戻したいので、ご指導やご指摘をいただければ幸いです。 よろしくお願いいたします。 よろしくお願いいたします。 マテウス・アウベス QorIQ LS1デバイス Re: LS1021A-IoT: Request for SDK and Original 8GB SD Card Image LFGP様 迅速なご対応誠にありがとうございます。迅速な対応とご助力に本当に感謝しています。 私はすでにそのページからIndustrial IoT Gateway LEDE Release v1.0イメージをダウンロードし、dd を使用してキットに付属する元の SD カードにフラッシュしました。 sudo dd if=firmware_sdcard.bin of=/dev/sdc bs=1M conv=fsync [sudo] password for mateus: 124+1 records in 124+1 records out 130023428 bytes (130 MB, 124 MiB) copied, 6.18025 s, 21.0 MB/s フラッシュ後、SD カードに次のパーティションが作成されました。 $ sudo fdisk -l /dev/sdc Disk /dev/sdc: 7,4 GiB, 7948206080 bytes, 15523840 sectors Disk model: STORAGE DEVICE Units: sectors of 1 * 512 = 512 bytes Sector size (logical/physical): 512 bytes / 512 bytes I/O size (minimum/optimal): 512 bytes / 512 bytes Disklabel type: dos Disk identifier: 0x5452574f Device Boot Start End Sectors Size Id Type /dev/sdc1 * 4096 45055 40960 20M c W95 FAT32 (LBA) /dev/sdc2 49152 253951 204800 100M 83 Linux 最初のパーティション (FAT) 内では、ファイルは次のように配置され、U-Boot バイナリはバックアップ ディレクトリ内にあります。 $ ls -l /media/mateus/4741-B09E total 4558 drwxr-xr-x 2 mateus mateus 2048 Dec 26 2017 backup -rw-r--r-- 1 mateus mateus 15706 Dec 26 2017 ls1021a-iot.dtb -rw-r--r-- 1 mateus mateus 4648056 Dec 26 2017 uImage $ ls -l /media/mateus/4741-B09E/backup total 2108 -rw-r--r-- 1 mateus mateus 2155903 Dec 26 2017 root.ext4.gz.uboot -rw-r--r-- 1 mateus mateus 200 Dec 26 2017 version.json $ tree /media/mateus/4741-B09E /media/mateus/4741-B09E ├── backup │   ├── root.ext4.gz.uboot │   └── version.json ├── ls1021a-iot.dtb └── uImage 2 directories, 4 files しかし、この SD カードをボードに挿入して電源を入れると、シリアル コンソール (K22 によって公開される COM ポート) には何も表示されません。U-Boot 出力やブート ログは表示されません。 アドバイスをお願いします: このSDイメージは追加のフラッシュ手順なしで直接起動するか、 必要な設定(ディップ・スイッチ、ブートソースの選択、ボーレートなど)がある場合、または U-Boot は SD から直接ブートされるのではなく、他の場所 (QSPI/NAND) にフラッシュされることが予想されますか? 私のボードはLS1021A-IOT Rev B3です   改めましてサポートありがとうございます。 よろしくお願いします、 マテウス Re: LS1021A-IoT: Request for SDK and Original 8GB SD Card Image 親愛なる@mateuslimati様、 次のリンクを使用して、下にスクロールし、「 Industrial IoT Gateway LEDE Release v1.0」リンクを探してください。 https://www.nxp.com/design/design-center/development-boards-and-designs/LS1021A-IoT よろしくお願いします 」 Re: LS1021A-IoT: Request for SDK and Original 8GB SD Card Image LFGP様 ただ最新情報を提供したかっただけです。 ボードに適した機能的な SD カード イメージを見つけることができ、正常に起動できました。ブート ログから、私のボードはシリコン リビジョン v1.0を使用しているようです。これは、以前直面していた問題の原因である可能性があり、公開されているイメージのほとんどがCPU シリコン v2.0 をターゲットにしているように見えることから、今後の開発が制限される可能性があります。 以下は参考のための関連するブート出力です。 U-Boot 2014.01Layerscape-SDK-V1.3+g50d6848 (Dec 01 2014 - 13:42:50) CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110) Clock Configuration: CPU0(ARMV7):1000 MHz, Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate), Reset Configuration Word (RCW): 00000000: 0608000a 00000000 00000000 00000000 00000010: 20000000 08407900 60025a00 21046000 00000020: 00000000 00000000 00000000 00038000 00000030: 20024800 881b1340 00000000 00000000 Board: LS1021AIOT CPLD: Unknown (23000000) I2C: ready DRAM: 1 GiB (DDR3, 32-bit, CL=10.5, ECC off) MMC: FSL_SDHC: 0 In: serial Out: serial Err: serial SATA link 0 timeout. AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode Net: Phy not found PHY reset timed out eTSEC1, eTSEC2 [PRIME], eTSEC3 Hit any key to stop autoboot: 0 => このイメージは私のハードウェア上で正常に動作しています。TechNexion FTP サーバーの次の場所にアーカイブされているのを見つけました。 ftp://ftp.technexion.net/pub/demo_software/.IOT/ls1021a-iot-gw/archived 現時点では、シリコン v1.0 と v2.0 の違いが、新しいイメージが私のボードで起動しなかった主な理由であると理解しています。 作業を続けるために、 Layerscape-SDK-V1.3 (または LS1021A シリコン v1.0 を公式にサポートする同等の SDK バージョン) を入手できるかどうかを尋ねたいと思います。この SDK にアクセスできれば、ハードウェアに合わせてイメージを適切に再構築し、カスタマイズできるようになります。 改めましてごサポートとご指導に感謝申し上げます。 よろしくお願いします、 マテウス Re: LS1021A-IoT: Request for SDK and Original 8GB SD Card Image 親愛なる@mateuslimati あなたの発見を共有していただき、本当にありがとうございます。 残念ながら、LS1021A Rev1.0をサポートする新しいSDKsはありません。ご不便をおかけして申し訳ございません。 BR LFGP
記事全体を表示
S32K310 SRAM overflowed S32K3 AUTOMOTIVE-RTD  This week, when I was building the peripherals for an S32K310 project in my IDE, it reported an SRAM overflow error.   But, my project is brand new, and the main function is empty. There is no application code at all; I have only configured the necessary peripherals for my MCU. I checked the demo_310.map file to determine what was causing the excessive memory usage. I found that one of the files within the RTD package is taking up a significant amount of SRAM space. The SRAM address range for K310 is from 0×20400000 to 0×20404000, but the address allocation has now reached 0x20404200. The RTD/src/SchM_Gpt file alone occupies more than 2KB of space. Knowing that the external SRAM space for the S32K310 MCU is only 16KB, I believe there must be some issues within the RTD package. I opened the corresponding file and found the issue shown in the figure below. As shown in the figure, in the file, the length of the variable definition is set to 4 . I understand that this was prepared for multi-core systems. However, in my current project using S32K310, which has only one core, the RTD package still sets the number of cores to 4. This results in the space occupied by variables being expanded by a factor of four. After adjusting the core number configuration and rebuild the project, I can see that the space occupied by RTD/src/SchM_Gpt has decreased from 0x860 to 0x218, which is quite significant. So, please explain why a single-core device like the S32K310 still sets the number of cores to 4. Is this a bug? The version I am using is as follows: S32S32 Design Studio for  S32 Platform 3.6.2 S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610 I have also uploaded my project files in the attachment for your confirmation. I look forward to your reply very much because this is important to me. Thank you. Re: S32K310 SRAM overflowed Hi@khty I have reported this issue to the RTD design team, and it will take some time to get a response. Re: S32K310 SRAM overflowed Hi@khty I received a reply from the design team, and they confirmed that this is a bug. For now, you can manually change the number of cores to 1. I will notify you again when there is an official workaround or version fix.
記事全体を表示
RTC PCF2131 EPAD 连接 你好 您能否就PCF2131实时时钟集成电路(CIN# 202411003I)裸露焊盘连接要求的变更提供一些信息? 更新了第 3.2 节:从 “中心焊盘 必须连接到地面 (VSS)” 更改为 “中心焊盘必须保持 浮空”。 因为我们有两块板(6 层/10 层)正在生产中,它们是根据之前的应用笔记设计的,该笔记规定它必须连接到 VSS。 我们需要知道这对我们的设备的影响,例如我们必须把已经生产的板扔掉吗? 谢谢 奥托 Re: RTC PCF2131 EPAD Connection 我打算这样做,但您是否知道为什么要更改? 我们需要知道我们需要如何处理已经使用连接到 GND 平面的 EPAD 制造的板。 Re: RTC PCF2131 EPAD Connection 你好 还是建议你重新设计两块板,以适应有关EP连接的新变化。 Re: RTC PCF2131 EPAD Connection 我稍后会给您发送有关此主题的私人邮件。
記事全体を表示
Maximum Junction temperature and (RθJA) Hi Team, Regarding  Maximum Junction temperature and (RθJA)  Part Number : PCA9685BS,118 For this part number I need Maximum Junction temperature & RθJA (Thermal resistance for junction to ambient). Please provide these information. Regards, Suriya devan C
記事全体を表示
LPC1768 XPresso 板 SSP0 从属模式 我有一个 LPC1768 XPresso 板,将 SSP0 端口配置为从机端口。主设备是ADI公司的 AD73322 编解码器。 将 SSP 端口配置为 TI 模式并启用端口后,我将两个值载入数据寄存器。 我在逻辑分析仪上看到,如 UM10360(LPC176X 用户手册)图 77 第 425 页所示,主控器正在发送 SCLK 和 FS,但 LPC1768 并没有在 MISO0 引脚上传输数据寄存器的内容。 我尝试了很多配置更改,但至今仍无法正常工作。 但是,我确实让这个编解码器在 SSP 总线上用作主编解码器,以 LPC2138 作为从属设备。 您有什么想法吗? Re: LPC1768 XPresso board SSP0 slave mode 你好@kk7xo 您能分享一下您的代码吗? BR 哈利 Re: LPC1768 XPresso board SSP0 slave mode 就像经常发生的那样,当我创建了一个最小的程序来演示我遇到的问题时,我设法解决了它。 我把配置数据写错了寄存器。 现在一切正常了。 感谢您的回复。
記事全体を表示
当音频停止时,HDMI 音频会导致内核崩溃 HI 在 i.MX 8QM 系统上,通过 HDMI 播放音频后,内核会崩溃。 内核版本基于 lf-6.12.20-2.0.0。看起来这个问题在 lf-6.12.49-2.2.0 中仍然存在。 看起来提交 c91c717f7113 ("LF-13883:drm:bridge:mhdp:Add info frame remove function") 引入了一个回归,因为它没有使用寄存器访问辅助程序 cdns_mhdp_bus_write(),因此 i.MX 8QM 不能以应有的方式写入寄存器。 所附的补丁解决了我的问题。 此致 最大值 Re: Audio over HDMI Creates a Kernel Panic When Audio Stops 你好@maxkrummenacher 已报告,等待内部答复。 致敬, Zhiming Re: Audio over HDMI Creates a Kernel Panic When Audio Stops 嗨 @maxkrummenacher 预计 第二季度的 电路板支持包 将解决这个问题。 致敬, Zhiming
記事全体を表示
RW612 IEEE802.11mc/azサポート RW612 の IEEE 802.11mc サポートに関して質問があります。 最近、 FRDM-RW612ボード2枚を使った距離測定のデモンストレーションを見ました。NXP FAE では、最初は FRDM-RW612 の購入を推奨しています。それに基づいて、私は自分で FRDM-RW612 ボードを購入し、 SDK_25.9.0をインストールし、 wpa_supplicant サンプル アプリケーション (wifi_cli も)を実行しました。 しかし、wlan-ftm-ctrlなどのコマンドを使用しようとすると、すべてのftmコマンドがHostCmd_RESULT_NOT_SUPPORT(=2)を返します。 サンプル アプリケーションでは、wifi_config.h は次のように構成されています。 #CONFIG_11MC 1を定義します #CONFIG_11AZ 1を定義します #CONFIG_CSI 1を定義する #CONFIG_WLS_CSI_PROC 1を定義します ファームウェア情報は、WLANファームウェアバージョン:rw610w-V2、IMU、FP99、18.99.6.p46、PVE_修正 1 以下の点を知りたいです: RW612でIEEE 802.11mc(FTM)が正式にサポートされているかどうか もしそうなら、それを有効にするにはどのような追加の設定やソフトウェアが必要ですか? どのようなご指導でもいただければ幸いです。 Re: RW612 IEEE802.11mc/az support こんにちは@wireless123 RW61X では 802.11mc/az はサポートされていません。 どのドキュメントを参照したかを共有していただけますか。CSI 機能を参照した可能性があります。 よろしくお願いいたします。 ショーン Re: RW612 IEEE802.11mc/az support 88W8987 は 802.11mc/az をサポートしていますか?802.11mc/az をサポートしているデバイスを教えてください。 よろしくお願いいたします。
記事全体を表示
S32 闪存工具-QSPI/或非 闪存 你好、 我在刷新 S32G-VNP-RDB2 板时遇到了问题,我正在尝试通过 QSPI/或非 Flash 启动它 开关设置按默认设置进行,并更改 SW4 - 第 7 次关闭 我正在使用 S32 Flash 工具为 M7 Core 刷板 我的初始化设置为 选择目标和算法 - S32G2xxx 目标 - FLASH 算法 - MX25UW51245G 我已经用 1 启动了这个 过程 。)选择 COM 端口-测试连接- 板已连接 (成功) 2.) 擦除内存范围 -- 0x0 至 0x10000 3.) 将目标和算法上传到硬件 -- 加载算法文件 4.)将文件上传到设备-我已经添加了从 S32DS 的 IVT 工具生成的二进制文件(我不确定这是否适合上传) 5.) 获取闪存 ID 如果这些步骤有误,请纠正我,因为预期的 CAN 线路消息没有到来,但是当我在 Debug_RAM 中运行时能够看到 CAN 消息, 所以闪存问题和相关的二进制文件无法按预期运行,所以我们该如何检查和验证 Re: S32 Flash tool - QSPI/NOR Flash 你好,@阿特金森 感谢您的回复。 可能是 IVT 设置和/或应用程序初始化部分出了问题。 默认 CAN 示例基于环回模式,您可能需要额外修改代码,使其能够发送 CAN 帧进行测试。 我建议直接共享检查问题的步骤/项目设置,如果不方便共享,我们可以创建一个支持案例以方便您。 BR 切宁 Re: S32 Flash tool - QSPI/NOR Flash 您好@chenyin_h 感谢您的回复!! 1.)我目前使用自定义应用程序来发送 CAN 帧,该程序每 5 秒钟发送一次 CAN 消息,因此我使用 S32G 调试器进行了验证,结果与预期的一样工作正常。虽然我已经使用IVT工具生成了二进制文件,但我通过S32 Flash工具刷新了该二进制文件,但无法按预期运行,无法看到任何日志,也不知道如何进行验证。 2.)我不认为是代码的问题,因为通过调试器可以正常工作。 你能不能记下启动 S32G-VNP-RDB2 板 闪存设置的程序我不确定要为 S32G 板 构建二进制文件然后通过 S32G 刷新 3。) 既然我使用了自定义应用程序,我对任何通过 CAN_LLCE2 发送消息的示例应用程序都没问题,所以到目前为止,如果有任何示例应用程序运行这个我没问题,或者如果有任何能理解 M7 内核的应用程序被刷新和某些应用程序正在运行以对其进行验证。 能否向我推荐一个应用程序,作为验证目的的运行示例? Re: S32 Flash tool - QSPI/NOR Flash 你好,@阿特金森 感谢您的来信。 1.所以你的意思是,通过调试器运行的原始 elf 可以用来发送 CAN 帧,而生成的二进制文件(可能闪存到 QSPI?)开启板时无法按预期正常运行代码? 2。如果是这样,在闪存开机时,我建议先将调试器连接到板上,以检查代码卡在哪里。 3.这个测试是由演示程序还是您的自定义应用程序完成的? BR 切宁
記事全体を表示
DMAの例Lpspi_Ip_Transfer_S32K344を実行しようとしています DMA サンプル Lpspi_Ip_Transfer_S32K344 を実行しようとすると、以下のエラーが発生します。S32 Design Studio バージョン 3.5 と S32K3 リアルタイム・ドライバ AUTOSAR 4.4 バージョン 2.0.0 があります。 コンパイルしようとすると、#include "StandardTypes.h" などのインクルード ファイルが見つからないというエラー メッセージが表示されます。 spi 経由で DMA をサポートするにはどのバージョンを使用する必要があるか教えてください。 Re: Trying to run DMA example Lpspi_Ip_Transfer_S32K344 こんにちは@jnaus DMA を使用した RTD 2.0.0 では問題はありません。 「Dma」を追加した後、「コードを更新」をクリックするだけです。
記事全体を表示
S32K312 HSE 升级失败 恩智浦专家,你好、 1.我使用的是 s32k312,HSE 版本为 1.13.0、2.40.0,我想升级到 1.13.0。 2.55.0. 2.我试着用一些方法来做,现在看来是砖块。 芯片在 cust_del,只写入 hse fw,没有写入其他 OTP 参数。 这是我的步骤: 1.我构建项目,使用 " HSE_SRV_ID_FIRMWARE_UPDATE " 更新 fw 2.55,将代码放入 0x500000,fw 放入 0x400000,服务恢复正常,但服务器重启后,它仍然返回 2.40 版本。 2.我通过 HSE 服务"HSE_SRV_ID_ERASE_FW" 删除了 fw ,然后使用"HSE_Install_FW_312" 项目安装"1.13.0 2.55.0。" ,它不起作用,每次重启后都停留在 "while ((HSE_STATUS_INIT_OK& HSE_MU_GetHseStatus(0)) == 0)" 我的问题是: 1. 在这种情况下,如何安装 hse 1.13.0 2.55.0,可以吗? 2.对于 HSE 1.13.0 2.55.0,是否需要升级 sbaf 固件,如果需要,如何获取固件。 谢谢。 Re: s32k312 hse upgrade failed 嗨,胜利、 对不起,我们在线技术支持团队的 HSE 专家正在放圣诞假,所以我现在无法给您准确的答复。 请参考表 168。RM758225-RM00286 HSE-B 固件参考手册中 S32K312、S32K342、S32K322 和 S32K341 设备的 SBAF 和 HSE 固件版本兼容性-V2.5 (2.5) .pdf。遵循备注栏中的建议,确保不存在 HSE_FW 和 SBAF 不兼容问题。 另请参阅6 HSE FW 和 SBAF的兼容性 HSE_FW_S32K312_0_2_55_0_ReleaseNotes.pdf。 此外,我找不到"HSE_Install_FW_312" 项目。今后,请告诉我们您从哪里获得的示例代码,以便我们在该项目上进行测试。 请注意,在圣诞假期期间,我们的支持响应时间可能会比平时长。在某些情况下,您的请求可能会在新年后得到处理。感谢您的理解。 祝好, Robin ------------------------------------------------------------------------------- 注: - 如果本帖回答了您的问题,请点击"ACCEPT AS SOLUTION" 按钮。谢谢! - 我们会在最后一次发帖后的 7 周内跟踪主题,之后的回复将被忽略 如果您以后有相关问题,请另开新主题,并参考已关闭的主题。 -------------------------------------------------------------------------------
記事全体を表示
[ABUSE] Post By: @JohnKlug / Board: imx-processors / Reported by: ustjxdlc ustjxdlc has reported the post Could not invoke dnf for external kernel module in Yocto kirkstone posted by @JohnKlug for the following reasons: Reason: Harassment Details: http://ph-ed-plus.nspu.ru/article/17938"> http://ru.ph-ed-plus.nspu.ru/article/17947"> https://escolesvalenciades.grupotecopy.es/val/node/1295"> https://escolesvalenciades.grupotecopy.es/val/node/1295"> https://jeunescathos-bxl.org/fr/content/pharmacy-online-0"> https://enki.ua/applications/16928"> https://www.trustcirclenetworks.org/issues/2222"> http://www.batshaw.qc.ca/fr/node/164"> https://spdm.dambo.me/forums/miscellaneous/advertisement/pharmacy-online-0"> http://03otvet.ru/voprosy/urologiya/pharmacy-online"> https://obzorpoker.info/forum/pharmacy-online-1"> https://www.thebiketube.com/salsa-aryanna"> https://www.intimuscare.com/pharmacy-online-19"> http://lsdsng.com/node/4269"> http://pi5ny.com/node/4953"> http://ph-ed-plus.nspu.ru/article/17938"> https://www.twelvestepjournaling.com/content/pharmacy-online"> http://pi5ny.com/node/4953"> http://sp-journal.ru/article/19179"> http://old.jeunescathos.org/fr/content/pharmacy-online-10"> http://www.hudebniburza.cz/dilo/pharmacy-online-7"> https://californiaweddingday.com/your-couple-name-2386"> http://www.gradspot.com/qa/pharmacy-online-7"> https://recruitment.kenet.or.ke/node/2040"> https://www.intimuscare.com/pharmacy-online-19"> https://www.spinsheet.com/racing-team-log/pharmacy-online-3"> http://www.le-cercle-des-sourires.fr/evnementunique/pharmacy-online"> https://www.vgame.ca/node/46840"> http://03otvet.ru/voprosy/urologiya/pharmacy-online"> https://whs6570.com/node/2095"> https://hetnieuweteamwerken.be/forums/forum/pharmacy-online-11"> https://www.intellectualpedia.org/audiologistwholesale-pharmacy-online-5"> http://xn--37-6kci4a9aahjr0a.xn--p1ai/pharmacy-online-ivanovo-5"> https://actipedia.org/gallery/pharmacy-online"> http://www.hudebniburza.cz/dilo/pharmacy-online-7"> https://jeunescathos-bxl.org/fr/content/pharmacy-online-0"> https://actipedia.org/gallery/pharmacy-online"> http://ysrp.bnl.bm/review/pharmacy-online-9"> https://dev.worldwar1luton.com/forum-topic/pharmacy-online-2"> http://ysrp.bnl.bm/review/pharmacy-online-9"> Post link: https://community.nxp.com/t5/i-MX-Processors/Could-not-invoke-dnf-for-external-kernel-module-in-Yocto/m-p/1627964#M203740 Post author: @JohnKlug | Email Author Reported by: ustjxdlc | Email Reporter The reported post has 2 replies.
記事全体を表示
"LPC1769FBD100/P1 型号中的 "P1 "是什么意思?" 大家好, 最近,我收到了一包 LPC1769 芯片。奇怪的是,它后面的编号是 P1,这似乎有点特别,我一直没有找到 LPC1769 作为 P1 的具体含义和使用手册。 因此,我特地来向大家请教,希望得到大家的帮助。 谢谢~~~ LPC1769FBD100 大家好, 最近我收到一包lpc1769芯片,奇怪的是它的末尾编号是p1,似乎有些特殊,而且未能查到有关于lpc1769这款p1的具体含义以及手册。 所以,特地前来,咨询大家,希望得到大家的帮助。谢谢大家。 LPC1769FBD100 注:所附图片已删除。 LPC17xx Re: What`s the meaning of the 'P1' in the type of "LPC1769FBD100/P1" 嗨,@Kuroky_Rasum、 P1 是内部标识符,不影响 MCU 的功能。 您可以在下面的社区帖子中找到更多详细信息。 LPC1769FBD100、551 / LPC1769FBD100K / LPC1769FBD100/P1K 之间的区别 - NXP Community 最佳问候, Pablo
記事全体を表示
如何使用 ICU 读取 PWM 数据? 我使用的是 S32K389 芯片。 我正在尝试使用 ICU 读取 PWM 输入数据,但没有成功。 如下图所示,PTF17 引脚被设置为 emios_1_ch_1_h 输入引脚。 然后,如下图所示,添加了一个元器件。 在 ICU 元器件中,ICUChannels、icuemiOS 和 ICUHWInterruptConfigList 设置为下图所示的值。 Mcl 元器件中的 emiosCommon 设置值的设置如下图所示。 IntCtrl 元器件的中断控制器设置值的设置如下图所示。 最后,对 Siul2_Port 元器件的 PortConfigSet 设置值进行了设置,如下图所示。 当我使用主函数中的 Emios_Icu_Ip_GetDutyCycleValues 函数读取 PWM 数据时,它不起作用。 下面的代码是经过测试的源代码。 ==================================================================== #define INSTANCE_1(uint8)1U #defineCHANNEL_0 (uint8)0U eMios_Icu_Ip_DutyCycleTypeic_result_temp; int main(void) { /* 初始化时钟 */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* 使用 驱动程序驱动程序初始化所有引脚 */ Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_VS_0, g_pin_mux_InitConfigArr_PortContainer_0_VS_0); /* 安装 EmiosISR */ IntCtrl_Ip_Init(&IntCtrlConfig_0); /*Emios Mcl 启动*/ Emios_Mcl_Ip_Init(INSTANCE_1,&Emios_Mcl_Ip_Sa_1_Config_VS_0); /* 初始化 Icu驱动程序 */ Emios_Icu_Ip_Init(INSTANCE_1,&eMios_Icu_Ip_1_Config_PB_VS_0); /* 启动 eMIOS 通道的信号测量*/ Emios_Icu_Ip_StartSignalMeasurement(INSTANCE_1, CHANNEL_0); 同时(1) { Emios_Icu_Ip_GetDutyCycleValues(INSTANCE_1,CHANNEL_0,&ic_result_temp); //如果被捕获 如果(ic_result_temp.PeriodTime) { /停止测量 Emios_Icu_Ip_StopSignalMeasurement(INSTANCE_1, CHANNEL_0); 打破; } delay(); } Exit_Example(TRUE); 返回(0U); } ==================================================================== Emios_Icu_Ip_GetDutyCycleValues 函数中的 EMIOS_ICU_DUTY_CYCLE 检查部分总是 EMIOS_ICU_NO_MEASUREMENT(eMios_Icu_Ip_axChState[eMios_Icu_Ip_u8IndexInChState[instance][hwChannel]].测量)。 谢谢! Re: How can I read PWM data using ICU? 你好@jeff_choi_0662 我也遇到了类似的问题,如果您解决了测量频率的问题,能否分享一下配置或代码?
記事全体を表示