Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Touch Controller IC Part Number for iMXEBOOKDC5 Dear Team, I am using the iMXEBOOKDC5 together with the i.MX8ULP EVK. So far, everything is working well. The E-Ink display is functioning correctly, and both the buttons and joystick are operating as expected. I would now like to enable the touch panel on the display. However, I cannot identify the part number of the touch controller IC used on the EPD module because the marking on the IC appears to have been erased by laser marking. I have tried to find the information myself, but without success. Could you please share: The touch controller IC part number used on the iMXEBOOKDC5 display. Any available Linux driver, library, or software package for supporting the touch functionality. Thank you for your help. Best regards, Evaluation Board Re: Touch Controller IC Part Number for iMXEBOOKDC5 Hello, The touch controller IC used is the GT911, manufactured by Goodix Technology. You can take a look into the driver in the next link: https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/drivers/input/touchscreen/goodix.c Best regards. Re: Touch Controller IC Part Number for iMXEBOOKDC5 Dear, Thanks for your support BTW, can you help to provide the wayform bin file for the e-ink panel? BRs, Ryder
View full article
How do you evaluate IPTV service quality on Android TV devices based on NXP i.MX processors? Hello everyone, I'm currently evaluating IPTV playback performance on Android TV devices powered by NXP i.MX processors. Rather than comparing providers based only on channel count, I'm interested in the technical aspects that affect playback quality. Some of the metrics I'm testing include: Stream stability during peak viewing hours Hardware video decoding performance HLS and MPEG-TS compatibility Channel switching latency Buffer management EPG loading performance Ethernet versus Wi-Fi reliability For anyone working with Android TV or embedded multimedia systems, what criteria do you consider most important when evaluating a streaming service? As part of my research, I recently wrote an article discussing the factors to consider when choosing an IPTV provider for users in the USA, Canada, and the UK. It focuses on technical evaluation rather than marketing. If anyone is interested, the article is available on Medium. I'd also appreciate hearing about your experiences with ExoPlayer, VLC, or other playback frameworks on i.MX platforms. Thank you!
View full article
Facemesh Landmark 模型 ptq 转换中的性能下降 本仓库中使用的是 NXP 在 ptq 之后发布的 Google FaceMesh 模型: nxp-demo-experience-demos-list/downloads.json 位于 lf-6.12.3_1.0.0 · nxp-imx-support/nxp-demo-experience-demos-list 但该模型基于谷歌旧的 FaceMesh 模型,该模型有 468 个地标点。 现在我们想升级到谷歌新的 FaceMesh 模型,它有 478 个地标点。我们希望在 iMX 95 FRDM 板 NPU 上运行此程序。所以,我们想把它量化。我们使用的是NXP的eIQ-neutron-sdk-linux-3.1.3量化该模型。 经过量化之后,我们发现模型性能显著下降,几乎无法实际使用。 最初我们使用 MIN-MAX 选项对其进行量化。那个模型根本没法用。然后我们尝试使用百分位数选项,发现将百分位数设置为 95 时性能更好(即使这是回归器的输出)。 但这仍然无法带来理想的性能。 1)NXP为旧版FaceMesh(468)模型创建ptq文件时,使用了MIN-MAX选项吗?或者百分位数? 2)量化后性能急剧下降时,我们还需要检查其他方面吗? 3) 我们使用 CelebA 数据集进行性能分析,在 scripts 目录中使用 serialize_image.py 脚本并设置了模型特定选项。我们应该运行完整的媒体管道并创建校准数据集,还是应该修改 serialize 脚本? 提供的选项 serialize_image.py : -i //218 x 178 正面 RGB 图像 -o -f bin -t float32 -m 0到1 -s 256,256 -布局 NHWC -co RGB tflite-profiler: --input --dataset --输出 tflite-quantizer: --input --profile --quantize-inputs=false --quantize-outputs=false --quantization-calibration-method= //最小值、最大值或百分位数 Re: Performance degradation in Facemesh Landmark model ptq conversion 嗨@dhilshad , 感谢您联系恩智浦技术支持! 1)很遗憾,我们目前没有相关信息。 2)这种行为是预期的。量化只是部署过程的一部分;将模型转换为嵌入式硬件上执行并进行优化还涉及几个额外的步骤,例如图优化、运算符映射、硬件特定的转换和运行时验证。因此,即使模型已经量化,模型的行为和性能也可能发生变化。 对于新的设计和评估,我建议使用 eIQ Olive,因为它为 NXP i.MX 平台上的模型优化和部署提供了一个更现代化的框架。它包括更新的工作流程和对当前机器学习部署场景的改进支持。 更多信息请参考以下教程和文档: https://eiq.nxp.com/learning-hub/tools/olive/index.html 这些资源涵盖了在 i.MX 设备上部署机器学习模型的推荐工作流程和最佳实践。 此致, 查维拉 Re: Performance degradation in Facemesh Landmark model ptq conversion @Chavira你好,谢谢你的回复。并指出相关文档 在这里需要澄清的是,我们主要关注的是模型的准确性。对于 FaceMesh 模型,我们发现输出的特征点精度不足以满足我们的应用需求。正如我之前所说,我们发现保持 95 百分位截断值比 MIN MAX 截断值略好一些。但仍然无法与 NXP 的 ptq 模型(FaceMesh 468)的精度相提并论。 我们还有一点需要说明: 1)我们尝试只提供生产环境中的 8 个样本作为代表性数据集。这样略微改善了结果。然后我们添加了来自同一环境的 250 张图像,并进行了分析和量化。但这导致准确率下降。 你知道这种行为可能是什么原因造成的吗? 2)另外,NXP 是否已经将 Google 的新 FaceMesh 模型(具有 478 个地标)转换为 ptq 模型?
View full article
ICODE SLIはICODE SLIXに切り替えられません クライアントは私が提供したICODE SLIチップを使っていますが、このチップは終了しています。ICODE SLIXへの切り替えを試みていますが、クライアントのRFIDリーダーが認識できません。 Re: ICODE SLI can't be switch to ICODE SLIX こんにちは、 ICODE SLIXはISO15693レベルでICODE SLIと後方互換性を持つことを意図しているため、リーダーは少なくとも在庫管理時にSLIX UIDを検出すべきです。リーダーが認識できない場合は、まず故障がRFインベントリレベルにあるのか、アプリケーションのタグ識別ロジックにあるのかを確認してください。一般的な原因には、AFI/UIDフィルタリング、SLI製品認識のハードコード、古いリーダーファームウェア、または移行時のSLIX特有のセキュリティや機能の使用などがあります。最初のテストでは、AFIフィルタリングとタグホワイトリストを無効にし、標準ISO15693インベントリを実行し、UID/DSFID/AFIを読み取り、アプリケーションの受け入れロジックを旧SLIタグと比較します。 よろしくお願いします。 Re: ICODE SLI can't be switch to ICODE SLIX このスレッドを適切なコミュニティに移してください。これはColdfireや68kの部品ではありません。
View full article
dtb 是否会更改 LAW 配置(T2080RDB)? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 我使用的是 T2080RDB。我想更改 PCI 设备的内存位置。我已经更换了 dtb。但是,由于 LAW 寄存器没有被修改,因此它不起作用。 我想知道是否必须更改 uboot 和 dtb(两者)才能获得正常功能。 BR QorIQ T4 设备 Re: Does dtb change the LAW configuration (T2080RDB)? 关于 LAW 配置的变化,这是一个有趣的问题。在许多情况下,即使是微小的调整也会影响功能,因此最好还是通过可靠的资源进行交叉检查。我发现,查看结构化指南(如蜂巢规划器设置)确实有助于了解配置如何与不同的设置保持一致。此外,还强烈建议在受控环境中跟踪更新和测试更改。 Re: Does dtb change the LAW configuration (T2080RDB)? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 设备树仅反映由引导加载程序建立的本地地址映射。Linux 不会改变法律。 如果你想更改 LAW 设置,请在 U-启动 中的主板专用代码中进行更改,然后调整设备树 因此。 Re: Does dtb change the LAW configuration (T2080RDB)? 有趣的问题。据我观察,更新 DTB 通常会更改硬件描述和启动设置,而不是直接修改 LAW 配置,除非固件或板级支持包明确地将它们绑定在一起。我在查看Tarrant 属性详细信息时发现了一些有用的背景信息,这让我意识到验证配置更改的重要性,而不是想当然地认为它们是自动生效的。比较前后设置可能是确认 LAW 是否真正受到影响的最安全方法。 Re: Does dtb change the LAW configuration (T2080RDB)? T2080RDB 上采用 LAW 配置的 DTB 行为可能取决于所使用的具体设置和软件版本。查看配置文件和相关文档可能有助于确认参数的应用方式。有关组织化记录系统的更多参考资料,例如DeSoto Court Appeals等资源可以提供结构化数据访问的示例。检查日志并在受控环境中测试更改也有助于确定确切的影响。
View full article
ICODE SLI can't be switch to ICODE SLIX My client has been using the ICODE SLI chip I provided, but this chip has been EOL. We are trying to switch to the ICODE SLIX, but the client's RFID reader cannot recognize it. Re: ICODE SLI can't be switch to ICODE SLIX Hello, ICODE SLIX is intended to be backward compatible with ICODE SLI at the ISO15693 level, so the reader should at least detect the SLIX UID during inventory. If the reader cannot recognize it, please first check whether the failure is at RF inventory level or in the application’s tag-identification logic. Common causes are AFI/UID filtering, hardcoded SLI product recognition, old reader firmware, or use of SLIX-specific security/features during migration. For the first test, disable AFI filtering and tag whitelisting, perform a standard ISO15693 inventory, read UID/DSFID/AFI, then compare the application’s acceptance logic against the old SLI tag. Regards Re: ICODE SLI can't be switch to ICODE SLIX Please move this thread to the appropriate community. This isn't a Coldfire or 68k part.
View full article
Facemesh Landmarkモデルptq変換におけるパフォーマンス低下 このリポジトリでは、ptq後にNXPがリリースしたGoogleのFaceMeshモデルを使っていました: nxp-demo-experience-demos-list/downloads.json at lf-6.12.3_1.0.0 ·NXP-IMX-support/NXP-demo-experience-demos-list しかしこのモデルは、468のランドマークポイントを持つGoogleの旧FaceMeshモデルに基づいています。 次に、Googleの新しいFaceMeshモデルに移行したいと考えています。これには478のランドマークポイントがあります。これをiMX 95 FRDMボードのNPU上で実行したいと考えています。そこで、これを量子化したかったのです。NXPのeIQ-neutron-sdk-linux-3.1.3を使っていますこのモデルを量子化するために。 この量子化の後、モデルのパフォーマンスは著しく劣化し、実際に使うにはほとんど使えない状態です。 当初はMIN-MAXオプションを使用して量子化していました。そのモデルは使い物にならなかった。次に、パーセンタイルオプションを使用してみたところ、パーセンタイルを95に設定した方がパフォーマンスが向上することがわかりました(これは回帰モデルの出力でしたが)。 しかし、それでも十分な性能は得られていません 1) NXPが古いFaceMesh(468)モデルのptqファイルを作成した際、どのオプションを使っていましたか?MIN-MAX?それともパーセンタイル? 2) 量子化後にパフォーマンスが著しく低下した場合、他に確認すべき事項はありますか? 3) CelebAデータセットでプロファイリングを行い、スクリプトのserialize_image.pyをモデルオプションで使いました。メディアパイプ全体を実行してキャリブレーションデータセットを作成するか、シリアル化スクリプトで変更すべきか オプション提供 serialize_image.py: -i //218 x 178 前面向けRGB画像 -<パス/トゥ/calib_bins> -Fビン -T float32 -0to1 -256、256 -NHWCレイアウト -コRGB TFLITE-Profiler: --input --データセット --出力 TFLITE-クオンタイザ: --input --プロファイル --quantize-inputs=false --quantize-outputs=false --量子化-キャリブレーション-方法= //最小最大値またはパーセンタイル Re: Performance degradation in Facemesh Landmark model ptq conversion こんにちは@dhilshad。 NXPサポートにご連絡いただきありがとうございます! 1) 残念ながら、現時点ではその情報は入手できません。 2) この挙動は想定内です。クオンタイズは展開プロセスの一部に過ぎません。組み込みハードウェア上でモデルを変換・最適化するには、グラフ最適化、演算子マッピング、ハードウェア固有の変換、ランタイム検証など、いくつかの追加ステップが必要です。その結果、モデルがすでに量子化されていても、モデルの挙動や性能は異なることがあります。 新しいデザインや評価には、eIQ Oliveの使用をおすすめします。NXP i.MX プラットフォームでのモデル最適化と展開のためのよりモダンなフレームワークを提供するからです。ワークフローの更新と、現在の機械学習展開シナリオへのサポート強化が含まれています。 詳細については、以下のチュートリアルおよびドキュメントをご参照ください。 https://eiq.nxp.com/learning-hub/tools/olive/index.html これらのリソースは、i.MX デバイスに機械学習モデルを導入するための推奨ワークフローやベストプラクティスをカバーしています。 よろしくお願いします、 チャビラ Re: Performance degradation in Facemesh Landmark model ptq conversion こんにちは、 @Chavira さん。返信ありがとうございます。そして、ドキュメントを指摘しています ここで念のために言うと、主な関心はモデルの正確さです。FaceMeshモデルの場合、出力するランドマークポイントはアプリケーションに対して十分に正確でないことがわかります。先ほど申し上げたように、95パーセンタイルをカットオフ値として設定する方が、MIN MAXよりもわずかに良い結果が得られることが分かりました。しかし、それでもNXPのptqモデル(FaceMesh 468)で見られる精度には及びません。 もう一つ気づいた点があります。 1) 代表的なデータセットとして、本番環境から8つのサンプルだけを用意して試してみました。これは結果をわずかに改善させた。次に、同じ環境から250枚の画像を追加し、プロファイリングと量子化を行った。しかし、これによって精度が低下した。 なぜこのような行動が起こるのか、何か心当たりはありますか? 2) また、NXPはすでにGoogleの新しいFaceMeshモデル(478ランドマーク搭載)をPTQに変換していますか?
View full article
ICODE SLI 无法切换到 ICODE SLIX 我的客户一直在使用我提供的 ICODE SLI 芯片,但该芯片已经停产了。我们正在尝试切换到 ICODE SLIX,但客户的 RFID 阅读器无法识别它。 Re: ICODE SLI can't be switch to ICODE SLIX 你好, ICODE SLIX 旨在向后兼容 ISO15693 级别的 ICODE SLI,因此读卡器至少应该在盘点期间检测到 SLIX UID。如果读卡器无法识别,请先检查故障是出在射频存货层面还是出在应用程序的标签识别逻辑层面。常见原因包括 AFI/UID 过滤、硬编码的 SLI 产品识别、旧的读卡器固件,或者在迁移过程中使用 SLIX 特有的网络安全/功能。对于第一个测试,禁用 AFI 过滤和标签白名单,执行标准的 ISO15693 清单,读取 UID/DSFID/AFI,然后将应用程序的接受逻辑与旧的 SLI 标签进行比较。 此致 Re: ICODE SLI can't be switch to ICODE SLIX 请将此帖移至合适的社区。这不是Coldfire或68k零件。
View full article
Front and Rear Lights – Logic Control 1 Table of Contents • Introduction • Simulink Model Overview • Inputs • Algorithm • LED Output • Diagnostics • References • Conclusion 2 Introduction This article describes how the Front Lights System (FLS) and the Rear Lights System (RLS) applications work internally, by walking through the Simulink models and describing how signals travel from the CAN bus all the way to the LED strip on the evaluation board. The goal is to give a practical understanding of what each model does, from the moment a command is received up to the moment the corresponding lamp is turned on. Both nodes are described together because they share the same overall architecture, the same execution pattern, and almost the same set of subsystems. The differences between them are limited to the lighting functions that only make sense on one side of the vehicle (Daytime Running Lights on the front, Stop Lights on the rear) and to a few CAN identifiers. Presenting them side by side keeps the article shorter and highlights how the same design pattern is reused across projects. Earlier articles in this series introduced the boards, the toolchain, and the general project layout. This article focuses on the application logic. 3 Simulink Model Overview Each application is implemented as an individual Simulink model, one for the Front Node and one for the Rear Node, structured into communication, control, and output subsystems. From a model perspective, the application can be divided into four logical areas: CAN reception and unpacking Per-function logic control LED aggregation Diagnostics Figure 1 - Front Lights main Simulink application Figure 2 - Rear Lights main Simulink application The reception area receives CAN frames from the Central Controller and makes the extracted signals available to the rest of the model through shared Data Store Memory blocks. The control area contains one Stateflow chart per lighting function and decides which lamps should be on or off. The output area builds the color pattern from the lamp requests. This separation keeps the model modular and makes it easier to add new lighting functions without changing the reception or the actuation logic. 4 Inputs Each node receives information from three main categories of inputs. CAN Network Inputs CAN communication is the main source of information for both applications. All messages come from the Central Controller and are defined in the DBC file that ships with each project. On the Front Lights node the application consumes: Gear Mode - 4 bits Activate Headlights - 0 = OFF, 1 = LOW BEAM, 2 = HIGH BEAM Activate Fog Lights - 1-bit on/off command Turn Commands - packs the signals: Activate Hazard Lights Turn Left Turn Right On the Rear Lights node the set is almost the same, with Gear Mode replaced by Press Brake - an 8-bit signal that carries the brake pedal position. The other three messages are shared with the front node. Local Fault Input On top of the CAN traffic, each node reads a digital fault input through a DIO block. The value of this pin is stored in a shared Data Store ( FLS_Fault or RLS_Fault ) and is consumed by every logic-control chart. When the fault is asserted, the charts switch to a dedicated fault branch and the LEDs display a blink pattern to signal the condition visually. Configuration Inputs Before normal operation begins, each model runs an Initialize Function that sets up the peripherals used by the application. Figure 3 - Initialize Function This subsystem enables the CAN controller interrupts and moves the controller into the started mode. 5 Algorithm Internally, each node performs four main processing activities. Message Reception The first step consists of collecting the incoming CAN traffic. Reception is interrupt-driven: a Can_RxIndication handler is registered at the top level of the model and fires a function-call trigger every time a new frame arrives. The trigger runs the CAN Unpack subsystem exactly once and captures the frame identifier, the payload, and the length. Model Representation of Message Reception Inside the CAN Unpack subsystem there is one CAN Unpack block per DBC message. Each block decodes the incoming frame and extracts the signals declared in the DBC file. Figure 4 - Front Lights CAN reception subsystem Figure 5 - Rear Lights CAN reception subsystem Overall, the reception subsystem receives the CAN frames, decodes the payload into named signals, and places them into the shared Data Stores. Per-Function Logic Control Every lighting function is implemented as a dedicated Stateflow chart. All charts follow the same skeleton: an Idle state where the lamp is OFF, one or more active states covering the operating modes, and a small fault branch ( Fault_Detected and Fault_Detected_Off ) that toggles a per-function fault flag whenever the shared fault input is asserted. Head Lights Logic Control The head lights chart reads CCS_ActivateHeadLights and moves from Idle to Head_Lights_LowBeam when the command equals 1, and to Head_Lights_HighBeam when it equals 2. Direct crossovers between the two beams are allowed without going through Idle. When the fault input is asserted, the chart enters the fault branch and toggles Low_Beam and High_Beam to create a blink pattern. Figure 6 - Head Lights logic control chart Fog Lights Logic Control The fog lights chart moves from Idle to Fog_Lights_Active when CCS_ActivateFogLights is 1 and returns to Idle when the command drops back to 0. The fault branch is identical to the one used by the head lights chart. Figure 7 - Fog Lights logic control chart DRL Logic Control (Front only) The DRL chart only exists on the front node. It keeps the daytime running lights on whenever the vehicle is in a drive gear: Idle moves to DRL_Active when CCS_GearMode is between 1 and 4, and drops back to Idle when the gear returns to 0. Fault handling is identical to the other charts. Figure 8 - DRL logic control chart (Front Lights only) Stop Lights Logic Control (Rear only) The stop lights chart keeps the stop lights on as long as the brake pedal is pressed: Idle transitions to Brake_Active when CCS_PressBrake is different from 0, and returns to Idle when the pedal is released. The fault branch is identical to the other charts. Figure 9 - Stop Lights logic control chart (Rear Lights only) Turn Lights (Turn Signals and Hazards) The turn lights chart handles both the direction indicators and the hazard lights, and also generates the blinking pattern. It uses parallel states: an outer super-state selects between Idle, Turn_Left_Active, Turn_Right_Active and Hazard_Active, while inside each active super-state a pair of On and Off states swaps every 500 ms using after(0.5, sec) transitions. From Idle, the chart enters Turn_Left_Active when CCS_TurnLeft is asserted, Turn_Right_Active when CCS_TurnRight is asserted, and Hazard_Active when CCS_ActivateHazardLights is asserted. Direct crossovers between left and right are allowed. When the fault input is asserted, the chart moves into the fault branch. Figure 10 - Turn Lights logic control chart 6 LED Output The per-function charts do not drive the LED strip directly. They only produce simple lamp requests, and a central Stateflow chart is in charge of turning those requests into a color pattern that the LED strip can display. Each lighting mode has its own state inside this chart, and every state sets the colors that represent that mode on the strip. For example, the head lights use white, the fog lights light up a few dedicated pixels, and the turn signals move step by step across one side of the strip. The hazard mode reuses the same effect on both sides at the same time. On the front node the chart also includes a state for the daytime running lights, and on the rear node it includes a state for the stop lights. Once the color pattern is ready, it is passed to a Function-Call Subsystem that sends it to the physical LED strip. This subsystem takes care of the low-level details, so the rest of the model only deals with lighting behavior. Figure 11 - LED output chart 7 Diagnostics Alongside the normal lighting behavior, each node also reports its own health to the rest of the system. A local fault input is read at runtime and made available to every logic chart, so the lamps can switch to a fault indication whenever a problem is detected on the board. The same fault information is also sent back to the Central Controller over CAN, using a short dedicated message. This way, the rest of the vehicle can react to a lighting-node fault without having to check anything manually. In addition, the model exposes its internal signals to FreeMASTER, which allows the developer to observe the CAN commands, the lamp requests, and the fault flags live during development and troubleshooting. 8 References Front and Rear Lights - Overview Front and Rear Lights - SW & HW Environment Model-Based Design Toolbox (MBDT) Community Model-Based Design Toolbox (MBDT) - S32K3 - How To MATLAB® and Simulink® Documentation 9 Conclusion This article described the internal behavior of the Front Lights and Rear Lights nodes by looking at how information flows through the models. It explained how CAN commands are received, interpreted by dedicated Stateflow charts, and finally turned into the corresponding lighting behavior on the LED strip, while the local fault status is reported back to the Central Controller. Because both applications share the same architecture, they were presented together. The only real differences are the set of lighting functions specific to each side of the vehicle (DRL on the front, Stop Lights on the rear) and the identifiers used for the fault message. The next articles in the series will take a closer look at specific parts of these applications, such as the CAN communication, the LED driving, and the tools used to validate and troubleshoot the lighting behavior.
View full article
imx8mmini sai1 最大サンプルレート hi SAI1 Connectのコーデックはサンプルレート768kHz/32bitに対応しています。 SAI1-RX0 codec_DOUT接続。 768kHz/32bitおよびL/Rチャネルで読み取れるデータはありませんが、SAI1-TXFS/SAI1-TXCは768kHz/49.152Mhzを出力可能です。768khz/16bitおよび384khz/32bitのL/Rチャネル読み取りは問題ありません。カーネルバージョン6.1.36です。 ありがとうございます。 Re: imx8mmini sai1 max sample rates コーデックdtsについては以下の通りです。 「-f S32_LE -r 384000 -c 2 -d 1 test.wav」を指定して arecord コマンドを実行します。または「-f S16_LE -r 786000 -c 2 -d 1 test.wav」でも問題ありません。しかし、「-f S32_LE -r 768000 -c 2 -d 1 test.wav」で実行すると、test.wav は NULL になります。 Re: imx8mmini sai1 max sample rates こんにちは、 デバイスツリーの設定を教えていただけますか? どのコーデックを使用していますか? よろしくお願いいたします。 Re: imx8mmini sai1 max sample rates こんにちは、 サンプルレートに関連するエラーが出る場合、クロックソースがそのサンプルレートに必要な周波数を生成できないため、原因かもしれません。 特定のサンプリングレートを得るためには、外部クロックなどの専用のクロックソースを使用する必要がある場合があります。 よろしくお願いいたします。 Re: imx8mmini sai1 max sample rates こんにちは、 テスト中にアンダーフローエラーやオーバーフローエラーが発生しますか? よろしくお願いいたします。 Re: imx8mmini sai1 max sample rates 768kHzの32ビット×2チャンネルで読み取ると、SAI1_TXFS/SAI1_TXC出力は正常(768kHz/49.152MHz)です。コーデックのデータ出力ピン(SAI1_RX0に接続)は、オシロスコープで確認するとデータ出力があります。imx8mminiのSDMAが動作していない可能性はありますか? Re: imx8mmini sai1 max sample rates テスト中に以下のようなカーネル出力エラーが発生しました。 [ 506.336480] [858] wait_for_avail:1936: asoc-simple-card sound-pcmdev: キャプチャ書き込みエラー (DMA または IRQ の問題?) Re: imx8mmini sai1 max sample rates こんにちは、 dmesg の内容を共有してください。 dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai" そのエラーログではオーバーランが原因かもしれません。例えば、期間とバッファサイズを増やしてみてください。 arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav よろしくお願いいたします。 Re: imx8mmini sai1 max sample rates こんにちは、ホルヘカスさん: ご返信ありがとうございます。 期間とバッファサイズを増やした場合も同じエラーが発生します。 ------------------------------------ root@mx8mm:/tmp# arecord -v -D hw:0,0 -f S16_LE -r 768000 -c 2 -d 1 test.wav WAVEファイル「test.wav」を録音しています:署名付き16ビットリトルエンディアン、レート768000 Hz、ステレオ ハードウェアPCMカード0 'pcmdev-オーディオ' device 0 subdevice 0 その構成は以下の通りです: ストリーム:キャプチャ アクセス:RW_INTERLEAVED フォーマット:S16_LE サブフォーマット:STD チャネル数:2 レート:768000 正確なレート:768000(768000/1) MSBITS:16件 buffer_size:131064 period_size:16383 period_time:21332 tstamp_mode:なし tstamp_type:単調 period_step : 1 avail_min:16383 period_event : 0 start_threshold : 1 stop_threshold:131064 silence_threshold:0 silence_size : 0 境界:9222809086901354496 appl_ptr : 0 hw_ptr : 0 root@mx8mm:/tmp# test.wav -la -rw-r--r-- 1 ルート 7月22日 22:09 test.wav 3072044 root@mx8mm:/tmp# arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav WAVEファイル「test.wav」を録音しています:署名付き32ビットリトルエンディアン、レート768000 Hz、ステレオ arecord: pcm_read:2221: read error: input/output error root@mx8mm:/tmp# dmesg |grep -i -E "xrun|overrun|dma|fifo|sdma|sai" [ 0.00000] OF: 予約済みメモリ:初期化されたNode Linux、CMA、互換性ID Shared-DMA-プール [ 0.000000] 予約メモリ:0x00000000b8400000にDMAメモリプールを作成、サイズ1 MiBで [ 0.00000] OF: 予約済み メモリ: 初期化されたノードvdevbuffer@b8400000、互換性のあるid shared-dma-pool(共有済みDMA-プール) [0.000000] DMA [記憶0x0000000040000000-0x00000000bfffffff] [ 0.000000] DMA32 空 [ 0.000000] ポリシーゾーン:DMA [ 0.043871] DMA:原子力割り当て用に事前割り当てされた256 KiB GFP_KERNELプール [ 0.044176 DMA: 事前割り当て256 KiB GFP_KERNEL|GFP_DMA原子割り当てプール [ 0.044364] DMA: 事前割り当て256 KiB GFP_KERNEL|GFP_DMA32原子割り当てプール [ 0.105243] iommu: DMAドメインTLB無効化ポリシー:厳格モード [ 0.195002] IMX-SDMA 302C0000.DMA-コントローラー:imx/sdma/sdma-imx7d.binの直接ファームウェアロードがエラー-2で失敗しました [ 0.195018] IMX-SDMA 302C0000.DMA-コントローラー:sysfsへのフォールバック:imx/sdma/sdma-imx7d.bin [ 0.199761] MXS-DMA 3300000.DMA-コントローラー:初期化 [ 1.996379] mmc2: 30b60000.mmc 上のSDHCIコントローラ [30b60000.mmc]ADMAの使用 [ 2.786360] mmc1: 30b50000.mmc 上のSDHCIコントローラー [30b50000.mmc]ADMAの使用 [ 8.812860] IMX-SDMA 302C0000.DMA-コントローラー:ファームウェアが見つかりました。 [ 8.818748] IMX-SDMA 30BD0000.DMA-コントローラー:ファームウェアが見つかりました。 [ 8.825901] IMX-SDMA 30BD0000.DMA-コントローラ:ファームウェア4.6をロードしました [ 91.326700] [857] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec:ASoC: pcmdevice-codec <-> 30010000.sai 情報: [ 91.326722] [857] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec:ASoC: レートマスク 0x154c0 [ 91.326728] [857] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec:ASoC: ch 最小2 最大8 [ 91.326734] [857] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec:ASoC: レート最小 44100 最大 768000 [ 91.342776] [857] fsl_sai_set_bclk:460: fsl-sai 30010000.sai:クロック周波数49152000Hzに基づく周波数24576000Hzの比率2 [ 91.342784] [857] fsl_sai_set_bclk:481: fsl-sai 30010000.sai:最適な適合: 時計ID=1、div=2、偏差=0 [ 91.343315] [857] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai:30010000.saiキャプチャのDAIルートを更新します [ 113.965788] [861] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec:ASoC: pcmdevice-codec <-> 30010000.sai 情報: [ 113.965809] [861] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec:ASoC: レートマスク 0x154c0 [ 113.965816] [861] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec:ASoC: ch 最小2 最大8 [ 113.965822] [861] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec:ASoC: レート最小 44100 最大 768000 [ 113.977610] [861] fsl_sai_set_bclk:460: fsl-sai 30010000.sai:クロック周波数49152000Hzに基づく周波数49152000Hzの比率1 [ 113.977618] [861] fsl_sai_set_bclk:481: fsl-sai 30010000.sai:最適な適合: 時計ID=1、div=1、偏差=0 [ 113.978149] [861] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai:30010000.saiキャプチャのDAIルートを更新します [ 124.127055] [861] wait_for_avail:1936: asoc-simple-card sound-pcmdev: キャプチャ書き込みエラー (DMA または IRQ の問題?) root@mx8mm:/tmp# ls test.wav -la -rw-r--r-- 1 root root 44 7月 22 22:09 test.wav root@mx8mm:/tmp#
View full article
i.MX 9 准备好了吗? 几年前我开始了一个项目,当时 NXP 的 i.MX 9 系列 MPU 开始发布,但它们基本上无法获得,所以我选择了性能强大的 i.MX 8。现阶段,它的性能远远超过我的需求,我想换用性能小得多的微处理器。我原本打算买最小的 i.MX 8,但他们最小的 CPU 是 i.MX91。我一直在想,如果选择91型而不是更成熟的8型,会不会更好。散热是我最关心的问题,所以我认为新的总是更好,但我不知道它们是否已经“达到标准”,因为它们还比较新。更公平的比较,例如将港口升级到 8 级,也可能是一个激励因素。
View full article
About the Finite-State Machine (FSM) of i.MX8Mplus We use Toradex's Veridin i.MX8Mplus at our company. At that time, the SOM_PW_ON signal is input to control the SoM's power supply. (Directly connected to the ON/OFF signal of the i.mx8MPlusSoC). *Please refer to the waveform on the attached oscilloscope.   Due to the circuit configuration on the SoM side, the voltage should be High (1.8V), but for about 800 msec after startup, it remains at an intermediate potential of approximately 0.3-0.4V. I'd like to know how this voltage (0.3 to 0.4V) is handled as an ON/OFF signal on the SoC side. This information was not included in the datasheet or reference manual. I think that in cases of very short ON/OFF operations (<5s), the system may proceed to shutdown. Would the operation detection criteria be the transition from High to Low edge state and the duration of the Low state? I would also like to know the exact minimum/maximum times for those times. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MplusのFinite-State Machine (FSM)について For i.MX8M Plus, ONOFF is handled as a level-held button input with configurable 0/50/100/500 ms qualification and 5/10/15 s forced-off timing, and your observed 0.3–0.4 V on a 1.8 V ONOFF net is most consistently interpreted as logic Low by the available input-threshold documentation. Re: i.MX8MplusのFinite-State Machine (FSM)について Thank you for your reply. The observed V values of 0.3–0.41.8V on the ONOFF network are most consistently interpreted as logically low by the available input threshold documentation. By the way, could you also tell me about the voltage threshold that is interpreted as logically low? Furthermore, if interpreted as logically low, the ON/OFF state will remain logically low for approximately 800 msec after startup before changing to logically high. In that case, would it be considered that a button input occurred? My concern is whether a button press might cause the system to automatically shut down immediately after startup. Re: i.MX8MplusのFinite-State Machine (FSM)について By the way, could you also tell me about the voltage threshold that is interpreted as logically low? I apologize. I would like to know the voltage threshold at which the logic value is interpreted. Re: i.MX8MplusのFinite-State Machine (FSM)について Thank you for your reply. The observed V values of 0.3–0.41.8V on the ONOFF network are most consistently interpreted as logically low by the available input threshold documentation. By the way, could you also tell me about the voltage threshold that is interpreted as the logical high? Furthermore, if interpreted as logically low, the ON/OFF state will remain logically low for approximately 800 msec after startup before changing to logically high. In that case, would it be considered that a button input occurred? My concern is whether a button press might cause the system to automatically shut down immediately after startup. To the NXP TechSupport representative What do you think about this matter? I have one more question: ON/OFF is processed as a level hold button input, with conditions of 0/50/100/500 ms. Regarding that point, I believe the default is 0. In this case, if the level momentarily exceeds the logical high or logical low threshold due to noise or other factors, will the level be held? I am concerned that with this default setting, if noise is received, there is a possibility of malfunction if something that causes a logic judgment opposite to the currently held level logic is introduced, even for a moment. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang I have added a few more questions. We apologize for the inconvenience, but please provide your response. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang How is the confirmation process going? Please provide an answer. Re: i.MX8MplusのFinite-State Machine (FSM)について Sorry to miss your message, I can help checking it and will give you reply next week. Wish you have a nice day Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang Thank you for your assistance. This is Mori from Pal Giken. It's been almost a week now, how is the response going? Thank you for your cooperation.
View full article
关于 i.MX8Mplus 的有限状态机 (FSM) 我们公司使用的是 Toradex 的 Veridin i.MX8Mplus。 此时,输入 SOM_PW_ON 信号以控制 SoM 的电源。(直接连接到 i.mx8MPlusSoC 的 ON/OFF 信号)。*请参考所附示波器上的波形。   由于 SoM 侧的电路配置,电压应为高电压 (1.8V),但在启动后约 800 毫秒内,电压保持在约 0.3-0.4V 的中间电位。 我想知道 SoC 端是如何处理 0.3 至 0.4V 电压作为 ON/OFF 信号的。 该信息未包含在数据表或参考手册中。 我认为,在极短的开/关操作(<5秒)的情况下,系统可能会关机。操作检测标准是否应该是从高电平到低电平的转换以及低电平状态的持续时间? 我还想知道这些时间段的具体最短/最长时间。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MplusのFinite-State Machine (FSM)について 对于 i.MX8M Plus,ONOFF 被处理成一个按住按钮输入,可配置 0/50/100/500 毫秒的延迟和 5/10/15 秒的强制关机时间,并且观察到 0.3–0.4根据现有的输入阈值文档,1.8V ONOFF 网络上的 V 最常被解释为逻辑低电平。 Re: i.MX8MplusのFinite-State Machine (FSM)について 感谢你的回复。 根据现有的输入阈值文档,观察到的 ONOFF 网络上的 V 值在 0.3–0.41.8V 范围内最一致地被解释为逻辑上的低值。 顺便问一下,您能否也告诉我一下逻辑上被解释为低电压的阈值是多少? 此外,如果解释为逻辑低,则 ON/OFF 状态在启动后将保持逻辑低约 800 毫秒,然后变为逻辑高。 在这种情况下,是否可以认为发生了按钮输入? 我担心按下按钮是否会导致系统在启动后立即自动关机。 Re: i.MX8MplusのFinite-State Machine (FSM)について 顺便问一下,您能否也告诉我一下逻辑上被解释为低电压的阈值是多少? 抱歉。我想知道逻辑值被解读时的电压阈值。 Re: i.MX8MplusのFinite-State Machine (FSM)について 感谢你的回复。 根据现有的输入阈值文档,观察到的 ONOFF 网络上的 V 值在 0.3–0.41.8V 范围内最一致地被解释为逻辑上的低值。 顺便问一下,您能否也告诉我一下被解释为逻辑高电平的电压阈值是多少? 此外,如果解释为逻辑低,则 ON/OFF 状态在启动后将保持逻辑低约 800 毫秒,然后变为逻辑高。 在这种情况下,是否可以认为发生了按钮输入? 我担心按下按钮是否会导致系统在启动后立即自动关机。 致恩智浦技术支持代表 你对此事有何看法? 我还有一个问题: ON/OFF 被处理为电平保持按钮输入,条件为 0/50/100/500 毫秒。 关于这一点,我认为默认值是 0。在这种情况下,如果由于噪声或其他因素导致电平瞬间超过逻辑高电平或逻辑低电平阈值,电平是否会被保持? 我担心,在这种默认设置下,如果接收到噪声,即使只是一瞬间,如果引入了导致逻辑判断与当前保持的逻辑电平相反的因素,也可能导致故障。 Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang 我又补充了一些问题。 给您带来的不便,我们深表歉意,请您尽快回复。 Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang 确认流程进展如何? 请提供答案。 Re: i.MX8MplusのFinite-State Machine (FSM)について 很抱歉错过了您的消息,我可以帮忙查看,下周会回复您。 祝你今天过得愉快 Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang 谢谢你的帮助。 这是Pal Giken的Mori。 已经过去快一周了,反响如何? 感谢您的合作。
View full article
i.MX 9は「もう完成形」と言えるのでしょうか? 数年前にプロジェクトを始めたのですが、NXPの i.MX 9シリーズMPUがリリースされ始めていましたが、ほとんど入手困難だったため、重い i.MX 8 にしました。現段階では、これは私の必要以上の性能なので、もっと小型のMPUに移行したいと考えています。最小の1 i.MX 8を買うつもりでしたが、i.MX91が彼らのCPUの中で最も小さいです。より成熟した8よりも91の方が良いのではないかと考えていました。サーマルが一番気になるので、新品の方が良いと思いますが、まだ新しいので「まだ成熟している」かはわかりません。8に移植されるのがより公平な動きも動機になるかもしれません。
View full article
imx8mmini sai1 最大采样率 hi sai1连接编解码器支持 768kHz/32bit 采样率。SAI1 -RX0 连接 codec_DOUT。 没有 768kHz/32bit 和 L/R 通道的数据可供读取。但SAI1-TXFS/SAI1-TXC 可以输出 768kHz/49.152MHz 的数据。读取 768kHz/16bit 和 384kHz/32bit 的 L/R 通道数据正常。内核版本 6.1.36。 谢谢。 Re: imx8mmini sai1 max sample rates 关于编解码器 DTS 的信息如下: 运行 arecord 命令,参数为“-f S32_LE -r 384000 -c 2 -d 1 test.wav”或者“-f S16_LE -r 786000 -c 2 -d 1 test.wav”也可以。但是运行“-f S32_LE -r 768000 -c 2 -d 1 test.wav”,test.wav 为 NULL。 Re: imx8mmini sai1 max sample rates 你好, 请问您能否分享一下您的设备树配置? 你使用的是哪种编解码器? 顺祝商祺! Re: imx8mmini sai1 max sample rates 你好, 如果出现与采样率相关的错误,可能是由于时钟源无法产生该采样率所需的频率造成的。 有时需要使用专用时钟源(例如外部时钟)来获得特定的采样率。 顺祝商祺! Re: imx8mmini sai1 max sample rates 当使用 768kHz 32bit x 2 通道读取时,SAI1_TXFS/SAI1_TXC 输出正常(768kHz/49.152MHz)。用示波器检查时,编解码器数据输出引脚(连接到 SAI1_RX0)有数据输出。imx8mmini sdma 是否有可能不工作? Re: imx8mmini sai1 max sample rates 你好, 测试过程中是否出现下溢或溢出错误? 顺祝商祺! Re: imx8mmini sai1 max sample rates 测试过程中出现如下内核打印错误: [ 506.336480] [858] wait_for_avail:1936: asoc-simple-card sound-pcmdev: 捕获写入错误(DMA 或 IRQ 问题?) Re: imx8mmini sai1 max sample rates 你好, 请分享您的 dmesg: dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai" 根据该错误日志,问题可能是由溢出引起的,请尝试增加周期和缓冲区大小,例如: arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav 顺祝商祺! Re: imx8mmini sai1 max sample rates 嗨JorgeCas : 谢谢你的回复。 增加周期和缓冲区大小时出现同样的错误。 ------------------------------------ root@mx8mm:/tmp# arecord -v -D hw:0,0 -f S16_LE -r 768000 -c 2 -d 1 test.wav 正在录制 WAVE 文件“test.wav”:有符号 16 位小端序,采样率 768000 Hz,立体声 硬件 PCM 卡 0 'pcmdev-audio' 设备 0 子设备 0 其结构如下: 流:捕获 访问权限:读写交错 格式:S16_LE 子格式:STD 通道数:2 利率:768000 准确汇率:768000 (768000/1) 毫秒比特:16 缓冲区大小:131064 period_size:16383 period_time:21332 tstamp_mode:无 tstamp_type:单调 period_step:1 可用最小值:16383 period_event:0 起始阈值:1 停止阈值:131064 沉默阈值:0 静音大小:0 边界:9222809086901354496 appl_ptr:0 hw_ptr:0 root@mx8mm:/tmp# ls test.wav -la -rw-r--r-- 1 root root 3072044 7月 22 22:09 test.wav root@mx8mm:/tmp# arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav 正在录制 WAVE 文件“test.wav”:有符号 32 位小端序,采样率 768000 Hz,立体声 arecord: pcm_read:2221: 读取错误: 输入/输出错误 root@mx8mm:/tmp# dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai" [ 0.000000] OF: 保留内存: 已初始化节点 linux,cma, 兼容 ID shared-dma-pool [ 0.000000] 保留内存:在 0x00000000b8400000 创建了大小为 1 MiB 的 DMA 内存池 [ 0.000000] OF:保留内存:已初始化节点 vdevbuffer@b8400000,兼容 ID shared-dma-pool [ 0.000000] DMA [内存 0x0000000040000000-0x00000000bfffffff] [ 0.000000] DMA32 为空 [ 0.000000] 政策区域:DMA [ 0.043871] DMA:已预分配 256 KiB GFP_KERNEL 池用于原子分配 [ 0.044176] DMA:已为原子分配预分配 256 KiB GFP_KERNEL|GFP_DMA 池 [ 0.044364] DMA:已为原子分配预分配 256 KiB GFP_KERNEL|GFP_DMA32 池 [ 0.105243] iommu:DMA 域 TLB 失效策略:严格模式 [ 0.195002] imx-sdma 302c0000.dma-controller:直接加载 imx/sdma/sdma-imx7d.bin 固件失败,错误代码 -2 [ 0.195018] imx-sdma 302c0000.dma-controller:回退到 sysfs 备选方案:imx/sdma/sdma-imx7d.bin [ 0.199761] mxs-dma 33000000.dma-controller:已初始化 [ 1.996379] mmc2:30b60000.mmc 上的 SDHCI 控制器 [30b60000.mmc]使用ADMA [ 2.786360] mmc1:30b50000.mmc 上的 SDHCI 控制器 [30b50000.mmc]使用ADMA [ 8.812860] imx-sdma 302c0000.dma-controller:已找到固件。 [ 8.818748] imx-sdma 30bd0000.dma-controller:已找到固件。 [ 8.825901] imx-sdma 30bd0000.dma-controller:已加载固件 4.6 [ 91.326700] [857] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec:ASoC:pcmdevice-codec <-> 30010000.sai 信息: [ 91.326722] [857] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec:ASoC:速率掩码 0x154c0 [ 91.326728] [857] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec:ASoC:通道数最少 2 个,最多 8 个 [ 91.326734] [857] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec:ASoC:速率最小值 44100 最大值 768000 [91.342776][857]fsl_sai_set_bclk:460:fsl-sai 30010000.sai:基于时钟频率 49152000Hz,频率为 24576000Hz 的比例为 2 [91.342784][857]fsl_sai_set_bclk:481:fsl-sai 30010000.sai:最佳拟合:时钟 id=1,div=2,偏差=0 [ 91.343315] [857] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai:更新 30010000.sai 捕获的 DAI 路由 [ 113.965788] [861] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec:ASoC:pcmdevice-codec <-> 30010000.sai 信息: [ 113.965809] [861] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec:ASoC:速率掩码 0x154c0 [ 113.965816] [861] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec:ASoC:通道数最少 2 个,最多 8 个 [ 113.965822] [861] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec:ASoC:速率最小值 44100 最大值 768000 [113.977610][861]fsl_sai_set_bclk:460:fsl-sai 30010000.sai:基于时钟 49152000Hz,频率为 49152000Hz 的比例为 1 [113.977618][861]fsl_sai_set_bclk:481:fsl-sai 30010000.sai:最佳拟合:时钟 id=1,div=1,偏差=0 [ 113.978149] [861] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai:更新 30010000.sai 捕获的 DAI 路由 [ 124.127055] [861] wait_for_avail:1936: asoc-simple-card sound-pcmdev: 捕获写入错误(DMA 或 IRQ 问题?) root@mx8mm:/tmp# ls test.wav -la -rw-r--r-- 1 root root 44 7月 22 22:09 test.wav root@mx8mm:/tmp#
View full article
SAF85xx HSEアップデート SMR こんにちは、NXPさん。 コードの内容変更 により署名バイトのみが変更され 、コードサイズ、開始アドレス、キー、署名へのポインタなどが変更されていない場合でも、SMRを更新する必要がありますか? Re: SAF85xx HSE Update SMR こんにちは、 SMR(セキュアメモリ領域)エントリには、HSEがアプリケーションイメージを検証するために使用するメタデータが含まれています。たとえ: サイズは変わりません 開始アドレスは変わりません キーハンドルは変更なし 署名ポインターは変更されません …コードの内容に変更を加えると署名が変わり、HSEは新しい署名を検証する必要がある。 このため、署名を保持するSMRエントリを更新された署名バイトで書き換える必要があります。 SMRエントリは認証済みブートチェーンの一部です。HSEは、対応するSMRエントリに新しい署名が反映されていない限り、更新されたバイナリを検証できません。 参考情報:AptivにはNXPの専属FAEがおりますので、詳細についてはお気軽にお問い合わせください。 よろしくお願いいたします。 ピーター Re: SAF85xx HSE Update SMR ご回答ありがとうございます。 Re: SAF85xx HSE Update SMR こんにちは、 もし私が新しいアプリケーション+新しい署名(新しいアプリケーションと地図)をフラッシュした場合はどうでしょうか。「コードサイズ、開始アドレス、キー、署名へのポインタ」が変更されない場合、SMRを再インストールする必要がありますか?
View full article
i.MX RT1050 下载算法 我现在开发环境是MCUXPRESSO IDE ,用的是i.MX RT1050 。我了解到因为i.MX RT1050 没有内部flash,所以在使用外部flash时需要下载算法。但是这个下载算法又和自己选用的flash有关。官方有没有说明怎么样得到自己想要的下载算法可以快速用起来? Re: i.MX RT1050 下载算法 Hi SDFDSFSF , 建议您按照以下顺序做: 1. 在工程属性里选择外部Flash下载算法,NXP提供了一些主流Flash下载算法。 您可以右键工程->Properties->MCU settings->Memory details选择NXP支持的flash驱动: MCUXpresso的flash驱动通常放在nxp\LinkServer_xx.x.xx\binaries\Flash下面,以.cfx为扩展名。 2. 如果选择的Flash支持SFDP,优先尝试SFDP driver 在MCUXpresso中可以选择类似MIMXRT1050_SFDP_QSPI.cfx这样的Driver。这类 SFDP driver 的意义是通过 flash 自描述参数减少对具体料号专用算法的依赖。 3. 使用模板自己做 请参考应用手册 https://www.nxp.com/docs/en/application-note/AN13386.pdf 生成客户自定义cfx文件。修改时关键参数要来自外部flash datasheet和SDK里的flexspi_nor_polling demo的测试结果。 除了下载算法,还需要XIP/Boot Header配置,请参考Solved: Flash interface initialization - NXP Community  以上是基本的方法。您可以告诉更具体的情况,比如您使用的是什么型号的Flash,您现在进行到哪一步遇到什么具体的困难,这样能更好的帮助到您。 Best Regards, Shelly Zhang i.MX RT1050 下载算法 我用的是JLINK,在MCUXpresso中选择的是MIMXRT1050_SFDP_QSPI.cfx。下载失败 Re: i.MX RT1050 下载算法 怎么样自己做一个JLINK在MCUXpresso ide里面用的 imxrt1052的现在算法? 我的flash是WINBOD 25Q256JVEQ. 我现在的MCUXpresso ide版本是MCUXpresso IDE v25.6。SDK_EVBK是26.06.00。我不知道用哪个例程可以修改生成自己想要的下载算法。 Re: i.MX RT1050 下载算法 Dear @SDFDSFSF , 参考示例在nxp/LinkServer目录下,工程名为iMXRT1050_QSPI: 如果你的引脚跟评估板不一样,需要修改引脚配置。Flash的配置也需要根据datasheet修改。 请确认以下事项: 1. Flash硬件引脚是否配置正确。必须根据RT1050硬件开发手册配置FlexSPI引脚: 只能选择A组或B组,FlexSPI_DQS需要悬空。 2. 在SDK中导入evkbimxrt1050_flexspi_nor_polling_transfer的example,根据flash的datasheet修改flash的配置。(这步可以省略,这步只是为了验证flash的配置是否正确) 3. 将正确的flash配置修改到工程iMXRT1050_QSPI。这步请参考 https://www.nxp.com/docs/en/application-note/AN13386.pdf Best Regards, Shelly Zhang Re: i.MX RT1050 下载算法 可能是您的硬件引脚配置跟评估板有差异,建议您修改iMXRT1050_QSPI工程自己生成cfx文件。 Re: i.MX RT1050 下载算法 我再MCUXpresso IDE下面用JLINK 有关系吗?我看到有的说在是MCXPpresso IDE算法仅能在CMSIS-DAP类型仿真器下使用?
View full article
S32K148EVB-Q176 收到的却是 UJA1131 而不是 UJA1132 您好, 我最近购买了一块S32K148EVB-Q176板。根据文档和原理图,我原本以为它会配备 UJA1132,但我收到的板子却是 UJA1131。 正因如此,我只有一个 LIN 接口,而我原本期望的是 UJA1132 的功能。 我只是想问一下这是否正常。S32K148EVB-Q176 是否有不同版本,配备不同的 SBC,还是我收到了错误的板? 谢谢! Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 你好@sousou54 , 感谢您提交的报告。目前该问题正在调查中。 请您提供产品包装盒上白色大标签的照片?标签上的信息可以帮助我们识别板的制造细节。 由于标签可能包含产品特定信息,您可以私信分享照片,或者通过开通支持案例(支持)来分享照片,而不是公开发布。 此致, 朱利安 Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 你好@sousou54 , 特此通知,我已收到您的照片,并已转发给相关团队。 我正在等待回复。感谢您的理解与合作。 此致, 朱利安 Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 嗨@sousou54 , 有关此事的更多信息,请联系您的 NXP 代表或您购买此套件的代理商。他们应该能够提供帮助。 此致, 朱利安
View full article
通过禁用 i.MX95 上的 CPU/GPU/VPU 来降低功耗 您好,NXP, 我们正在寻找降低基于 i.MX95 的系统整体功耗的方法。 请问您能否帮忙解答以下问题? 是否可以在不需要时完全关闭单个 CPU 核心的电源? 如果我们的应用程序不使用 GPU 和 VPU,是否可以完全关闭它们? 如果不需要使用 CPU/GPU/VPU,是否可以在启动后默认禁用它们以进一步降低功耗?(通过设备树?) 是否有推荐的软件配置或参考文档可以实现最低的功耗? 我们的电路板支持包 基于 Yocto 5.2 / Linux 6.12.x。 谢谢。 顺祝商祺! 肖恩 Linux Re: Reducing Power Consumption by Disabling CPU/GPU/VPU on i.MX95 关于您的问题: 是否可以在不需要时完全关闭单个 CPU 核心的电源? A:是的,可以。 如果我们的应用程序不使用 GPU 和 VPU,是否可以完全关闭它们? A:是的,如果不用它们的话。 如果不需要使用 CPU/GPU/VPU,是否可以在启动后默认禁用它们以进一步降低功耗?(通过设备树?) 答:是的,对于 GPU/VPU 类平台设备,通常的做法是将相关的设备树节点状态设置为“禁用”;这样 Linux 就不会注册/探测该设备。 是否有推荐的软件配置或参考文档可以实现最低的功耗? A:我们有 AN14449 — i.MX 95 功耗测量:测量低功耗用例、BCU 程序、DSM、Linux 挂起和 BBSM 的主要参考。 如有任何疑问,请随时联系我们。 祝你今天过得愉快
View full article
S32K344 QSPI Initializes SCLK不按我们希望出来 我用S32K344 LQFP176 做一个访问QSPI外设的产品,我们期望把QSPI做成和LSPI类似的应用,不是用QSPI访问FLASH,而是普通的设备。 我已经配置了时钟树QSPI_SFCK为20MHz,也将相关FLASH的寄存器关掉了,使用了LUT表,调试过程中也看到LUT执行了,但是QSPI的SCLK没有产生,SD0-SD3上面有超高速的波形出来。可以帮我看看怎么使用这个QSPI访问非FLASH设备吗? Re: S32K344 QSPI Initializes SCLK不按我们希望出来 S32K344 QuadSPI 模块主要用作串行闪存接口,而不是用作任意 QSPI 外设的通用 LSPI 类接口。QSPI_SFCK 时钟配置仅为 QuadSPI 模块提供时钟源;它不会自动生成外部 SCLK。外部 SCKFA 信号仅作为闪存导向的 LUT/IP 命令引擎执行的有效 QuadSPI 命令序列的一部分而生成。因此,如果连接的设备不遵循类似闪存的命令/地址/数据协议,或者 LUT 序列/引脚配置与此类事务不匹配,则该行为可能不适合此应用。对于通用外部设备,如果所需的协议可以在该设备中实现,则应使用 LSPI。如果必须使用 QuadSPI,则外部设备协议需要与 QuadSPI 闪存式事务模型兼容,并且需要相应地检查 LUT 序列、引脚复用、片选、命令/地址/数据阶段和 IP 命令触发。
View full article