Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Build Error for Sai_47478A_440_100 Example in S32DS 3.4 (S32K344) Hello, all I'm trying to build the Sai_47478A_440_100 example in S32DS 3.4 for S32K344, but I am encountering the following issues. 1. .mex File Load Error in Peripheral Mode When I select the project from the Peripheral tab, I get the following error: "error during opening configuration sai_~.mex processor s32k344, platformsdk_s32k3 version is not supported by current version of the tool" I'm using S32DS 3.4 and have installed SW32K3_RTD_4.4_1.0.0. How can I properly load the .mex file in Peripheral Mode? The goal is to integrate this code into RTD 5.0.0 in S32DS 3.5 If anyone has faced a similar issue, I would appreciate any guidance on resolving this. Thank you! Re: Build Error for Sai_47478A_440_100 Example in S32DS 3.4 (S32K344) The Sai_47478A_440_100 project is configured by EBTresos instead of S32 Configuration Tool(S32DS). You need to import the C:\NXP\S32K344_Whiteboard_Example_RTM_1.0.0\S32K344_Whiteboard_Example_RTM_1.0.0\SAI\Sai_47478A_440_100\Tresos_Project\Sai_47478A_440_100 by using EBTresos. Here is the configuration of LPI2C0: Sorry, I'm afraid you need to refer to EBTresos Project to migrate the project to RTD 5.0.0 in S32DS. Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
IOMUXC_GPR_GPR14 available information discrepancy Hi I have a question about register IOMUXC_GPR_GPR14 on RT1062 MCU In the reference manual (latest, rev.3) this register should be responsible for ACMP configuration. While when i search examples of FlexRAM configuration i find some info and code examples mentioning that register is responsible for some FlexRAM settings. For example this post https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/FlexRAM-configuration-for-OCRAM-0/m-p/1078440 and also AN12077 application note mentions it, and the Teensy 4.1 code do some strange setting on this register right after setting GRP17 and GPR16 so they used it for sure for FlexRAM not the analog comparators. In the SDK however (at least in version 2.16.100) all the code for IOMUXC_GPR_GPR14 is dedicated to ACMP1-4 I'm puzzled. Please bring some light on it Re: IOMUXC_GPR_GPR14 available information discrepancy That makes sense. Thanks, now i understand why the old code is that way but new code just ignores this register and only uses GPR17 and GPR16 for FlexRAM configuration Re: IOMUXC_GPR_GPR14 available information discrepancy Hi @Pencioner , Thanks for your interest in NXP MIMXRT series! This is not a bug, but the two FEATURES use different bit fields. About FlexRAM, in the previous version, IOMUXC_GPR_GPR14 provided 16-20bit for configuring the size of ITCM/DTCM, then it was found out that it works even if you don't configure these two bitfields, so the new version of RM about these two bitfields has been hidden.   And the configuration of ACMP uses the other bitfields of IOMUXC_GPR_GPR14, and the FlexRAM function does not affect each other. Best regards, Gavin
View full article
1170EVKBのMCU-Linkファームウェアを更新 1170EVK-BボードでMCUXpressoを使用しています。プロジェクトをデバッグしようとすると、次のようなファームウェア更新の警告が表示されます。 Firmware update requiredファームウェアのアップデートが必要です LinkServerと最新のファームウェアを https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK からダウンロードしました LinkServerを使用して自動的に更新しようとしましたが、成功しませんでした。 ./LinkServerプローブ「#1」更新自動情報:MCU-Linkファームウェア更新自動:サポートされていません-ファームウェア(V3.122以降)は、選択したプローブで手動でプログラムする必要があります([TQYQNHWCAQPZC][MCU-LINKオンボード(r0E2)CMSIS-DAP V2.250])ファームウェア更新自動:サポートされていません。 次に、ボードをブートローダーモードにして、次のようなさまざまな指示に基づいてファームウェアを更新できるようにしようとしました。 ※https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK ※ https://community.nxp.com/t5/i-MX-RT/Put-RT1170-EVK-in-quot-ISP-USB-quot-mode-for-MCU-Link-installer/m-p/1426988 ※ https://community.nxp.com/t5/i-MX-RT/Facing-issue-with-LPC-Link-2-with-iMX-RT-1170-Evk/m-p/1407341 ※https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418 ...しかし、失敗しました。私の問題は1170EVKと1170EVK-Bの違いから生じているのでしょうか、それとも何か明らかなものが欠けているのでしょうか? どうもありがとう Nick Re:1170EVKBのMCU-Linkファームウェアの更新 お知らせいただきありがとうございます! ディエゴ Re:1170EVKBのMCU-Linkファームウェアの更新 おかげで助かりました。 この記事は「JP3にジャンパを取り付けて、MCU-LinkをISPモードに強制する」に役立ちました - https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138 そうしたら: $ cd /Applications/LinkServer_1.5.30/MCU-LINK_installer/scripts J-Link firmware for MCU-Link programming script v1.0.8 March 2023. NOTE: J-Link firmware supports MCU-Link Pro and MCU-Link on-board systems that use an LPC55S69 in LQFP100 or BGA98 package. Although the firmware can be programmed in to MCU-Link and MCU-Link on-board systems that use LQFP64 package, the firmware will not run. Place the board in ISP USB mode using the appropriate jumper on your MCU-Link. Refer to the board documentation for more information. Connect board via USB then press Space. Programming Firmware_J-Link-MCU-Link_230502.s19 Programmed successfully. - To use: remove ISP jumper and reboot. 私はまだ問題を抱えていましたが、この投稿は役に立ちました:https://community.nxp.com/t5/i-MX-RT/Failed-to-power-up-DAP-ERROR-Could-not-connect-to-target/m-p/1503062#M20946 そして、ついにオンボードデバッガーが動作するようになりました。 Re:1170EVKBのMCU-Linkファームウェアの更新 こんにちは@nickager  お元気にお会いできることを願っています。 i.MX RT1170-EVKはLPC43xxをオンボードデバッガとして実装し、i.MX RT1170-EVKBはLPC55s69(MCU-Link)を実装しています。もしかしたら、それが問題があった理由かもしれません。 ここからLinkserverをダウンロードしてください Windows用Linkserver 1.5.30インストーラー 。SWをインストールした後、C:\nxp\LinkServer_1.5.30\MCU-LINK_installer\scriptsでアップデートスクリプトを実行します(デフォルトのインストールパスを使用)。 MCU-Link FWは、上記LinkServer for Microcontrollersのページで配布しています。 これがお役に立てれば幸いです。 ディエゴ
View full article
MK64 FlexBus FB_RW 我用的是MK64,写操作完成后FB_RW一直为低,读操作完成后FB_RW又恢复为高,好像是6800模式,我需要8080模式
View full article
Update MCU-Link firmware on 1170EVKB I am using MCUXpresso with an 1170EVK-B board. When I try to debug the project I receive the firmware update warning below: Firmware update requiredFirmware update required I have downloaded LinkServer and latest firmware from: https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK I've tried using LinkServer to automatically update without success: ./LinkServer probe '#1' update auto INFO: MCU-Link firmware update auto: not supported - the firmware (V3.122 or later) should manually programmed on the selected probe ([TQYQNHWCAQPZC] [MCU-LINK on-board (r0E2) CMSIS-DAP V2.250]) Firmware update auto: not supported and then tried to put the board into a boot loader mode where I can update the firmware based on various instructions such as: * https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK * https://community.nxp.com/t5/i-MX-RT/Put-RT1170-EVK-in-quot-ISP-USB-quot-mode-for-MCU-Link-installer/m-p/1426988 * https://community.nxp.com/t5/i-MX-RT/Facing-issue-with-LPC-Link-2-with-iMX-RT-1170-Evk/m-p/1407341 * https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418  ... but have failed. Could my problems stem from the difference between 1170EVK and 1170EVK-B or am I missing something obvious? Many thanks Nick Re: Update MCU-Link firmware on 1170EVKB Thanks for letting us know! Diego Re: Update MCU-Link firmware on 1170EVKB Thanks that helped.  I found this post helpful for "Install a jumper at JP3 to force the MCU-Link in ISP mode" - https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138 Then: $ cd /Applications/LinkServer_1.5.30/MCU-LINK_installer/scripts J-Link firmware for MCU-Link programming script v1.0.8 March 2023. NOTE: J-Link firmware supports MCU-Link Pro and MCU-Link on-board systems that use an LPC55S69 in LQFP100 or BGA98 package. Although the firmware can be programmed in to MCU-Link and MCU-Link on-board systems that use LQFP64 package, the firmware will not run. Place the board in ISP USB mode using the appropriate jumper on your MCU-Link. Refer to the board documentation for more information. Connect board via USB then press Space. Programming Firmware_J-Link-MCU-Link_230502.s19 Programmed successfully. - To use: remove ISP jumper and reboot. I still had problems but this post helped: https://community.nxp.com/t5/i-MX-RT/Failed-to-power-up-DAP-ERROR-Could-not-connect-to-target/m-p/1503062#M20946 and I finally have working onboard debugger. Re: Update MCU-Link firmware on 1170EVKB Hi @nickager  I hope to find you well.  The i.MX RT1170-EVK implements LPC43xx as the on-board debugger, and the i.MX RT1170-EVKB the LPC55s69, ( MCU-Link). Maybe that is the reason why you had issues.  Please make sure to download Linkserver from here  Linkserver 1.5.30 installer for Windows  . After installing the SW execute the update script at C:\nxp\LinkServer_1.5.30\MCU-LINK_installer\scripts (using default installation path) The MCU-Link FW is now being distributed at LinkServer for Microcontrollers page referecenced above.  I hope this could help you! Diego
View full article
MK64 FlexBus FB_RW I'm using MK64, the FB_RW keeps being low after the write operation is finished, and the FB_RW returns high after the read operation, which seems to be 6800 mode, I need 8080 mode Re: MK64 FlexBus FB_RW Hi, From the attached  FlexBus timing, it is incorrect, at least, the data bus should be valid until the rising edge of /CS signal. Pls try different parameter in the FB_CSCRn register, especially, WRAH and WS bits, do not use burst mode, set AA bit in 1. Pls have  a try. BR XiangJun Rong Re: MK64 FlexBus FB_RW The DM9000 write timing is shown in the figure, how does the MK64 FlexBUS implement it? Re: MK64 FlexBus FB_RW As you can see from the graph, the FB_RW stays low after the data is written Re: MK64 FlexBus FB_RW Hi, The Flex_Bus of K64 is in 8086 mode instead of 68K mode. This is the reading timing: This is writing timing: Compare the two timing, you can see that the /FB_OE  low and the FB_RW high are observed in reading timing, the /FB_OE  high and the FB_RW low are observed in writing timing. If the timing is 68K mode, the /FB_OE is always low no matter whether it is reading or writing. Hope it can help you BR XiangJun Rong
View full article
更新 1170EVKB 上的 MCU-Link 固件 我正在使用带有 1170EVK-B 板的 MCUXpresso。当我尝试调试项目时,我收到以下固件更新警告: Firmware update required需要固件更新 我已经从以下网址下载了 LinkServer 和最新固件: https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter :OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK 我尝试使用 LinkServer 自动更新,但没有成功: ./LinkServer 探针‘#1’自动更新信息:MCU-Link 固件自动更新:不支持 - 固件(V3.122 或更高版本)应在所选探针上手动编程([TQYQNHWCAQPZC] [MCU-LINK 板载(r0E2)CMSIS-DAP V2.250])固件自动更新:不支持 然后尝试将主板置于引导加载程序模式,我可以根据各种指令更新固件,例如: * https://www.nxp.com/design/design-center/software/sensor-toolbox/opensda-serial-and-debug-adapter:OPENSDA?tid=vanOpenSDA#MIMXRT1170-EVK * https://community.nxp.com/t5/i-MX-RT/Put-RT1170-EVK-in-quot-ISP-USB-quot-mode-for-MCU-Link-installer/mp/1426988 * https://community.nxp.com/t5/i-MX-RT/Facing-issue-with-LPC-Link-2-with-iMX-RT-1170-Evk/mp/1407341 * https://community.nxp.com/t5/i-MX-RT/i-MX-RT1170-with-MCU-Boot-Utility/td-p/1303418 ...但失败了。我的问题是否源于 1170EVK 和 1170EVK -B之间的差异,或者我是否忽略了一些明显的东西? 非常感谢 Nick 回复:更新 1170EVKB 上的 MCU-Link 固件 感谢您告知我们! 迭戈 回复:更新 1170EVKB 上的 MCU-Link 固件 谢谢,有帮助。 我发现这篇文章对“在 JP3 处安装跳线以强制 MCU-Link 处于 ISP 模式”很有帮助 - https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1170-EVKB/ta-p/1715138 然后: $ cd /Applications/LinkServer_1.5.30/MCU-LINK_installer/scripts J-Link firmware for MCU-Link programming script v1.0.8 March 2023. NOTE: J-Link firmware supports MCU-Link Pro and MCU-Link on-board systems that use an LPC55S69 in LQFP100 or BGA98 package. Although the firmware can be programmed in to MCU-Link and MCU-Link on-board systems that use LQFP64 package, the firmware will not run. Place the board in ISP USB mode using the appropriate jumper on your MCU-Link. Refer to the board documentation for more information. Connect board via USB then press Space. Programming Firmware_J-Link-MCU-Link_230502.s19 Programmed successfully. - To use: remove ISP jumper and reboot. 我仍然遇到问题,但这篇文章很有帮助: https://community.nxp.com/t5/i-MX-RT/Failed-to-power-up-DAP-ERROR-Could-not-connect-to-target/mp/1503062#M20946 我终于有了可以运行的板载调试器。 回复:更新 1170EVKB 上的 MCU-Link 固件 你好@nickager 我希望你一切都好。 i.MX RT1170-EVK 将 LPC43xx 实现为板载调试器,i.MX RT1170-EVKB 将 LPC55s69(MCU-Link)实现为板载调试器。也许这就是您遇到问题的原因。 请确保从此处下载适用于 Windows 的 Linkserver 1.5.30 安装程序。安装 SW 后,执行位于 C:\nxp\LinkServer_1.5.30\MCU-LINK_installer\scripts 的更新脚本(使用默认安装路径) MCU-Link FW 目前正在上述微控制器 LinkServer 页面上分发。 我希望这能对你有帮助! 迭戈
View full article
MK64 フレックスバスFB_RW MK64を使用していますが、書き込み操作が終了した後もFB_RWが低くなり続け、読み取り操作後にFB_RWがハイに戻り、6800モードのようですが、8080モードが必要です
View full article
Should the RT1021 use the FreeRTOS port ARM_CM4F or ARM_CM7? Hi, Which FreeRTOS port should the RT1021 be using? The SDK demo projects use ARM_CM4F, but there are comments in there that say that CM7 r0p1 versions should use the ARM_CM7 port. (Also I think the original SDK demos used the CM7 one a few years ago?) The RT1021 reference manual talks about the ETM Arm CoreSight™ ETM-M7 Revision: r0p1 Technical Reference Manual. Please clarify which port to use. Many thanks and kind regards. Re: Should the RT1021 use the FreeRTOS port ARM_CM4F or ARM_CM7? Thanks @MultipleMonomials @rshipman for providing this method. Yes, it is ARM_CM4F. Re: Should the RT1021 use the FreeRTOS port ARM_CM4F or ARM_CM7? Hmm, in the past I used the debugger to inspect the registers of my MIMXRT1050 and it came back as a Cortex-M7 r1p1, even though the manual for this one also references "Arm CoreSight™ ETM-M7 Revision: r0p1".  So, I think that using the Cortex-M4F port is correct. You can check it yourself by reading the CPUID register in the debugger (J-Link prints its value when connecting to the core, or you could read it manually).  Per here, the rightmost hex digit is the revision, and the sixth-from-the-right hex digit is the variant number.  For example, mine comes back as 0x411FC271, which would mean that it is r1p1.
View full article
S32K341EHT0MPAST Pinout I am wanting to use the S32K341EHT0MPAST and can't find a list of the functions associated with the pin to the 100 pins. Do you know where I can find the pinout information? Re: S32K341EHT0MPAST Pinout Hi @Capray986  Attached to the S32K3xx Reference Manual, Rev. 8 you can find the S32K342_S32K341_S32K322_IOMUX file, which contains the pins specifications of this device. B.R. VaneB
View full article
S32DS-S32K3xx SMP示例编译错误 我正在尝试编译 FreeRTOS_Toggle_Led_Example_S32K358_SMP 项目,它产生了以下错误: C:/NXP/workspaceS32DS.3.6.0/FreeRTOS_Toggle_Led_Example_S32K358_SMP/generate/include/FreeRTOSConfig.h:64:66:错误:函数“taskDISABLE_INTERRUPTS”的隐式声明[-Werror=implicit-function-declaration] arm-none-eabi-gcc“@RTD/src/Clock_Ip.args”-MMD-MP-MF“RTD/src/Clock_Ip_Monitor.d”-MT“RTD/src/Clock_Ip_Monitor.o”-o“RTD/src/Clock_Ip_Monitor.o”“../RTD/src/Clock_Ip_Monitor.c” 64 | #定义 configASSERT(x)if((x)==0){ taskDISABLE_INTERRUPTS(); 对于(;; ); } | ^~~~~~~~~~~~~~~~~~~~~~ ../FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1/portmacro.h:184:17: 注意:在宏“configASSERT”的扩展中 184 | configASSERT(Get_64(&ucRecursionCountByLock[ulLockNum])!= 255u); | ^~~~~~~~~~~~~~ 缺少#include? 有没有快速修复此问题的方法? 我正在使用 DS 3.6.0以及“适用于 S32K3XX 版本 5.0.0 的 FreeRTOS”包裹。示例取自“SW32K3 FreeRTOS 11.1.05.0.0上述包中的 CD1 D2409 示例项目部分。 谢谢 回复:S32DS-S32K3xx SMP示例编译错误 谢谢朱利安。成功了!
View full article
S32 Design Studio for ARM expires soon Hello support team, could you please extend my S32 Design Studio for ARM 2.2 license, it will expire in 15 days. My license details as follows: S32 Design Studio for ARM ActivationId: 0E6E-4188-1B59-C966 Evaluation Days: 15 Feature Version: 2.2 Feature Status: Evaluation (15 days) Thanks in advance. Kind regards, Andreas Re: S32 Design Studio for ARM expires soon Thanks for the quick help, I was able to re-register the extended license. Thank you and have a good time. Re: S32 Design Studio for ARM expires soon Hi Andreas,  your S32DS license has been extended. You can left your current license to expire or return it - on main menu bar click on Help -> NXP Licenses -> Open -> Return License and activate S32DS again with your old code. 
View full article
S32DS - S32K3xx SMP サンプルのコンパイル エラー プロジェクトをコンパイルしようとするとFreeRTOS_Toggle_Led_Example_S32K358_SMP次のエラーが発生します。 C:/ NXP / workspaceS32DS.3.6.0 / FreeRTOS_Toggle_Led_Example_S32K358_SMP / generate / include / FreeRTOSConfig.h:64:66:エラー:関数 'taskDISABLE_INTERRUPTS'の暗黙宣言[-Werror =暗黙の機能宣言] arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF "RTD/src/Clock_Ip_Monitor.d"-MT「RTD/src/Clock_Ip_Monitor.o」-o "RTD/src/Clock_Ip_Monitor.o""../RTD/src/Clock_Ip_Monitor.c" 64 |#define configASSERT(x) if((x)==0) { taskDISABLE_INTERRUPTS(); for( ;; ); } |^~~~~~~~~~~~~~~~~~~~~~ ../FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1/portmacro.h:184:17: ノート: マクロ 'configASSERT' の拡張中 184 |configASSERT( Get_64(&ucRecursionCountByLock[ulLockNum]) != 255u); |^~~~~~~~~~~~ #include がありませんか? これを修正する簡単な方法はありますか? DS 3.6.0 を使用していますおよび「FreeRTOS for S32K3XX バージョン 5.0.0」パッケージ。「SW32K3 FreeRTOS 11.1.0」から取得した例5.0.0上記パッケージのCD1 D2409 Example Projects」セクション。 感謝 Re: S32DS - S32K3xx SMP サンプルコンパイルエラー ありがとうジュリアン。うまく行きました!
View full article
Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Hello everyone, I'm tryng to build the imx-boot image by using imx-mkimage, following the steps I found for i.MX 93 A1 in Linux Users Guide (from 39/166 to 40/166): https://www.nxp.com/doc/IMX_LINUX_USERS_GUIDE I succesfully build u-boot.bin and u-boot-spl.bin (GitHub - nxp-imx/uboot-imx at lf_v2023.04) and I and I copied them in imx-mkimage/iMX93 (source: GitHub - nxp-imx/imx-mkimage: i.MX Mkimage Bootloader Tool 6.6.3_1.0.0). In the same folder I put bl31.bin, generated from  GitHub - nxp-imx/imx-atf: i.MX ARM Trusted firmware together with mx93a1-ahab-container.img (u-boot/doc/board/nxp/imx93_11x11_evk.rst at master · u-boot/u-boot · GitHub) . So the final content of the folder is this: When it comes to run the command: make SOC=iMX93 flash_singleboot The output gives the following error: Can anyone help me with this issue? I can't figure out what is going on. Thanks, in advance, Bob Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Thank you, now it works! Regards, Bob Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Hi, This is another issue missing DDR firmware. Follow the steps as below. wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.23.bin chmod +x firmware-imx-8.23.bin ./firmware-imx-8.23.bin copy missing ddr firmware from -> firmware-imx-8.23/firmware/ddr/synopsys/ Regards Harvey Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Hello, I tried to do the gitclone command as you suggested: git clone https://github.com/nxp-imx/imx-mkimage.git The download terminated succesfully, then I moved all the necessary files into iMX93 folder. Then I execute:  make SOC=iMX93 flash_singleboot this command returns: How can i go ahead? Regards, Bob     Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage This seems to be a problem with your git. or did you download the imx-mkimage in git clone? Regards Harvey Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Hello @Harvey021 , Thanks for responding, I tried the command you suggested and this is the output:   Can you tell me what I have to do next? Thanks, Bob Re: Error in building imx-boot image for iMX93 11x11 EVK using imx-mkimage Hi @Bob_NXP_user  It seems that the commit number has not been generated. please make sure your download. Have a run "git rev-parse --short=8 HEAD >> src/build_info.h" to see what it is. Regards Harvey
View full article
S32DS - S32K3xx SMP example compilation error I'm trying to compile FreeRTOS_Toggle_Led_Example_S32K358_SMP project and it produces the following error: C:/NXP/workspaceS32DS.3.6.0/FreeRTOS_Toggle_Led_Example_S32K358_SMP/generate/include/FreeRTOSConfig.h:64:66: error: implicit declaration of function 'taskDISABLE_INTERRUPTS' [-Werror=implicit-function-declaration] arm-none-eabi-gcc "@RTD/src/Clock_Ip.args" -MMD -MP -MF"RTD/src/Clock_Ip_Monitor.d" -MT"RTD/src/Clock_Ip_Monitor.o" -o "RTD/src/Clock_Ip_Monitor.o" "../RTD/src/Clock_Ip_Monitor.c" 64 | #define configASSERT(x) if((x)==0) { taskDISABLE_INTERRUPTS(); for( ;; ); } | ^~~~~~~~~~~~~~~~~~~~~~ ../FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1/portmacro.h:184:17: note: in expansion of macro 'configASSERT' 184 | configASSERT( Get_64(&ucRecursionCountByLock[ulLockNum]) != 255u); | ^~~~~~~~~~~~ Missing #include? Is there a quick way to fix this? I'm using DS 3.6.0 and 'FreeRTOS for S32K3XX version 5.0.0' package. Example taken from 'SW32K3 FreeRTOS 11.1.0 5.0.0 CD1 D2409 Example Projects' section of the above package. thanks Re: S32DS - S32K3xx SMP example compilation error Thanks Julian. It worked! Re: S32DS - S32K3xx SMP example compilation error Hi @ogai, This issue has already been reported to the SW team. The provided example is incomplete, and some workarounds are needed for it to work correctly:  1. Configuration .mex needs to be updated to include SMP support: 2. Calls to vPortGET_CORE_ID need to be replace with calls to portGET_CORE_ID.  3. In ASSERT(), change macro definition to "if((x)==0) {__asm volatile ( " cpsid i " ::: "memory" ); for( ;;); } Best regards, Julián
View full article
BLDC 电机控制 如何使用 NXP S32K3 微控制器控制 BLDC 电机 回复:BLDC电机控制 @Senlent 谢谢 回复:BLDC电机控制 有没有使用 s32k 微控制器控制无刷直流电机的源代码或参考代码 回复:BLDC电机控制 你好@Kalase 这就是我针对您的问题所找到的答案: S32K344-六步换向控制 https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-Six-step-commutation-control/ta-p/1804572
View full article
MC33978 SPI transfert mode Dear NXP community, I've got two question about MC333978 MSDI. Which SPI mode (0, 1, 2 or 3) should be used to communicate with MC33978 ? Indeed, I don't find it very clear in the datasheet (Figure 20 §7.9.4 Serial data input (MOSI)) Each transfert use a 32 bits word. Could it work with 4 groups of bytes transferts e.g. on this screenshot Thanks a lot in advance, Pascal Re: MC33978 SPI transfert mode Hello Tomas, thanks a lot for your help. I ported the MSDI_SDK_SW  to Microchip MPlab IDE. The API used to transfer a generic buffer to SPI worked in the wrong way, so that a uint32_t was transfered to SPI by LSB first. I'm going to open another subject because I've got another problem... Best regards, Pascal Re: MC33978 SPI transfert mode Hello Pascal, 1. The MC33978 uses SPI Mode 0 (CPOL = 0, CPHA = 0: CLK idle state = low, data sampled on rising edge and shifted on falling edge). 2. Yes, it should work this way. BRs, Tomas
View full article
S32G domain control - RHS Hello, Just one quick question. From https://www.nxp.com/design/training/introduction-to-the-concept-and-variations-of-domain-control:TIP-TD-AUT224 In page 12, it mentioned "Platform Scalability (increasing to RHS)" What does RHS stand for? Thanks Re: S32G domain control - RHS ok, thanks for the help. Re: S32G domain control - RHS Hello, @JasonTseng Thanks for the feedback. I feel sorry that it is difficult to get feedback from a document written several years ago, but I read it carefully and according to the contents and the context around it, I could almost confirm my understanding. I apologize for your inconvenience. Best Regards Chenyin Re: S32G domain control - RHS Hello Chenyin, Can you help contact the author and confirm your answer? Thanks Re: S32G domain control - RHS Hello, @JasonTseng Thanks for the questions. I have just read the document, from my opinion, the RHS there means “right-hand side” Best Regards Chenyin
View full article
For S32K3, does MBDT have access to the EEPROM functionality? Is there EEPROM access within the MBDT library? If not, how do we use custom linker, and how do we store variables declared in Simulink to store in the non-volatile memory, and how to access that memory from during run time? Or is there any other recommended method? Thank you. Re: For S32K3, does MBDT have access to the EEPROM functionality? Hello @Wei_H , The closest you could get to a behavior similar to reading/writing to/from EEPROM memory would be to use the FEE blocks. But this does not accomplish your goals of having persistent data, given the fact that FEE uses FLASH memory. As for the question about custom linker usage, you can find out more about the workflow by checking out Chapter 3.13 from the Release notes document, found inside the Toolbox installation at S32K3\src\mbdtbx_s32k3\help\docs\manual\Model_Based_Design_Toolbox_S32K3_Series_Release_Notes.pdf. In regards to the MX25L6433FM2I-08G chip on the board, it seems like it is connected through Quad SPI and the connections being made are:  - SIO0     -    QSPI_IO0    -    PTD11 - SIO1      -    QSPI_IO1     -    PTD7 - SIO2     -    QSPI_IO2    -    PTD12 - SIO3     -    QSPI_IO3    -    PTC2 - CS        -    QSPI_CS     -    PTC3 - SCLK    -    QSPI_SCK   -    PTD10 I assume you are using the MR-CANHUBK344 Q172 board and the previously mentioned connections have been taken out of its schematic. In case you are using a different board, please let me know. Since we do not support QuadSPI, your approach here would consist of adding the QSPI driver in the model's configuration, properly setting the parameters and all the necessary dependencies (e.g.: clocks, interrupts, pins etc.) and then using the QSPI protocol through custom code. For header insertions you could use the Model Header block, and for actual code, you could use the Subsystem Initialize block. An alternative to using these blocks would be to change the board initialization file to add these includes and instructions. I went ahead and tried to find any other threads about using this external flash on your board and here is a thread I found: https://community.nxp.com/t5/S32K/S32K344-MRCANHUBK344-QSPI-Example-Timeout/m-p/2054546 This thread also highlighted the fact that there's an S32 Design Studio example available that could serve as a starting point for your project: Regards, Robert V Re: For S32K3, does MBDT have access to the EEPROM functionality? Specially, we know that the S32K344 evaluation kit that has MX25L6433FM2I-08G chip for Non-Volatile memory.  My question is, to access the chip for flashing, how to set up SPI in the configure tool for MBDT and what is the SPI protocol to program it? Thanks.
View full article
[FLash] About the FLASH_DRV_EraseSector interface Dear NXPS: Chip: S32K146 OS: without OS Q: When the FLASH_DRV_EraseSector interface returns a value other than STATUS_SUCCESS, I want to call the FLASH_DRV_EraseSector interface again. How much time should pass between the two calls? Re: [FLash] About the FLASH_DRV_EraseSector interface Hello @Gideon, There is no delay required, it can be called again immediately. If you need the time required to erase one sector, refer to the S32K1xx DS, Table 35. Flash command timing specifications for S32K14x series Regards, Daniel
View full article